NXP Tech Blog

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tech Blog

gaurav_sharma
NXP Employee
NXP Employee

Hey everyone! This blog will cover the following: -

 

  1. System Overview
  2. Use-case
  3. What are Outbound and Inbound windows in PCIe and how do they work?
  4. What is ATU and why is it important in PCIe?
  5. How to configure the PCIe windows in LS1028 and iMX8QXP
  6. Code walkthrough
  7. Running the test case



System Overview

1.png

As depicted in the illustration above, the system has 2 main blocks: -

a. iMX8QXP [configured as PCIe Root Complex]
b. LS1028 [ configured as PCIe Endpoint]


Software components: -

iMX8QXP - Linux Factory 6.6.36
LS1028ARDB - LSDK-18.09

Hardware components: -

iMX8QXP MEK Board
LS1028ARDB Board
M.2 Key E PCIe Bridge


The root complex and endpoint are connected via a PCIe bridge on M.2 Key E connector of both the boards.
Reference clock used for both PCIe RC and EP - 100 MHz 




PCIe Bridge with M.2 Key E interfacePCIe Bridge with M.2 Key E interface

M.2 Key E PCIe Bridge


Use-case

 

There was a customer requirement wherein a software program was needed at Uboot to benchmark the PCIe to DDR transfers, involving cacheable and non-cacheable DRAM memory regions. 
 

The benchmark software periodically realizes several DMA transfers from PCIe space to DDR in the following way: -

 

1) Start PCIe to DDR DMA transfer (no descriptor). Data are transferred from PCIe to a non-cacheable buffer (A).

2) Wait for the DMA transfer to finish.

3) Copy received data from non-cacheable buffer (A) to a cacheable buffer(B).

 

4)  Check if there's a data mismatch and reports accordingly.


Note: -
There are 2 types of DMA transfers - Descriptor and Non-descriptor.
In Descriptor based DMA, the CPU sets up a list or chain of 'descriptors' in memory. Each descriptor is a data structure containing info such as source, destination, transfer size etc.

In Non-descriptor DMA, the CPU directly configures the DMA controller's registers to define parameters for a single, specific DMA transfer.

This use-case employs non-descriptor DMA transfers.

RC and EP will exercise the above use-case at Uboot itself. iMX8QXP by default acts as a RC. However, to configure LS1028 PCIe2 as EP, we have to configure the RCW[HOST_AGT_PEX] = 1 and then boot LS1028 with the modified RCW flashed onto the board.


To implement this use-case: -

On the iMX8QXP we will be adding our own functionality to the 'pci' utility by modifying the cmd/pci.c in the Uboot source code. After applying this patch, we can execute the test case at Uboot console by just executing this command - "pci p"

On LS1028A, we will simply be writing to the PCIe controller registers using the 'mw' command to set up the EP for the use-case.
 

What are Outbound and Inbound transactions in PCIe?

To explain the concept of outbound and inbound transactions, there are 2 entities that we need to keep in mind w.r.t the transactions that flow in the PCIe fabric:-

Initiator - component that initiates the transaction by sending a request. Example- Memory Read request sends the request for data.

Completer -  component that receives the request and eventually sends a response. Example - After receiving Memory Read request sent by the initiator to it, it sends the completion TLP containing the requested data back to the initiator.

 

3_memrd_write.png

 

Transactions in PCIe can be categorized into 2 parts, depending on the direction of data flow relative to a device [Root complex or End-point]  :-

Inbound - Data is coming into the device from the PCIe bus. From the device's perspective, the device is the completer of this request which was initiated by some other device. Example - Root complex[initiator] sending memory write TLP to an End-point[completer]. In this case EP will have inbound transactions coming from RC.

Outbound - Data is going out from the device to the PCIe bus. From the device's perspective, the device is the initiator of this request which will be completed by some other device. Example - End-point[Initiator] sending memory read TLP to a Root-complex[completer]. In this case, EP will have outbound transactions going towards RC.
 

What is ATU and why is it important in PCIe?

 

PCIe TLP transactions use PCIe addresses. These addresses are different from local internal bus addresses [like AXI, AHB] which are used in on-chip communication between CPU, memory and peripherals. So, we need an entity that maps the addresses from PCIe to local internal bus. Here comes the ATU: -

ATU is an Address Translation Unit that is responsible for address mapping between the device's address space and host's address space. It enables devices to access the host system's memory or other resources. Have a look at the following scenarios where ATU is needed: -

1. A PCIe device (such as network card, storage controller) needs to access the host's memory via DMA. So, the addresses that are issued by the device need to be translated via ATU so that the host can recognize and process these addresses.

 

2. A PCIe device wants to access a memory-mapped IO address. To do this, ATU is needed for translating device's requested address into an address that the host understands.

 

So, whenever a PCIe device initiates an access request like DMA memory read/write, the ATU translates the address issued by the device into the address of the host system as illustrated below: -

ATU TranslationATU Translation

 

Now that we know what Inbound/Outbound transactions are and how does ATU work in PCIe, we will now discuss how to enable the devices [RC/EP] to carry out these transactions. To achieve this, we configure Inbound and Outbound windows in the PCIe controller of a device by setting up ATU translation.
 

 

How to configure PCIe Outbound and Inbound windows in iMX8QXP & LS1028 respectively?



5_ib_ob.png

For our use-case, we will be configuring 1 outbound window on iMX8QXP [Root Complex] and 1 Inbound window on LS1028A[Endpoint].
 
a. To set up an Outbound window on iMX8QXP, we configure the following registers:-

iATU Index register
- defines which region is being accessed and its direction[Inbound/Outbound].


iATU Region Control 1 Register - To configure Max ATU Region size and other TLP attributes.


iATU Lower Base Address Register

                   &
iATU Upper Base Address Register


- These registers configure the start address of a window before the translation

 

iATU Limit Address Register - To configure the End-address of the window before the translation


iATU Lower Target Address Register
                    &

iATU Upper Target Address Register

- These registers configure the start and end addresses after the translation.
 

iATU Region Control 2 Register - To enable the REGION_EN bit and select match mode.

 

 

Outbound WindowOutbound Window

 

b. To set up an Inbound window on LS1028A, we configure the same set of registers :-

iATU Index Register
iATU Region Control 1 Register

iATU Lower Base Address Register

iATU Upper Base Address Register

iATU Limit Address Register

iATU Lower Target Address Register

iATU Upper Target Address Register

iATU Region Control 2 Register
 

Additionally, we will be configuring

PCI Express Command Register - to enable Bus master bit
PEX PF0 CONFIG Register - to set the Config Ready bit. Used by EP to indicate the RC that the controller has done its initialization.


 

The reason why we need to configure 2 additional registers on the EP side is that LS1028[EP] will be at Uboot console the whole time we are exercising our use-case. If it was in Linux, the PCIe drivers would have taken care of this.
 

 

Inbound WindowInbound Window

Code-walkthrough


There's a patch attached with this blog so that the readers can go through it and use it if required.

Note:-  In no way this claims itself to be a production level code, so readers are encouraged to only take it as a reference.
 

The Uboot patch achieves the following:-

 

  1. Configure MMU to make the DRAM range 80020000-88000000 non-cacheable. We are using the DRAM range 0x92000000-FE000000 as cacheable memory for our test case.  
  2. Creates an outbound window on iMX8QXP[connected to LS1028 End-point via PCIe bridge]. To complement this, an Inbound window will be configured on the LS1028.
  3. In a loop:-
    1. zeroize the cacheable and non-cacheable 1MB memory region.
    2. flushing the data cache for the cacheable 1MB region.
    3. configure and trigger DMA read to transfer 1MB of data from End-point’s DDR to RC’s non-cacheable memory region.
    4. copy 1MB data from non-cacheable to cacheable memory.
    5. compares the cacheable 1MB memory with the expected data. If mismatch occurs, we error out and break out of loop. Otherwise the   looping continues.


 

Executing ‘pci p’ command at U-boot console starts the above sequence.

 

After applying the patch in Uboot source, build the Uboot binary, then build SPL. Flash the SPL to iMX8QXP.

 

Running the test case


a. Connect RC [iMX8QXP] and EP[LS1028ARDB] via M.2 Key.E bridge, boot RC and EP till Uboot.


b. At Uboot console of LS1028, execute the following commands to configure the inbound window: -


 

mw.l 0x3500900 0x80000001

mw.l 0x3500904 0x0

mw.l 0x350090c 0x0

mw.l 0x3500910 0x0

mw.l 0x3500914 0x07ffff

 

mw.l 0x3500918 0xA0000000

mw.l 0x350091c 0x0

mw.l 0x3500908 0xC0000000

mw.b 0x3500004 0x06

mw.l  0x35C0014 0x00001001


The above registers are part of PCIe ATU configuration that was mentioned in the section -

How to configure PCIe Outbound and Inbound windows in iMX8QXP & LS1028 respectively

Please feel free to cross-check the Reference manual of LS1028A to verify the register addresses and their significance.
 

 c. On RC, execute 'pci p' -- this will trigger the DMA transfer use-case. 

 

This blog merely scratched the surface of PCIe inbound and outbound transactions. However it aimed at giving a raw view of how memory transfer can be triggered using DMA. For any queries, feel free to DM or send your questions in the comments section.

 

 

 

 

 



件数が多いもの
0 0 124
Keita_Nagashima
NXP Employee
NXP Employee

2025年よりNXP Japanから日本語の技術記事をたくさんユーザーに届けようとの想いの下、これまでに多数の技術記事(Tech Blog)を公開してまいりました。これらの情報をより体系的にご活用いただけるよう、このたびコンテンツ・マップ(PDF)を公開いたしました。

実装例やトラブルシューティングのヒントを含む実践的な内容が充実しており、開発現場での課題解決や新規プロジェクトの立ち上げ時に役立つ情報として、多くの技術者の皆様に活用いただいております。

(読了:5分)

詳細を読む...

件数が多いもの
0 0 444
araki
NXP Employee
NXP Employee

バッテリーマネジメントシステム (BMS)において3つの重要な指標について以下のように解説します。

管理すべき指標とBMSの重要性を理解いただけると幸いです。

(読了:10分)

詳細を読む...

件数が多いもの
0 0 328
shaojun_wang
NXP Employee
NXP Employee

OV5640 MINISASTOCSI is widely used in i.MX8. This article shows how to enable it on i.MX95 15x15 EVK board. The Linux version is 6.12.20.

詳細を読む...

件数が多いもの
0 0 277
KosukeSogawa
NXP Employee
NXP Employee

NXP車載向けマイコンの機能安全対応について、通常の(機能安全非対応)マイコンと何が違うのか説明します。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 499
araki
NXP Employee
NXP Employee

バッテリーマネジメントシステム (BMS)に関する内容を以下のようにまとめています。

BMSにこれから携わる方に読んでいただけると嬉しいです。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 691
akifumiokano
NXP Employee
NXP Employee

このブログでは,デジタル回路で使われる論理回路の種類(*TTL,*LVTTL,*CMOS)の電圧レベルの違いから,それを判断する上で重要なVOH/VOL/VIH/VILの意味について解説します.

さらに様々な変換の方法の中から,どのような電圧レベル・トランスレータを選べばよいかを解説します.

特に特別な扱いが必要となる,双方向オープンドレイン信号の変換について詳しく見てみます

詳細を読む...

件数が多いもの
0 0 734
Keita_Nagashima
NXP Employee
NXP Employee

この記事では、MyNXPアカウントの登録方法を分かりやすく説明します。

またMyNXPアカウントのメリットについても簡単にご紹介します。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 749
Keita_Nagashima
NXP Employee
NXP Employee

NXP製品の使用方法が分からない場合や、ドキュメントを読んでも内容が理解できないときのために、NXPでは問い合わせ窓口を用意しています。
この記事では、実際にどのように問い合わせを行えばよいのか、手順を分かりやすくご紹介します。
*2025年6月より、日本語での問い合わせが可能になりました。

詳細を読む...

件数が多いもの
1 0 884
Yutaka_Okui
NXP Employee
NXP Employee

ある、マイコン/プロセッサに適したNXP PMIC PFシリーズ を検索するときに、助けとなる情報をまとめています。

nxp.jpの「パワー・マネジメントIC (PMIC) とシステム・ベーシス・チップ (SBC)」ページで提供されている、プロセッサに適したPMICまたはSBCの検索ツール(製品セレクタ、およびクロス・リファレンス)とあわせて使用してください。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 836
Keita_Nagashima
NXP Employee
NXP Employee

プロセス・テクノロジーの微細化に伴い、28nm以降の世代では、従来からあるFlashメモリをマイコンへ搭載することが難しくなり、各社次世代マイコンに対してFlashメモリに代わる不揮発性メモリ(NVM)を検討しています。その中のひとつがMRAMです。

本記事では、MRAMの特徴を説明します。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 751
yutaka_ando
NXP Employee
NXP Employee

i.MXアプリケーション・プロセッサのLinux BSPに含まれるデモ・リポジトリ「GoPoint」を紹介します。
「GoPoint」には、物体/顔検出などのMachine Learning (ML)をはじめ、ビデオ再生カメラのISP調整3Dグラフィックス(OpenGL ES)などのマルチメディアのデモがあり、i.MXアプリケーション・プロセッサの各種機能を簡単に確認できますので、是非お試しください。

詳細を読む...

件数が多いもの
1 0 818
Yutaka_Okui
NXP Employee
NXP Employee

最適な電源ICを選ぶときに、どのような手順で、候補となる電源ICを絞り込んでいくのが良いのかを、大きく、以下の3つのステップでまとめてみました。

・Step 1 - 候補となる電源ICの選定

・Step 2 - 実装面積の確認

・Step 3 - 熱設計の確認

*第3回では、Step 3を説明します。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 931
Yutaka_Okui
NXP Employee
NXP Employee

最適な電源ICを選ぶときに、どのような手順で、候補となる電源ICを絞り込んでいくのが良いのかを、大きく、以下の3つのステップでまとめてみました。

・Step 1 - 候補となる電源ICの選定

・Step 2 - 実装面積の確認

・Step 3 - 熱設計の確認

*第2回では、Step 2を説明します。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 752
Yutaka_Okui
NXP Employee
NXP Employee

最適な電源ICを選ぶときに、どのような手順で、候補となる電源ICを絞り込んでいくのが良いのかを、大きく、以下の3つのステップでまとめてみました。

・Step 1 - 候補となる電源ICの選定

・Step 2 - 実装面積の確認

・Step 3 - 熱設計の確認

*第1回では、Step 1を説明します。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 994
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

 

前回まではG-cell MEMSについて説明しました。

第四回はこのG-cell MEMSのコンデンサ容量をASICで信号処理する機構について取り上げたいと思います。

詳細を読む...

件数が多いもの
1 0 1,030
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

 

前回はG-cell MEMSの概要について説明しました。

第三回は出力特性や特殊機能などについて取り上げます。

詳細を読む...

件数が多いもの
1 0 1,185
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

 

第二回は加速度センサの心臓部である、加速度を検知する機構について取り上げます。

詳細を読む...

件数が多いもの
1 0 977
satoshikamiya
NXP Employee
NXP Employee

セキュリティ要件適合評価及びラベリング制度(以後「JC-STAR」と表記します)は、独立行政法人情報処理推進機構(IPA)が運用する日本独自のIoT製品セキュリティ評価制度です。本稿では、JC-STARの概要と、NXPのセキュリティ製品について紹介します。

(読了:5分)

詳細を読む...

件数が多いもの
1 0 1,407
yutaka_ando
NXP Employee
NXP Employee

i.MX 8M Plusの評価ボード (EVK) を用いて、マルチメディア機能(ビデオ再生、オーディオの録音/再生、カメラ動作、Wi-Fi接続、NPU動作など)の動作を確認する方法について説明します。

詳細を読む...

件数が多いもの
1 0 1,258
YuseiUegama
NXP Employee
NXP Employee

組み込みデバイスの限られたリソースの中でLLMを使用するためには、RAGが必要となります。

本稿では、NXPの LLM + RAG ソリューション 「eIQ GenAI Flow」についてハンズオン形式で紹介します。

詳細を読む...

件数が多いもの
2 0 2,041
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

(読了:5分)

詳細を読む...

件数が多いもの
2 0 1,430
Keita_Nagashima
NXP Employee
NXP Employee

eIQ Time Series Studio(時系列モデル開発ツール)の概要から、プロジェクトの作成 → データセット → トレーニング → エミュレーション → デプロイメント → データロギングと、使い方の流れを記載しています。

本記事は、eIQ Time Series Studio v1.0.4を起動させた際に表示される"Documentation"メニューに記載されている資料を翻訳したものです。必ず最新の英語版をご確認いただき、本記事はあくまでも補足的な内容としてご利用ください。

詳細を読む...

件数が多いもの
1 0 3,785
Keita_Nagashima
NXP Employee
NXP Employee

CANバス/プロトコルの概要から特長について説明します。

NXPは古くからCANに携わっており、マイコン、プロセッサ、トランシーバと様々なCAN製品を提供しています。

詳細を読む...

件数が多いもの
1 0 2,346
yumb
NXP Employee
NXP Employee

2025年4月、当社のUniversity Programの一環として、徳島県の神山まるごと高専で jig.jp創業者・福野泰介氏が行う新入生向けの導入授業「ITブートキャンプ2025」に、ボランティア参加しました。本ブログではその体験を振り返りつつ、教育支援の現場でのMCX開発ボードの活用事例をご紹介します。

詳細を読む...

件数が多いもの
1 0 3,424
yutaka_ando
NXP Employee
NXP Employee

i.MXアプリケーション・プロセッサの評価ボードで消費電力を測定する方法をまとめたページです。

  • i.MX 8M Plus Power EVKをベースにしています。
  • 電力モードを切り替える方法についても説明します。
  • 動作周波数の変更方法や、使用しないブロックのディセーブル方法についても説明します。
詳細を読む...

件数が多いもの
2 0 1,748
akifumiokano
NXP Employee
NXP Employee

こどもパソコンIchigoJamは,LPC1114で動作する最初のバージョンが2014年に登場以来,教育の場だけに留まらず,様々な応用が広がっています.
2024年にはオープンソース化.さらに2025年にはNXPの最新マイコン:MCXシリーズのMCX-A153に対応.現在,GitHubで公開されているこのコードをMCX-A153を搭載した評価基板:FRDM-MCXA153で動作させてみるまでを解説します.

詳細を読む...

件数が多いもの
0 0 1,930
akifumiokano
NXP Employee
NXP Employee

NXPのマイコン:MCXシリーズのソフトウェア開発にはMCUXpresso IDEが無料で使えます.
またさまざまなMCUXpresso IDEで使えるサンプル・コードが提供されています.ここではIDEとSDKのインストールの手順を解説します.

これを読めば,誰でも簡単に開発環境&SDKをインストールできて,サンプル・コードまで動かすことができます!

詳細を読む...

件数が多いもの
0 0 2,265
Yutaka_Okui
NXP Employee
NXP Employee

「電源ってなに?」、という人に、最初に知っておいてほしいことを、まとめたページです。

第五回として、PMIC(Power Management Integrated Circuit)とSBC(System Basis Chip)について、説明しています。
(読了:5分)

詳細を読む...

件数が多いもの
1 0 1,508
Takayoshi_Obara
NXP Employee
NXP Employee

NXPのパワーマネージメントIC(PMIC/SBC)を車載向けマイコン(S32シリーズ)に使用するメリットを4つ説明します。

詳細を読む...

件数が多いもの
2 0 1,426