Motor Control and Smart Energy Knowledge Base

cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Control and Smart Energy Knowledge Base

Labels

Discussions

Sort by:
1. Purpose Multiple RT1XXX EVKs require extra wiring to support FRDM-MC-LVPMSM and enable Motor Control SDK examples. To solve this problem, the interconnection board was developed. You can find more about platforms supporting motor control on our MCUXpresso SDK for Motor Control page.     Resulted board:   2. Compatibility This table describes the compatibility of i.MX RT EVKs supporting Motor Control examples. EVK Wiring needed evkmimxrt1010 Works without extra wiring and without Interconnection board evkimxrt1020 Needs extra wiring, no Interconnection board evkimxrt1024 Works without extra wiring and without Interconnection board evkimxrt1040 Works with Interrconnection board evkbimxrt1050 Works with Interrconnection board evkimxrt1060 Works with Interrconnection board evkbimxrt1060 Works with Interrconnection board evkcimxrt1060 Works with Interrconnection board evkimxrt1064 Works with Interrconnection board evkmimxrt1160 Needs extra wiring, no Interconnection board evkmimxrt1170 Needs extra wiring, no Interconnection board evkbmimxrt1170 Works without extra wiring and without Interconnection board evkmimxrt1180 Works without extra wiring and without Interconnection board   3. Design files The complete design package is available and attached to this article.  
View full article
Question As we know, the TPPSDK supports S32K144 MCU and various Kinetis MCUs to initialize GD3000 in NXP MC solutions. Because of the release of S32K3 and related SW RTD, it’s necessary to expand the capability of TPPSDK to support S32K3 MC based RTD LLD driver or MCAL driver. Unfortunately, the AA team will not maintain the TPPSDK anymore.  How could we configure the GD3000 chip for S32K3 platform?   Answer I took some time to finish this work. Here I'd like to share you the The Expanded TPPSDK Based on S32K3 RTD that is suitable for S32K3 MC application. You can find the Application Note, the source code of new TPPSDK (GD3000 driver), two examples in the attachment. I hope these materials can help you get start with the expanded TPPSDK on S32K3. If you have any question or comment on this SW, please feel free to contact me.  
View full article
This community shares the information about motor control and smart energy in general.   Control of all motor types: PMSM, BLDC, ACIM, SR and smart energy topics could be discuss. Typically the applications are based on the Motor control library (FSLESL and API translator), and frameworks which makes the solution really simple.   Get start to contribute now !
View full article