KDS Document List

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS Document List

KDS Document List

This list includes all the documents in the NXP community Kinetis Design Studio space.

You can download the latest version of KDS on NXP web : Kinetis Design Studio Integrated Development |NXP .

 

Installation and Update

New Kinetis Design Studio v3.2.0 available

Kinetis Design Studio Update V3.1.0 available

New Kinetis Design Studio V3.0.0 available

Kinetis Design Studio V2.0.0 available on the Web!

Kinetis Design Studio V1.1.1 Released!

Kinetis Design Studio V1.1.0: Release Notes and News

Kinetis Design Studio V1.0.1 Beta Release Notes

KDS Install Guide

KSDK 1.3.0 Documents Plugin for KDS 3.0.0

Extended Device Support: Updated P&E Debug Plugin V1.1.4 for KDS V1.1.1

Kinetis Design Studio V1.0.1 Beta Release Notes

Support for Kinetis M (KM14, KM33, KM34) in Kinetis Design Studio

 

How to Use

 

Generate aligned HEX and S-record data output with GNU in KDS 3.2 

How to support multiple targets in CodeWarrior(Classic, Eclipse)/KDS 

Adding CMSIS-DSP Library to a KSDK 2.x project in Kinetis Design Studio 

Using KBOOT v2 on KDS in Debug Mode

Debugging Bootloader and Application using Kinetis Design Studio V3.2.0

Changing MCU for SDK2.0 project in KDS

How to start customized KSDK V1.2 project based on KSDK demo code

Tutorials using the Kinetis SDK V1.0.0 with Kinetis Design Studio 

How to Create a C++ Project Using MQX RTOS for KSDK1.2

Converting a non-Processor Expert Project into a Processor Expert Project

Creating KDS project based upon the KL46 from CW project

How to Add Existing Files to KDS

Relocating Code and Data Using the KDS GCC Linker File for Kinetis

Increasing Eclipse Heap Space to Improve Performance

Semihosting for Kinetis Design Studio

Getting started with CDE in Kinetis Design Studio

Getting started with SVN and Kinetis Design Studio

Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V...

Importing MCU V10.6 projects (sample, using PE and MQX) under KDS V1.1.1 

Quickstart Guide for KDS v1.0.1 beta

Using ESFC bit - Flash programming routines in Cotex M0+ kinetis MCU

Start working with NXP Touch Software library

How to Start CAN Module Development on KDS v3.2.0 + Processor Expert

 

Compiler and Linker

Changing the ARM GNU Tool Chain in Kinetis Design Studio

Extended Inline Assembly with Kinetis Design Studio

How to build BeeKit exported CodeWarrior 10.6 projects using KDS

How to add uninitialized data section to a GCC build

Merging applications using Kinetis Design Studio

 

Debugger Interface and firmware

GDB Debugging with Kinetis Design Studio

KDS Debug Configurations (OpenOCD, P&E, Segger)

Summary of FRDM-K64F open source debug interface

Summary of FRDM-K22F debug interface

Using FRDM-K64F with P&E and Segger OpenSDAv2 Firmware

FRDM-K22F: Debugging with P&E OpenSDAv2.1 Firmware

FRDM-K22F: Debugging with Segger J-Link OpenSDAv2.1 Firmware

OpenOCD support for K22FN512 & K24FN256 in KDS

How to setup SEGGER J-Link lite debugger connection in Kinetis Design Studio 1.1.1

Register Detail Debugging with KDS

 

KDS Application

KEA128 CAN Bootloader 

Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+

Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4

Using the FRDM-KL25 Board as a USB Keyboard in KDS

Using the FRDM-KL25 Board as a USB Mouse in KDS

KDS - Simple Air Mouse on a FRDM KL25Z

Hello World bare metal project for FRDM-KL25 using KDS

Using the Accelerometer on the FRDM-KL25 Board in KDS

Using the FRDM-KL46 Board as a USB Mouse in KDS

Using the FRDM-KL46 Board as a USB Keyboard in KDS

Using the LCD screen on a FRDM-KL46 Board as a timer using KDS

Using the LCD screen on a FRDM-KL46 Board to display accelerometer data using KDS

Using the LCD screen on a FRDM-KL46 Board to display temperature using KDS

Using the LCD screen on a FRDM-KL46 Board to light intensity using KDS

Baremetal code examples using FRDM-K64F

Using the FRDM-MK64 Board to write to an SD Card in KDS

Using the FRDM-MK64 Board to write to Accelerometer data to an SD Card in KDS

SD Card Bootloader :how to using SD card to update existing firmware on CodeWarriror or KDS

Using the Accelerometer on the FRDM-MK64 Board in KDS

Blinking an LED on a FRDM-MK64 Board in KDS

Reaction measuring game on a FRDM-KL46 board using KDS

Tutorials: WS2812B LED Stripes with the FRDM-K64F Board

Toggling the FRDM-K64F RGB LED using interrupts in Kinetis Design Studio (KDS)

How to use printf() to print string to Console and UART in KDS2.0

Disabling Watchdog for 'Bare' Projects

 

Bug and Workaround

Defect fix for KSDK1.2/KSDK1.3 MK02FN128 -- “xxx.elf uses VFP register arguments”

kds_quick_start has ommision error.

Uninstalling KDS: "Error opening installation log file."

 

KDS FAQ

KDS Frequently Asked Questions (FAQ)

标签 (1)
标记 (1)
无评分
版本历史
最后更新:
‎03-24-2016 11:19 PM
更新人: