Extended Device Support: Updated P&E Debug Plugin V1.1.4 for KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Extended Device Support: Updated P&E Debug Plugin V1.1.4 for KDS

Extended Device Support: Updated P&E Debug Plugin V1.1.4 for KDS

A new updated plugins is available from P&E with extended device support (see list at the end) for KDS V1.1.1:

 

NOTE: You need V1.1.1 for this update, as V1.1.0 has an issue with updating the P&E plugins, unless you apply a manual workaround. See the V1.1.0 release notes.

 

Use the menu Help > Install New software and use the PEmicro update site from the list:

14673_14673.pngpastedImage_0.png

Select the updated plugin, and press 'Next' to go through the installation.

At the end, you are asked to re-start KDS.

 

 

Release Note information:

KDS_513_b140905 includes the following features and bug fixes:

 

(*) Adds device support for the following devices:

(*) Add MBED/PEMICRO OpenSDA support for FRDM-K22F and FRDM-K64F boards

 

Kinetis - K24 Series

k24fn256m12

 

Kinetis - KL17/KL27/KL33/43 Series

kl17z32m4

kl17z64m4

kl17z128m4

kl17z256m4

kl27z32m4

kl27z64m4

kl27z128m4

kl27z256m4

kl33z128m4

kl33z256m4

kl43z128m4

kl43z256m4

 

Kinetis - KMx - Photon3

km14z64am5

km14z128am5

km33z64am5

km33z128am5

km34z128am5

 

Kinetis - KV4x

kv40f64m15

kv40f128m15

kv40f256m15

kv43f64m15

kv43f128m15

kv44f64m15

kv44f128m15

kv45f128m15

kv45f256m15

kv46f128m15

kv46f256m15

 

Kinetis - K11/K21 - K20 512k/1Mb

k11dn512am5

k11dx128am5

k11dx256am5

k21dn512am5

k21dx128am5

k21dx256am5

k21fn1m0am12

k21fx512am12

 

Kinetis- K02F Series:

K02F128M10

K02F64M10

 

Kinetis- KW Series:  

KW01Z128

KW21D256M5

KW21D512M5

KW22D512M5

KW24D512M5

 

Kinetis- K66/65 Series:

K66FX1M0M18

K65FX1M0M18

K66FN2M0M18

K65FN2M0M18

 

Kinetis - WPR Series alpha

WPR1516M2

 

KDS_506c_b140807 includes the following features and bug fixes:

 

Plugin Version 1.12.

 

ENGR00325552 - Includes changes to p2.inf to include both metadata and artifact repositories on the same line.

ENGR00325553 - Specify IP issue for Ethernet P&E interfaces (Cyclone MAX, Tracelink) is addressed.

Adds support for MBED Bootloader 2.1 on FRDM-K22F and FRDM-K64F boards.

 

 

 

Happy Updating :-)

Labels (1)
Comments

Hi Erich,

     How to add new product in KDS2.0, eg. KL33.

     I update http://www.pemicro.com/eclipse/updates in KDS2.0, but it still don't have KL33, how to solve it?

    Any reply will be appreciated.

Regards,

Jingjing

There is a new P&E update (Updated P&E GDB Server for Eclipse: Connect/Attach and Advanced Flash Programming | MCU on Eclipse) which includes KL33 device support.

If you install the Kinetis SDK for KL43Z, it includes KL33Z support. To show it up in Eclipse, install the eclipse update in

C:\Freescale\KSDK1.0.0_KL43Z_1.0.1\tools\eclipse_update

I hope this helps,

Erich

Thank you very much!

My question is solved after installing the KSDK for KL43Z.

Regards,

Jingjing

No ratings
Version history
Last update:
‎09-08-2014 08:34 AM
Updated by: