Using KBOOT v2 on KDS in Debug Mode

Document created by Alice_Yang Employee on May 23, 2016Last modified by Diana Torres on Feb 28, 2017
Version 3Show Document
  • View in full screen mode

The Kinetis Bootloader(KBOOT) v2 is now available on webpage, it supports building bootloader image on KDS v3.2  IDE. About how to use the KBOOT to load a user's application on kinetis MCU please refer to the DOC”Kinetis Bootloader Demo Application User’s Guide”(It is under the KBOOT install package: NXP_Kinetis_Bootloader_2_0_0\doc).


When using KDS build the bootloader image, there is one point need to be paid attention: the image size in debug mode build is over 0xa000(the 0xa000 is user's application start address). That is to say , if we download the debug build image to mcu, can’t use it . So this doc povides the correct way to use the KBOOT on KDS, the problem shows in FRDM-K64 and FRDM-K22 boards, on other chips , if they also have the out of range problem, the correct method is the same .


How to correctly use the KBOOT v2 on KDS ? Please check this DOC on attachment !