KEA128 CAN Bootloader

Document created by Alice_Yang Employee on Sep 1, 2016Last modified by ebiz_ws_prod on Dec 13, 2017
Version 10Show Document
  • View in full screen mode

In most cases, there is no debug interface for user to update the application or fix bugs , so user can use Bootloader. Bootloader is a small program put into a device that allows user using communication interfaces to upgrade application , such as use UART , I2C , USB, CAN and so on.


This application describe a bootloader based on the TRK-KEA128 board with CAN interface. The bootlaoder and user application code are written in separate projects , user can program the bootloader with tools such as J-Link ,Multilink, then boot the application file through CAN. The bootloader and application code are all provided , user can porting it to their own board of KEA/KE chips.

 

Pay attention to that, if your board is TRK-KEA128 Rev D, you need give a low signal to STB of PC33901 chip to set it in Normal mode:

    GPIOB_PDDR |= (1<<16);
    GPIOB_PCOR = (1<<16);

In other old version boards , for example Rev C, the STB have been connected to ground , so we needn't configure it .

 

 

IDE: Kinetis Design Sturio v3.2

Hardware: TRK-KEA128

 

About the detail code and introduction of this bootloader, please check the attachment .

 

Thanks for my colleague Jennie Zhang and  Kerry Zhou .

Welcome your valuable advice .

 

Best  Regards!

Alice

 

 

Original Attachment has been moved to: teraterm-4.89.exe.zip

Original Attachment has been moved to: Bootloader_TRK-KEA128.zip

Attachments

Outcomes