USB Mouse in KDS
Description:
A project made in KDS using the accelerometer on a FRDM-KL25Z128M4 board to control a USB mouse input.
The LED will flash red while not connected as a USB mouse, and flash green when it is.
The reset button will left click.
Sensitivity of the mouse can be changed by altering the HIDM1_Move command in main.c
Reset button can be changed from left to right click by altering comments in main.c
Sections of code taken from:
- http://mcuoneclipse.com/2012/09/21/tutorial-accelerating-the-kl25z-freedom-board/
- http://mcuoneclipse.com/2013/08/01/using-the-frdm-kl25z-as-a-usb-mouse-device/
Is it possible to adapt the board to use bluetooth, i.e. without using the debugging cable attached?
It may be possible with a Bluetooth to UART module. I will admit I am not experienced in this field though.