Support for Kinetis M (KM14, KM33, KM34) in Kinetis Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for Kinetis M (KM14, KM33, KM34) in Kinetis Design Studio

Support for Kinetis M (KM14, KM33, KM34) in Kinetis Design Studio

A service pack has been published in the download section of Kinetis Design Studio on http://www.freescale.com/kds which adds bare metal (no Processor Expert, no Kinetis SDK) support for the following Kinetis M devices:

76789_76789.pngpastedImage_1.png

 

The update is available for KDS v3.0.0 for Linux, Mac and Window:

76904_76904.pngpastedImage_3.png

 

The download is available for each of the host operating systems supported by KDS:

76788_76788.pngpastedImage_0.png

The downloaded archive (zip file) contains the release notes and the Eclipse update which gets installed into KDS using the menu Help > Install New software and then using the zip file inside the archive (unpack the archive first).

Labels (1)
No ratings
Version history
Last update:
‎09-17-2015 01:14 PM
Updated by: