i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
BSP: L5.4.47-2.2.0-rc2 Board: imx8QM B0 HW:  LVDS2HDMI , MIPIDSI2HDMI. It is the porting of i.MX8QM dpu loopback to isi. to the 5.4.y, with the addition of the MIPI-DSI loopback and the HDMI loopback.  Overview of the DC capture configuration: For enabling the capture: only DC 0 Stream 0  and DC 1 Stream 1 can be captured The pixel link Master address should be set to 3 because the Receiver Address at ISI is 3 and can't be changed. To continue displaying the stream, the Receiver Address at LVDS and DSI or HDMI should be changed to 3. It is possible to change the RA by using GPIO of the modules.   Patches: Create V4L2 device enabling the capture of by the ISI of DC loop-backs. Enable ISI capture from DSI 0 / LVDS 1 in 1920x1080 (at the same time.) Enable ISI capture from HDMI in 2840x2160 (half with even pixel) in 1920x2160. While capturing with the ISI, the captured screen continue to be displayed. Remark: Ov5640 cameras are also enabled in the same dtb. So 4 stream in 1920x1080 can be captured at the same time. Installation and gstreamer command: See readme
查看全文
       
查看全文
     
查看全文
Harware: - i.MX7D-SDB board - QCA9880 card with MINI PCIe Interface The Wifi module is connected to the PCIe slot on the board.     Software: - Ubuntu 18.04 LTS Host - L4.19.35_1.1.0 BSP   Tool: - uuu 1.2.68 for linux (run on ubuntu host)   Toolchain: - The toolchain can be obtained from the Yocto BSP. Please read and follow the steps in i.MX_Yocto_Project_User's_Guide to build the BSP and then read the Chapter of "How to build U-Boot and Kernel in standalone environment" in i.MX_Linux_User's_Guide to build the toolchain.   Build the Kernel: # mkdir imx_build # cd imx_build # git clone https://source.codeaurora.org/external/imx/linux-imx -b imx_4.19.35_1.1.0 # cd linux-imx # source /opt/fsl-imx-fb/4.19-warrior/imx6/environment-setup-cortexa9hf-neon-poky-linux-gnueabi # export ARCH=arm # make clean # make imx_v7_defconfig # make menuconfig - Select the PCIe driver and the Wifi support - PCI controller drivers--->                    DesignWare PCI Core Support----> - Networking support----->                             Wireless----->   - Select the ath10 driver (it supports QCA988X) Device Drivers---->             Network device support----->                                      Wirless LAN----> - Save and Exit. - Add the firmware in the .config file: Get the firmware file (e.g. firmware-2.bin) from your wifi vendor or download it from the web. Put the firmware in linux-imx/firmware/ folder. Edit the .config file and add these two lines: CONFIG_EXTRA_FIRMWARE="board.bin firmware-2.bin" CONFIG_EXTRA_FIRMWARE_DIR="/home/jimmy/imx_build/linux-imx/firmware" - Build the kernel # make Then the zImage will be obtained in arch/arm/boot.   Using uuu to program the SD card: - Downloading demo image of L4.19.35_1.10 from the nxp website. - Copy the zImage to the directory - Copy the uuu (V1.2.68) to the directory - Copy the samples/example_kernel_emmc.uuu to imx7d_kernel_emmc.uuu - Modify the image the imx7d_kernel_emmc.uuu - In the demo image, you will see the files like this: - run uuu and the script to program the images.   Wifi driver loaded and wlan0 is up: # dmesg | grep pci   # ifconfig -a   Reference Document: - i.MX_Linux_User's_Guide.pdf - i.MX_Porting_Guide.pdf  
查看全文
As of this writing, April 2015, the default sdcard image created from a Yocto Project build has all the software images nicely aligned to create a SDCARD. 10/7/2020: Update - SDCARD image names have been updated to images ending with .wic as the default from Yocto Project.  The process is the same for both .sdcard and .wic files.   There are two partitions within the image: A W95 FAT32 (LBA) partition that contains the Linux zImage, and various device tree binary (dtb) files A Linux root file system. Each partition can be mounted from your Linux host computer, then you can read or write the partition contents. Here are the steps based on the core-image-base recipe for the imx6sxsabresd machine using Yocto Project release L3.14.28_1.0.0_GA.   The name of the image: core-image-base-imx6sxsabresd.sdcard Run the fdisk command to view the contents of the image: $ fdisk -l core-image-base-imx6sxsabresd.sdcard Disk core-image-base-imx6sxsabresd.sdcard: 100 MB, 100663296 bytes 4 heads, 32 sectors/track, 1536 cylinders, total 196608 sectors Units = sectors of 1 * 512 = 512 bytes Sector size (logical/physical): 512 bytes / 512 bytes I/O size (minimum/optimal): 512 bytes / 512 bytes Disk identifier: 0x00074663 Device Boot Start End Blocks Id System core-image-base-imx6sxsabresd.sdcard1 8192 24575 8192 c W95 FAT32 (LBA) core-image-base-imx6sxsabresd.sdcard2 24576 188415 81920 83 Linux   Determine the byte offset into the sdcard image of where each partition starts:  core-image-base-imx6sxsabresd.sdcard1 starts at sector 8192. One sector unit is 512 bytes.                8192 * 512 = 4194304 core-image-base-imx6sxsabresd.sdcard2 starts at sector 24576. 24576 * 512 = 12582912   Mount Partitions First create mount points: $ sudo mkdir /mnt/{mp1,mp2}    sdcard1 partition $ sudo mount -o loop,offset=4194304 core-image-base-imx6sxsabresd.sdcard /mnt/mp1 NOTE: An alternate method for determining the offset, see below: $ sudo mount -o loop,offset=$((512 * 8192)) core-image-base-imx6sxsabresd.sdcard /mnt/mp1 sdcard2 partition $ sudo mount -o loop,offset=12582912 core-image-base-imx6sxsabresd.sdcard /mnt/mp2 View the contents of each mounted partition $ ls /mnt/mp1 imx6sx-sdb.dtb imx6sx-sdb-lcdif1.dtb imx6sx-sdb-reva.dtb imx6sx-sdb-sai.dtb imx6sx-sdb-emmc.dtb imx6sx-sdb-m4.dtb imx6sx-sdb-reva-ldo.dtb zImage $ ls /mnt/mp2 bin boot dev etc home lib lost+found media mnt proc run sbin sys tmp usr var   When done release the mount points and remove them from /mnt $ sudo umount /mnt/{mp1,mp2} $ sudo rm /mnt/{mp1,mp2}  
查看全文
To enable USB 2.0 port on BB for USB OTG, you need to apply below two changes: device/fsl.git   diff --git a/imx8q/mek_8q/init.usb.rc b/imx8q/mek_8q/init.usb.rc index af4e388..0f3ab0b 100644 --- a/imx8q/mek_8q/init.usb.rc +++ b/imx8q/mek_8q/init.usb.rc @@ -44,7 +44,7 @@ on early-boot      mount functionfs mtp /dev/usb-ffs/mtp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      mount functionfs ptp /dev/usb-ffs/ptp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      setprop sys.usb.mtp.device_type 3 -    setprop vendor.usb.config "5b110000.usb3" +    setprop vendor.usb.config "ci_hdrc.0"      write /sys/module/libcomposite/parameters/disable_l1_for_hs "y"      symlink /config/usb_gadget/g1/configs/b.1 /config/usb_gadget/g1/os_desc/b.1   vendor/nxp-opensource/kernel_imx.git           revert below patch:           commit 2f9586c120971312e61df464264993899cf34536           Author: yang.tian <yang.tian@nxp.com>           Date:   Tue Jan 7 13:30:02 2020 +0800       MA-15242 Set usb2.0 port as usb host only for mek_8q  
查看全文
This document is a user guide for the GStreamer version 1.0 based accelerated solution included in all the i.MX 8 family SoCs supported by NXP BSP L5.4.24_1.1.0. Some instructions assume a host machine running a Linux distribution, such as Ubuntu, connected to i.MX 8 device. These commands were tested using Ubuntu 18.04 LTD, and while Ubuntu is not required on the host machine, other distributions have not been tested. These instructions are targeted for use with the following hardware: • i.MX 8MQ EVK • i.MX 8MN EVK • i.MX 8MN EVK • i.MX 8QXP MEK B0 • i.MX 8QM MEK B0   Release History v1.0 - Mar 2020 - Initial release. v2.0 - Sep 2020: Added the following content: - Mux/Demux Examples - Audio Examples - Image Examples - Transcode Examples - Streaming Examples - Multi-Display Examples - Scaling and Rotation Examples - Zero-copy Examples - Debug Examples Maintainers: . Marco Franchi . Pedro Jardim
查看全文
1. HW Environment:     IMX8mp-evk board.     ITE6151 mipi dsi to eDP bridge board.   2. SW Environment:     IMX YOCTO 5.4.24-2.1.0 release.   3. Patch operation:     a. git clone https://source.codeaurora.org/external/imx/linux-imx.git     b. git checkout -b  imx_5.4.24_2.1.0 origin/imx_5.4.24_2.1.0     c. patch -p1 < ../ite6151_mipi2edp_linux_5.4.24_20200921.patch   4. Tested on imx8mp-evk board with DP monitor on 1080p mode: 5. Attached doc list:     IT6151 demo board user guide v1.0.pdf ------  ite6151 bridge board HW guide     it6151_qfn48_v20_20190905-01_end.pdf  ------  ite6151 bridge board SCH     imx8mp_ite6151_mipi2edp_linux_5.4.24_20200921.patch ------  Linux kernel driver patch     Image + imx8mp-evk-it6151.dtb  ------  test image and dtb  
查看全文
After following instructions on how to change DRAM PLL frequency, here is a quick comparison of Stream, running on the i.MX 8MM. Normalized to LPDDR4-3000, based on 5.4.24_2.1.0​ BSP Stream LP4-3000 LP4-2400 DDR4-2400 LPDDR-1866 Copy: 1 0.810 0.735 0.497 Scale: 1 0.896 0.765 0.756 Add: 1 0.899 0.683 0.762 Triad: 1 0.902 0.680 0.767      
查看全文
Description       This doc explain how to enable the plugin boot on i.MX6Q/6DL and which used for change the pll2 clock and add the spread spectrum support to pass the EMI test. we still list the source codes of 3.0.35 and 4.1.15. to explain the dts/non-dts kernel support.       本文旨在说明如何在i.MX6Q/6DL上实现plugin启动,以支持展频和改变pll2的频率,其目的是为了通过 EMI测试。也附上了基于3.0.35和4.1.15的源代码,以供参考   Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 SabreSDP https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false          Version: MX6Q_PLUGIN_FC_SSC_V7-20200915_chn..pdf(chinese version)add baidou support MX6Q_PLUGIN_FC_SSC_V7-20170504_eng-chapter-imx6dl.doc+MX6Q_PLUGIN_FC_SSC_V3-20170309_eng.doc(english version)      
查看全文
- In LTIB generate a rootfs.jffs2 with a erase block size of 16KB: ./ltib -c ---Target Image Generation   Options ---> ---Choose your root file system image type     Target image: (jffs2) --->   (16) jffs2 erase block size in KB - Copy the generated rootfs.jffs2 to /tftpboot : cp rootfs.jffs2 /tftpboot - Program 200732 Redboot binary. The 200732 Redboot is available in the 20071008 BSP iso. After mounting the iso go to the bootloaders directory, extract the redboot_200732.tar.gz file and use the pre-built mx31ads_redboot.bin inside the bin directory. - Boot from NAND and setup the network parameters fis init load -r -b 0x100000 /tftpboot/zImage fis create -l 0x200000 kernel load -r -b 0x100000 /tftpboot/rootfs.jffs2 fis create -l 0x1d000000 root - Pass the following kernel command line: fis load kernel exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock6 rootfstype=jffs2 init=linuxrc ip=none mtdparts=mx" You need to replace mtdblock6 with your rootfs partition, see below: mx31# cat /proc/mtd dev:    size  erasesize  name mtd0: 00040000 00020000 "RedBoot" mtd1: 001a0000 00020000 "kernel" mtd2: 0001f000 00008000 "FIS directory" mtd3: 00001000 00008000 "RedBoot config" mtd4: 00040000 00004000 "RedBoot" mtd5: 00200000 00004000 "kernel" mtd6: 01d00000 00004000 "root" mtd7: 00003000 00004000 "FIS directory" mtd8: 00001000 00004000 "RedBoot config" mx31#
查看全文
How to connect i.MX51 and Ubuntu using USB cable: i.MX51 Side Plug in USB cable. getprop debug.adb.usb - Shows that debug.adb.usb are not set by default setprop persist.service.adb.enable 0 -> disable adb setprop debug.adb.usb 1 - adb will be through USB (for Ethernet, use setprop debug.adb.usb 0) setprop persist.service.adb.enable 1 -> enable adb Example: # getprop debug.adb.usb  # # # setprop persist.service.adb.enable 0 disabling adb # adb_release android_usb gadget: high speed config #1: android setprop debug.adb.usb 1 # # setprop persist.service.adb.enable 1 enabling adb # adb_open adb_release adb_open android_usb gadget: high speed config #1: android # Ubuntu Side On Ubuntu side, the most important tip is regarding permission. ADB server MUST be started with root right. Example of right mistake: $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb devices List of devices attached ????????????    no permissions  $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb shell error: insufficient permissions for device How to proceed to get permission: $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb kill-server $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb start-server * daemon not running. starting it now * * daemon started successfully * $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb devices List of devices attached 0123456789ABCDEF    device  $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb shell ADB over Ethernet/Wi-Fi To make ADB work in i.MX51 using TCP: In your host machine: - Install Android SDK - export ADBHOST=BOARD_IP (setenv ADBHOST=xxx.xxx.xxx.xxx) - adb kill-server In your board: - make sure that ro.secure property is *not* set when the adbd daemon is launched, so edit the file default.prop - make sure that /dev/android_adb or /dev/android do *not* exist - stop adbd - start adbd Now you will be able to list the device: hamilton@saygon:/opt/work/androidsdk/android-sdk-linux_86/tools$ ./adb kill-server hamilton@saygon:/opt/work/androidsdk/android-sdk-linux_86/tools$ ./adb devices * daemon not running. starting it now * * daemon started successfully * List of devices attached emulator-5554   device
查看全文
Creating an image A kernel image and a root file system can be created using LTIB, or compiling the kernel and setting the correct set of files. Create a root file system image from a set of files converting the files to a jffs2 file system. For this, install the package mtd-tools. In Ubuntu type apt-get install mtd-tools For making an root file system for flash, use the jffs2 file system like: mkfs.jffs2 -r rootfs -e 0x40000 -s 0x800 -n -o rootfs.jffs2 Where rootfs/ is the original set of file for the file system and rootfs.jffs2 is the output image file. Flashing Some connection errors can be avoided by Configuring RedBoot. The process below uses TFTP to copy the files between host and target. Copy the kernel image and the root file system image to the TFTP dir. For example, in All Boards LTIB dir, type sudo cp ./rootfs/boot/zImage /tftpboot sudo cp rootfs.jffs2 /tftpboot/ Where /tftpboot is the dir configured for TFTP The next steps are performed in a Minicom session, and happens on the board. Formatting the flash: fis init Flashing kernel Load kernel image (zImage) using the command below. Remember to modify the host IP address: load -r -b 0x100000 /tftpboot/zImage -h 10.29.244.99 The address 0x100000 is used as a temporary location Create the kernel fis create -f 0x100000 kernel Flashing root file system Load root file system image (rootfs.jffs2) to the temporary address. Remember to modify the host IP address: load -r -b 0x100000 /tftpboot/rootfs.jffs2 -h 10.29.244.99 Create the root file system in the right address (0x600000, for i.MX35 PDK) fis create -f 0x600000 root You can now load your kernel in the flash by typing: fis load kernel To know if the root file system written in the flash was correctly saved, execute the NFS file system and mount the flash. For load the the root file system by NFS, type: exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.244.99:/tftpboot/ltib init=/linuxrc ip=10.29.241.6:10.29.244.99" Wait the system go up, then mount the flash at /mnt. Reminde that the flash has a jffs2 file system. mount -t jffs2 /dev/mtdblock8 /mnt ls /mnt List the /mnt contents. The output must be the right file system. Modifying the initial script Reset the board and press CTRL-C. Type fc to modify the configurations and insert the initialization script. RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> fis load kernel >> exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock8 rw rootfstype=jffs2 ip=dhcp" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> Remember to save the configuration in the flash by typing y Reset the system. To certify that the board is loading the system from flash, remove the Ethernet cable.
查看全文
In order to get USB cameras (web cams) working on i.MX 51 EVK board running Ubuntu, a few steps must be followed, and they are: Enable USB Camera's drivers on Kernel Test it using Gstreamer or another compatible software (as Cheese) Kernel Driver USB cameras (web cameras) on Linux work over GSPCA driver, to enable this driver you need to go to: ./ltib -c   [*] Configure the kernel     Device Drivers -->          Multimedia Devices -->               [*] Video Capture Adapters -->                    [*] V4L USB Devices -->                         <*> USB Video Class (UVC)                                      [*] UVC input events device support                         <*> GSPCA Based WebCams --> From this point, you need to choose your specific driver. If you don't know, you can select all of those options as a built-in module "<*>" that will work. GSPCA Drivers USB Camera Detection Connect your USB camera to the USB Host port on i.MX 51 EVK board and then type "dmesg", and also check if there is a video0 device using: ubuntu@ubuntu-desktop:~$ ls /dev/video0 /dev/video0 USB Camera Detection Gstreamer Command Line In order to test your USB camera using Gstreamer plugin, use the following command line to perform it: ubuntu@ubuntu-desktop:~$ gst-launch-0.10 v4l2src ! ffmpegcolorspace ! ximagesink and the results: Hi there !!! EOF !
查看全文
The system controller timer service is responsible for: Watchdog - The watchdog resource is managed by the SCU. The SCFW exposes a "virtual" watchdog to all CPUs. This virtual watchdog is managed by software and it is based on a low power timer, the SCU also features a physical watchdog timer that is used to ensure the correct operation of the device. Some of the features implemented by this watchdog service are: - Update of the watchdog timeout - Start/stop of the watchdog - Refresh of the watchdog - Return of the watchdog status such as maximum watchdog timeout that can be set, watchdog timeout interval, and watchdog timeout interval remaining. Since this is usually handled by the OS itself no examples are provided in this guide. Real Time Clock (RTC) - The SCFW is responsible for providing access to the RTC. The features supported by the API are: - Set/get time - Setting alarms Only the partition that owns the SC_R_SYSTEM resource is allowed to set the time, alarms and calibration values for the RTC. All other partitions are able to read the RTC time.  Here is an example on setting the RTC from the M4 side: struct time_date{ uint16_t year; uint8_t month; uint8_t day; uint8_t hour; uint8_t min; uint8_t sec; } rtc_time; sc_err_t sc_status; sc_ipc_t ipc; /* Open IPC channel */ sc_status = sc_ipc_open(&ipc, SC_IPC_AP_CH0); if(sc_status != SC_ERR_NONE) printf("Error opening Inter Processor Channel\n"); /* Initialize RTC */ /* Hard code RTC time to January 5th 2018 at 12:00 hours */ sc_status = sc_timer_set_rtc_time(ipcHandle, 2018, 1, 5, 12, 0, 0); if(sc_status != SC_ERR_NONE) printf("Error initializing RTC. \r\n"); /* Return time */ sc_status = sc_timer_get_rtc_time(ipcHandle, &(rtc_time.year), &(rtc_time.month), &(rtc_time.day), &(rtc_time.hour), &(rtc_time.min), &(rtc_time.sec)); printf("Year: %d, Month: %d, Day: %d, Hour: %d, Minutes: %d, Seconds: %d. \r\n", rtc_time.year, rtc_time.month, rtc_time.day, rtc_time.hour, rtc_time.min, rtc_time.sec);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ https://community.nxp.com/docs/DOC-342654 
查看全文
About this document This document describe the setup detail for Interfacing, Installing, programming (basis) and testing depth cameras with MX6QDL based boards using Ubuntu as rootfs on i.MX6 processors boards. Supported NXP HW boards: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board Depth sensors tested: Microsoft Kinect, ASUS Xtion. Prime Sense Carmine Software:   Gcc, Ubuntu 14.04v,  Openni, Python, ROS. 1. Depth Sensor Depth sensors are 3D vision sensors, mainly used in 3D vision application and motion gaming and robotics. For this paper we are going to use Kinect sensor and Asus Xtion connection to i.MX6 Processor boards and will get 3D images that are converted to finer points called point cloud. a) Microsoft Kinect Kinect mainly has an IR camera, IR projector and RGB camera, the IR and projector generates the 3D point cloud of the surroundings. It also has a mic array and motorized tilt for moving up and down. Kinect reveal that both the video and depth sensor cameras have a 640 x 480-pixel resolution and run at 30 FPS (frames per second). The RGB camera capture 2D color images, whereas the depth camera captures monochrome depth images. Kinect has a depth sensing range from 0.8mts to 3.5 mts b) Asus Xtion: Another alternative to kinect is Asus Xtion Pro.  Is a 3D sensor designed for motion sensing applications, this sensor is only for 3D sensing and it doesn’t have sound sensing. It has an infrared projector and a monochrome CMOS sensor to capture the infrared data. Xtion can be powered from USB itself and can calculate a sense depth from 0.8mts to 3.5 mts from the sensor. c) Prime Sense Carmine: The Prime Sense team (apple bought this company in November 2013) developed the Microsoft Kinect 3D vision, later develop their own 3D vision sensor Carmine. It also works with IR projector, RGB CMOS sensor and a depth CMOS sensor. All sensor are interfaced in System On Chip and is powered trough USB. Carmine capture 640x480 at 30 FPS and can sense from 0.35 mts to 3 mts. Developers can program the device using OpenNI and its wrapper libraries. All these sensors (Kinect, Carmine and Xtion) support the same software, so there is no special need for programming or general usage. Can be interface to i.MX processor using USB 2.0 interface and programmed using OPENNI and OPENCV. 2. Installation on Ubuntu For installation steps of Ubuntu trusty on iMX6 boards in your board, please follow up: https://community.freescale.com/docs/DOC-330147 Install the dependencies: $ sudo apt-get install -y g++ git python libusb-1.0-0-dev libudev-dev freeglut3-dev doxygen graphviz openjdk-6-jdk libxmu-dev libxi-dev Create a devel folder $  sudo mkdir –p devel $ cd devel Get OpenNI and the drivers $ git clone https://github.com/OpenNI/OpenNI.git -b unstable $ git clone git://github.com/ph4m/SensorKinect.git $ git clone https://github.com/PrimeSense/Sensor.git -b unstable Set the compile flags to build for the i.MX $ nano OpenNI/Platform/Linux/CreateRedist/Redist_OpenNi.py From: MAKE_ARGS += ' -j' + calc_jobs_number() To: MAKE_ARGS += ' –j2' Must also change the Arm compiler settings for this distribution $ nano OpenNI/Platform/Linux/Build/Common/Platform.Arm From: CFLAGS += -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp #-mcpu=cortex-a8 To: CFLAGS += -mtune=arm1176jzf-s -mfpu=vfp -mfloat-abi=hard Then run $ cd OpenNI/Platform/Linux/CreateRedist/ $ ./RedistMaker.Arm $ cd ../Redist/OpenNI-Bin-Dev-Linux-Arm-v1.5.x.x $ sudo ./install.sh Also edit the Sensor and SensorKinect makefile CFLAGS parameters $cd ~/devel/ $ nano Sensor/Platform/Linux/Build/Common/Platform.Arm $ nano  SensorKinect/Platform/Linux/Build/Common/Platform.Arm For both files From: CFLAGS += -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp #-mcpu=cortex-a8 To: CFLAGS += -mtune=arm1176jzf-s -mfpu=vfp -mfloat-abi=hard And the Sensor and SensorKinect redistribution scripts $ nano Sensor/Platform/Linux/CreateRedist/RedistMaker $ nano SensorKinect/Platform/Linux/CreateRedist/RedistMaker for both, change: make -j$(calc_jobs_number) -C ../Build to: make –j2 -C ../Build The create the redistributables Sensor (xtion and primesense) and Kinect (sensor Kinect) $ cd Sensor/Platform/Linux/CreateRedist/ $ ./RedistMaker Arm $ cd ~/devel/ $ cd SensorKinect/Platform/Linux/CreateRedist/ $ ./RedistMaker Arm $ cd ~/devel/ Then install PrimeSense and Kinect $ cd Sensor/Platform/Linux/Redist/Sensor-Bin-Linux-Arm-v5.1.x.x $ sudo ./install.sh $ cd ~/devel/SensorKinect/Platform/Linux/Redist/Sensor-Bin-Linux-Arm-v5.1.2.x $ sudo ./install.sh 3. Testing Installation: Connect the sensor power supply, Connect the Kinect to the NXP board USB port. (check with lsusb). For my board: Imx6q@imx6q:~/devel$ lsusb Bus 001 Device 022: ID 045e:02ae Microsoft Corp. Xbox NUI Camera Bus 001 Device 021: ID 045e:02ad Microsoft Corp. Xbox NUI Audio Bus 001 Device 019: ID 045e:02c2 Microsoft Corp. Kinect for Windows NUI Motor Now edit theglobal Kinect settings in Ubuntu $ sudo nano /usr/etc/primesense/GlobalDefaultsKinect.ini and uncomment this line UsbInterface=1 and changed it to 1 instead of 2 UsbInterface=2 $ sudo modprobe -r gspca_kinect And then blacklisting to avoid it to be auto-loaded on boot: $ sudo sh -c 'echo "blacklist gspca_kinect" > /etc/modprobe.d/blacklist-kinect.conf' Then: $ cd ~/devel/OpenNI/Platform/Linux/Bin/Arm-Release $ sudo ./Sample-NiSimpleRead You should get something like: Reading config from: '../../../../Data/SamplesConfig.xml' … Frame 40 Middle point is: 5050. FPS: 30.771788 Frame 41 Middle point is: 5050. FPS: 30.866173 Frame 42 Middle point is: 5050. FPS: 30.850958 Frame 43 Middle point is: 5050. FPS: 30.779032 Frame 44 Middle point is: 5050. FPS: 30.767746 Frame 45 Middle point is: 5050. FPS: 30.800463 Frame 46 Middle point is: 5050. FPS: 30.653118 Frame 47 Middle point is: 5050. FPS: 30.741659 Frame 98 Middle point is: 5050. FPS: 30.339321 LibFreenect: $ cd ~/devel/ $ git clone https://github.com/OpenKinect/libfreenect.git $ cd libfreenect $ mkdir build $ cd build $ cmake .. –L –DBUILD_AUDIO=ON $ make $ sudo make install Connect the kinect sensor power supply, connect the Kinect to the NXP board USB port and test any sample such as: $ sudo freenect-glview Note: If glview gives a shared library error: You need to refresh your ldconfig cache. The easiest way to do this is to create a file usr-local-libs.conf (or whatever name you wish) with the following lines: /usr/local/lib Switch to root account and move it to /etc/ld.so.conf.d/usr-local-libs.conf. Then update the ldconfig cache: $ su root $ mv ~/usr-local-libs.conf /etc/ld.so.conf.d/usr-local-libs.conf $ /sbin/ldconfig –v $ exit References: 1)      https://openkinect.org/ 2)      https://www.asus.com/us/3D-Sensor/Xtion_PRO_LIVE/ 3)      Learning Robotics using phyton by Lentin Joseph. http://www.amazon.com/Learning-Robotics-Python-Lentin-Joseph/dp/1783287535/ref=sr_1_1 4)      Computer Vision on i.MX Processors
查看全文
  1) Remove all "network" parameter from .../ltib-dir/rootfs/rc.d/rc.conf 2) Add the path of rootfs in the /etc/exports file: /home/user/ltib"dir/rootfs/rootfs *(rw,sync,no_root_squash)   then execute :- #exportfs -ra 3) Execute NFS server /etc/init.d/nfs restart  
查看全文
It is often not easy to use company network to flash application, due to network security (proxy, etc...). We will see in this tutorial, how to flash a Linux application in a SD card with ONLY a SD card reader and simple standard Linux commands. SD card Memory Map A Linux application is divided in 3 parts: the bootloader the Linux Kernel the Linux Rootfs We will flash sequentially these 3 parts Flashing U-boot With the SD card Reader, we will flash the yellow part. In the [...]/ltib/rootfs/boot/ folder $ sudo dd if=u-boot.bin of=/dev/sdb bs=512 skip=2 seek=2 && sudo sync Flashing Linux Kernel With the SD card reader, we will flash the green part. Keep in mind that 1MB=1048576B -> Kernel Offset. $ sudo dd if=uImage of=/dev/sdb bs=1048576 seek=1 && sudo sync Configure U-boot variables To launch the Kernel, you need to configure U-boot. Plug the serial cable on the EVK: 115kbps, 8 bits, 1 stop and no parity EVK switches must be configured as below: DS1 DS2 DS3 DS4 DS5 DS5 DS7 DS8 DS9 DS10 Boot from SD/MMC Card 0 0 0 0 0 0 1 1 0 0 Put the SD card in the EVK (bottom slot) and launch the app. In the hyperterminal type:   BBG U-Boot > printenv To print environnement variables Modify the bootcmd: BBG U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc read 0 ${loadaddr} 0x800 0x1800;bootm' "0x1800" is the size of the kernel. Must be bigger than uImage Kernel file (0x1800x512Byte=3MB) If you want to use the WVGA as display screen (kernel need to be configured with CLAA support), for LTIB1007 and after (before it was 'wvga' option): Script for LTIB1007's u-boot on i.MX51 EVK (copy/paste in the hyperterminal): setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bootm' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw  init=/init' setenv bootargs_base' setenv bootargs console=ttymxc0,115200 di1_primary console=tty1' setenv bootcmd 'run bootcmd_mmc' saveenv Script for LTIB1007's u-boot on i.MX53 EVK (copy/paste in the hyperterminal): setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bootm' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw  init=/init' setenv bootargs_base 'setenv bootargs console=ttymxc0,115200 di0_primary console=tty1' setenv bootcmd 'run bootcmd_mmc' saveenv You must have the following printenv: BBG U-Boot > printenv bootdelay=3 baudrate=115200 loadaddr=0x90800000 netdev=eth0 ethprime=FEC0 uboot_addr=0xa0000000 uboot=u-boot.bin kernel=uImage bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serveri p}:${nfsroot},v3,tcp bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; boot m load_uboot=tftpboot ${loadaddr} ${uboot} ethact=FEC0 bootargs=console=ttymxc0,115200 di1_primary root=/dev/mmcblk0p1 rootwait rw init =/init bootcmd_mmc=run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bo otm bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw init=/i nit bootargs_base=setenv bootargs console=ttymxc0,115200 di1_primary bootcmd=run bootcmd_mmc stdin=serial stdout=serial stderr=serial</br> Environment size: 748/131068 bytes BBG U-Boot > Create ext3 partition With the SD card reader, create an ext3 partition. You can use gparted, a graphical partition manager tool. Launch gparted: $ sudo gparted Create a new ext3 partition, with 20MB of offset: Copying Linux To copy rootfs folder generated by LTIB, type in the shell: $ sudo cp -r /[…]/ltib/rootfs/* /media/FreescaleSD/ && sudo sync Test application Put the SD in the slot slot and launch the application. Password is root.
查看全文
Yoctoproject Framework Installing any Needed Package Using Yocto and i.MX Boards Testing Yocto for i.MX6 i.MX53 QSB - Quick Start Board i.MX6 Sabre Lite Board Build the image SDCard Image Yoctoproject Framework Yoctoproject is a framework for creating Linux distributions for embedded devices. Its layering mechanism makes it easy to add Linux to new target devices highly customized for a particular platform; it can include custom start-up scripts, software packages built with a high degree of optimization for a particular architecture, and different user interfaces from full Gnome desktop to a simple a serial console. Yocto has 2 basic layers: board support packages layer and core layer. In the BSP layer is where all the custom software and configuration tweaks for a particular platform are included, while the core layer provides the common software stack to provide from a simple command line interface to Sato desktop interface (Matchbox based and Gnome mobile software stack). A third layer could be added to provide additional user interfaces LXDE, XFCE, and more; YP is quite flexible&emdash;one of it major strengths. Installing any Needed Package Go to Yocto Project Quick Start and double check that you have all the necessary packages installed for your machine. For example, if building machine was an Ubuntu machine: $ sudo apt-get install gawk wget git-core diffstat unzip texinfo  build-essential chrpath libsdl1.2-dev xterm curl Using Yocto and i.MX Boards Please, go to project's README file in order to see the recommended instructions to download the source code. Testing Yocto for i.MX6 How to test Yocto for i.MX 6 i.MX53 QSB - Quick Start Board Edit conf/local.conf user config file and set imx53 Quick start board machine and enable parallel build features. MACHINE ?= "imx53qsb" BB_NUMBER_THREADS = "4" PARALLEL_MAKE = "-j 4" i.MX6 Sabre Lite Board Edit conf/local.conf user config file and set i.MX6 Sabrelite board machine and enable parallel build features MACHINE ?= "imx6qsabrelite" BB_NUMBER_THREADS = "4" PARALLEL_MAKE = "-j 4" if you've been facing problems to get yocto's images working on your i.MX Sabre Lite board, please take a look on this comment Re: The kernel sometins hang  in L3.0.35_4.0.0_130424 release Build the image some example of available image: image name description core-image-minimal A small image just capable of allowing a device to boot. core-image-base A console-only image that fully supports the target device hardware. core-image-sato Image with sato, a mobile environment and visual style for mobile devices.  The image supports X11 with a Sato theme, Pimlico applications and contains terminal, editor and file manager. fsl-image-test Builds contents core-image-base plus Freescale test applications and multimedia components. fsl-image-gui Builds contents of core-image-sato with Freescale test applications and multimedia with hardware accelerated X11 To build the image: $ bitbake <image_name> Build using Dash instead can bring some problems. You can check what your system uses typing: "ls -l /bin/sh". On Ubuntu you can change it using "dpkg-reconfigure bash". Some Ubuntu releases you must use "dpkg-reconfigure dash" and choose Bash Built images are located in cd tmp/deploy/images SDCard Image sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdb i.MX Yocto Project: Frequently Asked Questions
查看全文
Ubuntu distro uses dash instead of bash as shell, then change it to bash: # cd /bin # sudo rm sh # sudo ln -s bash sh Install all necessary packages by typing: sudo apt-get install patch g++ rpm zlib1g-dev m4 bison libncurses5-dev libglib2.0-dev gettext \ build-essential tcl intltool libxml2-dev liborbit2-dev libx11-dev ccache flex uuid-dev liblzo2-dev If under Ubuntu 64bit, install ia32-libs package: sudo apt-get install ia32-libs If you will install Xorg in your ltib, you will need to install this package: sudo apt-get install x11proto-core-dev If you will install gtk+ in your ltib, you will need to install the following packages: sudo apt-get install libdbus-glib-1-dev libgtk2.0-dev libdbus-glib-1-dev Configure visudo file, as root using the command "/usr/sbin/visudo", and add the following line in the User privilege section: username ALL = NOPASSWD: /usr/bin/rpm, /opt/freescale/ltib/usr/bin/rpm Where username is your user name, the name you use to do logon in your system. Classic Error messages and solutions under Ubuntu Can't exec "mconf": No such file or directory at /home/tic/ltib/bin/Ltibutils.pm line 972. exec: mconf /home/tic/ltib/config/main.lkc: No such file or directory at /home/tic/ltib/bin/Ltibutils.pm line 972. traceback:   Ltibutils::system_nb:972   main::get_plat_dir:2947     main:548 Started: Tue Feb 16 18:01:38 2010 Ended:  Tue Feb 16 18:59:26 2010 Elapsed: 3468 seconds Build Failed Solution: edit the ltib script line 925:                   # install the new package           $cmd  = "$cf->{sudo} $cf->{rpm} ";           $cmd .= "--root $cf->{rpmroot} ";           $cmd .= "--dbpath $cf->{rpmdb} ";           $cmd .= "--prefix $cf->{rpmipfx} " if $cf->{rpmipfx};           $cmd .= "--ignorearch -ivh ";           $cmd .= "--force "  unless $cf->{conflicts} || $cf->{hostinst};           $cmd .= "--replacepkgs --replacefiles " if $cf->{hostinst};           $cmd .= "--nodeps " if $cf->{nodeps};           $cmd .= "--excludedocs "; +        $cmd .= "--force-debian " if $rpm =~ m/rpm-fs/ && `uname -a` =~ m/ubuntu/i;           $cmd .= "--define '_tmppath $cf->{tmppath}' ";           $cmd .= "$rpm"; error: cannot open Name index using db3 - No such file or directory (2) error: cannot open Name index using db3 - No such file or directory (2) sudo rpm --root / --dbpath /tmp/rpm-tic/rpmdb -e --allmatches --nodeps --define '_tmppath /home/tic/ltib/tmp' rpm-fs 2>/dev/null sudo rpm --root / --dbpath /tmp/rpm-tic/rpmdb --ignorearch -ivh --force --nodeps --excludedocs --define '_tmppath /home/tic/ltib/tmp'  /tmp/rpm-tic/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm rpm: please use alien to install rpm packages on Debian, if you are really sure use --force-debian switch. See README.Debian for more details. sudo /opt/freescale/ltib/usr/bin/rpm --root / --dbpath /opt/freescale/ltib/var/lib/rpm -Uv --justdb --notriggers --noscripts --nodeps  /tmp/rpm-tic/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm sudo: /opt/freescale/ltib/usr/bin/rpm: command not found mkdir: cannot create directory `/opt/freescale': Permission denied Cannot create the download directory:   /opt/freescale/pkgs Either change to a global directory you have write permissions to, or create it as root.  Please set the permissions to 777 traceback:   main::check_dirs:2469   main::host_checks:1426     main:542 Started: Wed Nov 25 01:56:53 2009 Ended:  Wed Nov 25 02:07:42 2009 Elapsed: 649 seconds Build Failed solution : sudo chmod 777 /opt make[1]: Entering directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8' Making all in tools make[2]: Entering directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8/tools' make[2]: *** No rule to make target `all'.  Stop. make[2]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8/tools' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8' make: *** [all] Error 2 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.U8vEdX (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.U8vEdX (%build) Build time for texinfo: 55 seconds Failed building texinfo Died at ./ltib line 1380. traceback:   main::build_host_rpms:1380   main::host_checks:1435     main:542 Started: Wed Nov 25 20:10:43 2009 Ended:  Wed Nov 25 20:31:42 2009 Elapsed: 1259 seconds These packages failed to build: texinfo Build Failed solution : install ccache package in host + cd /opt/freescale/ltib/usr/src/rpm/BUILD + cd lkc-1.4 + make -j1 conf mconf gcc -O0 -Wall -g -fPIC -c conf.c -o conf.o bison -l -b zconf -p zconf zconf.y flex -L -Pzconf zconf.l make: flex: Command not found make: *** [lex.zconf.c] Error 127 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.010CjL (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.010CjL (%build) Build time for lkc: 2 seconds Failed building lkc Died at ./ltib line 1380. traceback:   main::build_host_rpms:1380   main::host_checks:1435     main:542 Started: Thu Nov 26 00:33:46 2009 Ended:  Thu Nov 26 01:19:39 2009 Elapsed: 2753 seconds These packages failed to build: lkc Build Failed solution : install flex package in host Making all in po make[2]: Entering directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf/po' mv: cannot stat `t-ja.gmo': No such file or directory make[2]: *** [ja.gmo] Error 1 make[2]: *** Waiting for unfinished jobs.... mv: cannot stat `t-ru.gmo': No such file or directory make[2]: *** [ru.gmo] Error 1 make[2]: Leaving directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf/po' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf' make: *** [all-recursive] Error 1 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.93730 (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.93730 (%build) Build time for alsa-utils: 84 seconds Failed building alsa-utils f_buildrpms() returned an error, exiting traceback:   main:560 Started: Sat Nov 28 07:39:40 2009 Ended:  Sat Nov 28 08:17:18 2009 Elapsed: 2258 seconds These packages failed to build: alsa-utils Build Failed Exiting on error or interrupt solution : install package gettext and ja-trans checking for glib-genmarshal... no configure: error: Could not find a glib-genmarshal in your PATH error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.13030 (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.13030 (%build) Build time for glib2: 107 seconds Failed building glib2 f_buildrpms() returned an error, exiting traceback:   main:560 Started: Sat Dec  5 03:19:36 2009 Ended:  Sat Dec  5 03:29:46 2009 Elapsed: 610 seconds These packages failed to build: glib2 Build Failed Exiting on error or interrupt solution : install the package libglib2.0-dev
查看全文