i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
The purpose of this document is to provide supportive information for selection of suitable LPDDR4, DDR4 and DDR3L devices that are supported by i.MX 8M family of processors to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.  It is strongly recommended to consult with NXP and the memory vendor the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements. Please note that some of the LPDDR4 devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low speed operation is planned in the use case, please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs available on NXP.com Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.  LPDDR4 - maximum supported densities Please note that the SoCs only support memory devices that support either the LPDDR4 mode or support both LPDDR4 and LPDDR4X modes. Memory devices that support only the LPDDR4X mode are not supported. SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8M Quad 32-bit 32Gb/4GB dual rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 4 i.MX 8M Mini  32-bit 64Gb/8GB dual rank, dual-channel  device with 17-row addresses (R0-R16) 1, 2 i.MX 8M Nano  16-bit 32Gb/4GB dual rank, single-channel  device with 17-row addresses (R0-R16) 1, 2, 3, 12 i.MX 8M Plus  32-bit 64Gb/8GB dual rank, dual-channel  device with 17-row addresses (R0-R16)  1, 2   LPDDR4 - list of validated memories Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required. SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8M Quad  24Gb/3GB    Micron MT53B768M32D4NQ-062 WT:B  15 32Gb/4GB Micron MT53D1024M32D4DT-046 AAT:D  14 4Gb/512MB ISSI IS43LQ16256B-062BLI  5, 14 8Gb/1GB ISSI IS43LQ32256B-062BLI  5, 14 i.MX 8M Mini 16Gb/2GB Micron MT53D512M32D2DS-053 WT:D  15 16Gb/2GB    ESMT M56Z16G32512A-SMBIG 5, 14 32Gb/4GB Micron MT53E1G32D2FW-046 WT:A  5, 14 64Gb/8GB Micron MT53E2G32D4DT-046 AIT:A  5, 14 64Gb/8GB Micron MT53E2G32D4DE-046 AUT:C 5, 14 32Gb/4GB Intelligent Memory IMBG32L4KBB 5,14 32Gb/4GB Kingston B3221PM3BDGUI -U 5 16Gb/2GB Kingston D1621PM4CDGVIW-U related PNs also covered by the test: D1621PM4CDGUI-U D1621PM4CDGUIW-U D1621PM4CDGVI-U 5 i.MX 8M Nano  16Gb / 2GB  Kingston C1612PC2WDGTKR-U  15 16Gb / 2GB  Kingston  D1611PM3BDGUI-U 5,14 32Gb / 4GB Micron MT53E2G32D4DT-046 AIT:A  5, 13, 15 16Gb / 2GB Intelligent Memory  IMAG16L4KBB 5,14 4Gb / 512MB Nanya NT6AN256M16AV-J2 5,14 4Gb / 512MB  Winbond W66CP6RBQAHJ 5,14 8Gb / 1GB ISSI IS43LQ16512A-053BLI 5,14 8Gb / 1GB  Micron MT53D512M32D2DS-053 WT:D 13, 15   i.MX 8M Plus       48Gb/6GB  Micron MT53E1536M32D4DT-046 WT:A  15 64Gb/8GB  Micron MT53E2G32D4DE-046 AUT:C  5, 14 32Gb/4GB Samsung K4FBE3D4HB-KHCL  5, 14 32Gb/4GB Kingston B3221PM3BDGVIW-U 5, 14 64Gb/8GB Kingston Q6422PM3BDGVK-U  5, 14 8Gb/1GB Winbond W66DP2RQQAHJ  5, 14 32Gb/4GB ISSI IS46LQ32K01S2A-046BLA2 5, 14 16Gb/2GB ISSI IS46LQ32512A-046BLA3 5 32Gb/4GB ISSI IS43LQ32K01S2A-046BLI 5, 14 32Gb/4GB IM IMBG32LK4BBG-046I 5, 14 32Gb/4GB Nanya NT6AN1024F32AV-J2 5, 14 32Gb/4GB Nanya NT6AT1024T32AV-J1 5   LPDDR4 - list of incompatible devices Given the limitations mentioned in this document, the following memory devices were identified as incompatible with the particular SoCs as detailed in the following table:   Memory Vendor Memory Part# Density Incompatible SoCs Incompatibility reason Samsung K4FHE3S4HA-KU(H/F)CL 24Gb/3Gb i.MX 8M Quad  The memory device requires 17th row address bit to function. Samsung K4UHE3S4AA-KU(H/F)CL K4UJE3D4AA-KU(H/F)CL 24Gb/3Gb 48Gb/6GB i.MX 8M Quad i.MX 8M Mini i.MX 8M Nano i.MX 8M Plus The memory device only supports the LPDDR4X mode. Samsung K4FCE3Q4HB-KU(H/F)CL K4UCE3Q4AB-KU(H/F)CL 64Gb/8GB i.MX 8M Quad i.MX 8M Mini i.MX 8M Nano i.MX 8M Plus A byte mode memory device. The memory device only supports the LPDDR4X mode.    DDR4 - maximum supported densities SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8M Quad  32-bit 32Gb/4GB x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses 1, 6 i.MX 8M Mini  32-bit 64Gb/8GB x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses 1, 7 i.MX 8M Nano  16-bit 64Gb/8GB x8, 16Gb device with 2 bank group addresses, 17-row addresses and 10 column addresses 1, 8 i.MX 8M Plus  32-bit 64Gb/8GB x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses 1, 7   DDR4 - list of validated memories Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required.   SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8M Quad 32Gb/4GB Micron 4x MT40A512M16JY-083EAAT  15 i.MX 8M Mini  16Gb/2GB Micron 2x MT40A512M16LY-075:E  15 i.MX 8M Nano 16Gb/2GB Micron 1x MT40A1G16RC-062E:B  15 8Gb/1GB Rayson 1x RS512M16Z2DD-62DT 14 8Gb/1GB UniIC SCB12Q8G160BF-06SI 14 i.MX 8M Plus 64Gb/8GB Micron 4x MT40A1G16RC-062E:B  15 16Gb/2GB Nanya NT5AD512M16C4-JRI  14   DDR3L - maximum supported densities SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8M Quad  32-bit 32Gb/4GB x16, 8Gb device with 16-row addresses and 10 column addresses 1, 9 i.MX 8M Mini  32-bit 64Gb/8GB x8, 8Gb device with 16-row addresses and 11 column addresses 1, 10 i.MX 8M Nano  16-bit 32Gb/4GB x8, 8Gb device with 16-row addresses and 11 column addresses 1, 11 i.MX 8M Plus  i.MX 8M Plus does not support DDR3L   DDR3L - list of validated memories Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required. SoC Density Vendor Validated Memory Part#  Notes i.MX 8M Quad  16Gb/2GB Micron 4x MT41K256M16TW-107 AAT  14 i.MX 8M Mini  16Gb/2GB Micron 4x MT41K256M16TW-107 AAT  14              i.MX 8M Nano 8Gb/1GB Micron MT41K512M16VRN-107  15   Note 1: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, and on the JEDEC standards JESD209-4/JESD209-4A (LPDDR4), JESD279-4/JESD279-4A (DDR4), and JESD79-3E/JESD79-3F/JESD79-3-1A (DDR3/DDR3L). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The memory vendors often do not offer so many variants of single-channel memory devices. As an alternative, a dual-channel device with only one channel connected may be used. For example: A dual-rank, single-channel device with 16-row address bits has a density of 16Gb. If such a device is not available at the chosen supplier, a dual-rank, dual-channel device with 16-row address bits can be used instead. This device has a density of 32 Gb however since only one channel can be connected to the SoC, only half of the density is available (16 Gb). Usage of more than one discrete memory chips to overcome market constraints is not supported since only point-to-point connections are assumed for LPDDR4. Note 4: Devices with 17-row addresses (R0-R16) are not supported by the DDR Controller Note 5: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 6: The density can be achieved by connecting 2 single-rank discrete devices with one 16Gb die each. Since the SoC supports x8 devices and also has connectivity for a second rank, usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 32Gb/4GB of address space dedicated for the DDR. Two x16 16Gb devices giving 32Gb/4GB in total is, therefore, the optimal choice that balances the maximum density aspects, the signal integrity aspects (only two discrete devices used), and bandwidth aspects (full data bus width used). Note 7: The density can be achieved by connecting 4 single rank discrete devices with one 16Gb die each, 2 devices connected to each chip select. Since the SoC supports x8 devices, the usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 64Gb/8GB of address space dedicated for the DDR. Four x16 16Gb devices giving 64Gb/8GB in total is the optimal choice that balances the maximum density aspects, the signal integrity aspects (only four discrete devices used), and the bandwidth aspects (full data bus width used). Note 8: The density can be achieved by connecting 4 single rank discrete devices with one 16Gb die each, 2 devices connected to each chip select.  Note 9: The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select, or by connecting 2 dual rank discrete devices with two 8Gb dies each. Since the SoC supports x8 devices, the usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 32Gb/4GB of address space dedicated for the DDR. Four x16 8Gb devices giving 32Gb/4GB in total is, therefore, the optimal choice that balances the maximum density aspects, the signal integrity aspects (four discrete devices used), and bandwidth aspects (full data bus width used). Note 10: The density can be achieved by connecting 8 single rank discrete devices with one 8Gb die each, 4 devices connected to each chip select or by connecting 4 dual rank discrete devices with two 8Gb dies each. Note that the first option significantly exceeds the number of devices used on the validation board (4 discrete devices) therefore, it is not guaranteed that the i.MX would be able to drive the signals with margin to the required voltage levels due to increased loading on the traces. A significant effort would be required in terms of PCB layout and signal integrity analysis. Practically, it is not recommended to use more than 4 discrete DDR3L devices. This corresponds to the maximum density of 32Gb/4GB in the case of the single rank devices containing one 8Gb die or 64Gb/8GB in case of the dual-rank devices, each containing two 8Gb dies. Note 11: The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select or by connecting 2 dual rank discrete devices with two 8Gb dies each. Note 12: For single-channel (x16) memory devices, the current maximum available density in the market is 16Gb/2GB (Q1 2022). Note 13: Only one channel of the device (and hence, half of its density) was utilized due to the reduced data bus width (x16) of the SoC. Note 14: Part is active. Reviewed Jan 2026 Note 15: Part will either EoL or is not recommended for new designs by the respective vendor.   Additional Links https://community.nxp.com/t5/iMX-and-Vybrid-Support/i-MX-8-8X-8XL-maximum-supported-LPDDR4-and-DDR3L-densities/ta-p/1152715           
View full article
This page serves as a hub to gather the links to all the currently available ISP supported camera lists for the i.MX Applications processors.  Camera Compatibility Guides Processor/Family Link to Guide i.MX 8M Plus i.MX 8M Plus ISP Camera Compatibility Guide i.MX 95 i.MX 95 ISP Camera Compatibility Guide   Additional Resources i.MX Camera Software Pack AN AN14376: i.MX Camera Software Pack | NXP Semiconductors
View full article
Background: This article discusses the reboot mechanism on the i.MX8MP and i.MX93 platforms. It aims to help customers understand how the reboot command works. We will discuss two different kernel versions separately.   1. Linux version : LF_6.12.34_2.1.0 The executable file for the reboot command is as follows: When the ”reboot“ command is executed, the system enters the ”do_kernel_restart()“ function and executes the reboot mechanism by determining the priority of the registered functions. Since the ”reboot.c“ file does not print out the registered functions, a print function is added to the file to identify the function that is ultimately executed.   The print output is as follows: As shown in the figure above, in version 5.12, the reboot is performed via a reset executed by psci. Continuing to trace the ”psci_sys_reset()“ function, we can see that the system sends the function ID via the PSCI interface to initiate an SMC call, instructing the underlying firmware (ATF/EL3) to perform a system reboot (typically a cold reset). The value of PSCI_0_2_FN_SYSTEM_RESET is 0x80000009   According to the Arm Power State Coordination Interface Platform Design Document, this ID represents a cold reset of the system.     2. Linux version : LF_6.18.2_1.0.0 Use the same debugging method to examine the reboot mechanism in version 6.18 As shown in the output below, in version 6.18, the system reset is triggered by the `sys_off_notify()` function. The final execution function is pca9450_i2c_restart_handler()   By examining the `pca9450_i2c_restart_handler()` function, we can see that the system writes a `SW_RST_COMMAND` value to the PMIC via I²C, where `SW_RST_COMMAND = 0x14`. According to the PMIC data sheet, 10b = Cold Reset; all voltage regulators are reset except LDO1/LDO2   Summary: Regardless of the kernel version, the `reboot` command triggers a system cold reset. The triggering mechanism has been updated in versions 6.18 and later.
View full article
As part of this brief blog, we are enabling Asymmetric Multiprocessing (AMP) boot support for the Cortex-M7 core on the i.MX8MP SoC device model in Qemu. The M7 firmware can be loaded and started from Linux running on the Cortex-A53 cores via the remoteproc framework.
View full article
   Memory Compatibility Guides   Processor/Family Link to Guide i.MX 8/8X/8XLite DDR3L & LPDDR4 i.MX 8M Quad/8M Mini/8M Nano/8M Plus DDR3L, DDR4, LPDDR4 i.MX 8ULP  LPDDR3, LPDDR4 & LPDDR4x i.MX 91 LPDDR4 - New i.MX 93 LPDDR4/LPDDR4x i.MX 95 LPDDR5/LPDDR4x - New Ara240 - DNPU LPDDR4 - New Other Processor Families Please contact NXP Support or Sales   Additional Resources i.MX Memory Fact Sheet DDR memory selection & enablement for i.MX platforms Smarter World Blog Building Resilient Embedded Systems: NXP’s Approach to DDR Memory Selection and Support DDR Configuration Tools DDR Configuration tool for i.MX  Developer Resources i.MX Developer Resources SW & Tools
View full article
The purpose of this page is to provide supportive information for the selection of suitable camera modules that are supported by the i.MX 8M Plus (i.MX8MP). The guide is attached in this page. This helps customers evaluate project feasibility and integration aspects when considering i.MX 8MP SoCs for their products. It is strongly recommended to consult with NXP and the camera module vendor before finalizing the choice of the camera part number to ensure compatibility, availability, longevity, and pricing requirements. NXP Supported Sensors: Sensor Vendor Image Sensor Max Resolution Camera Module OmniVision OS08A20 8MP IMX-OS08A20 EXPI-OS08A20 OmniVision OV2775 2MP   Sony IMX219 8MP   Sony IMX477 12.3MP   Onsemi AR0144 1MP AR0144 Onsemi AR1335 13MP     Partner Enabled Sensors:   Partner Sensor Vendor Image Sensor Max Resolution ISP Tuning Camera Module Location FRAMOS Sony IMX415 8MP ✔   Munich, Germany/ Canada/USA Sony IMX662 2MP FSM:GO Sony IMX678 8MP Sony IMX900 3.2MP Sony IMX676 12MP Innowave Onsemi AR1335 13MP ✔   Austin, Texas, USA/Israel Sony IMX258 13MP Camera Modules Sony IMX219 8MP OmniVision OV5645 5MP   OmniVision OV2710 2MP   Basler Onsemi AR0821 8MP   Basler   Onsemi AR0521 5MP   Onsemi Onsemi AR0830 8MP   Image Sensors, Module available through Future Electronics   Onsemi AR0544 5MP Onsemi AR0821 8MP Onsemi AR0822 8MP Onsemi AR0145 1MP Onsemi AR0235 2MP Onsemi AR1335 13MP PHYTEC Onsemi AR0144 1MP     Germany/ China/India/ USA Onsemi AR0234 2.3MP   Onsemi AR0521 5MP   E-consystems Sony IMX662 2.4MP     Riverside, CA, USA/India Sony IMX900 3.2MP   Onsemi AR0234 2.3MP   CIS Corporation Sony IMX715 12MP ✔   Japan Sony IMX570 0.32MP   Onsemi AR0234CS 2MP   Sony Sony IMX500 12MP     Japan HINO Engg Sony IMX415 8MP ✔   Japan Sony IMX662 2MP   Leopard Imaging Sony IMX500 12MP ✔   Fremont, CA, USA/China   Note: CIS Corporation and HINO Engg currently only support customers in Japan market.
View full article
SW : uboot-imx lf_v2025.04 HW : i.MX 8MP EVK board, Oscilloscope   1. Introduction This guide explains the concept of DDR clock spread spectrum on the i.MX 8MP EVK platform. Note that the official NXP BSP does not enable this feature by default. Additionally, this guide provides an example code patch and verification steps to enable the LPDDR4 clock spread spectrum feature on the NXP i.MX 8MP EVK board.   2. What is Spread Spectrum? Spread Spectrum (SS) is a technique used to reduce electromagnetic interference (EMI) by slightly modulating the clock frequency around its nominal value. Instead of operating at a fixed frequency (e.g., 800 MHz), the clock signal is varied within a small range (e.g., ±0.5%). This modulation spreads the energy of the clock signal over a wider frequency band, reducing the peak energy at any single frequency. In other words, SS does not change the average clock speed significantly, but it helps to distribute the spectral energy, making the system less likely to violate EMI regulations.   3. Why Enable Spread Spectrum on DRAM Clock? Enabling Spread Spectrum on the DRAM clock helps reduce electromagnetic interference (EMI) by slightly modulating the clock frequency, lowering peak emissions and making it easier to meet regulatory standards such as FCC and CE. This approach improves system reliability by minimizing interference with other components, offers a cost-effective alternative to hardware changes like shielding or PCB redesign, and is widely adopted in high-speed interfaces such as DDR, PCIe, and SATA to ensure compliance without additional hardware complexity.   4. Related registers CCM_ANALOG_DRAM_PLL_SSCG_CTRL                             Note :  PLL_MFREQ_CTL[19 : 12] : Value of modulation frequency control The larger the mfr value, the lower the MF value (the slower the modulation); the smaller the mfr value, the higher the MF value. MF : The frequency of spread spectrum modulation is the speed at which the triangular/sawtooth modulated wave travels back and forth once per second, measured in Hz (commonly in the tens of kHz range). The speed of the spread spectrum "jitter" is determined. Usually, around 20–50 kHz is chosen to make the energy "swipe evenly" within the bandwidth of the EMI test receiver, thereby reducing the peak radiation at a certain frequency point. PLL_MRAT_CTL[9 : 4] : Value of modulation rate control The larger mrr is, the larger MR is (the wider the range); similarly, MR is also directly proportional to mfr and inversely proportional to m. MR : Peak-to-peak percentage of spread spectrum (the percentage of the total range of the clock frequency swinging around the center value). For example, MR = 0.5% means that the frequency swings around the center value by a total of 0.5% (if it is center-spread spectrum, it is usually ±0.25%).The MR determines the depth (width) of the spread spectrum. The larger the MR, the wider the spectral energy distribution and the lower the peak value, but it comes at the cost of jitter/timing margin (timing should be carefully selected for DDR, SerDes, etc.). 5. About Uboot code patch. Please refer the attachment patch file. At high DRAM frequency, Enable SS may cause not stable problem. So, in this case, I will choose 2400Mbps data clock run the test. Firstly, we should make sure that our code include the 2400Mbps PLL setting. DRAM data speed is 2400Mbps, the DRAM clock is 1200MHz. So the DDRC PLL clock should set up with 600MHz. For example, refer the below code. static struct imx_int_pll_rate_table imx8mm_fracpll_tbl[] = {     PLL_1443X_RATE(1000000000U, 250, 3, 1, 0),     PLL_1443X_RATE(933000000U, 311, 4, 1, 0),     PLL_1443X_RATE(900000000U, 300, 2, 2, 0),     PLL_1443X_RATE(800000000U, 200, 3, 1, 0),     PLL_1443X_RATE(750000000U, 250, 2, 2, 0),     PLL_1443X_RATE(650000000U, 325, 3, 2, 0),     PLL_1443X_RATE(600000000U, 300, 3, 2, 0), // 2400Mbps     PLL_1443X_RATE(594000000U, 99, 1, 2, 0),     PLL_1443X_RATE(400000000U, 400, 3, 3, 0),     PLL_1443X_RATE(266000000U, 266, 3, 3, 0),     PLL_1443X_RATE(167000000U, 334, 3, 4, 0),     PLL_1443X_RATE(100000000U, 200, 3, 4, 0), }; PLL output calculator formula is : PLL_out = 24MHz*mdiv/pdiv/(2^sdiv) So, 2400MHz * 300 / 3 / 2^2 = 600MHz   6. Test result Non Enable SS Enable SS with 1% MR and Down spread Enable SS with 2% MR and Down spread Enable SS with 2% MR and Center spread  
View full article
When working with an evaluation kit you will be provided with a System Controller Firmware (SCFW) binary included in your BSP. This scfw binary has been tailored for that specific board and you might need to modify some board dependencies to fit your specific hardware. This document aims to provide an overview on the SCFW porting process, for detailed information please refer to the System Controller Porting guide (sc_fw_port.pdf).   Setting up the system The SCFW is built on a Linux host. The steps to set-up your system are the following: Download the GNU ARM Embedded Toolchain: 6-2017-q2-update June 28, 2017 from the ARM website: Select a directory to untar the file unto, for instance: mkdir ~/gcc_toolchain cp ~/Downloads/gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 ~/gcc_toolchain/ cd ~/gcc_toolchain/ tar xvjf gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Set TOOLS environment variable to the directory containing the tool chain, "~/gcc_toolchain" on the example above, .bash_profile can also be modified to export this environment variable: export TOOLS=~/gcc_toolchain/ srec_cat is also necessary for the build, this is usually contained in the srecord package, on ubuntu you can do: sudo apt-get update sudo apt-get install srecord Now you can change to the porting kit directory (e.g. scfw_export_mx8qm) and build the scfw. System Controller Firmware Porting kit  The SCFW porting kit contains source files and object files that will allow you to modify the SCFW to work with your board. You can get the latest System Controller Firmware Porting kit from the i.MX Software and development webpage: Once you obtain the porting kit untar it: tar xvzf imx-scfw-porting-kit-1.1.tar.gz‍ You will see the following file structure: The porting kit is contained under packages, the README contains the instructions to extract the porting kit, basically: cd packages/ chmod a+x imx-scfw-porting-kit-1.1.bin ./imx-scfw-porting-kit-1.1.bin‍‍‍ You will be prompted to accept an End User License Agreement: Once you accept the agreement the porting kit will be extracted in a new folder, the folder structure is as follows: All documentation regarding SCFW is under doc/pdf or in html format if preferred, it is recommended to go over sc_fw_port.pdf. The porting kits for different SoC variants (QM A0, QM B0 and QXP B0) are under src packaged as tar.gz, all other files are SCFW libraries for different software packages, such as Linux, QNX, FreeRTOS, U-boot, ARM Trusted Firmware, etc...   If you will be working with several SoC variants (working with both QXP and QM) it is recommended to extract all porting kits into a single directory, that way you will be able to build for any variant from this directory, the command to do this is: cd imx-scfw-porting-kit-1.1/ cd src/ find scfw_export_mx8*.gz -exec tar --strip-components 1 --one-top-level=scfw_export_mx8 -xzvf {} \;‍‍‍ A scfw_export_mx8 folder will be created, from here you will be able to build SCFW for any supported variant. Or you can just extract the package for the variant you are interested on and use that. cd scfw_export_mx8/‍ All the build folders contain the results of building the SCFW and platform is where the source of the SCFW is stored.   All the code that is specific to a board configuration is under "platform/board/mx8<derivative>_<board_name>" where derivative is the i.MX8 silicon family such as QXP or QM, and board name is the name of the board the SCFW package is for. The first step in porting the SCFW to your board is to create a folder for your i.MX8 derivative and board, you can take one of the available board examples and rename the folder, that will provide you a project to get started with, for instance: cp -r platform/board/mx8qm_val/ platform/board/mx8qm_myBoard/‍‍‍‍‍‍‍‍‍‍ The board in this example will be called "myBoard" and it is for an i.MX8QM B0 device. To build a SCFW for this board simply call: make qm R=B0 B=myBoard‍‍‍‍‍‍‍‍‍‍‍‍ If the target is an i.MX8QXP simply take a board based on this device and change the call to "make qx". Additional information such as build options and in detailed boot information can be found in the SCFW porting guide (sc_fw_port.pdf), chapter 2 of this document is a great introduction to the porting process.   Overview and useful information Configuring the PMIC overview and board.c common modifications The main file that needs to be altered (if not the only) is the "board.c" file, it is located at "platform/board/mx8X_board/". The board.c file contains most of the board related information such as SCU UART ports, PMIC initialization routines, PMIC temperature alarms settings and you can also modify it to configure LDOs voltages and communicate with the PMIC in general. All functions in the board.c file are executed by the SCU itself and this gives you access to the I2C interface that is used to communicate with the PMIC. SoC resources that are powered by an external supply (PMIC LDO for instace) such as AP cores and GPUs are powered off/on by board_set_power_mode, the mapping of the resource to an specific PMIC supply happens in board_get_pmic_info, for instance in our i.MX8QM validation board using the A53 subsystem is powered by SW2 of the third PMIC (PMIC_2_ADDR addresses start at PMIC_0) on the PF100 PMIC card and by SW5 of the first PMIC (PMIC_0_ADDR) on the PF8100 PMIC card. case SC_SUBSYS_A53: pmic_init(); if (pmic_card == PF100) { pmic_id[0] = PMIC_2_ADDR; pmic_reg[0] = SW2; *num_regs = 1; } else {/* PF8100_dual Card */ pmic_id[0] = PMIC_0_ADDR; pmic_reg[0] = PF8100_SW5; *num_regs = 1; } break; ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The voltages of SoC resources that are powered by an external supply (AP cores, GPUs, etc...) are managed by board_set_voltage in the board.c file. The mapping of resource to power supply occurs in board_get_pmic_info as in the example above. Eight "board resources" (SC_R_BOARD_R0, ... SC_R_BOARD_R7) are available, these resources allow you to define components in your board that the SCU can manage, for instance a sensor on your board powered by one of the PMIC LDOs can be mapped to a board resource and the board.c file can be modified to power on/off the sensor as well as modifying its voltage. Modifying the voltage on a board resource can be either be done by modifying the voltage at board_trans_resource_power (see below) or if the voltage needs to change at run time the function board_set_control can be modified to change the voltage whenever a miscellaneous call (more details in the Miscellaneous Service 101) is made on that resource. For instance to change the voltage on SC_R_BOARD_R7 you would have the following case to board_set_control: case SC_R_BOARD_R7: if (ctrl == SC_C_VOLTAGE) { /* Example only PMIC_X_ADDR and PMIC_SUPPLY need to match an actual device */ pmic_interface.pmic_set_voltage(PMIC_X_ADDR, PMIC_SUPPLY, val, step); } else return SC_ERR_PARM; break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The case above will be executed by the SCU every time the application calls the function below: sc_misc_set_control( ipc, SC_R_BOARD_R7, SC_C_VOLTAGE, voltage_val);‍‍‍‍‍‍‍‍ Powering on/off a board resource happens at board_trans_resource_power in the board.c file. For instance in NXP's validation board the PTN5150 on the board is managed through a board resource 0, and the power on/off is managed as follows: case BRD_R_BOARD_R0 : /* PTN5150 (use SC_R_BOARD_R0) */ if (pmic_ver.device_id == PF100_DEV_ID) { if (to_mode > SC_PM_PW_MODE_OFF) { pmic_interface.pmic_set_voltage(PMIC_2_ADDR, VGEN6, 3300, SW_RUN_MODE); pmic_interface.pmic_set_mode(PMIC_2_ADDR, VGEN6, VGEN_MODE_ON); } else { pmic_interface.pmic_set_mode(PMIC_2_ADDR, VGEN6, VGEN_MODE_OFF); } } else {/* PF8100_dual Card */ if (to_mode > SC_PM_PW_MODE_OFF) { pmic_interface.pmic_set_voltage(PMIC_1_ADDR, PF8100_LDO1, 3300, REG_RUN_MODE); pmic_interface.pmic_set_mode(PMIC_1_ADDR, PF8100_LDO1, RUN_EN_STBY_EN); } else { pmic_interface.pmic_set_mode(PMIC_1_ADDR, PF8100_LDO1, RUN_OFF_STBY_OFF); } } break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Whenever the function below is called from the application side the SCU will execute the code above: sc_pm_set_resource_power_mode(ipc, SC_R_BOARD_R0, SC_PM_PW_MODE_ON/OFF);‍‍‍‍‍‍‍‍ board_config_sc is used to mark resources that the SCU needs, such as the I2C module and pads used to communicate with the PMIC, any resource needed by the board.c functions to work should be marked in this function as not movable, for instance to keep the SCU I2C module the following line is added: rm_set_resource_movable(pt_sc, SC_R_SC_I2C, SC_R_SC_I2C, false);‍‍‍‍‍‍‍‍‍ The following pads are part of the SCU and the application will not be able to access them: - SC_P_SCU_PMIC_MEMC_ON - SC_P_SCU_WDOG_OUT - SC_P_PMIC_EARLY_WARNING - SC_P_PMIC_INT_B - SC_P_SCU_BOOT_MODE0 through SC_P_SCU_BOOT_MODE5 board_system_config is where early resource management occurs, this function is only called when the alt_config flag is set in the image, and it can create partitions and allocate resources to it. More details are found in the resource management service 101. board_get_pcie_clk_src defines the clock that the PCIe uses, it can be either BOARD_PCIE_PLL_EXTERNAL or BOARD_PCIE_PLL_INTERNAL. board_print is very useful to debug your changes the syntax is as follows: board_print(3, "Debug printout %d\n", val);‍‍‍‍‍‍‍ Where the first parameter is the Debug Level and from there on it works as a standard printf. The output will only be visible on the SCU debug output whenever the SCU is built with the corresponding debug level, in the case above the SCFW needs to be built as follows in order to see the output: make qm B=myBoard‍‍‍‍ DL=3 or higher (debug level goes from 0 to 5)‍‍‍‍‍‍‍   Usage examples The following utility shows how to make System Controller Firmware requests and provides a way to make such requests through command line interface on both QNX and Linux System Controller Firmware Command Line Utility for Linux and QNX   System Controller Firmware 101  
View full article
Streaming different use case pipelines between i.MX 95 and i.MX 8M Plus LF-6.12.20
View full article
based on customer's issue when use PTF pins of imx8ulp as GPIO or gpio hog
View full article
This post contains a guide of how to use SDMA1 on Cortex M7 in parallel of Linux on A53. For i.MX 8M Plus, SDMA1 is a general-purpose DMA engine which can be used by low speed peripherals including UART, SPI and other peripherals. But some customers found issues when they are using SDMA1 on M7 core in parallel of Linux on A53. For example, if you try to run the sdma_uart_transfer example on the i.MX8M Plus EVK, the example works correctly when interfacing through the JLink debugger.  However, you will find that you can not run it from both the remoteproc interface and U-Boot.  It exits without error from the UART_SendSDMA function,  but the callback is never called and it seems to hang waiting for the information to be sent. On the i.MX 8MP EVK board,  uart4 is used for Cortex-M7 core. This article tries to provide an example to establish communication using UART3 and SDMA1 on the i.MX 8MP EVK, while Linux is running on Core A53.  This example is based on sdma_uart_transfer demo. The steps are verified with i.MX Linux 6.12.20_2.0.0  release and SDK_25.06.00. The software is compiled on an Ubuntu 22.04 host machine. This article is structured as follows:  1  Hardware requirements 2  Software Requirements 3  Modification in application      3.1 Pin changes     3.2 Clock changes     3.3 Application specific changes     3.4 Memory Region Control change 4  ATF changes     4.1 Download ATF source and change it      4.2 build ATF 5   U-BOOT change     5.1 build u-boot     5.2 make imx-boot image by using imx-mkimage     5.3 flash imx-boot image into i.MX 8MP EVK board 6  Running and Debugging     6.1    Debugging Cortex-M while Cortex-A is in U-BOOT     6.2   Debugging Cortex-M while Cortex-A is in Linux 7  Summary   1  Hardware requirements   -PC Host with MCUXpresso for VS Code installed -i.MX 8M Plus EVK (i.MX 8M Plus Power Evaluation Kit | NXP Semiconductors) -12V power supply -Micro USB Cable -J-Link Debug Probe. -USB To TTL( serial ) Converter   connect J21 (Pin6_GND  Pin8_UART3-TXD  Pin10_UART3-RXD) to Host PC via a USB to TTL converter.       2  Software Requirements   SDK_25_06_00_EVK-MIMX8MP This package can be download from https://mcuxpresso.nxp.com/ Next I will describe the detailed steps.   3  Modification in application     3.1 Pin changes   evkmimx8mp_iuart_sdma_transfer\pin_mux.c    3.2 Clock changes   evkmimx8mp_iuart_sdma_transfer\clock_config.c In function BOARD_BootClockRUN     3.3 Application specific changes   evkmimx8mp_iuart_sdma_transfer\board.h      app.h   Till now, we have completed all the changes for change uart4 to uart3. Compile , and debug with J-LINK, we can get the correct result.   Board receives 8 characters then sends them out.   However, if we try to load code on Cortex-M from U-Boot or Linux,  we can not get the expected results.   Below steps is a workaround to fix this issue. 3.4 Memory Region Control change   hardware_init.c In function BOARD_InitHardware ..... Then compile the application, the output are  iuart_sdma_transfer.bin and iuart_sdma_transfer_cm7.elf   4  ATF (ARM Trust Firmware)changes   4.1  Download ATF source and Change it  The RDC configuration in default BSP assign UART2 to domain 0 for A53,  and Domain 0 can read/write RDC,  and Domain 1 (M7) only can read it. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.12.3-1.0.0   GitHub - nxp-imx/imx-atf: i.MX ARM Trusted firmware plat/imx/imx8m/imx8mp/imx8mp_bl31_setup.c We need to assign UART3 to domain 1 so Cortex M7 can access   4.2 build ATF      $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.12.3-1.0.0 $ cd imx-atf $ source /opt/fsl-imx-xwayland/6.12-walnascar/environment-setup-armv8a-poky-linux $ export ARCH=arm64 $ unset LDFLAGS $ make PLAT=imx8mp bl31   This builds the bl31.bin binary, the location is : build/imx8mp/release/bl31.bin   5   U-BOOT change   5.1 Download and build u-boot please refer to chapter 4.5.13 How to build imx-boot image by using imx-mkimage ,   $ git clone https://github.com/nxp-imx/uboot-imx -b lf_v2025.04 $ cd uboot-imx/ $ source /opt/fsl-imx-xwayland/6.12-walnascar/environment-setup-armv8a-poky-linux $ export ARCH=arm64 $ make distclean $ make imx8mp_evk_defconfig $ make   The compiled u-boot.bin location uboot-imx/u-boot.bin   5.2 make imx-boot image by using imx-mkimage   My work folder The following steps allow you to build the bootable image for i.MX 8M Plus EVK, there are 9 files needed to generate a bootable image: ├── u-boot-spl.bin ├── u-boot-nodtb.bin   ├── imx8mp-evk.dtb ├── bl31.bin ├── signed_hdmi_imx8m.bin ├── lpddr4_pmu_train_1d_dmem_202006.bin ├── lpddr4_pmu_train_1d_imem_202006.bin ├── lpddr4_pmu_train_2d_dmem_202006.bin └── lpddr4_pmu_train_2d_imem_202006.bin   Once you have the nine files , use imx-mkimage tool. 5.2.1  Download source : $ git clone https://github.com/nxp-imx/imx-mkimage.git -b lf-6.12.20-2.0.0   5.2.2  Copy and rename mkimage from u-boot/tools/mkimage to imx-mkimage/iMX8M/mkimage_uboot. $ cp uboot-imx/tools/mkimage imx-mkimage/iMX8M/mkimage_uboot   5.2.3 Copy u-boot-spl.bin from u-boot/spl/u-boot-spl.bin to imx-mkimage/iMX8M/ $ cp uboot-imx/spl/u-boot-spl.bin imx-mkimage/iMX8M/   5.2.4 Copy u-boot-nodtb.bin from u-boot/u-boot-nodtb.bin to imx-mkimage/iMX8M/ $ cp uboot-imx/u-boot-nodtb.bin imx-mkimage/iMX8M/   5.2.5 Copy  imx8mp-evk.dtb from u-boot/arch/arm/dts/ to imx-mkimage/iMX8M/. $cp uboot-imx/u-boot.dtb imx-mkimage/iMX8M/imx8mp-evk.dtb   5.2.6 Copy bl31.bin from Arm Trusted Firmware (imx-atf) to imx-mkimage/iMX8M/ $ cp imx-atf/build/imx8mp/release/bl31.bin imx-mkimage/iMX8M/   5.2.7 Copy the LPDDR4 Training Firmware Download LPDDR Training Firmware cd ~/work wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.16.bin chmod +x firmware-imx-8.16.bin ./firmware-imx-8.16.bin   copy below files from firmware/ddr/synopsys of the firmware-imx package to imx-mkimage/iMX8M/ lpddr4_pmu_train_1d_dmem_202006.bin  lpddr4_pmu_train_1d_imem_202006.bin lpddr4_pmu_train_2d_dmem_202006.bin lpddr4_pmu_train_2d_imem_202006.bin    $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_1d_dmem_202006.bin imx-mkimage/iMX8M/ $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_1d_imem_202006.bin imx-mkimage/iMX8M/ $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_2d_dmem_202006.bin imx-mkimage/iMX8M/ $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_2d_imem_202006.bin imx-mkimage/iMX8M/    5.2.8 Copy firmware/hdmi/cadence/signed_hdmi_imx8m.bin from the firmware-imx package to imx-mkimage/iMX8M/.   $ cp firmware-imx-8.16/firmware/hdmi/cadence/signed_hdmi_imx8m.bin imx-mkimage/iMX8M/   The folder structure after copying all the necessary files     5.2.9 Build the bootable image run make SOC=iMX8MP flash_evk to generate imx-bootimage. $ cd imx-mkimage $ make SOC=iMX8MP flash_evk The compiled file is flash.bin and its location iMX8M/flash.bin   5.3 flash imx-boot image into i.MX 8MP EVK board   In order to flash the imx-boot image,  please follow the following steps -copy  uuu.exe and flash.bin in a folder -change the board's SW4 (boot mode) to 0001 to enter serial download mode  uuu.exe -b emmc  flash.bin   uuu.exe -b emmc flash.bin -power off the board, change SW4 to switch the board back to 0010 (eMMC boot mode).    6  Running and Debugging   Download the application (iuart_sdma_transfer.bin and iuart_sdma_transfer_cm7.elf) to /run/media/boot-mmcblk1p1   6.1    Debugging Cortex-M while Cortex-A is in U-BOOT   $ fatload mmc 2:1 0x48000000 iuart_sdma_transfer.bin $ cp.b 0x48000000 0x7e0000 30000; $ bootaux 0x7e0000   $ fatload mmc 2:1 0x48000000 iuart_sdma_transfer2.bin $ cp.b 0x48000000 0x7e0000 30000; $ bootaux 0x7e0000 From M7 console, we can see the output   6.2   Debugging Cortex-M while Cortex-A is in Linux   u-boot=> setenv fdtfile 'imx8mp-evk-rpmsg.dtb' u-boot=>run prepare_mcore u-boot=>boot   u-boot=> setenv fdtfile 'imx8mp-evk-rpmsg.dtb' u-boot=>run prepare_mcore u-boot=>boot Linux system boot up:   echo /run/media/boot-mmcblk2p1/iuart_sdma_transfer_cm7.elf > /sys/class/remoteproc/remoteproc0/firmware echo start > /sys/class/remoteproc/remoteproc0/state Then we can see the output from M7 console.   7  Summary   This is a workaround to run UART with SDMA1 enabled on Cortex-M7,  and Linux running on Cortex-A53 in parallel.  In order to do that, we need to modify the ATF, and U-BOOT, and application.   With the above modifications, I can get the expected results.   References: 1. UG10163: i.MX Linux User's Guide Rev LF6.12.20_2.0.0--26 June 2025        
View full article
Quickly develop and deploy IoT applications with Clea on your NXP device. This guide walks you through setting up Clea, managing devices remotely, and leveraging AI-powered telemetry for industrial applications.
View full article