i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
Build the tool chain image. It generates the toolchain that will be installed on your host machine and used to build any source code: $ bitbake meta-toolchain It does take some time to build. Why to create a toolchain? Yocto is not intended to be used to package development. Yocto is a linux distribution creator. It´s intended to be a image builder, a rootfs creator. (please, see more about "what is yocto" here and here) So, yocto itself should not be used to "develop" a new package. Although, Yocto can help creating a environment for development like meta-toolchain or Eclipse ADT. Go HOME Go Task #6 - Customize the image
記事全体を表示
Video, bad performance gst-launch filesrc location=test.mp4 typefind=true ! aiurdemux ! vpudec ! mfw_v4lsink Video, better performance gst-launch filesrc location=sample.mp4 typefind=true ! aiurdemux ! queue max-size-time=0 ! vpudec ! mfw_v4lsink # typefind=true allows to 'type find' the source file before negotiating # max-size-time=0 indicates to ignore possible blocking issues # In case of ASF files gst-launch filesrc location=sample.asf typefind=true ! aiurdemux ! queue max-size-time=0 ! mfw_wmvdecoder ! mfw_v4lsink Audio gst-launch filesrc location=sample.mp3  typefind=true ! beepdec ! audioconvert  ! 'audio/x-raw-int, channels=2' ! alsasink Audio with visualization gst-launch filesrc location=sample.mp3 typefind=true ! beepdec ! tee name=t ! queue ! audioconvert  ! 'audio/x-raw-int, channels=2' ! alsasink t. ! queue ! audioconvert ! goom ! autovideoconvert ! autovideosink Video/Audio long version gst-launch filesrc location=sample.avi typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink # queue properties, max-size-buffers=0 and max-size-time=0, allows a smoother playback; type 'gst-inspect queue' for more info VA short version gplay sample.avi VA short version gst-launch playbin2 uri=file://<full path to sample file>
記事全体を表示
The i.MX Android N7.1.2_2.0.0 GA release is now available on IMX_SW page.   Files available: # Name Description 1 android_N7.1.2_2.0.0_docs.tar.gz i.MX Android N7.1.2_2.0.0 BSP Documentation 2 android_N7.1.2_2.0.0_source.tar.gz Source Code of Android N7.1.2_2.0.0 BSP (4.1 kernel) for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite, i.MX6SX and i.MX7D 3 android_N7.1.2_2.0.0_image_6dqpsabreauto.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite 4 android_N7.1.2_2.0.0_image_6dqpsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite. 5 android_N7.1.2_2.0.0_image_6slevk.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - i.MX 6Sololite evaluation kit. 6 android_N7.1.2_2.0.0_image_6sxsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 6SoloX 7 android_N7.1.2_2.0.0_image_6sxsabreauto.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX 8 android_N7.1.2_2.0.0_image_7dsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 7Dual 9 fsl_aacp_dec.tar.gz AAC Plus Codec for N7.1.2_2.0.0 10 android_N7.1.2_2.0.0_tools.tar.gz Manufacturing Toolkit and VivanteVTK for N7.1.2_2.0.0   Supported Hardware SoC/Boards: i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform i.MX 6SoloLite EVK platform i.MX 6SoloX SABRE-SD board and platforms i.MX 6SoloX SABRE-AI board and platforms i.MX 7Dual SABRE-SD board and platform   Changes: Compared to the N7.1.1_1.0.0 release, this release has the following major changes: Upgraded the Android code base from android-7.1.1_r13 to android-7.1.2_r9. Upgraded U-Boot from v2015.04 to v2017.03. Upgraded the kernel from v4.1.15 to v4.9.17. Upgraded the GPU driver from 6.2.0.p2 to 6.2.2.p1. Upgraded the Wi-Fi BCMDHD release version to 1.141.100.6. Refine the Gralloc and HWC HAL. Enable the GPT partition to replace the MBR partition.   Feature: For features please consult the release notes.   Known issues For known issues and more details please consult the Release Notes.
記事全体を表示
This is sample code for CSC settings for /dev/fb1. It can calculating the CSC matrix and updates in real time from given parameters(Brightness,Contrast,Saturation,Hue, and gamma).
記事全体を表示
         In recent months, some I.MX customers hope to compile u-boot-fw-utils in yocto and get fw_printenv & fw_setenv tools.          Although there are u-boot-fw-utils bblayers in Yocto recipes, by default, u-boot-fw-utils is not based on u-boot-imx, but downloaded from the u-boot source website, when using bitbake When u-boot-fw-utils compiles it, it will fail to compile.          For example: # cd  ~/imx-yocto-bsp-5.4.3_1.0.0 # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source imx-setup-release.sh -b build_sabresd # bitbake u-boot-fw-utils -c compile          If changing .config to be mx6sxsabresd_optee_defconfig in the top directory of u-boot source code, new errors will occur, like descriptions in the link:          https://community.nxp.com/message/1318081?commentID=1318081#comment-1318081            The root cause is that the u-boot is not u-boot-imx.          If we did the test below, it is easy to validate it.      Compiling u-boot # bitbake u-boot-imx -c compile          After compilation is done, u-boot-imx source code will be released .      Changing u-boot source code of u-boot-fw-utils directory          Replace u-boot source code in u-boot-fw-utils directory with u-boot-imx source code. Then continue to compile u-boot-fw-utils # bitbake u-boot-fw-utils -c compile          We will find it can be compiled successfully. This shows that when u-boot-fw-utils is compiled, the downloaded u-boot source code must be u-boot-imx.          In order to achieve this, we need to add recipes to yocto's u-boot-imx, and we can successfully compile fw_printevn and fw_setenv through the bitbake command. Please follow these steps to add u-boot-fw-utils for i.mx to yocto! copy 2 files in attacments to ~/imx-yocto-bsp-5.4.3_1.0.0/sources/meta-imx/meta-bsp/recipes-bsp/u-boot cd ~/imx-yocto-bsp-5.4.3_1.0.0 run below comands # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source imx-setup-release.sh -b build_sabresd # bitbake u-boot-imx-fw-utils -c compile # bitbake u-boot-imx-fw-utils -c install   Then you will get fw_printenv & fw_setenv [Comment]          If i.MX users are using other version of linux BSP, she only need to modify the following content of u-boot-imx-common_2019.04.inc to compile u-boot-fw-utils. …… LIC_FILES_CHKSUM = "file://Licenses/gpl-2.0.txt;md5=b234ee4d69f5fce4486a80fdaf4a4263"   UBOOT_SRC ?= "git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https" SRCBRANCH = "lf-5.4.y_v2019.04" SRC_URI = "${UBOOT_SRC};branch=${SRCBRANCH} \ " SRCREV = "228843cdf5435d4bd69f42a6015f78761ff4cc0d" ……          Then compile it following above steps.          Example for L4.14.98_2.0.0: 1.Copy u-boot-imx-common_2019.04.inc & u-boot-imx-fw-utils_2019.04.bb to ~/imx-release-bsp-4.14.98-2.0.0/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/ 2.Rename files name according to u-boot version u-boot-imx-common_2018.03.inc     u-boot-imx-fw-utils_2018.03.bb 3.Modifying u-boot-imx-common_2018.03.inc In the directory, there is u-boot-imx_2018.03.bb file, open it, and find the link of u-boot and check sum, and use lines below to replace those lines in u-boot-imx-common_2018.03.inc In u-boot-imx_2018.03.bb file: …… LICENSE = "GPLv2+" LIC_FILES_CHKSUM = "file://Licenses/gpl-2.0.txt;md5=b234ee4d69f5fce4486a80fdaf4a4263"   UBOOT_SRC ?= "git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https" SRCBRANCH = "imx_v2018.03_4.14.98_2.0.0_ga" SRC_URI = "${UBOOT_SRC};branch=${SRCBRANCH}" SRCREV = "87a19df5e462f1f63e8a6d2973c7fb9e95284d04" …… Then in u-boot-imx-common_2018.03.inc, there is the same contents as above: Save it and exit. Go back to the top directory of yocto: ~/imx-release-bsp-4.14.98-2.0.0 # cd ~/imx-release-bsp-4.14.98-2.0.0 # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source fsl-setup-release.sh -b build_sabresd # bitbake u-boot-imx-fw-utils -c compile # bitbake u-boot-imx-fw-utils -c install          The same method can be used for other Linux BSP versions.       NXP TIC Team Weidong Sun 05/28/2020
記事全体を表示
To build Android version earlier than Lollipop from source code, you need the Sun's 1.6 SDK to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. You may still cannot get the Sun's JDK  with below instruction: $ sudo add-apt-repository "deb http://archive.canonical.com/ lucid partner" $ sudo apt-get update $ sudo apt-get install sun-java6-jdk    There are below options to help install the Sun's JDK  if you cannot find a valid source through apt-get commands: $ wget --no-cookies --header "Cookie: gpw_e24=http%3A%2F%2Fwww.oracle.com%2F" http://download.oracle.com/otn-pub/java/jdk/6u45-b06/jdk-6u45-linux-x64.bin $ chmod u+x jdk-6u45-linux-x64.bin $ ./jdk-6u45-linux-x64.bin $ sudo mv jdk1.6.0_45 /opt $ sudo update-alternatives --install /usr/bin/java java /opt/java/64/jdk1.6.0_45/bin/java 1 $ sudo update-alternatives --install /usr/bin/javac javac /opt/java/64/jdk1.6.0_45/bin/javac 1 $ sudo update-alternatives --install /usr/bin/jar jar /opt/java/64/jdk1.6.0_45/bin/jar 1 # if you have already install some other version of JDK, please export the JAVA_HOME env before your android build every time $ export JAVA_HOME=/opt/jdk1.6.0_45/ #or you can directly link the java binary to the sdk version you need as below: sudo ln -s /opt/java/64/jdk1.6.0_45/bin/jar /bin/jar sudo ln -s/opt/java/64/jdk1.6.0_45/java /bin/java sudo ln -s/opt/java/64/jdk1.6.0_45/javac /bin/javac sudo ln -s/opt/java/64/jdk1.6.0_45/javah /bin/javah sudo ln -s/opt/java/64/jdk1.6.0_45/javadoc /bin/javadoc sudo ln -s/opt/java/64/jdk1.6.0_45/javaws /bin/javaws    To built the Android version Lollipop and Marshmallow from source code, you need the OpenJDK 7 to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. $ sudo apt-get update $ sudo apt-get install openjdk-7-jdk You may have both openjdk7 and SUN JDK 1.6 intalled in your ubuntu to build different Android version. If you have default java SDK to be Sun's JDK 1.6, you can just use below commands to make android build system use the openjdk7 for Lollipop built $ export JAVA_HOME=/usr/lib/jvm/java-7-openjdk-amd64/ $ cd myandroid $ . ./build/envsetup.sh           //be sure to resetup the envsetup, and pick the platform to be built $ lunch
記事全体を表示
There is a very quick way to find out which line cause the crash in logcat, Generally, if some native service crashes, look in the crash log in logcat like this: I/DEBUG ( 2253): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** I/DEBUG ( 2253): Build fingerprint: 'freescale/sabresd_6dq/sabresd_6dq:4.0.4/R13.3-rc3/eng.b18293.20120710.124535:user/test-keys' I/DEBUG ( 2253): pid: 3043, tid: 3080 >>> /system/bin/mediaserver <<< I/DEBUG ( 2253): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad I/DEBUG ( 2253): r0 deadbaad r1 00000001 r2 a0000000 r3 00000000 I/DEBUG ( 2253): r4 00000000 r5 00000027 r6 00bfd370 r7 40c1ef18 I/DEBUG ( 2253): r8 00004349 r9 00000000 10 000003f5 fp 00000000 I/DEBUG ( 2253): ip ffffffff sp 418876a0 lr 400ff1b5 pc 400fb91c cpsr 60000030 I/DEBUG   ( 2253):  ip ffffffff  sp 418876a0  lr 400ff1b5  pc 400fb91c  cpsr 60000030 We can see it’s possibly related to some code that we debugged, but don’t know exactly where or which line of code, Android has a tool to convert this log to a more precise log. As a quick example, if you got this crash in logcat: F/libc ( 3043): Fatal signal 11 (SIGSEGV) at 0xdeadbaad (code=1) I/DEBUG ( 2253): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** I/DEBUG ( 2253): Build fingerprint: 'freescale/sabresd_6dq/sabresd_6dq:4.0.4/R13.3-rc3/eng.b18293.20120710.124535:user/test-keys' I/DEBUG ( 2253): pid: 3043, tid: 3080 >>> /system/bin/mediaserver <<< I/DEBUG ( 2253): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad I/DEBUG ( 2253): r0 deadbaad r1 00000001 r2 a0000000 r3 00000000 I/DEBUG ( 2253): r4 00000000 r5 00000027 r6 00bfd370 r7 40c1ef18 I/DEBUG ( 2253): r8 00004349 r9 00000000 10 000003f5 fp 00000000 I/DEBUG ( 2253): ip ffffffff sp 418876a0 lr 400ff1b5 pc 400fb91c cpsr 60000030 I/DEBUG ( 2253): d0 3e4ccccd00000000 d1 7e37e43c3e4ccccd I/DEBUG ( 2253): d2 0000004042000000 d3 4200000000000000 I/DEBUG ( 2253): d4 3ff0000000000000 d5 3ff0000000000000 I/DEBUG ( 2253): d6 4220000041300000 d7 3e4ccccd3e4ccccd I/DEBUG ( 2253): d8 000000000000685d d9 00000000010bee7c I/DEBUG ( 2253): d10 0000000000000000 d11 0000000000000000 I/DEBUG ( 2253): d12 0000000000000000 d13 0000000000000000 I/DEBUG ( 2253): d14 0000000000000000 d15 0000000000000000 I/DEBUG ( 2253): d16 0000000000000000 d17 3ff0000000000000 I/DEBUG ( 2253): d18 7e37e43c8800759c d19 0000000000000000 I/DEBUG ( 2253): d20 bfe0000000000000 d21 405443dab91ed79f I/DEBUG ( 2253): d22 0000000000000000 d23 3f40624dd2f1a9fc I/DEBUG ( 2253): d24 7fff80007fff0000 d25 3f6328e1cb8c85e0 I/DEBUG ( 2253): d26 0000000000000000 d27 0000000000000000 I/DEBUG ( 2253): d28 0000000000000000 d29 0000000000000000 I/DEBUG ( 2253): d30 0000000000000000 d31 0000000000000000 I/DEBUG ( 2253): scr 28000010 I/DEBUG ( 2253): I/DEBUG ( 2253): #00 pc 0001791c /system/lib/libc.so I/DEBUG ( 2253): #01 pc 00003f3e /system/lib/libcutils.so (__android_log_assert) I/DEBUG ( 2253): #02 pc 0006c436 /system/lib/libstagefright.so (_ZN7android8OMXCodec16drainInputBufferEPNS0_10BufferInfoE) I/DEBUG ( 2253): #03 pc 0006cbc2 /system/lib/libstagefright.so (_ZN7android8OMXCodec17drainInputBuffersEv) I/DEBUG ( 2253): #04 pc 0006f570 /system/lib/libstagefright.so (_ZN7android8OMXCodec4readEPPNS_11MediaBufferEPKNS_11MediaSource11ReadOpti onsE) I/DEBUG ( 2253): #05 pc 00051aba /system/lib/libstagefright.so (_ZN7android11AudioPlayer5startEb) I/DEBUG ( 2253): #06 pc 0005411e /system/lib/libstagefright.so (_ZN7android13AwesomePlayer18startAudioPlayer_lEb) I/DEBUG ( 2253): #07 pc 0005554a /system/lib/libstagefright.so (_ZN7android13AwesomePlayer6play_lEv) I/DEBUG ( 2253): #08 pc 000558e0 /system/lib/libstagefright.so (_ZN7android13AwesomePlayer4playEv) I/DEBUG ( 2253): #09 pc 00027f4e /system/lib/libmediaplayerservice.so (_ZN7android17StagefrightPlayer5startEv) I/DEBUG ( 2253): #10 pc 00024dda /system/lib/libmediaplayerservice.so (_ZN7android18MediaPlayerService6decodeEixxPjPiS2_) I/DEBUG ( 2253): I/DEBUG ( 2253): code around pc: I/DEBUG ( 2253): 400fb8fc 4623b15c 2c006824 e026d1fb b12368db \.#F$h.,..&..h#. I/DEBUG ( 2253): 400fb90c 21014a17 6011447a 48124798 24002527 .J.!zD.`.G.H'%.$ I/DEBUG ( 2253): 400fb91c f7f47005 2106ee22 eebef7f5 f04fa901 .p.."..!......O. I/DEBUG ( 2253): 400fb92c 460a5380 93032006 94029401 ea7af7f5 .S.F. ........z. I/DEBUG ( 2253): 400fb93c 4622a905 f7f52002 f7f4ea84 2106ee0e .."F. .........! I/DEBUG ( 2253): I/DEBUG ( 2253): code around lr: I/DEBUG ( 2253): 400ff194 41f0e92d 4c0c4680 447c2600 68a56824 -..A.F.L.&|D$h.h I/DEBUG ( 2253): 400ff1a4 e0076867 300cf9b5 dd022b00 47c04628 gh.....0.+..(F.G I/DEBUG ( 2253): 400ff1b4 35544306 37fff117 6824d5f4 d1ee2c00 .CT5...7..$h.,.. I/DEBUG ( 2253): 400ff1c4 e8bd4630 bf0081f0 00028346 41f0e92d 0F......F...-..A I/DEBUG ( 2253): 400ff1d4 9004b086 f602fb01 460c461f 46154814 .........F.F.H.F I/DEBUG ( 2253): I/DEBUG ( 2253): memory map around addr deadbaad: I/DEBUG ( 2253): becef000-bed10000 [stack] I/DEBUG ( 2253): (no map for address) I/DEBUG ( 2253): ffff0000-ffff1000 [vectors] I/DEBUG ( 2253): You can see it’s related to which lib, but don’t know which line. So, let’s go to your source code, for example: mydroid; after do $. build/envsetup.sh$ lunch sabresd_6dp-eng $ development/scripts/stack Then you have a prompt: Reading native crash info from stdin The you just copy all the crash log in above to this prompt. And then Key in EOF (CTRL+D) in this prompt. You will get output like this: Reading symbols from /home/b33651/proj/ics/out/target/product/sabresd_6dq/symbols pid: 3043, tid: 3080 >>> /system/bin/mediaserver <<< signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad   r0 deadbaad r1 00000001 r2 a0000000 r3 00000000   r4 00000000 r5 00000027 r6 00bfd370 r7 40c1ef18   r8 00004349 r9 00000000 10 000003f5 fp 00000000   ip ffffffff sp 418876a0 lr 400ff1b5 pc 400fb91c Stack Trace:   RELADDR FUNCTION FILE:LINE   0001791c __libc_android_abort+92 /home/b33651/proj/ics/bionic/libc/unistd/abort.c:82   00003f3e __android_log_assert+94 /home/b33651/proj/ics/system/core/liblog/logd_write.c:246   0006c436 android::OMXCodec::drainInputBuffer(android::OMXCodec::BufferInfo*)+138 /home/b33651/proj/ics/frameworks/base/media/libstagefright/OMXCodec.cpp:3181   0006cbc2 android::OMXCodec::drainInputBuffers()+102 /home/b33651/proj/ics/frameworks/base/media/libstagefright/OMXCodec.cpp:3125   0006f570 android::OMXCodec::read(android::MediaBuffer**, android::MediaSource::ReadOptions const*)+136 /home/b33651/proj/ics/frameworks/base/media/libstagefright/OMXCodec.cpp:4020   00051aba android::AudioPlayer::start(bool)+134 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AudioPlayer.cpp:93   0005411e android::AwesomePlayer::startAudioPlayer_l(bool)+70 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AwesomePlayer.cpp:953   0005554a android::AwesomePlayer::play_l()+202 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AwesomePlayer.cpp:888   000558e0 android::AwesomePlayer::play()+20 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AwesomePlayer.cpp:837   00027f4e android::StagefrightPlayer::start()+6 /home/b33651/proj/ics/frameworks/base/media/libmediaplayerservice/StagefrightPlayer.cpp:90   00024dda android::MediaPlayerService::decode(int, long long, long long, unsigned int*, int*, int*)+206 /home/b33651/proj/ics/frameworks/base/media/libmediaplayerservice/MediaPlayerService.cpp:1428 So, you get more reason logs. Note: The Android directory must have built once. The crash log better aligns with your Android build environment.
記事全体を表示
This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0.  It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-12.04.3-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1 $ sudo apt-get install uboot-mkimage $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source.tar.gz $ ./L3.0.35_4.1.0_130816_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_12.04_64bit_OS.patch The patch modifies the following files: dist/lfs-5.1/base_libs/base_libs.spec dist/lfs-5.1/ncurses/ncurses.spec E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
記事全体を表示
Purpose:  Introduce how to debug M4 using trace32 and the difference with general debug case.If you are using other jtag debug tools, maybe you need to do the similar configuration. Debug tools: Trace32 – you can refer to http://www.lauterbach.cn/ for more information about this tool. Firmware: Here we using Freertos as the example, but not limited to this. There is one small difference with general debug case to M4 in 6sx, which when you attach M4 and break M4, it may impact the peripheral that A9 is using. You may have found when you break M4, A9 uart console also was frozen at the same time. This is caused by that when M4 enter debug mode, the debug_req will also assert in the peripherals which you are using on the A9 system. So,need configure the peripherals to keep running when the debug_req is assert when do the M4/A9 debug separately. Need configure the DBGEN (*) register in the related peripherals to allow the eripherals not going into debug mode and keep running even if debug_req is HIGH. The peripherals we need take care are: CAN, UART, EPIT,GPT, ENET, PWM. Note: For the CAN, the register bit is called FRZ Here is the details of uart dbgen in the RM: So if we want debug M4 separately,we should disable this bit, as A9 was using this peripheral. Here we take Freertos as the example to illuminate how to debug M4 step by step: Enable DBGEN case: Load M4 image into memory and kick off M4. (You can refer to  for the details)           =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000               ##Starting auxiliary core at 0x9FF00000                ... Attach M4 using the m4.cmm file(attached): Note:  You can find the elf file at the same folder of binary: So now you can debug your code step by step.If you go back to A9 side uart console, you would find the console have been frozen. Disable DBGEN case at A9 side: Load M4 image into memory and kick off M4. (You can refer to  for imx6sx user guide  the details)           =>mm 0x20200b4                              020200b4:00000020 ? 0x820           =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000                ##Starting auxiliary core at 0x9FF00000                ... Attach M4 using the m4.cmm file(attached) In this case you will the A9 uart console still can work, after you break M4. Disable DBGEN case at M4 side: Load M4 image into memory and kick off M4.   =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                     reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000          ##Starting auxiliary core at 0x9FF00000 Attach M4 using the m4_disable_dbgen.cmm  file(attached) In this case you will the A9 uart console still can work, after you break M4.   Notes: For more trace32 usage, please refer to http://www.lauterbach.cn/           For more imx6sx information, please refer to i.MX 6SoloX Family of Applications Processors|NXP.
記事全体を表示
Current the SSI is set to I2S slave mode in FSL default release BSP. attached the code for how to set it to master mode.
記事全体を表示
The NXP i.MX 8M provides industry leading audio, voice and video processing for applications that scale from consumer home audio to industrial building automation and mobile computers. The i.MX 8M Quad supports multiple audio interfaces as listed below: Besides the general audio input/output function, the audio interfaces will supports following features: - SAI-1 supports up to 16-channels TX (8 lanes) and 16-channels RX (8 lanes) at 384KHz/32-bit. - SAI-5 supports up to 8-channels TX (4 lanes) and 8-channels RX (4 lanes) at 384KHz/32-bit. - SAI-2/3/6 supports up to 2-channels TX (1 lanes) and 2-channels RX (1 lanes) at 384KHz/32-bit. - SAI-2/3/6 support up to 2-channels TX (1 lane) and 2-channels RX (1 lane) at 384KHz/32-bit. - SAI-1 supports glue-less switching between PCM & DSD operation for popular audio DACs - SPDIF-1/2 supports raw capture mode that can save all the incoming bits into audio buffer The SAI-1/2/3/5/6 and SPDIF-1 share GPIO pads on the chip through IOMUX. Common use cases supported by the audio interfaces are listed in the table below (many other configurations are possible). The number is the data lanes supported. For the MCLK pin on each SAI module, it can be configured as either input or output. When configured as output, the SAI_CLK_ROOT from CCM will be routed to the pad output. When configured as input, the external input to the pad will be routed to SAI.MCLK, which can be used as master clock for SAI. Below is the diagram showing the both input/output options, by using SAI1 as the example. Each SAI module supports up to 3 master clock inputs. The TX and RX sub-module inside each SAI can independently select one of the clock inputs as its master clock. This allows TX and RX of one SAI to run from different clock source. The master clock inputs have following options: - SAI.MCLK[1] can be selected from SAI_CLK_ROOT from CCM or SAI.MCLK from IOMUX. This is the most straight-forward clock routing in which SAI only use its own clock source from CCM or IO pad. - SAI.MCLK[2] can be selected from following clock sources:       Any of the SAI_CLK_ROOT from CCM;       Any of the SAI.MCLK from IOMUX;       Other clock sources from SPIDF; - SAI.MCLK[3] has exact same clock source options as SAI.MCLK[2]. This allows both TX and RX can have access to all the options without any dependency between each other. The clock options for master clock on SAI are shown in the diagram blow, by using SAI-1 as an example. The options on MCLK[1] is also available on MCLK[2] and MCLK[3]. The reason to keep this options is to provide the similar SAI clock structure as i.MX6/i.MX7 processors. The configuration of the MUX for master clock are controlled by IOMUXC_GPR registers. They should be configured before SAI clock is enabled to avoid glitches on the clock. Note: Because those MUX on clocks are missed during the design, the actual implementation in the silicon is simplified as shown in the following diagram. All the SAI and SPDIF instances have SDMA support. In order to meet the audio data rate, two SDMA modules are used. Because the SAI-2/3 and SPDIF-1/2 do not require high data throughput, they are assigned to SDMA-1, shared with other peripherals such as UART/SPI. SAI-1/4/5/6 need to support high sample rate & multichannel audio, they are assigned to SDMA-2, which is a dedicated SDMA engine for audio. The SDMA-2 frequency is increased to 500/250 instead of 133/66 to make sure it has enough throughput. In order to allow SW tracking the progress of audio DMA, the TX_SYNC and RX_SYNC of SAI modules are routed to GPT as the external clock input. Since there are totally 6 SAI modules, these signals will be MUXed when connection to GPT. - GPT-4/5/6 external clock input can be selected from the TX_SYNC or RX_SYNC of any 6 SAI modules; - The MUX select is controlled by IOMUXC_GPR register; - The MUX select register for GPT-4/5/6 are fully independent of each other.
記事全体を表示
This is a copy of the currently posted i.MX 6DQ reference manual, revision 2, published Jun 2014.  This is part 1 of 2, and includes the first 43 chapters.  Go here for part 2: i.MX 6DQ Reference Manual (IMX6DQRM R2, Part 2) This document is to be used to enter community comments.  Please feel free to add inline comments in this reference manual. You can point out where more information is needed or where existing information is incorrect.  You can also enter information in your comment that expands on existing information in the document, based on your experience with the device.  If you are pointing out that more information is needed in a paragraph or a section, please be very specific, not “needs more information”.  Your comments in this manual may help other members and will drive improvements in this and future documentation. Note: The doc viewer does not support going directly to a specified page.  Instead of manually paging through one page at a time, you can do a search on a string on a page such as "types of resets", or you can go to chapter links listed in the inline comments.  To do this, page down to the comments below the doc view, select "Inline Comments", sort the comments by "page", and then select the chapter you want to view. You may find it easier to use this manual by downloading and viewing it in your local Adobe Reader.  Then when you have a comment/question to add to this review copy, navigate to the chapter as described above and then do a search on the text for which you want to add a comment.  This will take you to that page the quickest.
記事全体を表示
You already know. Your source code is one week old now, so please, update it! $ repo sync What was the changes? Please, read the output and determinate what file was changed. Directory tree This is what I have under fsl-community-bsp directory: $ tree -d -L 2 -A . ├── build_mx53 │   ├── conf │   ├── sstate-cache │   └── tmp ├── build_mx6 │   ├── conf │   ├── sstate-cache │   └── tmp ├── downloads │   └── git2 └── sources     ├── base     ├── meta-fsl-arm     ├── meta-fsl-arm-extra     ├── meta-fsl-demos     ├── meta-openembedded     └── poky Sstate-cache keeps the pre-build packages cache so once one package is built, and it´s not changes, no need to re-build it again. If a team shares the same build environment, the sstate-cache folder can be shared as well. I´m not personally used to configure it, so, please, follow the doc: Yocto Project Reference Manual The downloads folder is shared for any build folder. It holds every package´s source code. For example, the ssh source code (and this source code can be built for any architecture) In addition, you may want to share the download folder with your team (one download folder for the complete team), so please, go to Yocto Project Reference Manual and look for DL_DIR. Build_mx6 tree .../build_mx6$ tree -d -L 2 -A . ├── conf ├── sstate-cache └── tmp     ├── buildstats     ├── cache     ├── deploy     ├── log     ├── pkgdata     ├── sstate-control     ├── stamps     ├── sysroots     ├── work     └── work-shared Inside tmp folder you will find images and build results. Images is placed inside deploy. Build statistics like initial and final time for each package/task are under buildstats The complete log for any 'bitbake' you did is under log. Take a look, for example, on the file  log/cooker/imx6qsabresd/11111111111.log. Please, notice that 111111111 is the PID number, so every time you run bitbake you have a different one. The source code, the patches, and the logs for the last bitbake, for each package is under work. Take a look on the files under tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/ for example, for the kernel. .../build_mx6$ tree -d -L 1 -A tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/ tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/ ├── deploy-linux-imx ├── deploy-rpms ├── git ├── image ├── license-destdir ├── package ├── packages-split ├── pkgdata ├── pseudo ├── sysroot-destdir └── temp Go under temp, and see a lot of log.* and run.*: .../build_mx6$ ls tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/temp/ log.do_bundle_initramfs             log.do_uboot_mkimage                run.do_package_write_rpm.28992      run.perform_packagecopy.16364 log.do_bundle_initramfs.28986       log.do_uboot_mkimage.2325           run.do_patch                        run.populate_packages.16364 log.do_compile                      log.do_unpack                       run.do_patch.2556                   run.read_shlibdeps.16364 log.do_compile.3483                 log.do_unpack.1155                  run.do_populate_lic                 run.read_subpackage_metadata.28992 log.do_compile_kernelmodules        log.task_order                      run.do_populate_lic.10988           run.split_and_strip_files.16364 log.do_compile_kernelmodules.29051  run.base_do_fetch.28859             run.do_populate_sysroot             run.split_kernel_module_packages.16364 log.do_configure                    run.base_do_unpack.1155             run.do_populate_sysroot.17692       run.split_kernel_packages.16364 log.do_configure.3048               run.BUILDSPEC.28992                 run.do_qa_configure.3048            run.sstate_create_package.10988 log.do_deploy                       run.debian_package_name_hook.16364  run.do_qa_staging.17692             run.sstate_create_package.16364 log.do_deploy.617                   run.do_bundle_initramfs             run.do_sizecheck                    run.sstate_create_package.17692 log.do_fetch                        run.do_bundle_initramfs.28986       run.do_sizecheck.2323               run.sstate_create_package.2724 log.do_fetch.28859                  run.do_compile                      run.do_strip                        run.sstate_create_package.28992 log.do_install                      run.do_compile.3483                 run.do_strip.2321                   run.sstate_create_package.617 log.do_install.2327                 run.do_compile_kernelmodules        run.do_uboot_mkimage                run.sstate_task_postfunc.10988 log.do_package                      run.do_compile_kernelmodules.29051  run.do_uboot_mkimage.2325           run.sstate_task_postfunc.16364 log.do_package.16364                run.do_configure                    run.do_unpack                       run.sstate_task_postfunc.17692 log.do_packagedata                  run.do_configure.3048               run.do_unpack.1155                  run.sstate_task_postfunc.2724 log.do_packagedata.2724             run.do_deploy                       run.emit_pkgdata.16364              run.sstate_task_postfunc.28992 log.do_package_write_rpm            run.do_deploy.617                   run.fixup_perms.16364               run.sstate_task_postfunc.617 log.do_package_write_rpm.28992      run.do_fetch                        run.package_depchains.16364         run.sstate_task_prefunc.10988 log.do_patch                        run.do_fetch.28859                  run.package_do_filedeps.16364       run.sstate_task_prefunc.16364 log.do_patch.2556                   run.do_install                      run.package_do_pkgconfig.16364      run.sstate_task_prefunc.17692 log.do_populate_lic                 run.do_install.2327                 run.package_do_shlibs.16364         run.sstate_task_prefunc.2724 log.do_populate_lic.10988           run.do_package                      run.package_do_split_locales.16364  run.sstate_task_prefunc.28992 log.do_populate_sysroot             run.do_package.16364                run.package_fixsymlinks.16364       run.sstate_task_prefunc.617 log.do_populate_sysroot.17692       run.do_packagedata                  run.package_get_auto_pr.16364       run.sysroot_cleansstate.3048 log.do_sizecheck                    run.do_packagedata.2724             run.package_get_auto_pr.2327        run.sysroot_stage_all.17692 log.do_sizecheck.2323               run.do_package_qa.16364             run.package_get_auto_pr.617         run.write_specfile.28992 log.do_strip                        run.do_package_rpm.28992            run.package_name_hook.16364 log.do_strip.2321                   run.do_package_write_rpm            run.patch_do_patch.2556 For each package, you will be able to see the log for the latest task, and what was done on the latest task. For example: log.do_compile - shows the log output from latest do_compile made for kernel run.do_compile - shows the compile command line log.do_compile.111111 - shows the log output from 1111111 time of do_compile In order to know the tasks and the task sequence, take a look to log.taskorder file For the images generated, you will find something like that: .../build_mx6$ ls -la tmp/deploy/images/imx6qsabresd/ total 146260 drwxr-xr-x 2 user user     4096 Mar  6 21:21 . drwxrwxr-x 3 user user     4096 Mar  6 21:12 .. -rw-r--r-- 1 user user 67108864 Mar  6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.ext3 -rw-r--r-- 1 user user 83886080 Mar  6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.sdcard -rw-r--r-- 1 user user 18782361 Mar  6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.tar.bz2 lrwxrwxrwx 1 user user       55 Mar  6 21:21 core-image-base-imx6qsabresd.ext3 -> core-image-base-imx6qsabresd-20140306173758.rootfs.ext3 lrwxrwxrwx 1 user user       57 Mar  6 21:21 core-image-base-imx6qsabresd.sdcard -> core-image-base-imx6qsabresd-20140306173758.rootfs.sdcard lrwxrwxrwx 1 user user       58 Mar  6 21:21 core-image-base-imx6qsabresd.tar.bz2 -> core-image-base-imx6qsabresd-20140306173758.rootfs.tar.bz2 -rw-rw-r-- 2 user user   439697 Mar  6 21:12 modules--3.0.35-r37.14-imx6qsabresd-20140306173758.tgz lrwxrwxrwx 2 user user       54 Mar  6 21:12 modules-imx6qsabresd.tgz -> modules--3.0.35-r37.14-imx6qsabresd-20140306173758.tgz -rw-rw-r-- 2 user user      294 Mar  6 21:20 README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt lrwxrwxrwx 2 user user       35 Mar  6 21:16 u-boot.imx -> u-boot-imx6qsabresd-v2013.10-r0.imx lrwxrwxrwx 2 user user       35 Mar  6 21:16 u-boot-imx6qsabresd.imx -> u-boot-imx6qsabresd-v2013.10-r0.imx -rwxr-xr-x 2 user user   297984 Mar  6 21:16 u-boot-imx6qsabresd-v2013.10-r0.imx lrwxrwxrwx 2 user user       53 Mar  6 21:12 uImage -> uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin -rw-r--r-- 2 user user  4042496 Mar  6 21:12 uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin lrwxrwxrwx 2 user user       53 Mar  6 21:12 uImage-imx6qsabresd.bin -> uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin You can access any generated image, the image name ending with the yearmothdaypid (long number) is the real image, and every time your bitbake complete, it generate a new image. The symbolic link points to the latest created image. The .ext3 file is the EXT3 image for the rootfs. (you can copy it directly to SD card using dd: $sudo dd if=core-image-base.ext3 of=/dev/sdb2 ) The .sdcard file is the complete image to be copied to sdcard. It´s u-boot+uImage+rootfs The .tar.bz2 file is the tarball for the rootfs, you can extract it on your PC. uImage is the latest kernel image u-boot is the latest u-boot image. and so on. Play around with generated files. A lot of them I don´t know. And a lot of them I don´t use. For a standard image generation you only need to know where the final images is placed. Any question, comment, issue, please let me know. Before you go, let your bitbake creates the biggest image ever: $ bitbake fsl-image-gui Note (24Feb2014): Required disk space for build image is ~44GB Start it and let it finish while you do something else. Go HOME Go to Task #2 Go to Task#4
記事全体を表示
We are pleased to announce that Pins Tool for i.MX Applications Processors v5 is now available.   The Pins Tool for i.MX Applications Processors is used for pin routing configuration, validation and code generation, including pin functional/electrical properties, power rails, run-time configurations. Features Desktop application Muxing and pin configuration with consistency checking Multicore support Localized for English and Simplified Chinese Mostly Connected: On-Demand device data download Integrates with any compiler and IDE Supports English and Chinese (simplified) languages, based on locale settings. Please refer to user manual for details. ANSI-C initialization code Graphical processor package view Multiple configuration blocks/functions Easy-to-use device configuration Selection of Pins and Peripherals Package with IP blocks Routed pins with electrical characteristics Registers with configured and reset values Power Groups with assigned voltage levels Source code for C/C++ applications Documented and easy to understand source code CSV Report and Device Tree File     Downloads To download the installer for all platforms, please login to our download site via:  http://www.nxp.com/pinsimx Please refer to Pins Tool Documentation  for installation and quick start guides.   Overview of Changes - version 5 New Configuration Wizard allows to specify the default core for multi-core processors. Data Manager - allows overview of downloaded data, their versions, tool support information, update out dated, or manually download new data. Copy/Paste of pin(s) supported in Routed Pins view. Added in-tool tutorials - eclipse Cheat Sheets integration. Overview of Changes - version 4.1 Undo/Redo supported. Product based on Eclipse Oxygen release 3. Unified import wizard. A single import source is implemented. It allows you to import all supported types of C files. Community i.MX Processors 
記事全体を表示
Hi All, The new i.MX 6 Q/D/DL/S/SL L3.0.35_4.1.0 GA release is now available on the http://www.freescale.com/site. ·         Files available                                   # Name Description 1 L3.0.35_4.1.0_LINUX_DOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP   Documentation. Includes Release Notes, Reference Manual, User guide. API   Documentation 2 L3.0.35_4.1.0_LINUX_MMDOCS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Multimedia Codecs Documentation.   Includes CODECs Release Notes and User's Guide 3 L3.0.35_4.1.0_SOURCE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP   Source Code Files 4 L3.0.35_4.1.0_MM_CODECS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Multimedia Codecs Sources 5 L3.0.35_4.1.0_AACP_CODECS i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux AAC Plus Codec 6 L3.0.35_4.1.0_DEMO_IMAGE_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux Binary Demo Files 7 L3.0.35_4.1.0_UBUNTU_RFS_BSP i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite  Linux File System for the Ubuntu Images 8 i.MX_6D/Q_Vivante_VDK_146_Tools Set   of applications for the Linux L3.0.35_4.1.0 BSP, designed to be used by   graphics application developers to rapidly develop and port graphics   applications. Includes applications, GPU Driver with vprofiler enabled and   documentation. 9 IMX_6DL_6S_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6DualLite and i.MX   6Solo. 10 IMX_6DQ_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6Quad and i.MX 6Dual. 11 IMX_6SL_MFG_TOOL Tool   and documentation for downloading OS images to the i.MX 6Sololite. ·         Target HW boards o   i.MX 6Quad SABRE-SDP o   i.MX 6Quad SABRE-SDB o   i.MX 6Quad SABRE-AI o   i.MX 6DualLite SABRE-SDP o   i.MX 6DualLite SABRE-AI o   i.MX 6SL EVK ·         New features o   BSP New Features on i.MX 6D/Q, i.MX 6DL/S and MX 6SL: §  HDCP §  CEC §  GPU4.6.9p12 §  Audio playback IRAM/SDMA §  V4L capture resize on MX6SL §  MX6DQ disable the double line fill feature of PL310 ·         Known issues o   For known issues and limitations please consult the release notes.
記事全体を表示
Setting up the clocks for PCIe is a bit tricky, especially for bare-metal or if not using the Linux BSP. The ENET PLL (PLL6) 100 MHz (SATA) PFD output MUST be enabled in order to access the registers in the PCIe IP block. (To enable this clock, set CCM_ANALOG_PLL_ENET[ENABLE_100M (bit 20)].) This is not well documented in the RM, but follow these steps to insure reliable performance.
記事全体を表示
Descriptions on the issue: running “uuu uuu-android-mx8mq-evk-emmc.lst” No any problem, downloading images is OK. running “uuu_imx_android_flash.bat -f imx8mq -a -e” Below lines will be showed on windows console: flash the file of u-boot-imx8mq.imx to the partition of bootloader0 <waiting for any devices>             Then downloading operation stopped. ------------------------------------------------------------------------                 In order to help uses save development time, I tested above 2 commands for downloading images on windows 7 64bit and windows 10 64bit respectively.                 Below is detailed steps for the operation: Hardware Preparations (1) Switch SW802 on i.MX8MQ EMEK, set 1-4 off, 2-3 on i.MX8MQ is at usb serial download mode. (2) Connecting J1701 to PC USB by a USB OTG cable. (3) Connecting J901(usb type c) to PC USB by a USB 3.0 cable. (4) Plugging [email protected] adapter into Power Jack (J902) (5) Power on I.MX8MQ board via SW701 Switch Software Preparations (1) Related windows drivers for i.MX8MQ MEK                 Windows 7 64bit or windows 10 64bit will find new devices and begin to search and install corresponding drivers, like below:                 Probably windows 10 64bit can’t automatically install CP2105 driver from official website of manufacture: https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers                 Then installed it manually. (2) Power off i.MX8MQ MEK (3) Installing winusb driver by zadig                 According to method described in uuu.pdf, download zadig tool from https://zadig.akeo.ie/, and install it to windows 7 64bit . [Note] windows 10 64bit doesn’t need to install winusb driver. Press “Install WCID Driver” Button (4) Downloading Android SDK Manager Download SDK Manager from : http://visualgdb.com/android/install_redir?item=SDK After downloading it, decompress it, and run SDK Manager application: Press OK. Then press “Close” Close SDK Manager Installation Guide . Find the directory of SDK Manager installation, and enter into “platform-tools”, like below: D:\i.MX8-Projects\IMX8MQ-MEK-windows-drivers\android-sdk_r24.4.1-windows\android-sdk-windows\platform-tools Copy items in blue rectangle to C:\windows\system Copy items in red rectangle to C:\windows\system32     Beginning to download android images to I.MX8MQ MEK via UUU Tool (1) Downloading android DEMO images for i.MX8MQ MEK https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK?tab=Design_Tools_Tab After downloading it, decompress it to a directory.  Like below: (2) Downloading UUU Tool https://github.com/NXPmicro/mfgtools/releases After downloading uuu.exe,  copy it to the directory of android 9.0 demo image , see above. (3) Run command “uuu_imx_android_flash.bat -f imx8mq -a -e” ----Power on i.MX8MQ MEK. ----open a command line window ---open Hyper terminal ( set it 115200 bps) ---run “uuu_imx_android_flash.bat -f imx8mq -a -e”           For windows 10 64bit, downloading images will be done without any errors.    But for windows 7 64bit, downloading images will stop at “ waiting for any devices”.    It means Android ADB driver will be needed. Follow the steps below to solve the problem. Right button, click “update driver” Close it.           Then downloading operations will be automatically continued. OK, done. NXP TIC team Weidong Sun 02-25-2019
記事全体を表示
Quick guide on how to get started with Linux on i.MX 6UL EVK board using MfgTool from L3.14.52 release: Download MfgTool from here (Version is IMX6_L3.14.52_MFG_TOOL (REV L3.14.52_1.1.0) under “Programmers (Flash, etc.)”): http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6ultralite-processor-low-power-secure-arm-cortex-a7-core:i.MX6UL?fpsp=1&tab=Design_Tools_Tab Unpack the archive and unpack mfgtools-with-rootfs.tar.gz edit cfg.ini and change following entries: mmc needs to be set to 1 6uluboot needs to be set to evk 6uldtb needs to be set to 14x14-evk Connect USB cable, USB debug cable to your PC.Open terminal to serial port (115200, 8N1). Insert uSD card to the slot on i.MX 6UL CPU module Set boot switches on SW602 [2:1] to on:off Power on the board Start MfgTool2.exe. HID device should be detected. Press "Start" button. Downloading should start. Executed steps are visible in the debug terminal. When you see "Done" printed, downloading has succeeded. Set boot switches on SW602 [2:1] to off:on, SW601[4:1] TO off:on:off:on Reset i.MX 6UL EVK (or power off then on), and boot to Linux. In case of any error, inspect serial output on debug terminal to see what has gone wrong. This document was generated from the following discussion: Getting started with i.MX6UL EVK and MfgTool L3.14.52
記事全体を表示
According to EHSET_v1.01.pdf description (http://testusb.com/EHHS.html), the USB physical certification test are from 2 sides. One test case is PC running USB-IF HSET utility as being USB host to test the target board being USB device; the other case is target board acting as USB host to initate test signals to a test fixture. The principle of test modes supported are based on Vid/Pid pair  during enumration by host whoever takes. Apply the attached patch (I use r13.4.1 kernel_imx tree), then enable "FSL_USB_TEST_MODE" in kernel config, rebuild uImage to get the test modes support kernel.
記事全体を表示
The decommission of the git.freescale.com has caused some problems to BSPs dependent on packages stored in this repository. All contents on git.freescale.com have been moved to one of three locations: NXP · GitHub  (github.com/NXP) NXP Micro · GitHub  (github.com/NXPMicro) https://source.codeaurora.org/external/imx/   In the case of some older Android BSP this causes an error when fetching the imx-firmware packages originally stored in this repository. A workaround to this is to switch the original location to the new location. To do this we would need to manually create a build directory and initialize repo to locally load the manifest files and then make this change. Android BSP won’t require this workaround. Please note that this workaround only addresses this specific error that may show up when running the script included on the BSP release. We will be using the Oreo o8.0.0_1.0.0_ga BSP release as an example. Sources for this BSP can be found on the following link: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/android-os-for-i-mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab Documentation for this BSP can be found on the following link: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/android-os-for-i-mx-applications-processors:IMXANDROID?tab=Documentation_Tab    1) Initialize the repo. If you have tried running the imx_android_setup.sh script the android build directory should already have been created. If this is the case, please skip to the next step. If not, please create it either by running imx_android_setup.sh or manually with the following commands (using the android setup script is preferred): $ mkdir android_build Once inside the build directory, initialize the repo and then sync it: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest.git -b imx-android-oreo -m imx-o8.0.0_1.0.0_ga.xml $ repo sync   2) Find and edit the Android Manifest. Once inside the build directory after synching, enter the repo manifests directory by executing the following command while inside the android build directory $ cd .repo/manifests  And look for the corresponding Android manifest. In this case imx-o8.0.0_1.0.0_ga.xml Open this file in any text editor (use sudo if running in a directory which requires it) In this case we’ll exemplify with nano $nano imx-o8.0.0_1.0.0_ga.xml And change the git://git.freescale.com/proprietary/  to git://github.com/NXP/ Also the path for imx-firmware so the complete line goes from: <project path="vendor/nxp/imx-firmware" name="imx-firmware" remote="imx-proprietary" revision="87ba304b9efbb2e8dbdd54af4c087584fb259535" />‍‍‍ To the following: <project path="imx-firmware" name="imx-firmware" remote="imx-proprietary" revision="87ba304b9efbb2e8dbdd54af4c087584fb259535" />‍‍‍ The manifest should look like the following. Save the file with these changes.   Now you can run the imx_android_setup.sh build script successfully. Since the repo was already synced it won’t fetch the manifests again and the change we made will persist, which will allow to find the imx-firmware package on its new location.
記事全体を表示