i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
i.MX8M_DDR3L_register_programming_aid is created for DDR3L validation board.
記事全体を表示
Audio, from a file gst-launch filesrc location=test.wav ! wavparse ! mfw_mp3encoder ! filesink location=output.mp3 Audio Recording gst-launch alsasrc num-buffers=$NUMBER blocksize=$SIZE ! mfw_mp3encoder ! filesink location=output.mp3 # where #     duration = $NUMBER*$SIZE*8 / (samplerate *channel *bitwidth) # Example: 60 seconds recording # gst-launch alsasrc num-buffers=240 blocksize=44100 ! mfw_mp3encoder ! filesink location=output.mp3 # # To verify that is correct, do a normal audio playback gst-launch filesrc location=output.mp3 typefind=true ! beepdec ! audioconvert ! 'audio/x-raw-int,channels=2' ! alsasink Video, from a test source gst-launch videotestsrc ! queue ! vpuenc ! matroskamux ! filesink location=./test.avi Video, from a file gst-launch filesrc location=sample.yuv blocksize=$BLOCK_SIZE ! 'video/x-raw-yuv,format=(fourcc)I420, width=$WIDTH, height=$HEIGHT, framerate=(fraction)30/1' ! vpuenc codec=$CODEC ! matroskamux ! filesink location=output.mkv sync=false # where #     BLOCK_SIZE = WIDTH * HEIGHT * 1.5 #     CODEC = 0(MPEG4), 5(H263), 6(H264) or 12(MJPG). # # For example, encoding a CIF raw file gst-launch filesrc location=sample.yuv blocksize=152064 ! 'video/x-raw-yuv,format=(fourcc)I420, width=352, height=288, framerate=(fraction)30/1' ! vpuenc codec=0 ! matroskamux ! filesink location=sample.mkv sync=false Video, from Web camera # when the web cam is connected, the device node /dev/video0 should be present. In order to test the camera, without encoding gst-launch v4l2src ! mfw_v4lsink # in recording, run: # gst-launch v4l2src num-buffers=-1 ! queue max-size-buffers=2 ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false # # where sync=false indicates filesink to to use a clock sync # # In case a specific width/height is needed, just add the filter caps gst-launch v4l2src num-buffers=-1  ! 'video/x-raw-yuv,format=(fourcc)I420, width=352, height=288, framerate=(fraction)30/1' ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false # # In case you want to see in the screen what the camera is capturing, add a tee element # gst-launch v4l2src num-buffers=-1 ! tee name=t ! queue ! mfw_v4lsink t. ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false Video, from Parallel/MIPI camera # The camera driver needs to be loaded before executing the pipeline, refer to the BSP document to see which driver to load # MIPI (J5 port): modprobe ov5640_camera_mipi modprobe mxc_v4l2_capture   # Parallel (J9 port): modprobe ov5642_camera modprobe mxc_v4l2_capture   gst-launch mfw_v4lsrc ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false   # Do a 'gst-inspect mfw_v4lsrc' or 'gst-inspect vpuenc' to see other possible settings (resolution, fps, codec, etc.)
記事全体を表示
That Python script exercises the i.MX serial download protocol in UART mode. It can be used with i.MX21/27/25/31/35/51/53, since they are based on the same protocol. The details on the protocol can be found in the "System Boot" section of the used i.MX reference manual. Requirements: - Python 2.7 (not tested with other version) - Pyserial modules (http://pyserial.sourceforge.net) The i.MX must boot in serial mode with a serial cable connected to a host running the script. The COM1 is configured in 115200 - no parity - 1 stop bit - 8-bit. If another COM is used, you will have to make the appropriate changes in the script. That script uses only hexa formatted address and data for the command parameters. The following command returns the HAB status whenever it is used, so it helps to check that the setup is functional. Eventually, when some code was downloaded, this command triggers its execution. The returned value is only useful when doing a secure boot, and does not matter otherwise. By default, it returns in hexa format the following: > iMX_Serial_Download_Protocol.py get_status Status is: F0 F0 F0 F0 Typical usage to download and execute some code: 1. Ensure that the protocol is ready: > iMX_Serial_Download_Protocol.py get_status 2. Configure the memories and other things like I/O, such does the DCD: > iMX_Serial_Download_Protocol.py write_mem memory_address access_size data As this configures only one register at a time, it is necessary to call it several times to configure like a SDRAM. Of course, feel free to enhance that script by adding like a load from file memory write 🙂 3. Download the executable binary: > iMX_Serial_Download_Protocol.py write_file memory_address file memory_address is necessary a valid address from the i.MX memory map, meaning that it must be a directly accessible memory area by the ARM core (registers, RAM). 4. Run the executable by jumping from ROM code to this loaded code: > iMX_Serial_Download_Protocol.py get_status This must returns: 88 88 88 88, which signifies that the ROM has successfully jumped at the entry point of the executable. That entry point must be specified in the flash header or Image Vector Table (IVT) depending of the i.MX. As a consequence, a valid flash header or IVT must be placed at the offset 0x0 of the downloaded code. In each boot image, this is commonly placed at the offset 0x400, so it is easy to build another one at offset 0x0 which is usually an empty space. Pointer to DCD should remain null. The script is provided "as is" without any warranty, and is not an official tool supported by Freescale. The script is here: 19-iMX_Serial_Download_Protocol.py
記事全体を表示
This link contains the scripts, U-boot commands, and patch code shown on the application note AN5409 titled 'i.MX6 Dual/6 Quad Power Consumption Measurement'.
記事全体を表示
One of the most important features of Yocto is its ability to handle sublayers. To understand the sublayers please Yocto Project Development Manual Start creating meta-custom folder, then create the other folders. For example: meta-daiane/ ├── conf │   └── layer.conf ├── README ├── recipes-core │   └── helloworld │       ├── helloworld │       │   └── hello_world.c │       └── helloworld_0.0.bb └── recipes-daiane     └── images         └── dai-image-hello.bb It´s possible to create recipes-kernel and place there your defconfig, or create a bbappend to apply your patches to kernel, or even create a recipes-multimedia and place there custom application for gstreamer, for example. Here, the custom application example is a helloworld application. One important tip: Yocto see recipes name as PACKAGENAME_VERSION.bb, It means, yocto uses "_" (underline) to separate the package name from package version on a recipe file name. So, if you call your helloworld application as hello_world_1.0.bb Yocto will think your application is called "hello" and the version is something around "world_1.0" Please, be careful. LAYER.CONF This is the file that gives new layer live. Find the content of mine layer.conf below: # We have a conf and classes directory, add to BBPATH BBPATH .= ":${LAYERDIR}" # We have a packages directory, add to BBFILES BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \             ${LAYERDIR}/recipes-*/*/*.bbappend" BBFILE_COLLECTIONS += "daiane" BBFILE_PATTERN_daiane := "^${LAYERDIR}/" BBFILE_PRIORITY_daiane = "4" As soon as the new custom layer is created, it MUST include it to  conf/bblayers.conf file. Please see the example: LCONF_VERSION = "6" BBPATH = "${TOPDIR}" BSPDIR := "${@os.path.abspath(os.path.dirname(d.getVar('FILE', True)) + '/../..')}" BBFILES ?= "" BBLAYERS = " \   ${BSPDIR}/sources/poky/meta \   ${BSPDIR}/sources/poky/meta-yocto \   \   ${BSPDIR}/sources/meta-openembedded/meta-oe \   \   ${BSPDIR}/sources/meta-fsl-arm \   ${BSPDIR}/sources/meta-fsl-arm-extra \   ${BSPDIR}/sources/meta-fsl-demos \   \   ${BSPDIR}/sources/meta-daiane \ " Please, find the tarball with sample meta layer attached to this document. It includes one image that will install the Hello World application: $ bitbake dai-image-hello When the content of image tar ball is extracted, hello_world was installed and it was for ARM: $ find -name hello* ./usr/bin/hello_world $ file ./usr/bin/hello_world ./usr/bin/hello_world: ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.16, stripped Go to Yocto Training - HOME Go to Task #9 - How to add bad/ugly
記事全体を表示
Issue Description When WM8960 is working as master mode and target sample rate is 44100Hz or 48000Hz, it's found no sound can be heard on some i.MX boards. Impact Software Baseline: Linux 4.1.15_2.0.0 release or previous versions. Impact Hardware Platform: MCIMX6UL-EVKB, MCIMX6ULL-EVK and MX7SABRE boards which have WM8960 as Audio Codec. Root Cause When WM8960 is working as master mode, if input MCLK is 12.288MHz and configure "PLLPRESCALE =2 and SYSCLKDIV[1:0] =1", wrong BCLK and LRCLK output maybe got on some boards. And then it causes no sound output. Solutions After change the WM8960 PLL setting from “PLLPRESCALE =2 and SYSCLKDIV[1:0] =1” to “PLLPRESCALE =1 and SYSCLKDIV[1:0] =2”, the failure parts can work normally. See attached patch. The formal patch is also included into the releases starting from L4.1.15_2.0.1. See http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/meta-bsp/recipes-kernel/linux/files?id=imx_4.1.15_2.0.1
記事全体を表示
In traditional file system, the WinCE image is a signal file “NK.NB0”/”NK.BIN”. And when using NAND flash for storage, since it can’t support XIP, the total “NK.NB0” need be copied into RAM before running. The EBOOT will do this copy. In this way, there are two main shortages: Long boot time and big size RAM requirement. If the WinCE image is big (Included more features), these issues will be critical. The BINFS can fix those two issues fine. It gave the chance to use 32MB RAM run 64MB WinCE image, this can cost down the final products. In BINFS file system, the final WinCE image will be divided into multi-BIN files, and only the XIPKERNEL BIN (Less than 7 MB) need be copied into RAM by EBOOT. The files in other BIN will work with demand paging mode. These files will be loaded into RAM only when they need run.
記事全体を表示
Please find attached preliminary errata on the two i.MX security vulnerabilities: ERR010872 – Secure Boot Vulnerability when using the Serial Downloader (CVE-2017-7936) ERR010873 – Secure Boot Vulnerability when Authenticating a Certificate (CVE-2017-7932) These are preliminary versions of the errata. Final versions will be incorporated into the Chip Errata (CE) document for each impacted device at a later date. Customer Notification A Customer Information Notification(CIN 201704026I) with the affected part numbers has been sent out to impacted users. Updated Silicon Sample Availability An Advanced Product Change Notification (A-PCN 201705010A), that provides updated silicon availability information has also been sent out to impacted users. Mitigations An Engineering Bulletin (EB00854) on possible mitigation strategies is available to impacted users and can be requested through your NXP field support team or distributor.  Further Questions or Support Please contact your NXP support representative or enter a support request for further questions on this topic indicating the part number and the mass production start date.
記事全体を表示
The Linux L4.9.88_2.0.0 Rocko, i.MX7ULP Linux/SDK2.4 RFP(GA) release files are now available. Linux on IMX_SW web page, Overview -> BSP Updates and Releases ->Linux L4.9.88_2.0.0 SDK on https://mcuxpresso.nxp.com/ web page.   Files available: Linux:  # Name Description 1 imx-yocto-L4.9.88_2.0.0.tar.gz L4.9.88_2.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 L4.9.88_2.0.0_images_MX6QPDLSOLOX.tar.gz i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6Solox Linux Binary Demo Files 3 L4.9.88_2.0.0_images_MX6SLEVK.tar.gz i.MX 6Sololite EVK Linux Binary Demo Files 4 L4.9.88_2.0.0_images_MX6UL7D.tar.gz i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 L4.9.88_2.0.0_images_MX6SLLEVK.tar.gz i.MX 6SLL EVK Linux Binary Demo Files 6 L4.9.88_2.0.0_images_MX8MQ.tar.gz i.MX 8MQuad EVK Linux Binary Demo files 7 L4.9.88_images_MX7ULPEVK.tar.gz i.MX 7ULP EVK Linux Binary Demo Files  8 L4.9.88_2.0.0-ga_mfg-tools.tar.gz Manufacturing Toolkit for Linux L4.9.88_2.0.0 iMX6,7 BSP 9 L4.9.88_2.0.0_mfg-tool_MX8MQ.tar.gz Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX8MQ BSP 10 imx-aacpcodec-4.3.5.tar.gz Linux AAC Plus Codec for L4.9.88_2.0.0   SDK:   On https://mcuxpresso.nxp.com/, click the Select Development Board to customize the SDK based on your configuration then download the SDK package.    Target board: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6QuadPlus SABRE-AI Board i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board i.MX 6SoloLite EVK Board i.MX 6SoloX SABRE-SD Board i.MX 6SoloX SABRE-AI Board i.MX 7Dual SABRE-SD Board i.MX 6UltraLite EVK Board i.MX 6ULL EVK Board i.MX 6SLL EVK Board i.MX 7ULP EVK Board i.MX 8MQ EVK Board   What’s New/Features: Please consult the Release Notes.   Known issues For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-rocko ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-rocko
記事全体を表示
In many cases (test certain modules, first boot-ups, DDR is not available), writing bare-metal (SDK) code with runs on iRAM (OCRAM) is the only possible scenario. The first (attached) patch creates a new linker file with proper sections and the second includes a tiny app (it should be tiny, by definition) using the previous file. These are the steps to have the setup ready: 1. Dowload latest i.MX6 SDK (v1.1.0 is the latest when writing this document). 2. Let GIT take the control (git init; git add .; git commit -m '1st commit') 3. Apply patches (git am < patch1; git am < patch2 ) 4. Compile             # This example is intended for a mx6q sabreSD, revision C             $ ./tools/build_sdk -target=mx6dq \                                 -board=smart_device \                                 -board_rev=c \                                 -app=iram     5. SD Card Flashing & Running: 5.1. ELF file & U-boot:    # Output image is located on:                 #   elf=output/mx6dq/minimal/smart_device_rev_c/minimal.elf                 $ dd if=$elf \                      of=/dev/sdb \                      seek=2048 bs=512; sync                 # Boot your board with your favorite u-boot version, just make                 # sure the bootelf command is presnet                 > mmc dev Y                 > mmc read 0x10800000 0x800 XXX                 > bootelf 0x10800000                where Y is the SD device and XXX are the records seen when dd flashing.             5.2  BIN file:    # Output image is located on:                 #   bin=output/mx6dq/minimal/smart_device_rev_c/minimal.bin                 $ dd if=$bin \                      of=/dev/sdb \                      seek=2 skip=2 bs=512; sync                 # Place the SD into your board and power-on. NOTES: + The first patch was taken from the internal discussion MX6 SDK (PLATLIB): has anyone created a stripped down version that will run from internal RAM?
記事全体を表示
Hi, the document "how to create ubuntu hardfloat rootfs for imx6d/q" was shared by Junping Mao. https://community.freescale.com/docs/DOC-95387 Here, i build the OpenCV based on the ubuntu hardfloat rootfs for i.MX6Q sabre board. Details about building instruction pls refer to the attachment. Thanks! 
記事全体を表示
The following are a couple of recommendations for setting up a Host machine for building the Android Nougat 7.1.1_1.0.0 BSP. Some of these recommendations are not exclusive of the Nougat release and may help in other scenarios. These also apply to using Virtual Machines as Host. Installing Open JDK 8 on Ubuntu 14.04 As mentioned on the Android guide for Establishing a Build Environment (http://source.android.com/source/initializing.html) there are no available supported OpenJDK 8 packages for Ubuntu 14.04, which is the version recommended and tested on the Nougat Android BSP. An alternative is downloading the Ubuntu 15.04 Open JDK 8 packages and installing them manually, which can be done by following this procedure: Download the .deb packages for 64-bit architecture from archive.ubuntu.com: openjdk-8-jre-headless_8u45-b14-1_amd64.deb with SHA256 0f5aba8db39088283b51e00054813063173a4d8809f70033976f83e214ab56c0 http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jre-headless_8u45-b14-1_amd64.deb  openjdk-8-jre_8u45-b14-1_amd64.deb with SHA256 9ef76c4562d39432b69baf6c18f199707c5c56a5b4566847df908b7d74e15849 http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jre_8u45-b14-1_amd64.deb  openjdk-8-jdk_8u45-b14-1_amd64.deb with SHA256 6e47215cf6205aa829e6a0a64985075bd29d1f428a4006a80c9db371c2fc3c4c http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jdk_8u45-b14-1_amd64.deb  Once you have downloaded these three packages and checked the checksum for them install the packages (optional) install them by running: $ sudo apt-get update $ sudo dpkg -i openjdk-8-jre-headless_8u45-b14-1_amd64.deb $ sudo dpkg -i openjdk-8-jre_8u45-b14-1_amd64.deb $ sudo dpkg -i openjdk-8-jdk_8u45-b14-1_amd64.deb‍‍‍‍   Increasing SWAP to compensate for the lack of RAM Having insufficient RAM especially on the linking part of the image build may cause a number of issues that are difficult to troubleshoot. In these cases it’s good to take a look at the resource monitor to see if indeed the RAM was depleted. One way to make up for the limited RAM is using a bigger swap. Google recommends at least 16GB of RAM/swap so it’s not uncommon to create a 10GB swap when working in VM, to do this please use the following commands.    $ sudo fallocate -l 10g /mnt/10GB.swap $ sudo chmod 600 /mnt/10GB.swap $ sudo mkswap /mnt/10GB.swap $ sudo swapon /mnt/10GB.swap‍‍‍‍   Increasing heap size to avoid out of memory errors It is possible to encounter an out of memory error with the recommendation “try increasing heap size witj java option ‘-Xmx<size>’. If you encounter this error or would like to proactively avoid it you may run the following commands that will increase heap size to four gigabytes and then reset the Jack Server by killing it and starting it again. With the android environment initialized: $ cd my android $ export JACK_SERVER_VM_ARGUMENTS="-Dfile.encoding=UTF-8 -XX:+TieredCompilation -Xmx4g" $ jack-admin kill-server && jack-admin start-server‍‍‍‍‍‍  Fixing Jack Servers errors due to multiple users on the Host Android Nougat uses Jack Server as mono-user by default. If this is not the case for your host you would need to choose different port numbers for each user and adjust SERVER_NB_COMPILE accordingly. You can also disable the Jack server by setting SERVER=false in your $HOME/.jack. Alternatively, you may also use the patch available on the following link to myandroid/prebuilts/sdk. It will help to fix the mono-user build restriction. When installing the jack-server, it will detect if Jack server is running in the same build machine and then generate a random ports for my build instead of using the default one. https://groups.google.com/forum/#!topic/android-building/UWhJrXH8Vig
記事全体を表示
In an earlier topic (Linux fast boot on i.MX6 Sabresd board.) about Linux fast boot on i.MX6 SabreSD board, the demo showed an application startup procedure including u-boot boot, Linux kernel boot, rootfs mount, demo application load and run. Additionally, this demo shows a live video on a LVDS screen from board CSI camera. Its total boot up time is about 1.x seconds. Now, based on Linux fast boot, we integrate it with another demo application: surround view, this demo shows 4 different live videos on LVDS screen from 4 UDP data sockets. In this demo video is drawn by GPU to screen, that means the frame buffers decode by video decoder directly pass to GPU, which is not same as previous demo. The encode video format is also MJPEG in this demo. This demo creates 4 different threads every thread handle one UDP socket, receive buffer, push this buffer to video decoder, get frame buffer from video decoder, pass this buffer to GPU, start GPU render, command GPU draw the render buffer to the screen; this thread needs to occupy one ARM processor to show every video smoothly. So we need a i.MX 6DQ board in this demo. Hardware: i.MX 6DQ SabreSD board Software: 12.09 GA BSP Difference with previous fast boot demo: U-boot difference with previous fast boot demo. 1: Add logo show. (For remove CSI2, V4L2, Capture modules ) Kernel different with previous fast boot demo. 1: Add SMP support. 2: Add Network support. (IPV4, PHY, network driver(FEC)) 3: Remove CSI2, V4L2, Capture. (Remove this need in U-boot procedure Freescale logo show on the screen! ) 4: Add GPU support in kernel. Rootfs difference with previous fast boot demo: 1: Keep rc.s firstly run, while in previous fast boot demo, demo is the firstly running program on rootfs. 2: Get rid of almost all service in rc.conf just keep “mount /proc and /sys” service. Network performance on this demo Software : The default network receive buffer is about 128KB. This default size is too small for this demo; the demo application can't fetch receive buffer in time while kernel network stack will discard some UDP packets if we don't enlarge it. We enlarge this receive buffer through command in inittab before demo running. Hardware: i.MX6 DQ TOI less than 1.2 version has some Ethernet mac layer issue, this issue will also cause some UDP packets lost. So please ensure the SabreSD board i.MX6 DQ chip TOI version is equal 1.2 or more. Attached are some files for your reference. Below patches assume this SabreSD board boot from SD3 and default display port is LVDS1. 1: U-boot and kernel patches based on 12.09. 2: Demo application based on 12.09 vpu test program and vpu test program running configure file. 3: Rootfs startup scripts.
記事全体を表示
    Gigabit Ethernet should be one of most beautiful features in our imx6 platform which will bring more colorful dreams to many customers. But recently,many people responsed that there were great performance gaps between using Android and Linux. Now let me give an exploration here.     Same hardware, same kernel, different performance,why?     In linux, its data throughput can reach 400Mbps.In JB, it can only get to 200Mbps.     From the below info, we can see it should be related with frames dropping.      root@android:/ # busybox ifconfig eth0      eth0      Link encap:Ethernet  HWaddr 00:04:9F:02:6C:E1                inet addr:192.168.0.100  Bcast:192.168.0.255  Mask:255.255.255.0                inet6 addr: fe80::204:9fff:fe02:6ce1/64 Scope:Link                UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1                RX packets:7382672 errors:71828 dropped:789 overruns:71828 frame:71828                TX packets:4147006 errors:0 dropped:0 overruns:0 carrier:0                collisions:0 txqueuelen:1000                RX bytes:2568845018 (2.3 GiB)  TX bytes:284789020 (271.5 MiB)      In TCP stack, there are three buffers involved in iperf test case:tcp_mem; tcp_rmem; tcp_wmem.      All of them are described by three variables which will influence a lot for iperf test result.      In linux,I got a snapshot for them:      root@sabresd_6dq:/# cat /proc/sys/net/ipv4/tcp_mem      18240      24320     36480      root@sabresd_6dq:/# cat /proc/sys/net/ipv4/tcp_rmem      4096       87380     778240      root@sabresd_6dq:/# cat /proc/sys/net/ipv4/tcp_wmem      4096       16384     778240      In Android,I also got them to compare to:      root@sabresd_6dq:/# cat /proc/sys/net/ipv4/tcp_mem      9285      12380     18570      root@sabresd_6dq:/# cat /proc/sys/net/ipv4/tcp_rmem      4096       87380     396160      root@sabresd_6dq:/# cat /proc/sys/net/ipv4/tcp_wmem      4096       16384     396160      The tcp_mem varibles define how the TCP stack should behave in kernel memory management.The first value tells the kernel the low threshold. The second value tells the kernel at which point to start pressuing memory usage down. The third one tells the kernel how many memory pages it may use maximally. If it is reached,TCP streams and packets start geting dropped until to a safe level.      In tcp_rmem, the first value defines the minimum receive buffer for each TCP connection and this buffer is always allocated to a TCP socket.The second one defines the default receive buffer size. The third one specifies the maximum receive buffer that can be allocated for a TCP socket.      In tcp_wmem, three varibles also be given to describle the TCP send buffer for each TCP socket.      We can check how these values come from in kernel code.There is an algorithm in kernel_imx/net/ipv4/sysctl_net_ipv4.c +450.     limit = nr_free_buffer_pages() / 8;     limit = max(limit, 128UL);     sysctl_tcp_mem[0] = limit / 4 * 3;     sysctl_tcp_mem[1] = limit;     sysctl_tcp_mem[2] = sysctl_tcp_mem[0] * 2;     /* Set per-socket limits to no more than 1/128 the pressure threshold */     limit = ((unsigned long)sysctl_tcp_mem[1]) << (PAGE_SHIFT - 7);     max_wshare = min(4UL*1024*1024, limit);     max_rshare = min(6UL*1024*1024, limit);     sysctl_tcp_wmem[0] = SK_MEM_QUANTUM;     sysctl_tcp_wmem[1] = 16*1024;     sysctl_tcp_wmem[2] = max(64*1024, max_wshare);     sysctl_tcp_rmem[0] = SK_MEM_QUANTUM;     sysctl_tcp_rmem[1] = 87380;     sysctl_tcp_rmem[2] = max(87380, max_rshare);      From the above algorithm, we can see tcp_mem,tcp_wmem[2],tcp_rmem[2] all related with nr_free_buffer_pages() which stands for amount of free RAM allocatable within ZONE_DMA and ZONE_NORMAL.      So here, we can find the root cause of performance gap between Android and Linux. There is big gaps in free RAM while running different OS. In fact, in android, Google has introduced one mechanism to tune these values through propertity. Now we are using default AOSP's values, you can refer to them in device/fsl/imx6/etc/init.rc.For wifi and Ethernet, they are both using net.tcp.buffersize.wifi. # Define TCP buffer sizes for various networks #   ReadMin, ReadInitial, ReadMax, WriteMin, WriteInitial, WriteMax,     setprop net.tcp.buffersize.default 4096,87380,110208,4096,16384,110208     setprop net.tcp.buffersize.wifi    524288,1048576,2097152,262144,524288,1048576     setprop net.tcp.buffersize.lte     524288,1048576,2097152,262144,524288,1048576     setprop net.tcp.buffersize.umts    4094,87380,110208,4096,16384,110208     setprop net.tcp.buffersize.hspa    4094,87380,262144,4096,16384,262144     setprop net.tcp.buffersize.hsupa   4094,87380,262144,4096,16384,262144     setprop net.tcp.buffersize.hsdpa   4094,87380,262144,4096,16384,262144     setprop net.tcp.buffersize.hspap   4094,87380,1220608,4096,16384,1220608     setprop net.tcp.buffersize.edge    4093,26280,35040,4096,16384,35040     setprop net.tcp.buffersize.gprs    4092,8760,11680,4096,8760,11680     setprop net.tcp.buffersize.evdo    4094,87380,262144,4096,16384,262144 I tried to change the above values but unfortunately got no obvious improvement.Hi,why???? so another topic,how tcp_mem and tcp_rmem cowork in kernel? In android, we only have way to tuning tcp_rmem or tcp_wmem settings but not tc_mem. Take "iperf -c" for example, tcp_rmem will be filled up according to the frequency of Gigabit ethernet clock. And then it will be repacked acoording to the size of tcp_mem.If tcp_mem is smaller, more times will be triggered and if it has exceeds the max value dropping frames will be triggered. Then retransport will be launched in TCP. At last, performance will downgrade. It is just like go surfing using Gigabit but with a rubbish notebook. You still can't enjoy good performance of Gigabit ethernet. Why kernel calculate tcp_mem like this in ipv4? Maybe they consider the balance between single high-bandwidth and multiple connections. You can imagine if we change the tcp_mem to use a solid big value, it may cause the board deny connections because of a lack of memory allocation in tcp init. Here I will give out several method to improve our android ethernet performance. Enlarge your memory size in board design phase.      I have double checked it by testing in our SabreAuto board whose memory is 2G whose download speed can reach to 270 Mbps about 50Mbps over Sabresd. Try to use older version android, if you can use ICS, you can abandon JB4.3. Compared with newer android version, old version will take less memory and there will leave more free memory to use. Using ICS, we can reach 380 Mbps downloading while in JB4.3, it can only get to 210 Mbps. If you are using sabresd's Gigabit ethernet for a very important case, you can balance it if you can throw other memory eaters like GPU. I have checked it if we disable GPU, the performance can reached to 340 Mbps in JB4.3 with about 50% improvement. Change tcp_mem algorithm to enlarge its max value threshold. Like you can change  "sysctl_tcp_mem[2] = sysctl_tcp_mem[0] * 2" to "sysctl_tcp_mem[2] = sysctl_tcp_mem[0] * 3" above. You can see there won't be framedropping any more. Or you can also refer to How To: Network / TCP / UDP Tuning to hard code it. But like its author said in it, it is not recommended for those support multiple users or multiple connections. for it maybe cause the board to deny connections because of a lack of memory allocation. Tune tcp_rmem and tcp_wmem through the following patches in android. you will get bidirectional 320Mbps. But if you use ifconfig tool to set static ip you will not get these parameters set. For AOSP's framework only support DHCP now. For this case, you can manually echo these parameters in console before doing test.                Gerrit Code Review                Gerrit Code Review Change kernel's scheduler policy config.      Disable CONFIG_FAIR_GROUP_SCHED and only enable CONFIG_RT_GROUP_SCHED will contribute some enhancement.      With the above changes, I have tested on Sabresd RevC1 using android4.3GA, the bidirection speed can both reach 390~400Mbps.
記事全体を表示
    On latest iMX8QXP MEK board, the hardware connected the SCU_GPIO0_00 and SCU_GPIO0_01 pins for SCU debug UART, and customer can enable "#define ALT_DEBUG_SCU_UART" from "imx-scfw-porting-kit-1.1/src/scfw_export_mx8qx_b0/platform/board/mx8qx_mek/board.c" to open the SCFW debug UART for early board bring up.     And if customer enabled "#define ALT_DEBUG_UART" from board.c, then SCFW will use ADC_IN2 and ADC_IN3 pins for debug UART.     In this document, it is another choice, SCFW can also use UART0_RX and UART0_TX pins as SCU debug UART for early board bring up. It is based on released "imx-scfw-porting-kit-1.1.tar.gz".     That means on early MEK boards and customer boards which haven't reserved debug UART for SCU, they can also check the SCFW boot log from UART0 port. "scfw-porting-kit-1.1-sc_uart-on-uart0.patch" is the reference patch for such modification. Enable "#define ALT_DEBUG_SCU_UART_ON_UART0" to make it work. Note: since UART0 pins had been used in SCFW, they can't be used in UBoot and linux kernel at the same time, so when debuging UBoot and Linux kernel, you need disable "ALT_DEBUG_SCU_UART_ON_UART0" in SCFW, or you can use other UART port and pins.
記事全体を表示
The i.MX Android L5.1.1_2.1.0 GA release is now available on the Web Site.  (i.MX6 BSP Updates and Releases à Android) ·        Files available android_L5.1.1_2.1.0-ga_doc.tar.gz​​​ i.MX6 Android L5.1.1_2.1.0 BSP Documentation android_L5.1.1_2.1.0-ga_core_source.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite and i.MX6SX Android L5.1.1_2.1.0 BSP, Source Code for BSP and Codecs. android_L5.1.1_2.1.0-ga_images_6qsabreauto.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.1.1_2.1.0 BSP Binary Demo Files for the SABRE for Automotive Infotainment. android_L5.1.1_2.1.0-ga_images_6dqsabresd.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.1.1_2.1.0 BSP Binary Demo Files for the SABRE Platform and SABRE Board for Smart Devices. android_L5.1.1_2.1.0-ga_images_6slevk.tar.gz i.MX 6Sololite Android L5.1.1_2.1.0 BSP Binary Demo Files for the SoloLite evaluation kit. android_L5.1.1_2.1.0-ga_images_6sx.tar.gz i.MX 6SoloX Android L5.1.1_2.1.0 BSP Binary Demo Files. android_L5.1.1_2.1.0-ga_tools.tar.gz i.MX 6 Family Manufacturing Toolkit for L5.1.1_2.1.0 ·        Supported Hardware SoC/Boards: o  i.MX 6Quad SABRE-SD board and platform o  i.MX 6DualLite SABRE-SD platform o  i.MX 6Quad SABRE-AI board and platform o  i.MX 6QuadPlus SABRE-AI board and platform o  i.MX 6DualLite SABRE-AI board and platform o  i.MX 6SoloLite EVK platform o  i.MX 6SoloX SABRE-SD board o  i.MX 6SoloX SABRE-AI board and platform o  i.MX 7Dual SABRE-SD board and platform ·        Change List Compared to the L5.1.1_2.0.0_6qp-ga release, this release has the following major changes: o  Upgraded the Linux kernel version from the L3.14.38_6qp-ga release to the L3.14.52-ga release. o  Added i.MX 6QuadPlus SABRE-SD board support. o  Enabled Broadcom BCM4339 Wi-Fi and Bluetooth module. o  Fixed screen tearing in recovery mode during factory resetting and OTA upgrading. o  Fixed system hang-up issue when playing some short videos for a long time. o  Moved all Freescale extended API to freescale-extended.jar. o  Enabled the ZRAM function for Android platform to enlarge the memory size. o  Integrated 2015-11 AOSP Security patches. ·        Features For features please consult the release notes. ·        Known issues For known issues and more details please consult the release notes.
記事全体を表示
Before reading: only a personal works and sharing, not any form of "release". I didn't find any confidential information from the packages. So, I'm publishing it here. This is only for testing purpose. Do NOT use it for building a product. Use it at your own risk!! Yocto is flexible and powerful, and also, big and slow (when building). Sometimes we only need to build uboot or kernel or some piece of testing code. It's really a waste of time to build-up the whole Yocto environment which may cost over 50GB disk space and over 3 hours of building. I've made some scripts and sum them up to form a toolset for building uboot, kernel and some testing code out of Yocto environment. It's only a simple container and expect to use with uboot and kernel source code from formal Freescale release and a SDK built from Yocto project. GitHub source repo:       https://github.com/gopise/gopbuild What’s made off (a full package, not only the container): 1.    Some scripts and configurations files. 2.    SDK built from Yocto. 3.    Uboot/kernel from specific version. 4.    A hello-world to demonstrate how to build app in this environment. 5.    A slimmed rootfs binary from specific BSP pre-built as base. Will customize base on the source under “rootfs” folder. Only a placeholder in the container-only version. How to use it: Several common used board configurations have been included in the script: 6qsabresd/6qsabreai/6qpsabreai. You can add more into the “gopbuild” script easily. The “sabresd” has been set as default.      If you want to build all for sabresd (First of all, de-compress the package): cd <de-compressed-folder> source envsetup [It will prompt for selecting board configuration to be built. Choose one by input corresponding number or click <ENTER> for default board.] gmk ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍      If you want to build specific module for default board, such as uboot: gmk uboot ‍‍‍‍‍‍‍‍‍      Build kernel for sabreai board instead of default device: gmk kernel sabreai ‍‍‍‍‍‍‍‍‍      Clean everything? gmk all clean ‍‍‍‍‍‍‍‍‍ After a successfully full build, you will get everything under “output” folder, including a log folder contains full build log:      “u-boot.imx/zImage/rootfs.tar.bz2/*.dtb”, can be used with MFG or uuu.      “fsl-image.sdcard”, can be burn into SD card directly. "Ready-for-building" Package: The "gopbuild" itself is a "container-only" package which doesn't contain any source or SDK. I've also made some packages based on latest BSP release for i.MX6/i.MX7/i.MX8. These packages are "ready-for-build" package which you can de-compress and build it directly. -------------------------------------------------------------------------------------------------- URL:https://pan.baidu.com/s/1Xlh1OBGsTRXez_NQw-Rjxg Password: gdc9 -------------------------------------------------------------------------------------------------- Note: 1. To build for i.MX8 (8QM/8MQ/8QXP), you need L4.14.* or above. 2. To build for i.MX8, please download the SCFW from i.MX software page       i.MX Software and Development Tools | NXP      After download, decompress corresponding package for specific chip and put it under "/platform/scfw/". Take i.MX8QXP for example:             /platform/scfw/scfw_export_mx8qx/ All material (uboot/kernel/test code and SDK) are from official Yocto release. Thanks!
記事全体を表示
THE CONTENTS •Background Knowledge −Bootloader Introduction −U-boot Directory Structure of the Source Code •Bootloader Boot Procedure(e.g. U-boot) −i.MX6Q Introduction −Linux OS Boot Process −First Stage of Boot Sequence(Assembly Language) −Second Stage of Boot Sequence(Assembly + C Language)
記事全体を表示
Host Environment: ubuntu 16.04 LTS Linux BSP For i.MX : version 4.9.88 The document has 5 main contents: 1. Compiling core-image-base in Yocto BSP --Copy u-boot source code to a new directory --Copy linux kernel source code to a new directory 2. Exporting 4.9.88 toolchain from Freescale Yocto BSP (1) Using MACHINE=imx7dsabresd to export the toolchain (2) Using MACHINE=imx6qsabresd to export the toolchain. Actually above 2 are the same toolchain after exporting. Here , only show any one of boards(not ARM64) can be used for MACHINE. So users only need to export it for one time, select (1) or (2) to export toolchain. (3) Using MACHINE=imx8mqevk to export ARM64 toolchain 3. Compling u-boot & linux kernel under Stanalone iMX7DSabreSD --Compiling  u-boot for imx7dsabresd --Compiling kernel and dtb for imx7dsabresd iMX8MQEVK --Compiling u-boot for imx8mqevk --Compiling kernel and dtb for imx8mqevk 4. Compiling OS Firmware for i.MX7DSabreSD board --u-boot for mfg tools --kernel and dtb for mfg tools 5. Copy OS Firmware to the related path of MFG tools --------------------------------------------------------------------------------------------------------------------------- [Content of Document] 1. Compiling core-image-base in Yocto BSP          After repo syn is done according to “i.MX_Yocto_Project_User's_Guide.pdf”, Use the command to compile linux BSP, u-boot & kernel source code will be released. # DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source fsl-setup-release.sh -b build-fb # bitbake core-image-base          After compiling is done, u-boot & linux kernel source code is in the path below: u-boot: ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git linux: ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/git          We can create a new directory for uboot and linux kernel source code. Here I created a directory named disk2. # cd ~/ # mkdir disk2 # cd disk2 # mkdir u-boot-2017-03 # mkdir linux-imx-4.9.88 --Copy u-boot source code to a new directory # cd ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git # cp –r ./* ~/disk2/u-boot-2017-03 --Copy linux kernel source code to a new directory # cd ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/git # cp –r ./* ~/disk2/ linux-imx-4.9.88 2. Exporting 4.9.88 toolchain from Freescale Yocto BSP (1) Using MACHINE=imx7dsabresd to export the toolchain Step1: # cd ~/imx-yocto-bsp/ # DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source fsl-setup-release.sh -b build-minimal … … Do you accept the EULA you just read? (y/n)  y EULA has been accepted. Welcome to Freescale Community BSP The Yocto Project has extensive documentation about OE including a reference manual which can be found at:     http://yoctoproject.org/documentation For more information about OpenEmbedded see their website:     http://www.openembedded.org/ You can now run 'bitbake <target>' Common targets are:     core-image-minimal     meta-toolchain     meta-toolchain-sdk     adt-installer     meta-ide-support Your build environment has been configured with:     MACHINE=imx7dsabresd     SDKMACHINE=i686     DISTRO=fsl-imx-fb     EULA= BSPDIR= BUILD_DIR=. meta-freescale directory found Here “build-minimal” is a directory for compiling source code, users can also set it other name. In ~/imx-yocto-bsp/build-minimal, Begin to export toolchain with the command. Step2: # DISTRO=fsl-imx-fb MACHINE=imx7dsabresd bitbake core-image-minimal -c populate_sdk [Comment-1] About DISTRO and MACHINE on above 2 commands MACHINE can be set the values below. imx6qpsabreauto imx6qpsabresd imx6ulevk imx6ull14x14evk imx6ull9x9evk imx6dlsabreauto imx6dlsabresd imx6qsabreauto imx6qsabresd imx6slevk imx6solosabreauto imx6solosabresd imx6sxsabresd imx6sxsabreauto imx6sllevk imx7dsabresd imx7ulpevk imx8mqevk   So MACHINE’s value is the name each Evaluation Borad. DISTRO can be set the values below: fsl-imx-x11 - X11 graphics are not supported on i.MX 8. fsl-imx-wayland - Wayland weston graphics. fsl-imx-xwayland - Wayland graphics and X11. X11 applications using EGL are not supported. fsl-imx-fb - Frame Buffer graphics - no X11 or Wayland. Frame Buffer is not supported on i.MX 8 bitbake rootfs type       core-image-minimal       core-image-base       core-image-sato       fsl-image-machine-test       fsl-image-validation-imx       fsl-image-qt5-validation-imx Below is the detailed description for above rootfs type: [Comment-2] Descriptions on difference of toolchain between i.MX6/7 and i.MX8MQ          i.MX6 and i.MX7 are both 32bit ARM processor, they use the same toolchain.          i.MX8MQ is 64bit ARM processor, so it’s toolchain is different from that of i.MX6/7. Setp 3:          After above compiling is done, enter into ~/imx-yocto-bsp/build-minimal/tmp/deploy/sdk # cd ~/imx-yocto-bsp/build-minimal/tmp/deploy/sdk # ls Run .sh file: Then continue operations according to guidance: Done: OK, Let us check /opt/fsl-imx-fb/ directory: # ls /opt/fsl-imx-fb/4.9.88-2.0.0/          Because we used MACHINE=imx7dsabresd, environment was named “cortex-A7”, compiler’s version is still 4.9.88. (2) Using MACHINE=imx6qsabresd to export the toolchain.          We can change “MACHINE=imx6qsabresd” and repeat above 3 steps, environment will be named “cortex-A9”.          Close the current terminal, and open a new one. # cd ~/ imx-yocto-bsp # DISTRO=fsl-imx-fb MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-A9-min            Then automatically enter “~/imx-yocto-bsp/build-A9-min”, run command below. # DISTRO=fsl-imx-fb MACHINE=imx6qsabresd bitbake core-image-minimal -c populate_sdk # ~/imx-yocto-bsp/build-A9-min/tmp/deploy/sdk # ls # ./ fsl-imx-fb-glibc-x86_64-core-image-minimal-cortexa9hf-neon-toolchain-4.9.88-2.0.0.sh   Set it up in another directory: /opt/fsl-imx-fb/4.9.88 (3) Using MACHINE=imx8mqevk to export ARM64 toolchain          Export Toolchain for i.MX8MQ, create a new terminal, then run these 2 commands below. # ~/imx-yocto-bsp # DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-xwayland # DISTRO=fsl-imx-fb MACHINE=imx8mqevk bitbake core-image-minimal -c populate_sdk Done.          Copy the toolchain to /opt/fsl-imx-fb directory # cd ~/imx-yocto-bsp/build-xwayland/tmp/deploy/sdk # ls #./fsl-imx-fb-glibc-x86_64-core-image-minimal-aarch64-toolchain-4.9.88-2.0.0.sh          I installed it to a new directory: /opt/fsl-imx-fb/4.9.88-arm64 #ls ls /opt/fsl-imx-fb/4.9.88-arm64/  OK, 64bit toolchain for i.MX8MQ has been exported to the directory. 3. Compling u-boot & linux kernel under Stanalone iMX7DSabreSD --Compiling  u-boot for imx7dsabresd # cd ~/disk2/u-boot-2017-03 # source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa7hf-neon-poky-linux-gnueabi # export ARCH=arm # make clean # make mx7dsabresd_defconfig # make u-boot.imx Done. --Compiling kernel and dtb for imx7dsabresd # cd ~/disk2/linux-imx-4.9.88/ [comment] If environment has been configured, that is, these 2 commands have been run on the current terminal, don’t need to run them again. “source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa7hf-neon-poky-linux-gnueabi” and “export ARCH=arm” # make clean # make imx_v7_defconfig # make            zImage is in “~/disk2/linux-imx-4.9.88/arch/arm/boot”          dtb is in “~/disk2/linux-imx-4.9.88/arch/arm/boot/dts”            Probably users want to run “make menuconfig”, and meet the errors like below. # sudo apt-get install libncurses*  (To solve the problem below) # make menuconfig [Comment-3]  Users can also use "environment-setup-cortexa9hf-neon-poky-linux-gnueabi" to compile u-boot and kernel. iMX8MQEVK --Compiling u-boot for imx8mqevk # cd ~/disk2/u-boot-2017-03 # source /opt/fsl-imx-fb/4.9.88-arm64/environment-setup-aarch64-poky-linux # export ARCH=arm64 # make clean # make imx8mq_evk_defconfig # make u-boot.imx Done. --Compiling kernel and dtb for imx8mqevk # cd ~/disk2/linux-imx-4.9.88/ [comment] If environment has been configured, that is, these 2 commands have been run on the current terminal, don’t need to run them again. “source /opt/fsl-imx-fb/4.9.88-arm64/environment-setup-aarch64-poky-linux” and “export ARCH=arm64” # make clean # make defconfig # make          Run the command to unset LDFLAGS: # unset LDFLAGS # make Done. 4. Compiling OS Firmware for i.MX7DSabreSD board --u-boot for mfg tools # make mx7dsabresd_config # make u-boot.imx          Then rename u-boot.imx to be “u-boot-mx7dsabresd-mfg.imx”. --kernel and dtb for mfg tools          Copy imx_v7_mfg_defconfig file to “arch/arm/configs”, then run commands below. # make imx_v7_mfg_defconfig # make          zImage will be generated at path arch/arm/boot.          dtb file will be generated at path arch/arm/boot/dts            Then rename zImage to be zImage-mx7dsabre-mfg,          Rename imx7d-sdb.dtb to be zImage-imx7d-sdb-mfg.dtb 5. Copy OS Firmware to the related path of MFG tools          Up to now, 3 files for OS Firmware has been generated, then copy these 3 files to mfgtools\Profiles\Linux\OS Firmware\firmware            When MFG Tools begins to run, these 3 files and ramdisk will be downloaded to SDRAM on board, then run them, and download images(u-boot\kernel\rootfs\)  which have been ready in  “mfgtools\Profiles\Linux\OS Firmware\files”.            Above steps and commands will be performed according to list in ucl2.xml. So customer will add a new list for her downloading or change an existing list according to image’s name. NXP TIC team Weidong Sun 04-25-2019
記事全体を表示
If you want to use a USB camera (these types of cameras are also called 'Web Cameras') with GStreamer on i.MX6 devices (Linux Kernel version >= 3.035), you need to either load the module dynamically or compile and link statically selecting (Y) the following config on the Kernel configuration      Device Drivers -> Multimedia support -> Video capture adapters -> V4L USB devices -> <*> USB Video Class (UVC) After the Kernel image has been built, flash it into the target, plug the web cam, then on a (target) terminal run      gst-launch v4l2src ! mfw_v4lsink You should see what the camera is capturing on the display. In case you need to encode the camera src data, you need to place the encoder into the pipeline      gst-launch v4l2src num-buffers=100  ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false We are using a certain codec (codec=0 means mpeg4), check options using 'gst-inspect vpuenc'.
記事全体を表示