This is a copy of the currently posted i.MX 6DQ reference manual, revision 2, published Jun 2014. This is part 1 of 2, and includes the first 43 chapters. Go here for part 2: i.MX 6DQ Reference Manual (IMX6DQRM R2, Part 2)
This document is to be used to enter community comments. Please feel free to add inline comments in this reference manual. You can point out where more information is needed or where existing information is incorrect. You can also enter information in your comment that expands on existing information in the document, based on your experience with the device. If you are pointing out that more information is needed in a paragraph or a section, please be very specific, not “needs more information”. Your comments in this manual may help other members and will drive improvements in this and future documentation.
Note: The doc viewer does not support going directly to a specified page. Instead of manually paging through one page at a time, you can do a search on a string on a page such as "types of resets", or you can go to chapter links listed in the inline comments. To do this, page down to the comments below the doc view, select "Inline Comments", sort the comments by "page", and then select the chapter you want to view. You may find it easier to use this manual by downloading and viewing it in your local Adobe Reader. Then when you have a comment/question to add to this review copy, navigate to the chapter as described above and then do a search on the text for which you want to add a comment. This will take you to that page the quickest.