You already know. Your source code is one week old now, so please, update it!
$ repo sync
What was the changes? Please, read the output and determinate what file was changed.
Directory tree
This is what I have under fsl-community-bsp directory:
$ tree -d -L 2 -A
.
├── build_mx53
│ ├── conf
│ ├── sstate-cache
│ └── tmp
├── build_mx6
│ ├── conf
│ ├── sstate-cache
│ └── tmp
├── downloads
│ └── git2
└── sources
├── base
├── meta-fsl-arm
├── meta-fsl-arm-extra
├── meta-fsl-demos
├── meta-openembedded
└── poky
Sstate-cache keeps the pre-build packages cache so once one package is built, and it´s not changes, no need to re-build it again.
If a team shares the same build environment, the sstate-cache folder can be shared as well. I´m not personally used to configure it, so, please, follow the doc: Yocto Project Reference Manual
The downloads folder is shared for any build folder. It holds every package´s source code. For example, the ssh source code (and this source code can be built for any architecture)
In addition, you may want to share the download folder with your team (one download folder for the complete team), so please, go to Yocto Project Reference Manual and look for DL_DIR.
Build_mx6 tree
.../build_mx6$ tree -d -L 2 -A
.
├── conf
├── sstate-cache
└── tmp
├── buildstats
├── cache
├── deploy
├── log
├── pkgdata
├── sstate-control
├── stamps
├── sysroots
├── work
└── work-shared
Inside tmp folder you will find images and build results. Images is placed inside deploy.
Build statistics like initial and final time for each package/task are under buildstats
The complete log for any 'bitbake' you did is under log. Take a look, for example, on the file log/cooker/imx6qsabresd/11111111111.log. Please, notice that 111111111 is the PID number, so every time you run bitbake you have a different one.
The source code, the patches, and the logs for the last bitbake, for each package is under work. Take a look on the files under tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/ for example, for the kernel.
.../build_mx6$ tree -d -L 1 -A tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/
tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/
├── deploy-linux-imx
├── deploy-rpms
├── git
├── image
├── license-destdir
├── package
├── packages-split
├── pkgdata
├── pseudo
├── sysroot-destdir
└── temp
Go under temp, and see a lot of log.* and run.*:
.../build_mx6$ ls tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r37.14/temp/
log.do_bundle_initramfs log.do_uboot_mkimage run.do_package_write_rpm.28992 run.perform_packagecopy.16364
log.do_bundle_initramfs.28986 log.do_uboot_mkimage.2325 run.do_patch run.populate_packages.16364
log.do_compile log.do_unpack run.do_patch.2556 run.read_shlibdeps.16364
log.do_compile.3483 log.do_unpack.1155 run.do_populate_lic run.read_subpackage_metadata.28992
log.do_compile_kernelmodules log.task_order run.do_populate_lic.10988 run.split_and_strip_files.16364
log.do_compile_kernelmodules.29051 run.base_do_fetch.28859 run.do_populate_sysroot run.split_kernel_module_packages.16364
log.do_configure run.base_do_unpack.1155 run.do_populate_sysroot.17692 run.split_kernel_packages.16364
log.do_configure.3048 run.BUILDSPEC.28992 run.do_qa_configure.3048 run.sstate_create_package.10988
log.do_deploy run.debian_package_name_hook.16364 run.do_qa_staging.17692 run.sstate_create_package.16364
log.do_deploy.617 run.do_bundle_initramfs run.do_sizecheck run.sstate_create_package.17692
log.do_fetch run.do_bundle_initramfs.28986 run.do_sizecheck.2323 run.sstate_create_package.2724
log.do_fetch.28859 run.do_compile run.do_strip run.sstate_create_package.28992
log.do_install run.do_compile.3483 run.do_strip.2321 run.sstate_create_package.617
log.do_install.2327 run.do_compile_kernelmodules run.do_uboot_mkimage run.sstate_task_postfunc.10988
log.do_package run.do_compile_kernelmodules.29051 run.do_uboot_mkimage.2325 run.sstate_task_postfunc.16364
log.do_package.16364 run.do_configure run.do_unpack run.sstate_task_postfunc.17692
log.do_packagedata run.do_configure.3048 run.do_unpack.1155 run.sstate_task_postfunc.2724
log.do_packagedata.2724 run.do_deploy run.emit_pkgdata.16364 run.sstate_task_postfunc.28992
log.do_package_write_rpm run.do_deploy.617 run.fixup_perms.16364 run.sstate_task_postfunc.617
log.do_package_write_rpm.28992 run.do_fetch run.package_depchains.16364 run.sstate_task_prefunc.10988
log.do_patch run.do_fetch.28859 run.package_do_filedeps.16364 run.sstate_task_prefunc.16364
log.do_patch.2556 run.do_install run.package_do_pkgconfig.16364 run.sstate_task_prefunc.17692
log.do_populate_lic run.do_install.2327 run.package_do_shlibs.16364 run.sstate_task_prefunc.2724
log.do_populate_lic.10988 run.do_package run.package_do_split_locales.16364 run.sstate_task_prefunc.28992
log.do_populate_sysroot run.do_package.16364 run.package_fixsymlinks.16364 run.sstate_task_prefunc.617
log.do_populate_sysroot.17692 run.do_packagedata run.package_get_auto_pr.16364 run.sysroot_cleansstate.3048
log.do_sizecheck run.do_packagedata.2724 run.package_get_auto_pr.2327 run.sysroot_stage_all.17692
log.do_sizecheck.2323 run.do_package_qa.16364 run.package_get_auto_pr.617 run.write_specfile.28992
log.do_strip run.do_package_rpm.28992 run.package_name_hook.16364
log.do_strip.2321 run.do_package_write_rpm run.patch_do_patch.2556
For each package, you will be able to see the log for the latest task, and what was done on the latest task. For example:
log.do_compile - shows the log output from latest do_compile made for kernel
run.do_compile - shows the compile command line
log.do_compile.111111 - shows the log output from 1111111 time of do_compile
In order to know the tasks and the task sequence, take a look to log.taskorder file
For the images generated, you will find something like that:
.../build_mx6$ ls -la tmp/deploy/images/imx6qsabresd/
total 146260
drwxr-xr-x 2 user user 4096 Mar 6 21:21 .
drwxrwxr-x 3 user user 4096 Mar 6 21:12 ..
-rw-r--r-- 1 user user 67108864 Mar 6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.ext3
-rw-r--r-- 1 user user 83886080 Mar 6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.sdcard
-rw-r--r-- 1 user user 18782361 Mar 6 21:21 core-image-base-imx6qsabresd-20140306173758.rootfs.tar.bz2
lrwxrwxrwx 1 user user 55 Mar 6 21:21 core-image-base-imx6qsabresd.ext3 -> core-image-base-imx6qsabresd-20140306173758.rootfs.ext3
lrwxrwxrwx 1 user user 57 Mar 6 21:21 core-image-base-imx6qsabresd.sdcard -> core-image-base-imx6qsabresd-20140306173758.rootfs.sdcard
lrwxrwxrwx 1 user user 58 Mar 6 21:21 core-image-base-imx6qsabresd.tar.bz2 -> core-image-base-imx6qsabresd-20140306173758.rootfs.tar.bz2
-rw-rw-r-- 2 user user 439697 Mar 6 21:12 modules--3.0.35-r37.14-imx6qsabresd-20140306173758.tgz
lrwxrwxrwx 2 user user 54 Mar 6 21:12 modules-imx6qsabresd.tgz -> modules--3.0.35-r37.14-imx6qsabresd-20140306173758.tgz
-rw-rw-r-- 2 user user 294 Mar 6 21:20 README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt
lrwxrwxrwx 2 user user 35 Mar 6 21:16 u-boot.imx -> u-boot-imx6qsabresd-v2013.10-r0.imx
lrwxrwxrwx 2 user user 35 Mar 6 21:16 u-boot-imx6qsabresd.imx -> u-boot-imx6qsabresd-v2013.10-r0.imx
-rwxr-xr-x 2 user user 297984 Mar 6 21:16 u-boot-imx6qsabresd-v2013.10-r0.imx
lrwxrwxrwx 2 user user 53 Mar 6 21:12 uImage -> uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin
-rw-r--r-- 2 user user 4042496 Mar 6 21:12 uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin
lrwxrwxrwx 2 user user 53 Mar 6 21:12 uImage-imx6qsabresd.bin -> uImage--3.0.35-r37.14-imx6qsabresd-20140306173758.bin
You can access any generated image, the image name ending with the yearmothdaypid (long number) is the real image, and every time your bitbake complete, it generate a new image.
The symbolic link points to the latest created image.
The .ext3 file is the EXT3 image for the rootfs. (you can copy it directly to SD card using dd: $sudo dd if=core-image-base.ext3 of=/dev/sdb2 )
The .sdcard file is the complete image to be copied to sdcard. It´s u-boot+uImage+rootfs
The .tar.bz2 file is the tarball for the rootfs, you can extract it on your PC.
uImage is the latest kernel image
u-boot is the latest u-boot image.
and so on.
Play around with generated files. A lot of them I don´t know. And a lot of them I don´t use. For a standard image generation you only need to know where the final images is placed.
Any question, comment, issue, please let me know.
Before you go, let your bitbake creates the biggest image ever:
$ bitbake fsl-image-gui
Note (24Feb2014): Required disk space for build image is ~44GB
Start it and let it finish while you do something else.
Go HOME
Go to Task #2
Go to Task#4