i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
Here is simple step to create a custom partition with AVB. Tested by i.MX8MN EVK and Android P9.0.0_2.3.1. Create image for xyz partition in 1024MB in Android build output folder # cd $OUT # mkdir xyz # echo "This is test txt file" > xyz/Readme.txt # make_ext4fs -l 1073672192 -s -a xyz xyz.ext4.img xyz   Apply the attached patch. uboot patch corrects the reading problem on avb footer.   Flash images by uuu # cd $OUT # sudo ./uuu_imx_android_flash.sh -f imx8mn   Check result.  Boot up and mount xyz partition # cd /data # mount /dev/block/mmcblk2p14 xyz # cat xyz/Readme.txt This is test txt file
記事全体を表示
      The i.MX6UL/LL/LZ processor supports 2 USB OTG interfaces, USB OTG1 and USB OTG2, and each USB interface can be configured as a device, host or dual role mode. On the EVK board of i.MX6UL/LL, USB OTG1 is designed as dual role mode, and USB OTG2 is designed as HOST mode. This is sufficient for most customers.       However, in actual applications, we may need 2 USB HOSTs, and at the same time, we don’t want to use MicroUSB to USB TYPE-AF cable for Host-Device mode conversion. Therefore, the design of the USB circuit needs to meet such requirements: 1. USB device mode We need a USB device to download the linux image to the flash or SD card on the board. 2. 2 USB HOSTs When the system is working normally, we need the board to support 2 USB HOST. i.MX6UL/LL/LZ has only 2 USB ports. How to design to meet this requirement without increasing the USB HUB? The following scheme is used as a reference, and I hope it will be helpful to customers with similar requirement: 6.png        The logic and application description of this Diagram:: Default—device mode In the process of debugging the software, we need to use the USB OTG interface to download the linux image, so it must work in device mode. What we need to do is: (1). Pull USB OTG ID up to 3.3V (2). The USB OTG D+/D- signal is switched to the MicroUSB connector. (3). The USB OTG VBUS is provided with 5V power from the external PC USB HOST. Usage:        -Use a jumper for Pin 1 and Pin2, USB OTG ID pin will be pulled up to High.        With the operation, SEL pin of USB Muxer is High, and USB signals are switched to port B, and USB differential signals are connected to MicroUSB connector. At the same time, MIC2026-1YM output is disabled. The USB OTG1 VBUS pin of CPU is supplied by VBUS of MicroUSB connector, that is to say, supplied by PC USB HOST.        In this mode, software engineer can use it to download images to flash on board. Normal Work—Host mode After the software debugging is completed, two HOSTs are needed on the board. At this time, we need to switch the USB OTG1 from device to HOST mode. What we need to do is: (1). Pull USB OTG1 ID down to LOW (2). The USB OTG D+/D- signal is switched to the USB Type-AF connector. (3). Board should supply 5V power for USB device connected USB Type-AF connector. Usage:        -Use a jumper for Pin 2 and Pin3, USB OTG ID pin will be pulled down to Low.        With the operation, USB OTG1 ID pin is pulled down to Low, SEL pin of USB Muxer is also LOW, USB signals are switched to Port A, and connected to USB type-AF connector. At the same time, MIC2026-1YM is enabled , OUTA will output 5V , which will supply USB device connected on USB type-AF connector.   [Note] Users need to pay attention to. When using the jumper with PIN1/2/3, the board needs to be powered off. In other words, when switching between device and host, you need to switch off the power, then power on, and restart the board. The solution can also be used for i.MX processors with USB 2.0 interface.   NXP CAS team Wedong Sun 01/15/2021
記事全体を表示
Recently, some customers are using i.MX processor, they want to add raid & LVM function support to the kernel, but they have encountered the problem that the compilation cannot pass. Tested it in L4.14.98, L4.19.35 & L5.4.x, Only L4.14.98 bsp exists the problem. Here are the experimental steps I have done, including the same problems I encountered with the customer, and how to modify the kernel to ensure that the compilation passes. 1. Exporting cross compilation tool chain from yocto BSP (1) Downloading Yocto BSP and compiling it. Following steps in i.MX_Yocto_Project_User's_Guide.pdf, download Yocto BSP and compile it successfully. (2) Exporting cross compilation tool chain Following methods described in i.MX_Linux_User's_Guide.pdf, export cross compilation tool chain from yocto BSP. See Chapter 4.5.12 of the document, please! Then cross compilation tool chain will be like below: 1.png (3) Copying linux BSP source code to a new directory # cd ~ # mkdir L4.14.98-2.0.0 # cd L4.14.98-2.0.0 # cp -r ~/imx-yocto-bsp/build-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.14.98- r0/git ./ Then all linux source code has been copied to L4.14.98-2.0.0, which is the top directory of linux kernel source code, I will compile kernel image here. 2. Compiling linux kernel # cd ~/L4.14.98-2.0.0 # source /opt/fsl-imx-fb/4.14-sumo/environment-setup-cortexa9hf-neon-poky-linux-gnueabi # export ARCH=arm # make imx_v7_defconfig # make menuconfig Then we will add RAID and LVM modules to linux kernel. In order to reproduce errors, I added all related modules to kernel. See below, please! Device drivers---->Multiple devices driver support (RAID and LVM) 2.png After save and exit, began to compile kernel. # make (make –j4) The following errors will occur: ------------------------------------------------------------------------------------------- drivers/md/dm-rq.c: In function ‘dm_old_init_request_queue’: drivers/md/dm-rq.c:716:2: error: implicit declaration of function ‘elv_register_queue’; did you mean ‘blk_register_queue’? [-Werror=implicit-function-declaration] elv_register_queue(md->queue); ^~~~~~~~~~~~~~~~~~ blk_register_queue cc1: some warnings being treated as errors scripts/Makefile.build:326: recipe for target 'drivers/md/dm-rq.o' failed make[2]: *** [drivers/md/dm-rq.o] Error 1 scripts/Makefile.build:585: recipe for target 'drivers/md' failed make[1]: *** [drivers/md] Error 2 Makefile:1039: recipe for target 'drivers' failed make: *** [drivers] Error 2 ------------------------------------------------------------------------------------------- 3. Finding out root cause and solving it (1) elv_register_queue( ) function The function is loaded in dm-rq.c : int dm_old_init_request_queue(struct mapped_device *md, struct dm_table *t) { … … elv_register_queue(md->queue); … … } BUT compiler didn’t find it’s declaration and entity. Searching source code, and found it declared in linux_top/block/blk.h: … … int elv_register_queue(struct request_queue *q); … … It’s entity is in linux_top/block/elevator.c: int elv_register_queue(struct request_queue *q) { … … } (2) Adding declaration and exporting the function --- Declaration Add the line below to dm-rq.c: … … extern int elv_register_queue(struct request_queue *q); … … --- Exporting the function(elevator.c) Add EXPORT_SYMBOL(elv_register_queue); to the end of function, see below. int elv_register_queue(struct request_queue *q) { … … } EXPORT_SYMBOL(elv_register_queue); 4. Re-compiling Linux Kernel The above error will not occur and the compilation will complete successfully.   NXP CAS team Weidong Sun
記事全体を表示
Environment: openjdk-8 with L5.4.24-2.1.0 and GCC-9 1. Clone meta-java with dedicated branch name: git clone git://git.yoctoproject.org/meta-java -b zeus 2. Update .bb file for compile error in meta-java: diff --git a/recipes-core/icedtea/icedtea7-native.inc b/recipes-core/icedtea/icedtea7-native.inc index 8d0dc71..153a604 100644 --- a/recipes-core/icedtea/icedtea7-native.inc +++ b/recipes-core/icedtea/icedtea7-native.inc @@ -26,7 +26,7 @@ CXXFLAGS_append = " -fno-tree-dse" CXX_append = " -std=gnu++98" # WORKAROUND: ignore errors from new compilers -CFLAGS_append = " -Wno-error=stringop-overflow -Wno-error=return-type" +CFLAGS_append = " -Wno-error=stringop-overflow -Wno-error=return-type -Wno-error=format-overflow" inherit native java autotools pkgconfig inherit openjdk-build-helper 3. Add meta-java layer into bblayers.conf: BBLAYERS += "${BSPDIR}/sources/meta-java" 4. Edit the conf/local.conf to add openjdk variables # Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" # Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "jamvm-native" # Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native" PREFERRED_PROVIDER_java2-runtime = " openjdk-7-jre" IMAGE_INSTALL_append = " openjdk-7-jdk " diff --git a/recipes-core/openjdk/openjdk-8-common.inc b/recipes-core/openjdk/openjdk-8-common.inc index d8b30b8..ed03d60 100644 --- a/recipes-core/openjdk/openjdk-8-common.inc +++ b/recipes-core/openjdk/openjdk-8-common.inc @@ -181,5 +181,5 @@ FLAGS_GCC9 = "-fno-lifetime-dse -fno-delete-null-pointer-checks" BUILD_CFLAGS_append = " ${@openjdk_build_helper_get_build_cflags(d)}" BUILD_CXXFLAGS_append = " ${@openjdk_build_helper_get_build_cflags(d)}" # flags for -cross -TARGET_CFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)}" +TARGET_CFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)} -Wno-error=format-overflow" TARGET_CXXFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)}" diff --git a/recipes-core/openjdk/openjdk-8-native.inc b/recipes-core/openjdk/openjdk-8-native.inc index 321a43d..97ff03f 100644 5. Switch the host GCC to gcc-8 and g++-8: sudo apt-get install gcc-8 g++-8 sudo update-alternatives --install /usr/bin/gcc gcc /usr/bin/gcc-8 --slave /usr/bin/g++ g++ /usr/bin/g++-8 --slave /usr/bin/gcov gcov /usr/bin/gcov-8 --slave /usr/bin/gcov-tool gcov-tool /usr/bin/gcov-tool-8 --slave /usr/bin/gcc-ar gcc-ar /usr/bin/gcc-ar-8 --slave /usr/bin/gcc-nm gcc-nm /usr/bin/gcc-nm-8 --slave /usr/bin/gcc-ranlib gcc-ranlib /usr/bin/gcc-ranlib-8 sudo update-alternatives --config gcc  6. And change the conf/local.conf from openjdk-7 -> openjdk-8: PREFERRED_PROVIDER_java2-runtime = " openjdk-8-jre" IMAGE_INSTALL_append = " openjdk-8 " 
記事全体を表示
UUU is an evolution of MFGTools. The introduction of UUU detail you can see the uuu.pdf file.. Please download uuu.exe and follow the UUU introduction. Here are some running examples. If you are not familiar with uuu, you can refer to them firstly. Under Windows (should be as admin): • For SD card:  Linux:  .\uuu -b sd_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard • For EMMC:  Linux:  .\uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard  or  .\uuu.exe uuu.auto  Android:  .\uuu_imx_android_flash.bat -f imx8mm -u trusty Under Linux: • For EMMC  Linux:  sudo .\uuu uuu.auto If you download BSP release from nxp.com, you could find a file uuu.auto in the package. This is a preset script that can be executed directly (default for EMMC). You could change the script based on your requirement. Copy the uuu.exe under the release package, then execute the instructions. For UUU tool the prebuilt image and document are here: • https://github.com/NXPmicro/mfgtools/releases • UUU.pdf is snapshot of wiki   Environment PC: Window 10 64bit Board: i.MX8MMLPDDR4 EVK BSP: Q10.0.0_2.0.0 Demo images Screen: MX8-DSI-OLED1 Downloading android images to i.MX 8M Mini EVK LPDDR4 via UUU Tool 1\Hardware Preparations (1) Make the board enter serial download mode. For Rev. B boards, change the first two bits of board's sw1101 to 10 (from 1-2 bit) to enter serial download mode. For Rev. C boards, change the first four bits of board's sw1101 to 1010 (from 1-4 bit) to enter serial download mode. (2) Connecting J901to PC USB by a USB OTG cable. (3) Connecting J301(usb type c) to PC USB. (4) Plugging adapter into Power Jack (J302) (5) Power on i.MX 8M Mini EVK LPDDR4 board via SW101 Switch When first connect the board to PC, windows 10 64bit can’t automatically install FT2232D  driver from official website of manufacture, you need to Install the usb to uart driver manually: https://www.ftdichip.com/Drivers/D2XX.htm Download the setup executable and then install it. When installed success you can see the usb serial port can be used. 2\Downloading UUU Tool For the UUU binary file, download it from github: uuu release page on github. For the Q10.0.0_2.0.0 version use the UUU 1.3.124 version. For Linux OS, download the file named "uuu". For Windows OS, download the file named "uuu.exe". Here I use win10 system, so I download the uuu.exe file.   3\Download the Q10.0.0_2.0.0 Demo images for i.MX8MM   Now all the android os for i.MX products are here: Android OS for i.MX Applications Processors. Decompress release_package/android-10.0.0_2.0.0_image_8mmevk.tar.gz for LPDDR4 board. The package contains the image files and uuu_imx_android_flash tool. Copy uuu.exe to the directory of Q10.0.0_2.0.0 Demo images. 4\ Execute the uuu_imx_android_flash to flash image Power on the board. Open the serial port terminal and setting as following: Open a command line window. For the use and the Options for uuu_imx_android_flash tool details can see the Table 2 in the Android_Quick_Start_Guide. Here I use the OLED screen, to test MIPI panel output, need execute the tool with "-d mipi-panel". So here I use the .\uuu_imx_android_flash.bat -f imx8mm -e -d mipi-panel . When I use the download I meet the follow question: C:\Work\Products\Android BSP\New folder\Q10.0.0_2.0.0 Demo images\android-10.0.0_2.0.0_image_8mmevk>.\uuu_imx_android_flash.bat -f imx8mm -e -d mipi-panel This script is validated with uuu 1.3.124 version, it is recommended to align with this version. dtbo is supported dual slot is supported dynamic partition is supported You do not have sufficient privilege to perform this operation.   So here can change to use the Windows PowerShell, it works well and finished download.   Power off the board. 5\Boot up the board from emmc Set boot mode For Rev. C boards: Change sw1101 to 0110110010 and change sw1102 to 0001101000 if you want to boot from SD card. Change sw1101 to 0110110001 and change sw1102 to 0001010100 if you want to boot from eMMC. Set the U-Boot environment variables for the MIPI panel display U-Boot > setenv bootargs console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init androidboot.console=ttymxc1 androidboot.hardware=freescale cma=800M@0x400M-0xb80M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware transparent_hugepage=never androidboot.wificountrycode=CN androidboot.lcd_density=240 U-Boot > saveenv Then use the boot to boot up and then display on OLED screen.   Hope this can do help for some users. Best Regards Rita
記事全体を表示
Hello everyone, In this document I'll explain on how to build the UUU (Universal Update Utility) using windows 10 PC. This may be useful in case of adding custom commands to run during the flash using built-in scripts, be it for debugging, fuse blowing, etc. First we need to download and install Visual Studio community, for this guide I'll use community 2019, version it is available here: https://visualstudio.microsoft.com/thank-you-downloading-visual-studio/?sku=Community&rel=16 For workloads select Universal Windows Platform development.   When installing, make sure to select and install the Git for windows complement, at the top select Individual components, this will display a new list, scroll down to code tools and you will find Git for windows, check this box In case Visual Studio is already installed, you may open the installer again and chose modify, this will let you install the complement as well. git_selection.png After the installation is complete we may run the git commands on the power shell. Now open the windows power shell and type the following commands: git clone https://github.com/NXPmicro/mfgtools.git // clones the MFGTool (UUU) source code from the github cd mfgtools // enters the mfgtools folder we just cloned git submodule init // creates the local configuration file for the submodules git submodule update // set the submodules to the commit specified by the main repository. At this point we can edit the built in scripts to add our custom commands, for this guide I'll add the printenv uboot command at the end of the flashing process. For this I'll enter the folder mfgtools/uuu, and edit emmc_burn_all.lst with any text editor, i.e. Notepad ++, add the command FB: ucmd printenv. add_printenv.png   Save and close the editor, it is possible to add most uboot commands like for example the fuse commands to burn eFuses. Then we can now build the tool, opening msvc/uuu-static-link.sln with Visual studio, select solution uuu-static-link.sln select_solution.png   And finally build the solution: build_solution.png The executable (uuu.exe) would be at the following path: mfgtools\msvc\x64\Debug   executable.JPG Finally we run the built in script we modified and check the results. Find attached both the powershell and uboot logs, I tested this using an i.MX8MN with L5.4.47_2.2.0, running the following command: ./uuu.exe -v -b emmc_all imx-boot-imx8mnevk-sd.bin-flash_evk imx-image-full-imx8mnevk.wic Hope this may found useful for anyone trying to achieve something similar.
記事全体を表示
Symptoms   Customer want to add gps dynamic link library as service in android system,but can not be allowed by Android SE Policy. Diagnosis   Customer didn't set the correct config file.   Solution ① Open the file android_build/device/fsl/imx8q/mek_8q/mek_8q.mk, add gnss service   # GNSS HAL PUALPRODUCT_PACKAGES += \[email protected] \[email protected]     ② Open the file android_build/device/fsl/imx8q/mek_8q/manifest.xml and add gnss hidl     android.hardware.gnsshwbinder 1.0 IGnss default     ③ Open the file android_build/device/fsl/imx8q/mek_8q/BoardConfig.mk, add   #GNSS PUALBOARD_HAS_GPS_HARDWARE := true     ④ Open the file android_build/device/fsl/imx8q/mek_8q/ueventd.freescale.rc, add   /dev/ttyLP1 0660 system gps       Add Selinux permissions     Add in device/fsl/imx8q/sepolicy/system_server.te:   allow hal_gnss_default vndbinder_device:chr_file {read };     After adding the test, there are also permission issues such as write, open, etc., we add it all at once:   allow hal_gnss_default vndbinder_device:chr_file {open read write execute getattr create ioctl map};
記事全体を表示
In this doc will show how to use i.MX8QXP DPU do image warp.   SW: i.MX Linux BSP L5.4.24_2.1.0 bsp release and patch in this doc HW: i.MX8QXP MEK board, ov5640 camera, HDMI display   Introduction Image Warping is the process of digitally manipulating image data such that the image’s projection precisely matches a specific projection surface or shape. 1.png   i.MX8QXP DPU controller could do image warp work by its blit engine and display engine. I choose to enable blit engine’s fetchwarp9 unit to do warp work. Check i.MX8QXP RM, Blit Engine support Image Warp as: “Performs a re-sampling of the source image with any pattern. The sample point positions are read from a compressed coordinate buffer.” So you need prepare two input buffers, one buffer store original image data, the other buffer store resample point coordinate, DPU blit engine will read that two buffer by fetchwarp9 unit, then output result image buffer which contain warped image data. Note i.MX8QXP DPU blit engine fetchwarp9 unit, for the input original image buffer, support RGB and YUV 4:4:4 format. The resample point coordinate buffer contents is depend on what kind warp transformation in your use case; and for each resample point coordinate format check i.MX8QXP RM fecthwarp unit description as below. In this doc, using the 2xs12.4 format, each point x coordinate use (12+4) bit, same as y coordinate. 2.png   For DPU fetchwarp9 unit, to enable it work for image warp, check i.MX8QXP RM: 3.png   2.Patch notes and test code imx8-dpu-warp-kernel.diff contain the kernel side change for drm ioctl api permission and add vmap function of ion dma_buf_ops. libg2d.so contain the binary for adding warp feature. g2d.h is header file which add define for G2D_WARP and G2D_YUV4. imx8-ov5640-dpu-warp-render.c is a sample code which show how to call g2d lib to image warp, need open the G2D_WARP flag. And this code contain some example calculate the coordinate buffer of rotate, swirl, barrel distortion, affine transformation, perspective transformation, wave transformation. And this code will show read camera input frame then add warp process , then render warp image frame to display.   The test cmd usage as below, read 1080P frame from ov5640 camera, do warp then render warp image to drm plane. Note as dpu fetchwarp9 unit support YUV 4:4:4 input image frame, so below cmd need set parameter YUV4, which will ask ISI driver output YUV 4:4:4 image frame. imx8-ov5640-dpu-warp-render  -i /dev/video0 -f YUV4  -S 1920,1080  -M imx-drm -p 91:38 -F XB24  -b 6  -e g2d  -t 5         -i <video-node> set video node (default: /dev/video0)         -f <fourcc>     set input format using 4cc         -S <width,height>       set input resolution         -s <width,height>@<left,top>    set crop area         -M <drm-module> set DRM module         -o <connector_id>:<crtc_id>:<mode>      set a mode         -p <connector_id>:<crtc_id>     output to a plane         -F <fourcc>     set output format using 4cc         -t <warptype>   set 0 neutual 1 rotate 2 swirl 3 divisionmodel 4 affine 5 perpsptive 6 wave         -b buffer_count set number of buffers        3.Example original image:   4.png     Untitled.png     Untitled.png Untitled.png   Untitled.png Untitled.png       Untitled.png   Reference: https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_MX8QXPC0&appType=license https://en.wikipedia.org/wiki/Image_geometry_correction https://lists.freedesktop.org/archives/dri-devel/2012-March/019778.html https://store.kde.org/p/1246558 https://github.com/ImageMagick/ImageMagick        
記事全体を表示
1. HW Environment:     IMX8mm-evk board.     ITE6122 mipi dsi to lvds bridge board.     B101UAN02.1 1920x1200 LVDS panel   2. SW Environment:     IMX YOCTO 4.14.98-2.0.0ga release.   3. Patch operation:     a. git clone https://source.codeaurora.org/external/imx/linux-imx.git     b. git checkout -b  imx_4.14.98_2.0.0_ga remotes/origin/imx_4.14.98_2.0.0_ga     c. patch -p1 < ../ite6122_imx8mm_4.14.98ga_18c3fd8837fc3c6_0512.patch   4. Tested on imx8mm-evk board:   5. Attached doc list:      i.MX8MM(MN)_IT6122FN_ user guide_V0.20.pdf ------  ite6122 bridge board HW guide      i.MX8MM(MN)_IT6122FN_V11_20200513.pdf  ------  ite6122 bridge board SCH      ite6122_imx8mm_4.14.98ga_18c3fd8837fc3c6_0512.patch  ------  Linux kernel driver patch      B101UAN02.1_Ver1.0.pdf -------  panel spec              2020/10/30: 6122-hw-version-2010-10-30.zip ------ updated new HW design.        
記事全体を表示
BSP: L5.4.47-2.2.0-rc2 Board: imx8QM B0 HW:  LVDS2HDMI , MIPIDSI2HDMI. It is the porting of i.MX8QM dpu loopback to isi. to the 5.4.y, with the addition of the MIPI-DSI loopback and the HDMI loopback.  Overview of the DC capture configuration: DC_loopback.png For enabling the capture: only DC 0 Stream 0  and DC 1 Stream 1 can be captured The pixel link Master address should be set to 3 because the Receiver Address at ISI is 3 and can't be changed. To continue displaying the stream, the Receiver Address at LVDS and DSI or HDMI should be changed to 3. It is possible to change the RA by using GPIO of the modules.   Patches: Create V4L2 device enabling the capture of by the ISI of DC loop-backs. Enable ISI capture from DSI 0 / LVDS 1 in 1920x1080 (at the same time.) Enable ISI capture from HDMI in 2840x2160 (half with even pixel) in 1920x2160. While capturing with the ISI, the captured screen continue to be displayed. Remark: Ov5640 cameras are also enabled in the same dtb. So 4 stream in 1920x1080 can be captured at the same time. Installation and gstreamer command: See readme
記事全体を表示
       
記事全体を表示
Harware: - i.MX7D-SDB board - QCA9880 card with MINI PCIe Interface The Wifi module is connected to the PCIe slot on the board. 1.png     Software: - Ubuntu 18.04 LTS Host - L4.19.35_1.1.0 BSP   Tool: - uuu 1.2.68 for linux (run on ubuntu host)   Toolchain: - The toolchain can be obtained from the Yocto BSP. Please read and follow the steps in i.MX_Yocto_Project_User's_Guide to build the BSP and then read the Chapter of "How to build U-Boot and Kernel in standalone environment" in i.MX_Linux_User's_Guide to build the toolchain.   Build the Kernel: # mkdir imx_build # cd imx_build # git clone https://source.codeaurora.org/external/imx/linux-imx -b imx_4.19.35_1.1.0 # cd linux-imx # source /opt/fsl-imx-fb/4.19-warrior/imx6/environment-setup-cortexa9hf-neon-poky-linux-gnueabi # export ARCH=arm # make clean # make imx_v7_defconfig # make menuconfig - Select the PCIe driver and the Wifi support 2.png - PCI controller drivers--->                    DesignWare PCI Core Support----> 3.png - Networking support----->                             Wireless-----> 4.png   - Select the ath10 driver (it supports QCA988X) Device Drivers---->             Network device support----->                                      Wirless LAN----> 5.png - Save and Exit. - Add the firmware in the .config file: Get the firmware file (e.g. firmware-2.bin) from your wifi vendor or download it from the web. Put the firmware in linux-imx/firmware/ folder. Edit the .config file and add these two lines: CONFIG_EXTRA_FIRMWARE="board.bin firmware-2.bin" CONFIG_EXTRA_FIRMWARE_DIR="/home/jimmy/imx_build/linux-imx/firmware" - Build the kernel # make Then the zImage will be obtained in arch/arm/boot.   Using uuu to program the SD card: - Downloading demo image of L4.19.35_1.10 from the nxp website. - Copy the zImage to the directory - Copy the uuu (V1.2.68) to the directory - Copy the samples/example_kernel_emmc.uuu to imx7d_kernel_emmc.uuu - Modify the image the imx7d_kernel_emmc.uuu - In the demo image, you will see the files like this: 6.png - run uuu and the script to program the images.   Wifi driver loaded and wlan0 is up: # dmesg | grep pci 7.png   # ifconfig -a 8.png   Reference Document: - i.MX_Linux_User's_Guide.pdf - i.MX_Porting_Guide.pdf  
記事全体を表示
As of this writing, April 2015, the default sdcard image created from a Yocto Project build has all the software images nicely aligned to create a SDCARD. 10/7/2020: Update - SDCARD image names have been updated to images ending with .wic as the default from Yocto Project.  The process is the same for both .sdcard and .wic files.   There are two partitions within the image: A W95 FAT32 (LBA) partition that contains the Linux zImage, and various device tree binary (dtb) files A Linux root file system. Each partition can be mounted from your Linux host computer, then you can read or write the partition contents. Here are the steps based on the core-image-base recipe for the imx6sxsabresd machine using Yocto Project release L3.14.28_1.0.0_GA.   The name of the image: core-image-base-imx6sxsabresd.sdcard Run the fdisk command to view the contents of the image: $ fdisk -l core-image-base-imx6sxsabresd.sdcard Disk core-image-base-imx6sxsabresd.sdcard: 100 MB, 100663296 bytes 4 heads, 32 sectors/track, 1536 cylinders, total 196608 sectors Units = sectors of 1 * 512 = 512 bytes Sector size (logical/physical): 512 bytes / 512 bytes I/O size (minimum/optimal): 512 bytes / 512 bytes Disk identifier: 0x00074663 Device Boot Start End Blocks Id System core-image-base-imx6sxsabresd.sdcard1 8192 24575 8192 c W95 FAT32 (LBA) core-image-base-imx6sxsabresd.sdcard2 24576 188415 81920 83 Linux   Determine the byte offset into the sdcard image of where each partition starts:  core-image-base-imx6sxsabresd.sdcard1 starts at sector 8192. One sector unit is 512 bytes.                8192 * 512 = 4194304 core-image-base-imx6sxsabresd.sdcard2 starts at sector 24576. 24576 * 512 = 12582912   Mount Partitions First create mount points: $ sudo mkdir /mnt/{mp1,mp2}    sdcard1 partition $ sudo mount -o loop,offset=4194304 core-image-base-imx6sxsabresd.sdcard /mnt/mp1 NOTE: An alternate method for determining the offset, see below: $ sudo mount -o loop,offset=$((512 * 8192)) core-image-base-imx6sxsabresd.sdcard /mnt/mp1 sdcard2 partition $ sudo mount -o loop,offset=12582912 core-image-base-imx6sxsabresd.sdcard /mnt/mp2 View the contents of each mounted partition $ ls /mnt/mp1 imx6sx-sdb.dtb imx6sx-sdb-lcdif1.dtb imx6sx-sdb-reva.dtb imx6sx-sdb-sai.dtb imx6sx-sdb-emmc.dtb imx6sx-sdb-m4.dtb imx6sx-sdb-reva-ldo.dtb zImage $ ls /mnt/mp2 bin boot dev etc home lib lost+found media mnt proc run sbin sys tmp usr var   When done release the mount points and remove them from /mnt $ sudo umount /mnt/{mp1,mp2} $ sudo rm /mnt/{mp1,mp2}  
記事全体を表示
To enable USB 2.0 port on BB for USB OTG, you need to apply below two changes: device/fsl.git   diff --git a/imx8q/mek_8q/init.usb.rc b/imx8q/mek_8q/init.usb.rc index af4e388..0f3ab0b 100644 --- a/imx8q/mek_8q/init.usb.rc +++ b/imx8q/mek_8q/init.usb.rc @@ -44,7 +44,7 @@ on early-boot      mount functionfs mtp /dev/usb-ffs/mtp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      mount functionfs ptp /dev/usb-ffs/ptp rmode=0770,fmode=0660,uid=1024,gid=1024,no_disconnect=1      setprop sys.usb.mtp.device_type 3 -    setprop vendor.usb.config "5b110000.usb3" +    setprop vendor.usb.config "ci_hdrc.0"      write /sys/module/libcomposite/parameters/disable_l1_for_hs "y"      symlink /config/usb_gadget/g1/configs/b.1 /config/usb_gadget/g1/os_desc/b.1   vendor/nxp-opensource/kernel_imx.git           revert below patch:           commit 2f9586c120971312e61df464264993899cf34536           Author: yang.tian <[email protected]>           Date:   Tue Jan 7 13:30:02 2020 +0800       MA-15242 Set usb2.0 port as usb host only for mek_8q  
記事全体を表示
This document is a user guide for the GStreamer version 1.0 based accelerated solution included in all the i.MX 8 family SoCs supported by NXP BSP L5.4.24_1.1.0. Some instructions assume a host machine running a Linux distribution, such as Ubuntu, connected to i.MX 8 device. These commands were tested using Ubuntu 18.04 LTD, and while Ubuntu is not required on the host machine, other distributions have not been tested. These instructions are targeted for use with the following hardware: • i.MX 8MQ EVK • i.MX 8MN EVK • i.MX 8MN EVK • i.MX 8QXP MEK B0 • i.MX 8QM MEK B0   Release History v1.0 - Mar 2020 - Initial release. v2.0 - Sep 2020: Added the following content: - Mux/Demux Examples - Audio Examples - Image Examples - Transcode Examples - Streaming Examples - Multi-Display Examples - Scaling and Rotation Examples - Zero-copy Examples - Debug Examples Maintainers: . Marco Franchi . Pedro Jardim
記事全体を表示
1. HW Environment:     IMX8mp-evk board.     ITE6151 mipi dsi to eDP bridge board.   2. SW Environment:     IMX YOCTO 5.4.24-2.1.0 release.   3. Patch operation:     a. git clone https://source.codeaurora.org/external/imx/linux-imx.git     b. git checkout -b  imx_5.4.24_2.1.0 origin/imx_5.4.24_2.1.0     c. patch -p1 < ../ite6151_mipi2edp_linux_5.4.24_20200921.patch   4. Tested on imx8mp-evk board with DP monitor on 1080p mode: ite6151-1.jpg ite6151-2.jpg 5. Attached doc list:     IT6151 demo board user guide v1.0.pdf ------  ite6151 bridge board HW guide     it6151_qfn48_v20_20190905-01_end.pdf  ------  ite6151 bridge board SCH     imx8mp_ite6151_mipi2edp_linux_5.4.24_20200921.patch ------  Linux kernel driver patch     Image + imx8mp-evk-it6151.dtb  ------  test image and dtb  
記事全体を表示
After following instructions on how to change DRAM PLL frequency, here is a quick comparison of Stream, running on the i.MX 8MM. Normalized to LPDDR4-3000, based on 5.4.24_2.1.0​ BSP Stream LP4-3000 LP4-2400 DDR4-2400 LPDDR-1866 Copy: 1 0.810 0.735 0.497 Scale: 1 0.896 0.765 0.756 Add: 1 0.899 0.683 0.762 Triad: 1 0.902 0.680 0.767   DDRComp.png    
記事全体を表示