NXP Tech Blog - Page 3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Tech Blog - Page 3

gaurav_sharma
NXP Employee
NXP Employee

Hey everyone!! This one is going to be a very brief blog. A lot of times, system developers encounter OOPS from the linux kernel while tweaking in the kernel drivers.
A kernel OOPS is a non-fatal but serious error that help developers debug the potential problems.
It is like the kernel is the patient with an illness trying to talk to a doctor and telling what is wrong with it so that the developers can identify the issue and fix it.

It generally occurs when the kernel detects an invalid operation such as an illegal memory access, NULL pointer dereferences, invalid instruction execution. An OOPS doesn't necessarily mean that the system will stop working right there and then. However, it does impact the reliability of the system until a point at which the system could potentially halt and stop working.

Read more...

More
1 0 3,833
gaurav_sharma
NXP Employee
NXP Employee

Hello to you all! In this blog, we will focus on low power management in PCIe. PCIe Power management aims at reducing power consumption in PCIe devices by putting them to low power states when they are idle and bringing them back to full power state when required.

Why does it matter ?  Because PCIe devices in the market such as graphic cards, storage devices, Network Interface Cards can consume significant power when they are active. Power management allows them to scale down their power consumption during idle or periods of low activity.

Read more...

More
1 0 10.9K
yuhe-r64908
NXP Employee
NXP Employee

このシリーズでは、低コストでコンパクトな開発ボード「FRDM i.MX 93 Development Board」を用いて、i.MX 93内のCortex-M33コア向けのSDKサンプルコードのビルドと実行方法を、ハンズオン形式で全3回にわたって解説します。

  • 【第1回】開発環境構築とMコアイメージのビルド
  • 【第2回】U-BootとremoteprocによるMコア実行(本記事)
  • 【第3回】ブートローダーによるMコアの自動起動
Read more...

More
1 0 2,578
yuhe-r64908
NXP Employee
NXP Employee

このシリーズでは、低コストでコンパクトな開発ボード「FRDM i.MX 93 Development Board」を用いて、i.MX 93内のCortex-M33コア向けのSDKサンプルコードのビルドと実行方法を、ハンズオン形式で全3回にわたって解説します。

  • 【第1回】開発環境構築とMコアイメージのビルド(本記事)
  • 【第2回】U-BootとremoteprocによるMコア実行
  • 【第3回】ブートローダーによるMコアの自動起動
Read more...

More
1 0 2,598
gaurav_sharma
NXP Employee
NXP Employee

Hey everyone! This blog will cover the following: -

 

  1. System Overview
  2. Use-case
  3. What are Outbound and Inbound windows in PCIe and how do they work?
  4. What is ATU and why is it important in PCIe?
  5. How to configure the PCIe windows in LS1028 and iMX8QXP
  6. Code walkthrough
  7. Running the test case
Read more...

More
0 0 3,212
Keita_Nagashima
NXP Employee
NXP Employee

2025年よりNXP Japanから日本語の技術記事をたくさんユーザーに届けようとの想いの下、これまでに多数の技術記事(Tech Blog)を公開してまいりました。これらの情報をより体系的にご活用いただけるようコンテンツ・マップ(PDF)を公開しています。

実装例やトラブルシューティングのヒントを含む実践的な内容が充実しており、開発現場での課題解決や新規プロジェクトの立ち上げ時に役立つ情報として、多くの技術者の皆様に活用いただいております。

(読了:5分)

Read more...

More
1 0 5,822
araki
NXP Employee
NXP Employee

バッテリーマネジメントシステム (BMS)において3つの重要な指標について以下のように解説します。

管理すべき指標とBMSの重要性を理解いただけると幸いです。

(読了:10分)

Read more...

More
1 0 5,813
shaojun_wang
NXP Employee
NXP Employee

OV5640 MINISASTOCSI is widely used in i.MX8. This article shows how to enable it on i.MX95 15x15 EVK board. The Linux version is 6.12.20.

Read more...

More
1 0 2,040
KosukeSogawa
NXP Employee
NXP Employee

NXP車載向けマイコンの機能安全対応について、通常の(機能安全非対応)マイコンと何が違うのか説明します。

(読了:5分)

Read more...

More
2 0 4,096
araki
NXP Employee
NXP Employee

バッテリーマネジメントシステム (BMS)に関する内容を以下のようにまとめています。

BMSにこれから携わる方に読んでいただけると嬉しいです。

(読了:5分)

Read more...

More
1 0 5,420
akifumiokano
NXP Employee
NXP Employee

このブログでは,デジタル回路で使われる論理回路の種類(*TTL,*LVTTL,*CMOS)の電圧レベルの違いから,それを判断する上で重要なVOH/VOL/VIH/VILの意味について解説します.

さらに様々な変換の方法の中から,どのような電圧レベル・トランスレータを選べばよいかを解説します.

特に特別な扱いが必要となる,双方向オープンドレイン信号の変換について詳しく見てみます

スクリーンショット 2025-08-21 12.52.04.png

Read more...

More
0 0 5,087
Keita_Nagashima
NXP Employee
NXP Employee

この記事では、MyNXPアカウントの登録方法を分かりやすく説明します。

またMyNXPアカウントのメリットについても簡単にご紹介します。

(読了:5分)

Read more...

More
1 0 2,758
Keita_Nagashima
NXP Employee
NXP Employee

NXP製品の使用方法が分からない場合や、ドキュメントを読んでも内容が理解できないときのために、NXPでは問い合わせ窓口を用意しています。
この記事では、実際にどのように問い合わせを行えばよいのか、手順を分かりやすくご紹介します。
*2025年6月より、日本語での問い合わせが可能になりました。

Read more...

More
1 0 3,779
Yutaka_Okui
NXP Employee
NXP Employee

ある、マイコン/プロセッサに適したNXP PMIC PFシリーズ を検索するときに、助けとなる情報をまとめています。

nxp.jpの「パワー・マネジメントIC (PMIC) とシステム・ベーシス・チップ (SBC)」ページで提供されている、プロセッサに適したPMICまたはSBCの検索ツール(製品セレクタ、およびクロス・リファレンス)とあわせて使用してください。

(読了:5分)

Read more...

More
1 0 4,197
Keita_Nagashima
NXP Employee
NXP Employee

プロセス・テクノロジーの微細化に伴い、28nm以降の世代では、従来からあるFlashメモリをマイコンへ搭載することが難しくなり、各社次世代マイコンに対してFlashメモリに代わる不揮発性メモリ(NVM)を検討しています。その中のひとつがMRAMです。

本記事では、MRAMの特徴を説明します。

(読了:5分)

Read more...

More
1 0 5,043
yutaka_ando
NXP Employee
NXP Employee

i.MXアプリケーション・プロセッサのLinux BSPに含まれるデモ・リポジトリ「GoPoint」を紹介します。
「GoPoint」には、物体/顔検出などのMachine Learning (ML)をはじめ、ビデオ再生カメラのISP調整3Dグラフィックス(OpenGL ES)などのマルチメディアのデモがあり、i.MXアプリケーション・プロセッサの各種機能を簡単に確認できますので、是非お試しください。

Read more...

More
1 0 2,840
Yutaka_Okui
NXP Employee
NXP Employee

最適な電源ICを選ぶときに、どのような手順で、候補となる電源ICを絞り込んでいくのが良いのかを、大きく、以下の3つのステップでまとめてみました。

・Step 1 - 候補となる電源ICの選定

・Step 2 - 実装面積の確認

・Step 3 - 熱設計の確認

*第3回では、Step 3を説明します。

(読了:5分)

Read more...

More
1 0 2,846
Yutaka_Okui
NXP Employee
NXP Employee

最適な電源ICを選ぶときに、どのような手順で、候補となる電源ICを絞り込んでいくのが良いのかを、大きく、以下の3つのステップでまとめてみました。

・Step 1 - 候補となる電源ICの選定

・Step 2 - 実装面積の確認

・Step 3 - 熱設計の確認

*第2回では、Step 2を説明します。

(読了:5分)

Read more...

More
1 0 2,214
Yutaka_Okui
NXP Employee
NXP Employee

最適な電源ICを選ぶときに、どのような手順で、候補となる電源ICを絞り込んでいくのが良いのかを、大きく、以下の3つのステップでまとめてみました。

・Step 1 - 候補となる電源ICの選定

・Step 2 - 実装面積の確認

・Step 3 - 熱設計の確認

*第1回では、Step 1を説明します。

(読了:5分)

Read more...

More
1 0 2,915
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

 

前回まではG-cell MEMSについて説明しました。

第四回はこのG-cell MEMSのコンデンサ容量をASICで信号処理する機構について取り上げたいと思います。

Read more...

More
1 0 3,629
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

 

前回はG-cell MEMSの概要について説明しました。

第三回は出力特性や特殊機能などについて取り上げます。

Read more...

More
1 0 3,454
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

 

第二回は加速度センサの心臓部である、加速度を検知する機構について取り上げます。

Read more...

More
1 0 2,850
satoshikamiya
NXP Employee
NXP Employee

セキュリティ要件適合評価及びラベリング制度(以後「JC-STAR」と表記します)は、独立行政法人情報処理推進機構(IPA)が運用する日本独自のIoT製品セキュリティ評価制度です。本稿では、JC-STARの概要と、NXPのセキュリティ製品について紹介します。

(読了:5分)

Read more...

More
1 0 3,957
yutaka_ando
NXP Employee
NXP Employee

i.MX 8M Plusの評価ボード (EVK) を用いて、マルチメディア機能(ビデオ再生、オーディオの録音/再生、カメラ動作、Wi-Fi接続、NPU動作など)の動作を確認する方法について説明します。

Read more...

More
1 0 3,364
Yusei_Uegama
NXP Employee
NXP Employee

組み込みデバイスの限られたリソースの中でLLMを使用するためには、RAGが必要となります。

本稿では、NXPの LLM + RAG ソリューション 「eIQ GenAI Flow」についてハンズオン形式で紹介します。

Read more...

More
3 0 5,779
atsuyoshiyamagu
NXP Employee
NXP Employee

NXPの車載向け加速度センサの原理・特徴・用途をまとめたページです。

(読了:5分)

Read more...

More
2 0 3,625
Keita_Nagashima
NXP Employee
NXP Employee

eIQ Time Series Studio(時系列モデル開発ツール)の概要から、プロジェクトの作成 → データセット → トレーニング → エミュレーション → デプロイメント → データロギングと、使い方の流れを記載しています。

本記事は、eIQ Time Series Studio v1.0.4を起動させた際に表示される"Documentation"メニューに記載されている資料を翻訳したものです。必ず最新の英語版をご確認いただき、本記事はあくまでも補足的な内容としてご利用ください。

Read more...

More
1 0 9,764
Keita_Nagashima
NXP Employee
NXP Employee

CANバス/プロトコルの概要から特長について説明します。

NXPは古くからCANに携わっており、マイコン、プロセッサ、トランシーバと様々なCAN製品を提供しています。

Read more...

More
1 0 9,512
yumb
NXP Employee
NXP Employee

2025年4月、当社のUniversity Programの一環として、徳島県の神山まるごと高専で jig.jp創業者・福野泰介氏が行う新入生向けの導入授業「ITブートキャンプ2025」に、ボランティア参加しました。本ブログではその体験を振り返りつつ、教育支援の現場でのMCX開発ボードの活用事例をご紹介します。

Read more...

More
1 0 6,583
yutaka_ando
NXP Employee
NXP Employee

i.MXアプリケーション・プロセッサの評価ボードで消費電力を測定する方法をまとめたページです。

  • i.MX 8M Plus Power EVKをベースにしています。
  • 電力モードを切り替える方法についても説明します。
  • 動作周波数の変更方法や、使用しないブロックのディセーブル方法についても説明します。
Read more...

More
2 0 3,299