i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Running Zephyr on i.MX9 A55 core brings a high performance, real-time (short interrupt, scheduler latency, etc.) OS experiences as well as the fast boot, small memory footprint features. This article provide all the information on how to run the Zephyr v4.1 on Cortex-A55 cores to support below features: Supported Features FRDM-IMX93 FRDM-IMX91 Description Zephyr RTOS code base     Based on Zephyr v4.1 FRDM-IMX93 board configure Yes   Board configuration, build, device tree files FRDM-IMX91 board configure   Yes Board configuration, build, device tree files Hello world Yes Yes   Dual Ethernet Yes   TY8521 Ethernet PHY support Display Yes   LCDIF, MIPI DSI, Waveshare 1024x600 7inch DSI LCD(C) Camera Yes   MIPI-CSI, ISI, AP1302 sensor Audio Yes   I2S with eDMA (Driver only) uSDHC Yes   SD card only USB Yes   USB CDC device class   The code has been release on github: Zephyr samples/drivers: https://github.com/nxp-zephyr/zephyr Zephyr HAL: https://github.com/nxp-zephyr/hal_nxp Tag: FRDM-IMX93-v4.1 How to doc is attached.  
View full article
share the document for ov5640 support on imx93 evk with 6.12 bsp
View full article
Hello everyone, in this post we will control one (or more) WS2812 LEDs from a Linux UserSpace application, communicating with Cortex M33 through RPMSG.  Required materials: FRDM-IMX93 WS2812 LED/Strip Attached wsled.c (userspace application) Attached ws2812_m33_project (Source code of firmware for M33)   Environment: Linux Kernel 6.6 arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-eabi SDK 24.12.00   This is the block diagram of the application:        CORTEX M33 SIDE.  From WS2812  LED datasheet, we can see the timing must be precise, that is the reason we will use the Cortex M33 (Real time applications):    As we can see, the timing just accept tolerance of 150ns, that is the reason is preferred to use the Cortex M33 instead of control with Linux that is in charge of other tasks.    The function that we will implement to send Zero and One is:  void WS2812B_send_bit(uint8_t bit) { if (bit) { // Send "1" RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 1); for (int i = 0; i < HIGH_ONE_CYCLES; i++) __asm__("NOP"); RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 0); for (int i = 0; i < LOW_ONE_CYCLES; i++) __asm__("NOP"); } else { // Send "0" RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 1); for (int i = 0; i < HIGH_ZERO_CYCLES; i++) __asm__("NOP"); RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 0); for (int i = 0; i < LOW_ZERO_CYCLES; i++) __asm__("NOP"); } }     Testing and measuring the toggle timing with the RGPIO driver of Cortex M33, we could find the best number of NOP instructions to adjust with the required timing according to datasheet, and the results with core running at 200MHz are:    Parameter  Number of NOP times  HIGH_ONE_CYCLES  22  (T1H: 700 ns)  LOW_ONE_CYCLES  12  (T1L: 600 ns)  LOW_ZERO_CYCLES  20  (T0L: 800 ns)  HIGH_ZERO_CYCLES  6    (T0H: 350 ns)      Zero:   One:   Taking in mind this information, we can start to develop our application. From Cortex M33, we created a little protocol, that will wait for instructions to do.    For example, the expected string to fill the RPMSG buffer is:    Index  Purpose  Example  app_buf[0]  Command ('c' or 't')  'c' = store color in buffer  't' = show colors on LEDs  app_buf[1]  Red component (0–255)  0xFF  app_buf[2]  Green component (0–255)  0x00  app_buf[3]  Blue component (0–255)  0x80  app_buf[4]  LED index (target LED position)  e.g. 0, 1, 2    Commands:    'c'  "Color store"  This command stores the RGB color value into a local buffer, targeting a specific LED (app_buf[4]).  It doesn't update the LED strip immediately, it just prepares the data.  Example of RPMSG received buffer from Cortex A (Linux):   app_buf = { 'c', 0xFF, 0x00, 0x00, 2 };  // Store red color for LED 2     't'  "Transfer"  This command sends the full color buffer to the WS2812 strip, updating the LED colors.  The RGB values in the buffer are ignored, it simply triggers an update based on previously stored data.  Example of RPMSG received buffer from Cortex A (Linux):  app_buf = { 't', 0, 0, 0, 0 };  // Transfer the buffered colors to the LED strip     You can modify the code to add your custom commands like change number of LEDs on the strip, or change the GPIO, etc. Currently, the number of WS2812 LEDs supported is defined in software by NUM_RGB_LEDS. As default is 8 LEDs.    I will attach the full code for Cortex M33 firmware, it was tested with arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-eabi and SDK 2_15, SDK 2_16 and SDK 24.    In this example, the EXP_GPIO_IO24 of FRDM-IMX93 was used to control the LED Strip.   CORTEX A55 SIDE.  For Cortex A55 (Linux side), we developed an userspace application, that will create the structure for the buffer to send to the Cortex M33 and send through RPMSG using the imx_rpmsg_tty included on the NXP BSP. You can find the userspace application attached.    As we know, the imx_rpmsg_tty creates the tty channel called ttyRPMSG31 under /dev. So, this userspace application communicates directly with the device /dev/ttyRPMSG31 to send the buffer with the required structure for Cortex M33.    EXAMPLE OF USAGE.    STEP 1. Compile firmware for Cortex M33 and store in FRDM-IMX93 under /lib/firmware to use with remoteproc:   STEP 2.  Compile or cross-compile the userspace application (attached.)  To compile on the platform:  root@imx93evk:~# gcc wsled.c -o wsled root@imx93evk:~# ls wsled wsled.c Also, we can copy the wsled under /bin to practicity. root@imx93evk:~# wsled Error: -c <red> <green> <blue> is required. WS2812 Usage: wsled -c <red> <green> <blue> [-n <led_position>] Load the color of exact LED to the buffer wsled -t Shows the colors to the LEDs   STEP 3. To run the entire example: boot the board and load the firmware for cortex M33 with remoteproc: root@imx93evk:~# cd /sys/class/remoteproc/remoteproc0 root@imx93evk:/sys/class/remoteproc/remoteproc0# echo ws2812_m33.elf > firmware root@imx93evk:/sys/class/remoteproc/remoteproc0# echo start > state  Then, we will receive this from Cortex M33 terminal: RPMSG String Communication Channel FreeRTOS RTOS M33 clock is at: 200000000 Hz Nameservice sent, ready for incoming messages from Cortex-A55! WSLED   Load the imx_rpmsg_tty module in Linux to initialize RPMSG: root@imx93evk:~# modprobe imx_rpmsg_tty   Then, we will have the hello world message from Cortex A (Linux side), but with our buffer format in Cortex M33 console: CMD: h [1]:0x65 [2]:0x6c [3]:0x6c [4]: 111 LEN = 12   Finally, we are ready change colors of the LEDs: Load the buffer (LED 1 = RED, LED 2 = Green, LED 3 = Blue). root@imx93evk:~# wsled -c 0x55 0x00 0x00 -n 1 root@imx93evk:~# wsled -c 0x00 0x55 0x00 -n 2 root@imx93evk:~# wsled -c 0x00 0x00 0x55 -n 3   Show colors on LEDs. root@imx93evk:~# wsled -t    
View full article
What we need?  USB cable Windows Host PC MCU-LINK PRO What Do You Gain? With this firmware upgrade, you will be able to debug the M core of i.MX processors (such as i.MX8 and i.MX9). Also, the cost advantage due to the MCU-LINK PRO is currently the most affordable debugger available for i.MX processors.   Firmware Upgrade Steps   Install Required Tools Install the MCUXpresso IDE, or use the MCUXpresso Installer for VS Code to install the necessary software tools.     Download Firmware Get the latest firmware from the Segger web page   Save Firmware Save the downloaded firmware in the following directory: C:\nxp\LinkServer_1.6.133\MCU-LINK_installer\probe_firmware   Backup Old Firmware Rename the existing firmware file to keep a backup.   Example: Rename firmware.s19 to old_firmware.s19   Set Jumper and Connect Place a jumper on J4 and connect the MCU-LINK PRO to the host PC via USB.   Open LinkServer CLI Launch the LinkServer CLI. If it's not installed, download it from NXP web page.   Run the Update Script Execute the following commands in the terminal: $ cd MCU-LINK_installer $ scripts\program_JLINK.cmd   Start Firmware Flash Once the MCU-LINK PRO is detected, press any key to flash the Segger firmware.     Finalize Update After a successful update, remove the jumper from J4, disconnect and reconnect the MCU-LINK PRO   Verify Installation You can confirm that the debug probe is recognized using MCUXpresso IDE, or MCUXpresso for VS Code     References: MCU-Link installation   
View full article
This article explains how to get started with JTAG debugging of the Linux kernel running on the A55 of iMX93EVK. We will be using Lauterbach Trace32 to debug iMX93EVK. Here is a list of pre-requisites that is expected from the readers:- 1. Basic knowledge to get started on Trace32 - Please refer Learning and Training | Lauterbach TRACE32 2. You should have Linux source code and steps to build the kernel. 3. Trace32 Software with a license to debug A55 COMPONENTS   Hardware required: -   iMX93EVK running 6.6.52 BSP Lauterbach Power Debug E40 with a Debug cable Software required: - Trace32 Linux kernel source code   Linux Kernel Modifications Step 1:- In arch/arm64/configs/imx_v8_defconfig, please make sure that:- CONFIG_DEBUG_INFO_REDUCED=n CONFIG_DEBUG_INFO = y CONFIG_KALLSYMS=y   Step-2 :- Enabling JTAG debugging in Linux On iMX93EVK LPUART5 is MUX'd with the JTAG pins   so if we want to debug the linux kernel via JTAG, we will have to disable it. Go to the device tree source file - arch/arm64/boot/dts/freescale/imx93-11x11-evk.dts Change the status of the following node to 'disabled'     Step 2:- Build the kernel. vmlinux will be created as part of this. This has the Linux kernel along with the debug symbols required for Trace32 debugging. Step-3 At this point either you can copy the linux-imx folder to your local windows machine where Trace32 is installed, or you can simply map the linux machine as a network drive so that the same folder '/opt/samba/nxg05261/linux-imx' is accessible on windows. The motive of this exercise is to use 'vmlinux' and the linux source files present in this folder from trace32 cmm scripts that we will be executing.   Step-4 Replace the newly built kernel 'Image' - arch/arm64/boot/Image with the one present in the boot partition of imx93evk. You can simply copy this Image to iMX93EVK via scp and copy it to the folder - /run/media/boot-mmcblk0p1 Note:- Please make sure that the kernel version that is running on the box and the one you have built should be the same otherwise there will be debug symbols mismatch After copying the Image, reboot iMX93EVK. Debugging with Trace32 Step-1 Configuring Uboot bootargs Cpu idle state interferes with the JTAG debugging by impacting the clocks so we need to disable the cpu idle power management. We do this by appending "cpuidle.off=1" to the bootargs:- a. Stop at Uboot prompt. b. Execute command - setenv mmcargs "setenv bootargs ${jh_clock} ${mcore_clk} console=${console} root=${mmcroot}  cpuidle.off=1" [do not omit the inverted commas in the command] Step-2 Boot to Linux prompt   Step-3 Connect the USB cable of Lauterbach Power Debug probe to your windows machine and Open t32 - C:\T32\bin\windows64\t32start.exe   Select 'PowerView Instance' and click on 'Start'. A window like below will appear: -   Step- 4 Extract MMU translation info for the debugger For this either you can execute the below commands on the T32 in sequence: -   RESet SYStem.RESet SYStem.CPU IMX93-CA55 SYStem.JtagClock 10MHz SYStem.CONFIG.DEBUGPORTTYPE JTAG SYStem.Option EnReset OFF CORE.ASSIGN 1. 2. SYStem.Option MMUSPACES ON SYStem.Option IMASKASM ON SYStem.Mode Attach Data.LOAD.Elf <path_of_vmlinux> /NoCODE DO ~~/demo/arm/kernel/linux/board/generic-template/detect_translation.cmm OR simply edit the attached cmm script - detect_address_translation.cmm and modify the <path_of_vmlinux> as per your file location. Then execute it like this:- Do <file_path>/detect_address_translation.cmm In my case, this command was: - Do C:\Users\nxg05261\Documents\cmm_scripts\detect_address_translation.cmm Note:- <path_of_vmlinux> in my case was  C:\T32\demo\arm\bootloader\uboot\vmlinux. You can modify it as per the location where you have copied 'vmlinux' -- After executing the above commands, debugger address translation will be displayed: -    Now we will copy the above highlighted lines and paste it in the final cmm script that we will use for debugging. For readers' convenience this info has been collated into the final script - 'linux_attach_t32.cmm', attached with this blog.   Disclaimer:- The lines that are highlighted depends on the kernel version and customer design decisions, so it is strongly advised to take the output of detect_translation.cmm for your system and then paste it in the cmm script, instead of using the exact output that I have shown in the above picture. File -> Open File -> linux_attach_t32.cmm -- Click on 'Do' button to execute the script till the end. -- Set a breakpoint at start_kernel b.s start_kernel /Onchip   [Optional]Check the breakpoint via 'b.l'   -- Hit 'go' at t32 to let the cores execute the instructions, you will see 'running' state   -- Enter 'reboot' at Linux prompt and stop at Uboot command line prompt you will see trace32 at 'system down' state: - -- Execute 'system.mode.attach' at t32 to attach to the system, you will again see 'running' state -- Execute 'break' to stop the running state -- Check if the breakpoint 'start_kernel' still exist via command 'b.l' -- If you see the breakpoint is still set, Execute 'go' at t32 to take the cores to the running state. -- Then, at Uboot prompt, execute 'boot' so that it may load the linux kernel to the memory.   As soon as you do that you would see that Uboot will try to load kernel. The last print you will see on the serial console will be: - "Starting kernel …' the execution will stop and at t32 you will see that the breakpoint is hit, meaning the Program Counter is at the address of the function 'start_kernel'   Note- The Warning that you might observe[like in the above picture] means that trace32 is not able to find the source file 'main.c'. So you will not be able to see the 'C' source code at this point. To resolve this:- -- Right click on the 'List.auto' window where you see the assembly code. Click on 'Resolve Path' and navigate to the init/main.c in your kernel source code folder and click Open. You would see that the source path translation is now correct and you're able to view the disassembly as well as the source code: -     Now we will load kernel symbols and apply 2 breakpoints in the linux kernel to demonstrate kernel debugging:-   -- Load the kernel symbols Data.LOAD "C:\T32\demo\arm\bootloader\uboot\vmlinux"  H:0x0::0x0 /NoCODE /SOURCEPATH Z:\linux-imx   -- Apply breakpoints at t32 window b imx_rpmsg_init b imx_drm_bind   [Optionally] you can verify the breakpoints via 'b.l' These breakpoints are temporary as you can see in the above snapshot. That means after they are hit, they will be removed, so to make them permanent:- Right click the breakpoint -> Change -> Uncheck Temporary -> Click Ok like depicted in the following snapshots: -       Now, to reach the next breakpoint, execute 'go' on the t32 At this point linux kernel execution has reached the function imx_rpmsg_init   Again, to reach the next breakpoint, execute 'go'   So this is how you start debugging the linux kernel. Apart from this, there is a nice t32 feature called 'linux awareness' which allows you to easily debug the kernel loadable modules, user space applications amongst other things. To explore 'linux awareness', you can go about checking the 'Linux' drop down menu present at the top. Plenty of support documents are available on the web.       Feel free to drop in the comments section or DM if you have any queries. Happy debugging!!🙂🙂🙂🙂  
View full article
This guide provides a step-by-step approach for beginners looking to flash a custom Kernel Image or device tree on an NXP i.MX board. Sometimes, we need to customize the Kernel Image or modify the device tree for our board. Fortunately, NXP provides the UUU (Universal Update Utility) tool, which allows us to flash and use a custom Kernel Image or update the device tree on our board.   Requirements Before proceeding, ensure you have the following: - The latest version of the UUU Tool. - An i.MX EVK board (i.MX6, i.MX7, i.MX8, i.MX9). - The power supply for the board. - Two USB cables (USB-C or Micro USB, depending on your board).   Preliminary Steps To customize the Kernel Image or device tree, refer to the following community posts: - How to Fix FRDM-IMX93 Linux Kernel BSP - How to Compile Linux Kernel Image and Device Tree Using Yocto SDK   Once you have your customized Linux Kernel Image or device tree ready, follow the steps below to deploy it to your board.   Flashing the Kernel Image or Device Tree Connect and Prepare the Board 1. Connect the USB debug cable and the OTG cable from your board to your host computer. 2. Power on your board and stop the boot process at the U-Boot stage by pressing a key in the terminal. 3. Enter fastboot mode by running the following command in the U-Boot terminal: u-boot -> fastboot 0   Flash the Custom Kernel Image or Device Tree   4. Open a terminal on your host computer and navigate to the directory containing the new Kernel Image or device tree. 5. Flash the new files using the following command: $ uuu -b fat_write <file_name> mmc <device>:<partition> <file_name_in_board> Example: $ uuu -b fat_write imx93-11x11-evk.dtb mmc 0:1 imx93-11x11-evk-custom.dtb In this example, the file imx93-11x11-evk.dtb stored on the host machine is flashed to the board's eMMC device, saving it as imx93-11x11-evk-custom.dtb.   Note: If you are using Linux, run the command with sudo. - For eMMC and SD card, the command is the same; just ensure you use the correct device number. - On the i.MX93, device 0 corresponds to eMMC, and device 1 corresponds to the SD card.   Update U-Boot Environment Variables   6. Exit fastboot mode by pressing CTRL+C. This returns you to the U-Boot terminal. 7. Set up the environment variablesto use the new files: For the Kernel Image: u-boot -> setenv image <custom_image_name> u-boot -> saveenv u-boot -> reset For the Device Tree: u-boot -> setenv fdtfile <custom_device_tree_name> u-boot -> saveenv u-boot -> reset The board should now boot using your modified Kernel Image and device tree.  
View full article
This guide provides step-by-step instructions for setting up and applying necessary patches to the Linux kernel for the FRDM-IMX93 development board. The process involves cloning the required repositories, applying patches, and preparing the kernel for customization and compilation.   Prerequisites Required Software: A Linux-based operating system (Ubuntu/Debian recommended). Git installed (sudo apt install git). Yocto dependencies: $ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 python3-subunit zstd liblz4-tool file locales libacl1 ​   Hardware: FRDM-IMX93 Board Sufficient storage space   1. Downloading the Repository Start by downloading the necessary tools and repository. If the ~/bin folder does not already exist, create it: $ mkdir ~/bin (this step may not be needed if the bin folder already exists) $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo $ export PATH=~/bin:$PATH   2. Compile the Yocto SDK: $: mkdir Yocto_SDK $: cd Yocto_SDK $: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml $: repo sync $: MACHINE=imx93evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland $: bitbake imx-image-full -c populate_sdk   Run the generated .sh file to install the SDK: sudo ./fsl-imx-xwayland-glibc-x86_64-imx-image-full-armv8a-imx93evk-toolchain-6.6-scarthgap.sh   The final .sh file is located in: bld-xwayland/tmp/deploy/sdk/   3. Creating the Working Directory First, create a dedicated directory for the kernel setup and navigate into it: $ mkdir FRDM-IMX93-Kernel $ cd FRDM-IMX93-Kernel   4. Cloning the Kernel patches Retrieve the necessary kernel patches from the NXP repository: $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git -b lf-6.6.36-2.1.0   5. Cloning the Kernel Repository (linux-imx repository) Clone the kernel source of Yocto SDK that you built earlier: $ git clone https://github.com/nxp-imx/linux-imx.git -b lf-6.6.36-2.1.0 6. Applying Kernel Patches Apply the necessary patches to the kernel: $ cd linux-imx/ $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0001-gpio-pca953x-fix-pca953x_irq_bus_sync_unlock-race.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0002-arm64-dts-add-i.MX93-11x11-FRDM-basic-support.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0003-arm64-dts-add-imx93-11x11-frdm-mt9m114-dts.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0004-Add-DSI-Panel-for-imx93.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0005-Add-CTP-support-for-waveshare-panel.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0006-arm64-dts-add-imx93-11x11-frdm-tianma-wvga-panel-dts.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0007-arm64-dts-add-imx93-11x11-frdm-aud-hat-dts.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0008-arm64-dts-add-button-support.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0009-arm64-dts-add-imx93-11x11-frdm-ov5640-dts.patch $ cd linux-imx/ $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0010-arm64-dts-add-imx93-11x11-frdm-ld.dts-for-lpm.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0011-arm64-dts-add-pwm-function-of-the-LED.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0012-arm64-dts-add-imx93-11x11-frdm-8mic.dts.patch $ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0013-arm64-dts-add-imx93-11x11-frdm-lpuart.dts.patch   7. Customizing the Device Tree Device trees can be modified or created based on your hardware setup.   Device Tree Locations: arch/arm64/boot/dts/freescale/   If you create a new device tree, add it to the respective Makefile: arch/arm64/boot/dts/freescale/Makefile   8. Setting Up the Cross-Compilation Environment To prepare for kernel compilation, source the environment setup script. Assuming the Yocto SDK is installed in /opt, run:   EXAMPLE: $ source /opt/fsl-imx-xwayland/6.6-scarthgap/environment-setup-armv8a-poky-linux   9. Configuring the Kernel Make configuration adjustments as needed in the file: arch/arm64/configs/imx_v8_defconfig Use the appropriate configuration command: $: make imx_v8_defconfig   10. Compiling Device Trees Only To compile only the device tree files, run: $: make dtbs   11. Compiling the Kernel Finally, compile the kernel image using: $ make -j $(nproc)   The resulting kernel image will be located in: arch/arm64/boot/   References: IMX YOCTO PROJECT USERS GUIDE IMX LINUX USERS GUIDE  IMX REFERENCE MANUAL 
View full article
We are pleased to announce that Config Tools for i.MX v24.12 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) • DDR tool – Support for the custom System Manager image import is added. – i.MX 95 advanced tests are enabled: Vref for DQ and Vref for CA optimization • SerDes tool – Additional parameters for TX configuration on GUI (swing, margin, equalization) for i.MX 95 are added. – PCIe Gen1/Gen2/Gen3 switch on pattern generation. • Clocks – Modular clocks initialization is supported. – Initialization mode is visible in the Clocks diagram and Details view. – New Modular Initialization view for configuration of the initialization mode and core selection of the module is created. • TEE – Configuration and overview of areas with the same address and different address space is supported. – Code generation can be toogled for global options groups. – The process for releasing ELE crypto before setting up TRDC is supported. • Pins – Miscellaneous tab for various Pins configuration options is added. – Filtering for routing dialogs is added.
View full article
Config Tool Introduction and Use From i.MX93 using the Config Tool for the DDR configure. The Config Tools for i.MX is a suite of evaluation and configuration tools that help users from initial evaluation to production software development. Config Tools for i.MX is an easy-to-use way to configure the pins and DDR of the i.MX processor devices. The software, in general, enables you to create, inspect, change, and modify any aspect of the pin configuration and muxing of the device. It also allows you to configure and validate DDR settings. 1 Download and install The link in website: https://www.nxp.com/design/design-center/software/i-mx-developer-resources:IMXSW_HOME   The Config Tools for i.MX is installed as a desktop tool which then loads additional device information through a network connection, but does otherwise not need internet connection. It does not require a project setup, as all the settings are stored in text and generated source files, which then can be easily stored in a version control system or exchanged with other users. Config Tool function For the Config Tool have two function, one is the Pins tool another is the DDR tool functions. 1.1 Pins tool The Pins Tool makes pin configuration easier and faster with an intuitive and easy user interface, which then generates normal C code that can then be used in any C and C++ application. The Pins Tool configures pin signals from multiplexing (muxing) to the electrical properties of pins, and it also creates Device Tree Snippets Include (.dtsi) files and reports in CSV format. Pins Tool Configuration of pin routing/muxing Managing different functions used for routing initialization Configuration of pin functional/electrical properties Generation of code for routing and functional/electrical properties 1.2 DDR Tool   The DDR tool provides two main functionalities: configuration and validation. The DDR configuration provides a user-friendly graphical interface to configure the DDR controller and the DDR PHY. It can be used for tweaking some of the configuration parameters when you want to use different memory modules than the ones received with the board or when you want to optimize the configuration. DDR validation provides different scenarios to verify the DDR performance, by downloading a test image to the processor’s internal RAM through a USB connection. The result is sent to the DDR tool via the UART. DDR validation can help verify DDR stability on the board in a non-OS environment.   DDR Tool The DDR tool is designed for: Configuration of DDR controllers Validation of DDR configuration Support for i.MX 8M and i.MX93 families Configuration: Simplified UI for device configuration Advanced board configuration options Stressing: Stress tests with overnight option Optimization: Sweep ODT configuration and optimization of Vref for DQ and CA Virtual Timing Signal Analysis (vTSA) support: RX and TX data eye, CA BUS signals margin and CA Eye test for LPDDR4 DRAM Generation of C code for U-boot SPL driver The DDR tool allows you to view and configure basic DDR attributes, such as memory type, frequency, number of channels and others and test the DDR configuration by a variety of tests. After you have specified the connection type, you can choose scenarios, tests to run in these scenarios, and view the test results, logs, and summary.         2 Install Download Config_Tools_for_i.MX_v16_x64.exe   Note: In our company PC we need to apply the Admin Manage:   Config Tools for i.MX is available offline (local)  Minimum system requirements One of the following graphical operating systems: – Microsoft Windows 10 (64-bit) – Ubuntu 22.04 LTS Note: Linux-hosted variants of tools are distributed on Linux as 64-bit binaries, which may not work on 32-bit systems. – Supported desktop environments: GNOME – Mac OS X (12.x) 4 GB RAM Display with resolution 1024 x 768 Internet connection for dynamic download from processor database Note: If the MacOS is set to Traditional Chinese, Config Tools for i.MX starts in English and not Chinese. This is intended. 2 The use of the Config tool Configuration of DDR controllers 2.1 Creating a new configuration create a configuration from the Start development wizard or by selecting File > New from the Menubar. If you start creating your development for any NXP board or kit, we recommended you start with example to create a configuration for a board or a kit. Such configuration contains board-specific settings. If you select a processor, the configuration will be empty. 2.2 Run the Config tool Open the Config tool, choose the Creating a new standalone configuration for a processor, board, or kit   Choose the Processor   Choose the i.MX93 part number product     Choose DDR Under the tool select the tools---->DDR Three sections need to mentioned: Make DDR configure right and make the DDR is enabled already.   Two sections are very important the same as the tool we supply before in the old product: DDR paramaters configuration DDR stress test(Validation)   DDR parameters configuration:   This is the UART Port configure, for the i.MX93 EVK Board default use the UART1 for A55 core debug, if in customer’s design use others port can choose here and also need modify the register settings manually.       Advanced parameters config, it is very important:   General advice The I2C connection between MX and PMIC should be consistent with the development board, using the same pad. If choose different , Need to modify I2C     Validation of DDR configuration In the previous DDR stress test tool, only two functions were provided: DDR calibration and stress test. In the new Config tool, more testing items are provided for customers to debug DDR, totaling four items.   When finished the DDR configuration then go to do the validation.     Test DDR initialization script, Perform basic read and write operations   If pass the test, it will be OK. If failed, we need to fail shooting for it. According to the log output information, check boot mode/UART/USB, etc If the test fails, first check the boot mode configuration and UART/USB interface. The previous DDR stress test tool would output statements such as "Please set in serial download mode" or "Please connect UART port", which are obvious. The current Config tool outputs all log information of the code, with a lot of content and no erroneous conclusions. We need to carefully review the log output to identify where the problem lies. Test on the i.MX93 EVK Board, if the boot mode not right and the USB is not connected, when do the test there will be the ERROR Messages in the logs:   Test on the i.MX93 EVK Board, if not with proper UART port, the ERROR Messages in the logs:   Optimization test This requires detailed ODT, driver strength testing, and scanning of all DQ IO configuration options, Test whether each configuration is passed or failed. Finally, output the mapping between the read/write drive strength and ODT output. For the test result when reading, the impedance of DRAM driven strength and PHY ODT cannot be set too big, (Green - pass, Orange - fail)   When determining the optimal ODT/driver strength value for the customer's board, this mapping diagram can be used as a reference, but it cannot be the sole basis for making this decision. If the customer fully references the NXP development board for design, they can first use the default configuration of the development board for testing. Then fine tune it.     VTSA (Virtual Timing Signal Analysis) Generate write and read data eye diagrams by running a series of write/read operations. (Different from using a high-speed oscilloscope for manual physical TSA (pTSA) measurement). Use the DDR controller itself to test margin by writing margin (Diag Write Margin)/diagnosing read margin (Diag Draw a virtual data eye diagram for each DQ channel during the Read Margin test. This tool differs from the actual eye diagram results and is for reference only.     DDR Stress Test The last step, stress test, customer can choose long time test:     Code generate In the right side we can see the lpddr4_timing.c generate, using for the uboot. For this tool, the code can be automatically generated and automatically generated code when the registers change, and do not need to run the test on the board, this is difference with the old tool.   3 i.MX93 UBOOT and Kernel DDR configuration 3.1 The DDR configuration in the Uboot (1) Copy the generated lpddr4x_timing.c to uboot path: board/freescale/imx93_evk/lpddr4x_timing.c       (2) DDR Size setting uboot-imx/include/configs/imx93_evk.h The default size is 2GB for the i.MX93 EVK board.   For the i.MX93EVK uses 2GB LPDDR4X. If using 1GB/512MB LPDDR4, it is important to note that the size of the DDR is related to the memory map address.   According to the Memory map, starting from 0xC000_0000 is 1GB of DRAM space, and starting from 0xA000_0000 is 512MB of DRAM space.               3.2 The DDR configuration align in the Kernel For the 1GB LDDR4/4X device tree modify For the i.MX93 the NPU is accessed through M-core, so a section of DRAM memory is reserved. Regardless of whether NPU is used or not, ethos must be changed here, otherwise starting the kernel may result in errors. Change the address space to within 1GB and appropriately reduce the memory allocation size. arch/arm64/boot/dts/freescale$ vi imx93-11x11-evk.dts         Summary: Config tool is NXP's new DDR script generation/stress testing/OMUX allocation tool, which is required for i.MX93. Other i MX chips can also use this tool. The Config tool provides more DDR testing projects, including testing ODT/driver capabilities and outputting mapping maps, generating DDR virtual eye diagrams, etc., making it easy to test DDR conditions from multiple perspectives. It is recommended to use the Config tool to debug ODT/driver capabilities and other parameters, which is also applicable to all i MX chip, as a debugging tool for reference. The theoretical parameters of the actual board should refer to the simulation results of the board or the measured results of DDR signals. Any questions contact us freely.  
View full article
This document is about enable iMX93 PWM and PWM led HW:   iMX93 11x11 EVK SW:   lf-6.6.3-1.0.0 PWM: TPM3 CH0, CH2            TPM4 CH2 Note: The i.MX PWM and           PWM led are already            enabled in lf-6.6.3-1.0.0  
View full article
Overview This document explains how to use Pulse Width Modulation (PWM) on the iMX93 EVK Board. Attached to this post is a patch to enable this functionality, which can be integrated into either Yocto or a standalone kernel compilation.   This procedure was tested on iMX93 EVK A0 silicon version with BSP 6.1.22 version, this feature should work on A1 silicon version too but is not tested yet.   Kernel Configuration: To enable PWM support, modify the imx_v8_defconfig  file by adding the following line: CONFIG_PWM=y CONFIG_PWM_ADP5585=y CONFIG_PWM_CROS_EC=m CONFIG_PWM_FSL_FTM=m CONFIG_PWM_IMX27=y CONFIG_PWM_RPCHIP=y CONFIG_PWM_SL28CPLD=m + CONFIG_PWM_IMX_TPM=y​ # Add this line   Device Tree Modifications: You will need to add the following nodes to the device tree to configure the TPM (Timer/Pulse Width Modulation) controller:   + &tpm4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_tpm4>; + status = "okay"; + }; ... + pinctrl_tpm4: tpm4grp { + fsl,pins = < + MX93_PAD_GPIO_IO05__TPM4_CH0 0x19e //EXP_GPIO_IO05 J1001 29 + >; + };​   Compiling and Flashing: After making the above changes, compile the kernel and device tree. Once the compilation is complete, flash the new image and device tree to the iMX93 EVK Board.  PWM Configuration on the Board After flashing, you can configure the PWM settings on the board. Open a terminal and execute the following commands: $ cd /sys/class/pwm/pwmchip1/ $ echo 0 >> export $ echo echo 2000000 >> pwm0/period # Set period to 2,000,000 ns (2 ms) $ echo echo 1000000 >> pwm0/duty_cycle # Set duty cycle to 1,000,000 ns (1 ms) $ echo 1 >> pwm0/enable   Validation To validate the PWM output signal, check pin 29 of connector J1001 on the iMX93 EVK Board.   Conclusion Following these steps should enable PWM functionality on your iMX93 EVK Board. If you encounter any issues, please refer to the documentation or reach out for assistance. Best Regards! Chavira
View full article
The Gui-guilder doesn't provide remote debug function in IDE and we still need use Yocto to build project or copy binary to board rootfs. This knowledge base will provide a solution about how to use VSCode to remote debug LVGL project on i.MX93 EVK board.    Yocto toolchain: L6.6.x GUI GUILDER: v1.8.0   Need to open GUI GUILDER project in VSCode.   1.Scripts in VScode   1.1 build.sh Modify build.sh in <LVGL project>/ports/linux     #!/bin/sh toolchain=$1 if [ -z "$toolchain" ];then toolchain=/opt/fsl-imx-xwayland/6.1-mickledore/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake if [ ! -r $toolchain ];then toolchain=/opt/fsl-imx-xwayland/6.1-langdale/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake fi fi toolchain_path=$(echo $toolchain |sed -E 's,^(.*)/sysroots/.*,\1,') toolchain_arch=armv8a-poky-linux if [ ! -r $toolchain -o ! -r "$toolchain_path/environment-setup-$toolchain_arch" ];then echo "ERROR: Yocto Toolchain not installed?" exit 1 fi if [ -n "$BASH_SOURCE" ]; then ROOTDIR="`readlink -f $BASH_SOURCE | xargs dirname`" elif [ -n "$ZSH_NAME" ]; then ROOTDIR="`readlink -f $0 | xargs dirname`" else ROOTDIR="`readlink -f $PWD | xargs dirname`" fi BUILDDIR=$ROOTDIR/../build rm -fr $BUILDDIR mkdir $BUILDDIR . "$toolchain_path/environment-setup-$toolchain_arch" echo "start build..." cd $ROOTDIR/linux/lv_drivers/wayland/ cmake . make cd $BUILDDIR toolchain_path=/opt/fsl-imx-wayland/6.6-scarthgap/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake cmake -G 'Ninja' .. -DCMAKE_TOOLCHAIN_FILE=$toolchain_path -Wno-dev -DLV_CONF_BUILD_DISABLE_EXAMPLES=1 -DLV_CONF_BUILD_DISABLE_DEMOS=1 -DCMAKE_CXX_FLAGS="-ggd3 -O0" -DCMAKE_BUILD_TYPE=Debug ninja if [ -e gui_guider ];then echo "Binary locates at $(readlink -f gui_guider)" ls -lh gui_guider fi # Copy binary to board scp $BUILDDIR/gui_guider root@192.168.31.243:/opt     1.2 tasks.json     { "version": "2.0.0", "tasks": [ { "label": "Build", "type": "shell", "command": "./build.sh /opt/fsl-imx-wayland/6.6-scarthgap", "options": { "cwd": "${workspaceFolder}/ports/linux" }, "problemMatcher": [ "$gcc" ], } ] }       1.3 launch.json   miDebuggerServerAddress is board ip address.     { "version": "0.2.0", "configurations": [ { "name": "(gdb) Launch", "preLaunchTask": "Build", "type": "cppdbg", "request": "launch", "program": "${workspaceFolder}/build/gui_guider", "args": [], "stopAtEntry": false, "cwd": "${workspaceFolder}/", "environment": [], "externalConsole": false, "MIMode": "gdb", "logging": { "engineLogging": true, "trace": true, "traceResponse": true }, "debugStdLib":true, "miDebuggerPath":"/usr/bin/gdb-multiarch", //DO NOT USE GDB IN SDK!!!! "miDebuggerServerAddress": "192.168.31.243:12345", "setupCommands": [ { "description": "Enable pretty-printing for gdb", "text": "-enable-pretty-printing", "ignoreFailures": true, "text": "set remotetimeout 100", } ] }] }       2. Launch gdbserver on board     export SHELL=/opt/gui_guider gdbserver 192.168.31.243:12345 /opt/gui_guider       3. Debug in VSCode   Click (gdb)launch, the source code will be compiled. Then you will see the breakpoint in program. Enjoy your debug~    
View full article
Ftrace is powerful tracing utility embedded in Linux kernel. It provides a very good method for kernel developer to get insights of the kernel behavior. While official kernel doc for ftrace is somehow long and complex, this document provides a quicker and simpler way to get start with ftrace.
View full article
Hello! In this time, we will look how the i.MX93 GPIOs IRQs works, also I will focus on Cortex M33 side with SDK 2_16_0 but also tested on 2_15.   We can see in this other post, how the i.MX8M family works, but for i.MX93 this is a little different because there are a Secure/Non-Secure options and Privilege/Non-Privilege.   According to reference Manual and SDK LED example, we must to set the PCNS and ICNS registers to 0x00 to set in Secure access.    Materials Used: i.MX93EVK Jumper cable to connect GPIO2_IO02 with GPIO2_IO03 SDK 2_16_0 from MCUXpresso SDK Builder Source power for i.MX93EVK USB C Cable for serial debug USB C Cable to transfer .bin ro EVK   The Cortex-M33 processor supports Secure and Non-secure security states, Thread and Handler operating modes, and can run in either Thumb or Debug operating states. In addition, the processor can limit or exclude access to some resources by executing code in privileged or unprivileged mode. Code can execute as privileged or unprivileged. Unprivileged execution limits or excludes access to some resources appropriate to the current security state. Privileged execution has access to all resources available to the security state. Handler mode is always privileged. Thread mode can be privileged or unprivileged. You can find this information in the ARM documentation.   To resume this post, we will focus just in the necessary registers to configure properly a GPIO as IRQ input.   On this example, we will take the i.MX93EVK board. The GPIO2_IO02 will be configured as an output and the GPIO2_IO03 will be configured as an input with Rising edge IRQ. On each GPIO2_IO02 Rising edge, the software will detect an IRQ.     At first, we need to configure our IOMUX: void BOARD_InitPins(void) { IOMUXC_SetPinMux(IOMUXC_PAD_GPIO_IO02__GPIO2_IO02, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_GPIO_IO03__GPIO2_IO03, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_UART2_RXD__LPUART2_RX, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_UART2_TXD__LPUART2_TX, 0U); IOMUXC_SetPinConfig(IOMUXC_PAD_GPIO_IO02__GPIO2_IO02, IOMUXC_PAD_DSE(15U) | IOMUXC_PAD_FSEL1(2U) | IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_GPIO_IO03__GPIO2_IO03, IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_UART2_RXD__LPUART2_RX, IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_UART2_TXD__LPUART2_TX, IOMUXC_PAD_DSE(15U)); }   Then, we can start to code. Using as an starting point we can use the SDK/boards/mcimx93evk/driver_examples/rgpio/led_output example. Our definitions (PIN_OUT_RGPIO and PIN_IN_RGPIO are the same GPIO2 but it is just for good practice):😞 /******************************************************************************* * Definitions ******************************************************************************/ #define PIN_OUT_RGPIO GPIO2 #define PIN_IN_RGPIO GPIO2 #define PIN_OUT_RGPIO_PIN 2U #define PIN_IN_RGPIO_PIN 3U   Then, our IRQ handler: void Reserved73_IRQHandler(void) { RGPIO_ClearPinsInterruptFlags(PIN_IN_RGPIO, kRGPIO_InterruptOutput0, 1U << PIN_IN_RGPIO_PIN); PRINTF("\r\n IRQ.........\r\n"); SDK_ISR_EXIT_BARRIER; }   Why Reserved73_IRQHandler? That is the correspondent for GPIO2, you can look this on SDK/devices/MIMX9352/gcc in the file called startup_MIMX9352_cm33.S:   Basically, the interruption will clear the IRQ flag and print a little message.   Now, here we have the complete main function, we will break down the most important points. int main(void) { /* Define the init structure for the output pin*/ rgpio_pin_config_t pin_out_config = { kRGPIO_DigitalOutput, 0, }; rgpio_pin_config_t pin_in_config = { kRGPIO_DigitalInput, 0, }; /* Board pin, clock, debug console init */ /* clang-format off */ const clock_root_config_t rgpioClkCfg = { .clockOff = false, .mux = 0, // 24Mhz Mcore root buswake clock .div = 1 }; /* clang-format on */ BOARD_InitBootPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); CLOCK_SetRootClock(EXAMPLE_RGPIO_CLOCK_ROOT, &rgpioClkCfg); CLOCK_EnableClock(EXAMPLE_RGPIO_CLOCK_GATE); CLOCK_EnableClock(kCLOCK_Gpio2); /* Set PCNS register value to 0x0 to prepare the RGPIO initialization */ PIN_OUT_RGPIO->PCNS = 0x0; PIN_IN_RGPIO->ICNS = 0x0; /* Print a note to terminal. */ PRINTF("\r\n RGPIO Driver example\r\n"); PRINTF("\r\n An IRQ will happen each GPIO2_IO02 Rising edge\r\n"); /* Init output PIN GPIO. */ RGPIO_PinInit(PIN_OUT_RGPIO, PIN_OUT_RGPIO_PIN, &pin_out_config); /* Init Input with IRQ Pin GPIO*/ RGPIO_SetPinInterruptConfig(PIN_IN_RGPIO, PIN_IN_RGPIO_PIN, kRGPIO_InterruptOutput0, kRGPIO_InterruptRisingEdge); EnableIRQ(GPIO2_0_IRQn); RGPIO_PinInit(PIN_IN_RGPIO, PIN_IN_RGPIO_PIN, &pin_in_config); while (1) { SDK_DelayAtLeastUs(1000000U, SystemCoreClock); RGPIO_PortToggle(PIN_OUT_RGPIO, 1u << PIN_OUT_RGPIO_PIN); } }   As we can see, we need set the GPIO2 PCNS register to 0x00:   Pin Control Nonsecure (PCNS) Configures secure or nonsecure access protection for each pin. You can write to this register only in the Secure-Privilege state if it is not locked (LOCK[PCNS] = 0).   Also the ICNS register to 0x00.   Interrupt Control Nonsecure (ICNS) Configures secure and nonsecure access protection for each interrupt, or DMA request. You can update this register only in the Secure-Privilege state if it is not locked (LOCK[ICNS] = 0).   Now, we can compile and run the example. On each GPIO2_IO02 Rising edge, the CM33 will detect an IRQ in GPIO2_IO03 (short those pads as showed in the image at first of the post).     I will attach the full .c file.   I hope this information can helps to everyone.   Best regards, --... ...-- Salas.
View full article
The following steps allow to make use of device tree overlay files, a definition of device tree overlay provided by kernel.org is the next:  "A Devicetree’s overlay purpose is to modify the kernel’s live tree, and have the modification affecting the state of the kernel in a way that is reflecting the changes. Since the kernel mainly deals with devices, any new device node that result in an active device should have it created while if the device node is either disabled or removed all together, the affected device should be deregistered." Knowing that, in this post will be used as an example the baseboard "i.MX 93 EVK" and will be added with device tree overlay an LVDS panel, adding an automatic detection from u-boot, and will be used a host with linux version Ubuntu 20.04.2. Note: It only works for linux kernel version 6.6.3-nanbield onward. Linux device-tree overlay from linux-imx   This section explains all about device tree overlay compilation and building, to create a .dtso file, the equivalent of .dts for overlays, adding some difference between them, using as base the linux-imx repository. It can be downloaded from the following repository:   git clone https://github.com/nxp-imx/linux-imx.git -b <branch version>   Branch version used by this post "lf-6.6.3-1.0.0". Device tree source overlay (.dtso)    It can be similar to a device tree source (.dts) but it had little difference between them, there are some difference in the next list: There's another type of files to be included, if is used pinmux it's necessary adding it with "#include "imx93-pinfunc.h"" and libraries from dt-bindings, it depends on the type of device tree to implement "#include <dt-bindings/<library>>" At initialization it needs to add: "/dts-v1/;"  "/plugin/;" Addition of "fragment" nodes, it allow override parts of a device tree,  it can be a specific node or create a new node. following structure it's the structure of a fragment:   { /* ignored properties by the overlay */ fragment@0 { /* first child node */ target=<phandle>; /* phandle target of the overlay */ or target-path="/path"; /* target path of the overlay */ __overlay__ { property-a; /* add property-a to the target */ node-a { /* add to an existing, or create a node-a */ ... }; }; } fragment@1 { /* second child node */ ... }; /* more fragments follow */ }   kernel.org Overlays can't delete a property or a node when it's applied, so can't be used "/delete-node/" nor "/delete-prop/", but it can be added to the node "status = "disabled";" to disable it.  Using as an example the file imx93-11x11-evk-boe-wxga-lvds-panel.dts located in the previous repository file direction <linux-imx path>/arch/arm64/boot/dts/freescale/ using it as a base tree:   // SPDX-License-Identifier: (GPL-2.0+ OR MIT) /* * Copyright 2022 NXP */ #include "imx93-11x11-evk.dts" / { lvds_backlight: lvds_backlight { compatible = "pwm-backlight"; pwms = <&adp5585pwm 0 100000 0>; enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>; power-supply = <&reg_vdd_12v>; status = "okay"; brightness-levels = < 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100>; default-brightness-level = <80>; }; ... }; ... &adv7535 { status = "disabled"; }; ...   imx93-11x11-evk-boe-wxga-lvds-panel.dts Using the previous points and making use of fragments, if we want adapt the node lvds_backlight as fragment, it will be  added in the section of overlay, and adding it to a target-path "/":   #include <dt-bindings/interrupt-controller/irq.h> #include "imx93-pinfunc.h" #include <dt-bindings/gpio/gpio.h> /dts-v1/; /plugin/; / { fragment@0 { target-path = "/"; __overlay__ { lvds_backlight: lvds_backlight { compatible = "pwm-backlight"; pwms = <&adp5585pwm 0 100000 0>; enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>; power-supply = <&reg_vdd_12v>; status = "okay"; brightness-levels = < 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100>; default-brightness-level = <80>; }; }; }; ... };   imx93-11x11-evk-test-lvds-panel.dtso In the case of adding a property to an existing node, it will look in the following way using as example the node adv7535.   ... / { ... fragment@2 { target = <&adv7535>; __overlay__ { status = "disabled"; }; }; ... };   imx93-11x11-evk-boe-wxga-lvds-panel.dts At the end of this post, will be attach the complete file used for LVDS panel named as imx93-11x11-evk-test-lvds-panel.dtso Build device tree blob for overlay (dtbo)   To compile the previous .dtso it's necessary to include it to linux-imx repository, linux device tree overlay was included in BSP from version 6.6.3-nanbield onward in Makefile, so it's only necessary adding it as files to be compiled as .dtso, at the end of the post will be a patch file named as linux-imx-makefile.patch to add LVDS-panel to Makefile from branch lf-6.6.3-1.0.0 Add previously file imx93-11x11-evk-test-lvds-panel.dtso to path <linux-imx path>/arch/arm64/boot/dts/freescale/ Add imx93-11x11-evk-test-lvds-panel.dtso as file to be compiled in Makefile, it is located in the next path <linux-imx path>/arch/arm64/boot/dts/freescale/Makefile, it can be added with the next sentence format: <overlay without extension>-dtbs := <file to be overlayed>.dtb <overlay>.dtbo Example of how to add LVDS panel to makefile  imx93-11x11-evk-test-lvds-panel-dtbs := imx93-11x11-evk.dtb imx93-11x11-evk-test-lvds-panel.dtbo Makefile From main path, make the configuration to be compiled with the following bash command: $ cd <linux-imx path>/ $ make -j$(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- imx_v8_defconfig​ Compile overlay to use $ make -j $(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- freescale/<overlay>.dtbo​ as example for LVDS panel $ make -j $(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- freescale/imx93-11x11-evk-test-lvds-panel.dtbo It will compile the device tree blob overlay to use. Copy .dtbo generated in memory used by i.MX 93, it can be sending it from scp. scp ./​<overlay>.dtbo​ root@<ip>:/run/media/<memory section used> u-boot   This section explain the procedure to load a device tree overlay, it will be from u-boot explaining commands used and using the LVDS panel as an example. Before applying overlay   Before applying, it's necessary had a device tree loaded so looking around in the process of booting in a i.MX 93 from u-boot, this process is defined by the enviroment variable "bsp_bootcmd" that calls the variable mmcboot, and looking what does these variables, it can be look in the following sentence:    bsp_bootcmd=echo Running BSP bootcmd ...; mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if test ${sec_boot} = yes; then if run loadcntr; then run mmcboot; else run netboot; fi; else if run loadimage; then run mmcboot; else run netboot; fi; fi; fi; fi; mmcboot=echo Booting from mmc ...; run mmcargs; if test ${sec_boot} = yes; then if run auth_os; then run boot_os; else echo ERR: failed to authenticate; fi; else if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if run loadfdt; then run boot_os; else echo WARN: Cannot load the DT; fi; fi;fi;   but reducing it in a normal situation, ignoring if else case and echoes, it can be simplify to:   mmc dev ${mmcdev}; run loadimage; run mmcargs; run loadfdt; run boot_os;   the device tree is load is in the section "run loadfdt" with fatload in his definition:   loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr_r} ${fdtfile}   So, it's necessary to applying device tree overlay after "run loadfdt". How to apply an overlay   To load correctly an overlay it's necessary to following some steps: Load flattened device tree (fdt). (executed by loadfdt) Configure fdt address.  In some cases it's necessary to expand fdt memory size Load overlay Apply overlay The full sentence to apply it, it's the following u-boot command:   u-boot=> setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr ${fdt_addr} && fdt resize ${fdt_buffer}; fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} <overlay>.dtbo && fdt apply ${fdtovaddr};   First of all, setexpr it's just to create a new variable, in this case these variable is an integer. Spliting the previously command we can found the steps to applying it. "fdt addr ${fdt_addr};" used to configure fdt address, and point to the space of memory previously charged. "fdt resize ${fdt_buffer};" expand fdt memory size, is used as a value 16384 just to get the enough space to charge dtbo, this number was related with 2 14 "fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} <overlay>.dtbo" Load device tree overlay using fdovaddr, that is fdt_addr adding an offset of memory space.  "fdt apply ${fdtovaddr};" apply device tree overlay Remembering about load overlay needs to be executed after loadfdt, it's possible to save the previous command to a variable and executing it after loadfdt with setexpr, in this case using as example lvds test.   u-boot=> setenv loadoverlay "setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr $\{fdt_addr\} && fdt resize $\{fdt_buffer\}; fatload mmc $\{mmcdev\}:$\{mmcpart\} $\{fdtovaddr\} imx93-11x11-evk-test-lvds-panel.dtbo && fdt apply $\{fdtovaddr\};"   and modifying mmcboot with loadoverlay after loadfdt   u-boot=> setenv mmcboot "run mmcargs; run loadfdt; run loadoverlay; run boot_os;"   to save the environment variables created, it can be saved from u-boot wit the following command.   u-boot=> saveenv   At the end, boot imx93   u-boot=> boot   The LVDS panel should be working using the original dtb (imx93-11x11-evk.dtb) applied the overlay. Automatize u-boot LVDS Panel   This section explain how can be automatize the u-boot load overlay using an LVDS panel, it can vary depending the device to used for, the method used is detecting it in u-boot initialization and if found any device it will generate an environment variable. All the steps was using as a base uboot-imx repository, it can be downloaded from the following repository, at the end of this post will be a patch with the changes.   git clone https://github.com/nxp-imx/uboot-imx.git -b <branch version>   Branch version used "lf-6.6.3-1.0.0". Base   Knowing more about LVDS Panel used by imx93 it's really hard know more information about registers, so in this example will be limited to detect that is connected the address to a corresponding bus from touch controller.  To know i2c address and bus used by LVDS panel it was used searching it from the original device tree in the next section:   &lpi2c1 { exc80h60: touch@2a { compatible = "eeti,exc80h60"; reg = <0x2a>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_ctp_int>; /* * Need to do hardware rework here: * remove R131, short R181 */ interrupt-parent = <&gpio2>; interrupts = <21 IRQ_TYPE_LEVEL_LOW>; reset-gpios = <&pcal6524 17 GPIO_ACTIVE_HIGH>; status = "okay"; }; };   imx93-11x11-evk-boe-wxga-lvds-panel.dts Previous node is related with touch controller from LVDS using lpi2c1, the first channel of i2c corresponding to i2c bus 0, and the register used express the address used to be detected by device tree, in this case was the address 0x2A. u-boot generating a trigger   About how it can be detected touch controller from u-boot, this procedure use a function named as "board_late_init", it can be found by his definition from u-boot readme:   Board initialization settings: ------------------------------ During Initialization u-boot calls a number of board specific functions to allow the preparation of board specific prerequisites, e.g. pin setup before drivers are initialized. To enable these callbacks the following configuration macros have to be defined. Currently this is architecture specific, so please check arch/your_architecture/lib/board.c typically in board_init_f() and board_init_r(). - CONFIG_BOARD_EARLY_INIT_F: Call board_early_init_f() - CONFIG_BOARD_EARLY_INIT_R: Call board_early_init_r() - CONFIG_BOARD_LATE_INIT: Call board_late_init()   u-boot README In the case of i.MX 93 this function can be found in the next path <u-boot path>/board/freescale/imx93_evk/imx93_evk.c. Using the library included, "uclass.h", it will create a function that, if detect in the bus 0 (LVDS i2c bus) the address 0x2A (i2c LVDS address), it will create an environment variable with the overlay used, it can be set with the function env_set(<String with the name of the variable>, <String with the content of the variable>), the following function can detect and create the environment variable mentioned, creating it with the name "device-tree-overlay" with the content "lvds-panel".   #define LVDS_TOUCH_I2C_BUS 0 #define LVDS_TOUCH_I2C_ADDR 0x2A static void detect_display_connected(void) { struct udevice *bus = NULL; struct udevice *i2c_dev = NULL; int ret; ret = uclass_get_device_by_seq(UCLASS_I2C, LVDS_TOUCH_I2C_BUS, &bus); if (ret) { printf("%s: Can't find bus\n", __func__); } else { ret = dm_i2c_probe(bus, LVDS_TOUCH_I2C_ADDR, 0, &i2c_dev); if (ret) { printf("%s: Can't find device id=0x%x\n", __func__, LVDS_TOUCH_I2C_ADDR); } else { env_set("device-tree-overlay", "lvds-panel"); } } }   imx93_evk.c At the end, add this function to the previously mention, named as board_late_init, in the section CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG, like the following snipped from code:   int board_late_init(void) { #ifdef CONFIG_ENV_IS_IN_MMC board_late_mmc_env_init(); #endif env_set("sec_boot", "no"); #ifdef CONFIG_AHAB_BOOT env_set("sec_boot", "yes"); #endif #ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG env_set("board_name", "11X11_EVK"); env_set("board_rev", "iMX93"); detect_display_connected(); #endif return 0; }   imx93_evk.c Now, when it's starting u-boot after flashing, it will generate the environment variable as trigger if something it's connected with that i2c address, else it doesn't do anything. u-boot applying device tree overlay through event   As was explained in the section "How to apply device tree overlay", applying the device tree overlay automatically after configure the trigger it's easy, just adding an if/else case for this example, it can be more ways to applying it, even it's possible adding more of one device tree overlay, but in this example will load one.  Using u-boot command "test -e <environment variable>" it will detect if exist this environment variable, adding it to an if/else sentence it can create the event and applying the overlay if was detected or not, for this solution will be added this if/else as input if exists loadoverlay variable with the following structure:   u-boot=> if test -e ${device-tree-overlay}; then <case exists device-tree-overlay variable> else <case doesn't exists device-tree-overlay variable>; fi;   adding it to loadoverlay, it will be written like the following command:   u-boot=> setenv loadoverlay "if test -e ${device-tree-overlay}; then setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr ${fdt_addr} && fdt resize $\{fdt_buffer\}; fatload mmc ${mmcdev}:${mmcpart} $\{fdtovaddr\} imx93-11x11-evk-test-lvds-panel.dtbo; fdt apply $\{fdtovaddr\} ; else echo no overlay; fi;"   A no recommended method it's that it can be saved the environment, and changing mmcboot variable with the following command:   u-boot=> setenv mmcboot "run mmcargs; run loadfdt; run loadoverlay; run boot_os;"; saveenv;   The problem about just saving it, it still necessary compile u-boot to load auto-detection of LVDS panel and flashing, another way to add the event trigger, it's adding it to u-boot as initial environment variable, it can be added in the header file of imx93, it is located in the next path <u-boot path>/include/configs/imx93_evk.h, line number 60, it can be added with the same string but it's recommended follow the same structure, like the following definition:   /* Initial environment variables */ #define CFG_EXTRA_ENV_SETTINGS \ ... "loadoverlay=echo loading overlays from mmc ...; " \ "if test -e ${device-tree-overlay}; then " \ "setexpr fdtovaddr ${fdt_addr} + 0xF0000; " \ "setexpr fdt_buffer 16384; " \ "fdt addr ${fdt_addr} && fdt resize ${fdt_buffer}; " \ "fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} imx93-11x11-evk-test-lvds-panel.dtbo && fdt apply ${fdtovaddr}; " \ "else " \ "echo no overlay; " \ "fi;\0" \ ...   imx93_evk.h it also it's necessary to change mmcboot environment variable adding loadoverlay after executing loadfdt.    /* Initial environment variables */ #define CFG_EXTRA_ENV_SETTINGS \ .. "mmcboot=echo Booting from mmc ...; " \ "run mmcargs; " \ "if test ${sec_boot} = yes; then " \ "if run auth_os; then " \ "run run boot_os; " \ "else " \ "echo ERR: failed to authenticate; " \ "fi; " \ "else " \ "if test ${boot_fit} = yes || test ${boot_fit} = try; then " \ "bootm ${loadaddr}; " \ "else " \ "if run loadfdt; then " \ "run loadoverlay; " \ "run boot_os; " \ "else " \ "echo WARN: Cannot load the DT; " \ "fi; " \ "fi;" \ "fi;\0" \ ...   imx93_evk.h To build u-boot, copy the following commands in main path from u-boot   $ cd <u-boot path> $ make -j $(nproc --all) clean PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu- $ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=aarch64-linux-gnu- imx93_11x11_evk_defconfig $ make -j $(nproc --all) PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu-   generating the files u-boot.bin and u-boot-spl.bin located in <uboot-imx path>/ and <uboot-imx path>/spl Build imx-boot image using imx-mkimage   To build the binary necessary to flash to iMX 93 EVK it's necessary build a file named as flash.bin, it can building using the next repository using the branch used for this example:    $ git clone https://github.com/nxp-imx/imx-mkimage.git -b lf-6.6.3_1.0.0   to build imx-boot image it's necessary adding some files to the path <imx-mkimage path>/iMX93, including 2 generated by u-boot, u-boot.bin and u-boot-spl.bin, move these files to iMX93 directory.   $ cp <uboot-imx path>/u-boot.bin <uboot-imx path>/spl/u-boot-spl.bin <imx-mkimage path>/iMX93/   follow the steps from imx linux users guide section 4.5.13 and imx linux release notes section 1.2 to build flash.bin, as an example of compile, there's the steps to compile for imx93. Get mx93a1-ahab-container.img $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-sentinel-0.11.bin $ chmod +x firmware-sentinel-0.11.bin $ ./firmware-sentinel-0.11.bin $ cp firmware-sentinel-0.11/mx93a1-ahab-container.img <imx-mkimage path>/iMX93/​ Get lpddr4_imem_1d_v202201.bin, lpddr4_dmem_2d_v202201.bin, lpddr4_imem_1d_v202201.bin and lpddr4_imem_2d_v202201.bin $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.23.bin $ chmod +x firmware-imx-8.23.bin $ ./firmware-imx-8.23.bin $ cp firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_dmem_1d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_dmem_2d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_imem_1d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_imem_2d_v202201.bin <imx-mkimage path>/iMX93/​ Get bl31.bin $ git clone https://github.com/nxp-imx/imx-atf.git -b lf-6.6.3-1.0.0 $ cd imx-atf $ make -j $(nproc --all) PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu- $ cp <imx-atf path>/build/imx93/release/bl31.bin <imx-mkimage path>/iMX93​ Compile flash.bin from imx-mkimage $ cd <imx-mkimage path>/ $ make SOC=iMX9 REV=A1 flash_singleboot​ it will generate the binary flash.bin located in the path <imx-mkimage path>/iMX93/flash.bin. Flashing u-boot   Flashing just u-boot image using flash.bin, will be used uuu.exe, it can be downloaded from the his repositroy, try using the most recent version taged as "Latest"    https://github.com/nxp-imx/mfgtools/releases   make sure is using i.MX 93 EVK in boot mode download and connect it to your host from download USB port, using uuu.exe run the next code:   .\uuu.exe -b emmc .\flash.bin   or it can be flashed the full image with flash.bin binary.   .\uuu.exe -b emmc_all .\flash.bin ..\uuu\imx-image-full-imx93evk.wic   after that, starting be will using the created u-boot environment. Result   Inside u-boot, when it's connected the LVDS panel, it will create the variable named "device-tree-overlay" and will be charged automatically LVDS panel overlay, enabling it, if not it will working normally using DSI as output. Note: Ensure to have imx93-11x11-evk-test-lvds-panel.dtbo in memory. Reference   Device tree overlay: https://docs.kernel.org/devicetree/overlay-notes.html  
View full article
  Some customers want to expose their i3c device on the /dev, In order to develop their i3c APP or operation the i3c device like I2C. But in our default BSP code, we do not support this feature for I3C device, This article will introduce how to make the i3c device expose to the user space. Board : i.MX 93 EVK BSP Version : lf-6.1.55-2.2.0 I3C device : LSM6DSOXTR Step 1 : Rework the i.MX93 EVK Board, Install the R1010.      Step 2 : Apply the add_i3c_device_to_dev.patch file to the linux kernel code              Command : git apply add_i3c_device_to_dev.patch Step 3 : Re-compile the kernel Image file.              Command : make imx_v8_defconfig                                  make Step 4 : Boot your board with "imx93-11x11-evk-i3c.dtb" file and see if you can see the I3C device on the /dev directory. Result : We can see the i3c device is appeared in /dev directory, The i2c-8 is an i2c device mounted to the i3c bus. The i3c is backward compatible with i2c device. It will simulate the I2C signal loading i2c device.                 PS : You can also use the i2ctool detect i2c-8 device. As shown in the following picture:   Note : If you need the patch file, Please contact me any time for free.
View full article
This article is now outdated - SCFW 1.16.0 fixes this issue and has now been released. All customers who are experiencing stability issues with the processors outlined below should update to SCFW >1.16.0. ------------------------------------------------------------------------------------------------------------------------------------- The i.MX 8QM and i.MX 8QP has been revised with lower clock speeds and higher core voltages to help improve instability issues found with the part. Old parts that have not been derated have an "FF" moniker in the part number, whereas new parts, releasing in June 2024, have an "FE" moniker. An example can be found below. SCFW (System Controller Firmware) 1.16.0, which will be released with the Q2 Linux Factory BSP (LF6.6.y_2.0.0), will make the necessary changes to increase core voltage for CPU and GPU cores in the 8QM/8QP, as well as reduce clock speeds. It may not be immediately apparent what changes must be made to derate these processors before the new parts and new SCFW version is released. To assist with these issues, we are providing the changes below as a workaround until SCFW 1.16.0 is released.     Recommended Changes until SCFW 1.16.0 is released 1. Increase voltages in pmic_init(). This function is found inside the respective board.c file within the SCFW porting kit. This is assuming that the customer has routed their VDD_A72 to PMIC_0 on SW3 and SW4, and routed their VDD_GPU0 and VDD_GPU1 to PMIC_1 on SW1 through SW4. +/* Set VDD_A72 to 1.1375V (1138mV) */ +BRD_ERR(PMIC_SET_VOLTAGE(PMIC_0_ADDR, PF8100_SW3, 1138, REG_RUN_MODE)) +BRD_ERR(PMIC_SET_VOLTAGE(PMIC_0_ADDR, PF8100_SW4, 1138, REG_RUN_MODE)) +/* Set VDD_GPU0 and VDD_GPU1 to 1.03125V (1032mV) */ +BRD_ERR(PMIC_SET_VOLTAGE(PMIC_1_ADDR, PF8100_SW1, 1032, REG_RUN_MODE)) +BRD_ERR(PMIC_SET_VOLTAGE(PMIC_1_ADDR, PF8100_SW2, 1032, REG_RUN_MODE)) +BRD_ERR(PMIC_SET_VOLTAGE(PMIC_1_ADDR, PF8100_SW3, 1032, REG_RUN_MODE)) +BRD_ERR(PMIC_SET_VOLTAGE(PMIC_1_ADDR, PF8100_SW4, 1032, REG_RUN_MODE))   2. Add +37.5mV offset for VDD_A72, +31.25mV offset for VDD_GPU0/VDD_GPU1. This is done in the function board_set_voltage, found in board.c of the respective processor in the SCFW porting kit. This ensures that voltages are set correctly if a frequency change occurs (like going from overdrive to nominal mode on GPU). /*--------------------------------------------------------------------------*/ /* Set the voltage for the given SS. */ /*--------------------------------------------------------------------------*/ sc_err_t board_set_voltage(sc_sub_t ss, uint32_t new_volt, uint32_t old_volt) { sc_err_t err = SC_ERR_NONE; pmic_id_t pmic_id[2] = {0U, 0U}; uint32_t pmic_reg[2] = {0U, 0U}; uint8_t num_regs = 0U; +// A72 cores are running on 1.1375V instead of 1.10V +if ((ss == SC_SUBSYS_A72) && (new_volt == 1100)) { +board_print(3, "Changing voltage from 1100 to 1138"); +new_volt = 1138; +} +// GPU is running on 1.03125V instead of 1.00V +if ((ss == SC_SUBSYS_GPU_0 || SC_SUBSYS_GPU_1) && (new_volt == 1000)) { +board_print(3, "Changing voltage from 1000 to 1032"); +new_volt = 1032; +} board_print(3, "board_set_voltage(%s, %u, %u)\n", snames[ss], new_volt, old_volt); board_get_pmic_info(ss, pmic_id, pmic_reg, &num_regs);   3. Remove 1.6GHz from Linux DTS OPP Table for A72 core. This is found in the device tree of the board. These are typically found in /arch/arm64/boot/dts/freescale/. /* opp-1596000000 { opp-hz = /bits/ 64 <1596000000>; opp-microvolt = <1100000>; clock-latency-ns = <150000>; opp-suspend; }; */ 4. Disable GPU overdrive mode - set to nominal mode using sysfs in Linux userland echo "nominal" > /sys/bus/platform/drivers/galcore/gpu_govern
View full article
This article is rather short that only mentions the script that is needed to make an iMX93EVK act as a USB mass storage device so that whenever you connect your iMX device to a windows/linux system via USB, it should get enumerated something like a usb drive.  The storage that is used in this example is mmc so the expectation is that you have inserted a mmc card in the slot. Below is the script:- #!/bin/sh   # This composite gadget include function: # - MASS STORAGE     # # Exit status is 0 for PASS, nonzero for FAIL # STATUS=0   # Check if there is udc available, if not, return fail UDC_DIR=/sys/class/udc if test "$(ls -A "$UDC_DIR")"; then echo "The available udc:" for entry in "$UDC_DIR"/* do echo "$entry" done else STATUS=1 echo "No udc available!" exit $STATUS; fi   id=1; udc_name=ci_hdrc.0 #back_file=/dev/mmcblk1 back_file=/tmp/lun0.img   mkdir /sys/kernel/config/usb_gadget/g$id cd /sys/kernel/config/usb_gadget/g$id   # Use NXP VID, i.MX8QXP PID echo 0x1fc9 > idVendor echo 0x12cf > idProduct   mkdir strings/0x409 echo 123456ABCDEF > strings/0x409/serialnumber echo NXP > strings/0x409/manufacturer echo "NXP iMX USB Composite Gadget" > strings/0x409/product   mkdir configs/c.1 mkdir configs/c.1/strings/0x409   echo 5 > configs/c.1/MaxPower echo 0xc0 > configs/c.1/bmAttributes   mkdir functions/mass_storage.1 echo $back_file > functions/mass_storage.1/lun.0/file ln -s functions/mass_storage.1 configs/c.1/   echo $udc_name > UDC First execute the script. After that insert the g_mass_storage module in the kernel by executing :- modprobe g_mass_storage file=/dev/mmcblk1 removable=1 In the dmesg output, you will see something like below:-   After that you can connect a C type USB cable to the USB1 port of imx93evk and the other end to any USB ports of a laptop. The moment it is connected, you would be able to see a USB drive similar to what you get when we connect a pen-drive. 
View full article
  Some customer need to config different I2C bus for their PMIC in DDR test period. There is a simple method can complete this, that is NXP DDR Config Tool. The tool download link is below: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX I'm going to use the i.MX 93 EVK board here as a demonstration. On i.MX 93 EVK board, the default PMIC I2C Bus is I2C2, I will show you how to change I2C2 to I2C1, the other i2c bus is same.  Step 1 : Rework the board and make sure the PMIC is connected to I2C1. Remove R714 R715, connnect I2C1_SCL(C20) to U701 pin 41  and I2C1_SDA(C21) tp U701 pin 42. Step 2 : Setup I2C1 PinMux: Config Tool UI:   Advance -> IOMUX config   Command:           Address                Size               Value memory   set     0x443c0170            32                   0x10 memory   set     0x443c0174            32                   0x10 memory   set     0x443c0320            32                   0x40000b9e memory   set     0x443c0324            32                   0x40000b9e Step 3 : Set PMIC VDDQ as 1.1 V Config Tool UI:   Advance -> Custom PMIC initialization enabled   #  PMIC commands        Value 0         pmic_cfg             0x0025       /*I2C bus 1,  PMIC address 0x25 */ (0 for I2C1, 1 for I2C2, 2 for I2C3, 3 for I2c4 …) 1         pmic_set             0x0C29       /* BUCKxOUT_DVS0/1, preset_buck1=0.8V, preset_buck2=0.7V, preset_buck3=0.8V PCA9451_BUCK123_DVS, 0x29 */ 2         pmic_set             0x1118      /*  BUCK1OUT_DVS0=0.9V   PCA9451_BUCK1OUT_DVS0, 0x18 */ 3         pmic_set             0x1718      /*  BUCK3OUT_DVS0=0.9V   PCA9451_BUCK3OUT_DVS0, 0x18 */ 4         pmic_set             0x1428      /*  Set VDDQ to 1.1V  PCA9451_BUCK2OUT_DVS0, 0x28  */ PS : About pmic register, The first two bytes are the register address and the next two bytes are the register setting. Step 4 : Run the DDR "Firmware init test" and see the test result. The success log is as follows: DEBUG memtool.comm.serial_channel ==================hardware_init======================= DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel Power up ddr... DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel DDRMIX power on done... DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel DDRPHY coldreset... DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel ********Found PMIC PCA945X********** DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel Set VDDQ to 1.1V for LPDDR4 DEBUG memtool.comm.serial_channel DEBUG memtool.comm.serial_channel ==================hardware_init exit==================    
View full article
this is tested with MX93(A1) EVK running 6.1.55_2.2.0 pre-build image.   USB can output test patterns with either one of the setup below: 1. through device node: root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# cat role gadget root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo host > role [ 2672.864083] ci_hdrc ci_hdrc.0: EHCI Host Controller [ 2672.868996] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1 [ 2672.893320] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00 [ 2672.899314] hub 1-0:1.0: USB hub found [ 2672.909235] hub 1-0:1.0: 1 port detected root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# cat role host root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 4 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 3 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 2 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 1 > port_test   2. use memtool to program registers for i in $(find /sys -name control | grep usb);do echo on > $i;echo "echo on > $i";done; echo host > /sys/kernel/debug/usb/ci_hdrc.0/role #Offset:184h USB_OTG1 base address: 4C10_0000h base address USB_OTG2 base address: 4C20_0000h Register address Register address:base address+offset $ /unit_tests/memtool 0x4c100184 1 # Force to output Test Packet for Eye Diagram Test $ /unit_tests/memtool 0x4c100184=0x18041215 #Force to output J_STATE $ /unit_tests/memtool 0x4c100184=0x18011215 #Force to output K_STATE $ /unit_tests/memtool 0x4c100184=0x18021215 #Force to output SE0 (host) / NAK (device) $ /unit_tests/memtool 0x4c100184=0x18031215
View full article