i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
Enter inside ~/ltibdir/rpm/BUILD and create a directory 'alpha': $ cd ltib/rpm/BUILD $ mkdir alpha Enter in 'alpha' dir and create setalpha.c file: $ cd alpha #include <stdio.h> #include <stdlib.h> #include <sys/types.h> #include <sys/stat.h> #include <fcntl.h> #include <sys/ioctl.h> #include <unistd.h> #include <asm/arch/mxcfb.h>  int main(int argc, char **argv) {              int fb_fd;              struct mxcfb_gbl_alpha gbl_alpha;               if(argc != 2){                       printf("Usage: %s alpha_val[0-255]\n",argv[0]);                       return -1;              }               fb_fd = open("/dev/fb0",O_RDWR,0);              gbl_alpha.enable = 1;              gbl_alpha.alpha = atoi(argv[1]);              ioctl(fb_fd, MXCFB_SET_GBL_ALPHA, &gbl_alpha);              close(fb_fd);              return 0; } Compile it using this command: ./ltib -m shell LTIB> cd rpm/BUILD/alpha LTIB> gcc -I../linux/include setalpha.c -o setalpha In your board execute it: root@freescale /home$ /unit_tests/mxc_v4l2_output.out -iw 320 -ih 240 -ow 480 -oh 640 -d 3 -r 4 -fr 5 qvga.yuv & While it is playing execute: root@freescale /home$ setalpha 128 root@freescale /home$ cat screen.raw > /dev/fb0 We used frame rate at 5 fps to have more time to execute next two commands.
記事全体を表示
How to change Linux Kernel configuration file in Yocto Project metalayer Preparing the requirements Download the metalayer Git clone the Linux Kernel source code Customize the configuration Copy the configuration to the metalayer Install the patch in the Linux Kernel recipe Build the new image with the different Linux Kernel configuration How to change Linux Kernel configuration file in Yocto Project metalayer It is common that the metalayer providing a Linux Kernel recipe includes a default configuration file for the Linux Kernel source code (the defconfig file). There are several approaches to customize the Linux Kernel source code and defconfig file. This article presents the option to patch the defconfig from the Linux Kernel source code and is a good approach to be used with meta-fsl-bsp-release or meta-imx . Preparing the requirements The list of requirements: the target metalayer (in this example, it's meta-imx:imx-5.4.3-2.0.0 ) the same Linux Kernel source code, but git cloned Download the metalayer For example, take BSP release imx-5.4.3-2.0.0 for meta-imx $ mkdir <BSP_DIR> $ cd <BSP_DIR> $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.3-2.0.0.xml $ repo sync $ MACHINE=imx8mnevk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Git clone the Linux Kernel source code Use the very same Linux Kernel source code from the metalayer. In this example, open the file sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb to get the git repository, and git commit. $ cd ~ $ git clone git://source.codeaurora.org/external/imx/linux-imx.git $ cd linux-imx $ git checkout fd263a3edd95dfe812397fabf1059b5f99bba2ab -b change_defconfig‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Customize the configuration Using the default defconfig as a base, configure the Linux Kernel, and then use make menuconfig to change the configuration as desired. After the customization, generate a new defconfig file and replace the default one. The step by step with all the commands can be see in next snippet: $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make defconfig $ make menuconfig $ make savedefconfig $ cp defconfig arch/arm64/configs/defconfig‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The customization can be highlighted by git, in this example the result is show in next log: $ git status On branch change_defconfig Changes not staged for commit: (use "git add <file>..." to update what will be committed) (use "git checkout -- <file>..." to discard changes in working directory) modified: arch/arm64/configs/defconfig Untracked files: (use "git add <file>..." to include in what will be committed) defconfig no changes added to commit (use "git add" and/or "git commit -a")‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Review the change and create a commit, with that commit, create a patch. TIP: The defconfig file can also be directly changed. The make menuconfig can be skipped in that case. $ git add arch/arm64/configs/defconfig $ git commit -s -m "defconfig: Customize defconfig" $ git format-patch -1 0001-defconfig-Customize-defconfig.patch‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Copy the configuration to the metalayer Now that the Linux Kernel configuration is customized, and a patch to the kernel is created, copy over that patch to the metalayer, and install it to the Linux Kernel recipe file. $ mkdir <BSP_DIR>/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx/ $ cp 0001-defconfig-Customize-defconfig.patch <BSP_DIR>/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx/‍‍ Install the patch in the Linux Kernel recipe The Linux Kernel recipe for this example is linux-imx_5.4.bb . Edit the file to install the patch. $ gedit <BSP_DIR>/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb‍ Add the following line: SRC_URI += "file://0001-defconfig-Customize-defconfig.patch "‍ The resultant change is show above: $ cd <BSP_DIR>/sources/meta-imx/ $ git diff diff --git a/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb b/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb index 214647abb..3f926314c 100644 --- a/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb +++ b/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb @@ -16,6 +16,7 @@ KERNEL_BRANCH ?= "imx_5.4.3_2.0.0" LOCALVERSION = "-2.0.0" KERNEL_SRC ?= "git://source.codeaurora.org/external/imx/linux-imx.git;protocol=https" SRC_URI = "${KERNEL_SRC};branch=${KERNEL_BRANCH}" +SRC_URI += "file://0001-defconfig-Customize-defconfig.patch " SRCREV = "fd263a3edd95dfe812397fabf1059b5f99bba2ab"‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Build the new image with the different Linux Kernel configuration Remember to change the current directory to the metalayer. Build the image again. The new image binary reflects the changes in Linux Kernel, and in case the change removes some kernel module, the rootfs also reflects the change. $ cd <BSP_DIR>/bld-xwayland $ bitbake‍ <image-name>‍‍‍‍‍‍‍‍‍‍
記事全体を表示
GTK+ is a highly usable, feature rich toolkit for creating graphical user interfaces which boasts cross platform compatibility and an easy to use API. GTK+ it is written in C, but has bindings to many other popular programming languages such as C++, Python and C# among others. GTK+ is licensed under the GNU LGPL 2.1 allowing development of both free and proprietary software with GTK+ without any license fees or royalties. [Source: gtk.org] As GTK+ is a graphical library, a program using GTK+ can be done in many languages like C, C++, Python, Perl, PHP, Ruby, and many others. Here a C example will be done. How to make a simple program with GTK An easier way to make a graphical interface (GUI) program using GTK+ is to use Glade as Graphical Editor. Glade3 Screenshot To install Glade on Ubuntu type: $sudo apt-get install glade-3 Old Glade versions used to generate C code. Currently version ONLY generates a .glade file that can be parsed in a .xml file which describes the hierachy of the widgets. Let's create, compile and test a sample program on host and after, cross-compile for iMX platform and check it running on a PDK i.MX31 Development kit. In order to develop on host PC, install libgtk2.0-dev typing: $sudo apt-get install libgtk2.0-dev
記事全体を表示
The System Controller Unit (SCU) is in charge of controlling several features related to power management of the whole system. The user gets access to the following features through the System Controller Firmware: Powering up/down the system,resources and partitions Configuring resource clocks Reset controls Configuring wake-up sources This document will cover the more commonly used features, for details on the full capabilities of the API please refer to the API document for your device. Resource Power Control The SCU is in charge of managing power control to the resources (peripherals) in the SoC. Attempting to access a resource on the OFF state will result in a bus error or a hang All resources are organized within several subsystems, subsystems group together resources with common functionality. Subsystems are independent of each other and have their own PLLs and power domains, this allows modular control of clocks and power to the resources. The System Controller Unit has a dedicated I2C channel to interact with the PMIC, this allows dynamic control of some power sources for resources like the GPUs and Cortex-A cores. The SCU can enable/disable the LDO that supplies power to the GPU for instance and also turn on/off the internal power domains. The mapping of PMIC supplies and resources happens on the board.c (included in the SCFW Porting kit) and it is part of the porting process of the SCFW to new boards. The function board_get_pmic_info is where the mapping of resources to supplies happen, see: /*--------------------------------------------------------------------------*/ /* Get the pmic ids and switchers connected to SS. */ /*--------------------------------------------------------------------------*/ static void board_get_pmic_info(sc_sub_t ss,pmic_id_t *pmic_id, uint32_t *pmic_reg, uint8_t *num_regs) { /* Map SS/PD to PMIC switch */ switch (ss) { case SC_SUBSYS_A53 : pmic_init(); {/* PF8100_dual Card */ pmic_id[0] = PMIC_0_ADDR; pmic_reg[0] = PF8100_SW5; *num_regs = 1U; } break; case SC_SUBSYS_A72 : pmic_init(); {/* PF8100_dual Card */ pmic_id[0] = PMIC_0_ADDR; pmic_reg[0] = PF8100_SW3; pmic_id[1] = PMIC_0_ADDR; pmic_reg[1] = PF8100_SW4; *num_regs = 2U; } break; case SC_SUBSYS_GPU_0 : pmic_init(); {/* PF8100_dual Card */ pmic_id[0] = PMIC_1_ADDR; pmic_reg[0] = PF8100_SW1; pmic_id[1] = PMIC_1_ADDR; pmic_reg[1] = PF8100_SW2; *num_regs = 2U; } break; case SC_SUBSYS_GPU_1 : pmic_init(); {/* PF8100_dual Card */ pmic_id[0] = PMIC_1_ADDR; pmic_reg[0] = PF8100_SW3; pmic_id[1] = PMIC_1_ADDR; pmic_reg[1] = PF8100_SW4; *num_regs = 2U; } break; default : ; /* Intentional empty default */ break; } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Only some subsystems have their own dedicated external power supplies, in the example above A cores and GPUs are the only ones with a dedicated external power supplies. Most of the other subsystems are powered from the main power supply and power gating happens internally, each subsystem contains different power domains that can be turned on/off to manage power consumption. The SCFW API used to power on/off resources is the following: sc_err_t sc_pm_set_resource_power_mode (sc_ipc_t ipc, sc_rsrc_t resource, sc_pm_power_mode_t mode)‍‍‍‍‍ Where: ipc - is the interprocessor communication channel used to communicate with the SCU (obtained by calling sc_ipc_open). resource - is the resource that will have the power mode change mode - is the power mode to change to The available power mode options are the following: Power mode Voltage Clocks SC_PM_PW_MODE_OFF OFF All clocks off SC_PM_PW_MODE_STBY ON All clocks off SC_PM_PW_MODE_LP ON PLLs off resource running from XTAL SC_PM_PW_MODE_ON ON PLLs on In order to be able to access a resource it must be at least on SC_PM_PW_MODE_LP mode, since that mode has the resource voltage on and the clock is supplied by the 24MHz crystal. For more details please refer to the SCFW API document. Clocks Configuration As in the power management case, clocks are also organized in a distributed manner within the device. Each subsystem has it's own PLLs and all of them are clocked by the 24MHz crystal. The number of PLLs in each subsystem varies between all subsystems. To see how many PLLs are within a subsystem please refer to the datasheet of the device you are interested on. For instance on the datasheet of the i.MX8QXP on table 16 in Chapter 4.3.1: It can be seen that the GPU subsystem contains two PLLs, the ADMA subsystem contains 4 PLLs, Display Controller 3, etc... The SCFW API used to configure a clock is the following: sc_err_t sc_pm_set_clock_rate ( sc_ipc_t ipc, sc_rsrc_t resource, sc_pm_clk_t clk, sc_pm_clock_rate_t ∗ rate )‍‍‍‍‍ Where: ipc - is the interprocessor communication channel used to communicate with the SCU (obtained by calling sc_ipc_open). resource - is the resource that will have the clock rate change clk - is the clock to set the rate to (each resource can have different clocks associated with it for instance the GPU resource has a clock associated for its shader and another for the GPU, this parameter is used to identify the clock) rate - this contains the desired clock rate, the SCFW will try to match the provided rate if not possible it will then set the closest possible value and return the value that was actually configured. To identify the clk that needs to be passed, please refer to the SCFW API chapter called "Clock List" That chapter contains a table with all the different clocks that are configurable by the SCFW, in the case of the GPUs for instance to select the rate for the Shader or GPU, either the SC_PM_CLK_MISC or SC_PM_CLK_PER options would have to be selected. Set=Y indicates the clock/PLL is not shared and the rate can be set via sc_pm_set_clock_rate(). Enable=Y indicates the clock is not auto gated and must be enabled via sc_pm_clock_enable(). As an example the following snippet configures the GPU_0 shader clock: sc_clock_rate_t shader_clk=700000000; // 700 MHz sc_pm_set_clock_rate(ipc, SC_R_GPU_0_PID0, SC_PM_CLK_MISC, &shader_clk);‍‍ System Controller Firmware 101 
記事全体を表示
Download Linux kernel 2.6.29: $ wget -c http://www.kernel.org/pub/linux/kernel/v2.6/linux-2.6.29.tar.bz2 Extract this: $ tar jxvf linux-2.6.29.tar.bz2 Apply the patches: $ cd linux-2.6.29 Edit the file drivers/net/cs89x0.c adding: #include <mach/hardware.h> Export CROSS_COMPILE environmet: $ export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" $ export CROSS_COMPILE=arm-none-linux-gnueabi- Unselect all no essentials features: $ make ARCH=arm allnoconfig Start the configuration menu: $ make ARCH=arm menuconfig Change/Select the kernel options below. Select the MXC/iMX platform and iMX31ADS board: System Type ->             ARM system type -> (X) Freescale MXC/iMX-based             Freescale MXC Implementations  ->                            MXC/iMX Base Type -> (X) MX3-based                            MX3 Options  -> [*] Support MX31ADS platforms (NEW) Select ARM EABI standard to compile the kernel: Kernel Features  --->           [*] Use the ARM EABI to compile the kernel Add support to Linux Binary Format ELF: Userspace binary formats ->              [*] Kernel support for ELF binaries Add support to Network (TCP/IP): [*] Networking support  ->          Networking options  ->                          [*] Packet socket                          [*] Unix domain sockets                          [*] PF_KEY sockets                          [*] TCP/IP networking                                   [*] IP: kernel level autoconfiguration                                   [*]     IP: DHCP support Select network driver (CS89x0), serial driver and unselect VGA console: Device Drivers  ->                      [*] Network device support  --->                                      [*]   Ethernet (10 or 100Mbit)  --->                                             [*]   CS89x0 support                      Character devices  ->                              Serial drivers  --->                                       [*] IMX serial port support                                       [*]   Console on IMX serial port                      Graphics support  ->                             Console display driver support  --->                                        [ ] VGA text console Add support to NFS and support to use it as root file system: File systems  ->                            [*] Network File Systems (NEW)  ->                                        [*]   NFS client support                                        [*]     Root file system on NFS Compile the kernel: $ make ARCH=arm Copy the created zImage to tftp directory: $ cp arch/arm/boot/zImage /tftpboot/ Configure your RedBoot to boots with this kernel: load -r -b 0x100000 /tftpboot/zImage exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.240.191:/tftpboot/rootfs ip=dhcp"
記事全体を表示
This document shows the necessary steps to configure the Eclipse IDE for development of Yocto applications. Requirements 1) Linux machine. Ubuntu 12.4 or higher is recommended. 2) Yocto Freescale BSP Release or Freescale Community BSP. For this example we'll use the Freescale BSP Release L3.14.28 but you may use the FSL Community BSP. - Freescale Community BSP FSL Community BSP - Freescale BSP Release  Documentation L3.14.28 (login required) https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&location=null&fpsp=1&WT_TYPE=Supporting%20In… 3) Poky Meta Toolchain (Poky 1.7 / L3.14.28 for our example but you should use the toolchain that corresponds to the BSP that will be used) For information on how to extract and install the meta toolchain please follow the steps on the next document. Task #7 - Create the toolchain 4) Eclipse Luna. We’ll use the Luna SR2 (4.4.2) version of the Eclipse IDE. You may find it on the following website: http://www.eclipse.org/downloads/packages/release/luna/sr2 Look for the “Eclipse IDE for C/C++ Developers”, which contains the Eclipse Platform, the Java Development Tools (JDT), and the Plug-in Development Environment. Once you have downloaded the tarball extract it. The following command unpacks and installs the downloaded Eclipse IDE tarball into a clean directory using the default name eclipse:      $ cd ~      $ tar -xzvf ~/Downloads/eclipse-cpp-luna-SR2-linux-gtk-x86_64.tar.gz Configuring the Eclipse IDE Once with Eclipse Luna installed you may run the Eclipse IDE with the following command: $ cd eclipse $ ./eclipse Select a new workspace. Chose "Install New Software" from the "Help" pull-down menu. Select the "Luna - http://download.eclipse.org/releases/luna" Find and expand the Linux Tools option and select: Linux Tools LTTng Tracer Control Linux Tools LTTng Userspace Analysis LTTng Kernel Analysis If some of these options are not listed it means that they are already installed. (To change this you may uncheck the Hide items that are already installed box) Find and expand the Mobile and Device Development and select the following:   C/C++ Remote Launch (Requires RSE Remote System Explorer)   Remote System Explorer End-user Runtime   Remote System Explorer User Actions   Target Management Terminal (Core SDK)   TCF Remote System Explorer add-in   TCF Target Explorer If some of these options are not listed it means that they are already installed. (To change this you may uncheck the Hide items that are already installed box) Expand Programming Languages and select:   C/C++ Autotools Support   C/C++ Development Tools Chose Next and accept the necessary EULA Clck on the Finish button. The selected packages will be downloaded and installed. You will be asked to restart Eclipse IDE to finish the installation. Adding the Yocto Plug-in to the Eclipse IDE Next step is to install the Eclipse Yocto Plug-in into the Eclipse IDE. We'll show how to install the pre-built plug in. Start the Eclipse IDE In Eclipse, select "Install new Software" from the "Help" menu Click the "Add..." button to add a repository and enter: Name: Any name, we will use Yocto Fio Location: http://downloads.yoctoproject.org/releases/eclipse-plugin/1.8/luna Click "Ok" and then chose this new repository on the "Work with" drop-down menu and select the following plug-ins from the list:   Yocto Project ADT Plug-in   Yocto Project Bitbake Commander Plug-in   Yocto Project Documentation plug-in Install these plug-ins and click "OK" when prompted about installing software that contains unsigned content. You may be asked to restart the Eclipse IDE. Configuring the Eclipse Yocto Plug-in With all the necessary packages installed we'll now configure the Eclipse Yocto Plug-in. In this steps we will configure the Cross Compiler options and the Target options. These will then be used as default for your projects from within your working workspace. Select "Preferences" from the "Window" menu. Click on Yocto Project ADT from the left options and then under Cross Compiler Options select the Standalone pre-built toolchain radio button. We need to point to the Toolchain Root location of our installed toolchain. This is covered on the following community document: Task #7 - Create the toolchain In this case we'll be using poky 1.7 tollchain which has the following default location: /opt/poky/1.7 As fo the Sysroot Location this would correspond to your build directory sysroot folder, which is located on the following path: <YOCTO_BSP_DIR>/<BUILD_DIR>/tmp/sysroots/<MACHINE> In our case our Tartget architecture would be the Cortex-A9, which correspond to the i.MX6 and which is also the only option installed on the chosen directory. For Target Options we would be using the actual HW in order to test our application so keep the External HW option selected. Creating a Hello World Project We are now ready to create our project. Just to test our configuration we'll create a Hello World project.We can do so by selecting File->New->C Project or C++ Project We must then select a Project name and in project type we can chose either an Empty project or as in our case a Hello World Project, all this under the Yocto Project ADT Autotools Project folder. We will have the GNU Autotools Tolchain selected. The next screen will show some of the Basic Properties for our project, including the GNU license. Fill these as required. You may clock on Finish at this point. We should see that the HelloWorld project was created. We should right-click on the project folder and then chose Reconfigure Project in order to fill the necessary libraries. After this is completed we can build our project either by choosing the hammer icon or in the Build Project option inside the Project menu. We can look for correct competition or any errors or warning on the Console tab. Further Application Development After this basic setup you may work on more complex examples like a GPU and a Gstreamer Application examples on the following nicely written document: Yocto Application Development Using Eclipse IDE
記事全体を表示
This document shows how to run the multicore communication examples from MCUXpresso SDK while running the Android BSP on Cortex-A7 on i.MX 7ULP-EVK. Though this document is focused on the multicore demos, similar procedures can be applied to run any other demo in the SDK. 1. Source code This document is based on the following releases: Board Android BSP MCUXpresso SDK imx7ulp-evk Android O8.1.0 for i.MX 7ULP GA SDK2.4 for i.MX 7ULP GA Download releases at i.MX Software. 2. Building the Cortex-M4 SDK There are at least two multicore demos in the SDK package, rpmsg_lite_pingpong_rtos and rpmsg_lite_str_echo_rtos. They are located at: <SDK_2.4.0_EVK-MCIMX7ULP_dir>/boards/evkmcimx7ulp/multicore_examples/ Build the rpmsg_lite_str_echo_rtos demo according to the SDK Getting Started Guide. Remember to also follow the Chapter 6, Step 4 of the document to generate the ram bootable image (sdk20-app.img). 3. Building the Android BSP 3.1. RPMsg kernel module Before building the BSP, add the following line to the BoardConfig.mk file (<android_build_dir>/device/fsl/evk_7ulp/BoardConfig.mk): BOARD_VENDOR_KERNEL_MODULES += \    $(KERNEL_OUT)/drivers/net/wireless/qcacld-2.0/wlan.ko \ + $(KERNEL_OUT)/drivers/rpmsg/imx_rpmsg_tty.ko 3.2. Cortex-M4 image Copy the SDK image file (sdk20-app.img) to the following directory in the Android source code: $ cp <SDK_2.4.0_EVK-MCIMX7ULP_dir>/tools/imgutil/evkmcimx7ulp/sdk20-app.img \   <android_build_dir>/vendor/nxp/fsl-proprietary/mcu-sdk/7ulp/sdk20-app.img Change the BoardConfig.mk file accordingly: # Copy prebuilt M4 demo image: PRODUCT_COPY_FILES += \ - vendor/nxp/fsl-proprietary/mcu-sdk/7ulp/imx7ulp_m4_demo.img:imx7ulp_m4_demo.img + vendor/nxp/fsl-proprietary/mcu-sdk/7ulp/sdk20-app.img:imx7ulp_m4_demo.img After these changes, build and flash Android as described in the BSP User's Guide. 4. Enabling the multicore communication While booting, the SoC automatically loads the Cortex-M4 image. After complete booting, install the imx_rpmsg_tty.ko module to create the multicore communication channel: $ su $ insmod vendor/lib/modules/imx_rpmsg_tty.ko To send messages from Cortex-A7 to Cortex-M4, use the /dev/ttyRPMSG* channel: $ echo "MESSAGE" > /dev/ttyRPMSG* /dev/ttyRPMSG* refers to the RPMsg device created on the board, so change the number accordingly. Cortex-M4 will echo all messages received from Cortex-A7. This is a simple example on how to communicate different cores on i.MX using Android but it can be used as a starting point for Android multicore applications.
記事全体を表示
Random Number Generator - RNGA Download rng-tools: http://downloads.sourceforge.net/sourceforge/gkernel/rng-tools-2.tar.gz This tool tests the link between a random number generator hardware and the kernel's PRNG (pseudo-random number generator). ./ltib -m shell LTIB> cd rpm/BUILD/ LTIB> cp ~/hwrandom/rng-tools-2.tar.gz . LTIB> tar zxvf rng-tools-2.tar.gz LTIB> cd rng-tools-2 LTIB> ./configure --host=arm-linux LTIB> make LTIB> sudo cp rngtest /tftpboot/ltib/home/ Restart your board and execute this command in the board's console: $ cat /dev/hwrng | /home/rngtest -c 1000
記事全体を表示
Flashing Kernel and Root File System using RedBoot Creating an image A kernel image and a root file system can be created using All Boards LTIB or compiling the kernel and setting the correct set of files. Create a root file system image from a set of files converting the files to a jffs2 file system. For this, install the package mtd-tools. In Ubuntu type apt-get install mtd-tools For making an root file system for flash, use the jffs2 file system like: mkfs.jffs2 -r rootfs/ -e 0x20000 -n -p -o rootfs.jffs2 Where rootfs/ is the original set of file for the file system and rootfs.jffs2 is the output image file. Flashing Some connections errors can be avoided by All Boards Configuring RedBoot. The process below uses TFTP to copy the files between host and target. See All Boards TFTP for detail in configurations. Copy the kernel image and the root file system image to the TFTP dir. For example, in  LTIB dir, type sudo cp ./rootfs/boot/zImage /tftpboot sudo cp rootfs.jffs2 /tftpboot/ Where /tftpboot is the dir configured for TFTP The next steps are performed in a Minicom session, and happens on the board. Formatting the flash: fis init Flashing kernel Load kernel image (zImage) using the command below. Remember to modify the host IP address: load -r -b 0x100000 /tftpboot/zImage -h 10.29.244.99 The address 0x100000 is used as a temporary location Create the kernel at the right address (0x200000, for IMX31PDK) fis create -f 0x200000 kernel Flashing root file system Load root file system image (rootfs.jffs2) to the temporary address. Remember to modify the host IP address: load -r -b 0x100000 /tftpboot/rootfs.jffs2 -h 10.29.244.99 Create the root file system in the right address (0x600000, for IMX31PDK. fis create -f 0x600000 root Testing You can now load your kernel in the flash by typing: fis load kernel To know if the root file system written in the flash was correctly saved, execute the NFS file system and mount the flash. For load the the root file system by NFS, type: exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.244.99:/tftpboot/rootfs init=/linuxrc ip=10.29.241.6:10.29.244.99" Wait the system go up, then mount the flash at /mnt. Reminde that the flash has a jffs2 file system. mount -t jffs2 /dev/mtdblock2 /mnt ls /mnt List the /mnt contents. The output must be the right file system. Modifying the initial script Reset the board and press CTRL-C. Type fc to modify the configurations and insert the initialization script. RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> fis load kernel >> exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock2 rw rootfstype=jffs2 ip=none" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> Remember to save the configuration in the flash by typing y Reset the system. To certify that the board is loading the system from flash, remove the ethernet cable.
記事全体を表示
One of the new feature of  the i.MX8 family is to support CAN FD. Fortunately the MEK board has a TJA1043 supporting CAN FD. The following document show you how to do simple CAN (FD) test under Linux. First of all let configure the CAN0 to be at 500kps in CAN, and 4Mbps in CAN FD: ip link set can0 up type can bitrate 500000 sample-point 0.75 dbitrate 4000000 dsample-point 0.8 fd on ‍‍‍‍‍‍‍ Let's do the same for CAN1: ip link set can1 up type can bitrate 500000 sample-point 0.75 dbitrate 4000000 dsample-point 0.8 fd on‍‍‍‍ Now you can do a bridge between CAN0 and CAN1 on the board. The easiest way is to put simple wires (pin 2 to pin 2 a,d pin 7 to pin 7), normally you have to twist your wires, but as it is on your desk, you can get rid of it): You can check the configurations of your FlexCAN: root@imx8qxpmek:~# ip -details link show can0 3: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 72 qdisc pfifo_fast state UNKNOWN mode DEFAULT group default qlen 10 link/can promiscuity 0 can <FD> state ERROR-WARNING (berr-counter tx 0 rx 0) restart-ms 0 bitrate 500000 sample-point 0.750 tq 25 prop-seg 29 phase-seg1 30 phase-seg2 20 sjw 1 flexcan: tseg1 2..64 tseg2 1..32 sjw 1..32 brp 1..1024 brp-inc 1 dbitrate 4000000 dsample-point 0.800 dtq 25 dprop-seg 3 dphase-seg1 4 dphase-seg2 2 dsjw 1 flexcan: dtseg1 1..39 dtseg2 1..8 dsjw 1..8 dbrp 1..1024 dbrp-inc 1 clock 40000000numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535 root@imx8qxpmek:~# ip -details link show can1 4: can1: <NOARP,UP,LOWER_UP,ECHO> mtu 72 qdisc pfifo_fast state UNKNOWN mode DEFAULT group default qlen 10 link/can promiscuity 0 can <FD> state ERROR-ACTIVE (berr-counter tx 0 rx 0) restart-ms 0 bitrate 500000 sample-point 0.750 tq 25 prop-seg 29 phase-seg1 30 phase-seg2 20 sjw 1 flexcan: tseg1 2..64 tseg2 1..32 sjw 1..32 brp 1..1024 brp-inc 1 dbitrate 4000000 dsample-point 0.800 dtq 25 dprop-seg 3 dphase-seg1 4 dphase-seg2 2 dsjw 1 flexcan: dtseg1 1..39 dtseg2 1..8 dsjw 1..8 dbrp 1..1024 dbrp-inc 1 clock 40000000numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535 root@imx8qxpmek:~#‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Now a simple test can be to send random CAN FD messages, for that use "cangen" to send random CAN FD messages (read "cangen" documentation: https://manpages.debian.org/stretch-backports/can-utils/cangen.1.en.html 😞 root@imx8qxpmek:~# cangen can0 -v -b -g 20 can1 3E6 [00] can1 735 [20] F9 ED 40 53 AC CF 48 34 F9 ED 40 53 AC CF 48 34 F9 ED 40 53 can1 513 [20] 92 D2 E7 32 48 E6 EA 39 92 D2 E7 32 48 E6 EA 39 92 D2 E7 32 can1 03B [12] 6D 34 2F 11 52 8A 52 50 6D 34 2F 11 can1 47D [24] 72 08 88 0D E0 04 F7 09 72 08 88 0D E0 04 F7 09 72 08 88 0D E0 04 F7 09 can1 245 [00] can1 6F6 [48] B9 82 A1 49 4E ED BA 06 B9 82 A1 49 4E ED BA 06 B9 82 A1 49 4E ED BA 06 B9 82 A1 49 4E ED BA 06 B9 82 A1 49 4E ED BA 06 B9 82 A1 49 4E ED BA 06 can1 1F4 [16] 03 5B 7C 00 DA E5 FA 03 03 5B 7C 00 DA E5 FA 03 can1 38A [48] 71 CE A3 1A C0 8A 4F 20 71 CE A3 1A C0 8A 4F 20 71 CE A3 1A C0 8A 4F 20 71 CE A3 1A C0 8A 4F 20 71 CE A3 1A C0 8A 4F 20 71 CE A3 1A C0 8A 4F 20 can1 4C9 [20] 6C 5A 98 54 DD D1 CB 09 6C 5A 98 54 DD D1 CB 09 6C 5A 98 54 can1 536 [48] 25 B8 B6 43 71 CD 54 71 25 B8 B6 43 71 CD 54 71 25 B8 B6 43 71 CD 54 71 25 B8 B6 43 71 CD 54 71 25 B8 B6 43 71 CD 54 71 25 B8 B6 43 71 CD 54 71 can1 308 [02] C3 57 can1 33E [05] 65 8C 7B 21 83 can1 3F5 [05] EA E0 07 63 EB can1 633 [03] 39 10 18 can1 25D [32] 01 4E 65 41 E8 4D 94 6F 01 4E 65 41 E8 4D 94 6F 01 4E 65 41 E8 4D 94 6F 01 4E 65 41 E8 4D 94 6F can1 2FB [03] A8 D8 E3 can1 0DE [04] A1 11 3F 32 can1 012 [06] 85 23 B2 07 1A 03 can1 658 [08] A0 8A 2D 67 97 79 A1 64 can1 37D [05] 1A 57 E8 4F 72 can1 70A [04] 5E 6A B8 0F can1 3A8 [07] 65 C5 48 76 05 B6 11 can1 5D4 [07] ED 03 A6 07 CF D8 DC can1 7DA [05] 94 18 50 09 B8 can1 7A9 [05] CC 5E 02 74 BC can1 3FC [01] D6 can1 599 [06] EB 23 02 61 16 D9 can1 47C [06] 88 20 F2 62 86 3B can1 30A [06] C4 98 57 61 B2 4E can1 57E [16] B8 04 86 5B 52 EB DF 45 B8 04 86 5B 52 EB DF 45 can1 191 [05] 22 C4 BC 26 6B can1 53B [06] 23 AA AA 00 E4 F4 can1 6EB [64] A0 64 BE 5E E7 FA 20 1D A0 64 BE 5E E7 FA 20 1D A0 64 BE 5E E7 FA 20 1D A0 64 BE 5E E7 FA 20 1D A0 64 BE 5E E7 FA 20 1D A0 64 BE 5E E7 FA 20 1D A0 64 BE 5E E7 FA 20 1D A0 64 BE 5E E7 FA 20 1D‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ You can check with a scope your CAN FD frame (here CAN High): And you can see the first part of the frame sent @500kps and the second part @4Mbps. If you unplug one wire, the messages will no longer be sent as no acknowlege will occurs. You can also send message without flexible datarate. In our case, we'll send long frame at 500kps (no more 4Mbps transfer for end of the frame): imx8qxpmek:~# cangen can0 -v -f -g 20 can0 6FE##0.6B.C6.BA.1A.82.2D.29.7E.6B.C6.BA.1A.82.2D.29.7E.6B.C6.BA.1A.82.2D.29.7E.6B.C6.BA.1A.82.2D.29.7E.6B.C6.BA.1A.82.2D.29.7E.6B.C6.BA.1A.82.2D.29.7E.6B.C6.BA.1A.82.2D.29.7E.6B.C6.BA.1A.82.2D.29.7E can0 3E2##0.D4.9E.3D can0 1DE##0.D0.D8.33.50.7E.39 can0 7CE##0.FA.68.25.74.86.E7.E1.4A.FA.68.25.74.86.E7.E1.4A.FA.68.25.74 can0 7C3##0.58.E6.F2.1E.BD.7D.F8.7F can0 32A##0.0D.06.98.0D.08.81.5C.4E.0D.06.98.0D.08.81.5C.4E.0D.06.98.0D.08.81.5C.4E.0D.06.98.0D.08.81.5C.4E.0D.06.98.0D.08.81.5C.4E.0D.06.98.0D.08.81.5C.4E can0 48B##0.76.48.B4.34.59.81.B9.47.76.48.B4.34.59.81.B9.47.76.48.B4.34.59.81.B9.47.76.48.B4.34.59.81.B9.47.76.48.B4.34.59.81.B9.47.76.48.B4.34.59.81.B9.47.76.48.B4.34.59.81.B9.47.76.48.B4.34.59.81.B9.47 can0 3FC##0.6E.70.F7.36.FB.82.B9.00.6E.70.F7.36.FB.82.B9.00.6E.70.F7.36.FB.82.B9.00.6E.70.F7.36.FB.82.B9.00.6E.70.F7.36.FB.82.B9.00.6E.70.F7.36.FB.82.B9.00.6E.70.F7.36.FB.82.B9.00.6E.70.F7.36.FB.82.B9.00 can0 4BE##0.7D.B0.E2.7E.A0.F0.DF.24.7D.B0.E2.7E can0 60C##0.0E can0 257##0.69.11.0C.4B.25.CA.16.65.69.11.0C.4B.25.CA.16.65.69.11.0C.4B.25.CA.16.65.69.11.0C.4B.25.CA.16.65.69.11.0C.4B.25.CA.16.65.69.11.0C.4B.25.CA.16.65 can0 0BA##0.AB.B1.F8 can0 0FC##0.3A.7E.FB.34 can0 452##0.2F.4D.04.26.DE.80.EA can0 2C7##0.37.02.A4.4D.C3 can0 0B4##0.BE.39.AD.3B.73 can0 17E##0.13.66.44.6A.8A.8F.CE.7A.13.66.44.6A.8A.8F.CE.7A.13.66.44.6A‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ You can also force the CAN to only send CAN 2.0b frames (not FD, you'll have 8-byte data max frames): imx8qxpmek:~# cangen can0 -v -g 20 can0 7FF#8F.04.3F.31.EB can0 135#92.7C.46.5C.95.4E.6C.48 can0 0F8#E3.E4.7E.4D.92.2A.1D.69 can0 68F#C6.B7.BA.35.78.06 can0 4EC#D8.D9.86.19.40.BE.64.05 can0 09F#EE.E1.70.7D.13.C9.18.53 can0 7CE#BB.CD.FE.50.3E.B6.A4.4A can0 3C7#04 can0 1F6#B2.E4.4B.42 can0 080#C1.81.65.41 can0 14C#0B.B4.7E.5D can0 15A#53 can0 1CF#86.D4.ED.11.6E.BA.20.14 can0 257#82.83.39.67 can0 2C1#64.20.DF.0D.89.0E.14.55 can0 45E#50.72.44.76.55.4E.96.0F can0 6FC#80.81 can0 046#F6 can0 1E5#6D can0 0D2# can0 7EB#0F.3D.29.78.42.72.60.61 can0 480#68 can0 1CE#CB.05.12.74.2D.0E.F2.14 can0 634#82.5C.88.24.31.75.AF.03 can0 71D#AE.4C can0 144#F5.A8.17.70 can0 2A5#69.BE can0 222#18.C6.AA.4A.0D.5A.EC.48 can0 5FA#4F.CC.4C.2A.7B.BA.31 can0 3B9#BD.B1.2F.3C.87.D5.D1 can0 583#B4.E3.C3.4E.B8.D3.22.43‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
記事全体を表示
Debugging with Eclipse and GDB on Linux user space This is a good open-source choice to debug i.MX processors. The integration of popular tools like Eclipse and GDB offers a good and stable connection between host and target. The first step is to install the tools on host. Click here to get instructions of how to install the tools. Let's debug a ready hello world program into the ltib. To extract the hello world package, type on ltib directory: $./ltib -m prep -p helloworld Change the code of hello.c to: #include <stdio.h> int main(int argc, char** argv) {     int i;     for (i = 0; i < 100; ++ i)     {         printf(“Welcome to GDB ! %d /n”, i);     }     return 0; } Change the Makefile to add debug symbols Change the two following lines from: CFLAGS = -Wall CXXFLAGS = -Wall To: CFLAGS = -Wall -g CXXFLAGS = -Wall -g Build and deploy the new source-code: $./ltib –p helloworld –m scbuild $./ltib –p helloworld –m scdeploy Configuring the Target On target, gdbserver needs to be run to perform debug. The gdbserver command has the following structure: gdbserver ip_host:port /full/path/app/app_name If gdbserver is not installed on target, select gdb package on ltib configuration. In this example our host has the 192.168.16.35 IP address and our HelloWorld application is located at /usr/bin/hello on the target board. Execute the gdbserver: gdbserver 192.168.16.35:10000 /usr/bin/hello You can use other port number as long as you use the same number when configuring the Eclipse. Setting a GDB Debug Session on Eclipse Now we will configure Eclipse C/C++ to start a GDB session with our remote i.MX board. We will need to know which is the target board’s IP address. To get your target’s IP address: /sbin/ifconfig In our example the target board has the 192.168.16.36 IP address. Open-up Eclipse and choose the C/C++ perspective. We will import the HelloWorld executable built by LTIB. Go to the menu File -> Import You will see the “Import” screen. Select “C/C++ Executable” option. Hit the “Next” button. Eclipse automaticaly creates a new project when whe use the “Import” option. In the next screen, select the “Search Directory” option and hit the “Browse” button. This session is incomplete and is being edited...
記事全体を表示
<analytics uacct="UA-5520491-1" /> How to enable WIFI support for i.MX53 QSB Android After applying every QSB patch, enable WiFi support according to your hardware. Android R4 can be downloaded from Adeneo´s website. AR6102  Change file device/fsl/imx53_loco/BoardConfig.mk -BOARD_WLAN_CHIP_AR6102  := false +BOARD_WLAN_CHIP_AR6102  := true AR6003  Change file device/fsl/imx53_loco/BoardConfig.mk -BOARD_WLAN_CHIP_AR6003  := false +BOARD_WLAN_CHIP_AR6003  := true After complete build ar6000.ko will be created under /system/etc/modules To turn WIFI on, go to Settings > Wireless & network s > Wi-Fi Error message case  In case logcat shows the following error message: E/WifiHW  ( 2086): Cannot access "/data/misc/wifi/wpa_supplicant.conf":Permission denied Reconfigure nfs server file /etc/default/nfs-kernel-server delete this line:   RPCMOUNTDOPT=--manage-gids
記事全体を表示
This post describes the setup detail for installing Ubuntu based distro in any i.Mx6x NXP Boards. Details are described on: 1. Select your board, Setting the host, Download and compile uboot , dtb and and the Kernel version on your board. 2. Installing the Ubuntu core, Lubuntu graphics desktop version and/or Build your own Ubuntu rootfs with debootstrap. 3. Modify rootfs and Installing needed packages 4. Setting with SD image. 5. Setting Ubuntu on target 6. Adding GPU acceleration 1: Select your board, Setting the host, Download and compile uboot , dtb and and the Kernel version on your board. Supported NXP HW boards: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board i.MX 6SoloX SABRE-SD Board i.MX 6SoloX SABRE-AI Board Install host dependences (version tested 14.04): $ sudo apt-get install gparted git build-essential libncurses5 wget u-boot-tools zlib1g-dev ncurses-dev \ cmake libc-dev-armhf-cross pkg-config-arm-linux-gnueabihf build-essential checkinstall cmake \ pkg-config lzop libc6 libstdc++6 debootstrap qemu-user-static binfmt-support Download the compiler toolchain and extract it: $ cd ~/ $ wget -c https://releases.linaro.org/14.09/components/toolchain/binaries/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux.tar.xz $ tar xf gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux.tar.xz Create general variable environments: $ export target=mx6q (e.g. processor: mx6sx, mx6d, mx6dl,etc) $ export board=sabresd (e.g. sabresd, sabreauto) $ export ARCH=arm $ export CROSS_COMPILE=../gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- $ unset LDFLAGS Download u-boot At the release of this document, latest uboot version was imx_3.14.52, it should work with other version as well, so please check the proper version for your board: $ cd ~/ $ wget –c http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/snapshot/uboot-imx-rel_imx_3.14.52_1.1.0_ga.tar.gz $ tar -xf uboot-imx-rel_imx_3.14.52_1.1.0_ga.tar.gz $ cd uboot-imx-rel_imx_3.14.52_1.1.0_ga $ make $targetboard_config    # e.g. mx6qsabresd_config $ make Linux Kernel, Firmware, headers, modules and DTS files $ cd ~/ $ wget –c http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/snapshot/linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga.tar.gz $ tar xf linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga.tar.gz $ cd linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga $ make imx_v7_defconfig $ make menuconfig $ make -j4 zImage modules dtbs $ cd ~/ move your image to binary folder: $ sudo cp –v uboot-imx-rel_imx_3.14.52_1.1.0_ga/u-boot.imx binary/ $ sudo cp –v linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga/arch/arm/boot/zImage binary/ $ sudo cp –v linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga/arch/arm/boot/dts/i$target-$board.dtb binary/ Now you have the bootloader, device tree and kernel image of your board ready, let’s create the rootfs. 2: Installing the Ubuntu core, Lubuntu graphics desktop version and/or Build your own Ubuntu rootfs with debootstrap. Installing ubuntu core: $ cd ~/ $ sudo mkdir –p core /media/rootfs /media/kernel $ wget –c http://cdimage.ubuntu.com/ubuntu-core/releases/14.04/release/ubuntu-core-14.04.4-core-armhf.tar.gz $ sudo tar –xf ubuntu-core-14.04.4-core-armhf.tar.gz –C core $ sudo cp -vr core/* /media/rootfs $ cd linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga $ sudo make modules_install firmware_install INSTALL_MOD_PATH=/media/rootfs/ ARCH=arm CROSS_COMPILE=../../gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- $ sudo make ARCH=arm CROSS_COMPILE=../../gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- headers_install INSTALL_HDR_PATH=/media/rootfs/usr Now you should have your ubuntu rootfs on /media/rootfs folder. and you can pass to part 3 of this post. Installing ubuntu Linaro LXDE: $ cd ~/ $ sudo mkdir –p core /media/rootfs /media/kernel $ wget https://releases.linaro.org/14.10/ubuntu/trusty-images/alip/linaro-trusty-alip-20141024-684.tar.gz $ sudo tar -xf linaro-trusty-alip-20141024-684.tar.gz –C core $ sudo mv core/binary/* core/ $ sudo rm –rf core/binary $ sudo cp -vr core/* /media/rootfs $ cd linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga $ sudo make modules_install firmware_install INSTALL_MOD_PATH=/media/rootfs/ ARCH=arm CROSS_COMPILE=../../gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- $ sudo make ARCH=arm CROSS_COMPILE=../../gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- headers_install INSTALL_HDR_PATH=/media/rootfs/usr Now you should have your ubuntu rootfs on /media/rootfs folder. and you can pass to part 3 of this post. Installing with debootstrap $ cd ~/ $ target=rootfs $ distro=trusty $ sudo debootstrap --arch=armhf --foreign --include=ubuntu-keyring,apt-transport-https,ca-certificates,openssl $distro "$target" http://ports.ubuntu.com $ sudo cp /usr/bin/qemu-arm-static $target/usr/bin $ sudo cp /etc/resolv.conf $target/etc Now have a minimal Ubuntu rootfs - chroot to it and perform the 2nd stage install: $ sudo chroot $target  //Now we are in chroot # distro=trusty # export LC_ALL=C LANGUAGE=C LANG=C # /debootstrap/debootstrap --second-stage Edit the sources.list repositories # cat <<EOT > /etc/apt/sources.list deb http://ports.ubuntu.com/ubuntu-ports/ $distro main restricted universe multiverse deb http://ports.ubuntu.com/ubuntu-ports/ $distro-updates main restricted universe multiverse deb http://ports.ubuntu.com/ubuntu-ports/ $distro-security main restricted universe multiverse EOT # apt-key adv --recv-keys --keyserver keyserver.ubuntu.com 40976EAF437D05B5 # apt-key adv --recv-keys --keyserver keyserver.ubuntu.com 3B4FE6ACC0B21F32 # apt-get update # apt -y -f install # apt-get upgrade # apt-get install nano Now you should be able to login without password, then use passwd command to set one. If you like to add custom users: # passwd root # adduser <myuser> # usermod -a -G tty myuser # usermod -a -G dialout, adm, sudo, dip, plugdev myuser # visudo Under the line that looks like: root ALL=(ALL:ALL) ALL add the following (change user with your actual username) <myuser> ALL=(ALL) ALL your rootfs is ready, exit chroot # exit $ sudo rm $target/etc/resolv.conf $ sudo rm $target/usr/bin/qemu-arm-static $ sudo mv rootfs/* /media/rootfs $ cd linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga $ sudo make modules_install firmware_install INSTALL_MOD_PATH=/media/rootfs/ ARCH=arm CROSS_COMPILE=../../gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- $ sudo make ARCH=arm CROSS_COMPILE=../../gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- headers_install INSTALL_HDR_PATH=/media/rootfs/usr Now you should have your ubuntu rootfs on /media/root. 3: Modify Rootfs and Install needed packages Edit and verify the sources.list repositories $ cd /media/rootfs $ sudo cat <<EOT > etc/apt/sources.list deb http://ports.ubuntu.com/ubuntu-ports/ trusty main restricted universe multiverse deb http://ports.ubuntu.com/ubuntu-ports/ trusty-updates main restricted universe multiverse deb http://ports.ubuntu.com/ubuntu-ports/ trusty-security main restricted universe multiverse EOT Edit networks interfaces and append in the existing file: $ sudo nano etc/network/interfaces auto lo iface lo inet loopback auto eth0 iface eth0 inet dhcp If you require Serial Console, remove and include an additional line at the end of the file for  ttymxc0 output as below, $ sudo nano etc/init/tty1.conf exec /sbin/getty -8 38400 tty1 exec /sbin/getty -L 115200 ttymxc0 If you like to change the localhostname: $ sudo nano etc/hostname and change to “your name” e.g. imx6Q. Set the date and time clock and update $ sudo nano /etc/rc.local  Add this: if [ `date +"%Y"` -eq "1970" ]; then                     date --set="2016-04-01" fi exit 0 (optional for Linaro rootfs) Edit passwd and remove the x in root and linaro lines $ sudo nano etc/passwd root:x:0:0:root:/root:/bin/bash linaro:x:0:0.. and change like this:                                   root::0:0:root:/root:/bin/bash linaro:::0:.. Now you are ready to program your sd image. 4: Setup microSD/SD card For these instructions, we are assuming: DISK=/dev/sdg on your HOST, cat /proc/partitions is very useful for determining the device id. $ cd ~/ $ export DISK=/dev/sdg Erase microSD/SD card: $ sudo dd if=/dev/zero of=${DISK} bs=1M count=10 Install Bootloader $ cd binary/ $ sudo dd if=u-boot.imx of=${DISK} bs=512 seek=2 $ sync Create Partition layout: $ cd ~/ $ sudo fdisk ${DISK} steps:        d ///delete all partitions currently on sd n // create new partition p // Primary partition 1 // partition number 1 2048 //default +1G // n // created 2d parition p 2 default default 1 // firts B // to be fat32 W // write partiotions $ sudo mkfs.vfat ${DISK}1 $ sudo mkfs.ext3  ${DISK}2 Mount ext3 SD partition to /media/rootfs: $ sudo mount ${DISK1} /media/kernel_target $ sudo mount ${DISK}2 /media/rootfs_target Copy Files on the SD. $ cd ~/ $ sudo cp –v binary/ i$target-$board.dtb /media/kernel_target $ sudo cp –v binary/zImage /media/kernel_target $ sudo mv /media/rootfs/* /media/rootfs_target Remove SD: $ sync $ sudo umount /media/kernel_target $ sudo umount /media/rootfs_target Boot the target, in console you should be login as root. root@imx6QSabreSD:~# 5: Setting Ubuntu on target Note: If you have issues with sudo on user UID, need to logout and log as root: imx6Q login: root Welcome to Ubuntu 14.04.4 LTS (GNU/Linux 3.14.52 armv7l) root@imx6Q:~# chown root:root /usr/bin/sudo root@imx6Q:~# chmod 4755 /usr/bin/sudo root@imx6Q:~# exit Login with <user $> or root # # apt-get update # apt-get –f install # apt-get install locales dialog wget # dpkg-reconfigure locales # apt-get upgrade Optional – install some useful packages: # apt-get install openssh-server can-utils usbutils build-essential automake autoconf libtool Get and Install the BSP packages (EULA required) # cd /home/user # mkdir –p vpu_pack # cd vpu_pack # wget http://www.nxp.com/lgfiles/NMG/MAD/YOCTO//firmware-imx-5.3.bin # wget http://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-5.4.32.bin # wget http://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libfslcodec-4.0.8.bin # wget http://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-lib-5.1.tar.gz # chmod +x * # ./firmware-imx-5.3.bin --auto-accept --force # mkdir –p /lib/firmware/vpu # cp -ravf firmware-imx-5.3/firmware/* /lib/firmware/ # ./imx-vpu-5.4.32.bin --auto-accept --force # cd imx-vpu-* # make PLATFORM=IMX6Q all # make install # tar -xf imx-lib-5.1.tar.gz # cd  imx-lib-5.1/ # make -j1 PLATFORM="IMX6Q" # make PLATFORM="IMX6Q" install # cd .. # ./libfslcodec-4.0.8 --auto-accept –force # cd libfslcodec-* # ./autogent.sh --prefix=/usr --enable-fhw --enable-vpu # make # make install # mv /usr/lib/imx-mm/video-codec/* /usr/lib # mv /usr/lib/imx-mm/audio-codec/* /usr/lib # rm –rf /usr/lib/imx-mm/ # cd .. # mkdir –p gpu_pack # cd gpu_pack # wget http://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-5.0.11.p7.4-hfp.bin # wget http://www.nxp.com/lgfiles/NMG/MAD/YOCTO//xserver-xorg-video-imx-viv-5.0.11.p7.4.tar.gz # chmod +x * # ./imx-gpu-viv-5.0.11.p7.4-hfp –-auto-accept -–force # cd imx-gpu* # cp g2d/usr/include/* /usr/include/ # cp -d g2d/usr/lib/* /usr/lib/ # cp -Pr gpu-core/usr/* /usr # optional: install demos # cp -r gpu-demos/opt / # optional: install gpu tools # cp -axr gpu-tools/gmem-info/usr/bin/* /usr/bin/ # cd .. Installing gstreamer-imx, IPU, VPU and GPU support: Install build deps, gstreamer1.x, this step could take some time (~350MB): # apt-get install python pkg-config git gstreamer1.0-x gstreamer1.0-tools gstreamer1.0-plugins-good gstreamer1.0-plugins-bad gstreamer1.0-alsa libgstreamer1.0-dev libgstreamer-plugins-base1.0-dev libgstreamer-plugins-good1.0-dev g++-multilib # git clone git://github.com/Freescale/gstreamer-imx.git # cd gstreamer-imx # ln –s /usr/lib/arm-linux-gnueabihf/gstreamer-1.0/ /usr/lib/gstreamer-1.0 # ./waf configure --prefix=/usr --kernel-headers=/include # ./waf # ./waf install # cd ../../ (optional) Install libimxvpuapi library: This library provides a community based open-source API to the NXP imx-vpu library (the low-level IMX6 VPU interface). # git clone git://github.com/Freescale/libimxvpuapi.git # cd libimxvpu* # ./waf configure –-prefix=/usr # ./waf # ./waf install # cd .. note './waf install' installs artifacts to its prefix + /lib/gstreamer-1.0 but they need to be installed to /usr/lib/arm-linux-gnueabihf/gstreamer-1.0 which is why we created a symlink above before installing note g2d lib required to build G2D note that x11 library is required to build EGL sink with Vivante direct textures (only needed for X11 support) note that libfslaudiocodec is required to build audio plugins Now you are ready to test gstreamer 6: Add GPU HW Acceleration for X11 NOTE: The original version of these build instructions can be found in the Gateworks wiki . Many thanks to them for writing this! IMX6 IPU, VPU, and GPU support via GStreamer and Gstreamer-imx plugins. Many of the pieces needed (firmware and source-code) are from NXP and not freely redistributable thus must be downloaded from their mirror and extracted from a shell script that forces you to read and agree to their End User License Agreement (EULA). The following instructions can be used on top of the debootstrap and should work on other sources of Ubuntu or other Linux distributions root filesystems as well You can easily add X11 support to a base image created with the debootstrap instructions above by adding a few package groups. You will need the following: X11 server - ie Xorg Display Manager - this controls the login to the X session Window Manager - manages window position, re-sizing, decorations, etc for X clients If in any case you have installed the Linaro LXDE rootfs, it includes the Xorg X11 server, the lxdm Display Manager, the openbox Window Manager, and others useful user applications including the Chromium browser, if you do not install linaro lxde and want to install it please do: this step could take some time (~650MB)   # apt-get install xinit lxde lxterminal lxappearance lxrandr lxshortcut lxinput xinit  xserver-xorg-dev mesa-utils mesa-utils-extra Notes: you will need to add a non-root user with adduser for Chromium browser to work. You may choose to set up auto-login for that user by editing /etc/lxdm/default.conf and setting the autologin property in the base section at the beginning of the config file. /etc/xdg/lubuntu/lxdm/lxdm.conf This document takes as based kernel version 3.14.52v, vivante 5.0.11p7.4 correspond to the kernel version used. you should check the BSP release notes in order to know which xserver and Vivante GPU files need to be downloaded from the NXP repos. $ sudo nano /etc/lxdm/default.conf    [base]    autologin=user To add hardware GPU acceleration to X11 you need to add some libraries and drivers provided by Freescale from the imx-gpu-viv package. This requires signing Freescales End User License Agreement (EULA). This package provides the following: libg2d - a documented low-level API to the GPU (used by things like libimxvpuapi for gstreamer-imx and the gpu-core drivers) gpu-core - provides all the various OpenGL libs (libGL, libGLESv1_CM, libGLESv1_CL, libGLESv2, libGLSLC, libCLC, libEGL, libGAL, libOpenCL, ls libOpenVG) typically provided by the mesa project. Note that several versions of libEGL/libGAL/libGLESv2/libVIVANTE are provided for different backend rendering systems: dfb, fb, wl, x11. # cd gpu_pack #cd imx-gpu-* # cp gpu-core/usr/lib/dri/vivante_dri.so /usr/lib/xorg/modules/drivers/ # chmod 644 /usr/lib/xorg/modules/drivers/vivante_dri.so # rm /usr/lib/arm-linux-gnueabihf/mesa/libGL.so* # rm /usr/lib/arm-linux-gnueabihf/mesa-egl/libEGL.so* # rm /usr/lib/arm-linux-gnueabihf/mesa-egl/libGLESv2.so* # rm /usr/lib/arm-linux-gnueabihf/mesa-egl/libOpenVG.so* # cd ../../ # cd gpu-pack # wget http://www.nxp.com/lgfiles/NMG/MAD/YOCTO//xserver-xorg-video-imx-viv-5.0.11.p7.4.tar.gz # tar –xf xserver* # cd xserver-org-video-imx* #looks lik have to made #git init # ./fastbuild.sh  BUILD_HARD_VFP=1 XSERVER_GREATER_THAN_13=1 # cd.. # cd kernel-modu* # make Switch to gpu-core x11 backend: # backend=x11 # ln -sf libEGL-${backend}.so /usr/lib/libEGL.so # ln -sf libEGL-${backend}.so /usr/lib/libEGL.so.1 # ln -sf libEGL-${backend}.so /usr/lib/libEGL.so.1.0 # ln -sf libGAL-${backend}.so /usr/lib/libGAL.so # ln -sf libGLESv2-${backend}.so /usr/lib/libGLESv2.so # ln -sf libGLESv2-${backend}.so /usr/lib/libGLESv2.so.2 # ln -sf libGLESv2-${backend}.so /usr/lib/libGLESv2.so.2.0.0 # ln -sf libVIVANTE-${backend}.so /usr/lib/libVIVANTE.so # ln -sf libGAL_egl.dri.so /usr/lib/libGAL_egl.so # for i in egl glesv1_cm glesv2 vg; do         cp /usr/lib/pkgconfig/${i}_${backend}.pc/usr/lib/pkgconfig/${i}.pc     done #rm /usr/lib/*-dfb.so /usr/lib/*-fb.so /usr/lib/*-wl.so (Optional in case you deploy your kernel version with GPU as module) make vivante kernel module (GPU kernel driver) load on boot: # echo vivante >> /etc/modules # nano /etc/udev/rules.d/10-imx.rules KERNEL=="galcore",  MODE="0660", GROUP="video" KERNEL=="mxc_asrc",  MODE="0666" Create an xorg.conf configured for the Vivante fbdev driver: # nano /etc/X11/xorg.conf Section "Device"     Identifier "i.MX Accelerated Framebuffer Device"     Driver "vivante"     Option "fbdev" "/dev/fb0"     Option "vivante_fbdev" "/dev/fb0"     Option "HWcursor" "false" EndSection Section "ServerFlags"     Option "BlankTime"  "0"     Option "StandbyTime"  "0"     Option "SuspendTime"  "0"     Option "OffTime"  "0" EndSection # cd .. Make sure the files copied into the correct places. If all compiled and copied, you should now see a bunch of new libraries in /usr/lib! Congratulations! After you finish you can reboot your system and start playing. Testing Gstreamer examples: show gstreamer-imx plugins: # gst-inspect-1.0 | grep imx imxvpu:  imxvpuenc_mjpeg: Freescale VPU motion JPEG video encoder imxvpu:  imxvpuenc_mpeg4: Freescale VPU MPEG-4 video encoder imxvpu:  imxvpuenc_h264: Freescale VPU h.264 video encoder imxvpu:  imxvpuenc_h263: Freescale VPU h.263 video encoder imxvpu:  imxvpudec: Freescale VPU video decoder imxv4l2videosrc:  imxv4l2videosrc: V4L2 CSI Video Source imxg2d:  imxg2dcompositor: Freescale G2D video compositor imxg2d:  imxg2dvideotransform: Freescale G2D video transform imxg2d:  imxg2dvideosink: Freescale G2D video sink imxipu:  imxipucompositor: Freescale IPU video compositor imxipu:  imxipuvideosink: Freescale IPU video sink imxipu:  imxipuvideotransform: Freescale IPU video transform imxpxp:  imxpxpvideotransform: Freescale PxP video transform imxpxp:  imxpxpvideosink: Freescale PxP video sink imxipuvideosink: # gst-launch-1.0 videotestsrc ! imxipuvideosink imxg2dvideosink: # gst-launch-1.0 videotestsrc ! imxg2dvideosink The imxeglvivsink allows hardware accelerated display to a window on the X11 host # export DISPLAY=:0.0 # gst-launch-1.0 videotestsrc ! imxeglvivsink To test if you have graphics support you can run any glmark2 and/or mesa-utils or can run example of the next route: # cd /opt/viv_samples/vdk/ # ./tutorial1                                                                      //any example root@imx6Q:~# glxgears -info GL_RENDERER   = Vivante GC2000 GL_VERSION    = 2.1 2.0.1 GL_VENDOR     = Vivante Corporation GL_EXTENSIONS = WGL_ARB_extensions_string WGL_EXT_extensions_string WGL_EXT_swap_control GL_EXT_texture_env_add GL_ARB_multitexture GL_ARB_multisample GL_ARB_texture_env_add GL_ARB_texture_compression GL_ARB_texture_env_combine GL_ARB_depth_texture GL_ARB_window_pos …. 1606 frames in 5.0 seconds = 321.130 FPS 1650 frames in 5.0 seconds = 329.834 FPS L_RENDERER   = Vivante GC2000 GL_VERSION    = 2.1 2.0.1 GL_VENDOR     = Vivante Corporation1629 frames in 5.0 seconds = 325.644 FPS 1621 frames in 5.0 seconds = 324.072 FPS 1650 frames in 5.0 seconds = 329.806 FPS 1651 frames in 5.0 seconds = 330.079 FPS
記事全体を表示
For more information verify the U-Boot User Manual[1].   First all configure your board IP, your host IP and the gateway IP:   => setenv ipaddr 10.29.244.91   => setenv serverip 10.29.244.27   => setenv gatewayip 10.29.244.27 You don't need to set the gatewayip when using cross'cable! Save this configuration to flash: => saveenv   Download the file to board RAM: => tftp 0x80000000 zImage   Where:   400000 is the memory position where the file will be placed;   zImage is the file that will be downloaded from TFTP server.  
記事全体を表示
How to load the camera driver modprobe ov3640_camera modprobe mxc_v4l2_capture How to encode audio gst-launch alsasrc ! mfw_mp3encoder ! filesink location= audio.mp3 Encoding an AVI audio only gst-launch alsasrc ! mfw_mp3encoder ! avimux ! filesink location=audio.avi You can use audiotestsrc instead of alsasrc Encoding Audio and Video (testsrc only) Raw video and Raw audio gst-launch videotestsrc num-buffers=250 ! 'video/x-raw-yuv,format=fourcc)I420,width=320,height=240,framerate=(fraction)25/1' ! queue ! mux. audiotestsrc num-buffers=440 ! audioconvert ! 'audio/x-raw-int,rate=44100,channels=2' ! queue ! mux. avimux name=mux ! filesink location=test.avi H.263 video and Raw audio gst-launch videotestsrc num-buffers=250 ! mfw_vpuencoder codec-type=1 ! queue ! mux. audiotestsrc num-buffers=440 ! audioconvert ! 'audio/x-raw-int,rate=44100,channels=2' ! queue ! mux. avimux name=mux ! filesink location=test.avi H.263 video and MP3 audio gst-launch videotestsrc num-buffers=250 ! mfw_vpuencoder codec-type=1 ! queue ! mux. audiotestsrc num-buffers=440 ! audioconvert ! mfw_mp3encoder ! queue ! mux. avimux name=mux ! filesink location=test.avi Real Source gst-launch-0.10 mfw_v4lsrc capture-mode=5 num-buffers=300 capture-width=320 capture-height=240 fps-n=15 blocksize=115200 ! queue2 max-size-buffers=1000 max-size-bytes=0 max-size-time=0 ! mfw_vpuencoder framerate=15 codec-type=2 name=venc  alsasrc num-buffers=300 ! audio/x-raw-int,rate=32000,channels=1,depth=16 ! audioconvert ! queue2 max-size-buffers=1000 max-size-bytes=0 max-size-time=0 ! mfw_mp3encoder name=aenc avimux name=mux ! filesink location=all_in_one.avi aenc. ! mux. venc. ! mux. The movie isn't that good, but you can improve that increasing num-buffers, width and heigh, and even framerate! STAMP If you face synchronization issues, you can try to use a non-standard plugin called stamp. Use the spec file gst-entrans.spec and this command line: gst-launch-0.10 mfw_v4lsrc capture-mode=5 num-buffers=160 capture-width=320 capture-height=240 fps-n=15 blocksize=115200 !  stamp sync-margin=1 sync-interval=1 ! queue2 max-size-buffers=1000 max-size-bytes=0 max-size-time=0  !  mfw_vpuencoder framerate=15 codec-type=2 name=venc  alsasrc num-buffers=160  !  audio/x-raw-int,rate=32000,channels=1,depth=16     !  audioconvert ! queue2 max-size-buffers=1000 max-size-bytes=0 max-size-time=0      !  mfw_mp3encoder name=aenc avimux name=mux ! filesink location=test_ALL.avi aenc. ! mux. venc. ! mux. Donwload the package from here: http://gentrans.sourceforge.net/ (source for stamp topic: http://blog.buberel.org/2008/03/using-a-usb-web.html)
記事全体を表示
LTIB Creating Uimage Uboot Configuration file for fw_(printenv/saveenv) utility Add new i.MX5x board on LTIB LTIB Creating Uimage Uboot U-boot expects uImage format for the kernel image. In order to LTIB generate a uImage file: $ export SYSCFG_KTARG=uImage $ ./ltib -p kernel Setup in U-Boot the kernel bootargs: u-boot> setenv bootargs noinitrd console=ttymxc0,115200 init=/linuxrc root=/dev/nfs nfsroot=10.29.244.27:/tftpboot/rootfs ip=dhcp Change 10.29.244.27 to your host IP. The procedure above is needed when default bootloader used by ltib was redboot. In some ltib releases (before 2010) default bootloader is u-boot. In this case, ltib will create uImage by default Configuration file for fw_(printenv/saveenv) utility # Configuration file for fw_(printenv/saveenv) utility. # Up to two entries are valid, in this case the redundant # environment sector is assumed present. # Notice, that the "Number of sectors" is ignored on NOR.               # MTD device name Device offset Env. size Flash sector size Number of sectors #/dev/mtd1 0x0000 0x4000 0x4000 #/dev/mtd2 0x0000 0x4000 0x4000 # NAND example /dev/mtd0 0x80000 0x40000 0x20000 2 Add new i.MX5x board on LTIB After porting u-boot to your i.MX5x board you might want add it on LTIB menu, "Choose your board for u-boot" section. For this, edit ltib/config/platform/imx/main.lkc to add your board: Enter board on menu: comment "Choose your board for u-boot" choice prompt "board" default BOARD_MX51_BBG depends on PLATFORM = "imx51" help This menu will let you choose the board you use. ... + config BOARD_MX53_MYBOARD + bool "mx53_myboard" ... endchoice Add the "mx53_myboard_config" that matches your board configuration on the u-boot Makefile to PKG_U_BOOT_CONFIG_TYPE: config PKG_U_BOOT_CONFIG_TYPE   string   ... + default "mx53_myboard_config" if ( PLATFORM = "imx51" && BOARD_MX53_MYBOARD && !PKG_KERNEL_UPDATER )   ...
記事全体を表示
This patch implements (or exposes) routines to poll the imx uarts. The KGDB drivers need these methods to be implemented or the ttymxc driver is not sufficient. The synthetic CONFIG_CONSOLE_POLL value activates these routines (or CONFIG_SERIAL_MXC_CONSOLE for the polled write). There is still no poll routines in -855-ge067785, which is the September 2010 Linux release from Freescale. Also not in Linux 2.6.36 drivers/serial/imx.c either. $ git diff drivers/serial/mxc_uart.c diff --git a/drivers/serial/mxc_uart.c b/drivers/serial/mxc_uart.c index ae6d2e1..728b607 100644 --- a/drivers/serial/mxc_uart.c +++ b/drivers/serial/mxc_uart.c @@ -1551,6 +1551,28 @@ mxcuart_pm(struct uart_port *port, unsigned int state, unsigned int oldstate)                             clk_enable(umxc->clk);    }  +#ifdef CONFIG_CONSOLE_POLL +/* + * Read a character from the UART. + */ +static inline int mxcuart_console_read_char(struct uart_port *port) +{ +       volatile unsigned int status; +    int ch; + +       do { +               status = readl(port->membase + MXC_UARTUSR2); +       } while ((status & MXC_UARTUSR2_RDR) == 0); +       ch = readl(port->membase + MXC_UARTURXD); +/* Ignore parity errors, etc. */ +/*  status = ch | UART_CREAD_BIT; */ +    ch &= 0xff; + +    return ch; +} +static void mxcuart_console_write_char(struct uart_port *port, char ch); +#endif +    /*!     * This structure contains the pointers to the control functions that are     * invoked by the core serial driver to access the UART hardware. The @@ -1575,14 +1597,18 @@ static struct uart_ops mxc_ops = {                 .config_port = mxcuart_config_port,                 .verify_port = mxcuart_verify_port,                 .send_xchar = mxcuart_send_xchar, +#ifdef CONFIG_CONSOLE_POLL +              .poll_put_char = mxcuart_console_write_char, +              .poll_get_char = mxcuart_console_read_char, +#endif };  -#ifdef CONFIG_SERIAL_MXC_CONSOLE +#if defined(CONFIG_SERIAL_MXC_CONSOLE) || defined (CONFIG_CONSOLE_POLL)     /*     * Write out a character once the UART is ready     */ -static inline void mxcuart_console_write_char(struct uart_port *port, char ch) +static void mxcuart_console_write_char(struct uart_port *port, char ch)    {            volatile unsigned int status;  @@ -1592,6 +1618,10 @@ static inline void mxcuart_console_write_char(struct uart_port *port, char ch)                writel(ch, port->membase + MXC_UARTUTXD);     }  +#endif + +#ifdef CONFIG_SERIAL_MXC_CONSOLE +    /*!     * This function is called to write the console messages through the UART port.     *
記事全体を表示
The i.MX6SX series of applications processors are powered by two asymmetrical cores: one ARM Cortex-A9 and one Cortex-M4. It allows the coexistence of real-time and non-real-time applications on the same processor (M4 core running an RTOS, and A9 core running Linux or Android). This document will explain how to compile and download a customized MQX application to the QSPI Flash of the IMX6SX-SDB board using a Ubuntu host. The example application will be connecting a 16x2 LCD to GPIO pins of the i.MX6SX. As the IMX6SX-SDB board doesn’t have GPIO header, we will use the pins from SD3 socket, so, it will be required to add the proper pin definitions to the MQX BSP. First of all, the Yocto image will be used as base to boot the A9 core (BSP L3.14.28_1.0.0), because it is the main core and the M4 core will be held on reset until the A9 removes the reset from it. The Yocto image includes many device tree files on the FAT partition, and the default DTB doesn’t consider the existence of the M4 core (only required when Linux applications would consider the M4 core as a resource), so, for changing the DTB file, launch the following command on U-Boot: => setenv fdt_file imx6sx-sdb-m4.dtb We are going to download and uncompress MQX 4.1 for i.MX6SX (Linux hosted) from the following link: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX In this example, GCC compiler for ARM will be used, so, download and uncompress gcc-arm-none-eabi-4_8-2014q1 from the link below: https://launchpad.net/gcc-arm-embedded/+download Additional Linux commands consider that MQX and GCC were uncompressed on /home/user folder. In order to avoid compiler error, it will be required to set a couple of environments variables: $ export TOOLCHAIN_ROOTDIR=/home/user/gcc-arm-none-eabi-4_8-2014q1 $ export PATH=$PATH:/home/user/gcc-arm-none-eabi-4_8-2014q1/bin/ Before building any MQX example applications, it is required to build MQX libraries (included BSP and PSP), so, navigate to the next folders and launch the build script in each of them: $ cd /home/user/ Freescale_MQX_4.1.0_i.MX_6SoloX /mqx/build/make/bsp_imx6sx_sdb_m4/ $ ./build_gcc_arm.sh $ cd /home/user/ Freescale_MQX_4.1.0_i.MX_6SoloX /mqx/build/make/psp_imx6sx_sdb_m4/ $ ./build_gcc_arm.sh Now we can compile the example applications like the GPIO demo (that will be used as base for our customized application): /home/user/Freescale_MQX_4.1.0_i.MX_6SoloX/mqx/examples/gpio/ Our example application will configure the 6 pins of the SD3 socket (LWGPIO_PIN_SD3_DATA0, LWGPIO_PIN_SD3_DATA1, LWGPIO_PIN_SD3_DATA2, LWGPIO_PIN_SD3_DATA3, LWGPIO_PIN_SD3_CMD, LWGPIO_PIN_SD3_CLK) for using them by the M4 core on MQX; so, it will be required to add the proper definitions on the board’s header file for each pin (in this case, “imx6sx_sdb_m4.h”). The following corresponds to the LWGPIO_PIN_SD3_DATA0 pin (we are naming them as “SD2GPIO0 – SD2GPIO5”): #define BSP_SD2GPIO0_PROMPT         "SD2GPIO0" #define BSP_SD2GPIO0                (LWGPIO_PIN_SD3_DATA0) #define BSP_SD2GPIO0_MUX_GPIO       (LWGPIO_MUX_SD3_DATA0_GPIO) #define BSP_SD2GPIO0_MUX_IRQ        (LWGPIO_MUX_SD3_DATA0_GPIO) As this file is part of the BSP, it will be required to recompile the BSP after applying these modifications. The modified header file could be found on the attachments of this document. Now, we are going to copy the entire folder of the “gpio” example to the same location, and we will rename it as “sd2gpio”. Inside such folder, we should also rename the “gpio.c” file to “sd2gpio.c”. Besides, it is required to edit the “Makefile” file in order to redirect the included paths to the new folder. It is basically done on the following two lines: NAME = sd2gpio SOURCES += $(MQX_ROOTDIR)/mqx/examples/sd2gpio/sd2gpio.c The modified “Makefile” file is also available on the attachments. The “sd2gpio.c” file includes the main MQX task that will initialize the LWGPIOs using the definitions declared on the board’s header file. It also includes the functions used by the 16x2 LCD driver. This file is also included on the attachments of this thread. With all the modifications done and the BSP recompiled, we can now compile our customized application by launching the command: $ ./build_gcc_arm.sh Located on the following path: /home/user/Freescale_MQX_4.1.0_i.MX_6SoloX/mqx/examples/gpio/build/make/ gpio_imx6sx_sdb_m4/ The output file (an ELF file) will be located at the following path: /home/user/Freescale_MQX_4.1.0_i.MX_6SoloX/mqx/examples/gpio/build/make/ gpio_imx6sx_sdb_m4/cd gcc_arm/extflash_debug/ Now, we are going to move to this folder, and launching the following command to convert the ELF file to a BIN file. It is required because we will flash the QSPI Flash using the A9 core, and the symbols data of the ELF file is not required (actually, the flashing applications looks for “m4_qspi.bin” file): $ arm-none-eabi-objcopy -O binary sd2gpio_imx6sx_sdb_m4.elf m4_qspi.bin Next, copy the BIN file to the FAT partition of the SD card (considering it is mounted over /media/ 😞 $ cp m4_qspi.bin /media/Boot\ imx6sx/ && sync Now we will place the SD card on the SDB board and boot it. Stop the boot process on U-Boot and launch the following command for flashing the QSPI Flash from the BIN file: => run update_m4_from_sd Finally, start the MQX application by releasing the reset of the M4 by launching the following command: => run m4boot The figure below shows the LCD with the application working: Additional tests: If you want to run the M4 application out of reset you could modify the environment variable ‘bootcmd’. For displaying the default variable value, launch the following command: => printenv bootcmd So, for just removing the reset from M4 core without booting Linux, launch the command below: => setenv bootcmd=‘run m4boot’ If you want to avoid the count-down delay (for a faster boot), you could try the following command: => setenv bootdelay 0 Finally, if Linux is also boots after the M4, it will change some clock settings, and also mounts the SD3 driver, so, the pin configurations will be overrode. In order to avoid clock issues on the M4, add to boot parameters ‘uart_from_osc' like command below: => setenv mmcargs 'setenv bootargs no_console_suspend clk_ignore_unused uart_from_osc console=${console},${baudrate} root=${mmcroot}' Don’t forget to save the environment after changing environments variables and then, reboot: => saveenv
記事全体を表示
Video in Host Side Converting images (png, jpg, etc) to YUV format ffmpeg -f image2 -i test.png -pix_fmt yuv420p test.yuv Converting AVI files to YUV format To convert AVI to YUV you can use the lav2yuv program. In Ubuntu Linux this program is in mjpegtools package. This is the way to convert: lav2yuv myfile.avi > myfile.yuv Converting YUV video files to AVI (DivX) Use the ffmpeg tool: ffmpeg -s 176x144 -i kuuba_maisema_25fps_qcif.yuv -vcodec mpeg4 -sameq -aspect 4:3 ~/kuuba.avi You need to specify the video dimensions (176 × 144), the video codec (mpeg4), and the aspect ratio (4:3). Converting MP4 to AVI Use the mencoder tool: mencoder Bike1.mp4 -ovc lavc -oac lavc -o NewBike1.avi
記事全体を表示
Building Linux Kernel Building Linux Kernel Building Using LTIB Building Outside LTIB Downloading and installing GNU Toolchain and git Building Kernel from Freescale git repository Building Kernel Mainline About Linux Building Using LTIB Linux kernel can be easily built using Ltib. On Ltib menu, just select: [*] Configure the Kernel When you exit this menu, Ltib will show the Kernel Menuconfig as below: This is the Kernel Menuconfig, where it's possible to configure kernel options and drivers. After exit this menu, kernel will be built and stored at: <Ltib directory>/rootfs/boot Building Outside LTIB Downloading and installing GNU Toolchain and git When you install LTIB, a GNU toolchain is automatically installed on /opt/freescale/usr/local/ Kernel releases newer than 2.6.34 doesn't build on Toolchain 4.1.2, only on 4.4.1 or later Check on your host at /opt/freescale/usr/local/ the current installed Toolchain. Next step is to install GIT on host. For Ubuntu machines, use: sudo apt-get install git-core Building Kernel from Freescale git repository Freescale provides access to their own git kernel repository and can be viewed at: Freescale Public GIT To download the kernel source code, create a new folder and use the command: git clone git://git.freescale.com/imx/linux-2.6-imx.git OR git clone http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git After some minutes, a folder called linux-2.6-imx will be created containing the Linux kernel Create a local git branch from a remote branch you want to use. Let's use branch origin/imx_3.0.15 as example: cd linux-2.6-imx git checkout -b localbranch origin/imx_3.0.15 To check all available remote branches, use: git branch -r Export the cross compiler, architecture and the toolchain path: export ARCH=arm export CROSS_COMPILE=arm-none-linux-gnueabi- If using Toolchain 4.1.2: export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" OR If using Toolchain 4.4.4: export PATH="$PATH:/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/" Copy the config file for the wanted platform on linux folder as example: cp arch/arm/configs/imx6_defconfig .config All platform config files are located at <linux directory>/arch/arm/configs/ Call menuconfig and change configuration (if needed) make menuconfig Now it's ready to be built: make uImage The zImage and uImage will be located at /arch/arm/boot/ folder. Building Kernel Mainline Mainline Kernel can be viewed on this link: https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git To download the kernel source code, create a new folder and use the command: git clone git://git.kernel.org/pub/scm/linux/kernel/git/stable/linux-stable.git OR git clone http://git.kernel.org/pub/scm/linux/kernel/git/stable/linux-stable.git OR git clone https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux-stable.git After some minutes, a folder called linux will be created containing the Linux kernel Create a local git branch from a remote branch you want to use. Let's use branch origin/linux-3.8.y as example: cd linux git checkout -b localbranch origin/linux-3.8.y To check all available remote branches, use: git branch -r Export the cross compiler, architecture and the toolchain path: export ARCH=arm export CROSS_COMPILE=arm-none-linux-gnueabi- If using Toolchain 4.4.4: export PATH="$PATH:/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/" Configure to the platform you want to build kernel. For i.MX family, use imx_v6_v7_defconfig: make imx_v6_v7_defconfig All platform config files are located at <linux directory>/arch/arm/configs/ Call menuconfig and change configuration (only if needed, this is an optional step!) make menuconfig Now it's ready to be built: make -j4 uImage LOADADDR=0x70008000 - Use -j4 option to speed up your build in case or PC has 4 cores. It's optional. - IMPORTANT: Use the correct address for each processor. You can check the correct address value at linux/arch/arm/mach-imx/Makefile.boot. After build the uImage, build the dtb file (device tree binary). For i.MX53 QSB use: make imx53-qsb.dtb The uImage will be located at: linux/arch/arm/boot/ folder and dtb binary will be located at: linux/arch/arm/boot/dts About Linux For general Linux information, see About Linux
記事全体を表示