i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Play MPEG4 Video only gst-launch filesrc location=test.mpeg ! mfw_vpudecoder codec-type=std_mpeg4 ! mfw_v4lsink H.264 Video only gst-launch filesrc location=test.avi ! mfw_avidemuxer ! mfw_vpudecoder codec-type=std_avc ! mfw_v4lsink AVI(H264+MP3) gst-launch filesrc location=test.avi ! mfw_avidemuxer name=demux demux. !  mfw_vpudecoder \     codec-type=std_avc ! mfw_v4lsink demux. ! queue max-size-buffers=0 ! <mp3_decoder_plugin> ! alsasink MP4(H264+MP3) gst-launch filesrc location=test.mp4 ! mfw_mp4demuxer name=demux demux. ! \    mfw_vpudecoder codec-type=std_mpeg4 ! mfw_v4lsink demux. ! \    queue max-size-buffers=0 ! <mp3_decoder_plugin> ! alsasink <mp3_decoder_plugin> can be replaced by mad RAW Video Test gst-launch videotestsrc ! video/x-raw-yuv,format=\(fourcc\)I420 !  mfw_v4lsink
查看全文
The i.MX 8QXP MEK does not allow the OV5640/LVDS/LCD usage only by changing the device tree anymore. It occurs because the M4 owns the i2c resources, so the A core must use rpmsg to enable virtual drivers. Due to this, if the user changes the device tree, for instance, the *ov5640.dtb, the kernel won't boot, entering in the following loop: [    8.603353] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).      [    8.610025] [drm] No driver support for vblank timestamp query.              [    8.616077] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_) [    8.624978] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_op) [    8.632526] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_op) [    8.639833] imx-drm display-subsystem: failed to bind ldb@562210e0 (ops imx_7 [    8.648428] imx-drm display-subsystem: master bind failed: -517 With the approach provided in this post, it is possible to make this change manually, only by changing the flash.bin at U-boot for a non-m4 one. In order to make the changes to the flash.bin file, it’s needed to obtain the following files: - u-boot.bin from internal u-boot provided by NXP. - scfw_tcm.bin from SCFW porting kit - bl31.bin from ARM Trusted Firmware - SECO firmware container image Disclaimer The described procedures in this document target a GNU/Linux (Ubuntu 20.04 LTS) and it’s focused on iMX8QXP B0 + BSP L4.19.35_1.1.0. Required packages 1 - Install ARM64 ToolChain: 1.1 - Install ARM64 GCC and G++ cross-compilers: # apt install gcc-aarch64-linux-gnu g++-aarch64-linux-gnu 2 - Install ARM32 GCC6 ToolChain: 2.1 - Download the ARM32 6 Toolchain and install it: $ mkdir ~/gcc_toolchain $ cp ~/Downloads/gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 ~/gcc_toolchain/ $ cd ~/gcc_toolchain/ $ tar xvjf gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 # apt-get update # apt-get install srecord 3 - Download MKimage 3.1 - Create a new directory desired to the packages: $ mkdir flash_build $ cp flash_build 3.1 - Clone the MKimage: $ git clone https://source.codeaurora.org/external/imx/imx-mkimage -b imx_4.19.35_1.1.0 4 - U-boot build 4.1 - Clone the U-boot  $ git clone https://source.codeaurora.org/external/imx/uboot-imx -b imx_v2019.04_4.19.35_1.1.0 $ cd uboot-imx 4.2 - Export the ARM64 ToolChain:  $ export ARCH=arm64 $ export CROSS_COMPILE=/usr/bin/aarch64-linux-gnu- 4.3 - Build it:  $ unset LDFLAGS $ make -j4 imx8qxp_mek_defconfig $ make 4.4 - Copy the binary files to the MKimage/iMX8QX directory:  $ cp spl/u-boot-spl.bin ../imx-mkimage/iMX8QX/ $ cp u-boot-nodtb.bin ../imx-mkimage/iMX8QX/ $ cd ..   5 - ARM Trusted Firmware 5.1 - Clone the imx-atf:  $ git clone https://source.codeaurora.org/external/imx/imx-atf -b imx_4.19.35_1.1.0 $ cd imx-atf 5.2 - Build it:  $ unset LDFLAGS $ make PLAT=imx8qx bl31 5.3 - Copy the binary files to the MKimage/iMX8QX directory:  $ cp build/imx8qx/release/bl31.bin ../imx-mkimage/iMX8QX/ $ cd ..   6 - SCFW 6.1 - Export the ARM32 GCC6 Toolchain:  $ export TOOLS=~/gcc_toolchain/ 6.2 - Download the BSP L4.19.35_1.1.0_SCFW and copy it to the flash_build directory:  $ cp ~/Downloads/imx-scfw-porting-kit-1.2.7.1.tar.gz $ tar xvzf imx-scfw-porting-kit-1.2.7.1.tar.gz $ cd packages/ $ chmod a+x imx-scfw-porting-kit-1.2.7.1.tar.gz $ ./imx-scfw-porting-kit-1.2.7.1.bin 6.3 - Build it to i.MX 8QXP MEK B0:  $ cd imx-scfw-porting-kit-1.2.7.1/src/ $ tar xvzf scfw_export_mx8qx_b0.tar.gz $ cd scfw_export_mx8qx_b0/ $ make qx R=B0 B=mek 6.4 - Copy the binary file to the MKimage/iMX8QX directory:  $ cp build_mx8qx_b0/scfw_tcm.bin ../../../../imx-mkimage/iMX8QX/ $ cp ../../../../ 7 - SECO Firmware Container Image 7.1 - Download the SECO firmware binaries and copy it to the flash_build directory $ cp ~/Downloads/firmware-imx-7.9.bin . $ chmod a+x firmware-imx-7.9.bin 7.2 - Copy the binary files to the MKimage/iMX8QX directory:  $ cp firmware-imx-7.9/firmware/seco/mx8qx-ahab-container.img /imx-mkimage/iMX8QX/ 8 - Build flash.bin 8.1 - In a new terminal, open the imx-mkimage directory: $ cd flash_build/imx-mkimage 8.2 - Build it:  $ make SOC=iMX8QX flash 8.3 - Deploy it to the SDCard:  $ sudo dd if=iMX8QX/flash.bin of=/dev/sdX bs=1k seek=32 && sync Now, you are able to use any non-rpmsg.dtb without kernel errors. Author: Pedro Jardim: [email protected]
查看全文
U-boot expects uImage format for the kernel image. In order to LTIB generate a uImage file: $ export SYSCFG_KTARG=uImage $ ./ltib -p kernel Setup in U-Boot the kernel bootargs: u-boot> setenv bootargs noinitrd console=ttymxc0,115200 init=/linuxrc root=/dev/nfs nfsroot=10.29.244.27:/tftpboot/rootfs ip=dhcp Change 10.29.244.27 to your host IP. The procedure above is needed when default bootloader used by ltib was redboot. In some ltib releases (before 2010) default bootloader is u-boot. In this case, ltib will create uImage by default
查看全文
Tips collected from zhaoyang-b49593 and dandouglass-b41520 while enabling redundant boot: Using i.MX 8MQ, same method can be applied for other i.MX devices that support redundant boot, see SoC Reference Manual. As described on the RM, if primary image authentication fails the ROM can reset and try booting a secondary image. This feature is only available on closed mode with properly signed binaries, otherwise the ROM boots the primary image despite the auth failure. For the i.MX 8MQ, the secondary image must start with spl, not HDMI firmware. Note, there is no ROM redundancy for the hdmi fw, if it is corrupt user can store a 2nd copy on a different memory address and update at run time. Steps to generate a dual spl image: 1. Build and Sign bootable binary (spl, u-boot, atf, fw, etc) Use the Yocto BSP or follow this post to build outside the Yocto environment. To sign the binary, follow the documentation on u-boot source: <u-boot>/doc/imx/habv4/guides/mx8m_secure_boot.txt Program image to the SD card: dd if=signed_flash.bin of=<sd path> bs=1024 seek=33 After boot you can use "hab_status" to verify that no events were generated: u-boot=> hab_status Secure boot disabled HAB Configuration: 0xf0, HAB State: 0x66 2. Corrupt spl on your boot image You can corrupt anywhere on the spl signed area. For easier visualization at boot time we can corrupt the SPL banner. First create a copy: cp signed_flash.bin signed_flash_corrupt.bin Find the banner: hexdump -C signed_flash.bin | grep 2019 00020190 26 1c 40 92 04 00 80 d2 05 01 80 52 c4 20 04 aa |&[email protected]. ..| 0002eac0 32 30 31 39 2e 30 34 2d 30 30 30 32 39 2d 67 34 |2019.04-00029-g4| 000dde10 3a 20 20 00 55 2d 42 6f 6f 74 20 32 30 31 39 2e |: .U-Boot 2019.| 0002eac3 is on spl area, where "9" for 2019 is, replace by "X" printf "X" > X dd if=X of=signed_flash_corrupt.bin seek=$((0x2eac3)) bs=1 conv=notrunc Verify corrupt binary hexdump -C -s 0x2eac0 -n 64 signed_flash_corrupt.bin 0002eac0 32 30 31 58 2e 30 34 2d 30 30 30 32 39 2d 67 34 |201X.04-00029-g4| 0002ead0 37 63 31 39 32 32 20 28 41 70 72 20 32 37 20 32 |7c1922 (Apr 27 2| Transfer image to SD Card dd if=signed_flash_corrupt.bin of=<sd path> bs=1024 seek=33 Now, you should see hab events after running "hab_status" on u-boot 3. Create a secondary boot image This can be the same content as your primary image without the HDMI fw or it can be a different spl image. For easier visualization, we can change the SPL banner, on the code this time. Modify banner at ./common/spl/spl.c as: - puts("\nU-Boot " SPL_TPL_NAME " " PLAIN_VERSION " (" U_BOOT_DATE " - " + puts("\nSecondary U-Boot " SPL_TPL_NAME " " PLAIN_VERSION " (" U_BOOT_DATE " - " As mentioned above, we want our boot image without the HDMI fw, when running imx-mkimage use the flash_evk_no_hdmi target: make SOC=iMX8MQ flash_evk_no_hdmi Sign the image as in step 1. If you program the new image to the SD you should see the new banner. Make sure to run hab_status to confirm that no HAB events are generated. 4. Program SRK Hash and Close SoC Follow the documentation on u-boot source for SRK programming and closing the device: <u-boot>/doc/imx/habv4/guides/mx8m_secure_boot.txt Before closing the SoC, but after the SRK is programmed, try your images to confirm no HAB events are generated. Be careful with this step, errors could brick your board. This step is irreversible. After closing the SoC it will only boot signed images. 5. Create dual bootloader image We can concatenate our binaries to create a single file, let's use 2MB distance between primary and secondary images: For the working primary image: objcopy -I binary -O binary --pad-to 0x200000 --gap-fill=0x00 signed_flash.bin 1st-spl_pad.bin cat 1st-spl_pad.bin secondary2_nohdmifw_signed_flash.bin > 1st-spl_pad_2nd-spl.bin Or for the corrupt primary image experiment: objcopy -I binary -O binary --pad-to 0x200000 --gap-fill=0x00 signed_flash_corrupt.bin 1st-spl_pad.bin cat 1st-spl_pad.bin secondary2_nohdmifw_signed_flash.bin > 1st-spl_pad_2nd-spl.bin Program it to the SD card on 0x8400 offset (33k) dd if=1st-spl_pad_2nd-spl.bin of=<sd path> bs=1024 seek=33 && sync 6. Add Secondary image table Follow the format on the RM, this is only 20 bytes long. For a 2MB distance between the table and the secondary image we can use "0x1000" on the firstSectorNumber field. 2MB/512 = 4096 (0x1000) The perl script attached, genSecTable.pl, can be used to generate it. perl genSecTable.pl 0x1000 Program it to the SD card on 0x8200 offset dd if=secTable.bin of=<sd path> bs=1 seek=$((0x8200)) && sync 7. Verify secondary image is booting If using the corrupt primary image, you should see the spl with the "Secondary U-Boot SPL..." banner. You can also read the persist secondary boot bit. u-boot=> md.l 0x30390098 1 30390098: 40000000 ...@ The work can be extended patching spl for in case of u-boot authentication failure, spl can try to authenticate and jump to the secondary u-boot.
查看全文
Encode From YUV to H.264 gst-launch-0.10 filesrc location=file_in.yuv blocksize=w*h*1.5 ! \ mfw_vpuencoder codec type=std_avc framerate=fr ! filesink location=file_out.mpg Where: file_in.yuv: is the input file, a raw file. w*h*1.5: is the blocksize, it's calculated from input file dimensions: width * height * 1.5 mfw_vpuencoder: is the encoder with hardware acceleration for iMX27 std_avc: chooses the codec type for output file fr: indicates the framerate in that input file was created file_out.mpg: is the output file encoded in H.264 From Camera to H.264 gst-launch-0.10 mfw_v4lsrc ! mfw_vpuencoder codec-type=std_avc \ width=176 height=144 framerate=25 ! filesink location=test.video
查看全文
The resource management service offers the possibility to divide the system into groups of resources or partitions. Resources within a partition can not access resources outside of it's partition. Partitioning a system is useful to isolate resources from one another, this gives you the ability to have for instance FreeRTOS and Linux each running simultaneously with its own set of resources. In the FreeRTOS/Linux example you could partition/divide the system into two groups/partitions where all resources/peripherals needed by FreeRTOS would be completely isolated from the resources needed by Linux, if any of the resources on the Linux partition tried to access a resource on the FreeRTOS partition the transaction would result in a bus error, as if the resource tried to access a region outside of its memory map. The partitioning mechanism is enforced by hardware and the configuration of the underlying hardware is completely abstracted by the SCFW API. The system partitioning can be performed in two ways: At boot time by modifying the function board_system_config on the board.c portion of the SCFW porting kit that corresponds to your board. This is used for software that is loaded as part of the boot process. At run time by calling the resource management service functions available. This is used to partition software that is launched by an operating system, e.g. an M4 used as sensor fusion and loaded/started by Linux. A partition can have: Resources (peripherals) Pads Memory regions All of the items mentioned above can be grouped within a partition. It is important to note that: At boot time all resources are grouped into a single partition. Resources can only be assigned to another partition by a resource within it's own partition.  Initial partitioning state of the system At boot time the system is initially configured in three partitions: The first partition (SCFW) contains all the resources, pads and memory required by the System Controller Unit (SCU) to execute the System Controller Firmware. The second partition (SECO) contains all the resources required by the Security Controller to execute. The third partition (Boot) contains all of the remaining resources, pads and memory available for the whole system. Once Linux and the M4 boot a typical use case is to partition the system as follows: In this case the boot partition is split into the ATF/Linux partition and the M4 partition. The ARM Trusted Firmware environment add a layer of abstraction to secure the environment and it is assigned cores and memory to execute in this privileged state, all the remaining resources, pads and memory are assigned to the Linux partition. The M4 partition contains all the resources required by the M4 to execute, as well as the resources required by the application running on the M4. Resource partitioning - Boot time configuration The SCFW porting kit provides an example on doing boot time configuration at the board.c file under platform/board/mx8q<x or m>_<your board>/board.c, board_system_config is the function in charge of partitioning the system at boot time. From the sc_fw_port.pdf (porting guide) document included in the porting kit - Boot Flags chapter: Here are a few important points to highlight: The code will only execute if the SC_BD_FLAGS_ALT_CONFIG is set under the boot flags (more details in the Usage chapter of the sc_fw_port.pdf), the flags are set while building the image with mkimage. An example is provided to build an image with partitioning enabled: flash_linux_m4: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin u-boot-atf.bin m4_image.bin ./$(MKIMG) -soc QX -rev B0 -append mx8qx-ahab-container.img -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a35 0x80000000 -p3 -m4 m4_image.bin 0 0x34FE0000 -out flash.bin‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The example above can be found under your i.MX8 variant on the soc.mak file, in the example above the SC_BD_FLAGS_ALT_CONFIG flag is being set by -flags 0x00200000 and the partition for the M4 is defined as the third one by the -p3 parameter. Without the -flags 0x00200000 (setting SC_BD_FLAGS_ALT_CONFIG) parameter on mkimage NO partition happens at boot time, if the target used to build the image does not set this flag, then the SCU does not partition the system. On the board.c file the code in charge of checking for this flag is the following: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) {‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ if the alt_config flag is not set, then the partitioning is skipped. The function rm_dump(pt_boot); dumps the partitioning state of the whole system, it can be called before and after the partitioning to make sure the device was partitioned as expected. Here is how a partition dump looks like: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated Partition: 1 Parent: 0 DID: 0 Flags: Used Isolated Partition: 2 Parent: 0 DID: 1 Flags: Used Secure Restricted Isolated *** Resources *********************************** Partition: 0 SC_PID0 SC_SEMA42 SC_TPM SC_PIT SC_UART ... Continues .... DBLOGIC DRC_0 DRC_1 Partition: 1 SC_PID1 SC_PID2 SC_PID3 SC_PID4 ... Continues .... BOARD_R5 BOARD_R6 BOARD_R7 Partition: 2 SECO CAAM_JR1 CAAM_JR1_OUT *** Memory Regions ****************************** Partition: 0 000: 0x030FE0000 - 0x03101FFFF Partition: 1 001: 0x000000000 - 0x01BFFFFFF 002: 0x034000000 - 0x037FFFFFF 003: 0x038000000 - 0x03BFFFFFF 004: 0x060000000 - 0x06FFFFFFF 005: 0x070000000 - 0x07FFFFFFF 006: 0x080000000 - 0x0FFFFFFFF 007: 0x400000000 - 0x43FFFFFFF 008: 0x880000000 - 0xFFFFFFFFF Partition: 2 *** Pads **************************************** Partition: 0 M40_I2C0_SCL M40_I2C0_SDA ... Continues .... SCU_BOOT_MODE4 SCU_BOOT_MODE5 Partition: 1 SIM0_CLK SIM0_RST SIM0_IO ... Continues .... ENET1_RGMII_RXD2 ENET1_RGMII_RXD3 COMP_CTL_GPIO_1V8_3V3_ENET_ENETA Partition: 2‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The dump contains the configuration of the partition, for instance: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ On the example above the Partition parent is partition 0 (itself, this is the System Controller partition, all partitions spawn from this one). The Domain ID (DID) is 2, this ID is used to identify the partition by the hardware, it is used to enforce hardware isolation. It is also a secure and isolated partition, the meaning of these flags can be found below and in the sc_fw document: Secure - boolean indicating if this partition should be secure; only valid if caller is secure Isolated - boolean indicating if this partition should be HW isolated; set SC_TRUE if new DID is desired Restricted - boolean indicating if this partition should be restricted; set SC_TRUE if masters in this partition cannot create new partitions Grant - boolean indicating if this partition should always grant access and control to the parent Coherent - boolean indicating if this partition is coherent; set SC_TRUE if only this partition will contain both AP clusters and they will be coherent via the CCI The rest of the sections of the dump highlight all the resources, pads and memory regions enclosed in each partition. For more details on the definition of all the API calls please refer to the respective sc_fw_api document for each SoC variant. Resource partitioning - Run time configuration  The run time partitioning doesn't differ from the example provided on the porting kit, that example can be used as a base to create a partition at run time by calling the SCFW API.  Examples The following examples will show how to modify the default partition configuration on the evaluation boards, i.MX8QM MEK will be used as a reference. With BSP 4.14.98_2.3.0, the porting kit can be obtained from i.MX Software and Development Tools | NXP . Default configuration without partitioning First we will dump the default configuration without partition, e.g. without setting the ALT_CONFIG flag, most mkimage targets with a single image are configured this way, see the soc.mak and related files under scripts: soc.mak\iMX8QM - imx-mkimage - i.MX Mkimage Bootloader Tool  For details on how to create a bootable image see i.MX8 Boot process and creating a bootable image  We can see that the targets flash and flash_spl do not set any flags on the image, therefore no partition of the system will occur at boot time. flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍‍‍ We will build the SCFW with the Debug Monitor enabled in order to be able to dump the partitions: make qm R=B0 B=mek M=1‍‍‍‍ Now we copy the SCFW binary we just build (scfw_tcm.bin under build_mx8qm_b0) to the mkimage iMX8QM folder, along with the SECO FW, ATF (bl31.bin) and u-boot. On mkimage the flash target will be used to create a bootable image with the SCFW we just build: make SOC=iMX8QM flash‍‍‍‍‍ Flash the image to your sd card sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 sync‍‍‍‍‍‍‍‍ The MEK has two serial ports, the first one (usually ttyUSB0) is used by the A cores (u-boot/Linux in this case), the second one is used by one of the M4 cores OR the SCFW, in this case it will be used by the SCFW.  Unfortunately there aren't enough serial ports on the MEK board to allow a dedicated port for SCU, M4 cores and A cores, so in order to use the Debug Monitor on the MEK the SCFW has to take over the M4_0 UART terminal. On the SCFW Debug monitor terminal type "dump rm" this will dump all the partition information, the full log is attached to this document (imx8qm_mek_no_partition.txt). On this log it can be seen that 4 partitions are created: Partition 0 --> SCFW Partition 1 --> ATF Partition 2 --> SECO Partition 3 --> U-boot/Linux/M4 cores/Rest of the system The ATF partition is created at run time by the ATF to run in its secure state, no extra partition is created at boot time, if an image without ATF where to be used only three partitions would be seen: Partition 0 --> SCFW Partition 1 --> U-boot/Linux/M4 cores/Rest of the system Partition 2 --> SECO Default configuration with partitioning enabled Now we will create an image with the SC_BD_FLAGS_ALT_CONFIG flag set, so that partitioning occurs at boot time, for demonstration purpose we will use the same target previously used but we will modify it to set the ALT_CONFIG flag, so on mkimage modify the flash target as follows: On iMX8QM/soc.mak flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍ After the modification build the image again make clean make SOC=iMX8QM flash‍‍‍‍ On mkimage's output you should be able to see: FLAG: 0x00200000 Note how the same SCFW is used as in the previous example, same for ATF, SECO, U-boot the only required change in this case is to enable the ALT_CONFIG flag in the image. Flash the sd card with the new image sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Dumping again the partitioning on the Debug monitor shows how the system now created additional partitions for the M4 cores and a shared partition: Partition 0 --> SCFW Partition 1 --> ATF (Created at run time by the ARM Trusted Firmware) Partition 2 --> SECO Partition 3 --> M4_0 Partition 4 --> M4_1 Partition 5 --> Shared partition Partition 6 --> U-boot/Linux/rest of the system The full log is attached as well. Modifying default configuration Now we will modify the default SCFW configuration to move some resources/pads from the M4 partition to the A cores partition (u-boot/Linux). All FlexCAN resources and pads will be moved from the M4 partition to the A core partition. From sc_fw_api_qm_b0.pdf Resource List: From sc_fw_api_qm_b0.pdf Pad List: Not all resources are available on all variants, for details on what resources/pads are available on your device please refer to its respective api document. Go back to the SCFW porting kit and open platform/board/mx8qm_mek/board.c, go to the definition of board_system_config which is the function where partitioning occurs. The code first verifies if the alt_config flag is set, and if not it skips partitioning, so all partitioning happens within the following if statement: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) ‍‍‍‍‍‍‍‍‍‍‍ The following partitions and memory regions are declared within this if statement: sc_rm_pt_t pt_m4_0; sc_rm_pt_t pt_m4_1; sc_rm_mr_t mr_m4_0, mr_m4_1; sc_rm_pt_t pt_sh; sc_rm_mr_t mr_sh;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ pt_m4_0 is the partition for the M4_0 core, its memory region is declared as mr_m4_0. Likewise for the M4_1 pt_m4_1 and mr_m4_1 are the partitions and memory regions assigned to the M4. pt_sh and mr_sh are the shared partition and memory region. A shared partition is created but it can only have a shared memory region. Pads and resources CANNOT BE SHARED there is no mechanism to protect the pads and resources from contention, if access to a resource is required by multiple partitions a virtual resource needs to be created, in this way the partition that requires access asks the partition that owns the resource to configure/use the resource on its behalf. See the VIRT_I2C example on the Linux BSP. The partition that hosts all remaining resources is the pt_boot partition, this can be seen as the A cores partition, all resources and memory regions not assigned to the M4 partitions will be left on the pt_boot partition where the A cores are. The code is documented well and self-explanatory, for instance the following line marks all resources within the M4_0 subsystem to be moved to the M4_0 partition: /* Mark all M4_0 subsystem resources as movable */ BRD_ERR(rm_set_subsys_rsrc_movable(pt_boot, SC_R_M4_0_PID0, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_M40_I2C0_SCL, SC_P_M40_GPIO0_01, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The resource list in the sc_fw_api_qm_b0.pdf document shows what resources belong to the M4 subsystem: Next some other resources required by the M4 are assigned to its partition, such as MUs used to communicate with the other cores, timers and the IRQ steer resource. In this case we are interested on having the FlexCAN resources/pads on the A cores side, these resources/pads are being assigned to the M4_1 partition as can be seen on the previous partitions dumps and the following code: /* Move some resources not in the M4_1 subsystem */ BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_IRQSTR_M4_1, SC_R_IRQSTR_M4_1, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_UART_2, SC_R_UART_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_UART0_CTS_B, SC_P_UART0_RTS_B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_6B, SC_R_MU_6B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_7B, SC_R_MU_7B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_9B, SC_R_MU_9B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_GPT_3, SC_R_GPT_3, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_FSPI_0, SC_R_FSPI_0, SC_TRUE)); /* Move some pads not in the M4_1 subsystem */ BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_QSPI0A_DATA0, SC_P_COMP_CTL_GPIO_1V8_3V3_QSPI0, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Previous dump: *** Resources *********************************** Partition: 4 M4_1_PID0 UART_2 CAN_0 CAN_1 CAN_2 IRQSTR_M4_1 *** Pads **************************************** Partition: 4 M41_I2C0_SCL M41_I2C0_SDA M41_GPIO0_00 M41_GPIO0_01 UART0_RTS_B UART0_CTS_B FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX So we just need to remove the following lines from the board.c: BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ That way the resources/pads won't be marked to be moved to the M4_1 partition and they will be left on the pt_boot partition (A core partition). If a resource needs to be added to the M4 partition just add the calls to rm_set_resource_movable to assign it. Now we just need to rebuild the scfw and our image: make qm R=B0 B=mek M=1‍‍‍‍‍ Then on mkimage (with the flags set modification above): make SOC=iMX8QM flash‍‍‍‍ Flash the sd card with the new image: sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Now when the dump is done we can see that the FlexCAN resources and pads belong to the same partition as the A cores (partition 6). *** Resources *********************************** Partition: 6 FTM_1 CAN_0 CAN_1 CAN_2 DMA_1_CH0 *** Pads **************************************** Partition: 6 COMP_CTL_GPIO_1V8_3V3_GPIOLHT FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX COMP_CTL_GPIO_1V8_3V3_GPIOTHR The device tree would still need to be modified to configure the pads and FlexCAN resources. System Controller Firmware 101 
查看全文
First download and install imx31_ads_20071008-rel5b-ltib.iso. Download and extract u-boot-1.3.3.tar.bz2. Place toolchain on PATH: $ export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" Export the CROSS_COMPILE name to U-Boot $ export CROSS_COMPILE=arm-none-linux-gnueabi- Enter in the u-boot-1.3.3 directory. Create configuration to i.MX31ADS board: $ make mx31ads_config Compile U-Boot to selected board: $ make If compilation goes fine you will see the u-boot.bin on current directory.
查看全文
Recipes to include Amazon's Alexa Voice Services in your applications. Step 1 : Get iMX Yocto AVS setup environment Review the steps under Chapter 3 of the i.MX_Yocto_Project_User'sGuide.pdf on the L4.X LINUX_DOCS to prepare your host machine. Including at least the following essential Yocto packages $ sudo apt-get install gawk wget git-core diffstat unzip texinfo \   gcc-multilib build-essential chrpath socat libsdl1.2-dev u-boot-tools Install the i.MX NXP AVS repo Create/Move to a directory where you want to install the AVS yocto build enviroment. Let's call this as <yocto_dir> $ cd <yocto_dir> $ repo init -u https://source.codeaurora.org/external/imxsupport/meta-avs-demos -b master -m imx-alexa-sdk-4.9.11.xml Download the AVS BSP build environment: $ repo sync Step 2: Setup yocto for Alexa_SDK image with AVS-SETUP-DEMO script: Run the avs-setup-demo script as follows to setup your environment for the imx7d-pico board: $ MACHINE=imx7d-pico DISTRO=fsl-imx-x11 source avs-setup-demo.sh -b <build_sdk> Where <build_sdk> is the name you will give to your build folder. After acepting the EULA the script will prompt if you want to enable: a Sound Card selection The following Sound Cards are supported on the build: SGTL (In-board Audio Codec for PicoPi) 2-Mic Synaptics/Conexant 2-Mic TechNexion Voice Hat (with DSPConcepts SW) The script will prompt to select the soundcard you will be using: Which Sound Card are you going to use? Sigmatel .............................. 1 Synaptics/Conexant .................... 2 VoiceHat (for DSPConcepts SW) ......... 3 Type the number of your selection and press Enter... Install Alexa SDK Next option is to select if you want to pre-install the AVS SDK software on the image. Do you want to build/include the AVS_SDK package on this image(Y/N)? If you select YES, then your image will contain the AVS SDK ready to use (after authentication). Note this AVS_SDK will not have WakeWord detection support, but it can be added on runtime. If your selection was NO, then you can always manually fetch and build the AVS_SDK on runtime. All the packages dependencies will be already there, so only fetching the AVS_SDK source code and building it is required. Install WiFi support Te WiFi support is optional and requires to get from NXP an additional meta-picopi-wifi layer. Contact NXP to get this layer to be able to support WiFi on your image The image will prompt: Do you want to include WiFi support on this image(Y/N)? Select YES if you already have the complementary meta-avs-demos-wifi layer Finish avs-image configuration At the end you will see a text according with the configuration you select for your image build. Next is an example for a Preinstalled AVS_SDK with Synaptics Sound Card support and WiFi/BT not enabled for PicoPi board. ============================================================ AVS configuration is now ready at conf/local.conf - Sound Card = Synaptics - Alexa SDK 1.7 pre-installed - Wifi supported You are ready to bitbake your AVS demo image now: bitbake avs-image If you want to use QT5DisplayCards, use then: bitbake avs-image-qt5 ============================================================ Step 3: Build the AVS image Go to your <build_sdk> directory and start the build of the avs-image There are 2 options Regular Build: $ cd  <yocto_dir>/<build_sdk>   $ bitbake avs-image With QT5 support included: $ cd  <yocto_dir>/<build_sdk>   $ bitbake avs-image-qt5 The image with QT5 is useful if you want to add some GUI for example to render DisplayCards. Step 4 : Deploying the built images to SD/MMC card to boot on target board. After a build has succesfully completed, the created image resides at <build_sdk>/tmp/deploy/images/imx7d-pico/ In this directory, you will find imx7d-pico-avs--.sdcard image or imx7d-pico-avs-qt5--.sdcard, depending on the build you chose on Step3. To Flash the .sdcard image into the eMMC device of your PicoPi board follow the next steps: Download the bootbomb flasher Follow the instruction on Section 4. Board Reflashing of the Quick Start Guide for AVS kit to setup your board on flashing mode. Copy the built SDCARD file $ sudo dd if=imx7d-pico-avs.sdcard of=/dev/sd<partition> bs=1M && sync $ sync Properly eject the pico-imx7d board: $ sudo eject /dev/sd<partition> NXP Documentation Refer to the Quick Start Quide for AVS SDK to fully setup your PicoPi board with Synaptics 2Mic and PicoPi i.mx7D For a more comprehensive understanding of Yocto, its features and setup; more image build and deployment options and customization, please take a look at the i.MX_Yocto_Project_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document. For a more detailed description of the Linux BSP, u-boot use and configuration, please take a look at the i.MX_Linux_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document.
查看全文
A new version of the Pins Tool for i.MX Application Processors has been released and is available for download as desktop tool from Pins Tool for i.MX Application Processors|NXP. The pins Tool for i.MX Application Processors is used for pin routing configuration, validation and code generation, including pin functional/electrical properties, power rails, run-time configurations, with the following main features: Desktop application Muxing and pin configuration with consistency checking Multicore support ANSI-C initialization code Graphical processor package view Multiple configuration blocks/functions Easy-to-use device configuration Selection of Pins and Peripherals Package with IP blocks Routed pins with electrical characteristics Registers with configured and reset values Power Groups with assigned voltage levels Source code for C/C++ applications Documented and easy to understand source code CSV Report and Device Tree File Localized for English and Simplified Chinese Mostly Connected: On-Demand device data download Integrates with any compiler and IDE What's New Added Label support to give signals a name Added ‘Log’ and ‘Problems’ view to report conflicts between settings Added support for templates to store user configurations as starting point for new configurations Added ability to download and share data for devices, especially for off-network host machines i.MX header files are now automatically part of the device data Import of legacy Processor Expert .pe files Export of register defines Various bug fixes and documentation improvements The release notes of the desktop application are attached to this article. Import Processor Expert Files A new importer has been added to import legacy Processor Expert for i.MX files: Labels Signals can now have user defined labels: Templates, Kits, Boards and Processors When creating a new configuration, it offers Templates, Boards and Processors. Custom configurations can be stored as templates and then used for new configurations. Board Specific Functions With the provided board and kit configurations, there are now pre-configured initialization functions for major blocks on the board: Export Data To simplify downloading the device specific data for the desktop tool, the 'Export' function can be used to download and export the data. The data can be copied that way to another machine or all data for a set of devices can be loaded. Export Registers With the Export command the registers can be exported as text/source: This is used to store the register values: /*FUNCTION********************************************************************** * * Function Name : init_audmux_pins * Description   : Configures pin routing and optionally pin electrical features. * *END**************************************************************************/ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_DA_AMX_SELECT_INPUT_VALUE            0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_DA_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_TXCLK_AMX_SELECT_INPUT_VALUE         0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_TXCLK_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_TXFS_AMX_SELECT_INPUT_VALUE          0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_TXFS_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN02_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN02 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN03_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN03 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN04_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN04 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN15_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN15 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA16_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA16 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA18_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA18 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA19_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA19 */ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ We hope you will find this new release useful. Thanks for designing with NXP! 
查看全文
GTK+ GTK is a graphic library developed initially by Gimp (Gimp ToolKit). GTK was selected as default GUI to create the Gnome Desktop and currently it is used on many desktop environment (XFCE, LXDE, etc). When GTK was developed it was depending on X Server (X11) but currently it can run over DirectFB. In order to add GTK+ support on i.MX board you need first to choice DirectFB or X11 to be it's default graphic infrastructure. The following pages contain informations and instruction of how to compile and use them. If you want to compile GTK over DirectFB: All Boards DirectFB If you want to compile GTK over X11: All Boards X11 All Boards GTK Manually All Boards GTK Glade GTK Demo GTK2 package comes with "gtk-demo". It's a demo executable to demonstrate some GTK gadgets. In order to use it with DirectFB, compile the following packages using LTIB: [*] GTK2 [*] DirectFB [*]  configure for use with touchscreen [*]  DirectFB-examples "if you would like to test DirectFB" [*] Liberation fonts [*] Tslib After starting Linux on i.MX, load the following modules: mx# /etc/rc.d/init.d/gtk2 start gtk: creating gdk-pixbuf.loaders mx# /etc/rc.d/init.d/pango start pango: creating module list Execute gtk-demo: mx# /usr/bin/gtk-demo GTK Demo with X If you would like to test the gtk-demo application over X, start X first (tested on i.MX25 PDK): mx# Xfbdev -screen 480×640 -mouse tslib,,device=/dev/input/event1 & mx# export DISPLAY=:0.0 mx# /usr/bin/gtk-demo
查看全文
Changing the storage for U-boot environment variables   U-Boot on Freescale BSP has a compiling option that allows you to choose the storage for environment variables.   1 - Extract the u-boot source using LTIB: ./ltib -m prep -p u-boot   2 - The source will be extracted to <ltib path>/rpm/BUILD/u-boot-2009.08   3 - On u-Boot source locate the i.MXEVK config file, <ltib path>/rpm/BUILD/u-boot-2009.08/include/configs/mx51_bbg.h   4 - To change the storage of variables environment to SD card, on this file, comment out CONFIG_FSL_ENV_IN_SF and define CONFIG_FSL_ENV_IN_MMC:   //#define CONFIG_FSL_ENV_IN_SF   #define CONFIG_FSL_ENV_IN_MMC 5 - Adjust CONFIG_ENV_SECT_SIZE and CONFIG_ENV_OFFSET accordingly. Recall that sd card read block size is 512B.   For example:   #define CONFIG_ENV_SECT_SIZE (256 * 512)   #define CONFIG_ENV_SIZE CONFIG_ENV_SECT_SIZE   #if defined(CONFIG_FSL_ENV_IN_MMC)   #define CONFIG_ENV_IS_IN_MMC 1 #define CONFIG_ENV_OFFSET (1023 * 512)   6 - Save the file.   7 - Recompile u-boot: ./ltib -m scbuild -p u-boot   8 - Your new compiled u-boot image will be saved at: <ltib path>/rpm/BUILD/u-boot-2009.08/u-boot.bin
查看全文
Download ATK from Freescale Extract ATK: # unzip ATK_1_41_STD_installer.zip Get the wine-tricks script and install MFC-4.2 and VisualC++-6.0. ./winetricks  vcrun6sp6 Execute the default install process: # wine SETUP.EXE Edit the file /etc/udev/rules.d/50-udev-default.rules to set permission for everyone: KERNEL=="tty[A-Z]*|pppox*|ircomm*|noz*", GROUP="uucp", MODE="0666" Run ATK: # wine ADSToolkit_std.exe
查看全文
Recently I published this i.MX Dev Blog post about the Gateworks plugin gst-variable-rtsp-server support for i.MX 6. Now, you can check how to use it on i.MX 8 SoCs as well. 1. Preparing the image In order to use gst-variable-rtsp-server plugin, prepare your machine and distro: Add the following line to conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server gst-variable-rtsp-server" Download the attached patch and apply it by doing: $ cd <yocto_path>/sources/meta-fsl-bsp-release/ $ git am ~/Download/0001-Add-RTSP-support-for-i.MX-8-L4.14.78_ga1.0.0-or-olde.patch Note: This patch is not necessary for L4.14.98_ga2.0.0 BSP! Then, build the image with bitbake and deploy it to the SD card. 2. Video Test Source Example Server $ gst-variable-rtsp-server -p 9001 -u "videotestsrc ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client 2. Camera Example Server $ gst-variable-rtsp-server -p 9001 -u "v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client In order to use VLC or other application as the client, just enter the URL as shown in the image below:
查看全文
This is a workaround—this page needs to be updated to add instructions for multi-touch support. Based on Freescale BSP 11.05. The LVDS panel (MCIMX-LVDS1) has a serial multi-touch controller, eGalax. As a workaround to have it supported on directly on Qt, we can force the driver to behave as a single touch. To do this: 1 - Edit the file ltib/rpm/BUILD/linux-2.6.35.3/drivers/input/touchscreen/egalax_ts.c adding the following line: + #define FORCE_SINGLE_POINTER_SUPPORT 1 2 - Compile the kernel ./ltib -m scbuild -p kernel 3 - Copy the new kernel to Card/Memory and boot it. 4 - Start your Qt app: $ Xfbdev -screen 1024x768 -mouse tslib,,device=/dev/input/event0  & $ export DISPLAY=:0.0 $ ./yourQTapp Note: You can read the touch events with "evtest" $ evtest  /dev/input/event0 or tslib apps: $ export TSLIB_TSDEVICE=/dev/input/event0 $ ts_print
查看全文
Q: How to program i.MX6 eFUSE? A: what about using the mfg tool? In the end only the supplies, USB OTG and the boot mode pins need to be connected. The customers Idea was to have all devices (i.MX6 eFUSE, Flash, PFUZE, etc) pre- programmed before mounting on the board. I presented the flows we support (MFG Tool, Platform SDK) for eFUSE programming last Friday when I was at the customer. KITPF0100SKTEVBE Product Summary Page MfgTools is the most convenient way to burn eFuse. Or the customer can burn the fuse on their jig/socket board by the u-boot: How to Fuse in U-Boot U-Boot contains a tool, imxotp, which is used for fusing. U-Boot > imxotp imxotp - One-Time Programable sub-system Usage: imxotp imxotp read <index> - read fuse at 'index' imxotp blow [--force] <index> <value> - blow fuse at 'index' with hex value 'value' Tips: 'addr' to 'index': convert 'index' from 'address' index = (addr - otp_base) / 0x10 eg, addr is 0x021bc410, otp_base is 0x021bc400, the index = 1 '--force' must be present in order to blow the fuse. Command will abort if '--force' is missing. index = (addr - otp_base) / 0x10, where the addr is the address of the fuse you want to operate, the otp_base is the base address of the fuse block. 'value' should correspond to fuse settings according to the fuse map and desired fuse configuration. ---------------------------------- FIrst of all thanks for your reply. However both flow assumes the i.MX6 is already soldered on the board. Please note the specific request was if it is possible (and we can support a programming house) to pre program the efuses BEFORE they are soldered on the PCB thus on a standard programmer. Take an FLASH programmer as an example.
查看全文
In order to get Redboot running on i.MX35 PDK without a flashing procedure, a little modification in the binary file is needed. After that it can be loaded into RAM memory using the ATK tool. The Redboot Header To execute the binary Redboot file a header of 32 bytes long must be added: ddccbbaa0000000000000000hhggffee00000000000000000000000000000000 Where ddccbbaa is the 4-byte start address and hhggffee is the start address (all in Hexadecinal format) modified by the following procedure: value - 0x20 (or 32 decimal) + 0x08 (or 8 decimal) Note that in this header the values are placed from LSB to MSB bytes, so if the start address for MX35PDK is 0x87F00000 then the header should looks like: Start Address    --> 0x87F00000                                               --> 0000F087 Modified Address --> 0x87F00000 - 0x20 + 0x08 = 0x87EFFFE8 --> E8FFEF87 Header --> 0000F0870000000000000000E8FFEF8700000000000000000000000000000000 Now, this header must be appended to the beginning of the redboot.bin file.
查看全文
This tutorial has been done with an i.MX51 EVK. This example can be easily adapted to i.MX35 or i.MX53 that share the same GPU Core (Z160) and the same API (OpenVG 1.1). This tutorial show you how to do a simple image warp deformation with OpenVG 1.1.     Generation of Linux Image with 2D gpu support To support 2D/3D gpu, you need to select gpu driver in LTIB. In LTIB's "package list" select the following packages: [x] amd-gpu-bin-mx51 [x] libz160-bin Build your Linux Image and copy it to your SD card. Building OpenVG simple application Download the application (see attached archive) Untar/unbz2 the application source code. To build the simple OpenVG application, you need to adapt the Makerules file. First you have to indicate where your linux image has been generated withLTIB: ROOTFS = /home/fsl/LTIB_1_7/ltib/rootfs You also need to indicate the compiler path (usualy installed in /opt/freescale/usr/local/....): GNUTOOL_PATH=/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/ After that you have to copy gpu's driver headers files in the include folder of the project. You will find these header in /opt/freescale/pkgs/amd-gpu-bin-mx51-x.x.x.tar.gz archive: extract all the include folders/files in the include folder of the project. Now you can build the application:   fsl@fsl-laptop:~/SW/openVG_sample$ make /opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -mfloat-abi=softfp -mfpu=vfp -Wall -O3 -fsigned-char -D_LINUX -I/home/fsl/SW/openVG_sample/include -c warp.c -o warp.o In file included from warp.c:37: roselend_savoie_france_350x350.c:12391:66: warning: trigraph ??) ignored, use -trigraphs to enable roselend_savoie_france_350x350.c:12964:71: warning: trigraph ??/ ignored, use -trigraphs to enable roselend_savoie_france_350x350.c:14518:10: warning: trigraph ??- ignored, use -trigraphs to enable roselend_savoie_france_350x350.c:15118:67: warning: trigraph ??) ignored, use -trigraphs to enable roselend_savoie_france_350x350.c:15327:67: warning: trigraph ??' ignored, use -trigraphs to enable roselend_savoie_france_350x350.c:15795:62: warning: trigraph ??! ignored, use -trigraphs to enable /opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -I/home/fsl/SW/openVG_sample/include -lOpenVG -legl13 -Wl,--library-path=/home/fsl/LTIB_1_7/ltib/rootfs/usr/lib,-rpath-link=/home/fsl/LTIB_1_7/ltib/rootfs/usr/lib -o warp warp.o fsl@fsl-laptop:~/SW/openVG_sample$ Copy the application on your SD card Put the SD card in the i.MX51 and run the gpu drivers $ login:root $ modprobe gpu Run the application $ ./warp Modifying the image A simple way to modify the image, is to use The Gimp. When you want to save your image, choose "C source code format": Then choose the prefix name (here "roselend"): Click on "Save". The "C" file of your image is generated: /* GIMP RGBA C-Source image dump (roselend_savoie_france.c) */ static const struct {   guint        width;   guint        height;   guint        bytes_per_pixel; /* 3:RGB, 4:RGBA */   guint8       pixel_data[350 * 350 * 4 + 1]; } roselend = {   350, 350, 4,   "\265\303\357\376\264\304\357\376\262\304\357\376\260\304\356\376\260\303"   "\356\376\257\303\356\376\257\302\355\376\257\301\355\376\257\302\355\376"   "\257\302\355\377\256\302\356\376\256\302\357\376\256\302\356\377\255\302" "\357\376\254\302\360\376\253\302\357\376\254\302\355\376\255\302\357\376" ...
查看全文
The KTV Demo is a common user case for KTV OEM. In this charpter, we will see what it is and how to use it. HW Platform imx6qp-sabresd SW Platform 3.14.52_1.0.0-ga, fb backend Display Connection LVDS0 XGA 1024*768 RGB666                          - IPU1 DI0 HDMI Display1920*1080@60                              - IPU0 DI1 HDMI Display1920*1080@56 via sii902x            - IPU0 DI0 LVDS1 XGA 1024*768 RGB666                          - IPU1 DI1 User case The demo has following output: Display # UI Video Stream Output Resolution DISP0-LVDS0 3D Cube@60fps 1920x1080@24fps (overlay) XGA(1024x768,RGB666) DISP1-HDMI 3D Cube@60fps 720p@20fps (overlay) 1080P@60(1920x1080,RGB24) DISP2-SII902X 3D Cube@60fps N/A 1080P@56(1920x1080,RGB24) DISP3-LVDS1 N/A 720p@20fps XGA(1024x768,RGB666) The DISP0 and DISP1 has overlay framebufffer, so output UI to bottom framebuffer and output video stream to overlay framebuffer. Run Demo The customer can refer to following script: #!/bin/sh echo "KTV demo start!" # Set environment variables export FB_FRAMEBUFFER_0=/dev/fb0 export FB_FRAMEBUFFER_1=/dev/fb2 export FB_FRAMEBUFFER_2=/dev/fb4 export FB_FRAMEBUFFER_3=/dev/fb5 # Run cube on DISP0,DISP1, DISP3 echo 0 > /sys/class/graphics/fb0/blank ./cube display=0 & sleep 1 echo 0 > /sys/class/graphics/fb2/blank ./cube display=1 & sleep 1 echo 0 > /sys/class/graphics/fb4/blank ./cube display=2 & echo "Open DISP0(LVDS0)" gst-launch-1.0 playbin \   uri=file:///home/root/ktv_demo/1080p_24fps.mp4 \   video-sink="imxv4l2sink device=/dev/video17" & sleep 3 echo "Open DISP1(HDMI)" gst-launch-1.0 playbin \   uri=file:///home/root/ktv_demo/720p_20fps.mp4 \   video-sink="imxv4l2sink device=/dev/video19" & #sleep 3 echo "Open DISP3(LVDS1)" gst-launch-1.0 playbin \   uri=file:///home/root/ktv_demo/720p_20fps.mp4 \   video-sink="imxv4l2sink device=/dev/video21" & sleep 3 The demo image can be downloaded at: \\10.193.102.186\public_share\ZhengTao\KTV Demo​ VPU frequency The vpu can run at 352MHz or  266MHz. We run it at 352MHz in this demo. The customer can configure the VPU frequcency from Linux kernel Kconfig options. Performance Utilization: 33% Overall Bus Load: 71% For 1080p@24fps, the real fps can only up to 13.319fps. The GPU may influence VPU performance.
查看全文
Overview Measuring the power consumed an i.MX application processor can be a challenging undertaking. This document describes several boards designed to instrument i.MX application boards for current measurements. While this system does not offer many digits of accuracy, it can be used to quantify power consumed by application use cases as well as while in low power modes. The system can be used to instrument up to four power supply rails and measure current in two ranges. Range switching on the sensor boards is controlled via software running on the Kinetis K20 at the heard of the profiler board. Measured data is sent to a host computer over a virtual serial link over USB. Power for the profiler system is obtained from the USB connection although a external 5V supply may be used. Dual-Range Current Sensors INA250 + INA21x Sensor Circuit Description: The INA250 + INA21x Sensor board can measure two ranges using the INA250 and INA21x current sense amplifiers. The high range is measured with an INA250, which has an integrated 0.002 Ohm shunt, and is available in four output gains. The low range is measured with shunt R1 and the INA21x sense amp. The low range shunt is taken out of the circuit (by shorting it) with two paralleled, very low-Rds(on) FETs, Q1 and Q1. VCC_SENSE powers the two sense amplifiers. VCC_FET supplies the gate voltage on Q1 and Q2. The DMN1019 device has a Vgs max of 8V. The sources of both FETs are tied to the i.MX side of the current sense loop, so the gate voltage Q1 and Q2 see is VCC_FET-(rail voltage). The signal /LOW_EN controls the state of both Q1 and Q2. The sense amplifier outputs (HIGH_OUT1 and LOW_OUT1) and rail voltage (V_RAIL_MEASURE) are sent down the ribbon cable (X2) to the profiler board for measurement. When not used for a wire loop for a Hall-effect current probe, resistor R3 should be shorted with a solder bridge, a piece of wire, or a 0.001 Ohm resistor. Schematic: Board Layout: The two large vias by the current sense connection points are provided for use with a 0.1" header and jumper to short the low range shunt, allowing normal operation of the target board when the profiler is not powered. It should be noted a jumper will not be as effective for relatively large currents. BOM: Part   Device C1,C2  0.1uF 0805 Q1,Q2  DMN1019USN-13 SOT23 R1     2 1% 0805 (resize to change low range) R2     10k 0805 R3     Solder bridge/wire loop (see schematic) U1     INA250 TSSOP16 (choose gain, A3 [0.8V/A] or A4 [2.0V/A]) U2     INA21X SC70 (choose desired gain) X2     WM6769CT/0527460871 (bottom contacts) Dual INA21x Sensor Circuit Description: The Dual INA21x Sensor board can measure two ranges using two INA21x current sense amplifiers and two different shunts. The high range shunt (R1) is always in place. The low range shunt is taken out of the circuit (by shorting it) with two paralleled, very low-Rds(on) FETs, Q1 and Q1. VCC_SENSE powers the two sense amplifiers. VCC_FET supplies the gate voltage on Q1 and Q2. The DMN1019 device has a Vgs max of 8V. The sources of both FETs are tied to the i.MX side of the current sense loop, so the gate voltage Q1 and Q2 see is VCC_FET-(rail voltage). The signal /LOW_EN controls the state of both Q1 and Q2. The sense amplifier outputs (HIGH_OUT1 and LOW_OUT1) and rail voltage (V_RAIL_MEASURE) are sent down the ribbon cable (X2) to the profiler board for measurement. Schematic: Board Layout: The two large vias by the current sense connection points are provided for use with a 0.1" header and jumper to short the low range shunt, allowing normal operation of the target board when the profiler is not powered. It should be noted a jumper will not be as effective for relatively large currents. BOM: Part   Device C1,C2  0.1uF 0805 Q1,Q2  DMN1019USN-13 SOT23 R1     0.002 1% 0805 (resize to change high range) R2     0.05 1% 0805 (resize to change low range) R3     10k 0805 U1,U2  INA21X SC70 (choose desired gain) X2     WM6769CT/0527460871  (bottom contacts) Four-Channel Power Profiler Circuit Description: The Four-Channel Power Profiler board has at its heart a Kinetis K20 on a Teensy3.2 board. The ADCs of the K20 measure all the current sense amplifier's outputs, the voltage of each instrumented rail. There is provision for measuring temperature using up to three thermistors. GPIO provide control each sensor board's current range, and optionally, a hardware wake-up signal for the instrumented target board. Up to four dual-range sensor boards can be connected (either sensor board mentioned above). A micro-SD card socket is included for storing measured data (the SD card functionality has been tested but not implemented for use with measurements). Measured data is sent to the host computer over a virtual serial port using the Teensy's USB. Charge pump U1 boosts the 5V supply to 12V. The output is regulated down to 8V on VCC_FET via regulator U2. R2 and C5 provide filtering for the 3.3V supply from the Teensy that feeds the sensor boards through VCC_SENSE. FETs Q1 through Q4 provide voltage level translation which protect the Teensy's GPIO pins from the 8V that's placed on the gates of the shorting FETs on the sensor boards. Regulator IC2 provides power for the micro-SD socket, since the 3.3V regulator on the Teensy does not provide enough capacity. Since there are not "smarts" on the sensor boards, the Teensy has no way of knowing what kind of sensor board is connected or what shunt values and sense amplifier gains are in use. As currently implemented, current and voltage calculations are hard coded in the Teensy application code. Schematic: Board Layout: BOM: Part    Device C1,C2   0.22uF 0805 C3-C7   1uF 0805 C10,C12 1uF 0805 C11     0.1uF 0805 IC2     MCP1825ST-3302 SOT223 Q1-Q4   DMN1019USN SOT23 R2-R4   20k 1% 0805 R5-R8   10k 0805 R9      Ferrite bead 0805 S1-S4   WM6769CT/0527460871 (bottom contacts) U$1     101-00660-68-6-1-ND MICROSD U1      MAX662CPASO8 SO08 U2      78L08SMD SO08 Use mating Molex cables: 8in: 0150200087 or 10in: 0151660091 Using the Power Profiler Obtaining Sensor and Profiler Boards: Bare boards may be ordered directly from OSH Park using these links: INA250 + INA21x Sensor board (order with 2oz copper option selected) Dual INA21x Sensor board (order with 2oz copper option selected) Power Profiler board The sensor boards should be ordered with the 2oz copper option selected to reduce the trace resistance of the target board's current path. No special option is needed for the profiler board. Teensy3.2 boards may be ordered from OSH Park as well, and at a slightly lower price than the manufacturer (PJRC) sells them. Choosing Current Ranges: To choose the value of a shunt resistor, use the following equation: Rsh = Vfs / (Ifs * gain) where: Rsh is the shunt resistance Vfs is the full scale sense amplifier output voltage (3.3V here) Ifs is the full scale current to be measured gain is the gain of the sense amp to be used For example, to measure a 66mA full scale current with a sense amp of gain 1000, Rsh = 3.3V / (0.066A * 1000) = 0.050 Ohms. For sleep/leakage current, say 1mA full scale: Rsh = 3.3V / (0.001 * 1000) = 3.3 Ohms. The pads on both sensor boards for the shunt resistors have been laid out for 0805 SMT resistors. Precision resistors should be used, 1% or better. The highest power dissipation resistor available should be used to minimize resistance change from the shunt resistor heating up; 0805 resistors are typically available with 1/8, 1/4, 1/2 and 1 Watt dissipation. Building and Testing: These boards were designed to be assembled by hand in small quantities. The most difficult components to solder are the ribbon connectors and the SC70 packaged sense amplifiers. A fine tip soldering iron and a microscope are required. Solder wick is helpful for removing solder bridges from between pins (typically the ribbon connector and the sense amplifiers).  Early versions of the profiler board were assembled with header pins soldered to the Teensy and mating female recepticles soldered to the profiler board. Later versions (like in the example below) were assembled with male header pins between the Teensy and the profiler board.  To test the boards after assembly, check for the presence of 8V on the pull-up resistors R5-R8 when a USB cable is plugged into the Teensy. Program the Teensy with suitable application code. Connect the sensor boards to the profiler. Connect all the sensor boards together in series, positive of one to negative of the next and connect to a calibrated current source. (The image below shows an early prototype of the profiler with the sensor boards connected in series. Current is forced through them via the Kelvin contact clips.) Open a terminal window on the host computer. Force known currents and toggle the ranges of each sensor to verify that each sensor operates correctly in both ranges. To check that the profiler measures rail voltage correctly, disconnect the current source and apply the positive side of a voltage source to either side of the sensors still connected in series and connect the ground of the voltage source to a ground point on the profiler. The rail voltage measured by each sensor should match the supplied voltage (0 to 3.3V max). Accuracy/Calibration: After building in excess of 20 sensor boards and 6 profiler boards and checking their measurements against a Keysight B2902 SMU forcing known currents, the profiler system is fairly accurate. Measurements are good down to about 2% of any range's full scale; lower than that gets into the input offset range of the sense amplifier. Individual readings within 1% of that range's full scale when compared against forced current values. No calibration or tuning has been necessary. Measured values should only be considered good to at most 3 significant figures. Limitations: The maximum current through any sensor should be limited to a maximum of 4A. The current limit when using the low range needs to avoid exceeding the power dissipation of the low range shunt resistor. Particularly, the dissipation in the low range shunt resistor can cause resistance changes that would affect measurement accuracy. The voltage of any instrumented rail cannot be greater than 3.3V, the maximum input voltage of the K20's ADC inputs. Minimum resistance the sensor introduces is in high range is about 0.012 to 0.015 Ohms with a 0.002 Ohm shunt. At least 0.005 Ohms comes from the two shorting FETs on the sensor board. The rest comes from the traces on the board as well as the interconnect wires. The bottom line is: the sensor board has to be mounted as closely as possible to the current sense point on the target board. The maximum resistance the sensor introduces depends on the low range shunt. With a 0.020 Ohm low range shunt, the resistance is about 0.025 to 0.030 Ohms. With a 0.050 Ohm low range shunt, the resistance is about 0.065 to 0.075 Ohms. The sensor board needs to be rigidly mounted to prevent ripping up the current sense points on the target board. This can be a challenge when many rails are instrumented. Instrumenting Target Board: When instrumenting a target board, the on-board current sense resistor should be removed. The sensor board should be attached to the target board placed as close as possible to the sense resistor pads. Connection wires to the sensor board should be as short as possible to minimize series resistance. Great care should be taken to prevent movement of the sensor boards that could in turn lift the sense resistor pads off the target board. Foam double sticky tape should be used over clear areas of the target board to avoid dislodging components when the tape is removed. In the photos below, seven power supplies are instrumented on an interposer card. In this example, the sensor boards were affixed to perf board held in place by the headers. Because of the physical constraints of the target board and its power supply card, mounting the sensor boards directly to the interposer was not possible. Four sensors were mounted on one side and three on the other. Notches were cut in the perf board for the sensor's connection wires on the opposite side. Two profiler boards are required for simultaneous use. (Two were also required because the 0.1" headers and jumpers were not installed on the sensor boards to passively short the low-range shunts; all the sensor boards need to be powered to actively short the low-range shunts.)  The positive input of the sensor board (the center of the three connection points) goes to the regulator side of the current sense resistor. The negative input (either of the two outside connections) goes to the i.MX side of the sense resistor. [NOTE: In this example, the power profiler boards have not been fully populated: the thermistor-related components and the micro-SD card socket. The sensor boards were fully populated with the exception of the passive shorting jumper.] Here is another example of a board with six instrumented rails. The sensors in this case are mounted directly on the target board. In this example, the 12V rail is instrumented, which required modding to add a voltage divider to V_RAIL_LOWSIDE on that sensor board.  And here's yet another example of an instrumented i.MX6Q SDB (which still has wires on it from measuring it the old way...). Although it's difficult to see in this photo, all of the sensor boards have a jumper across the low range shunt which permits normal operation of the board without the profiler board attached to provide power to the shorting FETs. Profiler Application Code for Kinetis/Teensy: Below is sample application code for the Teensy for use with four INA250 + INA21x sensor boards populated with the INA250A3 (0.8V/A gain) for the high range and 0.05 Ohm shunts and INA212 (gain 1000). The current range of each channel can be independently changed. This code is also attached below as a file. Data is sent to the host computer over a USB virtual serial port. To reflash/update Teensy code, follow the instructions from PJRC. Download Windows virtual com port driver. /* MIT License (https://spdx.org/licenses/MIT.html) Copyright 2017 NXP Teensy Power Profiler v.2 (revised main board with individual Hi/Lo GPIO, fixed voltage levels, and on-board uSD card socket. Very basic code for the Teensy Power Profiler that sets up the ADCs and controls the GPIO with very basic, single-character serial commands... This version for all INA250A3 on high range, and 0.05Ohms+INA212 (1000 gain) on low range. */ // These constants won't change.  They're used to give names to the pins used: const int LoHiEn1 = 0; const int LoHiEn2 = 1; const int LoHiEn3 = 2; const int LoHiEn4 = 3; const int WakeUp = 5; const int Lo_1 = A0; const int Vrail_1 = A1; const int Hi_1 = A2; const int Lo_2 = A3; const int Vrail_2 = A4;  const int Hi_2 = A5; const int Lo_3 = A6; const int Vrail_3 = A7; const int Hi_3 = A8; const int Lo_4 = A9; const int Vrail_4 = A11; const int Hi_4 = A10; const int Therm1 = A14; #include <math.h> // thermistor temperature calculation stuff... int sensorValue = 0;        // value read from the pot float sensorValuef = 0.0; int B = 4334; // B25/100 value for thermistor NXRT15WF104FA1B040 // other stuff... int delayintvl = 20; int incomingByte; float vrefL = 3.3; float vrefH = 3.3; float vrefV = 3.3; bool one=true;   bool dispone=true; bool two=true;   bool disptwo=true; bool three=true; bool dispthree=true; bool four=true;  bool dispfour=true; int i,j; int num=100; float v1, v2, v3, v4, i1, i2, i3, i4; float il1, il2, il3, il4; void setup() {   // initialize serial communications at 115200 bps:   Serial.begin(115200);   // set analog resolution to 12 bits... (we want more than the 8 default bits...)   analogReadResolution(12);   // set up low/high range wakeup GPIO signals...   pinMode(LoHiEn1, OUTPUT); digitalWrite(LoHiEn1, HIGH);   pinMode(LoHiEn2, OUTPUT); digitalWrite(LoHiEn2, HIGH);   pinMode(LoHiEn3, OUTPUT); digitalWrite(LoHiEn3, HIGH);   pinMode(LoHiEn4, OUTPUT); digitalWrite(LoHiEn4, HIGH);   pinMode(WakeUp, OUTPUT); digitalWrite(WakeUp, HIGH); } void loop() {   // average voltages and currents...   v1=0; v2=0; v3=0; v4=0;   i1=0; i2=0; i3=0; i4=0;   il1=0; il2=0; il3=0; il4=0;   for (i=0; i<num; i++){     v1 = v1+ analogRead(Vrail_1)/4095.*vrefV;     i1 = i1+ analogRead(Hi_1)/4095.*vrefH/0.8*1000;     il1 = il1+ analogRead(Lo_1)/4095.*vrefH/0.05;     v2 = v2+ analogRead(Vrail_2)/4095.*vrefV;     i2 = i2+ analogRead(Hi_2)/4095.*vrefH/0.8*1000;     il2 = il2+ analogRead(Lo_2)/4095.*vrefH/0.05;     v3 = v3+ analogRead(Vrail_3)/4095.*vrefV;     i3 = i3+ analogRead(Hi_3)/4095.*vrefH/0.8*1000;     il3 = il3+ analogRead(Lo_3)/4095.*vrefH/0.05;     v4 = v4+ analogRead(Vrail_4)/4095.*vrefV;     i4 = i4+ analogRead(Hi_4)/4095.*vrefH/0.8*1000;     il4 = il4+ analogRead(Lo_4)/4095.*vrefH/0.05;   }   v1 = v1/num; v2 = v2/num; v3 = v3/num; v4 = v4/num;   i1 = i1/num; i2 = i2/num; i3 = i3/num; i4 = i4/num;   il1 = il1/num; il2 = il2/num; il3 = il3/num; il4 = il4/num;   // print the results to the serial monitor:   if (dispone) {   Serial.print(" RAIL1 (V)= ");  Serial.print(v1);  //Serial.print("\r\n");   if (!one) {Serial.print("    L1 (mA)= ");  Serial.print(il1, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H1 (mA)= ");  Serial.print(i1, 1); }   Serial.print("\r\n");   }   if (disptwo) {   Serial.print(" RAIL2 (V)= ");  Serial.print(v2);  //Serial.print("\r\n");   if (!two) {Serial.print("    L2 (mA)= ");  Serial.print(il2, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H2 (mA)= ");  Serial.print(i2, 1);}    Serial.print("\r\n");   }   if (dispthree) {   Serial.print(" RAIL3 (V)= ");  Serial.print(v3);  //Serial.print("\r\n");   if (!three) {Serial.print("    L3 (mA)= ");  Serial.print(il3, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H3 (mA)= ");  Serial.print(i3, 1);}    Serial.print("\r\n");   }   if (dispfour) {   Serial.print(" RAIL4 (V)= ");  Serial.print(v4);  //Serial.print("\r\n");   if (!four) {Serial.print("    L4 (mA)= ");  Serial.print(il4, 1);}  //Serial.print("\r\n");   if (1==1) {Serial.print("    H4 (mA)= ");  Serial.print(i4, 1);}    Serial.print("\r\n");   }   Serial.print("\r\n");   Serial.print("\r\n");   while (Serial.available()) {  // while there are characters in the buffer, grab them all...     incomingByte = Serial.read();  // will not be -1     Serial.print("Incoming byte: "); Serial.print(incomingByte);     // Serial.print("    Delay interval:"); Serial.print(delayintvl);  Serial.print("\r\n");     if (incomingByte == 'h' || incomingByte == 'H'){       Serial.print("\r\n\r\nHelp:\r\n\r\n");       Serial.print("  +/= delay interval +/- 10mS\r\n");       Serial.print("  /- delay interval 20msec/1sec\r\n");       Serial.print("  l/L all rails low/high range in unison\r\n");       Serial.print("  q/w/e/r toggle display of rail 1/2/3/4\r\n");       Serial.print("  1/2/3/4 high range of rail 1/2/3/4\r\n");       Serial.print("  !/@/#/$ low range of rail 1/2/3/4\r\n");       Serial.print("  h print this help...\r\n");       Serial.print("\r\n");       delay(2000);       }     // change delay interval...     if (incomingByte == '+') delayintvl = delayintvl + 10;     if (incomingByte == '=') delayintvl = delayintvl - 10;     if (incomingByte == '_') delayintvl = 20;     if (incomingByte == '-') delayintvl = 1000;     if (delayintvl<1) delayintvl = 20;     // toggle low/high range of all rails in unison...     if (incomingByte == 'L') {       digitalWrite(LoHiEn1, LOW);       digitalWrite(LoHiEn2, LOW);       digitalWrite(LoHiEn3, LOW);       digitalWrite(LoHiEn4, LOW);       one = true; two = true; three = true; four = true;     }     if (incomingByte == 'l') {       digitalWrite(LoHiEn1, HIGH);       digitalWrite(LoHiEn2, HIGH);       digitalWrite(LoHiEn3, HIGH);       digitalWrite(LoHiEn4, HIGH);       one = false; two = false; three = false; four = false;     }     // still unimplemented, but for wakeup of target board...     if (incomingByte == 'w') digitalWrite(WakeUp, LOW);     if (incomingByte == 'W') digitalWrite(WakeUp, HIGH);     // toggle display of rail...     if (incomingByte == 'q') dispone = !dispone;     if (incomingByte == 'w') disptwo = !disptwo;     if (incomingByte == 'e') dispthree = !dispthree;     if (incomingByte == 'r') dispfour = !dispfour;     // change between high/low range..     if (incomingByte == '1') { digitalWrite(LoHiEn1, LOW);  one = true; }     if (incomingByte == '!') { digitalWrite(LoHiEn1, HIGH); one = false;}     if (incomingByte == '2') { digitalWrite(LoHiEn2, LOW);  two = true;}     if (incomingByte == '@') { digitalWrite(LoHiEn2, HIGH); two = false;}     if (incomingByte == '3') { digitalWrite(LoHiEn3, LOW);  three = true;}     if (incomingByte == '#') { digitalWrite(LoHiEn3, HIGH); three = false;}     if (incomingByte == '4') { digitalWrite(LoHiEn4, LOW);  four = true;}     if (incomingByte == '$') { digitalWrite(LoHiEn4, HIGH); four = false;}     }   // wait delayintvl mS after the last reading:   delay(delayintvl); }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Future Work and Improvements Work on a "smart" sensor with a local Kinetis device (KL02Z or KL05Z) on the sensor board itself that has three separate sense amplifiers (one run/high current and two low) has begun. There are several advantages to having a microcontroller on each sensor board: All instrumented rails can be measured simultaneously The sampling rate can be increase over current generation's round robin Measured data is sent over I2C or UART, allowing arbitrary number of rails to be instrumented Each sensor board can provide all its shunt and gain info Sensor board can be used in isolation, i.e., without a master profiler board A GUI interface for the serial data output by the profiler would be really nice... Addditional Information For more information on current measurements in general, see this tutorial series: A Current Sensing Tutorial--Part 1: Fundamentals | EE Times  A Current Sensing Tutorial-Part II: Devices | EE Times  A Current Sensing Tutorial--Part III: Accuracy | EE Times  A Current Sensing Tutorial-Part IV: Layout and Troubleshooting Guidelines | EE Times 
查看全文
FAQ Question: I receive the following error message when compiling GTK2 using LTIB" Making all in demos make[2]: Entering directory `/home/ltib/rpm/BUILD/gtk+-2.14.3/demos' no --raw --build-list \         apple_red  ./apple-red.png \                 gnome_foot ./gnome-foot.png \         > test-inline-pixbufs.h \ || (rm -f test-inline-pixbufs.h && false) /bin/sh: no: command not found make[2]: *** [test-inline-pixbufs.h] Error 1 make[2]: Leaving directory `/home/ltib/rpm/BUILD/gtk+-2.14.3/demos' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/home/ltib/rpm/BUILD/gtk+-2.14.3' make: *** [all] Error 2 error: Bad exit status from /home/ltib/tmp/rpm-tmp.69212 (%build) Answer: Some packages on your host are missing, install the following packages: For deb distributions: sudo apt-get install libgtk2.0-dev or For Fedora distributions: sudo yum install gtk2-devel IMPORTANT: After install the package above, be sure to remove the installed GTK package on your ltib: On your LTIB directory: rm -rf rpm/BUILD/gtk+-2.14.3/ Question: I receive the following error message when booting through NFS: "Root-NFS: Server returned error -13 while mounting /tftpboot/ltib" Answer: Probabilty you remake your rootfs and forgot to restart NFS server. To solve this issue the command: "service nfs restart" Question: I am receiving "error: cannot open Name index using db3" when installing LTIB on new Ubuntu 9.10 Answer: Edit the file "ltib" and modify line 2428 to: $cf->{rpm}           = "rpm --force-debian"; Question: I receive the error message "Cannot create lockfile. Sorry." when I try to open minicom. Answer: This error message is generated because your user doesn't have permission to create a lock file in /var/lock. Change /var/lock permission: # chmod 777 /var/lock Question: I receive the error message "cannot open /dev/ttyS0: Permission denied" when I try to open minicom. Answer: This error message is generated because your user doesn't have permission to open /dev/ttyUSB0. Change /dev/ttyUSB0 permission: # chmod 777 /dev/ttyS0 Question: Compilation of e2fsprogs package or others packages with dependencies like Qtopia using LTIB in Debian derived linux system like Ubuntu makes an error like: make[1]: Leaving directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/tests/progs' making all in po make[1]: Entering directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/po' : --update cs.po e2fsprogs.pot rm -f cs.gmo && : -c --statistics -o cs.gmo cs.po mv: cannot stat `t-cs.gmo': No such file or directory make[1]: *** [cs.gmo] Error 1 make[1]: Leaving directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/po' make: *** [all-progs-recursive] Error 1 error: Bad exit status from /home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/tmp/rpm-tmp.66904 (%build) Answer: This error is caused by lack of the new version of package gettext. Install the gettext. For Ubuntu, the command line is: sudo apt-get install gettext But LTIB just recognize the existence of this package if it was installed before the LTIB installation. So, reinstall the LTIB. Question Compiling LTIB I got this error message: checking for glib-genmarshal... no configure: error: Could not find a glib-genmarshal in your PATH error: Bad exit status from /home/alan/ltib/tmp/rpm-tmp.48168 (%build) Answer: This error happen when you don't have glib2.0-dev in your system. To Ubuntu execute: sudo apt-get install libglib2.0-dev Question: How to convert an ELF binary to raw ARM binary? Answer: arm-none-linux-gnueabi-objcopy -O binary test.elf test.bin Question: How to inform to kernel to print all message on screen? Answer: echo 8 > /proc/sys/kernel/printk Question: How to disassembly an ARM binary? Answer: arm-none-linux-gnueabi-objdump -b binary -m arm -D test.bin Question: RedBoot returns invalid parameter: RedBoot> load -r -b 0x100000 zImage Using default protocol (TFTP) Can't load 'zImage': invalid parameter Answer: Verify if your tftp server is running correctly. If so, then verify if RedBoot network is configured correctly. You can use ping command to verify if communication with computer is working. Insert non-formatted text here Configure RedBoot to not use script and configure network: RedBoot> ^C RedBoot> fc Run script at boot: false Use BOOTP for network configuration: true. Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0xa1fe0000: . ... Erase from 0xa1fe0000-0xa2000000: . ... Program from 0x07ee0000-0x07f00000 at 0xa1fe0000: . RedBoot> Reset the board and then load the image Question: How can I test GPIO using a very simple test? Answer: You can find a very simple test here
查看全文