The i.MX 8QXP MEK does not allow the OV5640/LVDS/LCD usage only by changing the device tree anymore. It occurs because the M4 owns the i2c resources, so the A core must use rpmsg to enable virtual drivers.
Due to this, if the user changes the device tree, for instance, the *ov5640.dtb, the kernel won't boot, entering in the following loop:
[ 8.603353] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 8.610025] [drm] No driver support for vblank timestamp query. [ 8.616077] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_) [ 8.624978] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_op) [ 8.632526] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_op) [ 8.639833] imx-drm display-subsystem: failed to bind ldb@562210e0 (ops imx_7 [ 8.648428] imx-drm display-subsystem: master bind failed: -517
- u-boot.bin from internal u-boot provided by NXP.
- scfw_tcm.bin from SCFW porting kit
- bl31.bin from ARM Trusted Firmware
- SECO firmware container image
Disclaimer
The described procedures in this document target a GNU/Linux (Ubuntu 20.04 LTS) and it’s focused on iMX8QXP B0 + BSP L4.19.35_1.1.0.
Required packages
1 - Install ARM64 ToolChain:
1.1 - Install ARM64 GCC and G++ cross-compilers:
# apt install gcc-aarch64-linux-gnu g++-aarch64-linux-gnu2 - Install ARM32 GCC6 ToolChain:
2.1 - Download the ARM32 6 Toolchain and install it:
$ mkdir ~/gcc_toolchain
$ cp ~/Downloads/gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 ~/gcc_toolchain/
$ cd ~/gcc_toolchain/
$ tar xvjf gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2
# apt-get update
# apt-get install srecord
3 - Download MKimage
3.1 - Create a new directory desired to the packages:
$ mkdir flash_build
$ cp flash_build3.1 - Clone the MKimage:
$ git clone https://source.codeaurora.org/external/imx/imx-mkimage -b imx_4.19.35_1.1.0
4 - U-boot build
4.1 - Clone the U-boot
$ git clone https://source.codeaurora.org/external/imx/uboot-imx -b imx_v2019.04_4.19.35_1.1.0
$ cd uboot-imx4.2 - Export the ARM64 ToolChain:
$ export ARCH=arm64
$ export CROSS_COMPILE=/usr/bin/aarch64-linux-gnu-4.3 - Build it:
$ unset LDFLAGS
$ make -j4 imx8qxp_mek_defconfig
$ make4.4 - Copy the binary files to the MKimage/iMX8QX directory:
$ cp spl/u-boot-spl.bin ../imx-mkimage/iMX8QX/
$ cp u-boot-nodtb.bin ../imx-mkimage/iMX8QX/
$ cd ..
5 - ARM Trusted Firmware
5.1 - Clone the imx-atf:
$ git clone https://source.codeaurora.org/external/imx/imx-atf -b imx_4.19.35_1.1.0
$ cd imx-atf
5.2 - Build it:
$ unset LDFLAGS
$ make PLAT=imx8qx bl31
5.3 - Copy the binary files to the MKimage/iMX8QX directory:
$ cp build/imx8qx/release/bl31.bin ../imx-mkimage/iMX8QX/
$ cd ..
6 - SCFW
6.1 - Export the ARM32 GCC6 Toolchain:
$ export TOOLS=~/gcc_toolchain/
6.2 - Download the BSP L4.19.35_1.1.0_SCFW and copy it to the flash_build directory:
$ cp ~/Downloads/imx-scfw-porting-kit-1.2.7.1.tar.gz$ tar xvzf imx-scfw-porting-kit-1.2.7.1.tar.gz
$ cd packages/
$ chmod a+x imx-scfw-porting-kit-1.2.7.1.tar.gz
$ ./imx-scfw-porting-kit-1.2.7.1.bin
6.3 - Build it to i.MX 8QXP MEK B0:
$ cd imx-scfw-porting-kit-1.2.7.1/src/
$ tar xvzf scfw_export_mx8qx_b0.tar.gz
$ cd scfw_export_mx8qx_b0/
$ make qx R=B0 B=mek
6.4 - Copy the binary file to the MKimage/iMX8QX directory:
$ cp build_mx8qx_b0/scfw_tcm.bin ../../../../imx-mkimage/iMX8QX/
$ cp ../../../../
7 - SECO Firmware Container Image
7.1 - Download the SECO firmware binaries and copy it to the flash_build directory
$ cp ~/Downloads/firmware-imx-7.9.bin .
$ chmod a+x firmware-imx-7.9.bin
7.2 - Copy the binary files to the MKimage/iMX8QX directory:
$ cp firmware-imx-7.9/firmware/seco/mx8qx-ahab-container.img /imx-mkimage/iMX8QX/
8 - Build flash.bin
8.1 - In a new terminal, open the imx-mkimage directory:
$ cd flash_build/imx-mkimage
8.2 - Build it:
$ make SOC=iMX8QX flash
8.3 - Deploy it to the SDCard:
$ sudo dd if=iMX8QX/flash.bin of=/dev/sdX bs=1k seek=32 && sync
Now, you are able to use any non-rpmsg.dtb without kernel errors.
Author:
Pedro Jardim: pedro.jardim@nxp.com
I also see this same kernel error loop if I attempt to use xen (on the same i.MX 8QXP MEK board).
If you are doing your own Yocto build, I don't think you need to do all the steps indicated above.
In the tmp/deploy/images/imx8qxpmek/ directory you can find both:
I was able to get past the above error and boot dom0 by doing:
(on target)
dd if=imx-boot-imx8qxpmek-sd.bin-flash_spl bs=1k seek=32 of=/dev/mmcblk1
sync
reboot
(or on dev host)
dd if=imx-boot-imx8qxpmek-sd.bin-flash_spl bs=1k seek=32 of=/dev/sdX
sync
(re-mount sdcard)
(press return to enter u-boot)
The default dtb will not work now, however, I can then do:
=> run xenmmcboot
Thanks greglarson,
Hope more people can find this place and, thanks to you, we have more than one step-by-step to fix it.
Best Regards,
Marco