i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
Description       This doc explain how to enable the plugin boot on i.MX6Q/6DL and which used for change the pll2 clock and add the spread spectrum support to pass the EMI test. we still list the source codes of 3.0.35 and 4.1.15. to explain the dts/non-dts kernel support.       本文旨在说明如何在i.MX6Q/6DL上实现plugin启动,以支持展频和改变pll2的频率,其目的是为了通过 EMI测试。也附上了基于3.0.35和4.1.15的源代码,以供参考   Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 SabreSDP https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false          Version: MX6Q_PLUGIN_FC_SSC_V7-20200915_chn..pdf(chinese version)add baidou support MX6Q_PLUGIN_FC_SSC_V7-20170504_eng-chapter-imx6dl.doc+MX6Q_PLUGIN_FC_SSC_V3-20170309_eng.doc(english version)      
記事全体を表示
- In LTIB generate a rootfs.jffs2 with a erase block size of 16KB: ./ltib -c ---Target Image Generation   Options ---> ---Choose your root file system image type     Target image: (jffs2) --->   (16) jffs2 erase block size in KB - Copy the generated rootfs.jffs2 to /tftpboot : cp rootfs.jffs2 /tftpboot - Program 200732 Redboot binary. The 200732 Redboot is available in the 20071008 BSP iso. After mounting the iso go to the bootloaders directory, extract the redboot_200732.tar.gz file and use the pre-built mx31ads_redboot.bin inside the bin directory. - Boot from NAND and setup the network parameters fis init load -r -b 0x100000 /tftpboot/zImage fis create -l 0x200000 kernel load -r -b 0x100000 /tftpboot/rootfs.jffs2 fis create -l 0x1d000000 root - Pass the following kernel command line: fis load kernel exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock6 rootfstype=jffs2 init=linuxrc ip=none mtdparts=mx" You need to replace mtdblock6 with your rootfs partition, see below: mx31# cat /proc/mtd dev:    size  erasesize  name mtd0: 00040000 00020000 "RedBoot" mtd1: 001a0000 00020000 "kernel" mtd2: 0001f000 00008000 "FIS directory" mtd3: 00001000 00008000 "RedBoot config" mtd4: 00040000 00004000 "RedBoot" mtd5: 00200000 00004000 "kernel" mtd6: 01d00000 00004000 "root" mtd7: 00003000 00004000 "FIS directory" mtd8: 00001000 00004000 "RedBoot config" mx31#
記事全体を表示
How to connect i.MX51 and Ubuntu using USB cable: i.MX51 Side Plug in USB cable. getprop debug.adb.usb - Shows that debug.adb.usb are not set by default setprop persist.service.adb.enable 0 -> disable adb setprop debug.adb.usb 1 - adb will be through USB (for Ethernet, use setprop debug.adb.usb 0) setprop persist.service.adb.enable 1 -> enable adb Example: # getprop debug.adb.usb  # # # setprop persist.service.adb.enable 0 disabling adb # adb_release android_usb gadget: high speed config #1: android setprop debug.adb.usb 1 # # setprop persist.service.adb.enable 1 enabling adb # adb_open adb_release adb_open android_usb gadget: high speed config #1: android # Ubuntu Side On Ubuntu side, the most important tip is regarding permission. ADB server MUST be started with root right. Example of right mistake: $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb devices List of devices attached ????????????    no permissions  $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb shell error: insufficient permissions for device How to proceed to get permission: $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb kill-server $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb start-server * daemon not running. starting it now * * daemon started successfully * $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb devices List of devices attached 0123456789ABCDEF    device  $ sudo <AND_SDK_DIR>/android-sdk-linux_86/tools/adb shell ADB over Ethernet/Wi-Fi To make ADB work in i.MX51 using TCP: In your host machine: - Install Android SDK - export ADBHOST=BOARD_IP (setenv ADBHOST=xxx.xxx.xxx.xxx) - adb kill-server In your board: - make sure that ro.secure property is *not* set when the adbd daemon is launched, so edit the file default.prop - make sure that /dev/android_adb or /dev/android do *not* exist - stop adbd - start adbd Now you will be able to list the device: hamilton@saygon:/opt/work/androidsdk/android-sdk-linux_86/tools$ ./adb kill-server hamilton@saygon:/opt/work/androidsdk/android-sdk-linux_86/tools$ ./adb devices * daemon not running. starting it now * * daemon started successfully * List of devices attached emulator-5554   device
記事全体を表示
Creating an image A kernel image and a root file system can be created using LTIB, or compiling the kernel and setting the correct set of files. Create a root file system image from a set of files converting the files to a jffs2 file system. For this, install the package mtd-tools. In Ubuntu type apt-get install mtd-tools For making an root file system for flash, use the jffs2 file system like: mkfs.jffs2 -r rootfs -e 0x40000 -s 0x800 -n -o rootfs.jffs2 Where rootfs/ is the original set of file for the file system and rootfs.jffs2 is the output image file. Flashing Some connection errors can be avoided by Configuring RedBoot. The process below uses TFTP to copy the files between host and target. Copy the kernel image and the root file system image to the TFTP dir. For example, in All Boards LTIB dir, type sudo cp ./rootfs/boot/zImage /tftpboot sudo cp rootfs.jffs2 /tftpboot/ Where /tftpboot is the dir configured for TFTP The next steps are performed in a Minicom session, and happens on the board. Formatting the flash: fis init Flashing kernel Load kernel image (zImage) using the command below. Remember to modify the host IP address: load -r -b 0x100000 /tftpboot/zImage -h 10.29.244.99 The address 0x100000 is used as a temporary location Create the kernel fis create -f 0x100000 kernel Flashing root file system Load root file system image (rootfs.jffs2) to the temporary address. Remember to modify the host IP address: load -r -b 0x100000 /tftpboot/rootfs.jffs2 -h 10.29.244.99 Create the root file system in the right address (0x600000, for i.MX35 PDK) fis create -f 0x600000 root You can now load your kernel in the flash by typing: fis load kernel To know if the root file system written in the flash was correctly saved, execute the NFS file system and mount the flash. For load the the root file system by NFS, type: exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.244.99:/tftpboot/ltib init=/linuxrc ip=10.29.241.6:10.29.244.99" Wait the system go up, then mount the flash at /mnt. Reminde that the flash has a jffs2 file system. mount -t jffs2 /dev/mtdblock8 /mnt ls /mnt List the /mnt contents. The output must be the right file system. Modifying the initial script Reset the board and press CTRL-C. Type fc to modify the configurations and insert the initialization script. RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> fis load kernel >> exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock8 rw rootfstype=jffs2 ip=dhcp" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> Remember to save the configuration in the flash by typing y Reset the system. To certify that the board is loading the system from flash, remove the Ethernet cable.
記事全体を表示
In order to get USB cameras (web cams) working on i.MX 51 EVK board running Ubuntu, a few steps must be followed, and they are: Enable USB Camera's drivers on Kernel Test it using Gstreamer or another compatible software (as Cheese) Kernel Driver USB cameras (web cameras) on Linux work over GSPCA driver, to enable this driver you need to go to: ./ltib -c   [*] Configure the kernel     Device Drivers -->          Multimedia Devices -->               [*] Video Capture Adapters -->                    [*] V4L USB Devices -->                         <*> USB Video Class (UVC)                                      [*] UVC input events device support                         <*> GSPCA Based WebCams --> From this point, you need to choose your specific driver. If you don't know, you can select all of those options as a built-in module "<*>" that will work. GSPCA Drivers USB Camera Detection Connect your USB camera to the USB Host port on i.MX 51 EVK board and then type "dmesg", and also check if there is a video0 device using: ubuntu@ubuntu-desktop:~$ ls /dev/video0 /dev/video0 USB Camera Detection Gstreamer Command Line In order to test your USB camera using Gstreamer plugin, use the following command line to perform it: ubuntu@ubuntu-desktop:~$ gst-launch-0.10 v4l2src ! ffmpegcolorspace ! ximagesink and the results: Hi there !!! EOF !
記事全体を表示
The system controller timer service is responsible for: Watchdog - The watchdog resource is managed by the SCU. The SCFW exposes a "virtual" watchdog to all CPUs. This virtual watchdog is managed by software and it is based on a low power timer, the SCU also features a physical watchdog timer that is used to ensure the correct operation of the device. Some of the features implemented by this watchdog service are: - Update of the watchdog timeout - Start/stop of the watchdog - Refresh of the watchdog - Return of the watchdog status such as maximum watchdog timeout that can be set, watchdog timeout interval, and watchdog timeout interval remaining. Since this is usually handled by the OS itself no examples are provided in this guide. Real Time Clock (RTC) - The SCFW is responsible for providing access to the RTC. The features supported by the API are: - Set/get time - Setting alarms Only the partition that owns the SC_R_SYSTEM resource is allowed to set the time, alarms and calibration values for the RTC. All other partitions are able to read the RTC time.  Here is an example on setting the RTC from the M4 side: struct time_date{ uint16_t year; uint8_t month; uint8_t day; uint8_t hour; uint8_t min; uint8_t sec; } rtc_time; sc_err_t sc_status; sc_ipc_t ipc; /* Open IPC channel */ sc_status = sc_ipc_open(&ipc, SC_IPC_AP_CH0); if(sc_status != SC_ERR_NONE) printf("Error opening Inter Processor Channel\n"); /* Initialize RTC */ /* Hard code RTC time to January 5th 2018 at 12:00 hours */ sc_status = sc_timer_set_rtc_time(ipcHandle, 2018, 1, 5, 12, 0, 0); if(sc_status != SC_ERR_NONE) printf("Error initializing RTC. \r\n"); /* Return time */ sc_status = sc_timer_get_rtc_time(ipcHandle, &(rtc_time.year), &(rtc_time.month), &(rtc_time.day), &(rtc_time.hour), &(rtc_time.min), &(rtc_time.sec)); printf("Year: %d, Month: %d, Day: %d, Hour: %d, Minutes: %d, Seconds: %d. \r\n", rtc_time.year, rtc_time.month, rtc_time.day, rtc_time.hour, rtc_time.min, rtc_time.sec);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ https://community.nxp.com/docs/DOC-342654 
記事全体を表示
About this document This document describe the setup detail for Interfacing, Installing, programming (basis) and testing depth cameras with MX6QDL based boards using Ubuntu as rootfs on i.MX6 processors boards. Supported NXP HW boards: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board Depth sensors tested: Microsoft Kinect, ASUS Xtion. Prime Sense Carmine Software:   Gcc, Ubuntu 14.04v,  Openni, Python, ROS. 1. Depth Sensor Depth sensors are 3D vision sensors, mainly used in 3D vision application and motion gaming and robotics. For this paper we are going to use Kinect sensor and Asus Xtion connection to i.MX6 Processor boards and will get 3D images that are converted to finer points called point cloud. a) Microsoft Kinect Kinect mainly has an IR camera, IR projector and RGB camera, the IR and projector generates the 3D point cloud of the surroundings. It also has a mic array and motorized tilt for moving up and down. Kinect reveal that both the video and depth sensor cameras have a 640 x 480-pixel resolution and run at 30 FPS (frames per second). The RGB camera capture 2D color images, whereas the depth camera captures monochrome depth images. Kinect has a depth sensing range from 0.8mts to 3.5 mts b) Asus Xtion: Another alternative to kinect is Asus Xtion Pro.  Is a 3D sensor designed for motion sensing applications, this sensor is only for 3D sensing and it doesn’t have sound sensing. It has an infrared projector and a monochrome CMOS sensor to capture the infrared data. Xtion can be powered from USB itself and can calculate a sense depth from 0.8mts to 3.5 mts from the sensor. c) Prime Sense Carmine: The Prime Sense team (apple bought this company in November 2013) developed the Microsoft Kinect 3D vision, later develop their own 3D vision sensor Carmine. It also works with IR projector, RGB CMOS sensor and a depth CMOS sensor. All sensor are interfaced in System On Chip and is powered trough USB. Carmine capture 640x480 at 30 FPS and can sense from 0.35 mts to 3 mts. Developers can program the device using OpenNI and its wrapper libraries. All these sensors (Kinect, Carmine and Xtion) support the same software, so there is no special need for programming or general usage. Can be interface to i.MX processor using USB 2.0 interface and programmed using OPENNI and OPENCV. 2. Installation on Ubuntu For installation steps of Ubuntu trusty on iMX6 boards in your board, please follow up: https://community.freescale.com/docs/DOC-330147 Install the dependencies: $ sudo apt-get install -y g++ git python libusb-1.0-0-dev libudev-dev freeglut3-dev doxygen graphviz openjdk-6-jdk libxmu-dev libxi-dev Create a devel folder $  sudo mkdir –p devel $ cd devel Get OpenNI and the drivers $ git clone https://github.com/OpenNI/OpenNI.git -b unstable $ git clone git://github.com/ph4m/SensorKinect.git $ git clone https://github.com/PrimeSense/Sensor.git -b unstable Set the compile flags to build for the i.MX $ nano OpenNI/Platform/Linux/CreateRedist/Redist_OpenNi.py From: MAKE_ARGS += ' -j' + calc_jobs_number() To: MAKE_ARGS += ' –j2' Must also change the Arm compiler settings for this distribution $ nano OpenNI/Platform/Linux/Build/Common/Platform.Arm From: CFLAGS += -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp #-mcpu=cortex-a8 To: CFLAGS += -mtune=arm1176jzf-s -mfpu=vfp -mfloat-abi=hard Then run $ cd OpenNI/Platform/Linux/CreateRedist/ $ ./RedistMaker.Arm $ cd ../Redist/OpenNI-Bin-Dev-Linux-Arm-v1.5.x.x $ sudo ./install.sh Also edit the Sensor and SensorKinect makefile CFLAGS parameters $cd ~/devel/ $ nano Sensor/Platform/Linux/Build/Common/Platform.Arm $ nano  SensorKinect/Platform/Linux/Build/Common/Platform.Arm For both files From: CFLAGS += -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp #-mcpu=cortex-a8 To: CFLAGS += -mtune=arm1176jzf-s -mfpu=vfp -mfloat-abi=hard And the Sensor and SensorKinect redistribution scripts $ nano Sensor/Platform/Linux/CreateRedist/RedistMaker $ nano SensorKinect/Platform/Linux/CreateRedist/RedistMaker for both, change: make -j$(calc_jobs_number) -C ../Build to: make –j2 -C ../Build The create the redistributables Sensor (xtion and primesense) and Kinect (sensor Kinect) $ cd Sensor/Platform/Linux/CreateRedist/ $ ./RedistMaker Arm $ cd ~/devel/ $ cd SensorKinect/Platform/Linux/CreateRedist/ $ ./RedistMaker Arm $ cd ~/devel/ Then install PrimeSense and Kinect $ cd Sensor/Platform/Linux/Redist/Sensor-Bin-Linux-Arm-v5.1.x.x $ sudo ./install.sh $ cd ~/devel/SensorKinect/Platform/Linux/Redist/Sensor-Bin-Linux-Arm-v5.1.2.x $ sudo ./install.sh 3. Testing Installation: Connect the sensor power supply, Connect the Kinect to the NXP board USB port. (check with lsusb). For my board: Imx6q@imx6q:~/devel$ lsusb Bus 001 Device 022: ID 045e:02ae Microsoft Corp. Xbox NUI Camera Bus 001 Device 021: ID 045e:02ad Microsoft Corp. Xbox NUI Audio Bus 001 Device 019: ID 045e:02c2 Microsoft Corp. Kinect for Windows NUI Motor Now edit theglobal Kinect settings in Ubuntu $ sudo nano /usr/etc/primesense/GlobalDefaultsKinect.ini and uncomment this line UsbInterface=1 and changed it to 1 instead of 2 UsbInterface=2 $ sudo modprobe -r gspca_kinect And then blacklisting to avoid it to be auto-loaded on boot: $ sudo sh -c 'echo "blacklist gspca_kinect" > /etc/modprobe.d/blacklist-kinect.conf' Then: $ cd ~/devel/OpenNI/Platform/Linux/Bin/Arm-Release $ sudo ./Sample-NiSimpleRead You should get something like: Reading config from: '../../../../Data/SamplesConfig.xml' … Frame 40 Middle point is: 5050. FPS: 30.771788 Frame 41 Middle point is: 5050. FPS: 30.866173 Frame 42 Middle point is: 5050. FPS: 30.850958 Frame 43 Middle point is: 5050. FPS: 30.779032 Frame 44 Middle point is: 5050. FPS: 30.767746 Frame 45 Middle point is: 5050. FPS: 30.800463 Frame 46 Middle point is: 5050. FPS: 30.653118 Frame 47 Middle point is: 5050. FPS: 30.741659 Frame 98 Middle point is: 5050. FPS: 30.339321 LibFreenect: $ cd ~/devel/ $ git clone https://github.com/OpenKinect/libfreenect.git $ cd libfreenect $ mkdir build $ cd build $ cmake .. –L –DBUILD_AUDIO=ON $ make $ sudo make install Connect the kinect sensor power supply, connect the Kinect to the NXP board USB port and test any sample such as: $ sudo freenect-glview Note: If glview gives a shared library error: You need to refresh your ldconfig cache. The easiest way to do this is to create a file usr-local-libs.conf (or whatever name you wish) with the following lines: /usr/local/lib Switch to root account and move it to /etc/ld.so.conf.d/usr-local-libs.conf. Then update the ldconfig cache: $ su root $ mv ~/usr-local-libs.conf /etc/ld.so.conf.d/usr-local-libs.conf $ /sbin/ldconfig –v $ exit References: 1)      https://openkinect.org/ 2)      https://www.asus.com/us/3D-Sensor/Xtion_PRO_LIVE/ 3)      Learning Robotics using phyton by Lentin Joseph. http://www.amazon.com/Learning-Robotics-Python-Lentin-Joseph/dp/1783287535/ref=sr_1_1 4)      Computer Vision on i.MX Processors
記事全体を表示
  1) Remove all "network" parameter from .../ltib-dir/rootfs/rc.d/rc.conf 2) Add the path of rootfs in the /etc/exports file: /home/user/ltib"dir/rootfs/rootfs *(rw,sync,no_root_squash)   then execute :- #exportfs -ra 3) Execute NFS server /etc/init.d/nfs restart  
記事全体を表示
It is often not easy to use company network to flash application, due to network security (proxy, etc...). We will see in this tutorial, how to flash a Linux application in a SD card with ONLY a SD card reader and simple standard Linux commands. SD card Memory Map A Linux application is divided in 3 parts: the bootloader the Linux Kernel the Linux Rootfs We will flash sequentially these 3 parts Flashing U-boot With the SD card Reader, we will flash the yellow part. In the [...]/ltib/rootfs/boot/ folder $ sudo dd if=u-boot.bin of=/dev/sdb bs=512 skip=2 seek=2 && sudo sync Flashing Linux Kernel With the SD card reader, we will flash the green part. Keep in mind that 1MB=1048576B -> Kernel Offset. $ sudo dd if=uImage of=/dev/sdb bs=1048576 seek=1 && sudo sync Configure U-boot variables To launch the Kernel, you need to configure U-boot. Plug the serial cable on the EVK: 115kbps, 8 bits, 1 stop and no parity EVK switches must be configured as below: DS1 DS2 DS3 DS4 DS5 DS5 DS7 DS8 DS9 DS10 Boot from SD/MMC Card 0 0 0 0 0 0 1 1 0 0 Put the SD card in the EVK (bottom slot) and launch the app. In the hyperterminal type:   BBG U-Boot > printenv To print environnement variables Modify the bootcmd: BBG U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc read 0 ${loadaddr} 0x800 0x1800;bootm' "0x1800" is the size of the kernel. Must be bigger than uImage Kernel file (0x1800x512Byte=3MB) If you want to use the WVGA as display screen (kernel need to be configured with CLAA support), for LTIB1007 and after (before it was 'wvga' option): Script for LTIB1007's u-boot on i.MX51 EVK (copy/paste in the hyperterminal): setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bootm' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw  init=/init' setenv bootargs_base' setenv bootargs console=ttymxc0,115200 di1_primary console=tty1' setenv bootcmd 'run bootcmd_mmc' saveenv Script for LTIB1007's u-boot on i.MX53 EVK (copy/paste in the hyperterminal): setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bootm' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw  init=/init' setenv bootargs_base 'setenv bootargs console=ttymxc0,115200 di0_primary console=tty1' setenv bootcmd 'run bootcmd_mmc' saveenv You must have the following printenv: BBG U-Boot > printenv bootdelay=3 baudrate=115200 loadaddr=0x90800000 netdev=eth0 ethprime=FEC0 uboot_addr=0xa0000000 uboot=u-boot.bin kernel=uImage bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serveri p}:${nfsroot},v3,tcp bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; boot m load_uboot=tftpboot ${loadaddr} ${uboot} ethact=FEC0 bootargs=console=ttymxc0,115200 di1_primary root=/dev/mmcblk0p1 rootwait rw init =/init bootcmd_mmc=run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bo otm bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw init=/i nit bootargs_base=setenv bootargs console=ttymxc0,115200 di1_primary bootcmd=run bootcmd_mmc stdin=serial stdout=serial stderr=serial</br> Environment size: 748/131068 bytes BBG U-Boot > Create ext3 partition With the SD card reader, create an ext3 partition. You can use gparted, a graphical partition manager tool. Launch gparted: $ sudo gparted Create a new ext3 partition, with 20MB of offset: Copying Linux To copy rootfs folder generated by LTIB, type in the shell: $ sudo cp -r /[…]/ltib/rootfs/* /media/FreescaleSD/ && sudo sync Test application Put the SD in the slot slot and launch the application. Password is root.
記事全体を表示
Yoctoproject Framework Installing any Needed Package Using Yocto and i.MX Boards Testing Yocto for i.MX6 i.MX53 QSB - Quick Start Board i.MX6 Sabre Lite Board Build the image SDCard Image Yoctoproject Framework Yoctoproject is a framework for creating Linux distributions for embedded devices. Its layering mechanism makes it easy to add Linux to new target devices highly customized for a particular platform; it can include custom start-up scripts, software packages built with a high degree of optimization for a particular architecture, and different user interfaces from full Gnome desktop to a simple a serial console. Yocto has 2 basic layers: board support packages layer and core layer. In the BSP layer is where all the custom software and configuration tweaks for a particular platform are included, while the core layer provides the common software stack to provide from a simple command line interface to Sato desktop interface (Matchbox based and Gnome mobile software stack). A third layer could be added to provide additional user interfaces LXDE, XFCE, and more; YP is quite flexible&emdash;one of it major strengths. Installing any Needed Package Go to Yocto Project Quick Start and double check that you have all the necessary packages installed for your machine. For example, if building machine was an Ubuntu machine: $ sudo apt-get install gawk wget git-core diffstat unzip texinfo  build-essential chrpath libsdl1.2-dev xterm curl Using Yocto and i.MX Boards Please, go to project's README file in order to see the recommended instructions to download the source code. Testing Yocto for i.MX6 How to test Yocto for i.MX 6 i.MX53 QSB - Quick Start Board Edit conf/local.conf user config file and set imx53 Quick start board machine and enable parallel build features. MACHINE ?= "imx53qsb" BB_NUMBER_THREADS = "4" PARALLEL_MAKE = "-j 4" i.MX6 Sabre Lite Board Edit conf/local.conf user config file and set i.MX6 Sabrelite board machine and enable parallel build features MACHINE ?= "imx6qsabrelite" BB_NUMBER_THREADS = "4" PARALLEL_MAKE = "-j 4" if you've been facing problems to get yocto's images working on your i.MX Sabre Lite board, please take a look on this comment Re: The kernel sometins hang  in L3.0.35_4.0.0_130424 release Build the image some example of available image: image name description core-image-minimal A small image just capable of allowing a device to boot. core-image-base A console-only image that fully supports the target device hardware. core-image-sato Image with sato, a mobile environment and visual style for mobile devices.  The image supports X11 with a Sato theme, Pimlico applications and contains terminal, editor and file manager. fsl-image-test Builds contents core-image-base plus Freescale test applications and multimedia components. fsl-image-gui Builds contents of core-image-sato with Freescale test applications and multimedia with hardware accelerated X11 To build the image: $ bitbake <image_name> Build using Dash instead can bring some problems. You can check what your system uses typing: "ls -l /bin/sh". On Ubuntu you can change it using "dpkg-reconfigure bash". Some Ubuntu releases you must use "dpkg-reconfigure dash" and choose Bash Built images are located in cd tmp/deploy/images SDCard Image sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdb i.MX Yocto Project: Frequently Asked Questions
記事全体を表示
Ubuntu distro uses dash instead of bash as shell, then change it to bash: # cd /bin # sudo rm sh # sudo ln -s bash sh Install all necessary packages by typing: sudo apt-get install patch g++ rpm zlib1g-dev m4 bison libncurses5-dev libglib2.0-dev gettext \ build-essential tcl intltool libxml2-dev liborbit2-dev libx11-dev ccache flex uuid-dev liblzo2-dev If under Ubuntu 64bit, install ia32-libs package: sudo apt-get install ia32-libs If you will install Xorg in your ltib, you will need to install this package: sudo apt-get install x11proto-core-dev If you will install gtk+ in your ltib, you will need to install the following packages: sudo apt-get install libdbus-glib-1-dev libgtk2.0-dev libdbus-glib-1-dev Configure visudo file, as root using the command "/usr/sbin/visudo", and add the following line in the User privilege section: username ALL = NOPASSWD: /usr/bin/rpm, /opt/freescale/ltib/usr/bin/rpm Where username is your user name, the name you use to do logon in your system. Classic Error messages and solutions under Ubuntu Can't exec "mconf": No such file or directory at /home/tic/ltib/bin/Ltibutils.pm line 972. exec: mconf /home/tic/ltib/config/main.lkc: No such file or directory at /home/tic/ltib/bin/Ltibutils.pm line 972. traceback:   Ltibutils::system_nb:972   main::get_plat_dir:2947     main:548 Started: Tue Feb 16 18:01:38 2010 Ended:  Tue Feb 16 18:59:26 2010 Elapsed: 3468 seconds Build Failed Solution: edit the ltib script line 925:                   # install the new package           $cmd  = "$cf->{sudo} $cf->{rpm} ";           $cmd .= "--root $cf->{rpmroot} ";           $cmd .= "--dbpath $cf->{rpmdb} ";           $cmd .= "--prefix $cf->{rpmipfx} " if $cf->{rpmipfx};           $cmd .= "--ignorearch -ivh ";           $cmd .= "--force "  unless $cf->{conflicts} || $cf->{hostinst};           $cmd .= "--replacepkgs --replacefiles " if $cf->{hostinst};           $cmd .= "--nodeps " if $cf->{nodeps};           $cmd .= "--excludedocs "; +        $cmd .= "--force-debian " if $rpm =~ m/rpm-fs/ && `uname -a` =~ m/ubuntu/i;           $cmd .= "--define '_tmppath $cf->{tmppath}' ";           $cmd .= "$rpm"; error: cannot open Name index using db3 - No such file or directory (2) error: cannot open Name index using db3 - No such file or directory (2) sudo rpm --root / --dbpath /tmp/rpm-tic/rpmdb -e --allmatches --nodeps --define '_tmppath /home/tic/ltib/tmp' rpm-fs 2>/dev/null sudo rpm --root / --dbpath /tmp/rpm-tic/rpmdb --ignorearch -ivh --force --nodeps --excludedocs --define '_tmppath /home/tic/ltib/tmp'  /tmp/rpm-tic/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm rpm: please use alien to install rpm packages on Debian, if you are really sure use --force-debian switch. See README.Debian for more details. sudo /opt/freescale/ltib/usr/bin/rpm --root / --dbpath /opt/freescale/ltib/var/lib/rpm -Uv --justdb --notriggers --noscripts --nodeps  /tmp/rpm-tic/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm sudo: /opt/freescale/ltib/usr/bin/rpm: command not found mkdir: cannot create directory `/opt/freescale': Permission denied Cannot create the download directory:   /opt/freescale/pkgs Either change to a global directory you have write permissions to, or create it as root.  Please set the permissions to 777 traceback:   main::check_dirs:2469   main::host_checks:1426     main:542 Started: Wed Nov 25 01:56:53 2009 Ended:  Wed Nov 25 02:07:42 2009 Elapsed: 649 seconds Build Failed solution : sudo chmod 777 /opt make[1]: Entering directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8' Making all in tools make[2]: Entering directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8/tools' make[2]: *** No rule to make target `all'.  Stop. make[2]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8/tools' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8' make: *** [all] Error 2 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.U8vEdX (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.U8vEdX (%build) Build time for texinfo: 55 seconds Failed building texinfo Died at ./ltib line 1380. traceback:   main::build_host_rpms:1380   main::host_checks:1435     main:542 Started: Wed Nov 25 20:10:43 2009 Ended:  Wed Nov 25 20:31:42 2009 Elapsed: 1259 seconds These packages failed to build: texinfo Build Failed solution : install ccache package in host + cd /opt/freescale/ltib/usr/src/rpm/BUILD + cd lkc-1.4 + make -j1 conf mconf gcc -O0 -Wall -g -fPIC -c conf.c -o conf.o bison -l -b zconf -p zconf zconf.y flex -L -Pzconf zconf.l make: flex: Command not found make: *** [lex.zconf.c] Error 127 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.010CjL (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.010CjL (%build) Build time for lkc: 2 seconds Failed building lkc Died at ./ltib line 1380. traceback:   main::build_host_rpms:1380   main::host_checks:1435     main:542 Started: Thu Nov 26 00:33:46 2009 Ended:  Thu Nov 26 01:19:39 2009 Elapsed: 2753 seconds These packages failed to build: lkc Build Failed solution : install flex package in host Making all in po make[2]: Entering directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf/po' mv: cannot stat `t-ja.gmo': No such file or directory make[2]: *** [ja.gmo] Error 1 make[2]: *** Waiting for unfinished jobs.... mv: cannot stat `t-ru.gmo': No such file or directory make[2]: *** [ru.gmo] Error 1 make[2]: Leaving directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf/po' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf' make: *** [all-recursive] Error 1 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.93730 (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.93730 (%build) Build time for alsa-utils: 84 seconds Failed building alsa-utils f_buildrpms() returned an error, exiting traceback:   main:560 Started: Sat Nov 28 07:39:40 2009 Ended:  Sat Nov 28 08:17:18 2009 Elapsed: 2258 seconds These packages failed to build: alsa-utils Build Failed Exiting on error or interrupt solution : install package gettext and ja-trans checking for glib-genmarshal... no configure: error: Could not find a glib-genmarshal in your PATH error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.13030 (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.13030 (%build) Build time for glib2: 107 seconds Failed building glib2 f_buildrpms() returned an error, exiting traceback:   main:560 Started: Sat Dec  5 03:19:36 2009 Ended:  Sat Dec  5 03:29:46 2009 Elapsed: 610 seconds These packages failed to build: glib2 Build Failed Exiting on error or interrupt solution : install the package libglib2.0-dev
記事全体を表示
MAX resolution 1024 x 768 Factory Details:      Long name:    Freescale: Hardware (VPU) Encoder      Class:            Codec/Encoder/Video      Description:    Encodes raw YUV 4:2:0 data to MPEG4 SP, H.264 BP or H.263 (Annex J, K (RS=0 and ASO=0) and T) elementary data;Enco des raw YUV 4:2:0, 4:2:2 horizontal, 4:2:2 vertical or 4:0:0 data into MJPEG elementary data;      Author(s):       Multimedia Team <[email protected]>      Rank:             primary (256) Plugin Details:      Name:                    mfw_vpuencoder      Description:            Encodes Raw YUV Data to MPEG4 SP, H.264 BP or H.263 data. For H.263 P0, the source frame rate must be 3000 0/1001 fps      Filename:               /usr/lib/gstreamer-0.10/libmfw_gst_vpu_enc.so      Version:                  2.0.2      License:                  unknown      Source module:        gst-fsl-plugin      Binary package:       Gstreamer Multimedia Plugins (Freescale)      Origin URL:              http://www.freescale.com GObject   +----GstObject         +----GstElement               +----MfwGstVPU_Enc Pad Templates:    SINK template: 'sink'       Availability: Always       Capabilities:          video/x-raw-yuv                   format: I420                   width: [ 48, 8192 ]                   height: [ 32, 8192 ]        video/x-raw-yuv                   format: YV12                   width: [ 48, 8192 ]                   height: [ 32, 8192 ]        video/x-raw-yuv                   format: NV12                   width: [ 48, 8192 ]                   height: [ 32, 8192 ]        video/x-raw-yuv                   format: Y42B                   width: [ 48, 8192 ]                   height: [ 32, 8192 ]        video/x-raw-yuv                   format: Y444                   width: [ 48, 8192 ]                   height: [ 32, 8192 ]    SRC template: 'src'        Availability: Always        Capabilities:            video/mpeg                             width: [ 48, 1280 ]                           height: [ 32, 720 ]                   mpegversion: 4                 systemstream: false            video/x-h263                             width: [ 48, 1280 ]                            height: [ 32, 720 ]            video/x-h264                             width: [ 48, 1280 ]                            height: [ 32, 720 ]            image/jpeg                             width: [ 48, 8192 ]                            height: [ 32, 8192 ] Element Flags:    no flags set Element Implementation:    Has change_state() function: 0x2b01c98c    Has custom save_thyself() function: gst_element_save_thyself    Has custom restore_thyself() function: gst_element_restore_thyself Element has no clocking capabilities. Element has no indexing capabilities. Element has no URI handling capabilities. Pads:    SRC: 'src'      Implementation:      Pad Template: 'src'    SINK: 'sink'      Implementation:        Has chainfunc(): 0x2b01de28        Has custom eventfunc(): mfw_gst_vpuenc_sink_event        Has bufferallocfunc(): mfw_gst_vpuenc_buffer_alloc      Pad Template: 'sink' Element Properties:    name                : The name of the object                          flags: readable, writable                          String. Default: null Current: "mfwgstvpu_enc0"    codec-type          : selects the codec type for encoding                          flags: readable, writable                          Enum "MfwGstVpuEncCodecs" Default: 2, "std_avc" Current: 2, "std_avc"                             (0): std_mpeg4        - STD_MPEG4                             (1): std_h263           - STD_H263                             (2): std_avc             - STD_AVC                             (7): std_mjpg           - STD_MJPG    profile             : enable time profile of the vpu encoder plug-in                          flags: readable, writable                          Boolean. Default: false Current: false    width               : width of the frame to be encoded                          flags: readable, writable                          Unsigned Integer. Range: 48 - 8192 Default: 48 Current: 0    height              : height of the frame to be encoded                          flags: readable, writable                          Unsigned Integer. Range: 32 - 8192 Default: 32 Current: 0    bitrate             : target bitrate (in kbps) at which stream is to be encoded - 0 for VBR and others for CBR                          flags: readable, writable                          Unsigned Integer. Range: 0 - 32767 Default: 0 Current: 32768    gopsize             : gets the GOP size at which stream is to be encoded                          flags: readable, writable                          Unsigned Integer. Range: 0 - 32767 Default: 30 Current: 30    qp                  : gets the quantization parameter - range is 0-51 - will be ignored for CBR (bitrate!=0)                          flags: readable, writable                          Unsigned Integer. Range: 0 - 51 Default: 15 Current: 4294967295    max-qp              : Maximum quantization parameter for CBR - range is 0-51 for H264 and 1-31 for MPEG4 - lower value brings be tter video quality but higher frame sizes                          flags: readable, writable                          Unsigned Integer. Range: 0 - 51 Default: 51 Current: 4294967295    min-qp              : Minimum quantization parameter for CBR - range is 0-51 for H264 and 1-31 for MPEG4 - lower value brings be tter video quality but higher frame sizes                          flags: readable, writable                          Unsigned Integer. Range: 0 - 51 Default: 0 Current: 4294967295    gamma               : gamma value for CBR - tells VPU the speed on changing qp - lower will cause better video quality                          flags: readable, writable                          Unsigned Integer. Range: 0 - 32768 Default: 24576 Current: 24576    intrarefresh        : 0 - Intra MB refresh is not used. Otherwise - At least N MB's in every P-frame will be encoded as intra MB 's.                          flags: readable, writable                          Unsigned Integer. Range: 0 - 3600 Default: 0 Current: 0    h263profile0        : enable encoding of H.263 profile 0 when codec-type is set to std_h263                          flags: readable, writable                          Boolean. Default: false Current: false    loopback            : disables parallelization for performance - turn off if pipeline with decoder                          flags: readable, writable                          Boolean. Default: true Current: true    intra-qp            : Quantization parameter for I frame. When this value is -1, the quantization parameter for I frames is auto matically determined by the VPU. In MPEG4/H.263 mode, the range is 1.C31; in H.264 mode, the range is from 0.C51. This is ignored for STD_MJPG                          flags: readable, writable                          Unsigned Integer. Range: 0 - 51 Default: 15 Current: 4294967295    crop-left           : The left crop value of input frame to be encoded                          flags: readable, writable                          Unsigned Integer. Range: 0 - 4294967295 Default: 0 Current: 0    crop-top            : The top crop value of input frame to be encoded                          flags: readable, writable                          Unsigned Integer. Range: 0 - 4294967295 Default: 0 Current: 0    crop-right          : The right crop value of input frame to be encoded                          flags: readable, writable                          Unsigned Integer. Range: 0 - 4294967295 Default: 0 Current: 0    crop-bottom         : The bottom crop value of input frame to be encoded                          flags: readable, writable                          Unsigned Integer. Range: 0 - 4294967295 Default: 0 Current: 0    rotation-angle      : Pre-rotation angle - should be 0, 90, 180 or 270                          flags: readable, writable                          Unsigned Integer. Range: 0 - 270 Default: 0 Current: 0    mirror-direction    : mirror direction from source image to encoded image                          flags: readable, writable                          Enum "MfwGstVpuEncMirDir" Default: 0, "none                " Current: 0, "none                "                             (0): none                     - MIRDIR_NONE                             (1): vertical mirroring     - MIRDIR_VER                             (2): horizontal mirroring - MIRDIR_HOR                             (3): both directions       - MIRDIR_HOR_VER    h264-byte-stream    : Generate H.264 byte stream format of NALU. Take effect for H.264 stream only.                          flags: readable, writable                          Boolean. Default: true Current: true
記事全体を表示
Flashing Kernel and Root File System using RedBoot Creating an image A kernel image and a root file system can be created using All Boards LTIB or compiling the kernel and setting the correct set of files. Create a root file system image from a set of files converting the files to a jffs2 file system. For this, install the package mtd-tools. In Ubuntu type apt-get install mtd-tools For making an root file system for flash, use the jffs2 file system like: mkfs.jffs2 -r rootfs -e 0x20000 -s 0x800 –n -o rootfs.jffs2 Where rootfs/ is the original set of file for the file system and rootfs.jffs2 is the output image file. Flashing Some connections errors can be avoided by Configuring RedBoot. The process below uses TFTP to copy the files between host and target. See All Boards TFTP for detail in configurations. Copy the kernel image and the root file system image to the TFTP dir. For example, in LTIB dir, type sudo cp ./rootfs/boot/zImage /tftpboot sudo cp rootfs.jffs2 /tftpboot/ Where /tftpboot is the dir configured for TFTP The next steps are performed in a Minicom session, and happens on the board. Formatting the flash: Format the flash redboot> fis init -f Make a Bad Block Table redboot> nand scan Flashing kernel Load kernel image (zImage) using the command below. Remember to modify the host IP address: redboot> load -r -b 0x100000 /tftpboot/zImage -h 10.29.244.99 The address 0x100000 is used as a temporary location Create the kernel at the right address (0x100000, for IMX27PDK) redboot> fis create -f 0x100000 kernel Flashing root file system Load root file system image (rootfs.jffs2) to the temporary address. Remember to modify the host IP address: redboot> load -r -b 0x100000 /tftpboot/rootfs.jffs2 -h 10.29.244.99 Create the root file system in the right address (0x600000, for IMX27PDK) redboot> fis create -f 0x600000 root Testing This step can be omitted! You can now load your kernel in the flash by typing: fis load kernel To know if the root file system written in the flash was correctly saved, execute the NFS file system and mount the flash. For load the the root file system by NFS, type: exec -c "noinitrd console=ttymxc0,115200 root=nfs nfsroot=<server_ip>:<root_path_on_server> ip=dhcp" Wait the system go up, then mount the flash at /mnt. Reminde that the flash has a jffs2 file system. mount -t jffs2 /dev/mtdblock4 /mnt ls /mnt List the /mnt contents. The output must be the right file system. For testing root file system on NAND, type exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock4 rw rootfstype=jffs2 ip=dhcp" Modifying the initial script Reset the board and press CTRL-C. Type fc to modify the configurations and insert the initialization script. RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> fis load kernel >> exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock4 rw rootfstype=jffs2 ip=dhcp" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> Remember to save the configuration in the flash by typing y Reset the system. To certify that the board is loading the system from flash, remove the ethernet cable.
記事全体を表示
When to enable CONFIG_DEBUG_LL, choose the debug port and then CONFIG_EARLY_PRINTK on i.MX6, system will hang. There is no error information there as below, Uncompressing Linux... done, booting the kernel. Booting Linux on physical CPU 0x0 Initializing cgroup subsys cpu Initializing cgroup subsys cpuacct Linux version 4.1.15-00001-gd582989-dirty (jay@jay-ubuntu) (gcc version 4.9 20 150123 (prerelease) (GCC) ) #10 SMP PREEMPT Mon Jul 17 15:08:55 CST 2017 CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Freescale i.MX6 Quad SABRE Smart Device Board bootconsole [earlycon0] enabled cma: Reserved 448 MiB at 0x2a000000 Memory policy: Data cache writealloc -------------- hang -----------------‍‍‍‍‍‍‍‍‍‍‍‍‍ The patch fix it on android n7.1.1_1.0.0, kernel: 4.1.15.
記事全体を表示
Copy redboot binary to /tftpboot. In this case: redboot.bin Load binary file to i.MX RAM memory: RedBoot> load -v -r -b 0x100000 /tftpboot/redboot.bin Run the loaded image RedBoot> run 0x100000 Enable NOR, NAND or MMC flash media for Redboot. In this case, NAND is beeing used. RedBoot> factive nand Update RedBoot in the flash with currently running image RedBoot> romupdate
記事全体を表示
Building Freescale U-boot The U-boot provided by Freescale can be downloaded in the following link: http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/ 1 - Set the cross compiler environment variables. When using Yocto, it can be made by the following command (see more details at Yocto Trainning Yocto Training - HOME ) source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi 2 - Download the source code using "git clone": git clone  http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git 3 - Create a local branch based on some remote branch. In this example, lets use branch origin/imx_v2014.04_3.14.28_1.0.0_ga cd uboot-imx git checkout -b imx_v2014.04_3.14.28_1.0.0_ga_local origin/imx_v2014.04_3.14.28_1.0.0_ga 4 - Configure the project with the board you want to build. All board are listed on file boards.cfg. Check the exactly name of the choosen board and add "_config" to build the project. In this example, lets use mx6qsabresd make mx6qsabresd_config make 5 - The binary file will be generated and will be located at project root folder. The generated file in this case will be u-boot.imx 6 - More details can be found on files doc/README.imx6 doc/README.imximage README Building Mainline U-boot The U-boot project is developed and maintained by Denx Computer Systems can be downloaded in the following link: http://git.denx.de/?p=u-boot.git;a=summary 1 - Set the cross compiler environment variables. When using Yocto, it can be made by the following command (see more details at Yocto Trainning Yocto Training - HOME ) source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi 2 - Download the source code using "git clone": git clone http://git.denx.de/u-boot.git 3 - Check the name of the board on "configs" folder. In this case lets use mx6qsabresd_config make mx6qsabresd_config make 4 - The binary file will be generated and will be located at project root folder. The generated file in this case will be u-boot.imx
記事全体を表示
ATK (Advanced Toolkit) ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. It can be downloaded here. Using ATK This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board. Set red and cream switches as below: Switch SW5 -> 000000 Switch SW4 -> 1000000 {{Note|On SW5 and SW4, "1" means the keys selected towards the edge of the board.} 3 - Run ATK (1.6 or above) going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit Set the options: i.MX CPU -> i.MX35_TO2 Device memory -> DDR2; Custom Initial File -> (keep it unmarked) Communication Channel -> Serial Port (Usually COM1) If you are using TO1, Device Memory -> MDDR 4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO NAND Flash Erasing 1- Configure the Dip Switch of Personality Board: Switch 1 2 3 4 5 6 7 8 SW1 OFF OFF OFF OFF N/A N/A N/A N/A SW2 ON OFF OFF ON ON OFF OFF OFF 2- Choose NAND model K9LAG08U8M 3- Continue the steps Remember to select the checkbutton BBT (Back Block Table)
記事全体を表示
Yocto Project versions and names Preparing host environment For virtual machine (VirtualBox): Download the source code from NXP Code Aurora Yocto Project versions and names See here the list of all yocto version names: Releases - Yocto Project  The current stable release is Zeus Preparing host environment For virtual machine (VirtualBox): Please set memory size minimal to 1GB and disk size to 32GB. (24Feb2014 Ubuntu 12.04LTS)   First, make sure your host PC has the required packages to run Yocto The essential packages you need for a supported Ubuntu distribution are shown in the following command: $ sudo apt-get build-dep qemu $ sudo apt-get remove oss4-dev $ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \   build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \   xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \   xterm‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ For other Linux distribution or newer Yocto Project release see here the updated list. Download the source code from community Install the repo $ sudo apt-get install repo‍‍‍‍ Download the BSP source: $ mkdir fsl-community-bsp $ cd fsl-community-bsp $ repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b zeus $ repo sync‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Download the source code from NXP Code Aurora See here the list of all BSP releases from NXP: imx-manifest - i.MX Release Manifest  Currently, the latest NXP release how to is here: README - imx-manifest - i.MX Release Manifest  To understand the difference between the 2 source code (community X NXP BSP) see here Go to https://community.nxp.com/docs/DOC-94849  Go to Task #2
記事全体を表示
Booting Linux Directly from SD/MMC Card     You can create a self-bootable SD or MMC card with Linux.     This tutorial describes how to create a complete Linux system (bootloader + Linux kernel + root file system) that boots from SD/MMC card.     This is very useful for people willing to demonstrate several Linux images that can be self-contained in SD/MMC cards. Flashing RedBoot on MMC using ATK     To boot Linux from a SD card, the first thing to do is to program the bootloader to the card. For this, click on the link below:     I.MX35 PDK Board Flashing SDCard Flashing RedBoot on MMC using DD     You can also use dd on any linux system to load redboot:   $ sudo dd if=./Desktop/mx35_3stack_redboot_mmc.bin of=/dev/sdd bs=512 skip=2 seek=2 Configuring Kernel to Boot From SD/MMC     Creating a Linux bootable MMC/SD Card.     Execute LTIB:   $ ./ltib -c     Choose configure the kernel:   [*] Configure the kernel     Change image generation to NFS:     Target Image Generation     Options --->     (X) NFS only     Compile Linux kernel with built-in support to MMC/SD and ext3:     Follow that sequence:     Device Drivers --->     <*> MMC/SD card support --->     <*> UniFi SDIO glue for Freescale MMC/SDIO     <*> Freescale i.MX Secure Digital Host Controller Interface support       File systems --->     <*> Ext3 journalling file system support     After the compilation copy the file ~/ltib/rootfs/boot/zImage to tftpboot directory:   $ cp ~/ltib/rootfs/boot/zImage /tftpboot Creating RedBoot Kernel Partition     Create RedBoot partitions and copy Linux kernel to it:     Turn MMC active:   RedBoot> factive MMC     Initialize flash partitions:   RedBoot> fis init       RedBoot> fis list     ... Read from 0x07ee0000-0x07eff000 at 0x00060000: .     Name FLASH addr Mem addr Length Entry point     RedBoot 0x00000000 0x00000000 0x00040000 0x00000000     FIS directory 0x00060000 0x00060000 0x0001F000 0x00000000     RedBoot config 0x0007F000 0x0007F000 0x00001000 0x00000000     Load kernel to RAM:   RedBoot> load -r -b 0x100000 /tftpboot/zImage     Using default protocol (TFTP)     Raw file loaded 0x00100000-0x002c31b7, assumed entry at 0x00100000     Create a kernel partition with content of kernel image loaded to RAM:       RedBoot> fis create -f 0x200000 kernel         RedBoot> fis list     ... Read from 0x07ee0000-0x07eff000 at 0x00060000: .     Name FLASH addr Mem addr Length Entry point     RedBoot 0x00000000 0x00000000 0x00040000 0x00000000     FIS directory 0x00060000 0x00060000 0x0001F000 0x00000000     RedBoot config 0x0007F000 0x0007F000 0x00001000 0x00000000     kernel 0x00200000 0x00100000 0x001E0000 0x00100000     If you reset your board you need to see:   Booting from [SD card, CSD Version 1.0]     If instead you see this message:   Booting from [unknown version card ]     This means your card is not support, please replace it with other card. Creating the Root File System     After storing the kernel image in the SD card, remove the card from the target board and insert it in your computer (running Linux).     In this example, Linux detected the SD card as /dev/sdb.     Now we need to create two partitions. The first partition will not be used, this is just reserved to RedBoot and kernel. The second partition will be used to store Linux Root File System.   # fdisk /dev/sdb     Device contains neither a valid DOS partition table, nor Sun, SGI or OSF disklabel     Building a new DOS disklabel with disk identifier 0x526c22da.     Changes will remain in memory only, until you decide to write them.     After that, of course, the previous content won't be recoverable.         Warning: invalid flag 0x0000 of partition table 4 will be corrected by w(rite)         Command (m for help): p         Disk /dev/sdb: 1023 MB, 1023934464 bytes     32 heads, 62 sectors/track, 1008 cylinders     Units = cylinders of 1984 * 512 = 1015808 bytes     Disk identifier: 0x526c22da           Device Boot Start End Blocks Id System     Create the first partition with 8 MB; it already contains RedBoot and the kernel, as we stored previously:             Command (m for help): n     Command action       e extended       p primary partition (1-4)     p     Partition number (1-4): 1     First cylinder (1-1008, default 1):     Using default value 1     Last cylinder, +cylinders or +size{K,M,G} (1-1008, default 1008): +8M     Now, create the second partition using all remaining space on SD card:       Command (m for help): n     Command action       e extended       p primary partition (1-4)     p     Partition number (1-4): 2     First cylinder (10-1008, default 10):     Using default value 10     Last cylinder, +cylinders or +size{K,M,G} (10-1008, default 1008):     Using default value 1008         Command (m for help): p         Disk /dev/sdb: 1023 MB, 1023934464 bytes     32 heads, 62 sectors/track, 1008 cylinders     Units = cylinders of 1984 * 512 = 1015808 bytes     Disk identifier: 0x526c22da     Device Boot Start End Blocks Id System     /dev/sdb1 1 9 8897 83 Linux     /dev/sdb2 10 1008 991008 83 Linux         Command (m for help): w   Now format the second partition as EXT3: # mkfs.ext3 /dev/sdb2   Remove the SD card from your computer and insert again. Probably your Linux distribution will dectect it and will mount automatically.   On Ubuntu 8.10 it was mounted on /dev/media:   # mount   ...   /dev/sdb2 on /media/disk type ext3 (rw,nosuid,nodev,uhelper=hal) If your Linux didn't mount it, then you can mount it manually:   # mkdir -p /media/disk   # mount /dev/sdb2 -t ext3 /media/disk   Enter in your LTIB directory and copy the rootfs content to SD card:   # cd /home/alan/ltib-imx35/rootfs/   # cp -a * /media/disk/   Verify if it was copied correctly:   # ls -l /media/disk/   total 80   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 bin   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 boot   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 dev   drwxr-xr-x 6 root root 4096 2009-03-12 14:41 etc   drwxr-xr-x 3 root root 4096 2009-03-12 09:53 home   drwxr-xr-x 4 root root 4096 2009-03-12 09:55 lib   lrwxrwxrwx 1 root root 11 2009-03-12 14:47 linuxrc -> bin/busybox   drwx------ 2 root root 16384 2009-03-12 14:37 lost+found   drwxr-xr-x 7 root root 4096 2009-03-12 09:53 mnt   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 opt   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 proc   drwxr-xr-x 2 root root 4096 2009-03-12 10:10 root   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 sbin   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 sys   drwxrwxrwt 3 root root 4096 2009-03-12 09:53 tmp   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 unit_tests   drwxr-xr-x 9 root root 4096 2009-03-12 09:55 usr   drwxr-xr-x 11 root root 4096 2009-03-12 09:55 var   root@urubu:~/ltib-imx25/rootfs#     Now umount the SD card:   # umount /media/disk Configuring RedBoot to Load Kernel and Rootfs from SD/MMC Card     Remove the SD card from your computer and place again in the board.     Configure RedBoot to load the kernel from SD/MMC card and set up the kernel command parameter "root" to load the root file system from second SD/MMC card partition (/dev/mmcblk0p2)     RedBoot> fc     Run script at boot: true     Boot script:     Enter script, terminate with empty line     >> fis load kernel     >> exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/mmcblk0p2 init=/linuxrc ip=none"     >>     Boot script timeout (1000ms resolution): 1     Use BOOTP for network configuration: false     Gateway IP address: 10.29.244.254     Local IP address: 10.29.244.135     Local IP address mask: 255.255.0.0     Default server IP address: 10.29.240.182     Board specifics: 0     Console baud rate: 115200     Set eth0 network hardware address [MAC]: false     Set FEC network hardware address [MAC]: false     GDB connection port: 9000     Force console for special debug messages: false     Network debug at boot time: false     Default network device: lan92xx_eth0     Update RedBoot non-volatile configuration - continue (y/n)? y     ... Read from 0x07ee0000-0x07eff000 at 0x00060000: .     ... Erase from 0x00060000-0x00080000: .     ... Program from 0x07ee0000-0x07f00000 at 0x00060000: .       Now just reset the board and it will boot directly from SD/MMC card.
記事全体を表示
About this document This document describe the setup detail for Robot Operating systems on  ubuntu 14.04 running on MX6QDL based boards. 1. Software & Hardware requirements Supported NXP HW boards: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board i.MX 6SoloX SABRE-SD Board i.MX 6SoloX SABRE-AI Board i.MX 7D Sabre Board Software:  Gcc toolchain, Ubuntu 14.04v installed on your board. 2. Installation For install ROS on iMX boards you need to have Ubuntu 14.04 rootfs installed in your board, for installation steps please follow up: https://community.freescale.com/docs/DOC-330147 Run your rootfs target and Configure your Ubuntu repositories to allow "restricted," "universe," and "multiverse.  $sudo nano /etc/apt/sources.list Your file should then look like this: deb http://ports.ubuntu.com/ubuntu-ports/ trusty main universe multiverse restricted deb-src http://ports.ubuntu.com/ubuntu-ports/ trusty main universe multiverse restricted deb http://ports.ubuntu.com/ubuntu-ports/ trusty-updates main universe multiverse restricted Make your installation up to date: $ sudo apt-get update $ sudo apt-get upgrade Set your locale: $ sudo update-locale LANG=C LANGUAGE=C LC_ALL=C LC_MESSAGES=POSIX Add ROS ARM repos & Key $ sudo sh -c 'echo "deb http://packages.ros.org/ros/ubuntu $(lsb_release -sc) main" > /etc/apt/sources.list.d/ros-latest.list' $ sudo apt-key adv --keyserver hkp://pool.sks-keyservers.net --recv-key 0xB01FA116 $ sudo apt-get update There are many different libraries and tools in ROS - not all compile fully on ARM. In this case we are going to install the ROS Base, however any other packages can be installed individually ROS-Base: (Bare Bones) ROS package, build, and communication libraries. No GUI tools. $ sudo apt-get install python-rosdep python-wstool build-essential cmake xserver-xorg-dev-lts-utopic mesa-common-dev-lts-utopic \ libxatracker-dev-lts-utopic libopenvg1-mesa-dev-lts-utopic libgles2-mesa-dev-lts-utopic libgles1-mesa-dev-lts-utopic\ libgl1-mesa-dev-lts-utopic libgbm-dev-lts-utopic libegl1-mesa-dev-lts-utopic Alternatively, try installing just this to fix dependency issues, and then install ROS base (includes ROS package, build, and communication libraries. No GUI tools.😞 $ sudo apt-get install libgl1-mesa-dev-lts-utopic $ sudo apt-get install ros-indigo-ros-base Before you can use ROS, you will need to initialize rosdep. It enables you to easily install system dependencies for source you want to compile and is required to run some core components in ROS. $ sudo rosdep init $ rosdep update Install rosinstall: $ sudo apt-get install python-rosinstall Verifying OS name. If you installed the Linaro ALIP rootfs, make sure your OS name defined at /etc/lsb-release is as the following. Since ros does not recognize Linaro as an OS, this is necessary. $ lsb_release -a You should get: No LSB modules are available. Distributor ID: Ubuntu Description:    Ubuntu 14.04.4 LTS Release:        14.04 Codename:       trusty In any case you get a different output, the following is for Ubuntu 14.04, trusty. Modify the release number and name as per your target. DISTRIB_ID=Ubuntu DISTRIB_RELEASE=14.04 DISTRIB_CODENAME=trusty DISTRIB_DESCRIPTION="Ubuntu 14.04" 3. Testing The Installation Run ROS $ roscore You should get: ... logging to /root/.ros/log/1c07caa4-1dd3-11b2-b860-00049f0399fe/roslaunch- imx6q-2707.log Checking log directory for disk usage. This may take awhile. Press Ctrl-C to interrupt Done checking log file disk usage. Usage is <1GB. Started roslaunch server http://i.Mx6q:37547/ ros_comm version 1.11.16 SUMMARY ======== PARAMETERS * /rosdistro: indigo * /rosversion: 1.11.16 NODES auto-starting new master process[master]: started with pid [2718] ROS_MASTER_URI=http://imx6q:11311/ setting /run_id to 1c07caa4-1dd3-11b2-b860-00049f0399fe process[rosout-1]: started with pid [2731] started core service [/rosout] Open a new Terminal and Create the user catkin_ws Workspace. The catkin_ws workspace will contain the user packages. $ source /opt/ros/indigo/setup.bash $ mkdir -p ~/catkin_ws/src $ cd ~/catkin_ws/src $ catkin_init_workspace $ cd ~/catkin_ws/ $ catkin_make The  catkin_make command is a convenience tool for working with catkin_workspace. If you look in your current directory you should now have a 'build' and 'devel' folder. Inside the 'devel' folder you can see that there are now several setup.*sh files. Sourcing any of these files will overlay this workspace on top of your environment. To understand more about this see the general catkin documentation: http://wiki.ros.org/catkin Before continuing source your new setup.*sh file: $ source devel/setup.bash To make sure your workspace is properly overlayed by the setup script, make sure ROS_PACKAGE_PATH environment variable includes the directory you're in. $ echo $ROS_PACKAGE_PATH /home/youruser/catkin_ws/src:/opt/ros/indigo/share:/opt/ros/indigo/stacks Next you should go ahead and learn how to use the workspace. If you are following the ROS tutorials series instead of the catkin tutorials, please continue with Creating a ROS Package. For more testing on your installation, you can try the ROS Tutorials (http://wiki.ros.org/ROS/Tutorials)
記事全体を表示