i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
D1 Capture - kernel 2.6.22 diff --exclude CVS -uNr linux-2.6.22/include/asm-arm/arch-mxc/memory.h linux-2.6.22.modified/include/asm-arm/arch-mxc/memory.h --- linux-2.6.22/include/asm-arm/arch-mxc/memory.h     2009-07-16 16:29:45.000000000 -0300 +++ linux-2.6.22.modified/include/asm-arm/arch-mxc/memory.h     2009-07-15 15:38:34.000000000 -0300 @@ -28,6 +28,7 @@     /* Size of contiguous memory for DMA and other h/w blocks */     #define CONSISTENT_DMA_SIZE     SZ_16M    +     /*!      * @defgroup Memory_MX27 Memory Map      * @ingroup MSL_MX27 @@ -48,7 +49,7 @@     #ifdef CONFIG_DMA_ZONE_SIZE     #define MXC_DMA_ZONE_SIZE     ((CONFIG_DMA_ZONE_SIZE * SZ_1M) >> PAGE_SHIFT)     #else    -#define MXC_DMA_ZONE_SIZE     ((12 * SZ_1M) >> PAGE_SHIFT)   +#define MXC_DMA_ZONE_SIZE     ((20 * SZ_1M) >> PAGE_SHIFT)     #endif      static inline void __arch_adjust_zones(int node, unsigned long *zone_size, diff --exclude CVS -uNr linux-2.6.22/drivers/media/video/mxc/capture/mxc_v4l2_capture.c linux-2.6.22.modified/drivers/media/video/mxc/capture/mxc_v4l2_capture.c ---    linux-2.6.22/drivers/media/video/mxc/capture/mxc_v4l2_capture.c     2009-07-16 16:29:43.000000000 -0300 +++ linux-2.6.22.modified/drivers/media/video/mxc/capture/mxc_v4l2_capture.c     2009-07-16 16:08:02.000000000 -0300 @@ -1650,9 +1650,9 @@                  /* setup cropping */                 cam->crop_bounds.left = 0; -             cam->crop_bounds.width = 640; +             cam->crop_bounds.width = 800;                 cam->crop_bounds.top = 0; -             cam->crop_bounds.height = 480; +             cam->crop_bounds.height = 600;                 cam->crop_current = cam->crop_defrect = cam->crop_bounds;                 ipu_csi_set_window_size(cam->crop_current.width,                                                       cam->crop_current.height); @@ -1663,7 +1663,7 @@                 cam->standard.id = V4L2_STD_UNKNOWN;                 cam->standard.frameperiod.denominator = 30;                 cam->standard.frameperiod.numerator = 1; -             cam->standard.framelines = 480; +             cam->standard.framelines = 600;                 cam->streamparm.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;                 cam->streamparm.parm.capture.timeperframe =                 cam->standard.frameperiod; cam->streamparm.parm.capture.capability = V4L2_CAP_TIMEPERFRAME; diff --exclude CVS -uNr linux-2.6.22/drivers/media/video/mxc/capture/ov2640.c linux-2.6.22.modified/drivers/media/video/mxc/capture/ov2640.c ---    linux-2.6.22/drivers/media/video/mxc/capture/ov2640.c     2009-07-16 16:29:45.000000000 -0300 +++ linux-2.6.22.modified/drivers/media/video/mxc/capture/ov2640.c     2009-07-16 16:07:03.000000000 -0300 @@ -698,12 +698,12 @@     #endif                            g_cam->streamparm.parm.capture.capturemode = 1;                 } else { -          out_width = 640; -          out_height = 480; +          out_width = 800; +          out_height = 600;                 g_cam->crop_bounds.left = 0; -          g_cam->crop_bounds.width = 640; +          g_cam->crop_bounds.width = 800;                 g_cam->crop_bounds.top = 0; -          g_cam->crop_bounds.height = 480; +          g_cam->crop_bounds.height = 600;                 g_cam->crop_current = g_cam->crop_defrect = g_cam->crop_bounds;     #ifdef CONFIG_ARCH_MX3                              ipu_csi_set_window_size(g_cam->crop_current.width ,
記事全体を表示
Gingerbread (GB) Prepare the SD Card root/ : root file system (including init, init.rc, etc). Mounted at / system/:  Android system binary/libraries. Mounted at /system data/: Android data area. Mounted at /data recovery/: root file system when booting in "recovery" mode. Not directly used. Partition Description Type Size Header 8 BOOT raw area for bootloader and MEDIA DATA CACHE RECOVERY An example of partition a 4 GB SD card: Copy the system to SD card # sudo dd if=u-boot.bin of=/dev/sdx bs=1K skip=1 seek=1; sync # sudo dd if=u-boot-no-padding.bin of=/dev/sdx bs=1K seek=1; sync # sudo dd if=uImage of=/dev/sdx bs=1M seek=1; sync # sudo dd if=uramdisk.img of=/dev/sdx bs=1M seek=6; sync # sudo dd if=system.img of=/dev/sdx2; sync # sudo dd if=recovery.img of=/dev/sdx4; sync Ice Cream Sandwich (ICS)
記事全体を表示
i.MX27 PDK Board Flashing This tutorial teaches how to flash bootloader using ATK. To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot. Using ATK ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. This section will describe the procedure to erase the flash memory and program the bootloader. 1 - Connect a serial cable between PC and i.MX board. 2 - Some hardware configurations (switches) must be done to flash the board. Set red and cream switches as below: Switch SW5 -> 00000 Switch SW4 -> 10000001 Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe Next Step To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot. PS: On SW5 and SW4, "1" means the keys selected towards the edge of the board. 3 - Run ATK by clicking Start -> Programs -> AdvancedToolKit -> AdvancedToolKit       Set the options:    Device memory -> DDR; Custom Initial File -> (keep it unmarked)    Communication Channel -> Serial Port (Usually COM1) 4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO. Flash Erasing 1 - To erase Flash memory, select the parameters as shown in the figure below: 2 - Turn on the board and press Erase. 3 - ATK shows this message when flash is erased Flash Programming The next step is to program the bootloader image into the board's Flash following the steps below. 1 - Select the parameters as shown in the figure below and press Program. The bootloader binary image file can be found into your Board Support Package Set Program, NAND, Address: 0x00000000 2 - Add it on Image File field and press Program. 3 - Close ATK, turn off the board and set switch back as shown in the picture below. Installing ATK on Linux Download ATK: Download. Extract ATK: # unzip ATK_1_41_STD_installer.zip Execute the default install process: # wine SETUP.EXE Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32) Run ATK: # wine ADSToolkit_std.exe Next Step To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot.
記事全体を表示
Quick Steps Four quick steps to build and flash a UBIFS image on i.MX35 NAND (K9LBG08U0D-PCB0), for information on how to you another memory, please see next section. Enable MTD_UBI and UBIFS_FS on kernel Create UBI image from rootfs (used for NFS) - ON PC mkfs.ubifs -v -r rootfs -m 2048 -e 258048 -c 966 -o ubifs.img ubinize -o ubi.img -m 2048 -p 256KiB -s 2048 ubinize.cfg Format NAND using UBI image - ON TARGET ubiformat -f ubi.img /dev/mtd8 Load UBI file system load -r -b 0x100000 zImage fis create -f 0x300000 kernel fis load kernel exec -c "noinitrd console=ttymxc0 115200 ubi.mtd=8 root=ubi0:rootfs rw rootfstype=ubifs ip=none" How To First of all, install mtd-utils on both target and host: Target: ./ltib -c Package list [*] mtd-utils Host sudo aptget install mtd-utils 1. Enable MTD_UBI and UBIFS_FS on kernel MTD_UBI -> Device Drivers     -> Memory Technology Device (MTD) support (MTD [=y])           -> UBI - Unsorted block images                   <*> Enable UBI                    (4096) UBI wear-leveling threshold (NEW)                    (1) Percentage of reserved eraseblocks for bad eraseblocks handling (NEW)                 < > MTD devices emulation driver (gluebi) (NEW)                    ** UBI debugging options **                    [ ] UBI debugging (NEW) UBIFS_FS -> File systems         ->Miscellaneous filesystems             <*> UBIFS file system support                 [ ] Extended attributes support (NEW)                 [ ] Advanced compression options (NEW)                 [ ] Enable debugging (NEW) 2. Create UBI image On TARGET Collect some information needed in order to create the UBI image according to your NAND device root@freescale \~$ cat /proc/mtd dev:   size   erasesize name mtd0: 00080000 00020000 "Bootloader" mtd1: 00400000 00020000 "nor.Kernel" mtd2: 01e00000 00020000 "nor.userfs" mtd3: 01c00000 00020000 "nor.rootfs" mtd4: 00003000 00020000 "FIS directory" mtd5: 02001000 00020000 "Redboot config" mtd6: 00300000 00040000 "nand.bootloader" mtd7: 00500000 00040000 "nand.kernel" mtd8: 10000000 00040000 "nand.rootfs" mtd9: 00800000 00040000 "nand.configure" mtd10: 6f000000 00040000 "nand.userfs" I will use mtd8, because I want the NAND rootfs MTD partition. More on [1] root@freescale ~$ ubiattach /dev/ubi_ctrl -m 8 UBI: attaching mtd8 to ubi0 UBI: physical eraseblock size:   262144 bytes (256 KiB) UBI: logical eraseblock size:    258048 bytes UBI: smallest flash I/O unit:    2048 UBI: VID header offset:          2048 (aligned 2048) UBI: data offset:                4096 UBI: empty MTD device detected UBI: create volume table (copy #1) UBI: create volume table (copy #2) UBI: attached mtd8 to ubi0 UBI: MTD device name:            "nand.rootfs" UBI: MTD device size:            256 MiB UBI: number of good PEBs:        979 UBI: number of bad PEBs:         45 UBI: max. allowed volumes:       128 UBI: wear-leveling threshold:    4096 UBI: number of internal volumes: 1 UBI: number of user volumes:     0 UBI: available PEBs:             966 UBI: total number of reserved PEBs: 13 UBI: number of PEBs reserved for bad PEB handling: 9 UBI: max/mean erase counter: 0/0 UBI: image sequence number: 0 UBI: background thread "ubi_bgt0d" started, PID 2098 UBI device number You will need: -p = physical eraseblock size = 256KiB -e = logical eraseblock size = 258048 -m = smallest flash I/O unit = 2048 -s = VID header offset = 2048 -c = available PEB = 966 Values only for iMX35 PDK NAND - K9LBG08U0D-PCB0 3. ON HOST - Now, create the images (two steps) You need to create ubinize.cfg file! ubinize.cfg [ubifs] mode=ubi image=ubifs.img vol_id=0 vol_size=237MiB vol_type=dynamic vol_name=rootfs vol_flags=autoresize $ mkfs.ubifs -v -r rootfs -m 2048 -e 258048 -c 966 -o ubifs.img mkfs.ubifs      root:                rootfs/      min_io_size:    2048      leb_size:         258048      max_leb_cnt:   966      output:            ubifs.img      jrn_size:          8388608      reserved:         0      compr:            lzo      keyhash:         r5      fanout:            8      orph_lebs:       1      super lebs:      1      master lebs:    2      log_lebs:         4      lpt_lebs:          2      orph_lebs:       1      main_lebs:       132      gc lebs:           1      index lebs:       2      leb_cnt:           142      UUID:              CC2057F9-B20F-46D1-A399-1FCA95DCAFF7 Success\! $ ubinize -o ubi.img -m 2048 -p 256KiB -s 2048 ubinize.cfg $ ls -lh u* -rw-r--r-- 1 daiane daiane 35M 2010-11-26 15:21 ubifs.img -rw-r--r-- 1 daiane daiane 36M 2010-11-26 15:22 ubi.img -rw-r--r-- 1 daiane daiane 113 2010-11-26 15:22 ubinize.cfg $ sudo cp ubi.img rootfs/home/ 4. Format NAND using UBI image - ON TARGET Turn on target (or reset it) and format MTD partition $ cd /home $ ubiformat -f ubi.img /dev/mtd8 5. Load UBI file system Reset and change redboot script: .. fis load kernel .. exec -c "noinitrd console=ttymxc0 115200 ubi.mtd=8 root=ubi0:rootfs rw rootfstype=ubifs ip=none"
記事全体を表示
i.MX evaluation board can be a simple solution to program i.MX boards in a factory for instance. i.MX evaluation board are not for industrial usage, but you can find plenty of cheap i.MX insdustrial boards on the web. Here I am using an i.MX8QXP rev B0 MEK board and I will program an i.MX6Q SABRE SD board. The first step is to generate your image. Follow the documentation steps to generate the "validation" image. You will have to customize a little bit the local.conf file (in conf/local.conf) to have git, cmake, gcc and other missing package. edit local.conf and add the following lines at the end of the file: IMAGE_INSTALL_append = " git cmake htop packagegroup-core-buildessential xz p7zip rsync"‍‍‍‍‍ I have added rsync package in local, it can replace cp (copy) but with the --progress option you can see the copy progression. P7zip replace unzip for our images archives avaialable on nxp.com as unzip as issues with big files. then rebake your image: bitbake -k fsl-image-validation-imx‍‍‍‍‍ When it is done, go in tmp/deploy/image/<your image generated> and use uuu to program your board (I use a sd card; thus I can increase the partition esily): sudo ./uuu -b sd_all imx-boot-imx8qxpmek-sd.bin-flash fsl-image-validation-imx-imx8qxpmek.sdcard.bz2/*‍‍‍‍‍ As the rootfs can be too small, use gparted under Linux for instance to increase the size of the partition. Put the SD card and start your board. Here here the dirty part... You may know archlinux|ARM websitesite (Arch Linux ARM ), you have a lots of precompiled packages. Thus on the board you can download it, and copy the file in /usr folder (you can use it to have the latest openSSL for  instance!). Plug an ethernet cable on the board and check if it is up: ifconfig -a ifconfig eth0 up‍‍‍‍‍‍‍‍‍‍ Now you should have access to the internet. On uuu webpage you can find all the packages you need (here I am using a 4.14.98_2.0.0 Linux): mkdir missinglibs cd missinglibs wget http://mirror.archlinuxarm.org/aarch64/core/bzip2-1.0.8-2-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/core/nettle-3.5.1-1-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/core/libusb-1.0.22-1-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/extra/libzip-1.5.2-2-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/core/zlib-1:1.2.11-3-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/extra/p7zip-16.02-5-aarch64.pkg.tar.xz cd ..‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Wait all the archives are downloaded (otherwise you'll decompress before the archive is downloaded) as wget is running in background! Now untar the archives and copy it in the rootfs (dirty): tar -xJf libzip-1.5.2-2-aarch64.pkg.tar.xz tar -xJf libusb-1.0.22-1-aarch64.pkg.tar.xz tar -xJf nettle-3.5.1-1-aarch64.pkg.tar.xz tar -xJf bzip2-1.0.8-2-aarch64.pkg.tar.xz cp zlib-1:1.2.11-3-aarch64.pkg.tar.xz zlib tar -xJf zlib tar -xJf p7zip-16.02-5-aarch64.pkg.tar.xz cd usr sudo cp -R . /usr cd ../../ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Download and compile uuu: git clone git://github.com/NXPmicro/mfgtools.git cd mfgtools/ cmake . make‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Download an image on nxp.com for instance. I have downloaded on the i.MX6 4.14.98_2.0.0 image and put it on a usb key. then unzip it in the uuu folder: 7z e L4.14.98_2.0.0_ga_images_MX6QPDLSOLOX.zip‍‍‍‍ As mentionned before unzip cannot hadle big files... so use 7z as me plug the i.MX6Q SABRE SD to the i.MX8X and program your i.MX6 board: ./uuu uuu.auto-imx6qsabresd‍ uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.74-0-g64eeca1 Success 1 Failure 0 ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
記事全体を表示
Configuring RedBoot The configuration is made using a Minicom session that need to be established between host and target through serial port. To have an operational system been executed just on the power on, configure the right for Boot script. The chooses are shown in Boot Script section. To avoid the start of operational system, power on the board and press CTRL-C immediately. Wait until RedBoot> prompt appears. Overview The main command for beginners is fconfig -l that can be abbreviated as fc -l    This command shows the actual configuration of Redboot, like: RedBoot> fc -l Run script at boot: true Boot script: .. load -r -b 0x100000 /tftpboot/zImage .. exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/n" Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false RedBoot> Run script at boot: set true for booting with a script or false to always enter on prompt directly Boot script: define what commands to execute as script at the startup Boot script timeout: how many time to wait before execute boot script Use BOOTP for network configuration: set true for getting configuration from BOOTP or false for manually configuring gateway and IP address Gateway IP address: The IP address of the gateway Local IP address: The board IP address Local IP address mask: The board IP mask address Default server IP address: The host IP address when NFS and TFTP server are running Configuring Network Execute the command to configure network parameters: RedBoot> fc This step guarantee the possibilities to load images from some server previously connected and configured. For Use BOOTP for network configuration: answer false. For Gateway IP address: type the gateway IP address of your network; For Local IP address: type an IP address to your board, it needs to be a valid IP in your network; For Local IP address mask: type the IP mask address; For Default server IP address: type the IP of your host server where are running TFTP and NFS. Pay special attencion for Update RedBoot non-volatile configuration - continue (y/n)?. Answer y to have your configuration saved in the flash. To verify if your configuration is working use ping, be patient this command is very slow: RedBoot" ping -h 10.29.244.99 Network PING - from 10.29.241.6 to 10.29.244.99 PING - received 10 of 10 expected Use the "-n" option to change the number of pings and the "-r" option to speed things up, such as: ping -n 3 -h 10.29.244.99 -r 10. The boot script configuration is done in the next section. Boot Script NFS Boot In NFS Boot mode, a kernel image and a root file system image are loaded from a configured server through TFTP and NFS that can be executed doing the development more easy. To configure RedBoot for NFS Boot reset the board and press CTRL-C immediately. In a Minicom session type fc to modify the configuration boot. Enter the script boot below: RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> load -r -b 0x100000 /tftpboot/zImage >> exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.244.99:/tftpboot/rootfs init=/linuxrc ip=10.29.241.6:10.29.244.99" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> The script is composed by two lines. The first line load the kernel image (zImage) by TFTP from /tftpboot, the directory configured in TFTP.\ The second line executes the kernel and mount the root file system using NFS. The path /tftpboot/ltib indicates the path that should be exported in the host machine. (It's the path in the /etc/exports) 10.29.244.99 is the host IP address 10.29.241.6 is the target IP address Flash Boot For flash boot the Boot Script differs a little bit: fis init kernel exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock8 rw rootfstype=jffs2 ip=none" The value for root can be different for each board type.
記事全体を表示
Before QT5 Qt3D was a separate project and was maintained separately.  Now it is offered along with other official plugins. QT3D supports the addition of 3D elements. In order to install it this is needed: Clone the git Qt3D repository $ git clone git://gitorious.org/qt/qt3d.git Using the Qmake that you already created when installing Qt5, this will setup the Makefile in order to cross compile the plugin. $ qmake $ make $ sudo make install Ready to play with Qt3D! This is the HelloWorld of 3D,  teapot.bez  is a bezier curves file with the forms of the famous teapot. import QtQuick 2.0 import Qt3D 1.0 Viewport{    width: 640; height: 480    Item3D{    id: teapot    mesh: Mesh { source: "teapot.bez" }    effect: Effect {}   } }
記事全体を表示
Getting Started for i.MX53 Quick Start Board Here is a quick overview you can follow to get your very first contact with i.MX53 QSB. Introduction Out of box i.MX53 QSB video booting up Ubuntu Original Video: Out of box i.MX53 QSB video booting up Ubuntu with some demo (GPU and VPU) Original Video: How to load a pre-built image Here, you should have loaded your board with the out-of-box SD card. Next step is create your own SD card with some pre-built image. You can find pre-built image packages from Freescale for Linux look for Linux Binary Demo file Please, go to Timesys wikipage[1] and see how to load a pre-built image. You can use some Freescale image or some Timesys image. Both will work! For loading linux OS you need at least 3 images: bootloader image kernel image root file system image or tarball Bootloader For iMX53QSB the default bootloader provided by Freescale is u-boot.You can build your own image using LTIB following the same procedure from here. Kernel You can build a new uImage (kernel binary image to be loaded by u-boot) using LTIB, and you can follow the instructions from here Root File System Root file system is a set of directories and files that become the system environment. How to Built Your Own Image Take BSP package on Freescale i.MX53 QSB web site. Prepare your computer to LTIB installation, see that you need All Boards LTIB. Transfer all images to the SD Card (it will be placed under <ltib_dir>/rootfs/boot). Configure your u-boot environment variable. Boot your board. In case you want to boot via NFS, please follow the next procedure instead. Take BSP package on Freescale i.MX 53 QSB web site. Prepare your computer to LTIB installation, see that you need @all_boards_ltib Configure your computer to be able to provide NFS service: Configure your TFTP server. Configure your NFS server. Configure your u-boot environment variable. Boot your board. Be aware the kernel command line you set on u-boot variable can configure the display.
記事全体を表示
This document explains how to bring-up u-boot & Linux via JTAG This procedure has been tested on: i.MX6 Solo X Sabre SD i.MX6UL EVK Prerequistes: Get the latest BSP for your board. This procedure was tested with L4.1.15. Build the 'core-image-minimal' image to bring-up your board (Detailed steps here) Optional- Build a meta-toolchain for your device 1.- Set board to boot from Serial dowloader mode or set it to boot from the SD card and remove the sd card We basically want the board to stall in boot ROM to attach to the target. 2.- Connect JTAG probe and turn on the board The device should stall trying to establish a connection to download an image, this will allow us to attach to the target. 3.- Load Device Configuration Data In 'normal' boot sequence the boot ROM takes care of reading the DCD and configuring the device accordingly, but in this case we are skipping this sequence and we need to configure the device manually. The script used by Lauterbach to parse and configure the device is called dcd_interpreter.cmm and can be found here. Search for the package for your specific device. The DCD configuration for your board should be on your u-boot directory: yocto_build_dir/tmp/work/<your board>imx6ulevk/u-boot-imx/<u-boot_version>2016.03-r0/git under board/freescale/<name of your board>mx6ul_14x14_evk/imximage.cfg This file (imximage.cfg) contains all the data to bring up DRAM among other early configuration options. 4.- Load U-boot If an SREC file of U-boot is not present build it (meta-toolchain installed required) the SREC file contains all the information required by the probe to load it and makes this process easier. To build the SREC simply type: make <your board defconfig>mx6ul_14x14_evk_defconfig  (all supported boards are found under u-boot_dir/configs) make If you cannot build an SREC or do not want to, you can use the u-boot.imx (located under yocto_build_dir/tmp/deploy/images/<your board name>/) or u-boot.bin files but you will need to figure out the start address and load address for these files, this can be done by examining the IVT on u-boot.imx (here is a useful document explaining the structure of the IVT). Let U-boot run and you should see its output on the console I will try to boot from several sources but it will fail and show you the prompt. 5.- Create RAMDisk After building the core-image-minimal you will have all the required files under yocto_build_dir/tmp/deploy/images/<your board name>/ You will need: zImage.bin - zImage--<Linux Version>--<your board>.bin Device tree blob - zImage--<Linux Version>--<your board>.dtb Root file system - core-image-minimal-<your board>.rootfs.ext4 We need to create a RAMDisk out of the root file system we now have, these are the steps to do so: Compress current Root file system using gzip: gzip core-image-minimal-<your board>.rootfs.ext4 If you want to keep the original file use: gzip -c core-image-minimal-<your board>.rootfs.ext4 > core-image-minimal-<your board>.rootfs.ext4.gz Create RAMDisk using mkimage: mkimage -A arm -O linux -T ramdisk -C gzip -n core-image-minimal -d core-image-minimal-<your board>.rootfs.ext4.gz core-image-minimal-RAMDISK.rootfs.ext4.gz.u-boot Output: Image Name: core-image-minimal Created: Tue May 23 11:28:55 2017 Image Type: ARM Linux RAMDisk Image (gzip compressed) Data Size: 3017939 Bytes = 2947.21 kB = 2.88 MB Load Address: 00000000 Entry Point: 00000000 Here are some details on mkimage usage Usage: mkimage -l image -l ==> list image header information mkimage [-x] -A arch -O os -T type -C comp -a addr -e ep -n name -d data_file[:data_file...] image -A ==> set architecture to 'arch' -O ==> set operating system to 'os' -T ==> set image type to 'type' -C ==> set compression type 'comp' -a ==> set load address to 'addr' (hex) -e ==> set entry point to 'ep' (hex) -n ==> set image name to 'name' -d ==> use image data from 'datafile' -x ==> set XIP (execute in place) mkimage [-D dtc_options] [-f fit-image.its|-F] fit-image -D => set options for device tree compiler -f => input filename for FIT source Signing / verified boot not supported (CONFIG_FIT_SIGNATURE undefined) mkimage -V ==> print version information and exit 6.- Modify U-boot's environment variables Now we need to modify U-boot's bootargs as follows: setenv bootargs console=${console},${baudrate} root=/dev/ram rw We need to find out the addresses where u-boot will expect the zImage, the device tree and the initial RAMDisk, we can do it as follows: => printenv fdt_addr fdt_addr=0x83000000 => printenv initrd_addr initrd_addr=0x83800000 => printenv loadaddr loadaddr=0x80800000 Where: fdt_addr -> Device tree blob load address initrd_addr -> RAMDisk load address loadaddr -> zImage load address 7.- Load zImage, DTB and RAMDisk Now we know where to load our zImage, device tree blob and RAMDisk, on Lauterbach this can be achieved by running the following commands: Stop the target and execute: data.load.binary zImage.bin 0x80800000 data.load.binary Your_device.dtb 0x83000000 data.load.binary core-image-minimal-RAMDISK.rootfs.ext4.gz.u-boot 0x83800000 Let the device run again and deattach from the device in lauterbach this is achieved by: go SYStem.mode.NoDebug start the boot process on u-boot as follows: bootz ${loadaddr} ${initrd_addr} ${fdt_addr} You should now see the Linux kernel boot process on your terminal: After the kernel boots you should see its prompt on your terminal: Since we are running out of RAM there is no way for us to save u-boot's environment variables, but you can modify the source and compile u-boot with the new bootargs, by doing so you can create a Load script that loads all the binaries hits go and the boot process will continue automatically. One way to achieve this is to modify the configuration file under U-boot_dir/include/configs/<your board>.h find the mfgtool_args and modify accordingly. The images attached to this thread have been modified as mentioned.
記事全体を表示
Introduction This is a brief guide showing how to integrate the driver for the WF111 module to the i.MX6 BSP Release. In this case the WF111 driver is available on a repository and it’s in accordance with the Yocto Project, which allows to easily customize a linux distribution for your board. Requirements WF111 Documentation – Silicon Labs have made a great job of documenting the steps to add the WF111 driver to a Linux distribution and have created Application Note 996 (link below), which we will use as reference. http://www.silabs.com/documents/login/application-notes/AN996.pdf WF111 Driver - We will also be using the Yocto layer included on the following repository: https://github.com/engicam-stable/meta-engicam i.MX6 3.14.52 BSP Release – In out scenario the WF111 layer that will be imported includes a driver that it’s compatible with Linux Kernel 2.6.24 up to 4.1., which it’s important to keep in mind.   Installing the 3.14.52 BSP Release First, setup the 3.14.52 BSP as described on the i.MX Yocto Project User’s Guide.   Adding the WF111 Driver Layer Clone the WF111 Driver Layer to your sources folder inside the BSP Release directory. Since the 3.14.52 BSP Release is based on Fido we will clone the Fido branch of the driver repository. $ cd <BSP_RELEASE_DIR>/sources $ git clone https://github.com/engicam-stable/meta-engicam -b fido‍‍  Once the layer is cloned you would need to add the new later editing the bblayers.conf file located the following path: <BSP_RELEASE_DIR>/<BUILD_DIR>/conf/bblayers.conf By adding the following line to add the new layer.   BBLAYERS += " ${BSPDIR}/sources/meta-engicam "‍   This should make the wf111-driver available through bitbake since bitbake will now look into this layer for all available recipes. You can then add the driver to your image by adding the following line to the <BUILD_DIR>/conf/local.conf   IMAGE_INSTALL_append += "wf111-driver"‍ Or you may create a new image recipe that includes the wf111-driver package. However, there are certain kernel options that must be enabled for the driver to work.   Creating an append to configure the kernel options Before we can bake an image with the WF111 driver we would need to edit the kernel options as mentioned on Silabs AN996. The following kernel options must be enabled:   CONFIG_WIRELESS_EXT CONFIG_MODULES CONFIG_FW_LOADER We would need to add the CONFIG_WIRELESS_EXT as the other two options are enabled on the BSP by default.   This involves adding an addendum to the kernel recipe to change its configuration. You may either add this append to any layer. The best way to handle it would be using a new layer for all your customization. You can find how to create a new layer on the following document: https://community.nxp.com/docs/DOC-331917 We’ll use a new layer called meta-newlayer for this example. It’s important that this layer has a high priority so the changes from the bbappend are not overridden. The following alternative was suggested by Chris Hossack on the following thread: https://community.nxp.com/thread/376369 First, run the menuconfig tool on the bitbake environment: bitbake linux-imx -c menuconfig Enable the necessary options: Networking Support > Wireless > cfg80211 wireless extensions compatibility   Save the configuration and exit. Then run the following bitbake command, which will create a config fragment file that contains the changed made to the default kernel options. bitbake linux-imx -c diffconfig We’ll make an append file that adds the required options.  Content of the config fragment:   CONFIG_WIRELESS_EXT=y CONFIG_WEXT_CORE=y CONFIG_WEXT_PROC=y CONFIG_WEXT_SPY=y CONFIG_WEXT_PRIV=y CONFIG_CFG80211_WEXT=y CONFIG_LIB80211=y CONFIG_LIB80211_CRYPT_WEP=y CONFIG_LIB80211_CRYPT_CCMP=y CONFIG_LIB80211_CRYPT_TKIP=y # CONFIG_LIB80211_DEBUG is not set CONFIG_HOSTAP=y # CONFIG_HOSTAP_FIRMWARE is not set‍‍‍‍‍‍‍‍‍‍‍‍‍    Since we are appending the kernel layer we need to add the addendum on the same path as that of the original kernel recipe but within our layer and create the append file there. Also add the WF111.cfg file to the linux-imx directory:   We would need to copy (and you may rename it as well) to the folder where are will be creating the append recipe for the kernel. Copy:  <BSP_RELEASE>/<BUILD_DIR>/tmp/work/<MACHINE>-poky-Linux-gnueabi/linux-imx/<KERNEL_VERSION>/fragment.cfg To: <BSP_RELEASE>/sources/meta-newlayer/recipes-kernel/linux/linux-imx/WF111.cfg You can do so suing the following command: cp <BSP_RELEASE>/<BUILD_DIR>/tmp/work/<MACHINE>-poky-Linux-gnueabi/linux-imx/<KERNEL_VERSION>/fragment.cfg <BSP_RELEASE>/sources/meta-newlayer/recipes-kernel/linux/linux-imx/WF111.cfg‍ (Please note that the file was renamed for ease, but you may use any name for the config fragment)   We need to create the bbappend file on the following path (as it must be the same relative path as the original recipe it is appending) <BSP_RELEASE>/sources/meta-newlayer/recipes-kernel/linux/linux-imx_3.14.52.bbappend   The linux-imx_3.14.52.bbappend file would contain the following:   SRC_URI += "file://WF111.cfg"  do_configure_append() {          #this is run from         #./tmp/work/<MACHINE>-poky-linux-gnueabi/linux-imx/3.14.52-r0/git          cat ../*.cfg >> ${B}/.config  }‍‍‍‍‍‍    After creating this recipe you should be able to bake any image from the BSP and see the driver there. I tested with the core-minimal-image and found that the files were indeed added to /lib/firmware. $ bitbake core-image-minimal ‍‍‍
記事全体を表示
Copy Redboot binary to /tftpboot. In this case: redboot.bin Load binary file to i.MX ram memory: RedBoot> load -v -r -b 0x100000 /tftpboot/redboot.bin Run the loaded image RedBoot> run 0x100000 Enable NOR, NAND or MMC flash media for Redboot. In this case, NAND is beeing used. RedBoot> factive nand Update Redboot in the flash with currently running image RedBoot> romupdate Copy redboot binary to /tftpboot. In this case: redboot.bin Load binary file to i.MX ram memory: RedBoot> load -v -r -b 0x100000 /tftpboot/redboot.bin Run the loaded image RedBoot> run 0x100000 Enable NOR, NAND, or MMC flash media for Redboot. In this case, NAND is being used. RedBoot> factive nand Update Redboot in the flash with currently running image RedBoot> romupdate
記事全体を表示
For Fedora Users: Open a terminal as root Edit tftp file -> #gedit /etc/xinetd.d/tftp Add these lines: service tftp     {   socket_type = dgram   protocol = udp   wait = yes   user = root   server = /usr/sbin/in.tftpd   server_args = /tftpboot   disable = no   per_source = 100 2   flags = IPv4 } Restart the service: # /etc/init.d/xinetd restart OR # service xinetd restart
記事全体を表示
This document explains the pad implementation and its relationship with the System Controller Firmware pad configuration service. There are two components to pad configuration in the SCFW, there are the modules that generate the signals that will ultimately appear on the physical pad, let's say GPIO/Ethernet/I2C/UART etc... and then there is the part that configures the muxing of the pad (what signal is going to be outputted through the specific pad), the drive strength of the pad, pull selection, etc, this is the part that the SCFW pad service configures. Introduction‌ The i.MX8 has three types of I/Os: 1.8V only I/Os 3.3V only I/Os 1.8V / 3.3V I/Os Dual Voltage I/Os Note: USB High Speed Inter-Chip (HSIC) and Ethernet interfaces have specific integration schemes with dedicated features. They are a modified versions of the above I/O types. HSIC are a special kind of I/O modified to sustain 480Mbps data rates ENET I/Os are modified versions of Dual Voltage I/Os to support 2.5V operations All of these I/Os have "common features" and "technology specific features" which depend on the type of I/O and the chip manufacturing process (FDSOI in the i.MX8QM case) I/O common features Muxing capability of up to 4 signals Each Pad can have up to 4 signals, only one signal can be present in the pad. To select the signal that will output on the pad simply look at the Pinmux spreadsheet and use the desired alternative, for instance in the following image SCU_GPIO0_00 has 3 options, SCU_GPIO (ALT0 - GPIO controlled directly by the SCU), SCU_UART0_RX (ALT1 - SCU UART receiver) or LSIO_GPIO0_IO28 (ALT3 - Low speed I/O GPIO).   Pads without GPIO functionality (i.e. without the GPIO option in the pinmux spreadsheet) are implemented for one purpose only, these pins are connected directly to the module that drives them and they feature their own physical interface. Examples are XTAL pins, DDR pins and SCU PMIC interface (shown above). Mode of operation All GPIO types support four modes of operation: Normal mode Data is being driven directly to the pad (an internal signal of 1 shows in the pad as a 1 and vice-versa) and the pad works either as an output or as an input but not both at the same time. The output buffer while on this mode looks like this: Open drain Data is being driven through an open drain configuration, the output on the pad switches between 0 and high-z. The pad works either as an output or as an input but not both at the same time, e.g. if the Output Buffer is enabled the Input Buffer is disabled. This is how the output buffer looks like on Open drain mode: Open drain and input Output buffer acts as in open drain mode but with the input buffer enabled regardless of the output buffer state (enabled/disabled), this allows to simultaneously read the signal at the pad while driving it. Output and input Output buffer acts as in normal mode but with the input buffer enabled regardless of the output buffer state (enabled/disabled), this allows to read the signal at the pad while driving it. Wake-up capability Each I/O can be configured to wake-up the device, the following configuration options are available: OFF I/O cannot wake-up the system Low detect Generate wake-up event when the pad remains in low-level High detect Generate wake-up event when the pad remains in high-level Rising edge Generate wake-up event on rising edge detection Falling edge Generate wake-up event on falling edge detection Technology specific features Some of the available features for each pad depend on two factors: Chip manufacturing process (FDSOI or LPP) I/O type (1.8V, 3.3V or Dual Voltage) The i.MX8QM is manufactured using FDSOI technology and it features all of the three available I/O types. Drive strength Drive strength options vary within I/O types and chip manufacturing options. The available options for a FDSOI chip are: 1.8V Drive strength options 3.3V Drive strength options Dual Voltage drive strength options Drive strength of 1mA Drive strength of 2mA Low drive strength (50 ohms) Drive strength of 2mA Drive strength of 4mA High drive strength (33 ohms) Drive strength of 4mA Drive strength of 8mA Drive strength of 6mA Drive strength of 12mA Drive strength of 8mA Drive strength of 10mA Drive strength of 12mA High-speed drive strength Pull Select The pull select available options are almost the same for all I/O types (1.8V being the exception) and they also depend on chip manufacturing process. The available options for a FDSOI chip are: Pull select options for FDSOI Bus-keeper (only available for 1.8V) Pull-up Pull-down No Pull (Disabled) A bus-keeper or bus-holder is used to keep the last state on the bus. In normal operation it makes no difference, but once the bus is tri-stated it keeps the last logic level in the bus to prevent the bus from floating. Compensation The compensation feature is only available on Dual Voltage I/Os. Dual Voltage I/Os have a different implementation, they require: Voltage reference generator - which provides a voltage reference to the supply detector and compensation cell Supply detector - detects automatically whether the I/O is being supplied with 1.8V or 3.3V and broadcasts this information to compensation cell and I/O  Compensation cell - adjusts drive strength of dual voltage I/Os depending on Process Voltage and Temperature (PVT) conditions. The default configuration takes care of adjusting this parameters and no further modifications are required. Pad configuration service SCFW API Mux selection The very first function that needs to be called to configure a pad is: sc_err_t sc_pad_set_mux(sc_ipc_t ipc, sc_pad_t pad, uint8_t mux, sc_pad_config_t config, sc_pad_iso_t iso);‍‍‍‍‍‍‍‍‍‍‍‍‍‍ This function takes care of configuring the muxing alternative and setting the common features, its parameters are: ipc - The Inter Processor Communication (IPC) channel that you will use to communicate with the SCU. You need to call sc_ipc_open to obtain it. pad - The pad you want to configure, the different pad definitions are in imx8qm_pads.h, this is basically the same list that is included in the scfw_api_qm.pdf document (page 27 Chapter 5 Pad List) and it also mimics the Pinmux excel sheet. mux - The mux setting that you require, basically Alt0 -> 0, Alt1 -> 1, Alt2 -> 2 and Alt3-> 3, the pinmux spreadsheet contains the required information (take a look at I/O common features above). config - Used to select the desired mode of operation (take a look at I/O common features above), the available options are declared under sc_pad_config_t Normal mode - SC_PAD_CONFIG_NORMAL Open Drain mode - SC_PAD_CONFIG_OD Open Drain and input - SC_PAD_CONFIG_OD_IN Output and input - SC_PAD_CONFIG_OUT_IN iso - This is the low-power isolation configuration (take a look at I/O common features above). The available options are declared under sc_pad_iso_t ISO_OFF - SC_PAD_ISO_OFF ISO_EARLY - SC_PAD_ISO_EARLY ISO_LATE - SC_PAD_ISO_LATE ISO_ON - SC_PAD_ISO_ON For instance to configure M40_I2C0_SCL with its UART alternative in normal mode with low-power isolation off, the call would look like this: sc_pad_set_mux(ipc, SC_P_M40_I2C0_SCL, 1, SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF);‍‍‍‍‍‍‍‍‍‍ Pad configuration To configure drive strength and pull select options the technology specific functions need to be used (FDSOI for i.MX8QM): sc_pad_set_gp is being used by our Linux team because it admits the passing of the configuration parameters as a single value and this eases the handling on the device tree, but you should aim to use the technology specific functions. sc_err_t sc_pad_set_gp_28fdsoi(sc_ipc_t ipc, sc_pad_t pad, sc_pad_28fdsoi_dse_t dse, sc_pad_28fdsoi_ps_t ps);‍‍‍‍‍‍‍‍‍‍‍ This function takes care of configuring the drive strength (DSE) and pull select settings (PS) for the specified pad, here is a break down of the parameters it uses: ipc - The Inter Processor Communication (IPC) channel that you will use to communicate with the SCU. You need to call sc_ipc_open to obtain it. pad - The pad you want to configure, the different pad definitions are in imx8qm_pads.h, this is basically the same list that is included in the scfw_api_qm.pdf document (page 27 Chapter 5 Pad List) and it also mimics the Pinmux excel sheet. dse - The desired drive strength configuration (see Technology specific features above). DSE settings depend on the I/O type being used, the available options for each I/O type are defined under sc_pad_28fdsoi_dse_t: ENET pads capable of operating at 2.5V are a subset of dual voltage I/Os, the dse options available for these pads are the same as normal dual voltage I/Os. i.e. High drive and low drive. ps - The desired pull select configuration (see Technology specific features above). The available options are defined under sc_pad_28fdsoi_ps_t: To determine whether a GPIO pad is 1.8V, 3.3V or Dual Voltage one can look at the pinmux spread sheet, the supply for the pad will indicate what implementation of the GPIO is used. For instance: pads under VDD_SIM_1P8_3P3 are Dual voltage I/Os pads under VDD_SCU_1P8 are 1.8V I/Os pads under VDD_ADC_3P3 are 3.3V I/Os taking the same example as above we could configure the M40_I2C0_SCL as follows: sc_pad_set_gp_28fdsoi(ipc, SC_P_M40_I2C0_SCL, SC_PAD_28FDSOI_DSE_DV_LOW, SC_PAD_28FDSOI_PS_NONE);‍‍‍‍‍‍‍‍‍‍‍‍‍ Configuration under Linux Linux configures pads through the device tree, the full documentation of the binding is under Documentation/devicetree/bindings/pinctrl/fsl,imx8qxp-pinctrl.txt. but here is an extract: * Freescale i.MX8QXP IOMUX Controller Required properties: - compatible: "fsl,imx8qxp-iomuxc" - fsl,pins: each entry consists of 2 integers. Its format is <pin_id pin_config>. pin_config definition: - i.MX8QXP have different pad types, please refer to below pad register definitions, the pinctrl driver will just write the pin_config into the hardware register.‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The driver uses the following API: sc_err_t sc_pad_set_gp (sc_ipc_t ipc, sc_pad_t pad, uint32_t ctrl) ‍‍‍ Instead of configuring each parameter individually as done with sc_pad_set_gp_28fdsoi it configures the pad as if writing to a register, the bitfield format is under the binding documentation but it is as follows: struct _hw_pad_iomux_bitfields0 { uint32_t GP : 19; /*!< [18:0] GP controls. */ uint32_t WAKEUP : 3; /*!< [21:19] Wakeup controls. */ uint32_t WAKEUP_ENB : 1; /*!< [22] Wakeup write enable. */ uint32_t LPCONFIG : 2; /*!< [24:23] Low-power config. */ uint32_t CONFIG : 2; /*!< [26:25] Config. */ uint32_t IFMUX : 3; /*!< [29:27] Mux. */ uint32_t GP_ENB : 1; /*!< [30] GP write enable. */ uint32_t IFMUX_ENB : 1; /*!< [31] Mux write enable. */ } B; ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ All the configurations mentioned above can be configured, but they are done in a single pass, e.g. Muxing, Configuration (Norma, Open Drive, etc...), Wakeup control, and GP controls are for Pull Select Drive Strenght etc... Check the Reference Manual Chapter for IOMUXD for the register definition for each pad. References For more details refer to the sc_fw_api.pdf document: Chapter 1.3.3 Pad Configuration Service Chapter 6 Pad List Chapter 9.3 (SVC) Pad Service System Controller Firmware 101 
記事全体を表示
Play MPEG4 Video only gst-launch filesrc location=test.mpeg ! mfw_vpudecoder codec-type=std_mpeg4 ! mfw_v4lsink H.264 Video only gst-launch filesrc location=test.avi ! mfw_avidemuxer ! mfw_vpudecoder codec-type=std_avc ! mfw_v4lsink AVI(H264+MP3) gst-launch filesrc location=test.avi ! mfw_avidemuxer name=demux demux. !  mfw_vpudecoder \     codec-type=std_avc ! mfw_v4lsink demux. ! queue max-size-buffers=0 ! <mp3_decoder_plugin> ! alsasink MP4(H264+MP3) gst-launch filesrc location=test.mp4 ! mfw_mp4demuxer name=demux demux. ! \    mfw_vpudecoder codec-type=std_mpeg4 ! mfw_v4lsink demux. ! \    queue max-size-buffers=0 ! <mp3_decoder_plugin> ! alsasink <mp3_decoder_plugin> can be replaced by mad RAW Video Test gst-launch videotestsrc ! video/x-raw-yuv,format=\(fourcc\)I420 !  mfw_v4lsink
記事全体を表示
The i.MX 8QXP MEK does not allow the OV5640/LVDS/LCD usage only by changing the device tree anymore. It occurs because the M4 owns the i2c resources, so the A core must use rpmsg to enable virtual drivers. Due to this, if the user changes the device tree, for instance, the *ov5640.dtb, the kernel won't boot, entering in the following loop: [    8.603353] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).      [    8.610025] [drm] No driver support for vblank timestamp query.              [    8.616077] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_) [    8.624978] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_op) [    8.632526] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_op) [    8.639833] imx-drm display-subsystem: failed to bind ldb@562210e0 (ops imx_7 [    8.648428] imx-drm display-subsystem: master bind failed: -517 With the approach provided in this post, it is possible to make this change manually, only by changing the flash.bin at U-boot for a non-m4 one. In order to make the changes to the flash.bin file, it’s needed to obtain the following files: - u-boot.bin from internal u-boot provided by NXP. - scfw_tcm.bin from SCFW porting kit - bl31.bin from ARM Trusted Firmware - SECO firmware container image Disclaimer The described procedures in this document target a GNU/Linux (Ubuntu 20.04 LTS) and it’s focused on iMX8QXP B0 + BSP L4.19.35_1.1.0. Required packages 1 - Install ARM64 ToolChain: 1.1 - Install ARM64 GCC and G++ cross-compilers: # apt install gcc-aarch64-linux-gnu g++-aarch64-linux-gnu 2 - Install ARM32 GCC6 ToolChain: 2.1 - Download the ARM32 6 Toolchain and install it: $ mkdir ~/gcc_toolchain $ cp ~/Downloads/gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 ~/gcc_toolchain/ $ cd ~/gcc_toolchain/ $ tar xvjf gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 # apt-get update # apt-get install srecord 3 - Download MKimage 3.1 - Create a new directory desired to the packages: $ mkdir flash_build $ cp flash_build 3.1 - Clone the MKimage: $ git clone https://source.codeaurora.org/external/imx/imx-mkimage -b imx_4.19.35_1.1.0 4 - U-boot build 4.1 - Clone the U-boot  $ git clone https://source.codeaurora.org/external/imx/uboot-imx -b imx_v2019.04_4.19.35_1.1.0 $ cd uboot-imx 4.2 - Export the ARM64 ToolChain:  $ export ARCH=arm64 $ export CROSS_COMPILE=/usr/bin/aarch64-linux-gnu- 4.3 - Build it:  $ unset LDFLAGS $ make -j4 imx8qxp_mek_defconfig $ make 4.4 - Copy the binary files to the MKimage/iMX8QX directory:  $ cp spl/u-boot-spl.bin ../imx-mkimage/iMX8QX/ $ cp u-boot-nodtb.bin ../imx-mkimage/iMX8QX/ $ cd ..   5 - ARM Trusted Firmware 5.1 - Clone the imx-atf:  $ git clone https://source.codeaurora.org/external/imx/imx-atf -b imx_4.19.35_1.1.0 $ cd imx-atf 5.2 - Build it:  $ unset LDFLAGS $ make PLAT=imx8qx bl31 5.3 - Copy the binary files to the MKimage/iMX8QX directory:  $ cp build/imx8qx/release/bl31.bin ../imx-mkimage/iMX8QX/ $ cd ..   6 - SCFW 6.1 - Export the ARM32 GCC6 Toolchain:  $ export TOOLS=~/gcc_toolchain/ 6.2 - Download the BSP L4.19.35_1.1.0_SCFW and copy it to the flash_build directory:  $ cp ~/Downloads/imx-scfw-porting-kit-1.2.7.1.tar.gz $ tar xvzf imx-scfw-porting-kit-1.2.7.1.tar.gz $ cd packages/ $ chmod a+x imx-scfw-porting-kit-1.2.7.1.tar.gz $ ./imx-scfw-porting-kit-1.2.7.1.bin 6.3 - Build it to i.MX 8QXP MEK B0:  $ cd imx-scfw-porting-kit-1.2.7.1/src/ $ tar xvzf scfw_export_mx8qx_b0.tar.gz $ cd scfw_export_mx8qx_b0/ $ make qx R=B0 B=mek 6.4 - Copy the binary file to the MKimage/iMX8QX directory:  $ cp build_mx8qx_b0/scfw_tcm.bin ../../../../imx-mkimage/iMX8QX/ $ cp ../../../../ 7 - SECO Firmware Container Image 7.1 - Download the SECO firmware binaries and copy it to the flash_build directory $ cp ~/Downloads/firmware-imx-7.9.bin . $ chmod a+x firmware-imx-7.9.bin 7.2 - Copy the binary files to the MKimage/iMX8QX directory:  $ cp firmware-imx-7.9/firmware/seco/mx8qx-ahab-container.img /imx-mkimage/iMX8QX/ 8 - Build flash.bin 8.1 - In a new terminal, open the imx-mkimage directory: $ cd flash_build/imx-mkimage 8.2 - Build it:  $ make SOC=iMX8QX flash 8.3 - Deploy it to the SDCard:  $ sudo dd if=iMX8QX/flash.bin of=/dev/sdX bs=1k seek=32 && sync Now, you are able to use any non-rpmsg.dtb without kernel errors. Author: Pedro Jardim: pedro.jardim@nxp.com
記事全体を表示
U-boot expects uImage format for the kernel image. In order to LTIB generate a uImage file: $ export SYSCFG_KTARG=uImage $ ./ltib -p kernel Setup in U-Boot the kernel bootargs: u-boot> setenv bootargs noinitrd console=ttymxc0,115200 init=/linuxrc root=/dev/nfs nfsroot=10.29.244.27:/tftpboot/rootfs ip=dhcp Change 10.29.244.27 to your host IP. The procedure above is needed when default bootloader used by ltib was redboot. In some ltib releases (before 2010) default bootloader is u-boot. In this case, ltib will create uImage by default
記事全体を表示
Tips collected from zhaoyang-b49593 and dandouglass-b41520 while enabling redundant boot: Using i.MX 8MQ, same method can be applied for other i.MX devices that support redundant boot, see SoC Reference Manual. As described on the RM, if primary image authentication fails the ROM can reset and try booting a secondary image. This feature is only available on closed mode with properly signed binaries, otherwise the ROM boots the primary image despite the auth failure. For the i.MX 8MQ, the secondary image must start with spl, not HDMI firmware. Note, there is no ROM redundancy for the hdmi fw, if it is corrupt user can store a 2nd copy on a different memory address and update at run time. Steps to generate a dual spl image: 1. Build and Sign bootable binary (spl, u-boot, atf, fw, etc) Use the Yocto BSP or follow this post to build outside the Yocto environment. To sign the binary, follow the documentation on u-boot source: <u-boot>/doc/imx/habv4/guides/mx8m_secure_boot.txt Program image to the SD card: dd if=signed_flash.bin of=<sd path> bs=1024 seek=33 After boot you can use "hab_status" to verify that no events were generated: u-boot=> hab_status Secure boot disabled HAB Configuration: 0xf0, HAB State: 0x66 2. Corrupt spl on your boot image You can corrupt anywhere on the spl signed area. For easier visualization at boot time we can corrupt the SPL banner. First create a copy: cp signed_flash.bin signed_flash_corrupt.bin Find the banner: hexdump -C signed_flash.bin | grep 2019 00020190 26 1c 40 92 04 00 80 d2 05 01 80 52 c4 20 04 aa |&.@........R. ..| 0002eac0 32 30 31 39 2e 30 34 2d 30 30 30 32 39 2d 67 34 |2019.04-00029-g4| 000dde10 3a 20 20 00 55 2d 42 6f 6f 74 20 32 30 31 39 2e |: .U-Boot 2019.| 0002eac3 is on spl area, where "9" for 2019 is, replace by "X" printf "X" > X dd if=X of=signed_flash_corrupt.bin seek=$((0x2eac3)) bs=1 conv=notrunc Verify corrupt binary hexdump -C -s 0x2eac0 -n 64 signed_flash_corrupt.bin 0002eac0 32 30 31 58 2e 30 34 2d 30 30 30 32 39 2d 67 34 |201X.04-00029-g4| 0002ead0 37 63 31 39 32 32 20 28 41 70 72 20 32 37 20 32 |7c1922 (Apr 27 2| Transfer image to SD Card dd if=signed_flash_corrupt.bin of=<sd path> bs=1024 seek=33 Now, you should see hab events after running "hab_status" on u-boot 3. Create a secondary boot image This can be the same content as your primary image without the HDMI fw or it can be a different spl image. For easier visualization, we can change the SPL banner, on the code this time. Modify banner at ./common/spl/spl.c as: - puts("\nU-Boot " SPL_TPL_NAME " " PLAIN_VERSION " (" U_BOOT_DATE " - " + puts("\nSecondary U-Boot " SPL_TPL_NAME " " PLAIN_VERSION " (" U_BOOT_DATE " - " As mentioned above, we want our boot image without the HDMI fw, when running imx-mkimage use the flash_evk_no_hdmi target: make SOC=iMX8MQ flash_evk_no_hdmi Sign the image as in step 1. If you program the new image to the SD you should see the new banner. Make sure to run hab_status to confirm that no HAB events are generated. 4. Program SRK Hash and Close SoC Follow the documentation on u-boot source for SRK programming and closing the device: <u-boot>/doc/imx/habv4/guides/mx8m_secure_boot.txt Before closing the SoC, but after the SRK is programmed, try your images to confirm no HAB events are generated. Be careful with this step, errors could brick your board. This step is irreversible. After closing the SoC it will only boot signed images. 5. Create dual bootloader image We can concatenate our binaries to create a single file, let's use 2MB distance between primary and secondary images: For the working primary image: objcopy -I binary -O binary --pad-to 0x200000 --gap-fill=0x00 signed_flash.bin 1st-spl_pad.bin cat 1st-spl_pad.bin secondary2_nohdmifw_signed_flash.bin > 1st-spl_pad_2nd-spl.bin Or for the corrupt primary image experiment: objcopy -I binary -O binary --pad-to 0x200000 --gap-fill=0x00 signed_flash_corrupt.bin 1st-spl_pad.bin cat 1st-spl_pad.bin secondary2_nohdmifw_signed_flash.bin > 1st-spl_pad_2nd-spl.bin Program it to the SD card on 0x8400 offset (33k) dd if=1st-spl_pad_2nd-spl.bin of=<sd path> bs=1024 seek=33 && sync 6. Add Secondary image table Follow the format on the RM, this is only 20 bytes long. For a 2MB distance between the table and the secondary image we can use "0x1000" on the firstSectorNumber field. 2MB/512 = 4096 (0x1000) The perl script attached, genSecTable.pl, can be used to generate it. perl genSecTable.pl 0x1000 Program it to the SD card on 0x8200 offset dd if=secTable.bin of=<sd path> bs=1 seek=$((0x8200)) && sync 7. Verify secondary image is booting If using the corrupt primary image, you should see the spl with the "Secondary U-Boot SPL..." banner. You can also read the persist secondary boot bit. u-boot=> md.l 0x30390098 1 30390098: 40000000 ...@ The work can be extended patching spl for in case of u-boot authentication failure, spl can try to authenticate and jump to the secondary u-boot.
記事全体を表示
Encode From YUV to H.264 gst-launch-0.10 filesrc location=file_in.yuv blocksize=w*h*1.5 ! \ mfw_vpuencoder codec type=std_avc framerate=fr ! filesink location=file_out.mpg Where: file_in.yuv: is the input file, a raw file. w*h*1.5: is the blocksize, it's calculated from input file dimensions: width * height * 1.5 mfw_vpuencoder: is the encoder with hardware acceleration for iMX27 std_avc: chooses the codec type for output file fr: indicates the framerate in that input file was created file_out.mpg: is the output file encoded in H.264 From Camera to H.264 gst-launch-0.10 mfw_v4lsrc ! mfw_vpuencoder codec-type=std_avc \ width=176 height=144 framerate=25 ! filesink location=test.video
記事全体を表示
The resource management service offers the possibility to divide the system into groups of resources or partitions. Resources within a partition can not access resources outside of it's partition. Partitioning a system is useful to isolate resources from one another, this gives you the ability to have for instance FreeRTOS and Linux each running simultaneously with its own set of resources. In the FreeRTOS/Linux example you could partition/divide the system into two groups/partitions where all resources/peripherals needed by FreeRTOS would be completely isolated from the resources needed by Linux, if any of the resources on the Linux partition tried to access a resource on the FreeRTOS partition the transaction would result in a bus error, as if the resource tried to access a region outside of its memory map. The partitioning mechanism is enforced by hardware and the configuration of the underlying hardware is completely abstracted by the SCFW API. The system partitioning can be performed in two ways: At boot time by modifying the function board_system_config on the board.c portion of the SCFW porting kit that corresponds to your board. This is used for software that is loaded as part of the boot process. At run time by calling the resource management service functions available. This is used to partition software that is launched by an operating system, e.g. an M4 used as sensor fusion and loaded/started by Linux. A partition can have: Resources (peripherals) Pads Memory regions All of the items mentioned above can be grouped within a partition. It is important to note that: At boot time all resources are grouped into a single partition. Resources can only be assigned to another partition by a resource within it's own partition.  Initial partitioning state of the system At boot time the system is initially configured in three partitions: The first partition (SCFW) contains all the resources, pads and memory required by the System Controller Unit (SCU) to execute the System Controller Firmware. The second partition (SECO) contains all the resources required by the Security Controller to execute. The third partition (Boot) contains all of the remaining resources, pads and memory available for the whole system. Once Linux and the M4 boot a typical use case is to partition the system as follows: In this case the boot partition is split into the ATF/Linux partition and the M4 partition. The ARM Trusted Firmware environment add a layer of abstraction to secure the environment and it is assigned cores and memory to execute in this privileged state, all the remaining resources, pads and memory are assigned to the Linux partition. The M4 partition contains all the resources required by the M4 to execute, as well as the resources required by the application running on the M4. Resource partitioning - Boot time configuration The SCFW porting kit provides an example on doing boot time configuration at the board.c file under platform/board/mx8q<x or m>_<your board>/board.c, board_system_config is the function in charge of partitioning the system at boot time. From the sc_fw_port.pdf (porting guide) document included in the porting kit - Boot Flags chapter: Here are a few important points to highlight: The code will only execute if the SC_BD_FLAGS_ALT_CONFIG is set under the boot flags (more details in the Usage chapter of the sc_fw_port.pdf), the flags are set while building the image with mkimage. An example is provided to build an image with partitioning enabled: flash_linux_m4: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin u-boot-atf.bin m4_image.bin ./$(MKIMG) -soc QX -rev B0 -append mx8qx-ahab-container.img -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a35 0x80000000 -p3 -m4 m4_image.bin 0 0x34FE0000 -out flash.bin‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The example above can be found under your i.MX8 variant on the soc.mak file, in the example above the SC_BD_FLAGS_ALT_CONFIG flag is being set by -flags 0x00200000 and the partition for the M4 is defined as the third one by the -p3 parameter. Without the -flags 0x00200000 (setting SC_BD_FLAGS_ALT_CONFIG) parameter on mkimage NO partition happens at boot time, if the target used to build the image does not set this flag, then the SCU does not partition the system. On the board.c file the code in charge of checking for this flag is the following: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) {‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ if the alt_config flag is not set, then the partitioning is skipped. The function rm_dump(pt_boot); dumps the partitioning state of the whole system, it can be called before and after the partitioning to make sure the device was partitioned as expected. Here is how a partition dump looks like: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated Partition: 1 Parent: 0 DID: 0 Flags: Used Isolated Partition: 2 Parent: 0 DID: 1 Flags: Used Secure Restricted Isolated *** Resources *********************************** Partition: 0 SC_PID0 SC_SEMA42 SC_TPM SC_PIT SC_UART ... Continues .... DBLOGIC DRC_0 DRC_1 Partition: 1 SC_PID1 SC_PID2 SC_PID3 SC_PID4 ... Continues .... BOARD_R5 BOARD_R6 BOARD_R7 Partition: 2 SECO CAAM_JR1 CAAM_JR1_OUT *** Memory Regions ****************************** Partition: 0 000: 0x030FE0000 - 0x03101FFFF Partition: 1 001: 0x000000000 - 0x01BFFFFFF 002: 0x034000000 - 0x037FFFFFF 003: 0x038000000 - 0x03BFFFFFF 004: 0x060000000 - 0x06FFFFFFF 005: 0x070000000 - 0x07FFFFFFF 006: 0x080000000 - 0x0FFFFFFFF 007: 0x400000000 - 0x43FFFFFFF 008: 0x880000000 - 0xFFFFFFFFF Partition: 2 *** Pads **************************************** Partition: 0 M40_I2C0_SCL M40_I2C0_SDA ... Continues .... SCU_BOOT_MODE4 SCU_BOOT_MODE5 Partition: 1 SIM0_CLK SIM0_RST SIM0_IO ... Continues .... ENET1_RGMII_RXD2 ENET1_RGMII_RXD3 COMP_CTL_GPIO_1V8_3V3_ENET_ENETA Partition: 2‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The dump contains the configuration of the partition, for instance: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ On the example above the Partition parent is partition 0 (itself, this is the System Controller partition, all partitions spawn from this one). The Domain ID (DID) is 2, this ID is used to identify the partition by the hardware, it is used to enforce hardware isolation. It is also a secure and isolated partition, the meaning of these flags can be found below and in the sc_fw document: Secure - boolean indicating if this partition should be secure; only valid if caller is secure Isolated - boolean indicating if this partition should be HW isolated; set SC_TRUE if new DID is desired Restricted - boolean indicating if this partition should be restricted; set SC_TRUE if masters in this partition cannot create new partitions Grant - boolean indicating if this partition should always grant access and control to the parent Coherent - boolean indicating if this partition is coherent; set SC_TRUE if only this partition will contain both AP clusters and they will be coherent via the CCI The rest of the sections of the dump highlight all the resources, pads and memory regions enclosed in each partition. For more details on the definition of all the API calls please refer to the respective sc_fw_api document for each SoC variant. Resource partitioning - Run time configuration  The run time partitioning doesn't differ from the example provided on the porting kit, that example can be used as a base to create a partition at run time by calling the SCFW API.  Examples The following examples will show how to modify the default partition configuration on the evaluation boards, i.MX8QM MEK will be used as a reference. With BSP 4.14.98_2.3.0, the porting kit can be obtained from i.MX Software and Development Tools | NXP . Default configuration without partitioning First we will dump the default configuration without partition, e.g. without setting the ALT_CONFIG flag, most mkimage targets with a single image are configured this way, see the soc.mak and related files under scripts: soc.mak\iMX8QM - imx-mkimage - i.MX Mkimage Bootloader Tool  For details on how to create a bootable image see i.MX8 Boot process and creating a bootable image  We can see that the targets flash and flash_spl do not set any flags on the image, therefore no partition of the system will occur at boot time. flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍‍‍ We will build the SCFW with the Debug Monitor enabled in order to be able to dump the partitions: make qm R=B0 B=mek M=1‍‍‍‍ Now we copy the SCFW binary we just build (scfw_tcm.bin under build_mx8qm_b0) to the mkimage iMX8QM folder, along with the SECO FW, ATF (bl31.bin) and u-boot. On mkimage the flash target will be used to create a bootable image with the SCFW we just build: make SOC=iMX8QM flash‍‍‍‍‍ Flash the image to your sd card sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 sync‍‍‍‍‍‍‍‍ The MEK has two serial ports, the first one (usually ttyUSB0) is used by the A cores (u-boot/Linux in this case), the second one is used by one of the M4 cores OR the SCFW, in this case it will be used by the SCFW.  Unfortunately there aren't enough serial ports on the MEK board to allow a dedicated port for SCU, M4 cores and A cores, so in order to use the Debug Monitor on the MEK the SCFW has to take over the M4_0 UART terminal. On the SCFW Debug monitor terminal type "dump rm" this will dump all the partition information, the full log is attached to this document (imx8qm_mek_no_partition.txt). On this log it can be seen that 4 partitions are created: Partition 0 --> SCFW Partition 1 --> ATF Partition 2 --> SECO Partition 3 --> U-boot/Linux/M4 cores/Rest of the system The ATF partition is created at run time by the ATF to run in its secure state, no extra partition is created at boot time, if an image without ATF where to be used only three partitions would be seen: Partition 0 --> SCFW Partition 1 --> U-boot/Linux/M4 cores/Rest of the system Partition 2 --> SECO Default configuration with partitioning enabled Now we will create an image with the SC_BD_FLAGS_ALT_CONFIG flag set, so that partitioning occurs at boot time, for demonstration purpose we will use the same target previously used but we will modify it to set the ALT_CONFIG flag, so on mkimage modify the flash target as follows: On iMX8QM/soc.mak flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍ After the modification build the image again make clean make SOC=iMX8QM flash‍‍‍‍ On mkimage's output you should be able to see: FLAG: 0x00200000 Note how the same SCFW is used as in the previous example, same for ATF, SECO, U-boot the only required change in this case is to enable the ALT_CONFIG flag in the image. Flash the sd card with the new image sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Dumping again the partitioning on the Debug monitor shows how the system now created additional partitions for the M4 cores and a shared partition: Partition 0 --> SCFW Partition 1 --> ATF (Created at run time by the ARM Trusted Firmware) Partition 2 --> SECO Partition 3 --> M4_0 Partition 4 --> M4_1 Partition 5 --> Shared partition Partition 6 --> U-boot/Linux/rest of the system The full log is attached as well. Modifying default configuration Now we will modify the default SCFW configuration to move some resources/pads from the M4 partition to the A cores partition (u-boot/Linux). All FlexCAN resources and pads will be moved from the M4 partition to the A core partition. From sc_fw_api_qm_b0.pdf Resource List: From sc_fw_api_qm_b0.pdf Pad List: Not all resources are available on all variants, for details on what resources/pads are available on your device please refer to its respective api document. Go back to the SCFW porting kit and open platform/board/mx8qm_mek/board.c, go to the definition of board_system_config which is the function where partitioning occurs. The code first verifies if the alt_config flag is set, and if not it skips partitioning, so all partitioning happens within the following if statement: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) ‍‍‍‍‍‍‍‍‍‍‍ The following partitions and memory regions are declared within this if statement: sc_rm_pt_t pt_m4_0; sc_rm_pt_t pt_m4_1; sc_rm_mr_t mr_m4_0, mr_m4_1; sc_rm_pt_t pt_sh; sc_rm_mr_t mr_sh;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ pt_m4_0 is the partition for the M4_0 core, its memory region is declared as mr_m4_0. Likewise for the M4_1 pt_m4_1 and mr_m4_1 are the partitions and memory regions assigned to the M4. pt_sh and mr_sh are the shared partition and memory region. A shared partition is created but it can only have a shared memory region. Pads and resources CANNOT BE SHARED there is no mechanism to protect the pads and resources from contention, if access to a resource is required by multiple partitions a virtual resource needs to be created, in this way the partition that requires access asks the partition that owns the resource to configure/use the resource on its behalf. See the VIRT_I2C example on the Linux BSP. The partition that hosts all remaining resources is the pt_boot partition, this can be seen as the A cores partition, all resources and memory regions not assigned to the M4 partitions will be left on the pt_boot partition where the A cores are. The code is documented well and self-explanatory, for instance the following line marks all resources within the M4_0 subsystem to be moved to the M4_0 partition: /* Mark all M4_0 subsystem resources as movable */ BRD_ERR(rm_set_subsys_rsrc_movable(pt_boot, SC_R_M4_0_PID0, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_M40_I2C0_SCL, SC_P_M40_GPIO0_01, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The resource list in the sc_fw_api_qm_b0.pdf document shows what resources belong to the M4 subsystem: Next some other resources required by the M4 are assigned to its partition, such as MUs used to communicate with the other cores, timers and the IRQ steer resource. In this case we are interested on having the FlexCAN resources/pads on the A cores side, these resources/pads are being assigned to the M4_1 partition as can be seen on the previous partitions dumps and the following code: /* Move some resources not in the M4_1 subsystem */ BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_IRQSTR_M4_1, SC_R_IRQSTR_M4_1, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_UART_2, SC_R_UART_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_UART0_CTS_B, SC_P_UART0_RTS_B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_6B, SC_R_MU_6B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_7B, SC_R_MU_7B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_9B, SC_R_MU_9B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_GPT_3, SC_R_GPT_3, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_FSPI_0, SC_R_FSPI_0, SC_TRUE)); /* Move some pads not in the M4_1 subsystem */ BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_QSPI0A_DATA0, SC_P_COMP_CTL_GPIO_1V8_3V3_QSPI0, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Previous dump: *** Resources *********************************** Partition: 4 M4_1_PID0 UART_2 CAN_0 CAN_1 CAN_2 IRQSTR_M4_1 *** Pads **************************************** Partition: 4 M41_I2C0_SCL M41_I2C0_SDA M41_GPIO0_00 M41_GPIO0_01 UART0_RTS_B UART0_CTS_B FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX So we just need to remove the following lines from the board.c: BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ That way the resources/pads won't be marked to be moved to the M4_1 partition and they will be left on the pt_boot partition (A core partition). If a resource needs to be added to the M4 partition just add the calls to rm_set_resource_movable to assign it. Now we just need to rebuild the scfw and our image: make qm R=B0 B=mek M=1‍‍‍‍‍ Then on mkimage (with the flags set modification above): make SOC=iMX8QM flash‍‍‍‍ Flash the sd card with the new image: sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Now when the dump is done we can see that the FlexCAN resources and pads belong to the same partition as the A cores (partition 6). *** Resources *********************************** Partition: 6 FTM_1 CAN_0 CAN_1 CAN_2 DMA_1_CH0 *** Pads **************************************** Partition: 6 COMP_CTL_GPIO_1V8_3V3_GPIOLHT FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX COMP_CTL_GPIO_1V8_3V3_GPIOTHR The device tree would still need to be modified to configure the pads and FlexCAN resources. System Controller Firmware 101 
記事全体を表示
First download and install imx31_ads_20071008-rel5b-ltib.iso. Download and extract u-boot-1.3.3.tar.bz2. Place toolchain on PATH: $ export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" Export the CROSS_COMPILE name to U-Boot $ export CROSS_COMPILE=arm-none-linux-gnueabi- Enter in the u-boot-1.3.3 directory. Create configuration to i.MX31ADS board: $ make mx31ads_config Compile U-Boot to selected board: $ make If compilation goes fine you will see the u-boot.bin on current directory.
記事全体を表示