i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Installing the new release (Ubuntu 22.04) was detected some NXP boards as iMX8MNEVK, iMX8MM-EVK, iMX8MP-EVK and iMX8ULP-EVK had an issue with the WIFI module that basically it does not initialize at boot. Remember, the supported WIFI modules in Ubuntu 22.04 in the EVKs are the following:       • NXP 88W8987       • NXP 88W9098       • NXP 88W8997       • NXP IW416       • NXP 88W8801       • NXP IW612 To initialize the WIFI module of NXP EVKs in Ubuntu 22.04 you can set the following command in console:   sudo modprobe moal mod_para=nxp/wifi_mod_para.conf   That command find the correct driver for our WIFI module and then initialize it, but this only works when Ubuntu is working and if you reset the EVK you need to set the command again.   The definitive solution is create a custom startup script as a service:   Step 1: Go to etc/systemd/system   cd etc/systemd/system   Step 2: In this directory create a new file with the name of your preference but the extension must be .service. You can do it with nano or vim: sudo nano or sudo vim   The file must contain: [Unit] Description=”Wifi Start” [Service] ExecStart=sudo modprobe moal mod_para=nxp/wifi_mod_para.conf [Install] WantedBy=multi-user.target   Now save the file, in my case the name was wifi_start.service.   Step 3: Now we need to enable the script in the startup/boot sequence following the command: sudo systemctl enable wifi_start.service   Remember in wifi_start.service is the name as you saved your file.   Finally, each time you boot your board, the WIFI module will initialize automatically.   Boards tested: iMX8MN (With WIFI module NXP 88W8987) iMX8MM (With WIFI module NXP 88W8987) iMX8MP (With WIFI module NXP 88W8997) iMX8ULP (With WIFI module NXP IW416)  
查看全文
This demo for all(bootloader, device tree, Linux kernel, rootfs) in spi. It uses raw read(sf read)/raw write(sf write in uuu script) to achieve that. sf probe 0; sf read ${fdt_addr} 0x500000 0x100000; sf read ${loadaddr} 0x600000 0x1E00000; sf read ${initrd_addr} 0x2400000 0x600000; setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate} rdinit=/linuxrc; booti ${loadaddr} ${initrd_addr} ${fdt_addr} |-- 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch --- patch for this demo |-- demo_binary | |-- flash.b0.bin --- b0 bootloader | |-- flash.bin --- c0 bootloader | |-- Image-imx8qxpc0mek.bin --- Linux kernel | |-- imx8qxp-mek.dtb --- device tree | |-- uramdisk_boot.rootfs.aarch64.img --- ram disk | |-- uuu.qspi.all.b0.uuu --- uuu script for b0 | `-- uuu.qspi.all.uuu --- uuu script for c0 `-- readme.txt --- this file # The spi layout used is: # - --------- -------------------------------------------- # | | flash.bin | env | dtb | Image |rootfs| # - --------------- -------------------------------------- # ^ ^ ^ ^ ^ ^ ^ # | | | | | | | # 0 4kiB 4MiB 5MiB 6MiB 36MiB 42MiB 0x1000 0x400000 0x500000 0x600000 0x2400000 Test: HW: i.MX8QXP MEK SW: lf-5.10.72-2.2.0 + 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch Test log: SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB device 0 offset 0x500000, size 0x100000 SF: 1048576 bytes @ 0x500000 Read: OK device 0 offset 0x600000, size 0x1e00000 SF: 31457280 bytes @ 0x600000 Read: OK device 0 offset 0x2400000, size 0x600000 SF: 6291456 bytes @ 0x2400000 Read: OK [ 4.787552] imx6q-pcie 5f010000.pcie: unable to add pcie port. [ 4.797467] Freeing unused kernel memory: 2944K [ 4.807379] Run /linuxrc as init process Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting network: OK /bin/sh: can't access tty; job control turned off / #  
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519   To reduce the number of attachments, older RPAs may be found in the attached zip file. Note: Devices with 17-row addresses (R0-R16) are not supported by this SoC.  ***IMPORTANT: For SCFWv1.7.0 and later, you must use the following RPA versions or later: MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8QuadXPlus_DualXPlus_C0_B0_DDR3L_RPA_v22 MX8DualX_C0_B0_DDR3L_RPA_v20 Older versions of the RPA are not aligned to SCFWv1.7.0 and later.  If trying to use an older version of an RPA with SCFWv1.7.0, it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QXP/DualX: DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 and later (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QXP: [remove] #ifndef SCFW_DCD [remove] -/* For 1200MHz DDR, DRC 600MHz operation */ [remove] DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ [remove] #else <keep code as is> [remove] #endif
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519 Note: Devices with 17-row addresses (R0-R16) are not supported by this SoC.  To reduce the number of attachments, older RPAs may be found in the attached zip file.   ***IMPORTANT: For SCFWv1.7.0, you must use the following RPA versions or later: MX8QM_B0_LPDDR4_RPA_1.6GHz_v23 Older versions of the RPA are not aligned to SCFWv1.7.0.  If trying to use an older version of an RPA with SCFWv1.7.0, it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QM: DATA 4 0xff148000 0x00000885 /* DRC0 bringup */ DATA 4 0xff1a0000 0x00000885 /* DRC1 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QM: [remove] #ifndef SCFW_DCD [remove] /* For 1600MHz DDR, DRC 800MHz operation */ [remove] DATA 4 0xff148000 0x00000885 /* DRC0 bringup */ [remove] DATA 4 0xff1a0000 0x00000885 /* DRC1 bringup */ [remove] #else <keep code as is> [remove] #endif  
查看全文
In this article, I will explain how to set up the iMX8M Plus to use the 4K Dart BCON Basler Camera module. imx8mp.png Requirements: Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors) Basler Camera for i.MX 8M Plus (4K dart BCON for MIPI camera module for i.MX 8M Plus | NXP Semiconductors). Embedded Linux for i.MX Applications Processors (Embedded Linux for i.MX Applications Processors | NXP Semiconductors) (For this example we will use BSP version Linux 5.15.71_2.2.0) Serial Console Emulator Basler Camera Specifications and Manuals: Basler Camera Specifications at this link: Embedded Vision Kits daA3840-30mc-IMX8MP-EVK - Embedded Vision Kits (baslerweb.com). Basler Manual to identify and setting up the hardware at this link: daA3840-30mc-IMX8MP-EVK | Basler Product Documentation (baslerweb.com) Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor. (Video: Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor | NXP Semiconductors) Steps After setting up the hardware we will need to turn on the iMX8M Plus and follow these steps: 1. Stop the boot process on Uboot by pressing any key. 2. Use the following command to list interfaces. => mmc list Output example => FSL_SDHC: 1 (SD) => FSL_SDHC: 2 The above command will show you the device number in this example for SD, the device number is 1. 3. Then use fatls <interface> <device[:partition]> [<directory>] fatls mmc 1:1 (Device 1 : Partition 1) With this command, we will be able to list device tree files. => fatls mmc 1:1 4. Select imx8mp-evk-basler.dtb or imx8mp-evk-dual-basler.dtb and use the command editenv fdtfile.  => editenv fdtfile Output example edit: imx8mp-evk-basler.dtb 5. In edit command line put the selected device tree (*.dtb). 6. Use saveenv command to save environment and continue with the boot process. 7. Using the terminal and go to /opt/imx8-isp/bin and execute the script run.sh. $ ./run.sh -c basler_1080p60 -lm 8. Use the command gst-device-monitor-1.0 to list devices. Here you will find the path to the camera device. $ gst-device-monitor-1.0 Output example Device found: name : VIV class : Video/Source caps : video/x-raw, format=YUY2, width=[ 176, 4096, 16 ], height=[ 144, 3072, 8 ], pixel-aspect-ratio=1/1, framerate={ (fraction)30/1, (fraction)29/1, (fraction)28/1, (fraction)27/1, (fraction)26/1, (fraction)25/1, (fraction)24/1, (fraction)23/1, (fraction)22/1, (fraction)21/1, (fraction)20/1, (fraction)19/1, (fraction)18/1, (fraction)17/1, (fraction)16/1, (fraction)15/1, (fraction)14/1, (fraction)13/1, (fraction)12/1, (fraction)11/1, (fraction)10/1, (fraction)9/1, (fraction)8/1, (fraction)7/1, (fraction)6/1, (fraction)5/1, (fraction)4/1, (fraction)3/1, (fraction)2/1, (fraction)1/1 } ... properties: udev-probed = true device.bus_path = platform-vvcam-video.0 sysfs.path = /sys/devices/platform/vvcam-video.0/video4linux/video2 device.subsystem = video4linux device.product.name = VIV device.capabilities = :capture: device.api = v4l2 device.path = /dev/video2 v4l2.device.driver = viv_v4l2_device v4l2.device.card = VIV v4l2.device.bus_info = platform:viv0 v4l2.device.version = 393473 (0x00060101) v4l2.device.capabilities = 2216693761 (0x84201001) v4l2.device.device_caps = 69206017 (0x04200001) gst-launch-1.0 v4l2src device=/dev/video2 ! ... 9. Finally, use gstreamer to verify proper operation. (With this gstreamer pipeline you will see a new window with the camera output. Then, just rotate the lens to acquire the correct focus) $ gst-launch-1.0 -v v4l2src device=/dev/video2 ! "video/x-raw,format=YUY2,width=1920,height=1080" ! queue ! imxvideoconvert_g2d ! waylandsink Basic description of Gstreamer Pipeline gst-launch-1.0 -v: The option -v enables the verbose mode to get detailed information of process. v4l2src device=/dev/video2: Select input device in this case the camera is on path /dev/video3. "video/x-raw,format=YUY2,width=1920,height=1080": Received format from camera. queue: This command is a buffer between camera recording process and the following image process, this command help us to interface two process and prevent blocking where each process has different speeds, in other words, when a process A is faster than process B. imxvideoconvert_g2d: This proprietary plugin uses hardware acceleration to perform rotation, scaling, and color space conversion on video frames. waylandsink : This command creates its own window and renders the decoded frames processed previously. 10. Result Screenshot (46).png     I hope this article will be helpful. Best regards, Brian.
查看全文
This is about the case studay from two USB related issues: #1. Plugin detection issue caused by an errata in i.MX8/8X (host mode).       Very limited unit may encounter this problem. When issue happens, there will be totally no action on USB host port when a debug plugged in. #2: High Speed disconnection detection issue (host mode):       This may happen on some special USB design which have complex circuit and connector design on the USB path and long USB cable. The USB enumeration might be interrupted by an un-expected disconnection event. System log shows USB recognition started but failed at several different stages during handshake. For details, please refer to the doc attached (#1/#2). A reference patch for each has also been made by David.
查看全文
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
查看全文
We are pleased to announce that Config Tools for i.MX v13.1 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes 13.1 DDR tool     - i.MX93 support for A0 pre-production launch; sync with SW BSP release Pins tool     - Fix incomplete routing of deinit functions  
查看全文
    OpenSSL is popular software library for applications that secure communications over computer networks against eavesdropping or need to identify the party at the other end. It is widely used in internet web servers, serving a majority of all web sites. OpenSSL contains an open-source implementation of the Transport Layer Security (TLS) and Secure Sockets Layer (SSL) protocols, it is a robust, commercial-grade, and full-featured toolkit for the SSL and TLS protocols. OpenSSL is also a general-purpose cryptography library. Its core library, written in the C programming language, implements basic cryptographic functions and provides various utility functions. Wrappers allowing the use of the OpenSSL library in a variety of computer languages are available. More and more embeded systems, like IoT gateway, ePOS, based on i.MX use OpenSSL for their secure communications and cryptographic operations. But it's cryptography library is pure software implementation which need to occupy lots of CPU resouce and the perfermance is very weak than dedicated hardware IP (like CAAM).    CAAM is the i.MX's cryptographic acceleration and assurance module, which serves as NXP's latest cryptographic acceleration and offloading hardware. It combines functions previously implemented in separate modules to create a modular and scalable acceleration and assurance engine. It also implements block encryption algorithms, stream cipher algorithms, hashing algorithms, public key algorithms (i.MX6UL/i.MX7D/S), and a hardware random number generator.   The official Yocto release (L4.1.15_2.0.0-ga) of the i.MX only enable cryptodev for accelerating symmetric algorithms and hashing algorithms, not support asymmetric algorithms(RSA, ECC). And its engine in OpenSSL(version 1.0.2h) also miss some features which is used to support symmetric algorithms and hashing algorithms, for example, AES ECB, SHA224/256, etc. These patches in the post will close the above gaps for i.MX Linux system. The software environments as the belows: Linux kernel: imx_4.1.15_2.0.0_ga cryptodev: 1.8 OpenSSL: 1.0.2h The patches include the following key features: 1, Add public key cryptography part in CAAM driver, through protocol commands, to implement a number of public (and private) key functions. These are DSA and ECDSA sign/verify, Diffie-Hellman (DH) and ECDH key agreement, ECC key generation, DLC key generation, RSA encryption/decryption, RSA key-generation finalization. 2, Add big number operation and elliptic curve math in CAAM driver to implement addition, subtraction, multiplication, exponentiation, reduction, inversion, greatest common divisor, prime testing and point add, point double, point multiply. 3, Add API in cryptodev to support RSA encryption/decryption, DSA/ECDSA sign/verify, DH/ECDH key agreement, ECC & DLC & RSA key generation and big number operation and elliptic curve math. 4, Add public key cryptography functions, hardware rng, and missing hash symmetric algorithms in OpenSSL crytodev engine. Note: 1, You can refer to ecdhtest.c, ecdsatest.c, dhtest.c, dsatest.c, rsa_test.c for how to use crytodev engine in your applications based on libcryto.so. You can also find their executable programs in folder openssl-1.0.2h/test after compiling. 2, If you want to call crytodev API directly to accelerate public key cryptography operations, please refer to asymmetric_cipher.c in cryptodev-linux-1.8/tests. Current Limitation: 1, CAAM driver don't support AES GCM/CCM but hardware supporting. I plan to add the feature next version. 2, ECDSA sign/verify will fail on some binary curves (sect163r1, sect163r2, sect193r1, sect193r2, sect233r1, sect283r1, sect409r1, sect571r1 and X9.62 binary curves). I will try to find the root cause and fix it.   ==================================== for  some binary curves (sect163r1, sect163r2, sect193r1, sect193r2, sect233r1, sect283r1, sect409r1, sect571r1 and X9.62 binary curves)  are rarely used, so i will try to find the root cause when i'm free.  +++++++++++++++++++++++    updating for Linux-4.14.78-1.1.10 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux -4.14.78-1.1.10. The new software environments as the belows: Linux kernel: imx_4.14.78_1.1.10 cryptodev: 1.9 OpenSSL: 1.0.2p HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini, i.MX8/8X. The patches include the following new features: 1, support  RSA key generation but defaultly use openssl build-in function (BN_generate_prime_ex) to create prime p, q for higher security. If need to use CAAM accelerating,  please comment Macro USE_BUILTIN_PRIME_GENERATION, but don't confirm its security. 2, Add Manufacturing-protection feature, and you can refer to manufacturing_protection_test function in asymmetric_cipher.c. 3, Support AES GCM in cryptodev. 4, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-4.14.78-1.1.10 and copy meta-openssl-caam to folder <Yocto 4.14.78-1.1.10 dir>/sources/ 5, Run DISTRO=fsl-imx-wayland MACHINE=imx6ulevk source fsl-setup-release.sh -b build-imx6ulevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into /build-imx6ulevk/conf/bblayers.conf 6, bitbake fsl-image-validation-imx 7, Run the below command on your i.MX6UL EVK board. modprobe cryptodev openssl genrsa -f4 -engine cryptodev 512 -elapsed openssl speed dsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 1024 -elapsed openssl speed rsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 2048 -elapsed openssl speed ecdsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 3072 -elapsed openssl speed ecdh -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 4096 -elapsed openssl speed -evp sha256 -engine cryptodev -elapsed openssl speed -evp aes-128-cbc -engine cryptodev -elapsed openssl speed -evp aes-128-ecb -engine cryptodev -elapsed openssl speed -evp aes-128-cfb -engine cryptodev -elapsed openssl speed -evp aes-128-ofb -engine cryptodev -elapsed openssl speed -evp des-ede3 -engine cryptodev -elapsed openssl speed -evp des-cbc -engine cryptodev -elapsed openssl speed -evp des-ede3-cfb -engine cryptodev -elapsed +++++++++++++++++++++++    updating for Linux-4.14.98-2.3.3 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux -4.14.98-2.3.3. The new software environments as the belows: Linux kernel: imx_4.14.98-2.3.3 cryptodev: 1.9 OpenSSL: 1.0.2p HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano, i.MX8/8X. The patches include the following new features: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-4.14.98-2.3.3 and copy meta-openssl-caam to folder <Yocto 4.14.98-2.3.3 dir>/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into /build-imx8mmevk/conf/bblayers.conf 3, bitbake fsl-image-validation-imx 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl genrsa -f4 -engine cryptodev 512 -elapsed openssl speed dsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 1024 -elapsed openssl speed rsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 2048 -elapsed openssl speed ecdsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 3072 -elapsed openssl speed ecdh -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 4096 -elapsed openssl speed -evp sha256 -engine cryptodev -elapsed openssl speed -evp aes-128-cbc -engine cryptodev -elapsed openssl speed -evp aes-128-ecb -engine cryptodev -elapsed openssl speed -evp aes-128-cfb -engine cryptodev -elapsed openssl speed -evp aes-128-ofb -engine cryptodev -elapsed openssl speed -evp des-ede3 -engine cryptodev -elapsed openssl speed -evp des-cbc -engine cryptodev -elapsed openssl speed -evp des-ede3-cfb -engine cryptodev -elapsed +++++++++++++++++++++++    updating for Linux-4.19.35-1.1.2 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 4.19.35-1.1.2​​.  Software environments as the belows: Linux kernel: imx_4.19.35-1.1.2 cryptodev: 1.10 OpenSSL: 1.1.1l HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-4.19.35-1.1.2 and copy meta-openssl-caam to folder <Yocto 4.19.35-1.1.2 dir>/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 4.19.35-1.1.2 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake fsl-image-validation-imx. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed +++++++++++++++++++++++    updating for Linux-5.4.70-2.3.4 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.4.70_2.3.4​​.  Software environments as the belows: Linux kernel: imx_5.4.70_2.3.4 cryptodev: 1.10 OpenSSL: 1.1.1l HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-5.4.70-2.3.4  and copy meta-openssl-caam to folder <Yocto 5.4.70_2.3.4 dir>/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 5.4.70_2.3.4 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed     +++++++++++++++++++++++    updating for Linux-5.10.52-2.1.0 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.10.52_2.1.0​​.  Software environments as the belows: Linux kernel: lf-5.10.y cryptodev: 1.12 OpenSSL: 1.1.1l HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-5.10.52-2.1.0 and copy meta-openssl-caam to folder <Yocto 5.10.52_2.1.0 dir>/sources/ 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 5.10.52_2.1.0 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed   +++++++++++++++++++++++    updating for Linux-5.15.71-2.2.0 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.15.71-2.2.0​​.  Software environments as the belows: Linux kernel: lf-5.15.71-2.2.0 cryptodev: 1.12 OpenSSL: 3.1.0 HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-5.15.71-2.2.0 and copy meta-openssl-caam to folder <Yocto 5.15.71_2.2.0 dir>/sources/ 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 5.15.71_2.2.0 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed sm2 openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed    
查看全文
Platform: i.MX8MP SW:Linux 5.4.70.2.3.0 On current linux BSP, PCIE driver does not support Hot-plug, customers wants to turn off PCIE device to save power, attached is guide. Remove PCIE device driver Suspend PCIE driver Turn off PCIE device power supply Turn on PCIE device power supply Resume PCIE driver Rescan PCIE device Load PCIE device driver
查看全文
Platform: i.MX8MP EVK BSP: Linux 5.4.70.2.3.0 Customer reported UI on HDMI monitor is abnormal and has more line on left side when doing HDMI hot-plug on i.MX8MP running with L5.4.70.2.3.0. Lambert_0-1679058317200.png   This issue can’t be reproduced on latest BSP such as 5.10 and above, several patch for HDMI from latest BSP can fix this issue.  
查看全文
This doc will show: i.MX6SLL EVK board without connect hardware LCD display, using FreeRDP to share screen to remote PC which in same network, PC take this shared screen could run any command on i.MX6SLL EVK board. HW: i.MX6SLL EVK board, PC, usb network adapter SW: i.MX6SLL Linux 5.15.72_2.2.0 BSP release, and code change in this doc 1>yocto-5.15.72/6sll-bld/conf/local.conf, add below line, as freerdp depend on ffmpeg. LICENSE_FLAGS_ACCEPTED+="commercial" 2>pixman need switch to 0.42.0, enter folder yocto-5.15.72/6sll-bld/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/pixman/1_0.40.0-r0/pixman-0.40.0, fetch latest 0.42.0 version code from https://github.com/freedesktop/pixman.git 3>freerdp need use 2.8.0, enter folder yocto-5.15.72/6sll-bld/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/freerdp/1_2.6.1-r0/git should checkout to 2.8.0 tag; then to use neon accelerate freerdp related function, such as color space conversion, image codec encoding, apply patch freerdp-codechange-neon.diff. 4>Enter yocto-5.15.72/sources/meta-openembedded/meta-oe/recipes-support/freerdp, file freerdp_2.6.1.bb change as freerdp-2.6.1-bbfile.diff 5> bitbake -c compile ffmpeg bitbake -c install ffmpeg bitbake -c compile pixman bitbake -c install pixman bitbake -c compile freerdp bitbake -c install freerdp 6> Copy generated new libs to i.MX6SLL Linux rootfs: cp /root/imx6sllevk-linux-lib/lib* /usr/lib/ cd /usr/lib/ rm libfreerdp-client2.so.2 libfreerdp2.so.2 libpixman-1.so.0 libwinpr-tools2.so.2 libwinpr2.so.2 ln -s libfreerdp-client2.so.2.8.0 libfreerdp-client2.so.2 ln -s libfreerdp2.so.2.8.0 libfreerdp2.so.2 ln -s libpixman-1.so.0.42.0 libpixman-1.so.0 ln -s libwinpr-tools2.so.2.8.0 libwinpr-tools2.so.2 ln -s libwinpr2.so.2.8.0 libwinpr2.so.2 ln -s libavcodec.so.58.134.100 libavcodec.so.58 ln -s libavutil.so.56.70.100 libavutil.so.56 ln -s libswresample.so.3.9.100 libswresample.so.3 Make sure: libfreerdp-client2.so.2 -> libfreerdp-client2.so.2.8.0 libfreerdp2.so.2 -> libfreerdp2.so.2.8.0 libwinpr-tools2.so.2 -> libwinpr-tools2.so.2.8.0 libwinpr2.so.2 -> libwinpr2.so.2.8.0 libswresample.so.3 -> libswresample.so.3.9.100 libavutil.so.56 -> libavutil.so.56.70.100 libavcodec.so.58 -> libavcodec.so.58.134.100 7>i.MX6SLL Linux OS, file /etc/xdg/weston/weston.ini, change start-on-startup to true [screen-share] command=WLOG_APPENDER=file WLOG_FILEAPPENDER_OUTPUT_FILE_NAME=output.log WLOG_FILEAPPENDER_OUTPUT_FILE_PATH=/tmp /usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --no-clients-resize --rdp-tls-cert=/etc/freerdp/keys/server.crt --rdp-tls-key=/etc/freerdp/keys/server.key start-on-startup=true 8> i.MX6SLL Linux OS, run below cmd: mkdir /etc/freerdp mkdir /etc/freerdp/keys /root/imx6sllevk-linux-lib/winpr-makecert -path /etc/freerdp/keys mv /etc/freerdp/keys/imx6sllevk.crt /etc/freerdp/keys/server.crt mv /etc/freerdp/keys/imx6sllevk.key /etc/freerdp/keys/server.key service weston stop service weston start 9>Plug usb network adapter to i.MX6SLL EVK board J10; i.MX6SLL board and PC must in same network, ping without problem. i.MX6SLL Linux OS, there are two process name as "weston", one process is weston rdp backend will share screen to PC. If only one weston process, need check did miss copy any new lib or check libary file name. 10>PC side: wfreerdp.exe /v:IPADDRESS_OF_IMX6SLLEVK There will prompt dialog box for user name and password, just press ESC, then PC side will show i.MX6SLL Linux desktop screen; Click console button of i.MX6SLL Linux OS desktop, within that console input any i.MX6SLL Linux OS cmd, check result of it from PC side. Known issue: wfreerdp.exe is downloaded from https://ci.freerdp.com/job/freerdp-nightly-windows/ If run latest wfreerdp.exe but show nothing of remote desktop, try attached version wfreerdp.exe(3.0.0-dev). Also you can try check log files first: i.MX6SLL Linux OS file /tmp/output.log; PC side generated log file as: wfreerdp.exe /v:IPADDRESS_OF_IMX6SLLEVK /log-level:TRACE > rdp.log Reference: 1>https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat... 2>https://github.com/FreeRDP 3>https://github.com/freedesktop/pixman 4>https://github.com/DLTcollab/sse2neon    
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is the detailed programming aid for the registers associated with DRAM initialization (DDR3 and LPDDR2) of the MX6UL/ULL/ULZ (consolidated RPA). The last work sheet tab in the tool formats the register settings for use with the ARM DS5/RealView debugger. It can be manually converted by the user to a DCD file format used by uboot or other bootloaders (note the removal of debugger specific commands in this tab). The programming aids were developed for internal NXP validation and development boards.   This tool serves as an aid to assist with programming the DDR interface of the MX6UL/ULL/ULZ and is based on the DDR initialization scripts developed by the R&D team and no guarantees are made by this tool.   The following are some general notes regarding this tool: Refer to the "How To Use" tab in the tool as a starting point to use this tool. Note that in the "DStream .ds file" tab there are DS5 debugger specific commands that should be commented out or removed when using the DRAM initialization for non-debugger specific applications (like when porting to bootloaders). This tool may be updated on an as-needed basis for bug fixes or future improvements.  There is no schedule for aforementioned maintenance.  
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. i.MX 8/8X DDR Tools Overview   This page contains the latest releases for the i.MX 8/8X DDR Tools. The tools described on this page cover the following i.MX 8/8X Family SoCs with the System Controller Unit (SCU): i.MX 8QuadMax and its derivatives i.MX 8QuadPlus i.MX 8QuadXPlus and its derivatives i.MX 8DualXPlus and i.MX 8DualX  i.MX 8DXL (i.MX 8XLite) and its derivatives i.MX 8SXL  NOTE: For the i.MX 8M Family of DDR tools please refer to the : i.MX 8M Family DDR Tool Release                           The purpose of the i.MX 8/8X DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.).  This process equips the user to then proceed with the bring-up of a boot loader and an OS.  Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface.     The i.MX 8/8X DDR Tools consist of: DDR Register Programming Aid (RPA) DDR Stress test   For more details regarding these DDR tools and their usage, refer to the MX8X_DDR_Tools_quickstart_guide.pdf attached to this page.   i.MX 8/8X DDR Register Programming Aid (RPA)   The i.MX 8/8X DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization in two formats (in separate Excel worksheet tabs):   DDR Stress Test script: This format is used specifically with the DDR stress test by first copying the contents in this worksheet tab and then pasting it to a text file, naming the document with the “.ds” file extension. The user will select this file when executing the DDR stress test. DCD CFG file: This format is the configuration file used specifically by the SCU Firmware (SCFW). In this scenario, the user copies the contents in this worksheet tab and pastes it to a text file, naming the document with the “.cfg” file extension and placing this file in the appropriate SCFW board file directory.   i.MX 8/8X DDR Register Programming Aid (RPA): Current Versions Note: In all cases, the RPA revision is aligned to a minimum SCFW version as shown in the table below. In some cases, the BSP alignment is provided as extra detail, however, the RPA tool is specifically aligned to a minimum SCFW version and later. To obtain the latest RPAs, please refer to the following links (note, existing RPAs have been removed from this main page and moved to the SoC specific links below): i.MX8QM: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-DDR-Register-Programming-Aid-RPA/ta-p/1166307 i.MX8QXP/QXP/DX: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302 i.MX8DXL/SXL: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8DXL-DDR-Register-Programming-Aid-RPA/ta-p/1602262   Processor Mask Revisions Memory Supported Latest RPA Version * Notes i.MX 8QM B0 LPDDR4 Rev 23*** Rev 22** Rev 21** Rev 20** Rev 19** Rev 23: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev22: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  Rev 21: Fixed 1 DRC operation to comment out calls to VREF training to DRC1 and added DDRC_SCHED register programming to align with latest SCFW programming (refer to RPA revision history for more details). Rev 20: use with SCFW 1.4.0 and NXP BSP GA version L5.4.3_2_0_0 later (to support SW VREF training work around command) Rev 19: use with SCFW 1.3.1 and NXP BSP GA version L5.4.3_1_0_0 i.MX 8QXP C0, B0 LPDDR4 Rev 16*** Rev 15** Rev 14** Rev 13** Rev 16: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 15: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  Rev 14: use with SCFW 1.4.0 and NXP BSP GA version L5.4.3_2_0_0 later (to support SW VREF training work around command) Rev 13: use with SCFW 1.3.1 and NXP BSP GA version L5.4.3_1_0_0 i.MX 8QXP C0, B0 DDR3L Rev 23 Rev 22*** Rev 21 Rev 20 Rev 23:  -Corrected Register Configuration DDR_PHY_PTR4.tDINIT1 bit field programming. Previously, the calculation was based on tRFC only, however, the calculation should have been based on "tRFC+10ns". This was corrected. -Set DDRC_INIT4, DDR3 MR2.ASR=1 as the default setting to allow for the DRAM to select the self refresh rate automatically based on its case temperature (but user has the option to disable via pull-down menu). Also, removed conditional setting for DTCR0.DTRDBITR as it is not needed since DDR3 does not support DBI. Default setting of this was zero and will remain that way. -Provided option to user to select auto refresh rate based on the intended max temperature of the DDR3L device (1X, 2X, 4X). User should confirm with the DDR3L data sheet for supported temperature ranges and associated refresh rate. Rev 22: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 21: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW. -Compatible with SCFW 1.1.10 and later -Changes made to this revision do not affect the DCD CFG file output based on v19 -Issue discovered in the DDR stress test script, wherein certain commands were not being properly configured based on the ECC setting in the Register Configuration worksheet; this was resolved (cells A84, A87, A90, A93 ) -In addition, in both DCD CFG and DDR stress test script worksheets, all commands that depend on ECC config have been updated to include an "OR" with whether or not the data bus is configured for 16-bit (ECC is only supported for full 32-bit data bus width configurations) i.MX 8DualX C0, B0 LPDDR4 Rev 16*** Rev 15* Rev 14** Rev 13** Rev 16: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 15: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  Rev 14: use with SCFW 1.4.0 and NXP BSP GA version L5.4.3_2_0_0 later (to support SW VREF training work around command) Rev 13: use with SCFW 1.3.1 and NXP BSP GA version L5.4.3_1_0_0 i.MX 8DualX C0, B0 DDR3L Rev 21 Rev 20*** Rev 19 Rev 18 Rev 21: -Corrected Register Configuration DDR_PHY_PTR4.tDINIT1 bit field programming. Previously, the calculation was based on tRFC only, however, the calculation should have been based on "tRFC+10ns". This was corrected. -Set DDRC_INIT4, DDR3 MR2.ASR=1 as the default setting to allow for the DRAM to select the self refresh rate automatically based on its case temperature (but user has the option to disable via pull-down menu). Also, removed conditional setting for DTCR0.DTRDBITR as it is not needed since DDR3 does not support DBI. Default setting of this was zero and will remain that way. -Provided option to user to select auto refresh rate based on the intended max temperature of the DDR3L device (1X, 2X, 4X). User should confirm with the DDR3L data sheet for supported temperature ranges and associated refresh rate. Rev 20: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 19: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  -Compatible with SCFW 1.1.10 and later * For a history of the previous versions of an RPA, refer to the Revision History tab of the respective RPA.  ** In general, it is recommended to use the latest RPA tool even with a pre-released BSP as it ensures you are testing with the latest fixes and features. Older versions of the RPA may be provided to support existing/released versions of the BSP.  This only applies to those RPA tools that are compatible with pre-release BSPs but may not be compatible with released versions of the BSP.   ***IMPORTANT: as stated in the table above, for the noted RPA version, it is aligned to SCFWv1.7.0 (and later SCFW versions).  Older versions of the RPA are not aligned to SCFWv1.7.0 (and later SCFW versions).  If trying to use an older version of an RPA with SCFWv1.7.0 (and later SCFW versions), it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QXP/DualX: DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ For MX8QM: DATA 4 0xff148000 0x00000885 /* DRC0 bringup */ DATA 4 0xff1a0000 0x00000885 /* DRC1 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 (and later SCFW versions) (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QXP: [remove] ifndef SCFW_DCD [remove] /* For 1200MHz DDR, DRC 600MHz operation */ [remove] DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ [remove] #else <keep code as is> [remove] #endif Note: when it is stated "SCFWv1.7.0 (and later SCFW versions)", it implies SCFWv1.7.0, 1.7.1, 1.7.2... 1.8.0, 1.9.0, 1.10.0... etc., where "..." are minor versions/patches, so when you see 1.7.2... it implies 1.7.3, 1.7.4, etc.).  Unless otherwise noted, the latest RPA shown in the table above is aligned to the latest SCFW release.    i.MX 8/8X DDR Stress Test    The i.MX 8/8X DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational prior to building the SCFW for use with u-boot and OS bring-up. The DDR stress test uses the .ds DDR stress test script generated from the RPA tool along with a special build of the SCFW, built with option: DDR_CON=ddr_stress_test_parser Or in the case of i.MX 8QuadMax use of one DDR Controller: DDR_CON=ddr_stress_test_parser_DRC0_only The DDR stress test offers a Target option to dictate which SoC is under test. The following are Target options to select from: MX8QM – used to test i.MX 8QuadMax and its derivatives i.MX 8QuadPlus MX8QX – used to test i.MX 8QuadXPlus and its derivatives i.MX 8DualXPlus/DualX MX8DXL – used to test i.MX 8DXL and its derivatives i.MX8 SXL     To install the DDR Stress Test, save and extract the zip file mx8_ddr_stress_test_ERxx_installation.zip   (where 'xx' is the current version number) and follow the on-screen installation instructions. Note, when extracting the DDR Stress Test tool .zip file, it is recommended to perform an "Extract here" operation.  Some systems do not allow for the extracted installation executable to run from another folder and will only work when being executed from the same location as the original, downloaded zip file.  For more details on the DDR stress test usage, refer to the MX8_DDR_Tool_User_Guide found in the DDR Stress Test tool delivery. NOTE: Before using the DDR tools on a new custom board, the user should properly port the SCU Firmware (SCFW) to this new board. The DDR tools will not be able to run without a properly ported and working SCFW.            i.MX 8/8X DDR Stress Test Requirements The tool requires access to the Windows registry, hence users must run it in administrator mode. The tool cannot run on an OEM closed device that requires images signed by the customer When users design new i.MX 8/8X boards, please make sure to follow the rules outlined in the respective Hardware Developers Guide and the MX8_DDR_Tool_User_Guide, which can help users bring up DDR devices on their respective i.MX 8/8X boards.   i.MX 8/8X DDR Stress Test SECO Firmware It is generally not recommended to update the SECO (ahab) firmware that comes default with the DDR Stress Test. This is not recommended because the purpose of the DDR Stress Test is to test the DDR memory interface, not the entire SCFW to SECO firmware operation even though a newer version of the SCFW may complain that the SECO firmware version is not the latest. The SECO firmware version that comes with the DDR Stress Test has been tested and proven to work by the factory before the DDR Stress Test release; updating the SECO firmware to a different version may result in unintended consequences rendering the DDR stress test inoperable. In most cases, it is allowable to update only the SCFW without updating the SECO firmware. Should the user wish to update the SECO firmware version in the DDR Stress Test, then they will need to rename this firmware without the silicon version (for example, if updating the MX8QM SECO firmware, the user will need to rename mx8qmb0-ahab-container.img to mx8qm-ahab-container.img, basically remove the “b0”). The exception is for the MX8QXP, if updating the C0 silicon version SECO firmware, then the user should maintain the C0 nomenclature. If the user finds that the updated SECO firmware causes the DDR Stress Test to become inoperable, then it is recommended to revert to the default SECO firmware version that came with the DDR Stress Test release. i.MX 8/8X DDR Stress Test User Guide The i.MX 8/8X DDR Stress Test tool includes the document: MX8_DDR_Tool_User_Guide.pdf NOTE: Please read the MX8_DDR_Tool_User_Guide inside the package carefully before you use this tool.   DDR Stress Test Revision History   Rev Major Changes (Features) NXP BSP Software Version ER 14 Updated to support parsing of the VREF training command in the DDR Stress Test script This version is aligned with NXP BSP GA version L5.4.3_2_0_0 and later. ER15 - Support for i.MX 8Lite (aka DXL) - Provides more verbose output in event of data training failures, specifically on which byte lanes failed - Aids in debug of board layout issues This version is aligned with NXP BSP GA version Linux 5.15.71_2.2.0 and later.    Related Resources Links: i.MX 8ULP DDR tools: i.MX Software and Development Tools | NXP Semiconductors Scroll down to “Other Resources --> Tools --> DDR Tools” i.MX 8M Family DDR Tool Release  i.MX 6/7 DDR Stress test GUI Tool i.MX 8QM RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-DDR-Register-Programming-Aid-RPA/ta-p/1166307 i.MX 8QXP/DXP/DX RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302 i.MX 8DXL (i.MX 8XLite) RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8DXL-DDR-Register-Programming-Aid-RPA/ta-p/1602262   FAQs: Q. When the DDR stress test is running, it indicates testing region 1 and then region 2. What is region 1 and region 2? A. There are two distinct DDR memory regions in the i.MX8X series which is due to the architecture of Cortex A core and the associated memory map of the i.MX8X. Region 1 is the 32-bit region, starting at 0x080000000 and ending at 0x0FFFFFFFF (2GB total) Region 2 is the 64-bit region (for the Cortex A core architecture), starting at 0x880000000 and ends at the remaining density: • For 4GB total on board density, 2GB for region 1 and 2GB for region 2, so region 2 will end at 0x8FFFFFFFF (0x900000000 minus 1) • For 6GB total (NXP board density), 2GB for region 1 and 4GB for region 2, so region 2 will end at 0x97FFFFFFF (0x980000000 minus 1) • For 8GB total, 2GB for region 1 and 6GB for region 2, so region 2 will end at 0x9FFFFFFFF (0xA00000000 minus 1) Hence there is a “hole” in the memory map between region 1 and region 2. As such, the DDR stress test first tests the lower region (region 1) until it is exhausted (up to 2GB), and if the DDR density exceeds 2GB, the test will test the remaining density in region 2. Q. Do the i.MX8X series SoCs support LPDDR4 memories with 17 row addresses (R[16:0])? A. The i.MX8QM, i.MX8QXP, and i.MX8DXP SoCs and their derivatives cannot support newer 17-row-address LPDDR4 memories. This means, in order to support the maximum 4GB (32Gb) LPDDR4 density, the configuration must be 16-row, 2 rank (as opposed to the unsupported 17-row, 1 rank). The upcoming i.MX8DXL is planned to support 17-row address LPDDR4 devices. Q. I can select a different i.MX8X AP UART port when running the DDR Stress Test? A. It is highly recommended to follow NXP board designs including selecting the same UART ports; this eases the user’s software porting efforts and minimizes issues with needless debugging. The DDR Stress Test requires the use of the USB OTG port and the AP UART port (and it is highly recommended to connect the SCFW UART port for SCFW debug messages). To date, the factory sees no reason why the user would need to select a different AP UART port than what is used on NXP boards. Selecting the same AP UART port ensures a faster bring up of the DDR stress test rather than needlessly debugging why a different UART port is not working. In any event, some wish to use a different UART port for whatever reason, as such, NXP has placed work arounds to allow the selection of a different UART port. To select a different UART port (0,1, or 2), the user simply needs to add the following line to the end of the DDR Stress Test DDR initialization (.ds) script: memory set  0x5C01042C 32   <UART port value> memory set  0x5C01042C 32   0x00000000   # UART0 port selection for AP UART (default) memory set  0x5C01042C 32   0x00000001   # UART1 port selection for AP UART memory set  0x5C01042C 32   0x00000002   # UART2 port selection for AP UART Note that UART ports 0, 1, and 2 have pad names that are default UART pins (IOMUX ALT0 config). To date, the DDR tools do not support other UART ports that are mux’d out on other non-default UART pins. However, there is an exception for i.MX8QXP/DXP and the upcoming i.MX8DXL where UART3 mux’d out on FLEXCAN2 can be used. To select this, add the following to the end of the .ds file: memory set  0x5C01042C 32   0x00000003   # UART3 port selection for AP UART (exception for i.MX8QXP/DXP and i.MX8DXL) Some RPAs do have support built in (via a pull down menu) to select the UART port. For those RPAs that do not have this feature, this is due to the fact that these RPA (NXP boards) were not tested with a different UART port as the board requires cutting traces and re-wiring the UART signals and some boards may not have these UART traces readily available. However, the user is still able to manually add this UART port selection. Refer to the following RPAs to see the UART port select option: MX8QXP DDR3 MX8DXP DDR3 Q. Why does the DDR stress test appear to hang when testing [MX8QM with 8GB (64Gb) or MX8QXP with 4GB (32Gb)] of LPDDR4 memory? A. The issue is not caused by the DDR stress test itself but by the version of the SCFW being used. The default version of the SCFW binary pre-dates a change made by the SCFW to ignore DRAM density limitations when it detects that the DDR stress test is running. This version of the SCFW associated with the DDR stress test ER14 limits the testable DRAM density to [MX8QM: 6GB, MX8QXP: 3GB], as this version of the SCFW is configured to operate on NXP boards as a basis. As noted in the DDR stress test user guide, it is recommended for users to port the latest SCFW to their board first before using the DDR stress test to account for board differences between NXP’s board and their board.  In addition, the user has the following options to enable testing beyond [MX8QM: 6GB, MX8QXP: 3GB]; note it is the responsibility of the user to ensure a properly working, ported version of the SCFW prior to operating the DDR stress test. 1. The latest SCFW should contain an update that sets no density limit if it is detected that the SCFW is built for usage with the DDR Tool - the user can try to get the latest porting kit and build the new firmware.  This is the recommended change. 2. In board.c, function board_system_config(), there is this chunk of code (MX8QM example shown) if using an existing/older SCFW that pre-dates this change: /* Board has 6GB memory so fragment upper region and retain 4GB */         BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL,             0xFFFFFFFFFULL)); User can modify it as follows:     if (ddrtest == SC_FALSE)     {         sc_rm_mr_t mr_temp;         /* Board has 6GB memory so fragment upper region and retain 4GB */         BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL,             0xFFFFFFFFFULL));         BRD_ERR(rm_memreg_free(pt_boot, mr_temp));     } This is disables execution of this section of code if the SCFW is built for the DDR Tool (the same as 1. but needs to be done by the user manually when using an earlier firmware version). 3. Change 0x980000000 to 0xA00000000 in the above chunk of code. That should allow for 8GB density for MX8QM example shown above (for MX8QXP, change 0x8C0000000ULL to 0x900000000ULL for 4GB density).  
查看全文
From Android 12, NXP use GKI(Generl kernel image) instead of NXP's kernel code.  This follow up Android ASOP standard. This article described that when customer use Android 12 and later version, they need to pay attention on GKI development, which is different with previous version.
查看全文
We are pleased to announce that Config Tools for i.MX v13 are now available.
查看全文
Introduction This document intends to describe how to implement workaround for ERR050145 (ISI: Memory overwrite occurring outside of allocated buffer space corrupting system memory) based on Linux BSP. ERR050145 is applicable for i.MX8QM B0, i.MX8QXP B0 series products. qiang_limpu_se_0-1629784287984.png   Software Platform Reference patches stated into this document are developed and validated on L4.14.98_GA2.0.0 release.   Software Workaround As workaround stated, the xRDC can be programmed to grant write access to the ISI only within its allocated frame buffer space, which can prevent the corruption. So under Linux, we can consider to implement workaround like so: Create children partition for ISI and allocate buffers. Then Linux can access these buffers as normal, but ISI can't access other memory out of these buffers, it is limited by xRDC hardware. Considering the xRDC hardware can only support up to 16 memory regions, we may need to consider different workaround implementations for different camera use case scenarios.   For single camera use case, the required camera buffer number is usually less than 16. So “0001-iMX8QM-iMX8QX-ERR050145-ISI-overwrite-workaround.patch” is enough. No modification is needed for camera application in this case.   For multiple camera use case, all patches (0001~0003) are needed. If the camera application used VB2_MEMORY_MMAP memory mode, then no code modification is needed in application. The V4l2 ISI driver can handle everything (Allocate physical continued memory for each camera, and map them as one xRDC memory region for overwrite protect). If the camera application used VB2_MEMORY_USERPTR and VB2_MEMORY_DMABUF memory mode, then it needs allocate camera buffers with physical continued memory for each camera, then the driver will merge them as one xRDC memory region in SCFW.   How to prove workaround take effective? After applying the patches, the ISI will report AXI_WR_ERR due to it failed to write data out of the allocated buffers when the errata happens. To reduce the ISI interrupt, we can also change the ISI interrupt setting as followed: void mxc_isi_enable_irq(struct mxc_isi_dev *mxc_isi) {     u32 val;     val = CHNL_IER_FRM_RCVD_EN_MASK |         CHNL_IER_EXCS_OFLW_V_BUF_EN_MASK |         CHNL_IER_EXCS_OFLW_U_BUF_EN_MASK |         CHNL_IER_EXCS_OFLW_Y_BUF_EN_MASK;     writel(val, mxc_isi->regs + CHNL_IER); }   Add reference patch for L5.4.70_2.3.0 and L5.10.72_2.2.0.
查看全文
PCIE IP on i.MX8MM and i.MX8MP is same, customer can follow PCIE test Application note to do compliance test, if eye diagram failed, they can fine turn corresponding regs below: iMX8MMRM.pdf IMX8MPRM.pdf GEN1: Lambert_0-1671368933859.png   Lambert_1-1671368933876.png     Lambert_2-1671368933881.png   Lambert_3-1671368933900.png     GEN2: Lambert_4-1671368933905.png   Lambert_5-1671368933910.png     Lambert_6-1671368933914.png   Lambert_7-1671368933922.png         Related code in kernel Phy-fsl-imx8-pcie.c (kernel-source\drivers\phy\freescale)    3794      2020/11/4 static int imx8_pcie_phy_init(struct phy *phy) { ……          /* Configure TX drive level  */        writel(0x2d, imx8_phy->base + 0x404);          return 0; }   Thanks Lambert
查看全文
i.MX8 series contains internal HiFi4 DSP. It is targeted for Audio related signal processing. SOF (Sound Open Firmware) is open source audio DSP firmware, driver and SDK. This document introduces basic theory about IIR/FIR digital filters, how to design IIR/FIR digital filters and the Equalizer filters implementation by SOF. After that, the document also describes how HiFi4 DSP MAC engine accelerate the EQ filters calculation.
查看全文
1. Description: On the i.MX Android camera HAL, It only supports YUYV sensor, regardless of whether the sensor is connected to ISP or ISI. Some users want to customize the sensor format, such as UYVY or raw, they need a guide to do this, this document intends to describe how to implement raw camera sensor on i.MX8MP android, and output raw data. Note: Base on  i.MX 8M plus, Android12_1.0.0.  2. Camera HAL Android's camera hardware abstraction layer (HAL) connects the higher level camera framework APIs in android.hardware.camera2 to your underlying camera driver and hardware. For more detail information, please refer to AOSP document: https://source.android.google.cn/docs/core/camera/camera3_requests_hal?hl=en while on I.MX camera HAL, the camera subsystem can be divided into several parts: TonyLiao_suzhou_0-1669960499301.png   Camera framework:  frameworks\av\camera Camera service:    frameworks\av\services\camera\libcameraservice\ Camera provider: hardware/interfaces/camera/provider/ hardware/google/camera/common/hal/hidl_service/               hidl_service dlopen the camera HAL3. Camera HAL3:   vendor\nxp-opensource\imx\camera\ Camera driver:   vendor/nxp-opensource/kernel_imx/drivers/media/i2c  It's callstack can be list as follow:  TonyLiao_suzhou_1-1669960725413.png TonyLiao_suzhou_2-1669960738653.png There are 2 streams on pipeline, preview stream need 3 buffers and capture stream need 2 buffers: CameraDeviceSessionHwlImpl: ConfigurePipeline, stream 0: id 0, type 0, res 2592x1944, format 0x21, usage 0x3, space 0x8c20000, rot 0, is_phy 0, phy_id 0, size 8388608 CameraDeviceSessionHwlImpl: ConfigurePipeline create capture stream CameraDeviceSessionHwlImpl: ConfigurePipeline, stream 1: id 1, type 0, res 1024x768, format 0x22, usage 0x100, space 0x0, rot 0, is_phy 0, phy_id 0, size 0 CameraDeviceSessionHwlImpl: ConfigurePipeline create preview stream You can use this command to dump the stream input/output: "setprop vendor.rw.camera.test 1" to dump steam 0. "setprop vendor.rw.camera.test 2" to dump steam 1. Before you implement the command, you need to run “su; setenforce 0” to close the SeLinux, the data is dumped as "/data/x-src.data", "/data/x-dst.data", where "x" is the stream id as "0, "1,", "2", ...   Preview Stream Capture Stream ID 1 0 Resolution 1024*768 2592*1944 Format HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED (34) HAL_PIXEL_FORMAT_BLOB (33) Usage 0x900 GRALLOC_USAGE_HW_TEXTURE      (0x100) GRALLOC_USAGE_HW_COMPOSER  (0x800) 0x3 GRALLOC_USAGE_SW_READ_OFTEN Data space 0 HAL_DATASPACE_V0_JFIF  The following usage will be added by framework to distinguish preview and video:GRALLOC_USAGE_HW_VIDEO_ENCODER 3. Raw support  3.1 system modification  The default image for i.MX 8M Plus EVK supports basler + basler and the cameras can work after the image is flashed and boot up, it’s camera with ISP, but we need ISI to process raw. You should refer to Android_User’s_Guide.pdf, you need find the correct version, as Android12_2.0.0 is different with Android12_1.0.0. To make cameras work with Non-default images, execute the following additional commands: Only OV5640 (CSI1) on host: TonyLiao_suzhou_3-1669960978453.png As we use OV2775 which support 1920*1080, unpacked raw12, the json file: TonyLiao_suzhou_4-1669961020578.png 3.2 DTB modification  1. Firstly, change the BoardConfig.mk to generate dtbo-imx8mp-ov2775.img device\nxp\imx8m\evk_8mp\BoardConfig.mk: TARGET_BOARD_DTS_CONFIG += imx8mp-ov2775:imx8mp-evk-ov2775.dtb 2.  Secondly, add imx8mp-evk-ov2775.dts to vendor\nxp-opensource\kernel_imx\arch\arm64\boot\dts\freescale 3. Change imx8mp-evk-ov2775.dts, connect OV2775 to ISI: &isi_0 { status = "okay"; }; &isp_0 { status = "disabled"; }; &dewarp { status = "disabled"; }; 4. Build dtbo image and flash it to board: ./imx-make.sh dtboimage -j4 fastboot flash dtbo dtbo.img  3.3 Sensor driver modification  I use the OV2775 driver from the isp side, be careful that all the function such as g_frame_interval and enum_frame_size should be implemented, or the HAL will get wrong parameters and return error. static struct v4l2_subdev_video_ops ov2775_subdev_video_ops = { .g_frame_interval = ov2775_g_frame_interval, .s_frame_interval = ov2775_s_frame_interval, .s_stream = ov2775_s_stream, }; static const struct v4l2_subdev_pad_ops ov2775_subdev_pad_ops = { .enum_mbus_code = ov2775_enum_mbus_code, .set_fmt = ov2775_set_fmt, .get_fmt = ov2775_get_fmt, .enum_frame_size = ov2775_enum_frame_size, .enum_frame_interval = ov2775_enum_frame_interval, };  3.4 ISI driver modification  We need to add raw format on ISI driver: }, { .name = "RAW12 (SBGGR12)", .fourcc = V4L2_PIX_FMT_SBGGR12, .depth = { 16 }, .color = MXC_ISI_OUT_FMT_RAW12, .memplanes = 1, .colplanes = 1, .mbus_code = MEDIA_BUS_FMT_SBGGR12_1X12, }, { .name = "RAW10 (SGRBG10)", .fourcc = V4L2_PIX_FMT_SGRBG10, .depth = { 16 }, .color = MXC_ISI_OUT_FMT_RAW10, .memplanes = 1, .colplanes = 1, .mbus_code = MEDIA_BUS_FMT_SGRBG10_1X10, } 3.5 Camera HAL modification As there are preview stream and capture stream on the pipeline. GPU does not support raw format, it will print error log when application set raw format:    02-10 18:49:02.162 436 436 E NxpAllocatorHal: convertToMemDescriptor Unsupported fomat PixelFormat::RAW10 02-10 18:49:02.163 2390 2445 E GraphicBufferAllocator: Failed to allocate (1920 x 1080) layerCount 1 format 37 usage 20303: 7 02-10 18:49:02.163 2390 2445 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) dequeueBuffer: createGraphicBuffer failed 02-10 18:49:02.163 2390 2405 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) requestBuffer: slot 0 is not owned by the producer (state = FREE) 02-10 18:49:02.163 2148 2423 E Surface : dequeueBuffer: IGraphicBufferProducer::requestBuffer failed: -22 02-10 18:49:02.163 2390 2445 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) cancelBuffer: slot 0 is not owned by the producer (state = FREE) 02-10 18:49:02.164 2148 2423 E Camera3-OutputStream: getBufferLockedCommon: Stream 1: Can't dequeue next output buffer: Invalid argument (-22)   Modifying the gpu code is not recommended. When preview stream, it's pixel format is fixed to HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED, it needs YUYV format, in this patch, we don't convert raw12 to yuyv, just copy the buffer from input to output, so the preview stream is raw12 actually. When capture stream, we use the Blob format, which usually used for JPEG format. when we find the format is Blob pass down by application, camera HAL will copy the buffer from input to output directly. You can check the detail on function ProcessCapturedBuffer(),    4. Application and Tool 4.1 Application  The test application on the attachment “android-Camera2Basic-master_application.7z”, It's basically a common camera application, it set the capture stream format to blob:  Size largest = Collections.max( Arrays.asList(map.getOutputSizes(ImageFormat.JPEG)), new CompareSizesByArea()); mImageReader = ImageReader.newInstance(largest.getWidth(), largest.getHeight(), ImageFormat.JPEG, /*maxImages*/2); 4.2 Tool We use 7yuv tool to check the raw12 format, which is captured by applicable or dump by HAL, you need set the parameter on the right side:   TonyLiao_suzhou_5-1669966390009.png ImageJ tool also can be used to review raw format.
查看全文