Enable WIFI on Ubuntu 22.04 and Linux BSPs in iMX8 Family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable WIFI on Ubuntu 22.04 and Linux BSPs in iMX8 Family

Enable WIFI on Ubuntu 22.04 and Linux BSPs in iMX8 Family

Installing the new release (Ubuntu 22.04) was detected some NXP boards as iMX8MNEVK, iMX8MM-EVK, iMX8MP-EVK and iMX8ULP-EVK had an issue with the WIFI
module that basically it does not initialize at boot.

Remember, the supported WIFI modules in Ubuntu 22.04 in the EVKs are the following:


      • NXP 88W8987
      • NXP 88W9098
      • NXP 88W8997
      • NXP IW416
      • NXP 88W8801
      • NXP IW612

To initialize the WIFI module of NXP EVKs in Ubuntu 22.04 you can set the following
command in console:

 

sudo modprobe moal mod_para=nxp/wifi_mod_para.conf

 

That command find the correct driver for our WIFI module and then initialize it, but this
only works when Ubuntu is working and if you reset the EVK you need to set the command
again.

 

The definitive solution is create a custom startup script as a service:

 

Step 1: Go to etc/systemd/system

 

cd etc/systemd/system

 

Step 2: In this directory create a new file with the name of your preference but the
extension must be .service.

You can do it with nano or vim:

sudo nano 

or

sudo vim

 

The file must contain:

[Unit]
Description=”Wifi Start”
[Service]
ExecStart=sudo modprobe moal mod_para=nxp/wifi_mod_para.conf
[Install]
WantedBy=multi-user.target

 

Now save the file, in my case the name was wifi_start.service.

 

Step 3: Now we need to enable the script in the startup/boot sequence following the
command:

sudo systemctl enable wifi_start.service

 

Remember in wifi_start.service is the name as you saved your file.

 

Finally, each time you boot your board, the WIFI module will initialize automatically.

 

Boards tested:
iMX8MN (With WIFI module NXP 88W8987)
iMX8MM (With WIFI module NXP 88W8987)
iMX8MP (With WIFI module NXP 88W8997)
iMX8ULP (With WIFI module NXP IW416)

 

添付
コメント

Hi everyone,

I'm having issues in with the 8MNANOD4-EVK and the v6.1.1 Linux Distro version. I go through module activation with:

 

modprobe moal mod_para=nxp/wifi_mod_para.conf

After this, dmesg show:

Screenshot from 2023-06-19 17-00-56.png

Seems driver exists but its not  as verbose as i would like. Unfortunately, interface its not appearing

Screenshot from 2023-06-19 17-03-16.png

I tried to set the wifi network credentials in wpa_supplicant.conf and then updated with the command

wpa_supplicant -B -i wlan0 -c /etc/wpa_supplicant.conf -D nl80211

But seems not to brings up the interface

arrivederccimamasita_0-1687187229653.png

 

I tried this process with full and multimedia image in the application images provided. I also try v5-15.71 and v5.10.52, same results as above.

Someone have any idea what could be happening? Thanks!

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎06-07-2023 06:50 AM
更新者: