i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
The HSM Coding-Signing is new. When we follow the instructions in Code-Signing Tool User’s Guide , still has something to overcome, most of them are related to the OS. Actually, Code-Signing Tool User’s Guide  can not give detail every “obvious” step. The purpose of this document is to share the experiences on my system. Hope those experience can give you some clues on your system.     25JUL2024 - add pkcs11 proxy                         HSM Code-Signing Journey_25JUL2024.pdf                          HSM Code-Signing Journey_25JUL2024.txt  
記事全体を表示
i.MX93 eMMC Secondary Boot          i.MX93 eMMC Secondary Boot.zip   i.MX8MP eMMC Secondary Boot           i.MX8MP eMMC Secondary Boot.zip i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011   i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45    i.MX6 SDCARD Secondary Boot Demo           i.MX6_SDCARD_Secondary_Boot_Demo.pdf      
記事全体を表示
1 - Introduction: The Ultra Secured Digital Host Controller (uSDHC) provides the interface between the host processor and the SD/SDIO/MMC cards. Most recent versions provides the ability to automatically select a quantized delay (in fractions of the clock period) regardless of on-chip variations such as process, voltage, and temperature (PVT). The auto tuning is performed during runtime at hardware level, no software enablement is needed to drive this feature. 2 - Failure description: SDIO cards can implement an optional feature that uses DATA[1] to signal the card's interrupt to the i.MX device, this feature can be enabled by the SDIO card device and does not depends on i.MX uSDHC driver configuration. NXP Linux BSP is enabling the auto tuning for high SDIO frequencies (SDR104 and SDR50). Out of reset uSDHC_VEND_SPEC2 register is configured to use DATA[3:0] for calibration, this setup can conflict with the SDIO interrupt as DATA[1] signal can be asserted asynchronously. SDIO failures can be observed when running SDIO applications that requires high usage of the SDIO interface (e.g Download of large files), SDIO controller cannot return an accurate DLL causing failures such as "CMD53 read error". Failure can be observed on i.MX8MM EVK and i.MX8MN EVK boards, both devices are running 88w8987 Wi-Fi chipset at 208Mhz (SDR104). Users can observe an SDIO crash followed by error message below at Linux Kernel level. [ 401.945627] cmd53 read error=-84 [ 401.974677] moal_read_data_sync: read registers failed 3 - Impacted devices: The following devices are impacted by this limitation. - i.MX6 Family:   i.MX6SL, i.MX6SLL, i.MX6SX, i.MX6UL, i.MX6ULZ and i.MX6ULL. - All i.MX7 and i.MX7ULP family:   i.MX7D, i.MX7S and i.MX7ULP. - All i.MX8M Family:   i.MX8MQuad, i.MX8M Mini, i.MX8M Nano, i.MX8M Nano UL and i.MX8M Plus. - All i.MX8/8X Family:   i.MX8DQXP, i.MX8DX and i.MX8QM. NXP Linux BSP is enabling the auto tuning for SDR104 and SDR50 modes. Other operation modes are not impacted by this limitation. Users can poll uSDHCx_CLK_TUNE_CTRL_STATUS register when running SDIO applications to confirm. TAP_SEL_PRE field is updated automatically during run time and constant variations can point to an incorrect delay cell calculated by the uSDHC controller.   All NXP Wi-Fi chipsets are enabling SDIO interrupt during firmware load, failures can be observed with any Wi-Fi vendor enabling SDIO asynchronous interrupt. 4 - Software changes: Recommendation is to enable auto tuning for DATA[0] and CMD signals only, DATA[1] should not be used for auto calibration to avoid a possible conflict with SDIO interrupt. This setup can only be used if SDIO interface length are well matched. Software patches can be found at codeaurora.org. Fix is already included in L5.10.52-2.1.0 BSP, users can add fsl,sdio-interrupt-enabled property to uSDHC device tree node to enable SW workaround. https://github.com/nxp-imx/linux-imx/commit/3b3d6dec05277f7786d813592a31ea4a1ce60a74 https://github.com/nxp-imx/linux-imx/commit/b9b5a43df1d709809b2b654ad8f8181b00a4ee55 https://github.com/nxp-imx/linux-imx/commit/95a846af9f82dc6ea60064d9d12d5d2378e23941      
記事全体を表示
We are pleased to announce that Config Tools for i.MX v16.0 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) The product is based on Eclipse 2023-12 Framework – Enable the Peripherals tool in the Config Tools for i.MX – Enable the Clocks tool in the Config Tools for i.MX – A new command-line argument (- UpdateCode) has been added. It performs the same action as the Update Code button in the user interface. It must be used with -HeadlessTool. DDR tool – CA bus driver strength and ODT configuration for the mScale processors are added. – [MX 93/MX 91] The UART configuration from UI is added. – MX 91 DDR tool update for Config tools – MX 93 PF 09 DDR tool support is added. SerDes tool – MX 95 SerDes tool support is enabled. Pins tool – Simultaneous routing detection (routing of one signal may result in multiple signals being routed based on the same register settings) is added. In that case, such signals are offered to be added into the configuration. – Support of internal pins that are not available in the package is added.
記事全体を表示
Hello! In this time, we will look how the i.MX93 GPIOs IRQs works, also I will focus on Cortex M33 side with SDK 2_16_0 but also tested on 2_15.   We can see in this other post, how the i.MX8M family works, but for i.MX93 this is a little different because there are a Secure/Non-Secure options and Privilege/Non-Privilege.   According to reference Manual and SDK LED example, we must to set the PCNS and ICNS registers to 0x00 to set in Secure access.    Materials Used: i.MX93EVK Jumper cable to connect GPIO2_IO02 with GPIO2_IO03 SDK 2_16_0 from MCUXpresso SDK Builder Source power for i.MX93EVK USB C Cable for serial debug USB C Cable to transfer .bin ro EVK   The Cortex-M33 processor supports Secure and Non-secure security states, Thread and Handler operating modes, and can run in either Thumb or Debug operating states. In addition, the processor can limit or exclude access to some resources by executing code in privileged or unprivileged mode. Code can execute as privileged or unprivileged. Unprivileged execution limits or excludes access to some resources appropriate to the current security state. Privileged execution has access to all resources available to the security state. Handler mode is always privileged. Thread mode can be privileged or unprivileged. You can find this information in the ARM documentation.   To resume this post, we will focus just in the necessary registers to configure properly a GPIO as IRQ input.   On this example, we will take the i.MX93EVK board. The GPIO2_IO02 will be configured as an output and the GPIO2_IO03 will be configured as an input with Rising edge IRQ. On each GPIO2_IO02 Rising edge, the software will detect an IRQ.     At first, we need to configure our IOMUX: void BOARD_InitPins(void) { IOMUXC_SetPinMux(IOMUXC_PAD_GPIO_IO02__GPIO2_IO02, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_GPIO_IO03__GPIO2_IO03, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_UART2_RXD__LPUART2_RX, 0U); IOMUXC_SetPinMux(IOMUXC_PAD_UART2_TXD__LPUART2_TX, 0U); IOMUXC_SetPinConfig(IOMUXC_PAD_GPIO_IO02__GPIO2_IO02, IOMUXC_PAD_DSE(15U) | IOMUXC_PAD_FSEL1(2U) | IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_GPIO_IO03__GPIO2_IO03, IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_UART2_RXD__LPUART2_RX, IOMUXC_PAD_PD_MASK); IOMUXC_SetPinConfig(IOMUXC_PAD_UART2_TXD__LPUART2_TX, IOMUXC_PAD_DSE(15U)); }   Then, we can start to code. Using as an starting point we can use the SDK/boards/mcimx93evk/driver_examples/rgpio/led_output example. Our definitions (PIN_OUT_RGPIO and PIN_IN_RGPIO are the same GPIO2 but it is just for good practice):😞 /******************************************************************************* * Definitions ******************************************************************************/ #define PIN_OUT_RGPIO GPIO2 #define PIN_IN_RGPIO GPIO2 #define PIN_OUT_RGPIO_PIN 2U #define PIN_IN_RGPIO_PIN 3U   Then, our IRQ handler: void Reserved73_IRQHandler(void) { RGPIO_ClearPinsInterruptFlags(PIN_IN_RGPIO, kRGPIO_InterruptOutput0, 1U << PIN_IN_RGPIO_PIN); PRINTF("\r\n IRQ.........\r\n"); SDK_ISR_EXIT_BARRIER; }   Why Reserved73_IRQHandler? That is the correspondent for GPIO2, you can look this on SDK/devices/MIMX9352/gcc in the file called startup_MIMX9352_cm33.S:   Basically, the interruption will clear the IRQ flag and print a little message.   Now, here we have the complete main function, we will break down the most important points. int main(void) { /* Define the init structure for the output pin*/ rgpio_pin_config_t pin_out_config = { kRGPIO_DigitalOutput, 0, }; rgpio_pin_config_t pin_in_config = { kRGPIO_DigitalInput, 0, }; /* Board pin, clock, debug console init */ /* clang-format off */ const clock_root_config_t rgpioClkCfg = { .clockOff = false, .mux = 0, // 24Mhz Mcore root buswake clock .div = 1 }; /* clang-format on */ BOARD_InitBootPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); CLOCK_SetRootClock(EXAMPLE_RGPIO_CLOCK_ROOT, &rgpioClkCfg); CLOCK_EnableClock(EXAMPLE_RGPIO_CLOCK_GATE); CLOCK_EnableClock(kCLOCK_Gpio2); /* Set PCNS register value to 0x0 to prepare the RGPIO initialization */ PIN_OUT_RGPIO->PCNS = 0x0; PIN_IN_RGPIO->ICNS = 0x0; /* Print a note to terminal. */ PRINTF("\r\n RGPIO Driver example\r\n"); PRINTF("\r\n An IRQ will happen each GPIO2_IO02 Rising edge\r\n"); /* Init output PIN GPIO. */ RGPIO_PinInit(PIN_OUT_RGPIO, PIN_OUT_RGPIO_PIN, &pin_out_config); /* Init Input with IRQ Pin GPIO*/ RGPIO_SetPinInterruptConfig(PIN_IN_RGPIO, PIN_IN_RGPIO_PIN, kRGPIO_InterruptOutput0, kRGPIO_InterruptRisingEdge); EnableIRQ(GPIO2_0_IRQn); RGPIO_PinInit(PIN_IN_RGPIO, PIN_IN_RGPIO_PIN, &pin_in_config); while (1) { SDK_DelayAtLeastUs(1000000U, SystemCoreClock); RGPIO_PortToggle(PIN_OUT_RGPIO, 1u << PIN_OUT_RGPIO_PIN); } }   As we can see, we need set the GPIO2 PCNS register to 0x00:   Pin Control Nonsecure (PCNS) Configures secure or nonsecure access protection for each pin. You can write to this register only in the Secure-Privilege state if it is not locked (LOCK[PCNS] = 0).   Also the ICNS register to 0x00.   Interrupt Control Nonsecure (ICNS) Configures secure and nonsecure access protection for each interrupt, or DMA request. You can update this register only in the Secure-Privilege state if it is not locked (LOCK[ICNS] = 0).   Now, we can compile and run the example. On each GPIO2_IO02 Rising edge, the CM33 will detect an IRQ in GPIO2_IO03 (short those pads as showed in the image at first of the post).     I will attach the full .c file.   I hope this information can helps to everyone.   Best regards, --... ...-- Salas.
記事全体を表示
This document is about to build an image by Yocto , and it will disable a function that normal user can’t use command line of “ su ”.
記事全体を表示
The purpose of this document is to provide a guide on how to export new symbols using the Bazel Android server instead of the build_abi.sh script. For a better reference how to build Android i.MX image please look at the next chapter 3 Building the Android Platform for i.MX in the Android User's Guide 1. Compile full AOSP or only kernel Build full AOSP: $ source build/envsetup.sh $ lunch evk_8mp-eng $ ./imx-make.sh -j8  Only build the kernel: $ ./imx-make.sh kernel -j8 2. Generic Kernel Image GKI Development Download GKI outside of android_build (MY_ANDROID). # Make sure MY_ANDROID is set to the android_build folder. $ export MY_ANDROID=`pwd` # mkdir gki && cd gki (Make sure folder gki is not inside of ${MY_ANDROID}) $ repo init -u https://android.googlesource.com/kernel/manifest -b common-android14-6.1 $ repo sync $ cd common 3. Export New Symbols Switch the kernel in this common folder from AOSP to its device, and apply the patches required for your project. In this case Android $ cd common $ git remote add device https://github.com/nxp-imx/linux-imx.git $ git remote update $ git fetch device --tags $ git checkout android-14.0.0_1.2.0 $ cd .. $ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam $ ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex $ BUILD_FOR_GKI=yes BUILD_CONFIG=common/build.config.imx $ EXT_MODULES_MAKEFILE="verisilicon_sw_isp_vvcam/vvcam/v4l2/Kbuild" $ EXT_MODULES="nxp-mwifiex/mxm_wifiex/wlan_src" Note: Be sure that your Symbolic Link is pointing to the correct folder Open the Makefile in the following path ../gki/nxp-mwifiex/mxm_wifiex/wlan_src/ and erase some ifreq lines that will generate a No such file or directory error. #Automatically determine Android version from build information to streamline diff --git a/mxm_wifiex/wlan_src/Makefile b/mxm_wifiex/wlan_src/Makefile index 3ec5308..7b6ca47 100644 --- a/mxm_wifiex/wlan_src/Makefile +++ b/mxm_wifiex/wlan_src/Makefile @@ -139,20 +139,7 @@ CONFIG_ANDROID_KERNEL=y ifeq ($(ANDROID_PRODUCT_OUT),1) ccflags-y += -DANDROID_SDK_VERSION=$(ANDROID_SDK_VERSION) else -include $(ANDROID_BUILD_TOP)/build/make/core/build_id.mk -ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),R) - ccflags-y += -DANDROID_SDK_VERSION=30 -else ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),S) - ccflags-y += -DANDROID_SDK_VERSION=31 -else ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),T) - ccflags-y += -DANDROID_SDK_VERSION=33 -else ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),U) - ccflags-y += -DANDROID_SDK_VERSION=34 -else - # Default optimization or actions - ANDROID_SDK_VERSION := 0 - ccflags-y += -DANDROID_SDK_VERSION -endif +ccflags-y += -DANDROID_SDK_VERSION=34 endif endif endif -- Then you could update the symbol list by typing the following command. $ tools/bazel run //common:imx_abi_update_symbol_list After the build process is successful, you should get an output like the image below. Build GKI locally. $ tools/bazel run //common:kernel_aarch64_dist  You could follow the next chapters to update the GKI image to your boot image.
記事全体を表示
Preface With i.MX android, it is often infeasible to directly build an OTA package with a newer android version and apply that OTA package to a device running old version of Android. For example, the OTA package buit with i.MX android-13.0.0_2.0.0 release for evk_8mm cannot be direclty applied on the evk_8mm board running the image built with i.MX android-11.0.0_1.0.0. In this article, the reason why directly cross-version OTA is infeasible in i.mx android is firstly explained. Then what should be takein into consideration and done before cross-version OTA are described.   The way Google update the system for its device Once Google first time releases a device, it is called a "launch device". it has: codename. Take pixel 3a xl as an example, the codename is bonito Android version. For pixel 3a xl, it's Android 9.0 kernel version. For pixel 3a xl, it's 4.9 PRODUCT_SHIPPING_API_LEVEL. For pixel 3a xl, it is set to be 28, the same as the SDK version of that Android version. FCM target level. For pixel 3a xl, it's 3 After the system code is updated to a new version, an OTA package can be built with the lunch target aosp_bonito-user or aosp_bonito-userdebug for pixel 3a xl, let's call the updated device "retrofit device" codename is not changed. its device configuration still can be found in "device/google/bonito/" Android version. it is the version the OTA updated to. Four android versions are supported, here they are android 9, 10, 11, 12, which means pixel 3a xl can at most upgraded to android12. "device/google/bonito/" is introduced in android9, and removed in android13. kernel version. not changed after OTA PRODUCT_SHIPPING_API_LEVEL. Not changed in OTA, so after the OTA, the value of property "ro.product.first_api_level" is different from the SDK version. FCM target level. not changed after OTA. The FCM target level is in the device manifest.xml, corresponds to a specific version of system compatibility.matrix.xml, so HALs provided by this device does not need to have much changes if the FCM target level is not changed. This is the way Google maintains the system for their devices. This is not the way i.MX Android devices are maintained. The way i.MX Android update the system to a new version for maintained device when the code is upaded to a new version for maintained imx devices, all the device are taken as "launch device", so compaired to the previous version, in the new system for the device: the kernel version is changed PRODUCT_SHIPPING_API_LEVEL is changed FCM target level is changed. Physical partitions may also be changed The FCM target level change means there may be some big changes in the HALs provided by this device. The PRODUCT_SHIPPING_API_LEVEL change means quite many code logic based on the property "ro.product.first_api_level" execute in different flow. Fro the partition changes, the OTA package directly build with this updated code often cannot be applied, for example, a new image for the new partition cannot be applied on the board running old system, as it does not have the partition for the image. Things cannot be changed during OTA To make things more clear that why direct cross-version OTA is infeasible, it is necessary to know that there are things cannot be changed during OTA. 1. physical partitions cannot be changed during OTA. related features are: * dynamic partition * gki * boot header version 2. user data on theuserdata partition should not be changed, or data loss may occur during OTA. the related features are: * encryption options encryption options should not be changed, to make new version of android can recognize the data encrypted by the old version of android. For some  fs_mgr encrypt options, the product_shipping_api_level impacts on the final encryption parameters passed to the kernel. take a look at the following code, even with the same fs_mgr encryption option, if the first_api_level is different, the final encryption parameter is different in different android version. android10 system/extras/libfscrypt/fscrypt.cpp if (filenames_encryption_mode == FS_ENCRYPTION_MODE_AES_256_CTS) { // Use legacy padding with our original filenames encryption mode. return FS_POLICY_FLAGS_PAD_4; } else if (filenames_encryption_mode == FS_ENCRYPTION_MODE_ADIANTUM) { // ...snip... return (FS_POLICY_FLAGS_PAD_16 | FS_POLICY_FLAG_DIRECT_KEY); } // ...snip... return FS_POLICY_FLAGS_PAD_16; android11 system/extras/libfscrypt/fscrypt.cpp if (!is_gki && options->version == 1 && options->filenames_mode == FSCRYPT_MODE_AES_256_CTS) { options->flags |= FSCRYPT_POLICY_FLAGS_PAD_4; } else { options->flags |= FSCRYPT_POLICY_FLAGS_PAD_16; } android12 system/extras/libfscrypt/fscrypt.cpp if (first_api_level <= __ANDROID_API_Q__ && options->version == 1 && options->filenames_mode == FSCRYPT_MODE_AES_256_CTS) { options->flags |= FSCRYPT_POLICY_FLAGS_PAD_4; } else { options->flags |= FSCRYPT_POLICY_FLAGS_PAD_16; }  The fscrypt version will also impact the result. If not sepcified, the default "version" would be "v1" if the "product_shipping_api_level <= 29" or the default "version" would be "v2". Some fscrypt functions like "casefold" and "project id" will depend on fscrypt "v2", these functions are enabled by including the "$(call inherit-product, $(SRC_TARGET_DIR)/product/emulated_storage.mk)" in "device/nxp". The "emulated_storage.mk" must not be included if fscrypt "v1" is used.  * the userdata partition filesystem type ext4 (used before i.mx android 13.0.0) f2fs (used from i.mx android 13.0.0) * The filesystem for the emulated storage on the userdata partition sdcardfs fuse 3. The boot control info in misc partition should be able to be recognized before and after OTA related feature is: * bootcontrol HAL 4. The bootargs passed by u-boot to kernel cannot be changed if the bootloader is not updated The related feature is: * bootconfig is used to pass boot args from android12.0.0_1.0.0. used with vendor boot header v4.   it should be known that if dual bootloader of postinstall is used, bootloader can be updated.   For these related features. Google does not implement or change them for a "retrofit device", just imlement for change the features for a "launch device", makes direct cross-version OTA feasible for them, because things cannot be changed during OTA are the same between different android versions. For i.mx android, to implement new features for all maintaied devices, things can be changed during OTA are often changed when update to a new version of android. which makes direct cross-version OTA infeasible.    For the ease of reference, list some feature change history here: * physical partition change history   P9.0.0_2.3.0 10.0.0_1.0.0 10.0.0_2.0.0 11.0.0_1.0.0 12.0.0_1.0.0 12.1.0_1.0.0 13.0.0_1.0.0 14.0.0_1.0.0 bootloader_a/b 4MB 4MB 4MB 4MB 4MB 16MB 16MB 16MB dtbo_a/b 4MB 4MB 4MB 4MB 4MB 4MB 4MB 4MB boot_a/b 48MB 48MB 64MB 64MB 64MB 64MB 64MB 64MB init_boot_a/b - -   -   - 8MB 8MB vendor_boot_a/b - -   64MB 64MB 64MB 64MB 64MB misc 4MB 4MB 4MB 4MB 4MB 4MB 4MB 4MB metadata 2MB 2MB 2MB 2MB 16MB 16MB 64MB 64MB presistdata 1MB 1MB 1MB 1MB 1MB 1MB 1MB 1MB super - - 7168MB 3584MB 4096MB 4096MB 4096MB 4096MB fbmisc 1MB 1MB 1MB 1MB 1MB 1MB 1MB 1MB vbmeta_a/b 1MB 1MB 1mb 1MB 1MB 1MB 1MB 1MB system_a/b 2560MB 1536MB - -   - - - vendor_a/b 256MB 512MB - -   - - - product_a/b - 1792MB - -   - - -   boot_a/b: 48MB → 64MB, Image becames bigger ater enabling some debug options vendor_boot_a/b: boot header v3. Vendor boot and boot header v3 are MUST to enable GKI feature.  init_boot_a/b: The init binary in ramdisk is moved from boot.img to init_boot.img. flash gki image from Google does not impact on the vendor modifications on init.   for the metadata partition: 2MB → 16MB, requirement of vts "-m vts_gsi_boot_test -t MetadataPartition#MinimumSize" 16MB → 64MB, to make the partition be formated as f2fs, 32MB is not enough, 64MB is used. metadata partition was firstly mounted in android11, when enable the user data checkpoint feature * gki feature history Firstly introduced in android11. Some codes are built into modules, put the modules in vendor_boot_a/b partition. vendor_boot_a/b partitions are also firstly introduced in android11 GKI prebuilt binary was integrated from android12   The way to handle cross-version OTA for i.mx android Here are the steps align the partitions within the OTA base code and the OTA target code if the product may be in the development stage, and the OTA base  code can be modified: reserve partitions in OTA base code. for example, OTA from 10 to 11, reserver the vendor_boot partition in android10 partitiont able although there is not vendor_boot.img. change the selinux rules to have update_engine to be able to update this partition. enlarge some partitions in the OTA base code as in the OTA target code. for examples, the bootloader partitions is 16MB in android13. if OTA from android12 to android13 and the android 12 code can be modified, enlarge the bootloader partition to 16MB. as data in userdata and metadata partition is not touched during OTA, modify the mount options of userdata and metadata partitions in OTA target code to be the same as the one in OTA base code. if the product partitions are already shipped, only the OTA target code can be modified:  as data in userdata and metadata partition is not touched during OTA, modify the mount options of userdata and metadata partitions in OTA target code to be the same as the one in the OTA base code. change the partition size to align with the OTA base code partitions like vendor_boot and/or init_boot may need to be removed. remove/change the features related to the removed or changed partitions if dual bootloader is not used: recently in android version update, vendor_boot and init_boot partitions are added, this is related to boot image header version, the images in these partitions are loaded and verified by uboot, so if dual bootloader is not used, uboot code related to these things need to be changed. check the code related to "struct boot_img_hdr" in uboot. the a/b slot metadata format may be changed between the OTA base code and the OTA target code , this a/b slot metadata is accessed by both Android bootctrl HAL and uboot, as dual bootloader is not used, uboot is not upaded, the updated Android bootctrl HAL should also use the same format to access the file. a postinstall mechanism can be used to update the uboot images, but as there is no fallback for the update failure, the risks need to be evaluated. check whether the OTA package can be applied and whether the updated system can boot up an failure example: OTA from android10 to android12, the system fail to boot up because of the PRODUCT_SHIPPING_API_LEVEL/"ro.product.first_api_level" value difference, different encryption options are used for userdata partitions. so the PRODUCT_SHIPPING_API_LEVEL value need to be changed to be the same as the one in the OTA base code. as PRODUCT_SHIPPING_API_LEVEL is changed, the FCM target version and related HALs may also need to be changed, including changes in device manifest.xml and compatibility_matrix.xml. need to check the commit history about what is changed together with the FCM target version change.   For dynamic partitions, there are something to be noticed: OTA from the image without dynamic partitions to use dynamic partitions: Refer to the code in android10.0.0_2.0.0, there is a demonstration to update 10.0.0_1.0.0 to 10.0.0_2.0.0. In 0.0.0_1.0.0, dynamic partition is not enabled. check the variable "TARGET_USE_RETROFIT_DYNAMIC_PARTITION" and related configurations. OTA from dynamic partitions to virtual A/B, for example, OTA from android10 to android11 inherit the file "build/make/target/product/virtual_ab_ota_retrofit.mk" the first time when update from android10 to android11 with OTA, inherit the "build/make/target/product/virtual_ab_ota_retrofit.mk", the BOARD_NXP_DYNAMIC_PARTITIONS_SIZE is set as dynamic paritition is used. the second time, the device is runing android11 with retrofit virtual A/B feature, this time OTA again, but not cross version, inherit "build/make/target/product/virtual_ab_ota.mk" instead, and the BOARD_NXP_DYNAMIC_PARTITIONS_SIZE  can be set as virtual A/B feature is used. Devices that were upgraded to dynamic partitions can’t retrofit virtual A/B. if there are new dynamic partitions in OTA target code, like vendor_dlkm, no additional changes need to be made for it. Then the customers need to do full xTS test to guarantee the quality.  
記事全体を表示
Overview The purpose of this document is to provide a guide on how to enable Dual Ethernet with the GKI Development. Reference: How to enable dual ethernet on Android 11 For a better reference how to build Android i.MX image please look at the next chapter 3 Building the Android Platform for i.MX in the Android User's Guide 1. Build the Android Image with the next modifications The 2nd ethernet port is DWMAC from synopsys and phy used is realtek RTL8211F. To add them into the SharedBoardConfig.mk and remove the camera drivers. diff --git a/imx8m/evk_8mp/SharedBoardConfig.mk b/imx8m/evk_8mp/SharedBoardConfig.mk index f68eb49e..3e95708e 100644 --- a/imx8m/evk_8mp/SharedBoardConfig.mk +++ b/imx8m/evk_8mp/SharedBoardConfig.mk @@ -82,7 +82,12 @@ BOARD_VENDOR_KERNEL_MODULES += \ $(KERNEL_OUT)/drivers/rtc/rtc-snvs.ko \ $(KERNEL_OUT)/drivers/pci/controller/dwc/pci-imx6.ko \ $(KERNEL_OUT)/drivers/net/phy/realtek.ko \ - $(KERNEL_OUT)/drivers/net/ethernet/freescale/fec.ko + $(KERNEL_OUT)/drivers/net/ethernet/freescale/fec.ko \ + $(KERNEL_OUT)/drivers/net/phy/micrel.ko \ + $(KERNEL_OUT)/drivers/net/pcs/pcs_xpcs.ko \ + $(KERNEL_OUT)/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.ko \ + $(KERNEL_OUT)/drivers/net/ethernet/stmicro/stmmac/stmmac.ko \ + $(KERNEL_OUT)/drivers/net/ethernet/stmicro/stmmac/stmmac-platform.ko ifeq ($(POWERSAVE),true) BOARD_VENDOR_KERNEL_MODULES += \ $(KERNEL_OUT)/drivers/soc/imx/lpa_ctrl.ko \ @@ -219,15 +224,12 @@ BOARD_VENDOR_RAMDISK_KERNEL_MODULES += \ $(KERNEL_OUT)/drivers/perf/fsl_imx8_ddr_perf.ko \ $(KERNEL_OUT)/drivers/cpufreq/cpufreq-dt.ko \ $(KERNEL_OUT)/drivers/cpufreq/imx-cpufreq-dt.ko \ - $(KERNEL_OUT)/drivers/media/i2c/ov5640.ko \ $(KERNEL_OUT)/drivers/staging/media/imx/imx8-capture.ko \ $(KERNEL_OUT)/drivers/staging/media/imx/imx8-isi-capture.ko \ $(KERNEL_OUT)/drivers/staging/media/imx/imx8-isi-hw.ko \ $(KERNEL_OUT)/drivers/staging/media/imx/imx8-isi-mem2mem.ko \ $(KERNEL_OUT)/drivers/staging/media/imx/imx8-mipi-csi2-sam.ko \ $(KERNEL_OUT)/drivers/dma/imx-sdma.ko \ - $(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/basler-camera-driver-vvcam.ko \ - $(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/os08a20.ko \ $(KERNEL_OUT)/drivers/staging/media/imx/imx8-media-dev.ko \ $(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/vvcam-dwe.ko \ $(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/vvcam-isp.ko \​ To let the Android framework's EthernetTracker and EthernetNetworkFactory know which interfaces to manage, the framework level configure config_ethernet_iface_regex config_ethernet_interfaces must be overlay in device/nxp/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml: diff --git a/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml b/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml index 298d50cc..63f6787e 100644 --- a/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml +++ b/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml @@ -22,7 +22,12 @@ <resources> <!--For Android we support eth0 now --> - <string translatable="false" name="config_ethernet_iface_regex">eth0</string> + <string translatable="false" name="config_ethernet_iface_regex">eth\\d</string> + + <string-array translatable="false" name="config_ethernet_interfaces"> + <item>eth0;12,13,14,15,16,18,19</item> + <item>eth1;12,13,14,15,16,18,19</item> + </string-array> <!-- List of regexpressions describing the interface (if any) that represent tetherable USB interfaces. If the device doesn't want to support tething over USB this should -- Apply the patch 0001-PATCH-Add-defines-for-ETH-support-drivers.patch Build the Android Image # Change to the MY_ANDROID Directory $ source build/envsetup.sh $ lunch evk_8mp-userdebug $ ./imx-make.sh -j4 2>&1 | tee build-log.txt​   GKI Development Follow and apply the next community post: Export new symbols of GKI development Android 14 Set the GKI repo $ repo init -u https://android.googlesource.com/kernel/manifest -b common-android14-6.1 $ repo sync $ git remote add device https://github.com/nxp-imx/linux-imx.git $ git remote update $ git fetch device --tags $ git checkout android-14.0.0_1.2.0 $ cd .. #Be sure that symbolic links are created correctly $ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam $ ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex $ BUILD_FOR_GKI=yes $ BUILD_CONFIG=common/build.config.imx $ tools/bazel run //common:imx_abi_update_symbol_list Apply the following changes in the GKI Kernel tree: gki/common: Patch: 0001-PATCH-GKI-Kernel-tree-Drivers-for-the-ETH1-Interface.patch Build the GKI Image tools/bazel run //common:kernel_aarch64_dist​ Follow the build android boot.img and system_dlkm.img $ cp out/kernel_aarch64/dist/boot.img ${MY_ANDROID}/vendor/nxp/fsl-proprietary/ gki/boot.img $ cd ${MY_ANDROID} $ TARGET_IMX_KERNEL=true make bootimage # Change directory to the gki folder $ cp out/kernel_aarch64/dist/system_dlkm_staging_archive.tar.gz ${MY_ANDROID}/vendor/nxp/fsl-proprietary/gki/system_dlkm_staging_archive.tar.gz $ cd ${MY_ANDROID}/vendor/nxp/fsl-proprietary/gki $ tar -xzf system_dlkm_staging_archive.tar.gz -C system_dlkm_staging $ cd ${MY_ANDROID} $ make system_dlkmimag​e Create the tar.gz file for flash the android image (*.img, *.bat, *.sh, *.bin, *.imx) Boot the image and type lsmod to ensure the drivers are installed. Regards, Mario    
記事全体を表示
Debian is a free to use and redistribute Linux distribution that is widely used by the community for industrial and desktop applications.  This distribution started in 1993 as Debian Project with Ian Murdock inviting developers to contribute in one of the first Linux distributions.  Debian takes an important role in Linux world with a clear idea about be a full featured and free distribution with over than 59,000 packages provided as a free to use and distribute that supports a wide range of functionalities.  Currently, Debian 12 supports 9 architectures which makes it in a universal operating system that can be implemented in embedded systems, desktops or servers.  Finally, Debian has been an inspiration for well-known Linux distributions such as Kali and Ubuntu.  In this guide we will check the installation process of Debian 12 for NXP microprocessors i.MX family, specifically for i.MX8M Mini, i.MX8M Nano, i.MX8M Plus and i.MX93.  For this purpose, we divided the document in the following topics: Hardware Requirements Software Requirements Host Preparation SD Card Preparation Copying Bootloader  Copying Kernel and DTB files Debian Installation Configure Base System Boot your target References   Hardware Requirements Linux Host computer (Ubuntu 20.04 or later) USB Card reader or Micro SD to SD adapter SD Card Evaluation Kit Board for the i.MX8M Nano, i.MX8M Mini, i.MX8M Plus or i.MX93   Software Requirements Linux Ubuntu (20.04 and 24.04 tested) or Debian for host BSP version 6.1.55 for your specific target (Embedded Linux for i.MX Applications Processors | NXP Semiconductors)   Host Preparation For Debian installation we will require some specific packages for host.  You can download the packages using the following command: $ sudo apt install debian-archive-keyring debootstrap qemu-user-static We must validate the key to verify the archive using the command: $ sudo apt-key add /usr/share/keyrings/debian-archive-keyring.gpg If running an older release you need to get the unstable keyring package (because the version in your release is probably too old to have the current key) $ wget http://ftp.debian.org/debian/pool/main/d/debian-archive-keyring/debian-archive-keyring_2023.4_all.deb $ sudo dpkg -i debian-archive-keyring_2023.4_all.deb   SD Card Preparation The Linux kernel running on the Linux host assigns a device node to the SD/MMC card reader. The kernel might decide the device node name or udev rules might be used. In the following instructions, it is assumed that udev is not used. To identify the device node assigned to the SD/MMC card, carry out the following command: $ cat /proc/partitions   Partitioning the SD card On most Linux host operating systems, the SD card is mounted automatically upon insertion. Therefore, before running fdisk, make sure that the SD card is unmounted if it was previously mounted (through sudo umount /dev/sdx). Start by running fdisk with root permissions. Use the instructions above to determine the card ID. We are using sdx as an example. $ sudo fdisk /dev/sdx  Type the following parameters (each followed by <ENTER>): $fdisk: p # lists the current partitions $fdisk: d # to delete existing partitions. Repeat this until no unnecessary partitions $fdisk: n # create a new partition $fdisk: p # create a primary partition - use for both partitions $fdisk: 1 # the first partition $fdisk: 20480 # starting at offset sector $fdisk: 1024000 # ending position of the first partition to be used for the boot Images $fdisk: p # to check the partitions $fdisk: n # create a new partition $fdisk: p # create a primary partition $fdisk: 2 # the second partition $fdisk: 1228800 # starting at offset sector, which leaves enough space for the kernel, the bootloader and its configuration data $fdisk: <enter> # using the default value will create a partition that extends to the last sector of the media $fdisk: p # to check the partitions $fdisk: w # this writes the partition table to the media and fdisk exits   Copying Bootloader and Kernel In this section we will copy the bootloader and kernel image to SD card.  First, we can create a new directory to unzip the BSP downloaded from the NXP site.  $ mkdir debian-imx $ cd debian-imx $ unzip ~/Downloads/LF_v6.1.55-2.2.0_images_<board>.zip Where board is: IMX8MPEVK IMX8MNEVK IMX8MMEVK IMX93EVK Then, copy the U-Boot image. $ sudo dd if=<U-Boot_image> of=/dev/sdx bs=1k seek=<offset> conv=fsync Where offset is: 33 - for i.MX 8M Mini 32 - for i.MX 8M Nano, i.MX 8M Plus, and i.MX 9 The sectors of SD/eMMC before the “offset” KB are reserved. It may include the partition table.   Copying Kernel image and DTB files This section describes how to load the kernel image and DTB. The pre-built SD card image uses the VFAT partition for storing kernel image and DTB, which requires a VFAT partition that is mounted as a Linux drive, and the files are copied into it. This is the preferred method. Default: VFAT partition Format partition 1 on the card as VFAT with this command: $ sudo mkfs.vfat /dev/sdx1 Mount the formatted partition with this command: $ mkdir mountpoint $ sudo mount /dev/sdx1 mountpoint Copy the zImage and *.dtb files to the mountpoint by using cp. The device tree names should match $ sudo cp *.dtb mountpoint/ $sudo cp Image-<board_name>.bin mountpoint/Image Where board_name is: imx8mpevk imx8mnevk imx8mmevk imx93evk the one used by the variable specified by U-Boot. Unmount the partition with this command: $ sudo umount mountpoint   Debian Installation For Debian installation we will use the official tool debootstrap. This tool allows us to install Debian without a disk and run the system using qemu in a different architecture.  Before using debootstrap tool we need to format and mount the second partition of the SD card with the commands below: $ sudo mkfs.ext4 /dev/sdx2 $ sudo mount /dev/sdx2 mountpoint/ debootstrap can download the needed files directly from the archive when you run it. You can substitute any Debian archive mirror for http.us.debian.org/debian in the command below, preferably a mirror close to you network-wise. Mirrors are listed at http://www.debian.org/mirror/list $ sudo debootstrap --arch arm64 --foreign bookworm mountpoint/ http://ftp.debian.org/debian This step takes a while and depends on the resources of your host machine.   Configure Base System Now you’ve got a real Debian system, though rather lean, on disk. chroot into it: $ sudo cp /usr/bin/qemu-aarch64-static mountpoint/usr/bin $ sudo LANG=C.UTF-8 chroot mountpoint/ qemu-aarch64-static /bin/bash After chrooting you may need to set the terminal definition to be compatible with the Debian base system, for example: $ export TERM=xterm-color we need to finish the multi-stage boot strap $ /debootstrap/debootstrap --second-stage At this point /dev/ only contains very basic device files. For the next steps of the installation, additional device files may be needed. There are different ways to go about this and which method you should use depends on the host system you are using for the installation, whether you intend to use a modular kernel or not, and whether you want to use dynamic (e.g. using udev) or static device files for the new system. A few of the available options are: install the makedev package, and create a default set of static device files using (after chrooting) $ apt install makedev $ mount none /proc -t proc $ cd /dev $ MAKEDEV generic With these next steps we will be setting up the Debian system:   Setting fstab FSTAB is a configuration table designed to ease the burden of mounting and unmounting file systems to a machine. $ nano /etc/fstab # stock fstab - you probably want to override this with a machine specific one /dev/root / auto defaults 1 1 proc /proc proc defaults 0 0 devpts /dev/pts devpts mode=0620,ptmxmode=0666,gid=5 0 0 tmpfs /run tmpfs mode=0755,nodev,nosuid,strictatime 0 0 tmpfs /var/volatile tmpfs defaults 0 0 # uncomment this if your device has a SD/MMC/Transflash slot #/dev/mmcblk0p1 /media/card auto defaults,sync,noauto 0 0   Setting Timezone The following command allows you to choose your timezone. $ dpkg-reconfigure tzdata   Configure apt Debootstrap will have created a very basic /etc/apt/sources.list that will allow installing additional packages. However, you may want to add some additional sources, for example for source packages and security updates: $ nano /etc/apt/sources.list deb http://deb.debian.org/debian bookworm main non-free-firmware deb-src http://deb.debian.org/debian bookworm main non-free-firmware deb http://deb.debian.org/debian-security/ bookworm-security main non-free-firmware deb-src http://deb.debian.org/debian-security/ bookworm-security main non-free-firmware deb http://deb.debian.org/debian bookworm-updates main non-free-firmware deb-src http://deb.debian.org/debian bookworm-updates main non-free-firmware Make sure to run the apt update after you have made changes to the sources list   Configure locales and keyboard To configure your locale settings to use a language other than English, install the locales support package and configure it. Currently, the use of UTF-8 locales is recommended. $ apt install locales $ dpkg-reconfigure locales To configure your keyboard (if needed): $ apt install console-setup $ dpkg-reconfigure keyboard-configuration Note that the keyboard cannot be set while in the chroot, but will be configured for the next reboot   Adding Users $ apt install sudo $ adduser imx $ usermod -aG sudo imx $ nano /etc/sudoers imx ALL=(ALL:ALL) ALL   Tasksel Installation As mentioned earlier, the installed system will be very basic. If you would like to make the system a bit more mature, there is an easy method to install all packages with “standard” priority: $ tasksel install standard $ apt clean $ exit $ sudo umount mountpoint/ $sync   Boot your target Now, you can boot your target from your SD Card. (Review your specific target documentation)   Configure Networking (after booting target) Based on Debian official documentation for new systems the common names for network interfaces such as eth0 or wlan0 are not used. Therefore, we will need to list the interfaces using: $ ls /sys/class/net To have ethernet connection we will need to create a file in the path etc/network/. $ sudo nano etc/network/interfaces Type the following commands on the file: auto lo iface lo inet loopback auto end0 iface end0 inet dhcp   Install Neofetch (Optional) $ apt install neofetch   Outputs  Debian 12 running on i.MX8MP Debian 12 running on i.MX93   References Chapter 1. Definitions and overview. (2021, January). Retrieved May 30, 2024, from https://www.debian.org/doc/manuals/debian-faq/basic-defs.en.html Debian GNU/Linux Installation Guide. (2024). https://www.debian.org/releases/stable/i386/install.en.pdf Arm64Port. (n.d.). https://wiki.debian.org/Arm64Port i.MX Linux User's Guide (nxp.com)
記事全体を表示
The document will cover three parts, which include: A brief introduction to RSA algorithm How to compile boot image including OP-TEE-OS for Boot media - QSPI The steps to sign and verification The SoC for this experiment is based on i.MX8MP-EVK
記事全体を表示
Hello, on this post I will explain how to record separated audio channels using an 8MIC-RPI-MX8 Board. As background about how to setup the board to record and play audio using i.MX boards, I suggest you take a look on the next post: How to configure, record and play audio using an 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK. Linux Binary Demo Files - i.MX 8MMini EVK. 8MIC-RPI-MX8 Board. Serial console emulator (Tera Term, Putty, etc.). Headphones/speakers. Waveform Audio Format WAV, known for WAVE (Waveform Audio File Format), is a subset of Microsoft’s Resource Interchange File Format (RIFF) specification for storing digital audio files. This format does not apply compression to the information and stores the audio with different sampling rates and bitrates. WAV files are larger in size compared to other formats such as MP3 which uses compression to reduce the file size while maintaining a good audio quality but, there is always some lose on quality since audio information is too random to be compressed with conventional methods, the main advantage of this format is provide an audio file without losses that is also widely used on studio. This files starts with a file header with data chunks. A WAV file consists of two sub-chunks: fmt chunk: data format. data chunk: sample data. So, is structured by a metadata that is called WAV file header and the actual audio information. The header of a WAV (RIFF) file is 44 bytes long and has the following format: How to separate the channels? To separate each audio channel from the recording we need to use the next command that will record raw data of each channel. arecord -D plughw:<audio device> -c<number of chanels> -f <format> -r <sample rate> -d <duration of the recording> --separate-channels <output file name>.wav arecord -D plughw:2,0 -c8 -f s16_le -r 48000 -d 10 --separate-channels sample.wav This command will output raw data of recorded channels as is showed below. This raw data cannot be used as a “normal” .wav file because the header information is missing. It is possible to confirm it if import raw data to a DAW and play recorded samples: So, to use this information we need to create the header for each file using WAVE library on python. Here the script that I used: import wave import os name = input("Enter the name of the audio file: ") os.system("arecord -D plughw:2,0 -c8 -f s16_le -r 48000 -d 10 --separate-channels " + name + ".wav") for i in range (0,8): with open(name + ".wav." + str(i), "rb") as in_file: data = in_file.read() with wave.open(name + "_channel_" + str(i) +".wav", "wb") as out_file: out_file.setnchannels(1) out_file.setsampwidth(2) out_file.setframerate(48000) out_file.writeframesraw(data) os.system("mkdir output_files") os.system("mv " + name + "_channel_" + "* " + "output_files") os.system("rm " + name + ".wav.*") If we run the script, will generate a directory with the eight audio channels in .wav format. Now, we will be able to play each channel individually using an audio player. References IBM, Microsoft Corporation. (1991). Multimedia Programming Interface and Data Specifications 1.0. Microsoft Corporation. (1994). New Multimedia Data Types and Data Techniques. Standford University. (2024, January 30). Retrieved from WAVE PCM sound file format: http://hummer.stanford.edu/sig/doc/classes/SoundHeader/WaveFormat/
記事全体を表示
  Introduction   MATTER chip-tool android APK is a very useful tool for commission, control the MATTER network by smart phone. Vendor can add various features into the APK. It supports build by Android Studio and command line. The official build steps can be found here: https://github.com/project-chip/connectedhomeip/blob/master/docs/guides/android_building.md But the official guide does not cover how to build in a non-GUI linux distribution (without Android Studio installed). This article describes how to build under Ubuntu server. Install Android SDK  Install SDK command line from: https://developer.android.com/studio, And follow the steps: https://developer.android.com/tools/sdkmanager to install.  Install the Android-26 SDK and 23 NDK: $./sdkmanager "platforms;android-26" "ndk;23.2.8568313"  Export env  $export ANDROID_HOME=<SDK path>  $export ANDROID_NDK_HOME=<SDK path>/ndk/23.2.8568313/   Install kotlin (1.8.0)  $curl -s https://get.sdkman.io | bash  $sdk install kotlin 1.8.0  $whereis kotlin  $export PATH=$PATH:<patch of bin of kotlin>    Configure proxy for gradle  $ cat ~/.gradle/gradle.properties  # Set the socket timeout to 5 minutes (good for proxies)  org.gradle.internal.http.socketTimeout=300000  # the number of retries (initial included) (default 3)  org.gradle.internal.repository.max.retries=10  # the initial time before retrying, in milliseconds (default 125)  org.gradle.internal.repository.initial.backoff=500  systemProp.http.proxyHost=apac.nics.nxp.com  systemProp.http.proxyPort=8080  systemProp.http.nonProxyHosts=localhost|*.nxp.com  systemProp.https.proxyHost=apac.nics.nxp.com  systemProp.https.proxyPort=8080  systemProp.https.nonProxyHosts=localhost|*.nxp.com    Configure proxy  Configure proxy for download packages during build export FTP_PROXY="http://apac.nics.nxp.com:8080"  export HTTPS_PROXY="http://apac.nics.nxp.com:8080"  export HTTP_PROXY="http://apac.nics.nxp.com:8080"  export NO_PROXY="localhost,*.nxp.com"  export ftp_proxy="http://apac.nics.nxp.com:8080"  export http_proxy="http://apac.nics.nxp.com:8080"  export https_proxy="http://apac.nics.nxp.com:8080"  export no_proxy="localhost,*.nxp.com"    Patch for gradle java option  This step can be skipped if using OpenJDK16.  Otherwise if you're using OpenJDK 17 (Java 61), you have to upgrade the gradle from 7.1.1 to 7.3, and add java.io open to ALL-UNNAMED:  diff --git a/examples/android/CHIPTool/gradle.properties b/examples/android/CHIPTool/gradle.properties  index 71f72db8c8..5bce4b4528 100644  --- a/examples/android/CHIPTool/gradle.properties  +++ b/examples/android/CHIPTool/gradle.properties  @@ -6,7 +6,8 @@  # http://www.gradle.org/docs/current/userguide/build_environment.html  # Specifies the JVM arguments used for the daemon process.  # The setting is particularly useful for tweaking memory settings.  -org.gradle.jvmargs=-Xmx4096m -XX:MaxPermSize=2048m -XX:+HeapDumpOnOutOfMemoryError -Dfile.encoding=UTF-8  +#org.gradle.jvmargs=-Xmx4096m -XX:MaxPermSize=2048m -XX:+HeapDumpOnOutOfMemoryError -Dfile.encoding=UTF-8  +org.gradle.jvmargs=-Xmx4096m -XX:+HeapDumpOnOutOfMemoryError -Dfile.encoding=UTF-8  --add-opens=java.base/java.io=ALL-UNNAMED  # When configured, Gradle will run in incubating parallel mode.  # This option should only be used with decoupled projects. More details, visit  # http://www.gradle.org/docs/current/userguide/multi_project_builds.html#sec:decoupled_projects  diff --git a/examples/android/CHIPTool/gradle/wrapper/gradle-wrapper.properties b/examples/android/CHIPTool/gradle/wrapper/gradle-wrapper.properties  index 05679dc3c1..e750102e09 100644  --- a/examples/android/CHIPTool/gradle/wrapper/gradle-wrapper.properties  +++ b/examples/android/CHIPTool/gradle/wrapper/gradle-wrapper.properties  @@ -1,5 +1,5 @@  distributionBase=GRADLE_USER_HOME  distributionPath=wrapper/dists  -distributionUrl=https\://services.gradle.org/distributions/gradle-7.1.1-bin.zip  +distributionUrl=https\://services.gradle.org/distributions/gradle-7.3-bin.zip  zipStoreBase=GRADLE_USER_HOME  zipStorePath=wrapper/dists    Build & Install Clone all the modules from github: $git clone --single-branch --recurse-submodules https://github.com/project-chip/connectedhomeip.git Enviroment setup: $source scripts/bootstrap.sh Build: ./scripts/build/build_examples.py --target android-arm64-chip-tool build Install built apk into phone: $adb install out/android-arm64-chip-tool/outputs/apk/debug/app-debug.apk  
記事全体を表示
Hello everyone! In this document you'll find an example on how to setup your own recipe for Yocto Project to add your own custom changes, such as custom device tree, patches, custom drivers, etc. Linux kernel used in this guide 6.1.36_2.1.0 At least 120(250)GB HDD in the host PC Ubuntu 20.04 or later host PC ##Host Setup $ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev python3-subunit mesa-common-dev zstd liblz4-tool file locales -y $ sudo locale-gen en_US.UTF-8 ##Setup Repo utility $ mkdir ~/bin (this step may not be needed if the bin folder already exists) $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo $ export PATH=~/bin:$PATH ##Git Setup $ git config --global user.name "Your Name" $ git config --global user.email "Your Email" $ git config --list ##Yocto Setup $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml $ repo sync $ DISTRO=fsl-imx-wayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b buildwayland ##Create the new layer $ cd ../sources $ bitbake-layers create-layer meta-newlayer ##Add the new layer to the bblayers.conf in the build directory $ bitbake-layers add-layer meta-newlayer ##Check that it has been added correctly $ tree -L 4 ./meta-newlayer ##Edit the new layer and delete the samples created by yocto $ cd meta-newlayer $ rm -r recipes-example $ rm conf/layer.conf ##Use any text editor to create the layer configuration $ nano conf/layer.conf ##Add the following to the layer configuration file BBPATH .= ":${LAYERDIR}" BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \             ${LAYERDIR}/recipes-*/*/*.bbappend" BBFILE_COLLECTIONS += "meta-newlayer" BBFILE_PATTERN_meta-newlayer := "^${LAYERDIR}/" BBFILE_PRIORITY_meta-newlayer = "8" LAYERSERIES_COMPAT_meta-newlayer = "mickledore" ##Prepare bbappend files so the patches get applied $ mkdir -p recipes-kernel/linux $ cd recipes-kernel/linux $ nano linux-imx_%.bbappend ##Add the following to the .bbappend file FILESEXTRAPATHS:prepend := "${THISDIR}/files:" SRC_URI += "file://001-add-imx8mp-dts-test.patch" PACKAGE_ARCH = "${MACHINE_ARCH}" KERNEL_DEVICETREE:append = " freescale/imx8mp-evk-test.dtb" ##Copy the patches to the layer file path, for this example I have created a simple patch to just rename the default device tree. $ mkdir files $ cp ~/patches/001-add-imx8mp-dts-test.patch files ##Make sure that the layers is created correctly $ bitbake-layers show-layers  ##Finally we bitbake our image $ cd ~/imx-yocto-bsp/buildwayland $ bitbake imx-image-multimedia #All the images built should appear at  <build directory>/tmp/deploy/images/<machine> Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.  
記事全体を表示
The user interface has limited the use of the tool GUI Guider. Getting an interaction only through a mouse or touchscreen can be enough for some use cases. However, sometimes the use case requires to go beyond its limitations. This video/appnote explores the possibility of integrating voice by creating a bridge between a speech recognition technology, such as VIT, and the interface creator GUI Guider. It uses a universal way to link all the voice recognition commands and a wakeword to any interaction created by GUI Guider. The following video shows the steps necessary to create that connection by creating the voice recognition using VIT voice commands and wakewords, create an interface of GUI Guider using a template, how to connect between them using the board i.MX 93 evk and testing it. For more information consult the following links AppNote HTML: https://docs.nxp.com/bundle/AN14270/page/topics/abstract.html?_gl=1*1glzg9k*_ga*NDczMzk4MDYuMTcxNjkyMDI0OA..*_ga_WM5LE0KMSH*MTcxNjkyMDI0OC4xLjEuMTcxNjkyMDcyMy4wLjAuMA AppNote PDF: https://www.nxp.com/docs/en/application-note/AN14270.pdf Associated File: AN14270SW  
記事全体を表示
-- DTS for gpio wakeup   // SPDX-License-Identifier: (GPL-2.0+ OR MIT) /*  * Copyright 2022 NXP  */   #include "imx93-11x11-evk.dts"   / {         gpio-keys {                 compatible = "gpio-keys";                 pinctrl-names = "default";                 pinctrl-0 = <&pinctrl_gpio_keys>;                   power {                   label = "GPIO Key Power";                   linux,code = <KEY_POWER>;                   gpios = <&gpio2 7 GPIO_ACTIVE_LOW>;                   wakeup-source;                   debounce-interval = <20>;                   interrupt-parent = <&gpio2>;                   interrupts = <7 IRQ_TYPE_LEVEL_LOW>;                 };         }; };   &iomuxc {         pinctrl_gpio_keys: gpio_keys_grp {                 fsl,pins = <                         MX93_PAD_GPIO_IO07__GPIO2_IO07  0x31e                 >;         }; }; -- testing the switch GPIO  First check if your gpio dts configuration to make it act as a switch works or not After executing the command - 'evtest /dev/input/event1' Trigger an interrupt by connecting GPIO2 7 to GND, as soon as you do that, you will receive Event logs such as below:- This shows that your dts configuration for GPIO works.     -- Verify the interrupt         -- Go to sleep and then connect the GPIO to GND to trigger a wakeup, in the logs we see that kernel exits the suspend mode    
記事全体を表示
We are pleased to announce that Config Tools for i.MX v15.1 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...)   Version 15.1 • On MacOS aarch64, the missing Overview is fixed. • TEE – Pin tables now only contain items for specific configuration (mask/security/interrupts).
記事全体を表示
P3T1755DP is a ±0.5°C accurate temperature-to-digital converter with a -40 °C to +125 °C range. It uses an on-chip band gap temperature sensor and an A-to-D conversion technique with overtemperature detection. The temperature register always stores a 12-bit two's complement data, giving a temperature resolution of 0.0625 °C P3T1755DP which can be configured for different operation conditions: continuous conversion, one-shot mode, or shutdown mode.   The device has very good features but, unfortunately, is not supported by Linux yet!   The P31755 works very similarly to LM75, pct2075, and other compatibles.   We can add support to P3T1755 in the LM75.c program due to the process to communicate with the device is the same as LM75 and equivalents.   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.55-2.2.0/drivers/hwmon/lm75.c route: drivers/hwmon/lm75.c   The modifications that we have to do are the next:    1. We have to add the configurations to the kernel on the imx_v8_defconfig file CONFIG_SENSORS_ARM_SCMI=y CONFIG_SENSORS_ARM_SCPI=y CONFIG_SENSORS_FP9931=y +CONFIG_SENSORS_LM75=m +CONFIG_HWMON=y +CONFIG_I2C=y +CONFIG_REGMAP_I2C=y CONFIG_SENSORS_LM90=m CONFIG_SENSORS_PWM_FAN=m CONFIG_SENSORS_SL28CPLD=m    2. Add the part on the list of parts compatible with the driver LM75.c enum lm75_type { /* keep sorted in alphabetical order */ max6626, max31725, mcp980x, + p3t1755, pct2075, stds75, stlm75,   3. Add the configuration in the structure lm75_params device_params[]. .default_resolution = 9, .default_sample_time = MSEC_PER_SEC / 18, }, + [p3t1755] = { + .default_resolution = 12, + .default_sample_time = MSEC_PER_SEC / 10, + }, [pct2075] = { .default_resolution = 11, .default_sample_time = MSEC_PER_SEC / 10,   Notes: You can change the configuration of the device using .set_mask and .clear_mask, see more details on LM75.c lines 57 to 78   4. Add the ID to the list in the structure i2c_device_id lm75_ids and of_device_id __maybe_unused lm75_of_match    { "max31725", max31725, }, { "max31726", max31725, }, { "mcp980x", mcp980x, }, + { "p3t1755", p3t1755, }, { "pct2075", pct2075, }, { "stds75", stds75, }, { "stlm75", stlm75, },   + { + .compatible = "nxp,p3t1755", + .data = (void *)p3t1755 + },   5. In addition to all modifications, I modify the device tree of my iMX8MP-EVK to connect the Sensor in I2C3 of the board.  https://github.com/nxp-imx/linux-imx/blob/lf-6.1.55-2.2.0/arch/arm64/boot/dts/freescale/imx8mp-evk.dts   }; }; + + p3t1755: p3t1755@48 { + compatible = "nxp,p3t1755"; + reg = <0x48>; + }; + };   Connections: We will use the expansion connector of the iMX8MP-EVK and J9 of the P3T1755DP-ARD board.   P3T1755DP-ARD board   iMX8MP-EVK   P3T1755DP-ARD ----> iMX8MP-EVK J9              ---------->            J21 +3v3 (Pin 9) ---> +3v3 (Pin 1) GND(Pin 7) ---> GND (PIN 9) SCL (Pin 4) ---> SCL (Pin 5) SDA (Pin 3) ---> SDA (Pin 3)     Reading the Sensor We can read the sensor using the next commands:   Read Temperature: $ cat /sys/class/hwmon/hwmon1/temp1_input Reading maximum temperature: $ cat /sys/class/hwmon/hwmon1/temp1_max Reading hysteresis: $ cat /sys/class/hwmon/hwmon1/temp1_max_hyst   https://www.nxp.com/design/design-center/development-boards-and-designs/analog-toolbox/arduino-shields-solutions/p3t1755dp-arduino-shield-evaluation-board:P3T1755DP-ARD    
記事全体を表示
What is LGVL? LVGL is a graphics library to run on devices with limited resources. LVGL is fully open-source and has no external dependencies, works with any modern MCU or MPU, and can be used with any (RT)OS or bare metal setup. https://lvgl.io/   What is Framebuffer? The Linux framebuffer (fbdev) is a Linux subsystem used to show graphics on a display, typically manipulated on the system console   How to write on the frame buffer? The device is listed on de device list typically "fb0" on iMX.   1. Stop the window manager (Weston in our BSP) $ systemctl stop weston   2. Write random data on the frame buffer with the next command: $ cat /dev/urandom > /dev/fb0   You should see colored pixels on the screen   3. Restart the window manager. $ systemctl start weston     Cross-compiling the application   1. On the host computer we will clone the LGVL repo: $ git clone https://github.com/lvgl/lv_port_linux_frame_buffer.git -b release/v8.2 $ cd lv_port_linux_frame_buffer $ git submodule update --init --recursive 2. Configure the screen resolution, rotation, and the touch input.       2.1 The resolution is configured in lines 33 and 34 of the main.c disp_drv.hor_res = 1080; disp_drv.ver_res = 1920;           2.2 Rotation configured is on lines 32 and 57 of main.c. disp_drv.sw_rotate = 3; lv_disp_set_rotation(NULL, LV_DISP_ROT_270);     2.3 The touch input is configured on line 450 of lv_drv_conf.h # define EVDEV_NAME "/dev/input/event2"   Note: In my case is on /dev/input/event2 to check the inputs use the command "evtest"   3. Compile the application using the command "make"   Note: To compile the application on your host computer you have to set the environment.   4. Share the file called "demo" with your board and execute it on the board with the command $ ./demo   Note: You have to stop the weston service to run the application.     Notes: Tested on iMX8MN EVK with BSP 6.1.36 Works on Multimedia and Full image.
記事全体を表示
Sometime need standalone compile device tree. Only Linux headers and device tree directory are needed.         
記事全体を表示