Debian 12 Installation Guide for i.MX8MM, i.MX8MP and i.MX8MN: GPU, VPU and Multimedia Packages

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debian 12 Installation Guide for i.MX8MM, i.MX8MP and i.MX8MN: GPU, VPU and Multimedia Packages

Debian 12 Installation Guide for i.MX8MM, i.MX8MP and i.MX8MN: GPU, VPU and Multimedia Packages

This guide is a continuation from our latest Debian 12 Installation Guide for iMX8MM, iMX8MP, iMX8MN and iMX93.

Here we will describe the process to install the multimedia and hardware acceleration packages, specifically GPU, VPU and Gstreamer on i.MX8M Mini, i.MX8M Plus and i.MX8M Nano.

The guide is based on the one provided by our colleague Build Ubuntu For i.MX8 Series Platform - NXP Community, which requires to previously build an image using Yocto Project with the following distro and image name.

Distro name - fsl-imx-wayland
Image name – imx-image-multimedia

For more information please check our BSP documentation i.MX Yocto Project User’s Guide.

 

Hardware Requirements

  • Linux Host Computer (Ubuntu 20.04 or later)
  • USB Card reader or Micro SD to SD adapter
  • SD Card
  • Evaluation Kit Board for the i.MX8M Nano, i.MX8M Mini, i.MX8M Plus

 

Software Requirements

  • Linux Ubuntu (20.04 tested) or Debian for Host Computer
  • BSP version 6.1.55 built with Yocto Project

 

After built the image we can start the installation by following the steps below:

 

GPU Installation

The GPU Installation consists of copy the files from packages imx-gpu-g2d, imx-gpu-viv, libdrm to the Debian system. As our latest installation guide, we will continue naming “mountpoint” to the directory where Debian system is mounted on our host machine.
Regarding the path provided on each step, we put labels <build-path> and <machine> that you will need to change based on your environment. These are the paths that Yocto Project uses to save the packages. However, this could change on your environment and you can find the work directory from each package using the following command:

bitbake -e <package-name> | grep ^WORKDIR=

This command will show you the absolute path of the package work directory.

1. Install GPU Packages

$ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-gpu-g2d/6.4.11.p2.2-r0/image/* mountpoint

$ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-gpu-viv/1_6.4.11.p2.2-aarch64-r0/image/* mountpoint

$ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/libdrm/2.4.115.imx-r0/image/* mountpoint

 

2. Install Linux IMX Headers and IMX Parser

$ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/linux-imx-headers/6.1-r0/image/* mountpoint

$ sudo cp -Pra <build-path>/tmp/work/armv8a-poky-linux/imx-parser/4.8.2-r0/image/* mountpoint

 

3. Use chroot

$ sudo LANG=C.UTF-8 chroot mountpoint/ qemu-aarch64-static /bin/bash

 

4. Install Dependencies

$ apt install libudev-dev libinput-dev libxkbcommon-dev libpam0g-dev libx11-xcb-dev libxcb-xfixes0-dev libxcb-composite0-dev libxcursor-dev libxcb-shape0-dev libdbus-1-dev libdbus-glib-1-dev libsystemd-dev libpixman-1-dev libcairo2-dev libffi-dev libxml2-dev kbd libexpat1-dev autoconf automake libtool meson cmake ssh net-tools network-manager iputils-ping rsyslog bash-completion htop resolvconf dialog vim udhcpc udhcpd git v4l-utils alsa-utils git gcc less autoconf autopoint libtool bison flex gtk-doc-tools libglib2.0-dev libpango1.0-dev libatk1.0-dev kmod pciutils libjpeg-dev 

 

5. Create a folder for Multimedia Installation. Here we will clone all the multimedia repositories. 

$ mkdir multimedia_packages
$ cd multimedia_packages

 

6. Build Wayland

$ git clone https://gitlab.freedesktop.org/wayland/wayland.git
$ cd wayland
$ git checkout 1.22.0
$ meson setup build --prefix=/usr -Ddocumentation=false -Ddtd_validation=true
$ cd build
$ ninja install

 

7. Build Wayland Protocols IMX

$ git clone https://github.com/nxp-imx/wayland-protocols-imx.git
$ cd wayland-protocols-imx
$ git checkout wayland-protocols-imx-1.32
$ meson setup build --prefix=/usr -Dtests=false
$ cd build
$ ninja install

 

8. Build Weston

$ git clone https://github.com/nxp-imx/weston-imx.git
$ cd weston-imx
$ git checkout weston-imx-11.0.3
$ meson setup build --prefix=/usr -Dpipewire=false  -Dsimple-clients=all -Ddemo-clients=true -Ddeprecated-color-management-colord=false -Drenderer-gl=true -Dbackend-headless=false -Dimage-jpeg=true -Drenderer-g2d=true -Dbackend-drm=true -Dlauncher-libseat=false -Dcolor-management-lcms=false -Dbackend-rdp=false -Dremoting=false -Dscreenshare=true -Dshell-desktop=true -Dshell-fullscreen=true -Dshell-ivi=true -Dshell-kiosk=true -Dsystemd=true -Dlauncher-logind=true -Dbackend-drm-screencast-vaapi=false -Dbackend-wayland=false -Dimage-webp=false -Dbackend-x11=false -Dxwayland=false
$ cd build
$ ninja install

 

VPU Installation

To install VPU and Gstreamer please follow the steps below:

1. Install firmware-imx

$ sudo cp -Pra <build-path>/tmp/work/all-poky-linux/firmware-imx/1_8.22-r0/image/lib/* mountpoint/lib/

 

2. Install VPU Driver

$ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-vpu-hantro/1.31.0-r0/image/* mountpoint

$ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-vpuwrap/git-r0/image/* mountpoint

 

3. Use chroot

$ sudo LANG=C.UTF-8 chroot mountpoint/ qemu-aarch64-static /bin/bash

 

4. Install dependencies for Gstreamer Plugins

$ apt install libgirepository1.0-dev gettext liborc-0.4-dev libasound2-dev libogg-dev libtheora-dev libvorbis-dev libbz2-dev libflac-dev libgdk-pixbuf-2.0-dev libmp3lame-dev libmpg123-dev libpulse-dev libspeex-dev libtag1-dev libbluetooth-dev libusb-1.0-0-dev libcurl4-openssl-dev libssl-dev librsvg2-dev libsbc-dev libsndfile1-dev

 

5. Change directory to multimedia packages.

$ cd multimedia-packages

 

6. Build gstreamer

$ git clone https://github.com/nxp-imx/gstreamer -b lf-6.1.55-2.2.0
$ cd gstreamer
$ meson setup build --prefix=/usr -Dintrospection=enabled -Ddoc=disabled -Dexamples=disabled -Ddbghelp=disabled -Dnls=enabled  -Dbash-completion=disabled -Dcheck=enabled -Dcoretracers=disabled -Dgst_debug=true -Dlibdw=disabled -Dtests=enabled -Dtools=enabled -Dtracer_hooks=true -Dlibunwind=disabled -Dc_args=-I/usr/include/imx
$ cd build
$ ninja install

 

7. Build gst-plugins-base

$ git clone https://github.com/nxp-imx/gst-plugins-base -b lf-6.1.55-2.2.0
$ cd gst-plugins-base
$ meson setup build --prefix=/usr -Dalsa=enabled -Dcdparanoia=disabled -Dgl-graphene=disabled -Dgl-jpeg=disabled -Dopus=disabled -Dogg=enabled  -Dorc=enabled -Dpango=enabled -Dgl-png=enabled -Dqt5=disabled -Dtheora=enabled -Dtremor=disabled -Dvorbis=enabled -Dlibvisual=disabled -Dx11=disabled -Dxvideo=disabled -Dxshm=disabled -Dc_args=-I/usr/include/imx
$ cd build
$ ninja install

 

8. Build gst-plugins-good

$ git clone https://github.com/nxp-imx/gst-plugins-good -b lf-6.1.55-2.2.0
$ cd gst-plugins-good
$ meson setup build --prefix=/usr -Dexamples=disabled -Dnls=enabled -Ddoc=disabled -Daalib=disabled -Ddirectsound=disabled -Ddv=disabled -Dlibcaca=disabled -Doss=enabled -Doss4=disabled -Dosxaudio=disabled -Dosxvideo=disabled -Dshout2=disabled -Dtwolame=disabled -Dwaveform=disabled -Dasm=disabled -Dbz2=enabled -Dcairo=enabled -Ddv1394=disabled -Dflac=enabled -Dgdk-pixbuf=enabled -Dgtk3=disabled -Dv4l2-gudev=enabled -Djack=disabled -Djpeg=enabled -Dlame=enabled -Dpng=enabled -Dv4l2-libv4l2=disabled -Dmpg123=enabled -Dorc=enabled -Dpulse=enabled -Dqt5=disabled -Drpicamsrc=disabled -Dsoup=enabled -Dspeex=enabled -Dtaglib=enabled -Dv4l2=enabled -Dv4l2-probe=true -Dvpx=disabled -Dwavpack=disabled -Dximagesrc=disabled -Dximagesrc-xshm=disabled -Dximagesrc-xfixes=disabled -Dximagesrc-xdamage=disabled -Dc_args=-I/usr/include/imx
$ cd build
$ ninja install

 

9. Build gst-plugins-bad

$ git clone https://github.com/nxp-imx/gst-plugins-bad -b lf-6.1.55-2.2.0
$ cd gst-plugins-bad
$ meson setup build --prefix=/usr -Dintrospection=enabled -Dexamples=disabled -Dnls=enabled -Dgpl=disabled -Ddoc=disabled -Daes=enabled -Dcodecalpha=enabled -Ddecklink=enabled -Ddvb=enabled -Dfbdev=enabled -Dipcpipeline=enabled -Dshm=enabled -Dtranscode=enabled -Dandroidmedia=disabled -Dapplemedia=disabled -Dasio=disabled -Dbs2b=disabled -Dchromaprint=disabled -Dd3dvideosink=disabled -Dd3d11=disabled -Ddirectsound=disabled -Ddts=disabled -Dfdkaac=disabled -Dflite=disabled -Dgme=disabled -Dgs=disabled -Dgsm=disabled -Diqa=disabled -Dkate=disabled -Dladspa=disabled -Dldac=disabled -Dlv2=disabled -Dmagicleap=disabled -Dmediafoundation=disabled -Dmicrodns=disabled -Dmpeg2enc=disabled -Dmplex=disabled -Dmusepack=disabled -Dnvcodec=disabled -Dopenexr=disabled -Dopenni2=disabled -Dopenaptx=disabled -Dopensles=disabled -Donnx=disabled -Dqroverlay=disabled -Dsoundtouch=disabled -Dspandsp=disabled -Dsvthevcenc=disabled -Dteletext=disabled -Dwasapi=disabled -Dwasapi2=disabled -Dwildmidi=disabled -Dwinks=disabled -Dwinscreencap=disabled -Dwpe=disabled -Dzxing=disabled -Daom=disabled -Dassrender=disabled -Davtp=disabled -Dbluez=enabled -Dbz2=enabled -Dclosedcaption=enabled -Dcurl=enabled -Ddash=enabled -Ddc1394=disabled -Ddirectfb=disabled -Ddtls=disabled -Dfaac=disabled -Dfaad=disabled -Dfluidsynth=disabled -Dgl=enabled -Dhls=enabled -Dkms=enabled -Dcolormanagement=disabled -Dlibde265=disabled -Dcurl-ssh2=disabled -Dmodplug=disabled -Dmsdk=disabled -Dneon=disabled -Dopenal=disabled -Dopencv=disabled -Dopenh264=disabled -Dopenjpeg=disabled -Dopenmpt=disabled -Dhls-crypto=openssl -Dopus=disabled -Dorc=enabled -Dresindvd=disabled -Drsvg=enabled -Drtmp=disabled -Dsbc=enabled -Dsctp=disabled -Dsmoothstreaming=enabled -Dsndfile=enabled -Dsrt=disabled -Dsrtp=disabled -Dtinyalsa=disabled -Dtinycompress=enabled -Dttml=enabled -Duvch264=enabled -Dv4l2codecs=disabled -Dva=disabled -Dvoaacenc=disabled -Dvoamrwbenc=disabled -Dvulkan=disabled -Dwayland=enabled -Dwebp=enabled -Dwebrtc=disabled -Dwebrtcdsp=disabled -Dx11=disabled -Dx265=disabled -Dzbar=disabled -Dc_args=-I/usr/include/imx
$ cd build
$ ninja install

 

10. Build imx-gst1.0-plugin

$ git clone https://github.com/nxp-imx/imx-gst1.0-plugin -b lf-6.1.55-2.2.0
$ cd imx-gst1.0-plugin
$ meson setup build --prefix=/usr -Dplatform=MX8 -Dc_args=-I/usr/include/imx
$ cd build
$ ninja install

 

11. Exit chroot

$ exit

 

Verify Installation

For verification process, boot your target from the SD Card. (Review your specific target documentation)

1. Verify Weston

For this verification you will need to be root user.

# export XDG_RUNTIME_DIR=/run/user/0
# weston

 

2. Verify VPU and Gstreamer

Use the following Gstreamer pipeline for Hardware Accelerated VPU Encode.

# gst-launch-1.0 videotestsrc ! video/x-raw, format=I420, width=640, height=480 ! vpuenc_h264 ! filesink location=test.mp4

 

Then you can reproduce the file with this command:

# gplay-1.0 test.mp4

 

Finally, you have installed and verified the GPU, VPU and Multimedia packages. Now, you can start testing audio and video applications.

无评分
版本历史
最后更新:
‎08-09-2024 04:51 PM
更新人: