i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Agenda: 1. How-to M4 boot-up from TCM, DDR, OCRAM or QSPI in i.MX7D SABRE board 2. About multicore communication, Linux / Cortex-A and FreeRTOS / Cortex-M    a. RPMsg Ping-Pong FreeRTOS demo    b. RPMsg String Echo FreeRTOS demo 3. Multi-core Resource Sharing and Protection, RDC (Resource Domain Controller), Master Assignment Registers, Peripheral Mapping and Memory region Map 4. RDC settings in FreeRTOS BSP
View full article
Video decoding gst-launch filesrc location=sample.mp4 ! qtdemux ! ffdec_h264 ! mfw_v4lsink Notes: On LTIB BSP 3.0.35_4.0.0, prep the package and apply the attached patch on top, then build. On Yocto, the easy way to add the gst-ffmpeg package is by adding these two lines on the conf/local.conf file: IMAGE_INSTALL_append = " gst-ffmpeg" LICENSE_FLAGS_WHITELIST = 'commercial'
View full article
For OpenSuse Users: Open a terminal as root Edit tftp file # vi /etc/xinetd.d/tftp Change the disable to no: service tftp {   socket_type = dgram   protocol = udp   wait = yes   user = root   server = /usr/sbin/in.tftpd   server_args = -s /tftpboot   disable = no }
View full article
by b47504 Overview This document is intended to introduce debug tips about i.MX power management based on i.MX Android software. The following topics are involved in this document: How to debug suspend/resume issues How to do power optimization How to debug suspend/resume issues General method: Capture more PM  debug message Enable PM debug system to get more info about PM in kernel and debug interface Power management options  ---> [*] Power Management Debug Support                                     [*]   Extra PM attributes in sysfs for low-level debugging/testing Enable wakelock debug_mask to capture more message about wakelock root@android:/ # echo 15 > /sys/module/wakelock/parameters/debug_mask root@android:/ # echo 15 > /sys/module/userwakelock/parameters/debug_mask Enable earlysuspend debug_mask to capture more message about early suspend and late resume. root@sabresd_6dq:/ # echo 15 > /sys/module/earlysuspend/parameters/debug_mask Add no_console_suspend=1 to the boot option for kernel This makes the system print more useful info before entry in suspend Eg: --- a/sabresd_6dq/BoardConfig.mk +++ b/sabresd_6dq/BoardConfig.mk -BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale +BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale no_console_suspend=1 System cannot enter suspend mode Check below setting items have been disabled: §  Whether the usb cable has been removed(usb gadget will hold a wake lock) §  Setting->Display->Sleep, check whether the inactivity timeout period setting is longer than your expected time. §  Setting->System->Developer options->stay awake(stay awake not be set), check whether the option is disabled Check if all wake locks have been released(You can see which wake lock is held, and then debug into the specific module): root@sabresd_6dq:/ # cat /sys/power/wake_lock System could not resume from suspend/System crash when resume or suspend Check the PMIC_STBY_REQ signal. System use PMIC_STBY_REQ signal to notify power management IC to change voltage from standby voltage to functional voltage and vice versa. In general, pmic_stby_req pin is connected to pmic standby pin. So measure the pin to check whether the  de-assert signal is triggered. If the signal is not triggered, we may consider whether wake-up sources are correctly setup. If the signal is triggered, we may double-check whether the pmic supply power normally. And not limited to the two points, we should also double-check everything we doubt according to the system log and hardware measured waves.  Using Trace32 or ICE to locate the problem. Please view trace32 website to get more details. Track from mx6_suspend_enter in arch/arm/mach-mx6 .                Track "state" value and try to map to different the low power mode via function mxc_cpu_lp_set.                Check "mx6_suspend.S" which conduct the detailed operations in suspend: "MEM" is mapped to "dormant" mode. So goto "dormant" symbol and try to dump different operations to narrow down suspend/resume failure If this failure maybe related to DDR operation, try to dummy DDR IO relative low power operation. Using ram console to dump kernel log after reboot. Ram console will keep one kernel log copy into one certain memory space. You can use the following command to check last time kernel log, if memory power was not cut off during the reboot process. Eg(if it is the first time boot, you cannot find the /proc/last_kmsg file): root@sabresd_6dq:/ # cat /proc/last_kmsg Kernel resume back from suspend but android not This is usually introduced by the wrong key layout file Use getevent/sendevent tool to get power key scan code #getevent  Correct the Keylayout file    system/usr/keylayout/****.kl Correct the scandcode with your power key report value to Match the POWE key Suspend/Resume consume too much time: We can print the specific module name and time consume details, if the module's suspend/resume time consume more than the threshold parameter by read/write /sys/power/device_suspend_time_threshold file. By default, the parameter is setup to 0, via disabled the function. We can enable it by the following command: Eg: root@android:/ # echo 10  > /sys/power/device_suspend_time_threshold This command means that if the module's suspend/resume time consume more than 10 us, the system will print the module's detail out. If you want to know the more details how to implement it on kernel, please check kernel/power/main.c Notes: Can use the shell command to enter different system level low power modes for debug (For more details: you can check Linux_6DQ_RM.pdf): #echo mem > /sys/power/state #echo standby > /sys/power/state How to do power optimization Runtime Mode Check whether CPUFreq and  Bus_freq scale are enabled root@android:/ # cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor root@android:/ # cat /sys/devices/platform/imx_busfreq.0/enable More details about this, please refer to "Documentation/cpu-freq/ governors.txt” . Check whether the system bus is working on your expected frequency. For MX6Q: root@android:/ #  cat /sys/kernel/debug/clock/osc_clk/pll2_528_bus_main_clk/periph_clk/mmdc_ch0_axi_clk/rate Check CPU Loading and Interrupt(cat /proc/interrupts)                root@android:/ #  cat /proc/interrupts                Through this command you can check whether some module will trigger interrupt frequently.  And consider that whether we have some chances to reduce the interrupt count. Check clock tree carefully to see which clocks are not gated off  but no any modules need them. root@android:/ # powerdebug -d -c Reduce GPU frequency.GPU also offered interface to modify the frequency. According to your own product, you can reduce the gpu frequency. Default gpu3DMaxClock is set to 64 in init.rc file, we can tuning a suitable value by ourselves. diff --git a/imx6/etc/init.rc b/imx6/etc/init.rc index 8c420b5..eb11ffe 100755 --- a/imx6/etc/init.rc +++ b/imx6/etc/init.rc @@ -397,6 +397,9 @@ on boot #  Set GPU 3D minimum clock to 3/64     write /sys/module/galcore/parameters/gpu3DMinClock 3 +#  Set GPU 3D maximum clock to 64/64 +   write /sys/module/galcore/parameters/gpu3DMaxClock 64 + Suspend Mode Check whether all devices enter suspend mode or low power mode: Add debug message into devices drivers to check whether all devices driver suspend interface are called Use oscilloscope to measure the related signal (depend on specific device datasheet and custom hw design) to check whether every device enter low power mode Remove devices from the board(or rmmod the device driver) , and do hardware rework to exclude some hardware module if needed. Then we can figure out which module introduced the high consumption, and debug into the specific module. Add debug message in device drivers which may lead high power consumption, catch the waveform from these modules which may impact the high power consumption Check whether DDR enter in self-refresh mode(Please check the DDR datasheet to figure out which pin indicate self-refresh state, and check it with oscilloscope) Config GPIO PADs as output zero or input mode (depending to HW design) Cut off LDOs/DCDCs which no modules need (depending to HW design) Check all PLLs will cut off, just 32KHZ sleep clock living
View full article
Here are my experiences for compiling Qt5.3.0-beta1 on Yocto. Special thanks to Martin Jansa, the maintainer of the meta-qt5 layer and his help on this. My original procedure was based on this tutorial: Building Qt5 using yocto on Wandboard - Wandboard Wiki Reason: Qt5.3 contains a nice new plugin that allows the use of gstreamer output for textures without the CPU intensive step of copying them (Gerrit Code Review). This allows to play even full HD videos and apply all the power of Qt5 (e.g. shaders) to them. Steps: Setup your repo: repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b master-next; repo sync Download meta-qt5 branch: cd sources; git clone -b jansa/qt5-5.3.0-beta1 https://github.com/meta-qt5/meta-qt5.git Checkout a specific revision: cd meta-qt5; git checkout 92be18a3a14deed9d38b8fc6e89f09ba4d730597 Apply the following patch (maybe later no longer needed): diff --git a/recipes-qt/qt5/qt5.inc b/recipes-qt/qt5/qt5.inc index dfc1c76..a2f9a73 100644 --- a/recipes-qt/qt5/qt5.inc +++ b/recipes-qt/qt5/qt5.inc @@ -54,6 +54,7 @@ FILES_${PN}-tools-dbg = " \ " FILES_${PN}-plugins-dbg = " \      ${OE_QMAKE_PATH_PLUGINS}/*/.debug/* \ +    ${OE_QMAKE_PATH_PLUGINS}/*/*/.debug/* \ " # extra packages @@ -98,6 +99,7 @@ FILES_${PN}-tools = " \ " FILES_${PN}-plugins = " \      ${OE_QMAKE_PATH_PLUGINS}/*/*${SOLIBSDEV} \ +    ${OE_QMAKE_PATH_PLUGINS}/*/*/*${SOLIBSDEV} \ " FILES_${PN}-mkspecs = "\      ${OE_QMAKE_PATH_ARCHDATA}/mkspecs \ Define your machine: export MACHINE=xxx (replace with your board) Setup build environment: cd .. ; . setup-environment build edit your local layer conf ("conf/bblayers.conf") and add the following two lines:   ${BSPDIR}/sources/meta-openembedded/meta-ruby \   ${BSPDIR}/sources/meta-qt5 \ edit your local.conf and add the following lines: DISTRO_FEATURES_remove = "x11 wayland" IMAGE_INSTALL_append = " \     firmware-imx-vpu-imx6q \     firmware-imx-vpu-imx6d \ " IMAGE_INSTALL_append = " \     cpufrequtils \     nano \     packagegroup-fsl-gstreamer \     packagegroup-fsl-tools-testapps \     packagegroup-fsl-tools-benchmark \     gstreamer \     gst-plugins-base-app \     gst-plugins-base \     gst-plugins-good \     gst-plugins-good-rtsp \     gst-plugins-good-udp \     gst-plugins-good-rtpmanager \     gst-plugins-good-rtp \     gst-plugins-good-video4linux2 \     qtbase-fonts \     qtbase-plugins \     qtbase-tools \     qtbase-examples \     qtdeclarative \     qtdeclarative-plugins \     qtdeclarative-tools \     qtdeclarative-examples \     qtdeclarative-qmlplugins \     qtmultimedia \     qtmultimedia-plugins \     qtmultimedia-examples \     qtmultimedia-qmlplugins \     qtsvg \     qtsvg-plugins \     qtsensors \     qtimageformats-plugins \     qtsystems \     qtsystems-tools \     qtsystems-examples \     qtsystems-qmlplugins \     qtscript \     qt3d \     qt3d-examples \     qt3d-qmlplugins \     qt3d-tools \     qtwebkit \     qtwebkit-examples-examples \     qtwebkit-qmlplugins \     cinematicexperience \     " PACKAGECONFIG_append_pn-qtmultimedia = " gstreamer010" QT5_VERSION = "5.2.1+5.3.0-beta1+git%" PREFERRED_VERSION_qtbase-native = "${QT5_VERSION}" PREFERRED_VERSION_qtbase = "${QT5_VERSION}" PREFERRED_VERSION_qtdeclarative = "${QT5_VERSION}" PREFERRED_VERSION_qtjsbackend = "${QT5_VERSION}" PREFERRED_VERSION_qtjsbackend-native = "${QT5_VERSION}" PREFERRED_VERSION_qtgraphicaleffects = "${QT5_VERSION}" PREFERRED_VERSION_qtimageformats = "${QT5_VERSION}" PREFERRED_VERSION_qtmultimedia = "${QT5_VERSION}" PREFERRED_VERSION_qtquick1 = "${QT5_VERSION}" PREFERRED_VERSION_qtquickcontrols = "${QT5_VERSION}" PREFERRED_VERSION_qtsensors = "${QT5_VERSION}" PREFERRED_VERSION_qtserialport = "${QT5_VERSION}" PREFERRED_VERSION_qtscript = "${QT5_VERSION}" PREFERRED_VERSION_qtsvg = "${QT5_VERSION}" PREFERRED_VERSION_qttools-native = "${QT5_VERSION}" PREFERRED_VERSION_qtwebkit = "${QT5_VERSION}" PREFERRED_VERSION_qtwebkit-examples = "${QT5_VERSION}" PREFERRED_VERSION_qtxmlpatterns = "${QT5_VERSION}" build an image: bitbake core-image-minimal This image will build QT5.3 for framebuffer. If you want to use it with X11, then adapt according to this tutorial: Integrate Qt5 into yocto sato image on Wandboard - Wandboard Wiki Please tell me, if I missed something. I wrote this as I remembered the steps.
View full article
This is the prototype solution to enable second display showing different things on JB4.2.2 SabreSD. Make use of Class Presentation provided by android to be embedded into Status bar. When unlock the screen, the Presentation will show on second display. Now, the solution requires one .mp4 video placed in root sdcard. Of course, you may change it to show anything. The attached Files are a layout xml file, a patch and a recorded video. The layout file should be put into android/frameworks/base/packages/SystemUI/res/layout/ folder. The patch should be applied to frameworks/base.git. The recorded video shows the dual display demo as a reference.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345680 
View full article
When I use QMediaPlayer (Qt5.1.1) to play a FHD video, the CPU (imx6dl) usage turns very high and the output is not fluid and also has some frame drop. I found a patch that claims to solve this problem (links below are taking about the same thing) : adding zero-copy-QSGVideoNode for imx6 - Qt by Digia https://www.mail-archive.com/[email protected]/msg08580.html After patch appliance and recompilation of Qt Library and program rebuild, the performance issue remains the same. Does anybody know how to enable this property correctly? Have I missed some points or mandatory steps? Any comment will be appreciated, thanks!
View full article
hi daiane       find the attached log of gstreamer
View full article
The i.MX 6 D/Q/DL/S/SL  Linux L3.0.101_4.1.1 Patch release is now available on [www.freescale.com]www.freescale.com ·          Target HW boards o   i.MX6DL  SABRE SD board o   i.MX6Q  SABRE SD board o   i.MX6DQ SABRE AI board o   i.MX6DL SABRE AI board o   i.MX6SL EVK board This patch release is based on the i.MX 6 Linux 3.0.35_4.1.0 release. The purposes of this patch release are as follows: ·         To fix the BSP multimedia GPU bugs ·         To upgrade the Linux kernel to v3.0.101 ·         To upgrade the multimedia library ·         To upgrade the GPU driver and library to 4.6.9p13 Please consult the release notes for more details. ​
View full article
OpenCV (Open Source Computer Vision Library) is released under a BSD license and hence it’s free for both academic and commercial use. It has C++, C, Python and Java interfaces and supports Windows, Linux, Mac OS, iOS and Android. OpenCV was designed for computational efficiency and with a strong focus on real-time applications. Written in optimized C/C++, the library can take advantage of multi-core processing. Enabled with OpenCL, it can take advantage of the hardware acceleration of the underlying heterogeneous compute platform In current bsp , which supports opencv 2.4, but some customer wants to use the opencv 3.1, then one can use the morty yocto bsp to install the opencv. step 1: for how to install the package on ubuntu and how to build the environment, pls refer to the bsp user guide, for how to build the branch morty, try to use the command as below: MACHINE=imx6qsabresd source fsl-setup-release.sh -b build_qt5 -e fb step 2: for how to enable the opencv, pls add the command as below in the local.conf, the path is fsl-release-bsp/build/conf, "CORE_IMAGE_EXTRA_INSTALL += "libopencv-core-dev libopencv-highgui-dev libopencv-imgproc-dev libopencv-objdetect-dev libopencv-ml-dev" CORE_IMAGE_EXTRA_INSTALL += "opencv-apps opencv-dev python-opencv python-modules"" then build again by bitbake. then you can find the image in the fsl-release-bsp/build/tmp/deploy/images/im6qsabresd/, one can find the opencv libary when extracting the rootfs file step 3: then you can use dd command or mfgtool downloading the image file to the board and use the opencv libary file. other usage: one can install the populate_sdk to build the source code, for opencv 3.1, maybe you will find some g++ issue to fix, so just simple introduce this use the command: bitbake -c populate_sdk fsl-image-gui(for example)  then you can find the sdk install file in the fsl-release-bsp/build_x11/tmp/deploy/sdk, run the install file, set the installation file in the /opt/poky, then you can find the toolchain in the /opt/poky after install successfully.
View full article
New i.mx6Q core board from OpenEmbed.com
View full article
In every i.MX BSP you will find a pre-compiled binary to flash on your board, but if you need to recompile, this tutorial will be useful. Redboot source code and pre-built images for many platforms are available on Linux Board Support Package (BSP). As an example, let's compile redboot version 2009_10 that comes with Freescale Linux BSP.   For detailed information about Redboot, check <redboot_folder>/doc Locate the file ecostools.tar.gz and decompress it on /opt directory. (Create this folder if it is not there) $ cd /opt $ sudo tar zxvf <redboot_folder>/tools/ecos_config_tools.tar.gz $ sudo tar zxvf <redboot_folder>/tools/arm-2008q1.tar.gz This creates /opt/ecostools directory with two subdirectories: arm-2008q1 -- GNU tools for compiling, linking, etc. tools -- mainly to have ecosconfig utility program Add /opt/arm-2008q1/bin and /opt/tools/bin to your environment PATH variable. $ export PATH=$PATH:/opt/arm-2008q1/bin:/opt/tools/bin Generating RedBoot Image Decompress the ecos-trunk-080727.tar.bz2 base line source code into <redboot_folder>/src. There should be a 'packages' directory under <redboot_folder>/src/ecos if it is done correctly. $ tar xjvf ecos-trunk-080727.tar.bz2 Go to ecos subdirectory and apply the patches; $ cd ecos $ bunzip2 -c patch-redboot-200910-base.bz2 | patch -p1 The above command assumes the patch file is under the same directory as the <redboot_folder>/src/ecos. Specify the path name for the patch file if necessary. Apply the patch for specific platform. In this case, the used patch is: patch-redboot-200834-mx3.bz2 $ patch-redboot-200910-mx3.bz2 | patch -p1 Define the ECOS_REPOSITORY. On <redboot_folder>, put the entire (absolute) path to redboot folder. I.e. ~/<redboot_folder>/src/ecos/packages $ export ECOS_REPOSITORY=<redboot_folder>/src/ecos/packages To build redboot (for i.MX31 in this example), create a new folder in order to have a clean build: $ mkdir new_redboot $ cd new_redboot $ ecosconfig new mx31_3stack redboot $ ecosconfig import $ECOS_REPOSITORY/hal/arm/mx31/3stack/current/misc/redboot_ROMRAM.ecm $ ecosconfig tree $ make This creates the Redboot image (redboot.bin) under install/bin directory. This image can run from either SDRAM or flash. Note: You can change the board MACH-TYPE at this file: src/ecos/packages/hal/arm/mx27/ads/current/cdl/hal_arm_board.cdl
View full article
Continental Yocto Training Author:           Leonardo Sandoval Material: PDF Tutorial: i.MX Yocto Project: Freescale Yocto Project Tutorial Provided Virtual Machine Wandboard Dual Wandboard - Freescale i.MX6 ARM Cortex-A9 Opensource Community Development Board - BLOG Tasks: Task 1: Build and Boot your board in N-steps     1.    Create a new folder ($ mkdir conti-fsl-community-bsp)     2.    Follow all N-steps (from the tutorial, page 2) EXCEPT the baking     3.     Baking has been done for you, so assume that the bake is done!     4.    Flash:         conti-fsl-community-bsp $ cd         $ cd fsl-community-bsp/build         build $ dd if=tmp/deploy/images/core-image-minimal-wandboard-dual.sdcard of=/dev/sdb bs=1M         build $ sync # NEVER FORGET THIS STEP, You have been warned!     5.    Boot         Task 2:    Folders     1. Tree structure & size         fsl-comunity-bsp $ tree -d -L 2         fsl-comunity-bsp $ du -h --max-depth=2 Task 3:    Architecture Task 4:    Metadata Task 5:    Config files         build $ cat conf/local.conf         build $ cat conf/bblayer.conf Task 6:     Layers build $ bitbake-layers show-layers sources $ cat meta-fsl-arm/conf/layer.conf Task 7:    Adding an existing layer     1. Clone the repo sources $ git clone https://github.com/lsandoval/meta-fsl-test.git     2. Add the layer to build/bblayers.conf sources $ cd ../build build $ vi conf/bblayers.conf     3. Browse the new layer files     4. Compile the kernel build $ bitbake -f -c compile linux-wandboard build $ bitbake -c deploy linux-wandboard     5. Flash    build $ sudo mkdir /media/boot         build $ sudo mount /dev/sdb1 /media/boot         build $ cp tmp/deploy/images/uImage /media/boot         build $ sudo umount /media/boot     6. Boot Task 8: (Optional) Check the core-image-minimal-test image, bake and flash it. Run the 'helloworld' app Task 9: Q&A
View full article
RidgeRun provides a fully featured Embedded Linux Software Development Kit for Freescale iMX6 based applications processors. Freescale iMX6 platform delivers high performance, power efficient applications processors with a robust support network and software portfolio including open source. The complete platform allows for differentiation and rapid development of applications from wireless handsets to other multimedia-enhanced devices. The i.MX6 series processors are a scalable multicore platform that includes single-, dual- and quad-core families based on the ARM® Cortex™-A9 architecture. This architecture is a robust - cross industry and product platform. Whether your product is targeted at consumer electronics, industrial, automotive or security related, this flexible, scalable architecture combined with RidgeRun's easy-to-use SDK's and extension products allows you to concentrate your effort of differentiating features and not product infrastructure. FEATURES Boot loader 2013.07 Linux kernel 3.0.35-4.0.0 Gstreamer-0.10.36 Freescale gst-plugins 3.0.7 Hardware based audio and video codecs SD and NFS file system support Boot from SD3, SD4 or SPI-NOR with an easy installation (Boundary devices boards only) Toolchain to linaro 2012.03 for software floating point and 2013.03 for hardware floating point support For more info please contact: [email protected] or Please Click -> Contact Us
View full article
The i.MX27 Application Development System (MCIMX27ADSE) is a development tool which is designed to run software applications designed for the i.MX27 processor. Features i.MX27 Multimedia Application Processor Two clock-source crystals, 32 KHz and 26 MHz Power management & Audio IC (MC13783) included battery charging, 10bit ADC, buck switchers, boost switcher, regulators, amplifiers, CODEC, SSI audio bus, real time clock, SPI control bus, USB OTG transceiver & touchscreen interface Multi-ICE debug support Two 512Mbit DDR-SDRAM devices, configured as one 128MB, 32-bit device One 256Mbit Burst Flash with 128Mbit Pseudo Static RAM (PSRAM) memory device, configured as one 16MB flash with 8MB PSRAM, 16-bit device An single board system with connections for LCD display panel, Keypad and Image sensor. Complex Programmable Logic Device (CPLD) for reducing glue logic interface Software readable board revisions Configuration and user definable DIP switches Two SD/MMC, MS memory card connectors PCMCIA & ATA Hard Disk Drive (HDD) Two RS-232 transceivers and DB9 connectors (one configured for DCE and one for DTE operation) supporting on-chip UART ports External UART with RS-232 transceiver and DB9 connector Infrared transceiver that conforms to Specification 1.4 of the Infrared Data Association USB Host (HS & FS), USB OTG (HS & HS) interface Separate LCD panel assembly that connects to the main board Separate keypad unit with 36 push button keys Separate CMOS Image Sensor Card A 3.5 mm headset jack, a 3.5 mm line out jack, a 3.5 mm line in jack, a 3.5 mm microphone jack and a 2.5 mm microphone and headset jack Cirrus Logic CS8900A-CQ3Z Ethernet controller (10BASE-T), with RJ-45 connector AMD AM79C874 NetPHY (10BASE-T & 100BASE-X), with RJ-45 connector Two 32 × 3-pin DIN expansion connectors with most i.MX27 I/O signals Variable resistor for emulation of a battery voltage level NAND Flash card (Plugs into Main Board) which is included in the ADS kit LED indicators for power, Ethernet activity, and two LEDs for user defined status indication Universal power supply with 5 volt output @ 5 Amperes USB, RS-232 and RJ45 cables available in kit Kit Contains a main board an LCD display panel a keypad a NAND flash card an image sensor a TV encoder card, etc It supports application software, target-board debugging or optional extra memory.
View full article
File related to the following question: MX53 u-boot Splash Screen support
View full article
In Chinese Twitter: Sino Weibo, one famous distributor mentioned “i.MX28 is the best choice in ARM9 core-based processor, no ‘one of’”. With high integration of analog module and digital module, i.MX28 is attracting more and more engineers in various applications. Despite its advantage, there are some mistakes one may commit or issues they may meet. The note records a number of issues/mistakes. Each case in the note comes from a real story. I hope the note will help you in your development work. And It is definitely welcomed for everyone to add your own content to the note.The more you share, the more you get.
View full article
Question: How is mx6 PMIC_ON_REQ under SW control? mx6 PMIC_ON_REQ is hooked up to the PFUZE100's PWRON and Linux and our 3.0.35bsp is used. Mx6 SW control is to drive the PMIC_ON_REQ pin low.  It appears from the documentation that this pin can be controlled by either another imx6 pin OR through SW control. The issue is that the reference manual is not clear on how to do this. While doing an SR search (SR 1-877711457), it does appear the PMIC_ON_REQ is controlled by SW. Answer: In latest RM version, Figure 60-3. Chip on/off state flow diagram and Table 60-3. Power mode transitions in IMX6DQRM.pdf show two ways to make PMIC_ON_REQ go low. I'm sure in latest BSP SW method had been included. It turns out the SNVS module on the mx6s/dl is different from the mx6q/d which is again different from the mx6slx. The bottom line is that the requirements for the SNVS functionality came primarily from the Android market so many of the Linux use cases are not supported. SW control of the PMIC_ON_REQ pin is an example of this. This means that you are correct, there only 2 ways to get PMIC_ON_REQ to power up for the mx6q/d 1 -  a low on the ON/OFF pin greater than the debounce time (750ms) 2 - a wake-up/tamper event. For the mx6s/dl, there are 3 ways to get PMIC_ON_REQ to power up 1 - power-on-reset on the VSNVS  (i.e first applying VSNVS) 2 -  a low on the ON/OFF pin greater than the debounce time (750ms) 3 - a wake-up/tamper event. Note, in my case, where there is an external input that actually wakes up the system, turns on the PMIC and brings up the mx6 there is only 1 way to get PMIC_ON_REQ to go back high 1 - a low on the ON/OFF pin greater than the debounce time (750ms) As it turns out, when the VSNVS_HP section is powered (i.e VDDHIGH is applied), it gates off the wake-up timer.
View full article
       Overview The purpose of this document is to describe how to enable Bluetooth on i.MX 6Dual/Quad SabreSD board (RevC) for Android software. Hardware Changes i.MX 6Dual/Quad SabreSD board doesn't enable Bluetooth connection by default. To support bluetooth, the hardware rework is required. The above diagram shows the reserved connections for Bluetooth in SabreSD RevC board (All connections are marked as "DNP"). This Bluetooth cable connector is designed specifically for the WiFi/BT combo card SX-SDCAN-2830BT which is developed and sold by Silex Technology. Note that pin 1 (BT_DISABLE) of the cable connector on i.MX 6Dual/Quad SabreSD RevC is opposite Pin 20 of the WiFi/BT module. Note: when connecting Silex module and J13, the connection is reverted (For example, PIN 1 in J13 connects to PIN 20 in Silex module). To use the J13 connector, the following reworks are required:   R209-R211, R214-R215 need to be populated.           Where is them, you can refer to the below chart.   SPI nor flash U14 need to be depopulated. No other AUX boards should be connected.. Exchange UART5_RXD and UART5_TXD. Orange PAD connects to Orange PAD. Green PAD connects to Green PAD.      After hardware rework, the Bluetooth connection will like the following:   Pin on Silex Module Sabresd Board Mux Pad Pin-2  BT_UART_RTS  (output) UART5.RTS   (input) MX6Q_PAD_KEY_COL4__UART5_RTS Pin-3  BT_UART_TXD   (output) UART5.RXD   (input) MX6Q_PAD_KEY_ROW1__UART5_RXD Pin-4  BT_UART_CTS   (input) UART5.CTS   (output) MX6Q_PAD_KEY_ROW4__UART5_CTS Pin-5  BT_UART_RXD   (input) UART5.TXD   (output) MX6Q_PAD_KEY_COL1__UART5_TXD Pin-14  BT_PWD_L       (input) GPIO_2         (output) MX6Q_PAD_GPIO_2__GPIO_1_2   Software Information For earlier android version before Jelly Bean4.2 Take ICS as an example, for we didn't do this work when our last ICS version R13.4.1 released. So our formal release had no support on BT. Here will give out patches based on R13.4.1. Enable Bluetooth with the following setting (e.g. device/fsl/imx6/sabresd/init.rc)      # No bluetooth hardware present -    setprop hw.bluetooth 0 +    setprop hw.bluetooth 1 Ensure BOARD_HAVE_BLUETOOTH := true in device/fsl/imx6/sabresd/SabreSDBoardConfigComm.mk. Add BT feature support in device/fsl/imx6/sabresd/required_hardware.xml: <permissions>      <feature name="android.hardware.camera" /> +    <feature name="android.hardware.bluetooth" />   Add UART5 support in kernel: In this step you can refer to the attached (kernel patch for UART5 based on ICS.zip) to change PinMux PAD configuration for UART5.   Add AR3002 BT firmware support: Update external/linux-firmware with the attached patch(0001-ENGR00270791-BT-add-AR3002-firmware-support.patch) to add AR3002 BT firmware support for Silex's BT is AR3002.   Then you can manually run the command “hciattach -n -s 115200 /dev/ttymxc4 ath3k 115200 flow nosleep” in console to see whether bluetooth can attach HCI successfully.   At last, you need add rfkill for BT reset in kernel, here also give a patch for reference: 0001-ENGR00270791-BT-add-rfkill-for-bt-reset.patch   BT is not enable in kernel default. You can control whether to enable it in bootargs like the following  in device/fsl/sabresd_6dq/BoardConfig.mk. BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale  bluetooth For android version since Jelly Bean4.2 From Jelly Bean4.2, Bluez is no longer used.Android provides a default Bluetooth stack, BlueDroid, that is divided into two layers: The Bluetooth Embedded System (BTE), which implements the core Bluetooth functionality and the Bluetooth Application Layer (BTA), which communicates with Android framework applications. A Bluetooth system service communicates with the Bluetooth stack through JNI and with applications through Binder IPC. The system service provides developers access to various Bluetooth profiles. The following diagram shows the general structure of the Bluetooth stack: For bluedroid, we have supported it in our formal release including Android4.3. You can get it from our website. Or just get HAL code from attached(libbt-ath3k.zip). Known issue For  KEY_COL4 is both used by uart5 and pcie,  if you enable BT, 3G  mobile will not work. For its power disable pin is conflict with uart5's UART_RTS. This is also why we didn't enable BT in formal release. Supported and tested profile workable profile not tested profile Hid Handset & Handfree(not support for hardware restrict) A2DP Pbap Opp Pan
View full article