iMX 6 D/Q/DL/S/SL Linux 3.0.101_4.1.1 Patch Release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX 6 D/Q/DL/S/SL Linux 3.0.101_4.1.1 Patch Release

iMX 6 D/Q/DL/S/SL Linux 3.0.101_4.1.1 Patch Release

The i.MX 6 D/Q/DL/S/SL  Linux L3.0.101_4.1.1 Patch release is now available on [www.freescale.com]www.freescale.com

·          Target HW boards

o   i.MX6DL  SABRE SD board

o   i.MX6Q  SABRE SD board

o   i.MX6DQ SABRE AI board

o   i.MX6DL SABRE AI board

o   i.MX6SL EVK board

This patch release is based on the i.MX 6 Linux 3.0.35_4.1.0 release. The purposes of this patch release are as follows:

·         To fix the BSP multimedia GPU bugs

·         To upgrade the Linux kernel to v3.0.101

·         To upgrade the multimedia library

·         To upgrade the GPU driver and library to 4.6.9p13

Please consult the release notes for more details.

Labels (1)
Tags (1)
No ratings
Version history
Last update:
‎11-04-2014 09:57 AM
Updated by: