i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
Note: This guide is specifically for use with VS Code. For standalone with Segger software please refer to this guide. (How to Use Segger J-Link Plus with i.MX 8M Process... - NXP Community) In this guide we will describe the process to start using VS Code to debug an SDK application. The board used for this guide specifically is the i.MX 8M Nano EVK, but it also applies to all processors of the i.MX 8M Family. This guide covers the following topics: Hardware requirements Software requirements How to find, build, and download the i.MX SDK Debug Probe and i.MX 8M Nano EVK connection Create an SDK Application with MCUXpresso for VS Code Run and debug your SDK Application with MCUXpresso for VS Code Hardware requirements Evaluation Kit for the i.MX8M Nano Applications Processor (i.MX 8M Nano Evaluation Kit | NXP Semiconductors) Quick Start Guide for i.MX8M Nano (I.MX 8M Nano EVK Quick Start Guide (nxp.com)) J-Link Plus JTAG/SWD debug probe with USB interface (SEGGER J-Link PLUS) Features Download speed up to 1MB/s Unlimited breakpoints in flash memory Supports direct download into RAM and flash memory Supported NXP Devices Supported Devices - Search results "nxp" (segger.com) 9 Pin Cortex-M Adapter (9-Pin Cortex-M Adapter (segger.com)) Description Adapts from the 20-pin 0.1'' JTAG connector to a 9-pin 0.05'' Samtec FTSH connector as defined by Arm. Software requirements Windows 10 OS (host) J-Link Software and Documentation Pack for Windows (https://www.segger.com/products/debug-probes/j-link/models/j-link-plus/) i.MX 8M Nano SDK (Welcome | MCUXpresso SDK Builder (nxp.com)) VS Code for Windows (Installation Guide: Running Visual Studio Code on Windows) MCUXpresso Extension for VS Code (Installation Guide: Training: Walkthrough of MCUXpresso for VS Code - NXP Community)   How to find, build, and download the i.MX 8M Nano SDK Enter Welcome | MCUXpresso SDK Builder (nxp.com) Click on "Select Development Board"  Select EVK-MIMX8MN (MIMX8MN6xxxJZ) from Boards -> i.MX -> EVK-MIMX8MN Click on the Build MCUXpresso SDK button Click on Download SDK, you'll be redirected to the MCUXpresso SDK Dashboard Look for the i.MX 8M Nano SDK and click on Download SDK Click on Download SDK archive and documentation, accept the Software Terms and Conditions and the .zip file for the SDK will be downloaded. Debug Probe and i.MX 8M Nano EVK connection Connect the debug cable (USB-UART) to the board and the other end to your PC. Connect the power cable to the second USB-C port and to a wall socket. Don't turn on the board yet. Connect the JLink Plus to your PC with the USB cable. Connect the JLink Plus to the JTAG of the i.MX 8M Nano EVK board In this part we will need to identify pin number 1 from the 9 Pin Cortex-M adapter and from the i.MX 8M Nano EVK board. For the first one identifies pin 7 identifiable by a "non-connect pin". For the i.MX 8M Nano, you can identify easily with a number 1 in one corner of the connectors.    The whole setup should look similar to this:   Create an SDK Application with MCUXpresso for VS Code Before delving into the details of creating an SDK Application it is important to recognize the sections of VS Code User Interface. This will help us to describe accurately the buttons' position. Click on MCUXpresso for VS Code extension icon from the Activity Bar.  In the section “Quickstart Panel” located in the Side Bar click on “Import Repository.” On this window, go to “Local” and select your previously downloaded SDK folder location. Then, click on “Import.” Expand the section “Installed Repositories” from Side Bar and verify your selected SDK. Expand the section “Projects” from Side Bar and click on “Import Example from Repository” and complete the options: Choose a toolchain Choose a board Choose a template Name Location Finally, click on the "Create" button. Click on the gear icon located in the project folder to build the code. In “Projects” expand the “Settings” options and select “mcuxpresso-tools.json.” Here you will find a JSON file with different parameters. Defines the device that will be used to connect with the J-Link Plus. Code: “segger”: { “device”: “MIMX8MN6_M7” } Expand the section “Debug Probes” and verify that your J-Link Plus debug probe appears. Start SEGGER J-Link GDB Server. On section “Target Device” select MIMX8MN6_M7 and click “OK”. You will see the following window. Run and debug your SDK Application with MCUXpresso for VS Code Click on “Debug” located in the project folder, to start with the debugging session. In the Panel click on “Serial Monitor,” set it to the serial debug port with the lowest numbered port with the following settings: Baud rate: 115200 Line ending: None Click on "Start Monitoring" Use the debug controls to run the code. Verify your code output in the “Serial Monitor.”
記事全体を表示
Dynamic debug is designed to allow you to dynamically at runtime  enable/disable  kernel code to obtain additional kernel information. Currently, if ``CONFIG_DYNAMIC_DEBUG`` is set, then all ``pr_debug()``/``dev_dbg()`` and ``print_hex_dump_debug()``/``print_hex_dump_bytes()`` calls can be dynamically enabled per-callsite.    
記事全体を表示
Note: This guide is specifically for use with Segger software. For steps to use with the MCUXpresso extension for VSCode please refer to How to Use Segger J-Link Plus with i.MX 8M Process... - NXP Community This guide aims to be a technical reference to start using the SEGGER J-Link Plus debug probe on the i.MX 8M Family processors. The board used for this guide specifically is the i.MX 8M Nano EVK, but it also applies to all processors of the i.MX 8M Family. Here we will describe the process using the following structure: Hardware requirements Software requirements How to find, build, and download the i.MX SDK Host setup Build an example application Target setup Run an example application Hardware requirements Evaluation Kit for the i.MX8M Nano Applications Processor (i.MX 8M Nano Evaluation Kit | NXP Semiconductors) Quick Start Guide for i.MX8M Nano (I.MX 8M Nano EVK Quick Start Guide (nxp.com)) J-Link Plus JTAG/SWD debug probe with USB interface (SEGGER J-Link PLUS) Features Download speed up to 1MB/s Unlimited breakpoints in flash memory Supports direct download into RAM and flash memory Supported NXP Devices Supported Devices - Search results "nxp" (segger.com) 9 Pin Cortex-M Adapter (9-Pin Cortex-M Adapter (segger.com)) Description Adapts from the 20-pin 0.1'' JTAG connector to a 9-pin 0.05'' Samtec FTSH connector as defined by Arm. Software requirements Windows 10 OS (host) J-Link Software and Documentation Pack for Windows (https://www.segger.com/products/debug-probes/j-link/models/j-link-plus/) i.MX 8M Nano SDK (Welcome | MCUXpresso SDK Builder (nxp.com)) MinGW CMake GNU ARM Embedded Toolchain Terminal Emulator for serial port connection (Tera Term, PuTTY, etc.)   How to find, build, and download the i.MX 8M Nano SDK Enter Welcome | MCUXpresso SDK Builder (nxp.com) Click on "Select Development Board"  Select EVK-MIMX8MN (MIMX8MN6xxxJZ) from Boards -> i.MX -> EVK-MIMX8MN Click on the Build MCUXpresso SDK button Click on Download SDK, you'll be redirected to the MCUXpresso SDK Dashboard Look for the i.MX 8M Nano SDK and click on Download SDK Click on Download SDK archive and documentation, accept the Software Terms and Conditions and the .zip file for the SDK will be downloaded.   Host Setup J-Link Software and Documentation Pack for Windows Download J-Link Software and Documentation Pack for Windows (https://www.segger.com/products/debug-probes/j-link/models/j-link-plus/) Execute .exe file downloaded and then click on "Next" Follow the installation wizard with default parameters and click on "Finish".   MinGW Download the MinGW installer from MinGW - Minimalist GNU for Windows - Browse /Installer at SourceForge.net. Follow the installer instructions leaving all options in their default values. Click on Continue when the installer finishes. A MinGW Installation Manager window will pop up, select mingw32-base and msys-base from basic setup. Click on the Installation menu and select Apply Changes. On the next window, click on Apply and wait for the package to finish downloading. Add the appropriate item to the Windows operating system path environment variable. It can be found under Control Panel->System and Security->System->Advanced System Settings in the Environment Variables... section. The path is: \bin. Assuming the default installation path, "C:\MinGW". If the path is not set correctly, the toolchain does not work. Note: If you have C:\MinGW\msys\x.x\bin in your PATH variable (as required by KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.   CMake Download CMake Windows x64 Installer from  Download CMake. Scroll down to find the latest release for the installer: Run the installer and follow the instructions. Make sure to check the Add CMake to system PATH for all users option during the installation process. Restart your PC to apply changes. GNU ARM Embedded Toolchain Download the GNU ARM Embedded Toolchain installer from Downloads | GNU Arm Embedded Toolchain Downloads – Arm Developer, scroll down to find the latest release for the installer: Follow the installer instructions and check the Add to PATH option at the end of the process. Add a new system environment variable named ARMGCC_DIR with the GNU ARM embedded Toolchain installation path as its value ARMGCC_DIR=ARMGCC_DIR=C:\Program Files (x86)\GNU Arm Embedded Toolchain\10 2021.10​   Build and example application Press the Windows Key and search for GCC Command Prompt and run it. Change the directory to the example application project directory (inside the armgcc folder), for example: C:\Users/<user>\Documents\8MNANO\boards\evkmimx8mn\demo_apps\hello_world\armgcc Type build_debug.bat on the command line or double click the build_debug.bat file (inside the armgcc folder of the application project) through Windows Explorer Wait for the building process to end and make sure no error messages are shown. Target Setup Connect the debug cable (USB-UART) to the board and the other end to your PC. Connect the power cable to the second USB-C port and to a wall socket. Don't turn on the board yet. Connect the JLink Plus to your PC with the USB cable. Connect the JLink Plus to the JTAG of the i.MX 8M Nano EVK board In this part we will need to identify pin number 1 from the 9 Pin Cortex-M adapter and from the i.MX 8M Nano EVK board. For the first one identify pin 7 identifiable by a "Non-connect pin". For the i.MX 8M Nano, you can identify easily with a number 1 in one corner of the connectors.    The whole setup should look similar to this: Run an example application Open a terminal application (TeraTerm, PuTTY, etc.) on your host PC and set it to the serial debug port with the lowest numbered port with the following settings: Speed: 115200 Data: 8-bit Parity: none Stop bits: 1 bit Flow Control: none Start SEGGER J-Link GDB Server. On section “Target Device” select MIMX8MN6_M7 and click “OK”. You will see the following window. Open a new instance of GCC Command Prompt. Change to the directory with the example previously compiled. Here is the path to folder that contains the files: <install_dir>/boards/<boad_name>/<example_type>/<application_name>/armgcc/debug​ Run the command: arm-none-eabi-gdb.exe <application_name>.elf.​ Example: At this point you are in the GDB Command Prompt, run the following commands: target remote localhost:2331 monitor reset monitor halt load monitor go The application will be now running and you can see the “hello world” on your terminal (PuTTY,Tera Term, etc.).  
記事全体を表示
The default BSP is compiled based on the Yocto project, which is a streamlined production-level Linux BSP. However, for users who are accustomed to the Ubuntu environment, especially ROS users, the operation of Yocto will be relatively complicated. This article will introduce how to make an Ubuntu BSP for iMX8QM and demonstrate how to use ROS.   A complete Ubuntu BSP includes u-boot, Linux kernel and Ubuntu rootfs. We will use u-boot and Linux kernel in Yocto BSP official 6.1V BSP, and rootfs will still use ubuntu-base-18.04.4-base-arm64. The compilation method comes from the NXP forum. First download ubuntu-base-18.04.4-base-arm64.tar.gz from the link above, and then unzip it. $ mkdir ~/ubuntu-rootfs $ sudo tar vxf ubuntu-base-18.04.4-base-arm64.tar.gz -C ubuntu-rootfs Copy the script file and create ch-mount.sh. $ sudo chmod a+x ./ch-mount.sh The download above is a basic Ubuntu-base file system, which is missing many commonly used tools and requires us to install it. For this purpose, install the qemu-user-static software on your computer to simulate the arm64 operating environment. $ sudo apt install qemu-user-static Mount the Ubuntu-base file system and then operate directly in the arm64 environment. $ sudo ./ch-mount.sh -m ubuntu-rootfs/ Add a DNS server, such as 8.8.8.8, or other available DNS server IP. # echo nameserver 8.8.8.8 > /etc/resolv.conf Install relevant software, of course you can also add other software. # apt install language-pack-en-base sudo ssh net-tools \ network-manager iputils-ping rsyslog \ bash-completion htop resolvconf dialog \ vim nano v4l-utils alsa-utils git gcc \ less resolvconf autoconf autopoint libtool \ bison flex gtk-doc-tools glib-2.0 \ libglib2.0-dev libpango1.0-dev libatk1.0-dev kmod pciutils -y  Create a user and set a password, here the user name is ubuntu # useradd -s '/bin/bash' -m -G adm,sudo ubuntu # passwd ubuntu # passwd root # echo 'apalis-imx8' > /etc/hostname At this point basic Ubuntu has been configured. # exit $ sudo ./ch-mount.sh -u ubuntu-rootfs/  After the installation is complete, use the ubuntu user to log in to the debugging serial port, and the password is ubuntu. When starting for the first time after installation, it will wait for a long time due to initialization, and then enter the configuration interface including region, user settings, etc. Turn on Ethernet and set DNS server IP.  ubuntu@mx8QM:~$ sudo ifconfig eth0 up ubuntu@mx8QM:~$ sudo dhclient eth0 ubuntu@mx8QM:~$ sudo vi /etc/resolv.conf Start Weston: ubuntu@mx8QM:~$ export XDG_RUNTIME_DIR=/run/user/1000 ubuntu@mx8QM:~$ sudo -E weston --tty=1 & ubuntu@mx8QM:~$ weston-flower ROS test You can install ROS programs very conveniently in Ubuntu system. Please refer to the instructions below for details http://wiki.ros.org/melodic/Installation/Ubuntu http://wiki.ros.org/ROS/Tutorials ubuntu@mx8QM:~$ sudo apt install lsb-core ubuntu@mx8QM:~$ sudo sh -c 'echo "deb http://packages.ros.org/ros/ubuntu $(lsb_release -sc) main" > /etc/apt/sources.list.d/ros-latest.list' ubuntu@mx8QM:~$ sudo apt-key adv --keyserver 'hkp://keyserver.ubuntu.com:80' --recv-key C1CF6E31E6BADE8868B172B4F42ED6FBAB17C654 ubuntu@mx8QM:~$ sudo apt update ubuntu@mx8QM:~$ sudo apt install ros-melodic-desktop  Run the following commands on three SSH terminals to simulate communication between ROS nodes. ubuntu@mx8QM:~$ source /opt/ros/melodic/setup.sh ubuntu@mx8QM:~$ roscore ubuntu@mx8QM:~$ source /opt/ros/melodic/setup.sh ubuntu@mx8QM:~$ rosrun roscpp_tutorials talker ubuntu@mx8QM:~$ source /opt/ros/melodic/setup.sh ubuntu@mx8QM:~$ rosrun roscpp_tutorials listener Due to driver limitations, iMX8 does not support Xorg, so ROS's default graphical interface tools such as rqt cannot be used directly.        
記事全体を表示
1. MediaPlayer Architecture     MediaPlayer is the server, MediaPlayerService and MediaPlayerService :: Client is the client. MediaPlayerService realize the IMediaPlayerService, the main function is to create the right player through the url sent by MediaPlayer::setDataSource MediaPlayerService :: Client realize the IMediaPlayer, the main function is to call the player created by MediaPlayerService to do those specific start, stop, resume, pause…      Entering NuplayerDriver means entering Android MultiMedia Framework.   2. NuPlayer   The playback video is mainly completed through Nuplayer. The figure below includes parser, decoder and render.   NuPlayer::Source is the parser module. Its interface looks like a combination of MediaExtractor and MediaSource NuPlayer::Decoder connects to CCodec for decoding. CCodec has a state pattern and pass MediaBuffers around with messages. NuPlayer::Render is responsible for rendering audio and also controls when to post video buffers back to NativeWindow for A/V sync. 3. Decoding Framework 3.1 Framework of i.MX8MP, i.MX8MQ and i.MX8MM   Decoding Process between the framework, vendor decoder component and kernel as follows on i.MX8MP, i.MX8MQ and i.MX8MM.   3.2 Framework of i.MX8QM   Decoding Process between the framework, vendor decoder component and kernel as follows on i.MX8QM. stream on: start to decode/encode stream off: stop decoding/encoding qbuf:  Queue the v4l2buffer filled in the decoder into the buffer queue created in the vpu driver so that the VPU can obtain it for decoding. dqbuf: When the VPU decoding is completed, the buffer will be dequeueed so that the decoder/codec can continue to be used. 4. Decode Video and Display Process 4.1 i.MX8MM and i.MX8MP   For i.MX8MP and i.MX8MM, G2D is used to composite layers, and the buffer transmission is completed between Decoder and SurfaceFlinger through the BufferQueue mechanism. The process as follows:  BufferQueue: As the producer of BufferQueue, decoder provides the decoded buffer, and SurfaceFlinger, as the consumer of BufferQueue, composite the decoded video layer.  Display: Use G2D to composite Android layer and video layer on i.MX8MP. SurfaceFlinger will hand over all layers to Display HAL, and then composite them into the framebuffer by G2D. 4.2 i.MX8MQ   For i.MX8MQ, GPU3D is used to composite Android UI, DCSS is used to composite overlay and android UI. And the buffer transmission is completed between Decoder and SurfaceFlinger through the BufferQueue mechanism. The processing is as follows: BufferQueue: Decoder provides the decoded buffer as producer. SurfaceFlinger as the cosumer of BufferQueue.  Display: Using GPU3D to composite Android UI layers. And video layer will be submitted to DCSS (Display Controller) through Display HAL. DCSS:  Responsible for combining video overlay and Android UI for display. GLESRenderEngine: SurfaceFlinger calls the opengl interface through GLESRenderEngine to complete rendering composite. 4.3 i.MX8QM For i.MX8QM, GPU3D or DPU are used to composite. And the buffer transmission is completed between Decoder Filter Component and SurfaceFlinger through the BufferQueue mechanism. The processing as follows: Decoder Filter:  Because GPU3D cannot directly composite TILED type layers, it needs to be converted into Linear through Decoder Filter first, and then handed over to SurfaceFlinger. BufferQueue:  Decoder Fillter will receive the outputbuffer from Decoder. And Filter will be as producer of BufferQueue to provide the buffer. SurfaceFlinger will be as consumer of BufferQueue to consume the buffers. GLESRenderEngine: SurfaceFlinger calls the opengl interface through GLESRenderEngine to complete rendering composite. Note:  On i.MX8QM,  Not all situations are composited using the GPU3D. Please refer to the table below.   4.4 DRM Widevine (Secure Decoder)   Now we have enabled DRM Widevine on i.MX8MP/i.MX8MQ/i.MX8QM so that secure video can be played.  For i.MX8MP, Use OEMCrypto trusted application to decrypt the encrypted stream. And Use RDC/CSU to protected hardware for secure pipeline. The framework is as follows:   For i.MX8MQ, Use OEMCrypto trusted application to decrypt the encrypted stream. And Use RDC/CSU to protected hardware for secure pipeline. The framework is as follows:     OEMCrypto: It is a library as tipc client to send the encrypted data to Trusty OS. OEMCrypto Trusted Application: Used to decrypt the protected data into secure memory and send it to Media Framewrok. Secure Framebuffer: It is allocated from secure heap through libdmabufheap. Secure heap: Used to allocate secure memory.  Resources in domain2 can read and write secure memory, but cannot write normal memory. Resources in domain0 can write to secure memory, but cannot read normal memory. When playing secure video, VPU, GPU2D, and lcdif will be in domain2. Or they are in domain0. Resource Domain Controller (RDC): It provides support for the isolation of destination memory mapped locations such as peripherals and memory to a single core, a bus master, or set of cores and bus masters.  CSU Central Security Unit (CSU) : 1. Peripheral Access Policy - the appropriate bus master privilege and identity are required to access each peripheral. 2. Masters Privilege Policy - the CSU overrides the bus master privilege signals (secure/non-secure).  Configure the VPU so that it can only be accessed by the secure world. For i.MX8QM, also use OEMCrypto trusted application to decrypt the encrypted stream. But related hardware and memory are protected through the secure partition created by SCU. The framework is as follows: OEMCrypto: It is a library as tipc client to send the encrypted data to Trusty OS. OEMCrypto Trusted Application: Used to decrypt the protected data into secure memory and send it to Media Framewrok. Secure Framebuffer: It is allocated from secure heap through libdmabufheap. Secure heap: Used to allocate secure memory.  Only Secure partition can access secure memory. Frimware Loader: It is a trusted application in Trusty OS, It is responsible for loading the encrypted firmware into the specified memory. Secure Partition: Secure partitions are created using SCU and all hardware that needs to be protected are moved to secure partitions to isolate it from non-secure partitions. 5. Encoding Process 5.1 Encoding Process on i.MX8MP BufferQueue:  MediaFramework will create Surface and create BufferQueue, SurfaceFlinger will serve as the producer to provide the composite layers, and the Encoder component will encode it as the consumer of the BufferQueue. MPEG4Writer:  Responsible for writing the VPU-encoded data to the output file. 5.2 Encoding Process on i.MX8QM and i.MX8MM   BufferQueue:  MediaFramework will create Surface and create BufferQueue, SurfaceFlinger will serve as the producer to provide the composite layer, and the Encoder Filter component will be as the consumer of the BufferQueue. MPEG4Writer:  Responsible for writing the VPU-encoded data to the output file. 6. Buffer transfer and management 6.1 Transfer and release process of Input Buffer Input Buffer allocation: It is allocated in CCodecBufferChannel, and it is used to allocate inputbuffer and recycled. InputManager: Before the queue buffer into the decoder, it will be registered with the InputManager. When the VPU is finished using it, the InputManager will be notified to release it. Use of InputBuffer:  After the buffer is queued into the decoder, the input buffer information will be copied to v4l2buffer so that the VPU can use it. Note: For DRM Secure decoder, the VPU will only use the paddr of inputbuffer. 6.2 Transfer and release process of Output Buffer     Output Buffer allocation:  When use Surface for output, It is allocated through BufferQueueAllocator that is created in CCodecBufferChannel. It is used to allocate outputBuffer.  Management: When use Surface, OutputBuffer is managed through the BufferQueue mechanism. When the VPU filled the outputBuffer with data that can be displayed, it will notify the Consumer to acquire the buffer. Use of OutputBuffer: In the decoder, the output buffer information will be copied to v4l2buffer so that the VPU can use it. Note:  For situations where OutputSurface is not used, GrallocAllocator is used by default instead of BufferQueueAllocator. 6.3 Buffer Management of Encoder   For screen recording situations, the Encoder's buffer transfer is also managed through the BufferQueue mechanism. After SurfaceFlinger is producer to fill the GraphicBuffer of BufferQueue, the encoder is as consumer to encode the composited data.  
記事全体を表示
Device: i.MX93 A1. ELE FW version: 0.0.10 Some new test scripts are added to secure enclave library, please refer to attached files. Please note: the scripts attached are for internal test/debug purpose only. The summary is from our test results and understanding, it's preliminary and may have changes later.    1. All current and all GA Sentinel FWs do not use lifecycle for key derivation of HSM keystore. Keystore created in OEM_OPEN lifecycle can be directly used in OEM_CLOSED lifecycle.  A-> Different from previous SECO devices 2. Key has lifecycle attribute. This attribute defines in which device lifecycle the key is usable. This attribute is set at key creation operation (generate key, import key, key exchange …). Before executing a key depending cryptographic or data storage (export option) operation the key lifecycle is compared with the current device lifecycle. Operation is executed only if the key lifecycle includes the current device lifecycle. When mentioned in the API command message description, the key lifecycle could be set to the current device lifecycle if the value is set to 0x0. Lifecycle values are encoded as bitfield. Multiple values could be set. The key could be used in several lifecycles.   Tested cases:   The key lifecycle attribute is verified during the key usage, not when the key is created. If the key operation doesn’t match device lifecycle, it will report 0xe29 - The key is not usable in the current lifecycle.  Please see attached hsm_generate_key.c / hsm_generate_key_signature.c  for reference.   3. SYNC operation and MC increase are separate flag. The previous STRICT operation is used to store persistent key, during which the monotonic counter will increase if the device is closed. For ELE device, two flags are used: SYNC flag and MC flag. The ELE SYNC pushes persistent key(s) in the NVM. Without executing this operation, even if the key attribute is set as persistent at the key creation the key will not be stored in the NVM. This operation is set through a flag in key management operations arguments. SYNC is applicable only for persistent key/permanent key. MC flag is new on ELE device. When used in conjunction with SYNC, the request is completed only when the monotonic counter has been updated. MC flag can be used both in OPEN and CLOSED lifecycle and increase the monotonic counter value. -> different from previous SECO device. Note: MC flag is not defined in 0.0.10 secure enclave library, but user can test it by directly setting the corresponding bit of the flag.   4. If the generated key store is deleted accidently and the monotonic counter is not 0, reprovisioning function is needed.  This is applied to both OPEN and CLOSED device. We cannot directly create a keystore again. Reprovisioning method is not supported yet.   5. One keystore can store 100 key groups at most. 100 groups are available per key store. It must be a value in the range [0; 99]. The key group ID should be 0~99, or it will report 0x429- MU sanity check failed / Invalid parameters. To push persistent keys in the NVM, a flag (SYNC) needs to be set during key management operations (generate, import, manage, …). Pushing a key to the NVM will also push all the key group data. When in use, a key group is loaded from the NVM to the internal secure RAM. The number of key group present is limited (depends on the device). A key group present in internal memory and not used, can be swapped out and replaced by a new key group containing the key to be used when there is no more free space. Note that only key 2 groups per key store can be stored in the internal secure RAM. Note that volatile keys cannot be in the same key group than persistent keys.   One assumption based on tests: It looks that each key group has its own SW counter, which may record update time of this key group. This is the test on i.MX93: If we delete the key group #2 file 0000abcd00020004 only from NVM manually, then we cannot create key of group #2 again, but we can create key of group #1. The process might be: Try to create key in group #2 -> checked the counter value is not 0 -> try to import the chunk from NVM -> fail because the chunk is deleted. Each key group has its own counter, so key group #1 is not affected.   6. Key size in one keystore One key group can store 16 ECC(p256) keys, or 1 RSA 2k key, or 1 RSA 4k key. Size of key group on i.MX93 = 8448 bits (size defined to allow 4k modulus+ 4k private exponent + header). Storage file in NVM will have additional overhead, the 8448 size is purely related to key data storage. For ECC keys, only private keys are stored (public key can be derived from private key), so P256 key only needs 256 bits of key storage + 256 bits header = 512 bits. 16 * 512 = 8192 => fits within 8448.    7. Delete key To delete the key from the NVM, an SYNC operation (in “Flags” field) must be done. To delete a key, user need to provide the key identifier which is generated when creating this key. There is also “MC” flag which should can be used for anti-rollback protection. Deleting key will not decrease the size of key group file directly, but the space in the key group will be covered by new key generated later.  Please see attached hsm_delete_key.c for reference.   8. Generic API Generic API is not supported on i.MX93 A0 due to a lack of RAM, it is supported on i.MX93 A1. In lf-6.1.22_2.0.0 ELE library, the generic feature is set as none supported, need to change the src/plat/ele/sab_msg.def file as below to test it on i.MX93 A1 chip. -MT_SAB_GC_AKEY_GEN := ${NOT_SUPPORTED} -MT_SAB_GC_ACRYPTO := ${NOT_SUPPORTED} +MT_SAB_GC_AKEY_GEN := ${FMW} +MT_SAB_GC_ACRYPTO := ${FMW} Generic cryptographic APIs can be used to perform cryptographic operation without using the FW key store. The key buffer, in plaintext, is an input parameter of the API. No need to open hsm keystore before using generic APIs. Because it will not save the key to key store, so NVM thread is also not necessary. Please see attached hsm_generic_api.c for reference. Asymmetric key generate: Only RSA is supported on S401 for now. It will return the address of output RSA key modulus /output RSA private exponent /input RSA public exponent Asymmetric crypto User can choose different operation mode for Encryption / Decryption / Signature generation / Signature verification.    9. How to get chip MC value? Command “Get device information” can be used to get generic information regarding the user, the chip and the EdgeLock Enclave FW. It can return Chip UUID/lifecycle/monotonic counter etc. User can run this API before and after some MC operation to check if the counter value is increased. Please see the attached hsm_get_info.c for reference.   Best Regards, Tia
記事全体を表示
SoC: i.MX8MP LDP: Ubuntu22.04 and Ubuntu 20.04 Yocto: 6.1.22 mickledore   This doc includes two parts: 1)How to enable qt5 in LDP 2)How to enable qt5 in Yocto Linux 6.1.22     How to use qt5 in LDP(Linux Distribution Poc): The gcc and glibc is diffrent from Yocto Linux and Linux Distribution Poc. To cross compile the file between Linux and Ubuntu, we need to care about that.   To full enable the GPU usage of QT lib, please use "-gles" libs by apt-get command. Qt source code is not suggested, for it has not been tested. Building Qt5, for example: sudo apt-get update sudo apt-get -y install libqt5gui5-gles sudo apt-get -y install libqt5quick5-gles sudo apt-get -y install qtbase5-gles-dev   opengles test case glmark: sudo apt-get -y install glmark2-es2-wayland How to find the missing lib for apt-get: sudo apt-get install apt-file apt-file search xx   open wifi if needed NXP internal internet has limitation: sudo modprobe moal mod_para=nxp/wifi_mod_para.conf   and add "nameserver 8.8.8.8" in vi /etc/resolv.conf. You can also try:  echo "nameserver 8.8.8.8" | sudo tee /etc/resolv.conf > /dev/null   some times system time is not automatically update, and that cause apt-get update fail User and choose manually configure it by: sudo date -s "2023-08-31 14:00:00"   For Chinese support for ubuntu, please use: sudo apt-get install ttf-wqy-microhei ttf-wqy-zenhei xfonts-wqy   possible env path you need to export: XDG_RUNTIME_DIR="/run/user/1000" export QT_QPA_PLATFORM=wayland   User can choose root login by command like: user@imx8mpevk:~$ sudo passwd New password: Retype new password:   please use qmake to build qt project: 1)qmake -o Makefile HelloWorld.pro 2)make   some other qt libs: sudo apt-get install -y qtwayland5 sudo apt-get install -y qml-module-qtquick-controls sudo apt-get install -y qml-module-qtquick-controls2 sudo apt-get install -y qml-module-qtcharts sudo apt-get install -y libqt5multimedia5 sudo apt-get install -y libqt5serialport5 sudo apt-get install -y libqt5script5 sudo apt-get install -y qml-module-qt-labs-settings sudo apt-get install -y qml-module-qt-labs-platform sudo apt-get install -y qml-module-qtmultimedia sudo apt-get install -y libqt5webengine5 sudo apt-get install -y qml-module-qtwebengine sudo apt-get install -y qml-module-qtquick-dialogs     How to enable qt5 in Yocto 6.1.22: 1.download meta-qt5 git clone https://github.com/meta-qt5/meta-qt5.git git checkout origin/mickledore   copy Yocto version 5.10.72_2.2.0 sources\meta-imx\meta-sdk\dynamic-layers\qt5-layer to the same path of Yocto 6.1.22   2.apply two patches qt5-1.patch: modify the path from qt6 to qt5 qt5-2.patch: modify the qt5 related in meta-imx, including: 1)Yocto grammer update,from "_" to ":";  2)NXP grammer,from mx8 to mx8-nxp-sdk;  3)remove gstreamer1.0-plugins-good-qt, for qt5 has been natively added into gst-plugin-good-1.22(which is not in 1.18)   3.after input command like "DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build-xwayland", comment the "meta-nxp-demo-experience"   # i.MX Yocto Project Release layers BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-bsp" BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-sdk" BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-ml" BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-v2x" #BBLAYERS += "${BSPDIR}/sources/meta-nxp-demo-experience"      
記事全体を表示
The purpose of this document is to provide extended guidance for the selection of compatible LPDDR4/4X memory devices that are supported by the i.MX 93 series of processors. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs. The i.MX 93 series of processors supports different packages, and each have their own maximum supported LPDDR4/4x data rates. Please refer to the respective datasheets. Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. NOTE: Some of the LPDDR4/4X devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low-speed operation is planned in the use case, please consult with the memory vendor about the configuration aspects and possible customization of the memory device so correct functionality is ensured. LPDDR4/4X - Maximum Supported Densities SoC Max Data bus width Maximum density Assumed memory organization Notes i.MX 93 (i.MX 93xx) 16-bit 16 Gb / (2 GB) single rank, single channel device with 17-row addresses (R0 - R16) 1, 2, 3   LPDDR4/4X - List of Validated Memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part# Notes i.MX 93 16 Gb/ (2 GB) Micron LPDDR4/4x: MT53E1G16D1FW-046 AAT:A  (Z32N) MT53E1G16D1ZW-046 AAT:C (Z42N) 7   4, 8 8 Gb/ (1 GB) Micron LPDDR4/4x: MT53D512M16D1DS-046 AAT (Z11M) 4, 10 16 Gb/ (2 GB) Micron LPDDR4/4x: MT53E1G32D2FW-046 AUT:B (Z42M) 4, 5, 10 8 Gb/ (1 GB) Nanya LPDDR4: NT6AN512M16AV-J1I LPDDR4x: NT6AP512M16BV-J1I 4, 8 4 Gb/ (512 MB) Nanya LPDDR4x: NT6AP256M16AV  4, 8 16 Gb/ (2 GB) Kingston LPDDR4: D1611PM3BDGUI-U 4, 8 16 Gb/ (2 GB) Kingston LPDDR4: C1612PC2WDGTKR-U  7, 9 4 Gb/ (512 MB) ISSI LPDDR4: IS43LQ16256B-062BLI 4, 8 2Gb / (256 MB) ISSI LPDDR4: IS43LQ16128A-062BSLI 4, 6, 8   8 Gb/ (1 GB) CXMT LPDDR4/4x: CXDB4CBAM-EA-M 4, 9 16 Gb/ (2 GB) JSC LPDDR4x: JSL4BAG167ZAMF  4, 8 8 Gb/ (1 GB) JSC LPDDR4x: JSL4B8G168ZAMF-05x  4, 8 4 Gb/ (512 MB) JSC LPDDR4x: JSL4A4G168ZAMF-05 4, 8 2Gb / (256 MB) Winbond  LPDDR4x: W66BQ6NBHAGJ 4, 6, 8 8Gb / (1 GB) IM (Intelligent Memory) LPDDR4x: IM8G16L4JCB-046I 4, 11 16Gb / (2 GB) IM (Intelligent Memory) LPDDR4/4x: IMAG16L4KBBG 4, 8 4Gb / (512 MB) Samsung LPDDR4: K4F4E164HD-THCL 4, 8 8 Gb / (1 GB) AM (Alliance Memory) LPDDR4X: AS4C512M16MD4V-053BIN 4, 8 4 Gb / (512 MB) ISSI LPDDR4/4X: IS43LQ16256B-053BLI 4, 8 8 Gb / (1 GB) ISSI LPDDR4/4X: IS46LQ16512B-046BLA2 4, 8 32 Gb / (4GB) 16 Gb / (2Gb) usable by i.MX93 ISSI LPDDR4/4X: IS46LQ32K01B-046BLI 4, 8   Note 1: The numbers are based purely on the IP documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, SoC reference manual and on the JEDEC standards JESD209-4B/JESD209-4-1 (LPDDR4/4X). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4/4X devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The SoC also supports dual rank single channel devices therefore, 16Gb/2GB density can be also achieved by using a dual rank single channel device with 16-row addresses (R0 - R15). Note 4: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 5: This is a dual channel x32 device. Since i.MX93 only supports 16-bit LPDDR4/X data bus, it can only interface with one of the channels and therefore, utilize only half of the device's density. As indicated in the table - the device has 32Gb/4GB density however, only 16Gb/2GB can be used. There is no functional problem with using only one channel of a dual channel device as the channels are independent in LPDDR4/4X.  Note 6: This is a new JEDEC 100 ball package, half the size of the standard 200 ball package. This 100 ball package has the same performance and functionality as the 200 ball package, and has the added advantage of being smaller and cheaper than the standard package. Note 7: This device has been EoLed by the manufacturer and has been updated by a new memory part number  Note 8: Part is active. Reviewed Nov 2025 Note 9: Part is obsolete. Note 10: This device will be EoLed in Q2 24 by the manufacturer and will not be updated by a new memory part number Note 11: DQ eye marginalities were identified during TSA analysis. vTSA and stability testing did not identify any issues.
記事全体を表示
Customer is asking high-capacity external storage(for example >64GB) support on i.MX BSP, ext4 is ok for HC storage, but it can’t be supported by Windows. Pls find NFTS and exFAT support status on Linux BSP below: Updated test result on L5.4.70.2.3.0 and L6.1.22: L5.4.70.2.3.0 1.You can enable ntfs support in kernel config as below,  ntfs can be mounted normally, but you can only modify existing file content in disk, you can’t create/delete/rename file on disk. > File systems > DOS/FAT/NT Filesystems   Log: root@imx8mpevk:~# mount -t ntfs /dev/sda1 /mnt/fat/ [  662.732869] ntfs: volume version 3.1. root@imx8mpevk:~# cp ntfs-3g /mnt/fat/ cp: cannot create regular file '/mnt/fat/ntfs-3g': Permission denied root@imx8mpevk:~# ls /mnt/fat/ 111.png  Image_org  System Volume Information  gpuinfo.sh root@imx8mpevk:~# vi /mnt/fat/gpuinfo.sh root@imx8mpevk:~# umount /mnt/fat/ root@imx8mpevk:~# ntfs file system can be accessed via ntfs-3g in user space as below //build: wget https://tuxera.com/opensource/ntfs-3g_ntfsprogs-2017.3.23.tgz tar zxvf ntfs-3g_ntfsprogs-2017.3.23.tgz cd ntfs-3g_ntfsprogs-2017.3.23/ source ../../sdk/environment-setup-aarch64-poky-linux   ./configure --host=aarch64-linux --build=aarch64-poky-linux --disable-shared --enable-static   make   ls /src/ntfs-3g   //put it into rootfs cp ntfs-3g /bin   //test log: root@imx8mpevk:/# [ 1058.724471] usb 1-1: USB disconnect, device number 4 [ 1062.058613] usb 1-1: new high-speed USB device number 5 using xhci-hcd [ 1062.214029] usb-storage 1-1:1.0: USB Mass Storage device detected [ 1062.220986] scsi host0: usb-storage 1-1:1.0 [ 1063.235871] scsi 0:0:0:0: Direct-Access     VendorCo ProductCode      2.00 PQ: 0 ANSI: 4 [ 1063.246185] sd 0:0:0:0: [sda] 15728640 512-byte logical blocks: (8.05 GB/7.50 GiB) [ 1063.254023] sd 0:0:0:0: [sda] Write Protect is off [ 1063.259164] sd 0:0:0:0: [sda] No Caching mode page found [ 1063.264540] sd 0:0:0:0: [sda] Assuming drive cache: write through [ 1063.296946]  sda: sda1 [ 1063.300860] sd 0:0:0:0: [sda] Attached SCSI removable disk   root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh root@imx8mpevk:/# cp /unit_tests/memtool /mnt/fat/ root@imx8mpevk:/# umount /mnt/fat/ root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh  memtool root@imx8mpevk:/#   3.exFAT is not supported on this BSP..   L6.1.22(you can check it on L5.15 and above, should be the same) You can enable ntfs support in kernel config as below, full features can be supported. > File systems > DOS/FAT/EXFAT/NT Filesystems   Pls use ‘-t ntfs3’ during mounting, otherwise it will be mounted as ‘read-only’ Log: root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information' root@imx8ulpevk:~# root@imx8ulpevk:~# cp gpuinfo.sh /mnt/fat/ root@imx8ulpevk:~# umount /mnt/fat/ root@imx8ulpevk:~# root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information'   gpuinfo.sh root@imx8ulpevk:~#   exFAT has been supported in L6.1.22. > File systems > DOS/FAT/EXFAT/NT Filesystems   /dev/sda1 on /run/media/sda1 type exfat (rw,relatime,fmask=0022,dmask=0022,iocharset=utf8,errors=remount-ro) root@imx8ulpevk:~# ls /run/media/sda1 'Certificate of Completion.pdf'             carlife.MP4 Image_org                                  example.tflite L5.4.70_2.3.0                              mx8mp_vpu.txt NXP-5G.mp4                                 sd.mp4 'System Volume Information'                 vela.ini android_p9.0.0_2.1.0-auto-ga_image_8qmek root@imx8ulpevk:~# ls Image_org  gpuinfo.sh root@imx8ulpevk:~# cp gpuinfo.sh /run/media/sda1/ root@imx8ulpevk:~# umount /run/media/sda1 root@imx8ulpevk:~#
記事全体を表示
Hello everyone! In this quick example its focused on how to customize uboot code to generate an uboot image with a silent console so its speed up the flash and boot time, this may provide helpful for customers who have a bigger images or just want to have a silent console. Note: this should not be enabled if the image is still being under test, since this will disable all communication with the debug terminal and there won't be boot messages. Requirements: I.MX 8M Nano DDR4 EVK i.MX 8M Nano EVK Prebuilt image (6.1.1-1.0.0) UUU tool First clone the code from the uboot repository: $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.1.1-1.0.0 $ cd uboot-imx After we get the code, then proceed to enable the silent console in the uboot defconfig: $ nano configs/imx8mn_ddr4_evk_defconfig CONFIG_SILENT_CONSOLE=y CONFIG_SILENT_U_BOOT_ONLY=y For this to actually work we need to create the silent environmental variable and give it a value different from "0": $ nano include/configs/imx8mn_evk.h "silent=1\0"      \ As specified in our Linux porting guide: Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set Target-Machine to the machine you are building for. See Section "Build configurations" in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG) Set up the host terminal window toolchain environment: $ source/opt/fsl-imx-xwayland/6.1.1/environment-setup-aarch64-poky-linux $ export ARCH=arm64 Build uboot binary: $ make distclean $ make imx8mn_ddr4_evk_defconfig $ make Build ARM Trusted Firmware (ATF) $ cd .. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.1.1-1.0.0 $ cd imx-atf/ $ make PLAT=imx8mn bl31 In case you get the error aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' $ unset LDFLAGS Download the DDR training & HDMI binaries $ cd .. $ mkdir firmware-imx $ cd firmware-imx $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.19.bin $ chmod a+x firmware-imx-8.19.bin $ ./firmware-imx-8.19.bin Accept EULA and the firmware will be deployed. Download imx-mkimage and build the boot image $ cd .. $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.1.1-1.0.0 $ cd imx-mkimage $ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ $ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ $ cp ../uboot-imx/arch/arm/dts/imx8mn-ddr4-evk.dtb iMX8M/ $ cp ../imx-atf/build/imx8mn/release/bl31.bin iMX8M/ $ cp ../firmware-imx/firmware-imx-8.19/firmware/ddr/synopsys/ddr4_* iMX8M/ $ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot $ make SOC=iMX8MN flash_ddr4_evk After this we can download our uboot image to our board, we can either use the uboot image for boot or for flashing purpose only. We can compare the time it takes using UUU with a standard pre-built image uuu -V -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-full-imx8mnevk.wic It takes 485.5 seconds using normal uboot with debug console enabled. uuu -V -b emmc_all flash.bin imx-image-full-imx8mnevk.wic It takes 477.5 seconds using silent uboot console. Even if the speed is not greatly improved (~8 seconds), in larger files it could help to speed up flashing, even if wants to have the console silent is a good option. Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
記事全体を表示
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there.  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
記事全体を表示
We are pleased to announce that Config Tools for i.MX v14.0 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) The product is based on Eclipse 2022-12 Open JDK 17 is updated. Batch processing on command line is supported. Support for SDK 2.14 in Project cloner and Detect toolchain project is added. Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error. Search functionality to Code Preview is added. TEE Export TEE registers via wizard or command line is available. Boot ROM hiding feature is supported. Tier mode for TRDC is supported. Domain ambivalence for RDC masters is added. Master-specific memory alias Validation for A28 bit of MPU region address is added. Memory map filters are aligned with Arm terminology. Status bar is united with other tools. Pins Labels defined for Expansion header pins can be set as identifiers of the routed pin. Expansion headers can be locked for editing. Expansion headers and boards are added to the HTML and CSV reports. Pins filtering is added into the expansion header pin routing dialogs. Columns from Routing Details can be added to the External User Signals view. New External User Signals can be created for all routed pins that are missing in the signals table. Clocks Support for the same frequencies settings from different source for internal clocks is added.
記事全体を表示
vpuwraper can fulfill VPU decoder/encoder, if customer’s user case is simple, for example they just need to encode yuv stream to H264, or decode H264 stream to yuv, There is no need to use gstreamer or V4L2 complex framework, you can use vpuwraper. Platform: i.MX8MP + L5.4.70.2.3.0 Build Procedure: mkdir vpu cd vpu git clone https://github.com/nxp-imx/imx-vpuwrap   cd imx-vpuwrap/ git tag -l   git switch -c rel_imx_5.4.70_2.3.0   source ../../.././5.4.70.2.3.0/sdk/environment-setup-aarch64-poky-linux   make -f Makefile_8mp   Test on i.MX8MP EVK board Pls find attached test log for decode and encode If busChromaU in YUV file is null, you will failed to encode it, pls apply vpuwraper patch for L5.4.70.2.3.0.patch to fix it If YUV file is interleave format, you need to add interleave parameter : -interleave 1 ./test_enc_arm_elinux -i test.yuv -o aaa.h264 -f 2 -w 176 -h 96 -interleave 1   Thanks, Lambert
記事全体を表示
On customer design, they may need to fine tune LVDS driver strength for different case, for example, PCB impedance does not match, or the value of terminal resistor in panel side is lower or bigger. In IMX8MPRM.pdf, it has reg for this feature:         LVDS is constant current source, when voltage on terminal or panel side is lower than spec, you need to increase output current to get higher voltage to meet spec. otherwise ,you need to reduce it There is no detail description for these bits, pls refer to below: CC_ADJ = 000b => 3.5mA as default CC_ADJ = 001b => 3.5mA + 0.215mA x 1 CC_ADJ = 010b => 3.5mA + 0.215mA x 2 CC_ADJ = 011b => 3.5mA + 0.215mA x 4 CC_ADJ = 100b => 3.5mA - 0.215mA x 4 CC_ADJ = 101b => 3.5mA - 0.215mA x 3 CC_ADJ = 110b => 3.5mA - 0.215mA x 2 CC_ADJ = 111b => 3.5mA - 0.215mA x 1   Thanks, Lambert
記事全体を表示
  Solution           
記事全体を表示
Hello everyone, this document will share an step by step guide of the configuration needed in a Linux PC to compile the SDK examples we provide, as well as how to download them in an easy way. Requirements: I.MX 8M Mini EVK SDK package (for i.MX8MM) UUU tool First step would be to get the SDK package, this include documentation and code, which is available at the MCUXpresso builder webpage: https://mcuxpresso.nxp.com/en/welcome Click on the select a development board and select the package for your development kit or the i.MX MPU   This guide is focused on Linux build so will select GCC package and Linux host PC as the environment. Click on build and wait for the SDK package to be ready for download. Note1: Click on select all if the whole middleware package is desired Note2: it is possible to select each middleware that are desired. On new window select download SDK Select on new pop-up window download both SDK and documentation Read and accept EULA so the download start Decompress the package using the following command: $ tar -xvzf ~/SDK_2_13_0_EVK-MIMX8MM.tar.gz -C ~/SDK_2_13_0_EVK-MIMX8MM Next will be to download the GCC from the ARM webpage, gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 https://developer.arm.com/downloads/-/gnu-rm Note that the GCC version used is based on the minimum version required, since this was tested and supported, this could be found within the SDK documentation (~/SDK_2_13_0_EVK-MIMX8MM/docs/MCUXpresso SDK Release Notes for EVK-MIMX8MM) Once downloaded we can decompress and configure the environment: $ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ sudo apt-get install cmake  Check the version >= 3.0.x $ cmake --version Once this is done we enter the path of the example of our choice and compile using the script, as necessary using debug, release or all. $ cd ~/SDK_2_13_0_EVK-MIMX8MM/boards/evkmimx8mm/demo_apps/hello_world/armgcc $./build_release.sh The binary (elf and bin) will be found inside the folder according to whether we use debug or release script. For this example we used release script: $ cd release Once builded we can move/download the binaries from the Linux host PC to the board by using the UUU tool with the command fat_write #### we put the board in fastboot mode by entering the command in the uboot terminal fastboot 0 #### From the Linux terminal introduce the UUU command to  download to the FAT partition of the eMMC of the baord: ## For rproc it is needed the .elf binary ## $ uuu -v -b fat_write hello_world.elf mmc 0:1 hello_world.elf ## For bootaux it is needed the .bin binary ## $  uuu -v -b fat_write hello_world.bin mmc 0:1 hello_world.bin Once with the binaries in the FAT partition of the SD/eMMC of our board we can make the necessary modifications (device tree/bootargs) to test the Cortex-M examples. For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
記事全体を表示
  Platform: i.MX8MP EVK , L6.1.22-2.0.0 LT9211 is a chip that can realize the conversion of MIPI DSI signals to LVDS signals. This patch is based on this mainline driver:https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/gpu/drm/bridge/lontium-lt9211.c Keypoint Move lt9211_host_attach function to lt9211_attach to skip bridge attach error.  
記事全体を表示
1.Compile full aosp or only kernel Build full aosp: source build/envsetup.sh lunch evk_8mm-userdebug ./imx-make.sh -j8  Only build kernel: ./imx-make.sh kernel -j8 2.Build GKI locally Download GKI outside of android_build. mkdir gki && cd gki (Make sure folder gki is not inside of ${MY_ANDROID}) repo init -u https://android.googlesource.com/kernel/manifest -b commonandroid13-5.15 repo sync Build GKI locally. BUILD_CONFIG=common/build.config.gki.aarch64 build/build.sh 3. Export symbols After building GKI locally, you can copy linux-imx from /vendor/nxp-opensource/kernel_imx into common. cd common rm -r ./* cp ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/* ./ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex  Build GKI about i.MX: BUILD_FOR_GKI=yes BUILD_CONFIG=common/build.config.imx EXT_MODULES_MAKEFILE="verisilicon_sw_isp_vvcam/vvcam/v4l2/Kbuild" EXT_MODULES="nxp-mwifiex/mxm_wifiex/wlan_src" build/build_abi.sh --update-symbol-list -j8 Then the  common/android/abi_gki_aarch64_imx will be generated. cd gki cp common/android/abi_gki_aarch64_imx /tmp/abi_gki_aarch64_imx   Update GKI kernel rm -r common/* # delete imx kernel repo sync # recover aosp kernel cp /tmp/abi_gki_aarch64_imx android/abi_gki_aarch64_imx cd .. BUILD_CONFIG=common/build.config.gki.aarch64 build/build_abi.sh LTO=thin --update -j8  Then, common/android/abi_gki_aarch64.xml is updated.  
記事全体を表示
  Introduction   Platform: i.MX93 EVK Uboot: origin/lf_v2022.04(lf-6.1.1-1.0.0) The LVDS design and media block control in i.MX93 is very similiar with i.MX8MPlus.This article implements the LVDS driver in uboot. You need apply 0001-Add-fake-adp5585-pwm-driver.patch which implements the adp5585 pwm driver in uboot. This is a fake pwm driver only implement the pwm driver framework. You can't use pwm value to adjust brightness for the moment, but this is enough to enable the backlight. Then please apply 0002-Add-imx93-lvds-and-panel-driver.patch, you will see nxp logo with this panel: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/dy1212w-4856:DY1212W-4856   Porting suggestions   1. Modify panel timing in drivers/video/simple_panel.c /* define your panel timing here and * copy it in simple_panel_get_display_timing */ static const struct display_timing boe_ev121wxm_n10_1850_timing = { .pixelclock.typ = 71143000, .hactive.typ = 1280, .hfront_porch.typ = 32, .hback_porch.typ = 80, .hsync_len.typ = 48, .vactive.typ = 800, .vfront_porch.typ = 6, .vback_porch.typ = 14, .vsync_len.typ = 3, }; static int simple_panel_get_display_timing(struct udevice *dev, struct display_timing *timings) { memcpy(timings, &boe_ev121wxm_n10_1850_timing, sizeof(*timings)); return 0; }   2.Modify VIDEO_PLL The VIDEO_PLL = pixel clock * 7. For default panel, the pixel clock is 71.143MHz and VIDEO_PLL  is 498MHz. static struct imx_fracpll_rate_table imx9_fracpll_tbl[] = { FRAC_PLL_RATE(1000000000U, 1, 166, 4, 2, 3), /* 1000Mhz */ FRAC_PLL_RATE(933000000U, 1, 155, 4, 1, 2), /* 933Mhz */ FRAC_PLL_RATE(700000000U, 1, 145, 5, 5, 6), /* 700Mhz */ FRAC_PLL_RATE(498000000U, 1, 166, 8, 0, 1),/* rate, rdiv, mfi, odiv, mfn, mfd */ FRAC_PLL_RATE(484000000U, 1, 121, 6, 0, 1), FRAC_PLL_RATE(445333333U, 1, 167, 9, 0, 1), FRAC_PLL_RATE(466000000U, 1, 155, 8, 1, 3), /* 466Mhz */ FRAC_PLL_RATE(400000000U, 1, 200, 12, 0, 1), /* 400Mhz */ FRAC_PLL_RATE(300000000U, 1, 150, 12, 0, 1), }; 3. Modify lcdif node in dts <498000000>, <71142857>, <400000000>, <133333333>; <VIDEO PLL>,<PIX CLK>, <MEDIA_AXI>,<MEDIA_APB> &lcdif { status = "okay"; - assigned-clock-rates = <484000000>, <121000000>, <400000000>, <133333333>; + assigned-clock-rates = <498000000>, <71142857>, <400000000>, <133333333>; };  
記事全体を表示
The following setup is done on i.MX 93. For i.MX 8M the same steps are valid and can be followed. Prerequisites Prepare the Yocto environment. $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.0.xml $ repo sync  Set the build environment. $ DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source imx-setup-release.sh -b build-imx93 Add the 32-bit support to the image For i.MX 8M / i.MX 93, building 32-bit applications on 64-bit OS can be supported using the multilib configuration. Multilib offers the ability to build libraries with different target optimizations or architecture formats and combine these together into one system image.  Building a 32-bit application requires the following statements in conf/local.conf. The configuration specifies a 64-bit machine as the main machine type and adds multilib:lib32, where those libraries are compiled with the armv7athf-neon tune, and then includes to the image the lib32 packages. # Define multilib target require conf/multilib.conf MULTILIBS = "multilib:lib32" DEFAULTTUNE:virtclass-multilib-lib32 = "armv7athf-neon" # Add the multilib packages to the image IMAGE_INSTALL:append = " lib32-glibc lib32-libgcc lib32-libstdc++" Multilib is not supported with the debian package management. It requires the RPM system. Check and comment out the two package management lines in conf/local.conf to go to the default RPM. PACKAGE_CLASSES = "package_deb" EXTRA_IMAGE_FEATURES += "package-management" Build the image. bitbake imx-image-core Cross-compile a 32-bit application This section shows how to use the Linux SDK to cross-compile a simple C application into a 32-bit binary. Generate the SDK, which includes the tools, toolchain, and small rootfs to compile against to put on host machine: DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk bitbake core-image-minimal -c populate_sdk Set the SDK environment with the following command before building: source /opt/fsl-imx-wayland/6.1-langdale/environment-setup-armv7at2hf-neon-pokymllib32-linux-gnueabi Implement a simple hello world application: cat hello_world_32.c #include <stdio.h> int main() { printf("Hello, World!"); return 0; } $CC hello_world_32.c -o hello_world_32 Check the file's type: $ file hello_world_32 hello_world_32: ELF 32-bit LSB shared object, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, BuildID[sha1]=0a5042a0309858e0b10b12175a155cfbfb4c6a80, for GNU/Linux 3.2.0, with debug_info, not stripped Copy the binary to the Linux rootfs. Run the application on i.MX 93 Boot the board and run the application: root@imx93-11x11-lpddr4x-evk:~# ./hello_world_32 Hello, World!  
記事全体を表示