i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
  It is a Matter Demo setup guide to set up Matter OTBR on i.MX MPU Platfrom. i.MX 2023Q2 release is based on Matter v1.1  Current test solutions. i.MX6ULL + 88W8987(WiFi-BT combo Module) + K32W(OpenThread RCP module) i.MX8MM + 88W8987(WiFi-BT combo Module) + K32W(OpenThread RCP module) i.MX8MM + IW612-RD-EVK (WiFi-BT-Thread tri-radio single-chip module) i.MX93 + IW612 (WiFi-BT-Thread tri-radio single-chip module) Matter Zigbee Bridge  https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Matter-Zigbee-Bridge-base-on-i-MX-MPU-and-K32W/ta-p/1675962   if use imx8mm_k32w_matter.sh or imx93_matter.sh to setup OTBR, you need modify "SSID" and " WIFI_PWD" in the script.    
查看全文
Traditional non-matter devices cannot directly join the matter network. But Matter Bridge solves the problem. Matter bridge can join a Matter network as a Matter device and nonmatter devices need to be mapped to Matter network as a dynamic endpoint. In this way, other Matter devices can communicate with non-matter devices through dynamic endpoints. The Guide is a Matter Zigbee Bridge implement based on i.MX93 + K32W0.     Feature List • Matter over Ethernet • Matter over Wi-Fi • Register and Remove Zigbee Deivces • Connect Zigbee devices into Matter ecosystem seamlessly • Zigbee Devices • On/Off cluster • Temperature Sensor Cluster • Matter Actions • Start Zigbee Network • Zigbee Network Permit Join • Factory Reset • No limitation if migrating to other i.MX MPU like i.MX6ULL, i.MX8MP • OTBR and Zigbee bridge can be integrated into one single device
查看全文
The purpose of this document is to specify the maximum LPDDR3, LPDDR4, & LPDDR4X densities that are supported by i.MX 8ULP processor along with a running list of tested memories to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.  It is strongly recommended to consult with NXP and the memory vendor the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs. For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.  LPDDR4/LPDDR4X Maximum Support Density Please note that the SoC limits the addressable DDR memory map range to 2GB. SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8ULP 32-bit 16Gb/2GB single-rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 6,11   LPDDR4 - list of validated memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8ULP 16Gb/2GB Micron MT53D512M32D2DS-053 WT:D  10 16Gb/2GB Micron MT53E512M32D1ZW-046 WT:B  8 64Gb/8GB Micron MT53E2G32D4DE-046 WT:A  3, 4, 8 32Gb/4GB Micron MT53E1G32D2FW-046 AUT:B  3, 4, 10 16Gb/2GB Nanya NT6AN512T32AV-J2 3, 7, 8 8Gb/1GB Forsee FL4C2001G-D9  3, 10   LPDDR4x - list of validated memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Mamory Vendor Validated Memory Part# Notes i.MX 8ULP 16Gb/ 2GB Nanya NT6AP512T32AV-J2  3, 7, 8 2Gb/ 256MB Fidelix FMF2D32VAC-4CDIR 3 4Gb/ 512MB Winbond W66CQ2NQUAFJ  3, 8 8Gb/1GB Alliance Memory AS4C256M32MD4V-062BAN  3, 8 32Gb/4GB Micron MT53E1G32D2FW-046 AUT:B (Z42M) 3, 4, 10 16Gb/ 2GB Micron MT53D512M32D2DS-053 WT:D  10 16Gb/ 2GB Micron MT53E512M32D1ZW-046 WT:B  9   LPDDR3 Maximum Support Density Please note that the SoC limits the addressable DDR memory map range to 2GB. SoC Max data bus width Maximum density Assumed memory organization Notes i.MX 8ULP 32-bit 16Gb/2GB Single Channel, Dual Chip Select 5,11   LPDDR3 - list of validated memories The validation process is an ongoing effort - regular updates of the table are expected. SoC Density Memory Vendor Validated Memory Part#  Notes i.MX 8ULP 16Gb/2GB Micron  MT52L512M32D2PF-107 WT:B  8   Note 1: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC and on the memory device used on NXP evaluation boards, and on the JEDEC standards JESD209-4/JESD209-4B (LPDDR4/4X). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 4: As the i.MX 8ULP DDR memory map is limited to 2GB, only up to 2GB of the device can be utilized even though the device density exceeds the 2GB range. Note 5: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC and on the memory device used on NXP evaluation boards, and on the JEDEC standards JESD209-3C (LPDDR3). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk.  Note 6: The SoC supports also LPDDR4/4X devices with 17-row address bits however, given the SoC's memory map constraints (see Note 4), full density of those devices cannot be utilized since the dual channel (x32) 17-row address memory devices have the density of 4GB and higher. Note 7: By default, LPDDR4/4X devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity. Please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured. Note 8: Part is active. Reviewed Jan 2026 Note 9: Part is active as MT53E512M32D1ZW-046BWT:B.  Note 10: Part is obsolete. Note 11: i.MX 8ULP does not support Non-Power of 2 Memory densities (e.g. 3,6,12 Gb).
查看全文
1.Test environment Board: i.MX8MPlus, RM67199 BSP: uboot 2022.04, linux-6.1.1-1.0.1 2.Modification of uboot  In uboot, you need comment the video_link_shut_down and dm_remove_devices_flags in announce_and_cleanup function. #if defined(CONFIG_VIDEO_LINK) //video_link_shut_down(); #endif board_quiesce_devices(); printf("\nStarting kernel ...%s\n\n", fake ? "(fake run for tracing)" : ""); /* * Call remove function of all devices with a removal flag set. * This may be useful for last-stage operations, like cancelling * of DMA operation or releasing device internal buffers. */ // #ifndef CONFIG_POWER_DOMAIN // dm_remove_devices_flags(DM_REMOVE_ACTIVE_ALL | DM_REMOVE_NON_VITAL); // /* Remove all active vital devices next */ // dm_remove_devices_flags(DM_REMOVE_ACTIVE_ALL); // #endif cleanup_before_linux(); }  After doing this, the uboot logo will not be cleaned before Linux PM framework. 3.Modification of Linux You need add  CONFIG_LOGO=n into defconfig file to disable kernel logo.  3.1 Disable the power down of mediamix and mipi-dphy in gpcv2.c Please add below code into the beginning of  imx_pgc_power_down function if ((strcmp(genpd->name, "mipi-phy1") == 0) || (strcmp(genpd->name, "mediamix") == 0)) { return 0; }  3.2 Only reset lcdif in the last call of drm framework Please modify imx_lcdifv3_runtime_resume function like this. The imx_lcdifv3_runtime_resume function will be called two times, thus the lcdif will be reset two times.We can let it only reset last time,which before the rootfs mount. bool rst = false; ////////////////////////////// static int imx_lcdifv3_runtime_resume(struct device *dev) { int ret = 0; struct lcdifv3_soc *lcdifv3 = dev_get_drvdata(dev); if (unlikely(!atomic_read(&lcdifv3->rpm_suspended))) { dev_warn(lcdifv3->dev, "Unbalanced %s!\n", __func__); return 0; } if (!atomic_dec_and_test(&lcdifv3->rpm_suspended)) return 0; /* set LCDIF QoS and cache */ if (of_device_is_compatible(dev->of_node, "fsl,imx93-lcdif")) regmap_write(lcdifv3->gpr, 0xc, 0x3712); request_bus_freq(BUS_FREQ_HIGH); ret = lcdifv3_enable_clocks(lcdifv3); if (ret) { release_bus_freq(BUS_FREQ_HIGH); return ret; } ////////////////////////////// if (rst) { /* clear sw_reset */ writel(CTRL_SW_RESET, lcdifv3->base + LCDIFV3_CTRL_CLR); rst = false; } rst = true; ////////////////////////////// /* enable plane FIFO panic */ lcdifv3_enable_plane_panic(lcdifv3); return ret; } 4.Conclusion The uboot logo will be cleaned at log "imx-drm 1.0.0 20120507 for display-subsystem on minor 1". The boot time of  systemd service on evk is very long. For weston.service, it needs 3 seconds. From log here we test, the pcie and ethernet probe after drm system also cost about 1 second. If you want to reduce the boot time of other modules, you can try to reduce the system service and disable pcie/ethernet drivers if you don't need them. [ 2.505616] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1 [ 2.620324] imx6q-pcie 33800000.pcie: iATU unroll: enabled [ 2.620335] imx6q-pcie 33800000.pcie: iATU regions: 4 ob, 4 ib, align 64K, limit 16G [ 2.720689] imx6q-pcie 33800000.pcie: PCIe Gen.1 x1 link up [ 2.820996] imx6q-pcie 33800000.pcie: PCIe Gen.2 x1 link up [ 2.821003] imx6q-pcie 33800000.pcie: Link up, Gen2 [ 2.821010] imx6q-pcie 33800000.pcie: PCIe Gen.2 x1 link up [ 2.821112] imx6q-pcie 33800000.pcie: PCI host bridge to bus 0000:00 [ 2.821119] pci_bus 0000:00: root bus resource [bus 00-ff] [ 2.821126] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 2.821133] pci_bus 0000:00: root bus resource [mem 0x18000000-0x1fefffff] [ 2.821161] pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400 [ 2.821176] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff] [ 2.821187] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref] [ 2.821232] pci 0000:00:00.0: supports D1 [ 2.821237] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold [ 2.824664] pci 0000:01:00.0: [1b4b:2b42] type 00 class 0x020000 [ 2.824725] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x000fffff 64bit pref] [ 2.824761] pci 0000:01:00.0: reg 0x18: [mem 0x00000000-0x000fffff 64bit pref] [ 2.825066] pci 0000:01:00.0: supports D1 D2 [ 2.825072] pci 0000:01:00.0: PME# supported from D0 D1 D3hot D3cold [ 2.835499] pci 0000:00:00.0: BAR 0: assigned [mem 0x18000000-0x180fffff] [ 2.835511] pci 0000:00:00.0: BAR 15: assigned [mem 0x18100000-0x182fffff pref] [ 2.835519] pci 0000:00:00.0: BAR 6: assigned [mem 0x18300000-0x1830ffff pref] [ 2.835530] pci 0000:01:00.0: BAR 0: assigned [mem 0x18100000-0x181fffff 64bit pref] [ 2.835561] pci 0000:01:00.0: BAR 2: assigned [mem 0x18200000-0x182fffff 64bit pref] [ 2.835590] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 2.835598] pci 0000:00:00.0: bridge window [mem 0x18100000-0x182fffff pref] [ 2.835899] pcieport 0000:00:00.0: PME: Signaling with IRQ 218 [ 2.897767] Console: switching to colour frame buffer device 135x120 [ 3.098361] imx-drm display-subsystem: [drm] fb0: imx-drmdrmfb frame buffer device [ 3.111239] pps pps0: new PPS source ptp0 [ 3.316650] fec 30be0000.ethernet eth0: registered PHC device 0 [ 3.323645] imx-dwmac 30bf0000.ethernet: IRQ eth_lpi not found [ 3.329593] imx-dwmac 30bf0000.ethernet: force_sf_dma_mode is ignored if force_thresh_dma_mode is set. [ 3.340074] imx-dwmac 30bf0000.ethernet: User ID: 0x10, Synopsys ID: 0x51 [ 3.346883] imx-dwmac 30bf0000.ethernet: DWMAC4/5 [ 3.351684] imx-dwmac 30bf0000.ethernet: DMA HW capability register supported [ 3.358825] imx-dwmac 30bf0000.ethernet: RX Checksum Offload Engine supported [ 3.365966] imx-dwmac 30bf0000.ethernet: Wake-Up On Lan supported [ 3.372113] imx-dwmac 30bf0000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 3.379778] imx-dwmac 30bf0000.ethernet: Enabled L3L4 Flow TC (entries=8) [ 3.386573] imx-dwmac 30bf0000.ethernet: Enabled RFS Flow TC (entries=10) [ 3.393373] imx-dwmac 30bf0000.ethernet: Enabling HW TC (entries=256, max_off=256) [ 3.400950] imx-dwmac 30bf0000.ethernet: Using 34 bits DMA width [ 3.608045] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.613580] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1 [ 3.621621] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220fe6d hci version 0x110 quirks 0x0000002001010010 [ 3.631059] xhci-hcd xhci-hcd.1.auto: irq 226, io mem 0x38200000 [ 3.637197] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.642698] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2 [ 3.650365] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed [ 3.657695] hub 1-0:1.0: USB hub found [ 3.661473] hub 1-0:1.0: 1 port detected [ 3.665669] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 3.674445] hub 2-0:1.0: USB hub found [ 3.678220] hub 2-0:1.0: 1 port detected [ 3.683428] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 7 mkt segment 2 supported-hw 0x80 0x4 [ 3.693184] Hot alarm is canceled. GPU3D clock will return to 64/64 [ 3.702683] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO [ 3.703346] mxc-mipi-csi2-sam 32e40000.csi: supply mipi-phy not found, using dummy regulator [ 3.716645] : mipi_csis_imx8mp_phy_reset, No remote pad found! [ 3.722602] mxc-mipi-csi2-sam 32e40000.csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 500000000 [ 3.739353] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA [ 3.752018] isi-m2m 32e00000.isi:m2m_device: Register m2m success for ISI.0 [ 3.759172] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 3.768303] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 3.787598] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 3.795171] ALSA device list: [ 3.796227] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db [ 3.799186] No soundcards found. [ 3.819630] EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Quota mode: none. [ 3.828212] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 3.834944] devtmpfs: mounted
查看全文
This demo for all(bootloader, device tree, Linux kernel, rootfs) in spi. It uses raw read(sf read)/raw write(sf write in uuu script) to achieve that. sf probe 0; sf read ${fdt_addr} 0x500000 0x100000; sf read ${loadaddr} 0x600000 0x1E00000; sf read ${initrd_addr} 0x2400000 0x600000; setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate} rdinit=/linuxrc; booti ${loadaddr} ${initrd_addr} ${fdt_addr} |-- 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch --- patch for this demo |-- demo_binary | |-- flash.b0.bin --- b0 bootloader | |-- flash.bin --- c0 bootloader | |-- Image-imx8qxpc0mek.bin --- Linux kernel | |-- imx8qxp-mek.dtb --- device tree | |-- uramdisk_boot.rootfs.aarch64.img --- ram disk | |-- uuu.qspi.all.b0.uuu --- uuu script for b0 | `-- uuu.qspi.all.uuu --- uuu script for c0 `-- readme.txt --- this file # The spi layout used is: # - --------- -------------------------------------------- # | | flash.bin | env | dtb | Image |rootfs| # - --------------- -------------------------------------- # ^ ^ ^ ^ ^ ^ ^ # | | | | | | | # 0 4kiB 4MiB 5MiB 6MiB 36MiB 42MiB 0x1000 0x400000 0x500000 0x600000 0x2400000 Test: HW: i.MX8QXP MEK SW: lf-5.10.72-2.2.0 + 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch Test log: SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB device 0 offset 0x500000, size 0x100000 SF: 1048576 bytes @ 0x500000 Read: OK device 0 offset 0x600000, size 0x1e00000 SF: 31457280 bytes @ 0x600000 Read: OK device 0 offset 0x2400000, size 0x600000 SF: 6291456 bytes @ 0x2400000 Read: OK [ 4.787552] imx6q-pcie 5f010000.pcie: unable to add pcie port. [ 4.797467] Freeing unused kernel memory: 2944K [ 4.807379] Run /linuxrc as init process Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting network: OK /bin/sh: can't access tty; job control turned off / #  
查看全文
In this article, I will explain how to set up the iMX8M Plus to use the 4K Dart BCON Basler Camera module. Requirements: Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors) Basler Camera for i.MX 8M Plus (4K dart BCON for MIPI camera module for i.MX 8M Plus | NXP Semiconductors). Embedded Linux for i.MX Applications Processors (Embedded Linux for i.MX Applications Processors | NXP Semiconductors) (For this example we will use BSP version Linux 5.15.71_2.2.0) Serial Console Emulator Basler Camera Specifications and Manuals: Basler Camera Specifications at this link: Embedded Vision Kits daA3840-30mc-IMX8MP-EVK - Embedded Vision Kits (baslerweb.com). Basler Manual to identify and setting up the hardware at this link: daA3840-30mc-IMX8MP-EVK | Basler Product Documentation (baslerweb.com) Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor. (Video: Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor | NXP Semiconductors) Steps After setting up the hardware we will need to turn on the iMX8M Plus and follow these steps: 1. Stop the boot process on Uboot by pressing any key. 2. Use the following command to list interfaces. => mmc list Output example => FSL_SDHC: 1 (SD) => FSL_SDHC: 2 The above command will show you the device number in this example for SD, the device number is 1. 3. Then use fatls <interface> <device[:partition]> [<directory>] fatls mmc 1:1 (Device 1 : Partition 1) With this command, we will be able to list device tree files. => fatls mmc 1:1 4. Select imx8mp-evk-basler.dtb or imx8mp-evk-dual-basler.dtb and use the command editenv fdtfile.  => editenv fdtfile Output example edit: imx8mp-evk-basler.dtb 5. In edit command line put the selected device tree (*.dtb). 6. Use saveenv command to save environment and continue with the boot process. 7. Using the terminal and go to /opt/imx8-isp/bin and execute the script run.sh. $ ./run.sh -c basler_1080p60 -lm 8. Use the command gst-device-monitor-1.0 to list devices. Here you will find the path to the camera device. $ gst-device-monitor-1.0 Output example Device found: name : VIV class : Video/Source caps : video/x-raw, format=YUY2, width=[ 176, 4096, 16 ], height=[ 144, 3072, 8 ], pixel-aspect-ratio=1/1, framerate={ (fraction)30/1, (fraction)29/1, (fraction)28/1, (fraction)27/1, (fraction)26/1, (fraction)25/1, (fraction)24/1, (fraction)23/1, (fraction)22/1, (fraction)21/1, (fraction)20/1, (fraction)19/1, (fraction)18/1, (fraction)17/1, (fraction)16/1, (fraction)15/1, (fraction)14/1, (fraction)13/1, (fraction)12/1, (fraction)11/1, (fraction)10/1, (fraction)9/1, (fraction)8/1, (fraction)7/1, (fraction)6/1, (fraction)5/1, (fraction)4/1, (fraction)3/1, (fraction)2/1, (fraction)1/1 } ... properties: udev-probed = true device.bus_path = platform-vvcam-video.0 sysfs.path = /sys/devices/platform/vvcam-video.0/video4linux/video2 device.subsystem = video4linux device.product.name = VIV device.capabilities = :capture: device.api = v4l2 device.path = /dev/video2 v4l2.device.driver = viv_v4l2_device v4l2.device.card = VIV v4l2.device.bus_info = platform:viv0 v4l2.device.version = 393473 (0x00060101) v4l2.device.capabilities = 2216693761 (0x84201001) v4l2.device.device_caps = 69206017 (0x04200001) gst-launch-1.0 v4l2src device=/dev/video2 ! ... 9. Finally, use gstreamer to verify proper operation. (With this gstreamer pipeline you will see a new window with the camera output. Then, just rotate the lens to acquire the correct focus) $ gst-launch-1.0 -v v4l2src device=/dev/video2 ! "video/x-raw,format=YUY2,width=1920,height=1080" ! queue ! imxvideoconvert_g2d ! waylandsink Basic description of Gstreamer Pipeline gst-launch-1.0 -v: The option -v enables the verbose mode to get detailed information of process. v4l2src device=/dev/video2: Select input device in this case the camera is on path /dev/video3. "video/x-raw,format=YUY2,width=1920,height=1080": Received format from camera. queue: This command is a buffer between camera recording process and the following image process, this command help us to interface two process and prevent blocking where each process has different speeds, in other words, when a process A is faster than process B. imxvideoconvert_g2d: This proprietary plugin uses hardware acceleration to perform rotation, scaling, and color space conversion on video frames. waylandsink : This command creates its own window and renders the decoded frames processed previously. 10. Result     I hope this article will be helpful. Best regards, Brian.
查看全文
This is about the case studay from two USB related issues: #1. Plugin detection issue caused by an errata in i.MX8/8X (host mode).       Very limited unit may encounter this problem. When issue happens, there will be totally no action on USB host port when a debug plugged in. #2: High Speed disconnection detection issue (host mode):       This may happen on some special USB design which have complex circuit and connector design on the USB path and long USB cable. The USB enumeration might be interrupted by an un-expected disconnection event. System log shows USB recognition started but failed at several different stages during handshake. For details, please refer to the doc attached (#1/#2). A reference patch for each has also been made by David.
查看全文
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
查看全文
We are pleased to announce that Config Tools for i.MX v13.1 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes 13.1 DDR tool     - i.MX93 support for A0 pre-production launch; sync with SW BSP release Pins tool     - Fix incomplete routing of deinit functions  
查看全文
Platform: i.MX8MP SW:Linux 5.4.70.2.3.0 On current linux BSP, PCIE driver does not support Hot-plug, customers wants to turn off PCIE device to save power, attached is guide. Remove PCIE device driver Suspend PCIE driver Turn off PCIE device power supply Turn on PCIE device power supply Resume PCIE driver Rescan PCIE device Load PCIE device driver
查看全文
Platform: i.MX8MP EVK BSP: Linux 5.4.70.2.3.0 Customer reported UI on HDMI monitor is abnormal and has more line on left side when doing HDMI hot-plug on i.MX8MP running with L5.4.70.2.3.0.   This issue can’t be reproduced on latest BSP such as 5.10 and above, several patch for HDMI from latest BSP can fix this issue.  
查看全文
This doc will show: i.MX6SLL EVK board without connect hardware LCD display, using FreeRDP to share screen to remote PC which in same network, PC take this shared screen could run any command on i.MX6SLL EVK board. HW: i.MX6SLL EVK board, PC, usb network adapter SW: i.MX6SLL Linux 5.15.72_2.2.0 BSP release, and code change in this doc 1>yocto-5.15.72/6sll-bld/conf/local.conf, add below line, as freerdp depend on ffmpeg. LICENSE_FLAGS_ACCEPTED+="commercial" 2>pixman need switch to 0.42.0, enter folder yocto-5.15.72/6sll-bld/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/pixman/1_0.40.0-r0/pixman-0.40.0, fetch latest 0.42.0 version code from https://github.com/freedesktop/pixman.git 3>freerdp need use 2.8.0, enter folder yocto-5.15.72/6sll-bld/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/freerdp/1_2.6.1-r0/git should checkout to 2.8.0 tag; then to use neon accelerate freerdp related function, such as color space conversion, image codec encoding, apply patch freerdp-codechange-neon.diff. 4>Enter yocto-5.15.72/sources/meta-openembedded/meta-oe/recipes-support/freerdp, file freerdp_2.6.1.bb change as freerdp-2.6.1-bbfile.diff 5> bitbake -c compile ffmpeg bitbake -c install ffmpeg bitbake -c compile pixman bitbake -c install pixman bitbake -c compile freerdp bitbake -c install freerdp 6> Copy generated new libs to i.MX6SLL Linux rootfs: cp /root/imx6sllevk-linux-lib/lib* /usr/lib/ cd /usr/lib/ rm libfreerdp-client2.so.2 libfreerdp2.so.2 libpixman-1.so.0 libwinpr-tools2.so.2 libwinpr2.so.2 ln -s libfreerdp-client2.so.2.8.0 libfreerdp-client2.so.2 ln -s libfreerdp2.so.2.8.0 libfreerdp2.so.2 ln -s libpixman-1.so.0.42.0 libpixman-1.so.0 ln -s libwinpr-tools2.so.2.8.0 libwinpr-tools2.so.2 ln -s libwinpr2.so.2.8.0 libwinpr2.so.2 ln -s libavcodec.so.58.134.100 libavcodec.so.58 ln -s libavutil.so.56.70.100 libavutil.so.56 ln -s libswresample.so.3.9.100 libswresample.so.3 Make sure: libfreerdp-client2.so.2 -> libfreerdp-client2.so.2.8.0 libfreerdp2.so.2 -> libfreerdp2.so.2.8.0 libwinpr-tools2.so.2 -> libwinpr-tools2.so.2.8.0 libwinpr2.so.2 -> libwinpr2.so.2.8.0 libswresample.so.3 -> libswresample.so.3.9.100 libavutil.so.56 -> libavutil.so.56.70.100 libavcodec.so.58 -> libavcodec.so.58.134.100 7>i.MX6SLL Linux OS, file /etc/xdg/weston/weston.ini, change start-on-startup to true [screen-share] command=WLOG_APPENDER=file WLOG_FILEAPPENDER_OUTPUT_FILE_NAME=output.log WLOG_FILEAPPENDER_OUTPUT_FILE_PATH=/tmp /usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --no-clients-resize --rdp-tls-cert=/etc/freerdp/keys/server.crt --rdp-tls-key=/etc/freerdp/keys/server.key start-on-startup=true 8> i.MX6SLL Linux OS, run below cmd: mkdir /etc/freerdp mkdir /etc/freerdp/keys /root/imx6sllevk-linux-lib/winpr-makecert -path /etc/freerdp/keys mv /etc/freerdp/keys/imx6sllevk.crt /etc/freerdp/keys/server.crt mv /etc/freerdp/keys/imx6sllevk.key /etc/freerdp/keys/server.key service weston stop service weston start 9>Plug usb network adapter to i.MX6SLL EVK board J10; i.MX6SLL board and PC must in same network, ping without problem. i.MX6SLL Linux OS, there are two process name as "weston", one process is weston rdp backend will share screen to PC. If only one weston process, need check did miss copy any new lib or check libary file name. 10>PC side: wfreerdp.exe /v:IPADDRESS_OF_IMX6SLLEVK There will prompt dialog box for user name and password, just press ESC, then PC side will show i.MX6SLL Linux desktop screen; Click console button of i.MX6SLL Linux OS desktop, within that console input any i.MX6SLL Linux OS cmd, check result of it from PC side. Known issue: wfreerdp.exe is downloaded from https://ci.freerdp.com/job/freerdp-nightly-windows/ If run latest wfreerdp.exe but show nothing of remote desktop, try attached version wfreerdp.exe(3.0.0-dev). Also you can try check log files first: i.MX6SLL Linux OS file /tmp/output.log; PC side generated log file as: wfreerdp.exe /v:IPADDRESS_OF_IMX6SLLEVK /log-level:TRACE > rdp.log Reference: 1>https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat... 2>https://github.com/FreeRDP 3>https://github.com/freedesktop/pixman 4>https://github.com/DLTcollab/sse2neon    
查看全文
  Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/...  
查看全文
From Android 12, NXP use GKI(Generl kernel image) instead of NXP's kernel code.  This follow up Android ASOP standard. This article described that when customer use Android 12 and later version, they need to pay attention on GKI development, which is different with previous version.
查看全文
We are pleased to announce that Config Tools for i.MX v13 are now available.
查看全文
Updated for "phase 3" after a 3rd software lockup symptom found and fixed. Updated doc/patch: Software-lockup-issue-phase3_20260318-public.pdf 0001-clk-fix-sleeping-function-called-from-invalid-contex.patch 0001-ddr-perf-fix-sleeping-function-called-from-invalid-c.patch 0001-gpu-imx-dpu-Access-ExtDst-FetchUnit-Hscaler-Vscaler-new_L4.14.98.patch (this patch will depends on https://github.com/nxp-imx/linux-imx/commit/70744429841f08efc42a63380198cdae7f9a602f) --- 20260318   This is a summary for the software lockup issue found in the following platform: −i.MX8/8X −Linux 4.14.98_2.3.3   Issue description: •Issue happens during the boot procedure, at the systemd stage. •The symptom of the issue: −From user perspective, the symptom varies, but mainly fall into several types: §At the console, there may be login prompt, but no response (only echo) when input user/password. Unable to login. §Some user service in systemd failed to start. E.g. weston. −When checking the task status using sysrq (w/t), many tasks, including some kernel core tasks stays in “D” (uninterruptable sleep) state. E.g. agetty, login, chvt, etc. •Kernel itself is still alive. This can be verified by triggering some drivers, such as plugin a USB device. Issue can be reproduced on MEK through long time stress.   Please refer to the doc/patch attached for details.
查看全文
PCIE IP on i.MX8MM and i.MX8MP is same, customer can follow PCIE test Application note to do compliance test, if eye diagram failed, they can fine turn corresponding regs below: iMX8MMRM.pdf IMX8MPRM.pdf GEN1:             GEN2:                 Related code in kernel Phy-fsl-imx8-pcie.c (kernel-source\drivers\phy\freescale)    3794      2020/11/4 static int imx8_pcie_phy_init(struct phy *phy) { ……          /* Configure TX drive level  */        writel(0x2d, imx8_phy->base + 0x404);          return 0; }   Thanks Lambert
查看全文
i.MX8 series contains internal HiFi4 DSP. It is targeted for Audio related signal processing. SOF (Sound Open Firmware) is open source audio DSP firmware, driver and SDK. This document introduces basic theory about IIR/FIR digital filters, how to design IIR/FIR digital filters and the Equalizer filters implementation by SOF. After that, the document also describes how HiFi4 DSP MAC engine accelerate the EQ filters calculation.
查看全文
Hello, here Jorge. On this post I will explain how to configure, record and play audio using an i.MX 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK Linux Binary Demo Files - i.MX 8MMini EVK (L5.15.52_2.1.0) i.MX 8MIC-RPI-MX8 Board Serial console emulator (Tera Term, Putty, etc.) Headphones/speakers The 8MIC-RPI-MX8 accessory board is designed for voice enabled application prototyping and development on the i.MX 8M family. The board plugs directly into the 40-pin expansion connector on the i.MX 8M Mini and Nano EVK’s. Some features about this board are: 8 PDM Microphones 8 monochrome LEDs 4 multi-color LEDs 2 status LEDs 4 pushbuttons Microphone Mute Switch Microphone geometry switch Connecting the i.MX 8MIC-RPI-MX8 Board. The i.MX 8MIC-RPI-MX8 Board has a 40-pin expansion connector that you can plug it directly to the EVK board. Ensure that pin 1 of the 8MIC-RPI-MX8 is aligned with pin 1 on the EVK J1001 as is showed on the next figure:  Selecting the device tree on the board. Once the pre-compiled image is flashed on the board (Flashing Linux BSP using UUU) and you connected the 8MIC-RPI-MX8 it is necessary to select the correct device tree to handle 8MIC board. On U-boot check the available .dtb files on the BSP using the next command: u-boot=> fatls mmc 2:1 And you will get the corresponding list of .dbt files:  On this case we are working with an I.MX 8M Mini EVK and the corresponding .dtb file is: imx8mm-evk-8mic-revE.dtb To select it you need to set the environment variable and save it with: u-boot=> setenv fdtfile imx8mm-evk-8mic-revE.dtb u-boot=> saveenv Doble check it using: u-boot=> printenv fdtfile   Now it is time to boot Linux using the next command: u-boot=> boot Recording audio with the i.MX 8MIC-RPI-MX8 Board. The Advanced Linux Sound Architecture (ALSA) provides audio and MIDI functionality to the Linux operating system. ALSA has the following significant features: Efficient support for all types of audio interfaces, from consumer sound cards to professional multichannel audio interfaces. Fully modularized sound drivers. SMP and thread-safe design. User space library (alsa-lib) to simplify application programming and provide higher level functionality. Support for the older Open Sound System (OSS) API, providing binary compatibility for most OSS programs. Once we are on Linux, we can check our audio codecs detected on the board using: arecord -l   Now, to record audio we need to use the ALSA arecord command to start recording with IMX8 boards, there are different options that you can check on the next link. On this case we are going to use the next: arecord -D hw:imxaudiomicfil -c8 -f s16_le -r48000 -d10 sample.wav -D: selects the device. -c: selects the number of channels on the recording. -f: selects the format. -r: selects the sample rate. -d: determinate the duration recording time in seconds. sample.wav: Is the name of the resulting audio file. Running the last command, we started to record audio. It is time to make some noise and record it!   Playing audio from IMX8 boards. Now it is time to connect our headphones or speakers to the jack.   Also, as on arecord command you can check the devices where you can play audio from the board using the next command: aplay -l And you will get all the codecs to play audio:   To play our recordings we need to use the ALSA aplay command, it is important to select the correct audio codec to hear the audio from the jack on the board: aplay -Dplughw:3,0 sample.wav -D: selects the device. sample.wav: Is the name of audio file to play   Hope this will helpful for people who wants to record audio using PDM microphones and playing audio from IMX8 boards. Best regards.
查看全文
1. Description: On the i.MX Android camera HAL, It only supports YUYV sensor, regardless of whether the sensor is connected to ISP or ISI. Some users want to customize the sensor format, such as UYVY or raw, they need a guide to do this, this document intends to describe how to implement raw camera sensor on i.MX8MP android, and output raw data. Note: Base on  i.MX 8M plus, Android12_1.0.0.  2. Camera HAL Android's camera hardware abstraction layer (HAL) connects the higher level camera framework APIs in android.hardware.camera2 to your underlying camera driver and hardware. For more detail information, please refer to AOSP document: https://source.android.google.cn/docs/core/camera/camera3_requests_hal?hl=en while on I.MX camera HAL, the camera subsystem can be divided into several parts:   Camera framework:  frameworks\av\camera Camera service:    frameworks\av\services\camera\libcameraservice\ Camera provider: hardware/interfaces/camera/provider/ hardware/google/camera/common/hal/hidl_service/               hidl_service dlopen the camera HAL3. Camera HAL3:   vendor\nxp-opensource\imx\camera\ Camera driver:   vendor/nxp-opensource/kernel_imx/drivers/media/i2c  It's callstack can be list as follow:  There are 2 streams on pipeline, preview stream need 3 buffers and capture stream need 2 buffers: CameraDeviceSessionHwlImpl: ConfigurePipeline, stream 0: id 0, type 0, res 2592x1944, format 0x21, usage 0x3, space 0x8c20000, rot 0, is_phy 0, phy_id 0, size 8388608 CameraDeviceSessionHwlImpl: ConfigurePipeline create capture stream CameraDeviceSessionHwlImpl: ConfigurePipeline, stream 1: id 1, type 0, res 1024x768, format 0x22, usage 0x100, space 0x0, rot 0, is_phy 0, phy_id 0, size 0 CameraDeviceSessionHwlImpl: ConfigurePipeline create preview stream You can use this command to dump the stream input/output: "setprop vendor.rw.camera.test 1" to dump steam 0. "setprop vendor.rw.camera.test 2" to dump steam 1. Before you implement the command, you need to run “su; setenforce 0” to close the SeLinux, the data is dumped as "/data/x-src.data", "/data/x-dst.data", where "x" is the stream id as "0, "1,", "2", ...   Preview Stream Capture Stream ID 1 0 Resolution 1024*768 2592*1944 Format HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED (34) HAL_PIXEL_FORMAT_BLOB (33) Usage 0x900 GRALLOC_USAGE_HW_TEXTURE      (0x100) GRALLOC_USAGE_HW_COMPOSER  (0x800) 0x3 GRALLOC_USAGE_SW_READ_OFTEN Data space 0 HAL_DATASPACE_V0_JFIF  The following usage will be added by framework to distinguish preview and video:GRALLOC_USAGE_HW_VIDEO_ENCODER 3. Raw support  3.1 system modification  The default image for i.MX 8M Plus EVK supports basler + basler and the cameras can work after the image is flashed and boot up, it’s camera with ISP, but we need ISI to process raw. You should refer to Android_User’s_Guide.pdf, you need find the correct version, as Android12_2.0.0 is different with Android12_1.0.0. To make cameras work with Non-default images, execute the following additional commands: Only OV5640 (CSI1) on host: As we use OV2775 which support 1920*1080, unpacked raw12, the json file: 3.2 DTB modification  1. Firstly, change the BoardConfig.mk to generate dtbo-imx8mp-ov2775.img device\nxp\imx8m\evk_8mp\BoardConfig.mk: TARGET_BOARD_DTS_CONFIG += imx8mp-ov2775:imx8mp-evk-ov2775.dtb 2.  Secondly, add imx8mp-evk-ov2775.dts to vendor\nxp-opensource\kernel_imx\arch\arm64\boot\dts\freescale 3. Change imx8mp-evk-ov2775.dts, connect OV2775 to ISI: &isi_0 { status = "okay"; }; &isp_0 { status = "disabled"; }; &dewarp { status = "disabled"; }; 4. Build dtbo image and flash it to board: ./imx-make.sh dtboimage -j4 fastboot flash dtbo dtbo.img  3.3 Sensor driver modification  I use the OV2775 driver from the isp side, be careful that all the function such as g_frame_interval and enum_frame_size should be implemented, or the HAL will get wrong parameters and return error. static struct v4l2_subdev_video_ops ov2775_subdev_video_ops = { .g_frame_interval = ov2775_g_frame_interval, .s_frame_interval = ov2775_s_frame_interval, .s_stream = ov2775_s_stream, }; static const struct v4l2_subdev_pad_ops ov2775_subdev_pad_ops = { .enum_mbus_code = ov2775_enum_mbus_code, .set_fmt = ov2775_set_fmt, .get_fmt = ov2775_get_fmt, .enum_frame_size = ov2775_enum_frame_size, .enum_frame_interval = ov2775_enum_frame_interval, };  3.4 ISI driver modification  We need to add raw format on ISI driver: }, { .name = "RAW12 (SBGGR12)", .fourcc = V4L2_PIX_FMT_SBGGR12, .depth = { 16 }, .color = MXC_ISI_OUT_FMT_RAW12, .memplanes = 1, .colplanes = 1, .mbus_code = MEDIA_BUS_FMT_SBGGR12_1X12, }, { .name = "RAW10 (SGRBG10)", .fourcc = V4L2_PIX_FMT_SGRBG10, .depth = { 16 }, .color = MXC_ISI_OUT_FMT_RAW10, .memplanes = 1, .colplanes = 1, .mbus_code = MEDIA_BUS_FMT_SGRBG10_1X10, } 3.5 Camera HAL modification As there are preview stream and capture stream on the pipeline. GPU does not support raw format, it will print error log when application set raw format:    02-10 18:49:02.162 436 436 E NxpAllocatorHal: convertToMemDescriptor Unsupported fomat PixelFormat::RAW10 02-10 18:49:02.163 2390 2445 E GraphicBufferAllocator: Failed to allocate (1920 x 1080) layerCount 1 format 37 usage 20303: 7 02-10 18:49:02.163 2390 2445 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) dequeueBuffer: createGraphicBuffer failed 02-10 18:49:02.163 2390 2405 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) requestBuffer: slot 0 is not owned by the producer (state = FREE) 02-10 18:49:02.163 2148 2423 E Surface : dequeueBuffer: IGraphicBufferProducer::requestBuffer failed: -22 02-10 18:49:02.163 2390 2445 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) cancelBuffer: slot 0 is not owned by the producer (state = FREE) 02-10 18:49:02.164 2148 2423 E Camera3-OutputStream: getBufferLockedCommon: Stream 1: Can't dequeue next output buffer: Invalid argument (-22)   Modifying the gpu code is not recommended. When preview stream, it's pixel format is fixed to HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED, it needs YUYV format, in this patch, we don't convert raw12 to yuyv, just copy the buffer from input to output, so the preview stream is raw12 actually. When capture stream, we use the Blob format, which usually used for JPEG format. when we find the format is Blob pass down by application, camera HAL will copy the buffer from input to output directly. You can check the detail on function ProcessCapturedBuffer(),    4. Application and Tool 4.1 Application  The test application on the attachment “android-Camera2Basic-master_application.7z”, It's basically a common camera application, it set the capture stream format to blob:  Size largest = Collections.max( Arrays.asList(map.getOutputSizes(ImageFormat.JPEG)), new CompareSizesByArea()); mImageReader = ImageReader.newInstance(largest.getWidth(), largest.getHeight(), ImageFormat.JPEG, /*maxImages*/2); 4.2 Tool We use 7yuv tool to check the raw12 format, which is captured by applicable or dump by HAL, you need set the parameter on the right side:   ImageJ tool also can be used to review raw format.
查看全文