i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
    OpenSSL is popular software library for applications that secure communications over computer networks against eavesdropping or need to identify the party at the other end. It is widely used in internet web servers, serving a majority of all web sites. OpenSSL contains an open-source implementation of the Transport Layer Security (TLS) and Secure Sockets Layer (SSL) protocols, it is a robust, commercial-grade, and full-featured toolkit for the SSL and TLS protocols. OpenSSL is also a general-purpose cryptography library. Its core library, written in the C programming language, implements basic cryptographic functions and provides various utility functions. Wrappers allowing the use of the OpenSSL library in a variety of computer languages are available. More and more embeded systems, like IoT gateway, ePOS, based on i.MX use OpenSSL for their secure communications and cryptographic operations. But it's cryptography library is pure software implementation which need to occupy lots of CPU resouce and the perfermance is very weak than dedicated hardware IP (like CAAM).    CAAM is the i.MX's cryptographic acceleration and assurance module, which serves as NXP's latest cryptographic acceleration and offloading hardware. It combines functions previously implemented in separate modules to create a modular and scalable acceleration and assurance engine. It also implements block encryption algorithms, stream cipher algorithms, hashing algorithms, public key algorithms (i.MX6UL/i.MX7D/S), and a hardware random number generator.   The official Yocto release (L4.1.15_2.0.0-ga) of the i.MX only enable cryptodev for accelerating symmetric algorithms and hashing algorithms, not support asymmetric algorithms(RSA, ECC). And its engine in OpenSSL(version 1.0.2h) also miss some features which is used to support symmetric algorithms and hashing algorithms, for example, AES ECB, SHA224/256, etc. These patches in the post will close the above gaps for i.MX Linux system. The software environments as the belows: Linux kernel: imx_4.1.15_2.0.0_ga cryptodev: 1.8 OpenSSL: 1.0.2h The patches include the following key features: 1, Add public key cryptography part in CAAM driver, through protocol commands, to implement a number of public (and private) key functions. These are DSA and ECDSA sign/verify, Diffie-Hellman (DH) and ECDH key agreement, ECC key generation, DLC key generation, RSA encryption/decryption, RSA key-generation finalization. 2, Add big number operation and elliptic curve math in CAAM driver to implement addition, subtraction, multiplication, exponentiation, reduction, inversion, greatest common divisor, prime testing and point add, point double, point multiply. 3, Add API in cryptodev to support RSA encryption/decryption, DSA/ECDSA sign/verify, DH/ECDH key agreement, ECC & DLC & RSA key generation and big number operation and elliptic curve math. 4, Add public key cryptography functions, hardware rng, and missing hash symmetric algorithms in OpenSSL crytodev engine. Note: 1, You can refer to ecdhtest.c, ecdsatest.c, dhtest.c, dsatest.c, rsa_test.c for how to use crytodev engine in your applications based on libcryto.so. You can also find their executable programs in folder openssl-1.0.2h/test after compiling. 2, If you want to call crytodev API directly to accelerate public key cryptography operations, please refer to asymmetric_cipher.c in cryptodev-linux-1.8/tests. Current Limitation: 1, CAAM driver don't support AES GCM/CCM but hardware supporting. I plan to add the feature next version. 2, ECDSA sign/verify will fail on some binary curves (sect163r1, sect163r2, sect193r1, sect193r2, sect233r1, sect283r1, sect409r1, sect571r1 and X9.62 binary curves). I will try to find the root cause and fix it.   ==================================== for  some binary curves (sect163r1, sect163r2, sect193r1, sect193r2, sect233r1, sect283r1, sect409r1, sect571r1 and X9.62 binary curves)  are rarely used, so i will try to find the root cause when i'm free.  +++++++++++++++++++++++    updating for Linux-4.14.78-1.1.10 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux -4.14.78-1.1.10. The new software environments as the belows: Linux kernel: imx_4.14.78_1.1.10 cryptodev: 1.9 OpenSSL: 1.0.2p HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini, i.MX8/8X. The patches include the following new features: 1, support  RSA key generation but defaultly use openssl build-in function (BN_generate_prime_ex) to create prime p, q for higher security. If need to use CAAM accelerating,  please comment Macro USE_BUILTIN_PRIME_GENERATION, but don't confirm its security. 2, Add Manufacturing-protection feature, and you can refer to manufacturing_protection_test function in asymmetric_cipher.c. 3, Support AES GCM in cryptodev. 4, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-4.14.78-1.1.10 and copy meta-openssl-caam to folder <Yocto 4.14.78-1.1.10 dir>/sources/ 5, Run DISTRO=fsl-imx-wayland MACHINE=imx6ulevk source fsl-setup-release.sh -b build-imx6ulevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into /build-imx6ulevk/conf/bblayers.conf 6, bitbake fsl-image-validation-imx 7, Run the below command on your i.MX6UL EVK board. modprobe cryptodev openssl genrsa -f4 -engine cryptodev 512 -elapsed openssl speed dsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 1024 -elapsed openssl speed rsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 2048 -elapsed openssl speed ecdsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 3072 -elapsed openssl speed ecdh -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 4096 -elapsed openssl speed -evp sha256 -engine cryptodev -elapsed openssl speed -evp aes-128-cbc -engine cryptodev -elapsed openssl speed -evp aes-128-ecb -engine cryptodev -elapsed openssl speed -evp aes-128-cfb -engine cryptodev -elapsed openssl speed -evp aes-128-ofb -engine cryptodev -elapsed openssl speed -evp des-ede3 -engine cryptodev -elapsed openssl speed -evp des-cbc -engine cryptodev -elapsed openssl speed -evp des-ede3-cfb -engine cryptodev -elapsed +++++++++++++++++++++++    updating for Linux-4.14.98-2.3.3 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux -4.14.98-2.3.3. The new software environments as the belows: Linux kernel: imx_4.14.98-2.3.3 cryptodev: 1.9 OpenSSL: 1.0.2p HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano, i.MX8/8X. The patches include the following new features: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-4.14.98-2.3.3 and copy meta-openssl-caam to folder <Yocto 4.14.98-2.3.3 dir>/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into /build-imx8mmevk/conf/bblayers.conf 3, bitbake fsl-image-validation-imx 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl genrsa -f4 -engine cryptodev 512 -elapsed openssl speed dsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 1024 -elapsed openssl speed rsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 2048 -elapsed openssl speed ecdsa -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 3072 -elapsed openssl speed ecdh -engine cryptodev -elapsed openssl genrsa -f4 -engine cryptodev 4096 -elapsed openssl speed -evp sha256 -engine cryptodev -elapsed openssl speed -evp aes-128-cbc -engine cryptodev -elapsed openssl speed -evp aes-128-ecb -engine cryptodev -elapsed openssl speed -evp aes-128-cfb -engine cryptodev -elapsed openssl speed -evp aes-128-ofb -engine cryptodev -elapsed openssl speed -evp des-ede3 -engine cryptodev -elapsed openssl speed -evp des-cbc -engine cryptodev -elapsed openssl speed -evp des-ede3-cfb -engine cryptodev -elapsed +++++++++++++++++++++++    updating for Linux-4.19.35-1.1.2 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 4.19.35-1.1.2​​.  Software environments as the belows: Linux kernel: imx_4.19.35-1.1.2 cryptodev: 1.10 OpenSSL: 1.1.1l HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-4.19.35-1.1.2 and copy meta-openssl-caam to folder <Yocto 4.19.35-1.1.2 dir>/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 4.19.35-1.1.2 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake fsl-image-validation-imx. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed +++++++++++++++++++++++    updating for Linux-5.4.70-2.3.4 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.4.70_2.3.4​​.  Software environments as the belows: Linux kernel: imx_5.4.70_2.3.4 cryptodev: 1.10 OpenSSL: 1.1.1l HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-5.4.70-2.3.4  and copy meta-openssl-caam to folder <Yocto 5.4.70_2.3.4 dir>/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 5.4.70_2.3.4 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed     +++++++++++++++++++++++    updating for Linux-5.10.52-2.1.0 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.10.52_2.1.0​​.  Software environments as the belows: Linux kernel: lf-5.10.y cryptodev: 1.12 OpenSSL: 1.1.1l HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-5.10.52-2.1.0 and copy meta-openssl-caam to folder <Yocto 5.10.52_2.1.0 dir>/sources/ 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 5.10.52_2.1.0 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed   +++++++++++++++++++++++    updating for Linux-5.15.71-2.2.0 ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.15.71-2.2.0​​.  Software environments as the belows: Linux kernel: lf-5.15.71-2.2.0 cryptodev: 1.12 OpenSSL: 3.1.0 HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, git clone https://gitee.com/zxd2021-imx/meta-openssl-caam.git, git checkout Linux-5.15.71-2.2.0 and copy meta-openssl-caam to folder <Yocto 5.15.71_2.2.0 dir>/sources/ 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-openssl-caam " into <Yocto 5.15.71_2.2.0 dir>/build-imx8mmevk/conf/bblayers.conf. 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev openssl speed sm2 openssl speed dsa openssl speed rsa openssl speed ecdsa openssl speed ecdh openssl genrsa -f4 -engine devcrypto 512 openssl genrsa -f4 -engine devcrypto 1024 openssl genrsa -f4 -engine devcrypto 2048 openssl genrsa -f4 -engine devcrypto 3072 openssl genrsa -f4 -engine devcrypto 4096 openssl speed -evp sha256 -engine devcrypto -elapsed openssl speed -evp aes-128-cbc -engine devcrypto -elapsed openssl speed -evp aes-128-ecb -engine devcrypto -elapsed openssl speed -evp aes-128-cfb -engine devcrypto -elapsed openssl speed -evp aes-128-ofb -engine devcrypto -elapsed openssl speed -evp des-ede3 -engine devcrypto -elapsed openssl speed -evp des-cbc -engine devcrypto -elapsed openssl speed -evp des-ede3-cfb -engine devcrypto -elapsed    
查看全文
Platform: i.MX8MP SW:Linux 5.4.70.2.3.0 On current linux BSP, PCIE driver does not support Hot-plug, customers wants to turn off PCIE device to save power, attached is guide. Remove PCIE device driver Suspend PCIE driver Turn off PCIE device power supply Turn on PCIE device power supply Resume PCIE driver Rescan PCIE device Load PCIE device driver
查看全文
Platform: i.MX8MP EVK BSP: Linux 5.4.70.2.3.0 Customer reported UI on HDMI monitor is abnormal and has more line on left side when doing HDMI hot-plug on i.MX8MP running with L5.4.70.2.3.0.   This issue can’t be reproduced on latest BSP such as 5.10 and above, several patch for HDMI from latest BSP can fix this issue.  
查看全文
This doc will show: i.MX6SLL EVK board without connect hardware LCD display, using FreeRDP to share screen to remote PC which in same network, PC take this shared screen could run any command on i.MX6SLL EVK board. HW: i.MX6SLL EVK board, PC, usb network adapter SW: i.MX6SLL Linux 5.15.72_2.2.0 BSP release, and code change in this doc 1>yocto-5.15.72/6sll-bld/conf/local.conf, add below line, as freerdp depend on ffmpeg. LICENSE_FLAGS_ACCEPTED+="commercial" 2>pixman need switch to 0.42.0, enter folder yocto-5.15.72/6sll-bld/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/pixman/1_0.40.0-r0/pixman-0.40.0, fetch latest 0.42.0 version code from https://github.com/freedesktop/pixman.git 3>freerdp need use 2.8.0, enter folder yocto-5.15.72/6sll-bld/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/freerdp/1_2.6.1-r0/git should checkout to 2.8.0 tag; then to use neon accelerate freerdp related function, such as color space conversion, image codec encoding, apply patch freerdp-codechange-neon.diff. 4>Enter yocto-5.15.72/sources/meta-openembedded/meta-oe/recipes-support/freerdp, file freerdp_2.6.1.bb change as freerdp-2.6.1-bbfile.diff 5> bitbake -c compile ffmpeg bitbake -c install ffmpeg bitbake -c compile pixman bitbake -c install pixman bitbake -c compile freerdp bitbake -c install freerdp 6> Copy generated new libs to i.MX6SLL Linux rootfs: cp /root/imx6sllevk-linux-lib/lib* /usr/lib/ cd /usr/lib/ rm libfreerdp-client2.so.2 libfreerdp2.so.2 libpixman-1.so.0 libwinpr-tools2.so.2 libwinpr2.so.2 ln -s libfreerdp-client2.so.2.8.0 libfreerdp-client2.so.2 ln -s libfreerdp2.so.2.8.0 libfreerdp2.so.2 ln -s libpixman-1.so.0.42.0 libpixman-1.so.0 ln -s libwinpr-tools2.so.2.8.0 libwinpr-tools2.so.2 ln -s libwinpr2.so.2.8.0 libwinpr2.so.2 ln -s libavcodec.so.58.134.100 libavcodec.so.58 ln -s libavutil.so.56.70.100 libavutil.so.56 ln -s libswresample.so.3.9.100 libswresample.so.3 Make sure: libfreerdp-client2.so.2 -> libfreerdp-client2.so.2.8.0 libfreerdp2.so.2 -> libfreerdp2.so.2.8.0 libwinpr-tools2.so.2 -> libwinpr-tools2.so.2.8.0 libwinpr2.so.2 -> libwinpr2.so.2.8.0 libswresample.so.3 -> libswresample.so.3.9.100 libavutil.so.56 -> libavutil.so.56.70.100 libavcodec.so.58 -> libavcodec.so.58.134.100 7>i.MX6SLL Linux OS, file /etc/xdg/weston/weston.ini, change start-on-startup to true [screen-share] command=WLOG_APPENDER=file WLOG_FILEAPPENDER_OUTPUT_FILE_NAME=output.log WLOG_FILEAPPENDER_OUTPUT_FILE_PATH=/tmp /usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --no-clients-resize --rdp-tls-cert=/etc/freerdp/keys/server.crt --rdp-tls-key=/etc/freerdp/keys/server.key start-on-startup=true 8> i.MX6SLL Linux OS, run below cmd: mkdir /etc/freerdp mkdir /etc/freerdp/keys /root/imx6sllevk-linux-lib/winpr-makecert -path /etc/freerdp/keys mv /etc/freerdp/keys/imx6sllevk.crt /etc/freerdp/keys/server.crt mv /etc/freerdp/keys/imx6sllevk.key /etc/freerdp/keys/server.key service weston stop service weston start 9>Plug usb network adapter to i.MX6SLL EVK board J10; i.MX6SLL board and PC must in same network, ping without problem. i.MX6SLL Linux OS, there are two process name as "weston", one process is weston rdp backend will share screen to PC. If only one weston process, need check did miss copy any new lib or check libary file name. 10>PC side: wfreerdp.exe /v:IPADDRESS_OF_IMX6SLLEVK There will prompt dialog box for user name and password, just press ESC, then PC side will show i.MX6SLL Linux desktop screen; Click console button of i.MX6SLL Linux OS desktop, within that console input any i.MX6SLL Linux OS cmd, check result of it from PC side. Known issue: wfreerdp.exe is downloaded from https://ci.freerdp.com/job/freerdp-nightly-windows/ If run latest wfreerdp.exe but show nothing of remote desktop, try attached version wfreerdp.exe(3.0.0-dev). Also you can try check log files first: i.MX6SLL Linux OS file /tmp/output.log; PC side generated log file as: wfreerdp.exe /v:IPADDRESS_OF_IMX6SLLEVK /log-level:TRACE > rdp.log Reference: 1>https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat... 2>https://github.com/FreeRDP 3>https://github.com/freedesktop/pixman 4>https://github.com/DLTcollab/sse2neon    
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is the detailed programming aid for the registers associated with DRAM initialization (DDR3 and LPDDR2) of the MX6UL/ULL/ULZ (consolidated RPA). The last work sheet tab in the tool formats the register settings for use with the ARM DS5/RealView debugger. It can be manually converted by the user to a DCD file format used by uboot or other bootloaders (note the removal of debugger specific commands in this tab). The programming aids were developed for internal NXP validation and development boards.   This tool serves as an aid to assist with programming the DDR interface of the MX6UL/ULL/ULZ and is based on the DDR initialization scripts developed by the R&D team and no guarantees are made by this tool.   The following are some general notes regarding this tool: Refer to the "How To Use" tab in the tool as a starting point to use this tool. Note that in the "DStream .ds file" tab there are DS5 debugger specific commands that should be commented out or removed when using the DRAM initialization for non-debugger specific applications (like when porting to bootloaders). This tool may be updated on an as-needed basis for bug fixes or future improvements.  There is no schedule for aforementioned maintenance.  
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. i.MX 8/8X DDR Tools Overview   This page contains the latest releases for the i.MX 8/8X DDR Tools. The tools described on this page cover the following i.MX 8/8X Family SoCs with the System Controller Unit (SCU): i.MX 8QuadMax and its derivatives i.MX 8QuadPlus i.MX 8QuadXPlus and its derivatives i.MX 8DualXPlus and i.MX 8DualX  i.MX 8DXL (i.MX 8XLite) and its derivatives i.MX 8SXL  NOTE: For the i.MX 8M Family of DDR tools please refer to the : i.MX 8M Family DDR Tool Release                           The purpose of the i.MX 8/8X DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.).  This process equips the user to then proceed with the bring-up of a boot loader and an OS.  Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface.     The i.MX 8/8X DDR Tools consist of: DDR Register Programming Aid (RPA) DDR Stress test   For more details regarding these DDR tools and their usage, refer to the MX8X_DDR_Tools_quickstart_guide.pdf attached to this page.   i.MX 8/8X DDR Register Programming Aid (RPA)   The i.MX 8/8X DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization in two formats (in separate Excel worksheet tabs):   DDR Stress Test script: This format is used specifically with the DDR stress test by first copying the contents in this worksheet tab and then pasting it to a text file, naming the document with the “.ds” file extension. The user will select this file when executing the DDR stress test. DCD CFG file: This format is the configuration file used specifically by the SCU Firmware (SCFW). In this scenario, the user copies the contents in this worksheet tab and pastes it to a text file, naming the document with the “.cfg” file extension and placing this file in the appropriate SCFW board file directory.   i.MX 8/8X DDR Register Programming Aid (RPA): Current Versions Note: In all cases, the RPA revision is aligned to a minimum SCFW version as shown in the table below. In some cases, the BSP alignment is provided as extra detail, however, the RPA tool is specifically aligned to a minimum SCFW version and later. To obtain the latest RPAs, please refer to the following links (note, existing RPAs have been removed from this main page and moved to the SoC specific links below): i.MX8QM: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-DDR-Register-Programming-Aid-RPA/ta-p/1166307 i.MX8QXP/QXP/DX: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302 i.MX8DXL/SXL: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8DXL-DDR-Register-Programming-Aid-RPA/ta-p/1602262   Processor Mask Revisions Memory Supported Latest RPA Version * Notes i.MX 8QM B0 LPDDR4 Rev 23*** Rev 22** Rev 21** Rev 20** Rev 19** Rev 23: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev22: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  Rev 21: Fixed 1 DRC operation to comment out calls to VREF training to DRC1 and added DDRC_SCHED register programming to align with latest SCFW programming (refer to RPA revision history for more details). Rev 20: use with SCFW 1.4.0 and NXP BSP GA version L5.4.3_2_0_0 later (to support SW VREF training work around command) Rev 19: use with SCFW 1.3.1 and NXP BSP GA version L5.4.3_1_0_0 i.MX 8QXP C0, B0 LPDDR4 Rev 16*** Rev 15** Rev 14** Rev 13** Rev 16: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 15: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  Rev 14: use with SCFW 1.4.0 and NXP BSP GA version L5.4.3_2_0_0 later (to support SW VREF training work around command) Rev 13: use with SCFW 1.3.1 and NXP BSP GA version L5.4.3_1_0_0 i.MX 8QXP C0, B0 DDR3L Rev 23 Rev 22*** Rev 21 Rev 20 Rev 23:  -Corrected Register Configuration DDR_PHY_PTR4.tDINIT1 bit field programming. Previously, the calculation was based on tRFC only, however, the calculation should have been based on "tRFC+10ns". This was corrected. -Set DDRC_INIT4, DDR3 MR2.ASR=1 as the default setting to allow for the DRAM to select the self refresh rate automatically based on its case temperature (but user has the option to disable via pull-down menu). Also, removed conditional setting for DTCR0.DTRDBITR as it is not needed since DDR3 does not support DBI. Default setting of this was zero and will remain that way. -Provided option to user to select auto refresh rate based on the intended max temperature of the DDR3L device (1X, 2X, 4X). User should confirm with the DDR3L data sheet for supported temperature ranges and associated refresh rate. Rev 22: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 21: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW. -Compatible with SCFW 1.1.10 and later -Changes made to this revision do not affect the DCD CFG file output based on v19 -Issue discovered in the DDR stress test script, wherein certain commands were not being properly configured based on the ECC setting in the Register Configuration worksheet; this was resolved (cells A84, A87, A90, A93 ) -In addition, in both DCD CFG and DDR stress test script worksheets, all commands that depend on ECC config have been updated to include an "OR" with whether or not the data bus is configured for 16-bit (ECC is only supported for full 32-bit data bus width configurations) i.MX 8DualX C0, B0 LPDDR4 Rev 16*** Rev 15* Rev 14** Rev 13** Rev 16: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 15: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  Rev 14: use with SCFW 1.4.0 and NXP BSP GA version L5.4.3_2_0_0 later (to support SW VREF training work around command) Rev 13: use with SCFW 1.3.1 and NXP BSP GA version L5.4.3_1_0_0 i.MX 8DualX C0, B0 DDR3L Rev 21 Rev 20*** Rev 19 Rev 18 Rev 21: -Corrected Register Configuration DDR_PHY_PTR4.tDINIT1 bit field programming. Previously, the calculation was based on tRFC only, however, the calculation should have been based on "tRFC+10ns". This was corrected. -Set DDRC_INIT4, DDR3 MR2.ASR=1 as the default setting to allow for the DRAM to select the self refresh rate automatically based on its case temperature (but user has the option to disable via pull-down menu). Also, removed conditional setting for DTCR0.DTRDBITR as it is not needed since DDR3 does not support DBI. Default setting of this was zero and will remain that way. -Provided option to user to select auto refresh rate based on the intended max temperature of the DDR3L device (1X, 2X, 4X). User should confirm with the DDR3L data sheet for supported temperature ranges and associated refresh rate. Rev 20: IMPORTANT: this is aligned to SCFWv1.7.0 (and later SCFW versions). When using SCFWv1.7.0 (and later SCFW versions), you must use this version or later RPA and cannot use earlier versions of the RPA. See note at end of table. Rev 19: The following changes have no effect on the DDR IO interface. This updated setting basically adds a define in the DCD file for the total DDR density configured by the RPA. This defined is used by the SCFW.  -Compatible with SCFW 1.1.10 and later * For a history of the previous versions of an RPA, refer to the Revision History tab of the respective RPA.  ** In general, it is recommended to use the latest RPA tool even with a pre-released BSP as it ensures you are testing with the latest fixes and features. Older versions of the RPA may be provided to support existing/released versions of the BSP.  This only applies to those RPA tools that are compatible with pre-release BSPs but may not be compatible with released versions of the BSP.   ***IMPORTANT: as stated in the table above, for the noted RPA version, it is aligned to SCFWv1.7.0 (and later SCFW versions).  Older versions of the RPA are not aligned to SCFWv1.7.0 (and later SCFW versions).  If trying to use an older version of an RPA with SCFWv1.7.0 (and later SCFW versions), it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QXP/DualX: DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ For MX8QM: DATA 4 0xff148000 0x00000885 /* DRC0 bringup */ DATA 4 0xff1a0000 0x00000885 /* DRC1 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 (and later SCFW versions) (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QXP: [remove] ifndef SCFW_DCD [remove] /* For 1200MHz DDR, DRC 600MHz operation */ [remove] DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ [remove] #else <keep code as is> [remove] #endif Note: when it is stated "SCFWv1.7.0 (and later SCFW versions)", it implies SCFWv1.7.0, 1.7.1, 1.7.2... 1.8.0, 1.9.0, 1.10.0... etc., where "..." are minor versions/patches, so when you see 1.7.2... it implies 1.7.3, 1.7.4, etc.).  Unless otherwise noted, the latest RPA shown in the table above is aligned to the latest SCFW release.    i.MX 8/8X DDR Stress Test    The i.MX 8/8X DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational prior to building the SCFW for use with u-boot and OS bring-up. The DDR stress test uses the .ds DDR stress test script generated from the RPA tool along with a special build of the SCFW, built with option: DDR_CON=ddr_stress_test_parser Or in the case of i.MX 8QuadMax use of one DDR Controller: DDR_CON=ddr_stress_test_parser_DRC0_only The DDR stress test offers a Target option to dictate which SoC is under test. The following are Target options to select from: MX8QM – used to test i.MX 8QuadMax and its derivatives i.MX 8QuadPlus MX8QX – used to test i.MX 8QuadXPlus and its derivatives i.MX 8DualXPlus/DualX MX8DXL – used to test i.MX 8DXL and its derivatives i.MX8 SXL     To install the DDR Stress Test, save and extract the zip file mx8_ddr_stress_test_ERxx_installation.zip   (where 'xx' is the current version number) and follow the on-screen installation instructions. Note, when extracting the DDR Stress Test tool .zip file, it is recommended to perform an "Extract here" operation.  Some systems do not allow for the extracted installation executable to run from another folder and will only work when being executed from the same location as the original, downloaded zip file.  For more details on the DDR stress test usage, refer to the MX8_DDR_Tool_User_Guide found in the DDR Stress Test tool delivery. NOTE: Before using the DDR tools on a new custom board, the user should properly port the SCU Firmware (SCFW) to this new board. The DDR tools will not be able to run without a properly ported and working SCFW.            i.MX 8/8X DDR Stress Test Requirements The tool requires access to the Windows registry, hence users must run it in administrator mode. The tool cannot run on an OEM closed device that requires images signed by the customer When users design new i.MX 8/8X boards, please make sure to follow the rules outlined in the respective Hardware Developers Guide and the MX8_DDR_Tool_User_Guide, which can help users bring up DDR devices on their respective i.MX 8/8X boards.   i.MX 8/8X DDR Stress Test SECO Firmware It is generally not recommended to update the SECO (ahab) firmware that comes default with the DDR Stress Test. This is not recommended because the purpose of the DDR Stress Test is to test the DDR memory interface, not the entire SCFW to SECO firmware operation even though a newer version of the SCFW may complain that the SECO firmware version is not the latest. The SECO firmware version that comes with the DDR Stress Test has been tested and proven to work by the factory before the DDR Stress Test release; updating the SECO firmware to a different version may result in unintended consequences rendering the DDR stress test inoperable. In most cases, it is allowable to update only the SCFW without updating the SECO firmware. Should the user wish to update the SECO firmware version in the DDR Stress Test, then they will need to rename this firmware without the silicon version (for example, if updating the MX8QM SECO firmware, the user will need to rename mx8qmb0-ahab-container.img to mx8qm-ahab-container.img, basically remove the “b0”). The exception is for the MX8QXP, if updating the C0 silicon version SECO firmware, then the user should maintain the C0 nomenclature. If the user finds that the updated SECO firmware causes the DDR Stress Test to become inoperable, then it is recommended to revert to the default SECO firmware version that came with the DDR Stress Test release. i.MX 8/8X DDR Stress Test User Guide The i.MX 8/8X DDR Stress Test tool includes the document: MX8_DDR_Tool_User_Guide.pdf NOTE: Please read the MX8_DDR_Tool_User_Guide inside the package carefully before you use this tool.   DDR Stress Test Revision History   Rev Major Changes (Features) NXP BSP Software Version ER 14 Updated to support parsing of the VREF training command in the DDR Stress Test script This version is aligned with NXP BSP GA version L5.4.3_2_0_0 and later. ER15 - Support for i.MX 8Lite (aka DXL) - Provides more verbose output in event of data training failures, specifically on which byte lanes failed - Aids in debug of board layout issues This version is aligned with NXP BSP GA version Linux 5.15.71_2.2.0 and later.    Related Resources Links: i.MX 8ULP DDR tools: i.MX Software and Development Tools | NXP Semiconductors Scroll down to “Other Resources --> Tools --> DDR Tools” i.MX 8M Family DDR Tool Release  i.MX 6/7 DDR Stress test GUI Tool i.MX 8QM RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-DDR-Register-Programming-Aid-RPA/ta-p/1166307 i.MX 8QXP/DXP/DX RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302 i.MX 8DXL (i.MX 8XLite) RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8DXL-DDR-Register-Programming-Aid-RPA/ta-p/1602262   FAQs: Q. When the DDR stress test is running, it indicates testing region 1 and then region 2. What is region 1 and region 2? A. There are two distinct DDR memory regions in the i.MX8X series which is due to the architecture of Cortex A core and the associated memory map of the i.MX8X. Region 1 is the 32-bit region, starting at 0x080000000 and ending at 0x0FFFFFFFF (2GB total) Region 2 is the 64-bit region (for the Cortex A core architecture), starting at 0x880000000 and ends at the remaining density: • For 4GB total on board density, 2GB for region 1 and 2GB for region 2, so region 2 will end at 0x8FFFFFFFF (0x900000000 minus 1) • For 6GB total (NXP board density), 2GB for region 1 and 4GB for region 2, so region 2 will end at 0x97FFFFFFF (0x980000000 minus 1) • For 8GB total, 2GB for region 1 and 6GB for region 2, so region 2 will end at 0x9FFFFFFFF (0xA00000000 minus 1) Hence there is a “hole” in the memory map between region 1 and region 2. As such, the DDR stress test first tests the lower region (region 1) until it is exhausted (up to 2GB), and if the DDR density exceeds 2GB, the test will test the remaining density in region 2. Q. Do the i.MX8X series SoCs support LPDDR4 memories with 17 row addresses (R[16:0])? A. The i.MX8QM, i.MX8QXP, and i.MX8DXP SoCs and their derivatives cannot support newer 17-row-address LPDDR4 memories. This means, in order to support the maximum 4GB (32Gb) LPDDR4 density, the configuration must be 16-row, 2 rank (as opposed to the unsupported 17-row, 1 rank). The upcoming i.MX8DXL is planned to support 17-row address LPDDR4 devices. Q. I can select a different i.MX8X AP UART port when running the DDR Stress Test? A. It is highly recommended to follow NXP board designs including selecting the same UART ports; this eases the user’s software porting efforts and minimizes issues with needless debugging. The DDR Stress Test requires the use of the USB OTG port and the AP UART port (and it is highly recommended to connect the SCFW UART port for SCFW debug messages). To date, the factory sees no reason why the user would need to select a different AP UART port than what is used on NXP boards. Selecting the same AP UART port ensures a faster bring up of the DDR stress test rather than needlessly debugging why a different UART port is not working. In any event, some wish to use a different UART port for whatever reason, as such, NXP has placed work arounds to allow the selection of a different UART port. To select a different UART port (0,1, or 2), the user simply needs to add the following line to the end of the DDR Stress Test DDR initialization (.ds) script: memory set  0x5C01042C 32   <UART port value> memory set  0x5C01042C 32   0x00000000   # UART0 port selection for AP UART (default) memory set  0x5C01042C 32   0x00000001   # UART1 port selection for AP UART memory set  0x5C01042C 32   0x00000002   # UART2 port selection for AP UART Note that UART ports 0, 1, and 2 have pad names that are default UART pins (IOMUX ALT0 config). To date, the DDR tools do not support other UART ports that are mux’d out on other non-default UART pins. However, there is an exception for i.MX8QXP/DXP and the upcoming i.MX8DXL where UART3 mux’d out on FLEXCAN2 can be used. To select this, add the following to the end of the .ds file: memory set  0x5C01042C 32   0x00000003   # UART3 port selection for AP UART (exception for i.MX8QXP/DXP and i.MX8DXL) Some RPAs do have support built in (via a pull down menu) to select the UART port. For those RPAs that do not have this feature, this is due to the fact that these RPA (NXP boards) were not tested with a different UART port as the board requires cutting traces and re-wiring the UART signals and some boards may not have these UART traces readily available. However, the user is still able to manually add this UART port selection. Refer to the following RPAs to see the UART port select option: MX8QXP DDR3 MX8DXP DDR3 Q. Why does the DDR stress test appear to hang when testing [MX8QM with 8GB (64Gb) or MX8QXP with 4GB (32Gb)] of LPDDR4 memory? A. The issue is not caused by the DDR stress test itself but by the version of the SCFW being used. The default version of the SCFW binary pre-dates a change made by the SCFW to ignore DRAM density limitations when it detects that the DDR stress test is running. This version of the SCFW associated with the DDR stress test ER14 limits the testable DRAM density to [MX8QM: 6GB, MX8QXP: 3GB], as this version of the SCFW is configured to operate on NXP boards as a basis. As noted in the DDR stress test user guide, it is recommended for users to port the latest SCFW to their board first before using the DDR stress test to account for board differences between NXP’s board and their board.  In addition, the user has the following options to enable testing beyond [MX8QM: 6GB, MX8QXP: 3GB]; note it is the responsibility of the user to ensure a properly working, ported version of the SCFW prior to operating the DDR stress test. 1. The latest SCFW should contain an update that sets no density limit if it is detected that the SCFW is built for usage with the DDR Tool - the user can try to get the latest porting kit and build the new firmware.  This is the recommended change. 2. In board.c, function board_system_config(), there is this chunk of code (MX8QM example shown) if using an existing/older SCFW that pre-dates this change: /* Board has 6GB memory so fragment upper region and retain 4GB */         BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL,             0xFFFFFFFFFULL)); User can modify it as follows:     if (ddrtest == SC_FALSE)     {         sc_rm_mr_t mr_temp;         /* Board has 6GB memory so fragment upper region and retain 4GB */         BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL,             0xFFFFFFFFFULL));         BRD_ERR(rm_memreg_free(pt_boot, mr_temp));     } This is disables execution of this section of code if the SCFW is built for the DDR Tool (the same as 1. but needs to be done by the user manually when using an earlier firmware version). 3. Change 0x980000000 to 0xA00000000 in the above chunk of code. That should allow for 8GB density for MX8QM example shown above (for MX8QXP, change 0x8C0000000ULL to 0x900000000ULL for 4GB density).  
查看全文
From Android 12, NXP use GKI(Generl kernel image) instead of NXP's kernel code.  This follow up Android ASOP standard. This article described that when customer use Android 12 and later version, they need to pay attention on GKI development, which is different with previous version.
查看全文
We are pleased to announce that Config Tools for i.MX v13 are now available.
查看全文
Introduction This document intends to describe how to implement workaround for ERR050145 (ISI: Memory overwrite occurring outside of allocated buffer space corrupting system memory) based on Linux BSP. ERR050145 is applicable for i.MX8QM B0, i.MX8QXP B0 series products.   Software Platform Reference patches stated into this document are developed and validated on L4.14.98_GA2.0.0 release.   Software Workaround As workaround stated, the xRDC can be programmed to grant write access to the ISI only within its allocated frame buffer space, which can prevent the corruption. So under Linux, we can consider to implement workaround like so: Create children partition for ISI and allocate buffers. Then Linux can access these buffers as normal, but ISI can't access other memory out of these buffers, it is limited by xRDC hardware. Considering the xRDC hardware can only support up to 16 memory regions, we may need to consider different workaround implementations for different camera use case scenarios.   For single camera use case, the required camera buffer number is usually less than 16. So “0001-iMX8QM-iMX8QX-ERR050145-ISI-overwrite-workaround.patch” is enough. No modification is needed for camera application in this case.   For multiple camera use case, all patches (0001~0003) are needed. If the camera application used VB2_MEMORY_MMAP memory mode, then no code modification is needed in application. The V4l2 ISI driver can handle everything (Allocate physical continued memory for each camera, and map them as one xRDC memory region for overwrite protect). If the camera application used VB2_MEMORY_USERPTR and VB2_MEMORY_DMABUF memory mode, then it needs allocate camera buffers with physical continued memory for each camera, then the driver will merge them as one xRDC memory region in SCFW.   How to prove workaround take effective? After applying the patches, the ISI will report AXI_WR_ERR due to it failed to write data out of the allocated buffers when the errata happens. To reduce the ISI interrupt, we can also change the ISI interrupt setting as followed: void mxc_isi_enable_irq(struct mxc_isi_dev *mxc_isi) {     u32 val;     val = CHNL_IER_FRM_RCVD_EN_MASK |         CHNL_IER_EXCS_OFLW_V_BUF_EN_MASK |         CHNL_IER_EXCS_OFLW_U_BUF_EN_MASK |         CHNL_IER_EXCS_OFLW_Y_BUF_EN_MASK;     writel(val, mxc_isi->regs + CHNL_IER); }   Add reference patch for L5.4.70_2.3.0 and L5.10.72_2.2.0.
查看全文
This is a summary for the software lockup issue found in the following platform: −i.MX8/8X −Linux 4.14.98_2.3.3   Issue description: •Issue happens during the boot procedure, at the systemd stage. •The symptom of the issue: −From user perspective, the symptom varies, but mainly fall into several types: §At the console, there may be login prompt, but no response (only echo) when input user/password. Unable to login. §Some user service in systemd failed to start. E.g. weston. −When checking the task status using sysrq (w/t), many tasks, including some kernel core tasks stays in “D” (uninterruptable sleep) state. E.g. agetty, login, chvt, etc. •Kernel itself is still alive. This can be verified by triggering some drivers, such as plugin a USB device. Issue can be reproduced on MEK through long time stress.   Please refer to the doc/patch attached for details.
查看全文
PCIE IP on i.MX8MM and i.MX8MP is same, customer can follow PCIE test Application note to do compliance test, if eye diagram failed, they can fine turn corresponding regs below: iMX8MMRM.pdf IMX8MPRM.pdf GEN1:             GEN2:                 Related code in kernel Phy-fsl-imx8-pcie.c (kernel-source\drivers\phy\freescale)    3794      2020/11/4 static int imx8_pcie_phy_init(struct phy *phy) { ……          /* Configure TX drive level  */        writel(0x2d, imx8_phy->base + 0x404);          return 0; }   Thanks Lambert
查看全文
i.MX8 series contains internal HiFi4 DSP. It is targeted for Audio related signal processing. SOF (Sound Open Firmware) is open source audio DSP firmware, driver and SDK. This document introduces basic theory about IIR/FIR digital filters, how to design IIR/FIR digital filters and the Equalizer filters implementation by SOF. After that, the document also describes how HiFi4 DSP MAC engine accelerate the EQ filters calculation.
查看全文
1. Description: On the i.MX Android camera HAL, It only supports YUYV sensor, regardless of whether the sensor is connected to ISP or ISI. Some users want to customize the sensor format, such as UYVY or raw, they need a guide to do this, this document intends to describe how to implement raw camera sensor on i.MX8MP android, and output raw data. Note: Base on  i.MX 8M plus, Android12_1.0.0.  2. Camera HAL Android's camera hardware abstraction layer (HAL) connects the higher level camera framework APIs in android.hardware.camera2 to your underlying camera driver and hardware. For more detail information, please refer to AOSP document: https://source.android.google.cn/docs/core/camera/camera3_requests_hal?hl=en while on I.MX camera HAL, the camera subsystem can be divided into several parts:   Camera framework:  frameworks\av\camera Camera service:    frameworks\av\services\camera\libcameraservice\ Camera provider: hardware/interfaces/camera/provider/ hardware/google/camera/common/hal/hidl_service/               hidl_service dlopen the camera HAL3. Camera HAL3:   vendor\nxp-opensource\imx\camera\ Camera driver:   vendor/nxp-opensource/kernel_imx/drivers/media/i2c  It's callstack can be list as follow:  There are 2 streams on pipeline, preview stream need 3 buffers and capture stream need 2 buffers: CameraDeviceSessionHwlImpl: ConfigurePipeline, stream 0: id 0, type 0, res 2592x1944, format 0x21, usage 0x3, space 0x8c20000, rot 0, is_phy 0, phy_id 0, size 8388608 CameraDeviceSessionHwlImpl: ConfigurePipeline create capture stream CameraDeviceSessionHwlImpl: ConfigurePipeline, stream 1: id 1, type 0, res 1024x768, format 0x22, usage 0x100, space 0x0, rot 0, is_phy 0, phy_id 0, size 0 CameraDeviceSessionHwlImpl: ConfigurePipeline create preview stream You can use this command to dump the stream input/output: "setprop vendor.rw.camera.test 1" to dump steam 0. "setprop vendor.rw.camera.test 2" to dump steam 1. Before you implement the command, you need to run “su; setenforce 0” to close the SeLinux, the data is dumped as "/data/x-src.data", "/data/x-dst.data", where "x" is the stream id as "0, "1,", "2", ...   Preview Stream Capture Stream ID 1 0 Resolution 1024*768 2592*1944 Format HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED (34) HAL_PIXEL_FORMAT_BLOB (33) Usage 0x900 GRALLOC_USAGE_HW_TEXTURE      (0x100) GRALLOC_USAGE_HW_COMPOSER  (0x800) 0x3 GRALLOC_USAGE_SW_READ_OFTEN Data space 0 HAL_DATASPACE_V0_JFIF  The following usage will be added by framework to distinguish preview and video:GRALLOC_USAGE_HW_VIDEO_ENCODER 3. Raw support  3.1 system modification  The default image for i.MX 8M Plus EVK supports basler + basler and the cameras can work after the image is flashed and boot up, it’s camera with ISP, but we need ISI to process raw. You should refer to Android_User’s_Guide.pdf, you need find the correct version, as Android12_2.0.0 is different with Android12_1.0.0. To make cameras work with Non-default images, execute the following additional commands: Only OV5640 (CSI1) on host: As we use OV2775 which support 1920*1080, unpacked raw12, the json file: 3.2 DTB modification  1. Firstly, change the BoardConfig.mk to generate dtbo-imx8mp-ov2775.img device\nxp\imx8m\evk_8mp\BoardConfig.mk: TARGET_BOARD_DTS_CONFIG += imx8mp-ov2775:imx8mp-evk-ov2775.dtb 2.  Secondly, add imx8mp-evk-ov2775.dts to vendor\nxp-opensource\kernel_imx\arch\arm64\boot\dts\freescale 3. Change imx8mp-evk-ov2775.dts, connect OV2775 to ISI: &isi_0 { status = "okay"; }; &isp_0 { status = "disabled"; }; &dewarp { status = "disabled"; }; 4. Build dtbo image and flash it to board: ./imx-make.sh dtboimage -j4 fastboot flash dtbo dtbo.img  3.3 Sensor driver modification  I use the OV2775 driver from the isp side, be careful that all the function such as g_frame_interval and enum_frame_size should be implemented, or the HAL will get wrong parameters and return error. static struct v4l2_subdev_video_ops ov2775_subdev_video_ops = { .g_frame_interval = ov2775_g_frame_interval, .s_frame_interval = ov2775_s_frame_interval, .s_stream = ov2775_s_stream, }; static const struct v4l2_subdev_pad_ops ov2775_subdev_pad_ops = { .enum_mbus_code = ov2775_enum_mbus_code, .set_fmt = ov2775_set_fmt, .get_fmt = ov2775_get_fmt, .enum_frame_size = ov2775_enum_frame_size, .enum_frame_interval = ov2775_enum_frame_interval, };  3.4 ISI driver modification  We need to add raw format on ISI driver: }, { .name = "RAW12 (SBGGR12)", .fourcc = V4L2_PIX_FMT_SBGGR12, .depth = { 16 }, .color = MXC_ISI_OUT_FMT_RAW12, .memplanes = 1, .colplanes = 1, .mbus_code = MEDIA_BUS_FMT_SBGGR12_1X12, }, { .name = "RAW10 (SGRBG10)", .fourcc = V4L2_PIX_FMT_SGRBG10, .depth = { 16 }, .color = MXC_ISI_OUT_FMT_RAW10, .memplanes = 1, .colplanes = 1, .mbus_code = MEDIA_BUS_FMT_SGRBG10_1X10, } 3.5 Camera HAL modification As there are preview stream and capture stream on the pipeline. GPU does not support raw format, it will print error log when application set raw format:    02-10 18:49:02.162 436 436 E NxpAllocatorHal: convertToMemDescriptor Unsupported fomat PixelFormat::RAW10 02-10 18:49:02.163 2390 2445 E GraphicBufferAllocator: Failed to allocate (1920 x 1080) layerCount 1 format 37 usage 20303: 7 02-10 18:49:02.163 2390 2445 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) dequeueBuffer: createGraphicBuffer failed 02-10 18:49:02.163 2390 2405 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) requestBuffer: slot 0 is not owned by the producer (state = FREE) 02-10 18:49:02.163 2148 2423 E Surface : dequeueBuffer: IGraphicBufferProducer::requestBuffer failed: -22 02-10 18:49:02.163 2390 2445 E BufferQueueProducer: [ImageReader-1920x1080f25m2-2390-0](id:95600000002,api:4,p:2148,c:2390) cancelBuffer: slot 0 is not owned by the producer (state = FREE) 02-10 18:49:02.164 2148 2423 E Camera3-OutputStream: getBufferLockedCommon: Stream 1: Can't dequeue next output buffer: Invalid argument (-22)   Modifying the gpu code is not recommended. When preview stream, it's pixel format is fixed to HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED, it needs YUYV format, in this patch, we don't convert raw12 to yuyv, just copy the buffer from input to output, so the preview stream is raw12 actually. When capture stream, we use the Blob format, which usually used for JPEG format. when we find the format is Blob pass down by application, camera HAL will copy the buffer from input to output directly. You can check the detail on function ProcessCapturedBuffer(),    4. Application and Tool 4.1 Application  The test application on the attachment “android-Camera2Basic-master_application.7z”, It's basically a common camera application, it set the capture stream format to blob:  Size largest = Collections.max( Arrays.asList(map.getOutputSizes(ImageFormat.JPEG)), new CompareSizesByArea()); mImageReader = ImageReader.newInstance(largest.getWidth(), largest.getHeight(), ImageFormat.JPEG, /*maxImages*/2); 4.2 Tool We use 7yuv tool to check the raw12 format, which is captured by applicable or dump by HAL, you need set the parameter on the right side:   ImageJ tool also can be used to review raw format.
查看全文
BSP: L5.15.5_1.0.0   Platform: i.MX8MPlus EVK   1. Parameter preparation For more parameter calculation, please refer to: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M- Mini-Register-Programming-Aid-DRAM-PLL-setting/ta-p/111209  For 1866MHz LPDDR4, we need a DRAM PLL size of 933MHz. The PLL dividing parameters are: m=622,p=16,s=0, k=0.   2. Calibration and stress test with DDR Tool 2.1 Creating a test script for 1866MHz Here we copy the script from another file (e.g. 2000MHz) and modify the contents of the script.   2.2 Modify the script to adapt to 1866MHz 2.3 Download the test script After selecting the ddr script we created, click on the download button   2.4 Calibrating the stress test Set the core clock of the chip's cpu to 1.2GHz, then click the Calibration button to calibrate, then click Gen Code to generate the lpddr4_timing.c file. Set the start frequency to 1866MHz for the stress test.   2.5 Modify lpddr4_timing.c We need to modify the generated lpddr4_timing.c file to change the maximum speed to 3732MTS.   3. SPL patch After getting the correct lpddr4_timing.c file, the SPL code also needs to be modified to add support for the 933MHz DRAM PLL. diff --git a/arch/arm/mach-imx/imx8m/clock_imx8mm.c b/arch/arm/mach-imx/imx8m/clock_imx8mm.c index e39f238fdf...5622a6334e 100644 --- a/arch/arm/mach-imx/imx8m/clock_imx8mm.c +++ b/arch/arm/mach-imx/imx8m/clock_imx8mm.c @@ -55,6 +55,7 @@ static struct imx_int_pll_rate_table imx8mm_fracpll_tbl[] = { PLL_1443X_RATE(650000000U, 325, 3, 2, 0), PLL_1443X_RATE(600000000U, 300, 3, 2, 0), PLL_1443X_RATE(594000000U, 99, 1, 2, 0), + PLL_1443X_RATE(933000000U, 622, 16, 0, 0), PLL_1443X_RATE(400000000U, 400, 3, 3, 0), PLL_1443X_RATE(2660000U, 266, 3, 3, 0), PLL_1443X_RATE(167000000U, 334, 3, 4, 0), diff --git a/drivers/ddr/imx/imx8m/ddrphy_utils.c b/drivers/ddr/imx/imx8m/ddrphy_utils.c index 326b92d784..ebd005bc2b 100644 --- a/drivers/ddr/imx/imx8m/ddrphy_utils.c +++ b/drivers/ddr/imx/imx8m/ddrphy_utils.c @@ -117,6 +117,10 @@ void ddrphy_init_set_dfi_clk(unsigned int drate) dram_pll_init(MHZ(1000)); dram_disable_bypass(); break; + case 3732: + dram_pll_init(MHZ(933)); + dram_disable_bypass(); + break; case 3200: dram_pll_init(MHZ(800)); dram_disable_bypass();   4. Test results   Reference blog. DDR Tool: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467  RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352 
查看全文
Hello, here Jorge. On this post I will explain how to configure, record and play audio using an i.MX 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK Linux Binary Demo Files - i.MX 8MMini EVK (L5.15.52_2.1.0) i.MX 8MIC-RPI-MX8 Board Serial console emulator (Tera Term, Putty, etc.) Headphones/speakers The 8MIC-RPI-MX8 accessory board is designed for voice enabled application prototyping and development on the i.MX 8M family. The board plugs directly into the 40-pin expansion connector on the i.MX 8M Mini and Nano EVK’s. Some features about this board are: 8 PDM Microphones 8 monochrome LEDs 4 multi-color LEDs 2 status LEDs 4 pushbuttons Microphone Mute Switch Microphone geometry switch Connecting the i.MX 8MIC-RPI-MX8 Board. The i.MX 8MIC-RPI-MX8 Board has a 40-pin expansion connector that you can plug it directly to the EVK board. Ensure that pin 1 of the 8MIC-RPI-MX8 is aligned with pin 1 on the EVK J1001 as is showed on the next figure:  Selecting the device tree on the board. Once the pre-compiled image is flashed on the board (Flashing Linux BSP using UUU) and you connected the 8MIC-RPI-MX8 it is necessary to select the correct device tree to handle 8MIC board. On U-boot check the available .dtb files on the BSP using the next command: u-boot=> fatls mmc 2:1 And you will get the corresponding list of .dbt files:  On this case we are working with an I.MX 8M Mini EVK and the corresponding .dtb file is: imx8mm-evk-8mic-revE.dtb To select it you need to set the environment variable and save it with: u-boot=> setenv fdtfile imx8mm-evk-8mic-revE.dtb u-boot=> saveenv Doble check it using: u-boot=> printenv fdtfile   Now it is time to boot Linux using the next command: u-boot=> boot Recording audio with the i.MX 8MIC-RPI-MX8 Board. The Advanced Linux Sound Architecture (ALSA) provides audio and MIDI functionality to the Linux operating system. ALSA has the following significant features: Efficient support for all types of audio interfaces, from consumer sound cards to professional multichannel audio interfaces. Fully modularized sound drivers. SMP and thread-safe design. User space library (alsa-lib) to simplify application programming and provide higher level functionality. Support for the older Open Sound System (OSS) API, providing binary compatibility for most OSS programs. Once we are on Linux, we can check our audio codecs detected on the board using: arecord -l   Now, to record audio we need to use the ALSA arecord command to start recording with IMX8 boards, there are different options that you can check on the next link. On this case we are going to use the next: arecord -D hw:imxaudiomicfil -c8 -f s16_le -r48000 -d10 sample.wav -D: selects the device. -c: selects the number of channels on the recording. -f: selects the format. -r: selects the sample rate. -d: determinate the duration recording time in seconds. sample.wav: Is the name of the resulting audio file. Running the last command, we started to record audio. It is time to make some noise and record it!   Playing audio from IMX8 boards. Now it is time to connect our headphones or speakers to the jack.   Also, as on arecord command you can check the devices where you can play audio from the board using the next command: aplay -l And you will get all the codecs to play audio:   To play our recordings we need to use the ALSA aplay command, it is important to select the correct audio codec to hear the audio from the jack on the board: aplay -Dplughw:3,0 sample.wav -D: selects the device. sample.wav: Is the name of audio file to play   Hope this will helpful for people who wants to record audio using PDM microphones and playing audio from IMX8 boards. Best regards.
查看全文
Symptoms   Bridge mode on EQoS module will not work since Linux Kernel 5.10_2.2.0. Platforms impacted: i.MX8MP/i.MX8DXL/i.MX93   Diagnosis   When eqos module(eth1) is added to the bridge using brctl, it will first set eth1 to promiscuous mode and then set the VLAN for this bridge with a filter VID value of 1. Before adding Intel's patch, there is no problem. c89f44ff10fd net: stmmac: Add support for VLAN promiscuous mode However, when Intel's patch sets up the filter, if it finds that the promiscuous mode is turned on, it will turn off the VLAN Tag function. And it adds a judgment on whether promiscuous mode has been turned on in the function of configuring VID. Returns an error if promiscuous mode is found. Because the patch has turned off the VLAN tag function when promiscuous mode is enabled, which conflicts with continuing to configure the VID. Workaround   This patch is okay for aarch64 platform to solve this issue. diff --git a/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c b/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c index c25bfecb4a2d..2dc548b54b1c 100644 --- a/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c +++ b/drivers/net/ethernet/stmicro/stmmac/dwmac4_core.c @@ -481,12 +481,6 @@ static int dwmac4_add_hw_vlan_rx_fltr(struct net_device *dev, if (vid > 4095) return -EINVAL; - if (hw->promisc) { - netdev_err(dev, - "Adding VLAN in promisc mode not supported\n"); - return -EPERM; - } - /* Single Rx VLAN Filter */ if (hw->num_vlan == 1) { /* For single VLAN filter, VID 0 means VLAN promiscuous */ @@ -536,12 +530,6 @@ static int dwmac4_del_hw_vlan_rx_fltr(struct net_device *dev, { int i, ret = 0; - if (hw->promisc) { - netdev_err(dev, - "Deleting VLAN in promisc mode not supported\n"); - return -EPERM; - } - /* Single Rx VLAN Filter */ if (hw->num_vlan == 1) { if ((hw->vlan_filter[0] & GMAC_VLAN_TAG_VID) == vid) {  
查看全文
This article describes how to integrate NXP WiFi & BT module into i.MX platform, some debug tips, how to test, etc. Although it takes i.MX8MM as example, it is also suitable for all i.MX8 serials platform.
查看全文
   
查看全文
This hands on is based on the evkmimxrt1170_pxp_lab_cm7.zip which is from https://community.nxp.com/t5/i-MX-RT1170-CAS-Training/PXP-Multiple-Files/ta-p/1178709 this hands on give an example to understand pxp basic concept like letterbox background color, rotation, ps buffer coordination definition, output buffer coordination definition more clear   No Roation This test is based on no rotation, so define as below #define LAB1_BIT_BLIT_NO_ROTATION This demo output is that the rabbit picture shows on the upper left corner of lcd, and the offset width and height is 100   #ifdef LAB1_BIT_BLIT_NO_ROTATION     PXP_ps_bitblit(                    // input                    (void*)bmp_rabbit,                    PIXEL_BYTES,                    BMP_RABBIT_WIDTH,                    BMP_RABBIT_HEIGHT,                      // output                    s_BufferLcd[curLcdBufferIdx],                    DEMO_PANEL_WIDTH,                    DEMO_PANEL_HEIGHT,                    100,  // output offset x                    100,  // output offset y                    kPXP_No_Rotate); #endif       in this lab sample code, the background is set to black, PXP_SetProcessSurfaceBackGroundColor(APP_PXP, 0U);   The output is     If we want to set the background to lighter blue, this is what I want to get     then I modify the code to PXP_SetProcessSurfaceBackGroundColor(APP_PXP, 0xFFF0U);   But we get the same output like, without any difference         Check the code, find that the original code   void PXP_ps_sub_region_bitblit(…) { …..     outputBufferConfig.width = sub_region_width;     outputBufferConfig.height = sub_region_height;   …… }   This means that the output buffer width and height are the same as the picture width and height, so whatever background color you set, you couldn’t find anything difference, then change the output buffer width and height is the same as lcd width and height     void PXP_ps_sub_region_bitblit(…) { …..       outputBufferConfig.width = output_width;       outputBufferConfig.height= output_height;   …… }   Then the output change to     We can find the color on the top of display is still black and this isn’t what I need, still tracing the code   void PXP_ps_sub_region_bitblit(…) { …..  // Output buffer  outputBufferConfig.buffer0Addr   =  (uint32_t)output_buffer + output_offset_y * output_width * pic_bytes_per_pixel + output_offset_x * pic_bytes_per_pixel …… }   output_buffer is defined as lcd buffer start address, here the output buffer start address isn’t defined as lcd buffer start address(output_buffer), this is offset of lcd buffer start address, so change it like   void PXP_ps_sub_region_bitblit(…) { …..  // Output buffer  outputBufferConfig.buffer0Addr = (uint32_t)output_buffer …… }   Then the output is like       The output picture move to the upper left corner without offset, but this demo defines the offset is 100   void PXP_ps_sub_region_bitblit(…) { …..  // PS buffer PXP_SetProcessSurfacePosition(APP_PXP,0,0,BMP_RABBIT_WIDTH - 1U, BMP_RABBIT_HEIGHT - 1U); ….. }   In the original code, the PS buffer offset is 0, because the ps buffer start address is the same as the output buffer start address, and output buffer start address is offset + lcd output buffer start address, so set the PS output offset is 0, but I change the output buffer start address is the same as lcd buffer start address, so change the code   void PXP_ps_sub_region_bitblit(…) { …..             uint32_t psUlcX         = output_offset_x;             uint32_t psUlcY         = output_offset_y;             uint32_t psLrcX, psLrcY;             psLrcX = psUlcX   +  sub_region_width  - 1U;             psLrcY = psUlcY + sub_region_height- 1U;         // PS buffer         PXP_SetProcessSurfacePosition(APP_PXP,psUlcX,psUlcY,psLrcX,psLrcY); ….. }   The output is   \   Now this is what we need     Roation Set Macro to #define LAB2_BIT_90_DEGREE_ROTATION   The output is     When rotation is 90 degree and width is wider than the output height, the display part will be cut, so change the code from Before void PXP_ps_sub_region_bitblit(…) { …..       outputBufferConfig.width = output_width;       outputBufferConfig.height= output_height; ….. }   To   void PXP_ps_sub_region_bitblit(…) { …..  if  (rotate == kPXP_Rotate90)  {     outputBufferConfig.width          = output_height;        /*Joan*/     outputBufferConfig.height         = output_width;         /*Joan*/  } else {         outputBufferConfig.width          = output_width;         /*Joan*/         outputBufferConfig.height         = output_height;        /*Joan*/ }….. }   Because this demo only shows no rotation and 90 degree rotation, if customer needs 270 degree, 180 degree, can add by themselves
查看全文
This doc will show: i.MX8DXL EVK board without connect  hardware LCD display, using FreeRDP to share screen to remote PC which is in same network,  PC take this shared screen could  run any command on i.MX8DXL EVK board.   HW: i.MX8DXL EVK board,  PC  SW: i.MX8DXL Linux 5.15.32 BSP release, and code change in this doc   1> i.MX8DXL Linux kernel side, just use imx8dxl-evk-lcdif.dts, but did not connect any LCD display,  so Linux kernel could create related drm device, and weston could be start. But on 8DXL EVK board, ENET1_RGMII_TXD3 and ADMA_LCDIF_D03 pin conflict,  so need code change as 5.15.32-imx8dxl-evk-lcdif.dts.diff.   2> yocto/bld/conf/local.conf, add below line, as freerdp depend on ffmpeg. LICENSE_FLAGS_ACCEPTED+="commercial"   3> For i.MX8DXL,  weston use software pixman render, to use NEON optimization,  pixman need switch to  latest 0.42.0,  enter folder (yocto/bld/tmp/work/armv8a-poky-linux/pixman/1_0.40.0-r0/pixman-0.40.0),  git clone (https://github.com/freedesktop/pixman.git) and checkout to latest 0.42.0:  Also chaneg related build flag at bb file as pixman_0.40.0.bb.diff.     4> Default  freerdp need switch to 2.8.0, enter folder (yocto/bld/tmp/work/armv8a-poky-linux/freerdp/1_2.4.1-r0/git),  git clone (https://github.com/FreeRDP/FreeRDP.git), check out to 2.8.0; And to use neon accelerate freerdp related function, such as color space conversion, image codec encoding ,  need apply patch  freerdp-codechange-neon.diff. And related bb file compile flag change as freerdp_2.4.1.bb.diff     5> bitbake -c compile ffmpeg bitbake -c install ffmpeg   bitbake -c compile pixman  bitbake -c install pixman    bitbake -c compile  freerdp bitbake -c install  freerdp   Copy  generated new libs to default released i.MX8DXL rootfs, make sure ffmeg , pixman, freerdp related libs are  from your build, for example: libfreerdp-client2.so.2 -> libfreerdp-client2.so.2.8.0 libfreerdp2.so.2 -> libfreerdp2.so.2.8.0 libwinpr-tools2.so.2 -> libwinpr-tools2.so.2.8.0 libwinpr2.so.2 -> libwinpr2.so.2.8.0   6> i.MX8DXL Linux rootfs:  file /etc/xdg/weston/weston.ini,  change start-on-startup to true: [screen-share] command=/usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --no-clients-resize --rdp-tls-cert=/etc/freerdp/keys/serve start-on-startup=true   7> i.MX8DXL Linux OS, run below cmd: winpr-makecert -path $PWD copy generated files to /etc/freerdp/keys/server.crt and /etc/freerdp/keys/server.key   8> reboot i.MX8DXL EVK board,  make sure  EVK board and PC in the same network; check i.MX8DXL Linux OS , there are two process name as "weston", one process is weston rdp backend to share screen to PC.   9> PC side, get wfreerdp.exe from  https://github.com/FreeRDP/FreeRDP/wiki/Prebuilds PC side run cmd as: wfreerdp.exe /v:ipaddress_of_8DXLEVK     Reference: 1>https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX#design-resources 2>https://github.com/FreeRDP 3>https://github.com/freedesktop/pixman 4>https://github.com/DLTcollab/sse2neon  
查看全文