i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Introduction ARM SoC+FPGA/CPLD is widely used in some application like industry control and data acquisition system, there were many customers adopted i.MX6 EIM (a memory parallel interface) to access FPGA/CPLD, and archived good data throughput, but EIM is removed from i.MX8M and i.MX9, some customers is asking for such a compatible solution for i.MX8/8M and coming i.MX9 family.  FlexSPI is designed for connecting storage devices like NOR Flash, integrated in most of i.MXRT/i.MX8/LS products and provides flexible configuration for 4-wire/8wire working mode, this article provides a low-cost and efficiency demo to show how  to support CPLD/FPGA  via FlexSPI, as a replacement of EIM for EP i.MX8/9/LS products. key features Implement a  new kernel driver for FlexSPI to support read/write access to FPGA/CPLD. Support two type connections: Support 4-wire(QSPI) and 8-wire(HypeBUS, OctalSPI) Deliverables A new kernel driver for FlexSPI to support read/write access to FPGA/CPLD by AHB command A kernel patch to disable the QSPI Flash in kernel A test program shows how to do read/write performance test. Hardware Hardware Prepare: i.MX8MM-LPDDR4-EVK Lattice LFE5U EVK Figure1 4-wire SPI HW Block diagram Figure2 8-wire OctalSPI   Hardware Rework on i.MX8MM-EVK     1 Need to remove the SPI-Flash(U5, MT25QU256ABA) on the i.MX8MM-EVK board, and wire below signals: QSPI_DATA0 QSPI_DATA1 QSPI_DATA2 QSPI_DATA3 QSPI_SCLK QSPI_nSS0 VDD_1V8 GND Figure3 QPSI signals for FPGA/CPLD Figure4 Hardware rework on i.MX8MM-EVK board Note that, i.MX8MM-EVK QSPI power rails is 1.8v, so be careful that the FPGA/CPLD side IO should be 1.8V. Software BSP version 1 Linux BSP version: L5.10.52 Software Change  Apply 0001-FlexSPI-FPGA-need-to-disable-flexspi-for-fpga-usage.patch in Linux kernel and generate the new dtb extract the flexspi-fpga driver compile the flexspi-fpga driver with the kernel$ $make -C $(YOUR_KDIR) M=$(FlexSPI_FPGAW_DIVER_DIR) modules ARCH=arm64 CROSS_COMPILE=$(CROSS_COMPILE) Deployment  upload new generated i.mx8mm-evk.dtb to the target board(the 1st partition) upload the flex-spi driver and fpga/cpld test program to the target board   Test Test1: Set the flexspi working at 40Mhz   $insmod imx_flexspi_fpga.ko pre_div=2 post_div=5 Read/write FPGA/CPLD test .$/flexspi_fpga_test -p 0x08000000 -s 768 Test2: Set the FlexSPI working at 100MHz   $ insmod imx_flexspi_fpga.ko pre_div=1 post_div=4 Read/write FPGA/CPLD test $./flexspi_fpga_test -p 0x08000000 -s 768   Limitation FPGA and Flash devices can’t work at the same time due to just one FlexSPI controller. Due to the IO assignment conflict in i.MX8M EVK design, this demo just tested 4-wire(QSPI) mode at 50MHz and got data throughput as expected. Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
查看全文
Environment BSP: L6.1.22_2.0.0​ Platform: i.MX93 Links:  https://github.com/NXP/swupdate-scripts https://github.com/nxp-imx-support/meta-swupdate-imx   The AN13872 provides us the swupdate yocto layer, swupdate-scripts and test steps, but there is still much to add. The purpose of this knowledge base is to provide customized advice. 1.How to port meta-swupdate-imx to any yocto version you want? As meta-swupdate-imx only provide kirkstone version, we can upgrade or degrade it based on this version. We will take L6.1.22_2.0.0​ porting steps as an example. 1.1 Download Yocto layer  cd imx-yocto-bsp/sources git clone https://github.com/sbabic/meta-swupdate.git -b mickledore git clone https://github.com/nxp-imx-support/meta-swupdate-imx.git 1.2 Modify  Yocto layer  imx-yocto-bsp/sources/meta-swupdate-imx/conf/layer.conf   You can find swupdate version in imx-yocto-bsp/sources/meta-swupdate/recipes-support/swupdate/ 1.3 Handle patches in meta-swupdate-imx/recipes-bsp/u-boot/files/ About patchs in sources/meta-swupdate-imx/recipes-bsp/u-boot/files/ and imx-yocto-bsp/sources/meta-swupdate-imx/recipes-support/swupdate/files/, you need use devtool to unpack uboot and swupdate into workspace and add changes manunally for development. CONFIG_ENV_OFFSET_REDUND=CONFIG_ENV_OFFSET+CONFIG_ENV_SIZE   sources/meta-swupdate-imx/recipes-bsp/u-boot/u-boot-imx_%.bbappend 2.How to flash base image? Use uuu or dd command, just like common imx-image-xxx 3.swupdate-scripts porting suggestions 3.1 Partition table You can modify partition table refer the size of images. For different soc, the first offset is different. If you are porting i.MX8MP based on iMX8MM, the offset should be 32K.   3.2 Some errors 3.2.1 This error indicates that you need enlarge size of rootfs. e2fsck 1.45.5 (07-Jan-2020) The filesystem size (according to the superblock) is 887599 blocks The physical size of the device is 768000 blocks Either the superblock or the partition table is likely to be corrupt! Abort<y>?    3.2.2 You need upgrade e2fsck verison. e2fsck 1.46.5 (30-Dec-2021) /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4 has unsupported feature(s): FEATURE_C12 e2fsck: Get a newer version of e2fsck! /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4: ********** WARNING: Filesystem still has errors ********** resize2fs 1.46.5 (30-Dec-2021) resize2fs: Filesystem has unsupported feature(s) (/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_ass  solution: wget https://mirrors.edge.kernel.org/pub/linux/kernel/people/tytso/e2fsprogs/v1.47.0/e2fsprogs-1.47.0.tar.xz tar -xf e2fsprogs-1.47.0.tar.xz cd e2fsprogs-1.47.0/ ./configure make -j16 sudo make install   3.2.3 mtools /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 58: mdir: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 68: mdir: command not found solution: sudo apt-get install mtools
查看全文
We are pleased to announce that Config Tools for i.MX v14.0 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) The product is based on Eclipse 2022-12 Open JDK 17 is updated. Batch processing on command line is supported. Support for SDK 2.14 in Project cloner and Detect toolchain project is added. Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error. Search functionality to Code Preview is added. TEE Export TEE registers via wizard or command line is available. Boot ROM hiding feature is supported. Tier mode for TRDC is supported. Domain ambivalence for RDC masters is added. Master-specific memory alias Validation for A28 bit of MPU region address is added. Memory map filters are aligned with Arm terminology. Status bar is united with other tools. Pins Labels defined for Expansion header pins can be set as identifiers of the routed pin. Expansion headers can be locked for editing. Expansion headers and boards are added to the HTML and CSV reports. Pins filtering is added into the expansion header pin routing dialogs. Columns from Routing Details can be added to the External User Signals view. New External User Signals can be created for all routed pins that are missing in the signals table. Clocks Support for the same frequencies settings from different source for internal clocks is added.
查看全文
Issue description: ZQ calibration issue with LPDDR2 memory with two chip selects    Micron has verified it on my customer's board with i.MX6Q. (ECT-SYT-1163 for FIC.pdf) The patch is made based on lp 5.1, see attachment.
查看全文
On customer design, they may need to fine tune LVDS driver strength for different case, for example, PCB impedance does not match, or the value of terminal resistor in panel side is lower or bigger. In IMX8MPRM.pdf, it has reg for this feature:         LVDS is constant current source, when voltage on terminal or panel side is lower than spec, you need to increase output current to get higher voltage to meet spec. otherwise ,you need to reduce it There is no detail description for these bits, pls refer to below: CC_ADJ = 000b => 3.5mA as default CC_ADJ = 001b => 3.5mA + 0.215mA x 1 CC_ADJ = 010b => 3.5mA + 0.215mA x 2 CC_ADJ = 011b => 3.5mA + 0.215mA x 4 CC_ADJ = 100b => 3.5mA - 0.215mA x 4 CC_ADJ = 101b => 3.5mA - 0.215mA x 3 CC_ADJ = 110b => 3.5mA - 0.215mA x 2 CC_ADJ = 111b => 3.5mA - 0.215mA x 1   Thanks, Lambert
查看全文
  Solution           
查看全文
Hello everyone, this document will share an step by step guide of the configuration needed in a Linux PC to compile the SDK examples we provide, as well as how to download them in an easy way. Requirements: I.MX 8M Mini EVK SDK package (for i.MX8MM) UUU tool First step would be to get the SDK package, this include documentation and code, which is available at the MCUXpresso builder webpage: https://mcuxpresso.nxp.com/en/welcome Click on the select a development board and select the package for your development kit or the i.MX MPU   This guide is focused on Linux build so will select GCC package and Linux host PC as the environment. Click on build and wait for the SDK package to be ready for download. Note1: Click on select all if the whole middleware package is desired Note2: it is possible to select each middleware that are desired. On new window select download SDK Select on new pop-up window download both SDK and documentation Read and accept EULA so the download start Decompress the package using the following command: $ tar -xvzf ~/SDK_2_13_0_EVK-MIMX8MM.tar.gz -C ~/SDK_2_13_0_EVK-MIMX8MM Next will be to download the GCC from the ARM webpage, gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 https://developer.arm.com/downloads/-/gnu-rm Note that the GCC version used is based on the minimum version required, since this was tested and supported, this could be found within the SDK documentation (~/SDK_2_13_0_EVK-MIMX8MM/docs/MCUXpresso SDK Release Notes for EVK-MIMX8MM) Once downloaded we can decompress and configure the environment: $ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ sudo apt-get install cmake  Check the version >= 3.0.x $ cmake --version Once this is done we enter the path of the example of our choice and compile using the script, as necessary using debug, release or all. $ cd ~/SDK_2_13_0_EVK-MIMX8MM/boards/evkmimx8mm/demo_apps/hello_world/armgcc $./build_release.sh The binary (elf and bin) will be found inside the folder according to whether we use debug or release script. For this example we used release script: $ cd release Once builded we can move/download the binaries from the Linux host PC to the board by using the UUU tool with the command fat_write #### we put the board in fastboot mode by entering the command in the uboot terminal fastboot 0 #### From the Linux terminal introduce the UUU command to  download to the FAT partition of the eMMC of the baord: ## For rproc it is needed the .elf binary ## $ uuu -v -b fat_write hello_world.elf mmc 0:1 hello_world.elf ## For bootaux it is needed the .bin binary ## $  uuu -v -b fat_write hello_world.bin mmc 0:1 hello_world.bin Once with the binaries in the FAT partition of the SD/eMMC of our board we can make the necessary modifications (device tree/bootargs) to test the Cortex-M examples. For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
查看全文
  Platform: i.MX8MP EVK , L6.1.22-2.0.0 LT9211 is a chip that can realize the conversion of MIPI DSI signals to LVDS signals. This patch is based on this mainline driver:https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/gpu/drm/bridge/lontium-lt9211.c Keypoint Move lt9211_host_attach function to lt9211_attach to skip bridge attach error.  
查看全文
1.Compile full aosp or only kernel Build full aosp: source build/envsetup.sh lunch evk_8mm-userdebug ./imx-make.sh -j8  Only build kernel: ./imx-make.sh kernel -j8 2.Build GKI locally Download GKI outside of android_build. mkdir gki && cd gki (Make sure folder gki is not inside of ${MY_ANDROID}) repo init -u https://android.googlesource.com/kernel/manifest -b commonandroid13-5.15 repo sync Build GKI locally. BUILD_CONFIG=common/build.config.gki.aarch64 build/build.sh 3. Export symbols After building GKI locally, you can copy linux-imx from /vendor/nxp-opensource/kernel_imx into common. cd common rm -r ./* cp ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/* ./ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex  Build GKI about i.MX: BUILD_FOR_GKI=yes BUILD_CONFIG=common/build.config.imx EXT_MODULES_MAKEFILE="verisilicon_sw_isp_vvcam/vvcam/v4l2/Kbuild" EXT_MODULES="nxp-mwifiex/mxm_wifiex/wlan_src" build/build_abi.sh --update-symbol-list -j8 Then the  common/android/abi_gki_aarch64_imx will be generated. cd gki cp common/android/abi_gki_aarch64_imx /tmp/abi_gki_aarch64_imx   Update GKI kernel rm -r common/* # delete imx kernel repo sync # recover aosp kernel cp /tmp/abi_gki_aarch64_imx android/abi_gki_aarch64_imx cd .. BUILD_CONFIG=common/build.config.gki.aarch64 build/build_abi.sh LTO=thin --update -j8  Then, common/android/abi_gki_aarch64.xml is updated.  
查看全文
  Introduction   Platform: i.MX93 EVK Uboot: origin/lf_v2022.04(lf-6.1.1-1.0.0) The LVDS design and media block control in i.MX93 is very similiar with i.MX8MPlus.This article implements the LVDS driver in uboot. You need apply 0001-Add-fake-adp5585-pwm-driver.patch which implements the adp5585 pwm driver in uboot. This is a fake pwm driver only implement the pwm driver framework. You can't use pwm value to adjust brightness for the moment, but this is enough to enable the backlight. Then please apply 0002-Add-imx93-lvds-and-panel-driver.patch, you will see nxp logo with this panel: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/dy1212w-4856:DY1212W-4856   Porting suggestions   1. Modify panel timing in drivers/video/simple_panel.c /* define your panel timing here and * copy it in simple_panel_get_display_timing */ static const struct display_timing boe_ev121wxm_n10_1850_timing = { .pixelclock.typ = 71143000, .hactive.typ = 1280, .hfront_porch.typ = 32, .hback_porch.typ = 80, .hsync_len.typ = 48, .vactive.typ = 800, .vfront_porch.typ = 6, .vback_porch.typ = 14, .vsync_len.typ = 3, }; static int simple_panel_get_display_timing(struct udevice *dev, struct display_timing *timings) { memcpy(timings, &boe_ev121wxm_n10_1850_timing, sizeof(*timings)); return 0; }   2.Modify VIDEO_PLL The VIDEO_PLL = pixel clock * 7. For default panel, the pixel clock is 71.143MHz and VIDEO_PLL  is 498MHz. static struct imx_fracpll_rate_table imx9_fracpll_tbl[] = { FRAC_PLL_RATE(1000000000U, 1, 166, 4, 2, 3), /* 1000Mhz */ FRAC_PLL_RATE(933000000U, 1, 155, 4, 1, 2), /* 933Mhz */ FRAC_PLL_RATE(700000000U, 1, 145, 5, 5, 6), /* 700Mhz */ FRAC_PLL_RATE(498000000U, 1, 166, 8, 0, 1),/* rate, rdiv, mfi, odiv, mfn, mfd */ FRAC_PLL_RATE(484000000U, 1, 121, 6, 0, 1), FRAC_PLL_RATE(445333333U, 1, 167, 9, 0, 1), FRAC_PLL_RATE(466000000U, 1, 155, 8, 1, 3), /* 466Mhz */ FRAC_PLL_RATE(400000000U, 1, 200, 12, 0, 1), /* 400Mhz */ FRAC_PLL_RATE(300000000U, 1, 150, 12, 0, 1), }; 3. Modify lcdif node in dts <498000000>, <71142857>, <400000000>, <133333333>; <VIDEO PLL>,<PIX CLK>, <MEDIA_AXI>,<MEDIA_APB> &lcdif { status = "okay"; - assigned-clock-rates = <484000000>, <121000000>, <400000000>, <133333333>; + assigned-clock-rates = <498000000>, <71142857>, <400000000>, <133333333>; };  
查看全文
The following setup is done on i.MX 93. For i.MX 8M the same steps are valid and can be followed. Prerequisites Prepare the Yocto environment. $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.0.xml $ repo sync  Set the build environment. $ DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source imx-setup-release.sh -b build-imx93 Add the 32-bit support to the image For i.MX 8M / i.MX 93, building 32-bit applications on 64-bit OS can be supported using the multilib configuration. Multilib offers the ability to build libraries with different target optimizations or architecture formats and combine these together into one system image.  Building a 32-bit application requires the following statements in conf/local.conf. The configuration specifies a 64-bit machine as the main machine type and adds multilib:lib32, where those libraries are compiled with the armv7athf-neon tune, and then includes to the image the lib32 packages. # Define multilib target require conf/multilib.conf MULTILIBS = "multilib:lib32" DEFAULTTUNE:virtclass-multilib-lib32 = "armv7athf-neon" # Add the multilib packages to the image IMAGE_INSTALL:append = " lib32-glibc lib32-libgcc lib32-libstdc++" Multilib is not supported with the debian package management. It requires the RPM system. Check and comment out the two package management lines in conf/local.conf to go to the default RPM. PACKAGE_CLASSES = "package_deb" EXTRA_IMAGE_FEATURES += "package-management" Build the image. bitbake imx-image-core Cross-compile a 32-bit application This section shows how to use the Linux SDK to cross-compile a simple C application into a 32-bit binary. Generate the SDK, which includes the tools, toolchain, and small rootfs to compile against to put on host machine: DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk bitbake core-image-minimal -c populate_sdk Set the SDK environment with the following command before building: source /opt/fsl-imx-wayland/6.1-langdale/environment-setup-armv7at2hf-neon-pokymllib32-linux-gnueabi Implement a simple hello world application: cat hello_world_32.c #include <stdio.h> int main() { printf("Hello, World!"); return 0; } $CC hello_world_32.c -o hello_world_32 Check the file's type: $ file hello_world_32 hello_world_32: ELF 32-bit LSB shared object, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, BuildID[sha1]=0a5042a0309858e0b10b12175a155cfbfb4c6a80, for GNU/Linux 3.2.0, with debug_info, not stripped Copy the binary to the Linux rootfs. Run the application on i.MX 93 Boot the board and run the application: root@imx93-11x11-lpddr4x-evk:~# ./hello_world_32 Hello, World!  
查看全文
Installing the new release (Ubuntu 22.04) was detected some NXP boards as iMX8MNEVK, iMX8MM-EVK, iMX8MP-EVK and iMX8ULP-EVK had an issue with the WIFI module that basically it does not initialize at boot. Remember, the supported WIFI modules in Ubuntu 22.04 in the EVKs are the following:       • NXP 88W8987       • NXP 88W9098       • NXP 88W8997       • NXP IW416       • NXP 88W8801       • NXP IW612 To initialize the WIFI module of NXP EVKs in Ubuntu 22.04 you can set the following command in console:   sudo modprobe moal mod_para=nxp/wifi_mod_para.conf   That command find the correct driver for our WIFI module and then initialize it, but this only works when Ubuntu is working and if you reset the EVK you need to set the command again.   The definitive solution is create a custom startup script as a service:   Step 1: Go to etc/systemd/system   cd etc/systemd/system   Step 2: In this directory create a new file with the name of your preference but the extension must be .service. You can do it with nano or vim: sudo nano or sudo vim   The file must contain: [Unit] Description=”Wifi Start” [Service] ExecStart=sudo modprobe moal mod_para=nxp/wifi_mod_para.conf [Install] WantedBy=multi-user.target   Now save the file, in my case the name was wifi_start.service.   Step 3: Now we need to enable the script in the startup/boot sequence following the command: sudo systemctl enable wifi_start.service   Remember in wifi_start.service is the name as you saved your file.   Finally, each time you boot your board, the WIFI module will initialize automatically.   Boards tested: iMX8MN (With WIFI module NXP 88W8987) iMX8MM (With WIFI module NXP 88W8987) iMX8MP (With WIFI module NXP 88W8997) iMX8ULP (With WIFI module NXP IW416)  
查看全文
This demo for all(bootloader, device tree, Linux kernel, rootfs) in spi. It uses raw read(sf read)/raw write(sf write in uuu script) to achieve that. sf probe 0; sf read ${fdt_addr} 0x500000 0x100000; sf read ${loadaddr} 0x600000 0x1E00000; sf read ${initrd_addr} 0x2400000 0x600000; setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate} rdinit=/linuxrc; booti ${loadaddr} ${initrd_addr} ${fdt_addr} |-- 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch --- patch for this demo |-- demo_binary | |-- flash.b0.bin --- b0 bootloader | |-- flash.bin --- c0 bootloader | |-- Image-imx8qxpc0mek.bin --- Linux kernel | |-- imx8qxp-mek.dtb --- device tree | |-- uramdisk_boot.rootfs.aarch64.img --- ram disk | |-- uuu.qspi.all.b0.uuu --- uuu script for b0 | `-- uuu.qspi.all.uuu --- uuu script for c0 `-- readme.txt --- this file # The spi layout used is: # - --------- -------------------------------------------- # | | flash.bin | env | dtb | Image |rootfs| # - --------------- -------------------------------------- # ^ ^ ^ ^ ^ ^ ^ # | | | | | | | # 0 4kiB 4MiB 5MiB 6MiB 36MiB 42MiB 0x1000 0x400000 0x500000 0x600000 0x2400000 Test: HW: i.MX8QXP MEK SW: lf-5.10.72-2.2.0 + 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch Test log: SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB device 0 offset 0x500000, size 0x100000 SF: 1048576 bytes @ 0x500000 Read: OK device 0 offset 0x600000, size 0x1e00000 SF: 31457280 bytes @ 0x600000 Read: OK device 0 offset 0x2400000, size 0x600000 SF: 6291456 bytes @ 0x2400000 Read: OK [ 4.787552] imx6q-pcie 5f010000.pcie: unable to add pcie port. [ 4.797467] Freeing unused kernel memory: 2944K [ 4.807379] Run /linuxrc as init process Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting network: OK /bin/sh: can't access tty; job control turned off / #  
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519   To reduce the number of attachments, older RPAs may be found in the attached zip file. Note: Devices with 17-row addresses (R0-R16) are not supported by this SoC.  ***IMPORTANT: For SCFWv1.7.0 and later, you must use the following RPA versions or later: MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16 MX8QuadXPlus_DualXPlus_C0_B0_DDR3L_RPA_v22 MX8DualX_C0_B0_DDR3L_RPA_v20 Older versions of the RPA are not aligned to SCFWv1.7.0 and later.  If trying to use an older version of an RPA with SCFWv1.7.0, it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QXP/DualX: DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 and later (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QXP: [remove] #ifndef SCFW_DCD [remove] -/* For 1200MHz DDR, DRC 600MHz operation */ [remove] DATA 4 0xff190000 0x00000CC8 /* DRC0 bringup */ [remove] #else <keep code as is> [remove] #endif
查看全文
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519 Note: Devices with 17-row addresses (R0-R16) are not supported by this SoC.  To reduce the number of attachments, older RPAs may be found in the attached zip file.   ***IMPORTANT: For SCFWv1.7.0, you must use the following RPA versions or later: MX8QM_B0_LPDDR4_RPA_1.6GHz_v23 Older versions of the RPA are not aligned to SCFWv1.7.0.  If trying to use an older version of an RPA with SCFWv1.7.0, it will cause the SCFW not to boot.  The offending lines in the DCD output are as follows: For MX8QM: DATA 4 0xff148000 0x00000885 /* DRC0 bringup */ DATA 4 0xff1a0000 0x00000885 /* DRC1 bringup */ If the user wishes to use an older RPA with SCFW 1.7.0 (not recommended), then the above lines must be removed from older RPA DCD file outputs.  In addition, wrapping these lines are "#ifndef SCFW_DCD", "#else", and "#endif" preprocessor commands.  These should be removed as well.  For example of MX8QM: [remove] #ifndef SCFW_DCD [remove] /* For 1600MHz DDR, DRC 800MHz operation */ [remove] DATA 4 0xff148000 0x00000885 /* DRC0 bringup */ [remove] DATA 4 0xff1a0000 0x00000885 /* DRC1 bringup */ [remove] #else <keep code as is> [remove] #endif  
查看全文
In this article, I will explain how to set up the iMX8M Plus to use the 4K Dart BCON Basler Camera module. Requirements: Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors) Basler Camera for i.MX 8M Plus (4K dart BCON for MIPI camera module for i.MX 8M Plus | NXP Semiconductors). Embedded Linux for i.MX Applications Processors (Embedded Linux for i.MX Applications Processors | NXP Semiconductors) (For this example we will use BSP version Linux 5.15.71_2.2.0) Serial Console Emulator Basler Camera Specifications and Manuals: Basler Camera Specifications at this link: Embedded Vision Kits daA3840-30mc-IMX8MP-EVK - Embedded Vision Kits (baslerweb.com). Basler Manual to identify and setting up the hardware at this link: daA3840-30mc-IMX8MP-EVK | Basler Product Documentation (baslerweb.com) Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor. (Video: Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor | NXP Semiconductors) Steps After setting up the hardware we will need to turn on the iMX8M Plus and follow these steps: 1. Stop the boot process on Uboot by pressing any key. 2. Use the following command to list interfaces. => mmc list Output example => FSL_SDHC: 1 (SD) => FSL_SDHC: 2 The above command will show you the device number in this example for SD, the device number is 1. 3. Then use fatls <interface> <device[:partition]> [<directory>] fatls mmc 1:1 (Device 1 : Partition 1) With this command, we will be able to list device tree files. => fatls mmc 1:1 4. Select imx8mp-evk-basler.dtb or imx8mp-evk-dual-basler.dtb and use the command editenv fdtfile.  => editenv fdtfile Output example edit: imx8mp-evk-basler.dtb 5. In edit command line put the selected device tree (*.dtb). 6. Use saveenv command to save environment and continue with the boot process. 7. Using the terminal and go to /opt/imx8-isp/bin and execute the script run.sh. $ ./run.sh -c basler_1080p60 -lm 8. Use the command gst-device-monitor-1.0 to list devices. Here you will find the path to the camera device. $ gst-device-monitor-1.0 Output example Device found: name : VIV class : Video/Source caps : video/x-raw, format=YUY2, width=[ 176, 4096, 16 ], height=[ 144, 3072, 8 ], pixel-aspect-ratio=1/1, framerate={ (fraction)30/1, (fraction)29/1, (fraction)28/1, (fraction)27/1, (fraction)26/1, (fraction)25/1, (fraction)24/1, (fraction)23/1, (fraction)22/1, (fraction)21/1, (fraction)20/1, (fraction)19/1, (fraction)18/1, (fraction)17/1, (fraction)16/1, (fraction)15/1, (fraction)14/1, (fraction)13/1, (fraction)12/1, (fraction)11/1, (fraction)10/1, (fraction)9/1, (fraction)8/1, (fraction)7/1, (fraction)6/1, (fraction)5/1, (fraction)4/1, (fraction)3/1, (fraction)2/1, (fraction)1/1 } ... properties: udev-probed = true device.bus_path = platform-vvcam-video.0 sysfs.path = /sys/devices/platform/vvcam-video.0/video4linux/video2 device.subsystem = video4linux device.product.name = VIV device.capabilities = :capture: device.api = v4l2 device.path = /dev/video2 v4l2.device.driver = viv_v4l2_device v4l2.device.card = VIV v4l2.device.bus_info = platform:viv0 v4l2.device.version = 393473 (0x00060101) v4l2.device.capabilities = 2216693761 (0x84201001) v4l2.device.device_caps = 69206017 (0x04200001) gst-launch-1.0 v4l2src device=/dev/video2 ! ... 9. Finally, use gstreamer to verify proper operation. (With this gstreamer pipeline you will see a new window with the camera output. Then, just rotate the lens to acquire the correct focus) $ gst-launch-1.0 -v v4l2src device=/dev/video2 ! "video/x-raw,format=YUY2,width=1920,height=1080" ! queue ! imxvideoconvert_g2d ! waylandsink Basic description of Gstreamer Pipeline gst-launch-1.0 -v: The option -v enables the verbose mode to get detailed information of process. v4l2src device=/dev/video2: Select input device in this case the camera is on path /dev/video3. "video/x-raw,format=YUY2,width=1920,height=1080": Received format from camera. queue: This command is a buffer between camera recording process and the following image process, this command help us to interface two process and prevent blocking where each process has different speeds, in other words, when a process A is faster than process B. imxvideoconvert_g2d: This proprietary plugin uses hardware acceleration to perform rotation, scaling, and color space conversion on video frames. waylandsink : This command creates its own window and renders the decoded frames processed previously. 10. Result     I hope this article will be helpful. Best regards, Brian.
查看全文
This is about the case studay from two USB related issues: #1. Plugin detection issue caused by an errata in i.MX8/8X (host mode).       Very limited unit may encounter this problem. When issue happens, there will be totally no action on USB host port when a debug plugged in. #2: High Speed disconnection detection issue (host mode):       This may happen on some special USB design which have complex circuit and connector design on the USB path and long USB cable. The USB enumeration might be interrupted by an un-expected disconnection event. System log shows USB recognition started but failed at several different stages during handshake. For details, please refer to the doc attached (#1/#2). A reference patch for each has also been made by David.
查看全文
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
查看全文
We are pleased to announce that Config Tools for i.MX v13.1 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes 13.1 DDR tool     - i.MX93 support for A0 pre-production launch; sync with SW BSP release Pins tool     - Fix incomplete routing of deinit functions  
查看全文