i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
This is an example for user to transfer files between i.MX8MP Linux platform and other devices via Bluetooth. Environment : Hardware : i.MX8MP LPDDR4 EVK Board, Android Phone Software : L6.6.23-2.0.0   Step1 : Build Yocto image and burnt to the SD card or EMMC repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.23-2.0.0.xml repo sync DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build-xwayland Add the following code to "conf/local.conf"          IMAGE_INSTALL:append = " glibc-gconv-utf-16" bitbake imx-image-full uuu -b emmc_all imx-image-full-imx8mp-lpddr4-evk.rootfs-20240919015845.wic Step2 : Test steps Boot board with "imx8mp-evk-usdhc1-m2.dtb" file. load Wi-Fi Firmware           root@imx8mp-lpddr4-evk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf Load BT firmware and enable BT          root@imx8mp-lpddr4-evk:~# modprobe btnxpuart          root@imx8mp-lpddr4-evk:~# hciconfig           pengyong_zhang_3-1728113009623.png          root@imx8mp-lpddr4-evk:~# hciconfig hci0 up connect  the BT of Android Phone          root@imx8mp-lpddr4-evk:~# bluetoothctl          [bluetooth]# default-agent          [bluetooth]# agent on          [bluetooth]# discoverable on          [bluetooth]# scan on          [bluetooth]# scan off           pengyong_zhang_4-1728113009623.png          [bluetooth]# pair 90:F0:52:92:A6:6C          we need to type Yes on board and click 配对 on phone.          pengyong_zhang_5-1728113009624.png          pengyong_zhang_6-1728113009624.png         [bluetooth]# connect 90:F0:52:92:A6:6C         pengyong_zhang_7-1728113009625.png         [Meizu16m]# quit          pengyong_zhang_8-1728113009626.png Transfer file          1). Android Phone-> i.MX8MP EVK Board          root@imx8mp-lpddr4-evk:~# /usr/libexec/bluetooth/obexd -a -n -r /root/ & obexctl          pengyong_zhang_9-1728113009626.png          Then select a file on your phone ad choose transfer by Bluetooth.           pengyong_zhang_10-1728113009627.png         2).i.MX8MP EVK Board -> Android Phone          [obex]# connect 90:F0:52:92:A6:6C          pengyong_zhang_11-1728113009627.png          [90:F0:52:92:A6:6C]# send /home/root/test.txt          pengyong_zhang_12-1728113009628.png Note :  1. Do not suggestion use IOS phone. 2. If your i.MX8MP board can not scan your BT device, Suggest change the device BT name and run on "scan on" command again.  
View full article
This knowledge base add imx8ulp swupdate support based on AN13872. Uboot patch: add_swupdate_support_for_imx8ulp_in_uboot.patch swupdate-scripts patch: 0001-add-imx8ulp-support-in-swupdate-scripts.patch Note You must generate new key referring  5.4.3.3 Generating a key before build. Zhiming_Liu_0-1726298269688.png Commands 1. base image build command   ./assemble_base_image.sh -b imx8ulp -e emmc -d doublecopy -m   2. update image build command   ./swu_update_image_build.sh -e -s ./priv.pem -b imx8ulp -g   3. flash command:   uuu -b emmc_all .\imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot_m33 .\swu_doublecopy_rescue_imx8ulp_emmc_20240914.sdcard       Useful links: https://sbabic.github.io/swupdate/building-with-yocto.html#automatic-sha256-in-sw-description https://sbabic.github.io/swupdate/sw-description.html?highlight=hwrevision   
View full article
This article describes how to use the Preempt-RT Linux kernel in the i.MX Linux BSP 6.6.23_2.0.0. This is particularly useful for platforms such as i.MX 95, for which there is not yet a Real-Time Edge Software release.    How to do it    1. Follow the steps in the i.MX Yocto Project User's Guide and build your preferred image, for example core-image-minimal. Will further assume that the BSP is in the ~/imx-yocto-bsp directory and the build directory is ~/imx-yocto-bsp/build. 2. Unpack the attached archive in ~/imx-yocto-bsp/sources. This should create the ~/imx-yocto-bsp/sources/meta-otherkernels directory. This archive will work out of the box for i.MX 95 and i.MX 93, and may require some modifications for other platforms, as described below. 3. Add the meta-otherkernels to your build using the following command: bitbake-layers add-layer ~/imx-yocto-bsp/sources/meta-otherkernels 4. Add the OVERRIDES .= ":preempt-rt" to ~/imx-yocto-bsp/build/conf/local.conf file using the following command: echo 'OVERRIDES .= ":preempt-rt"' >> ~/imx-yocto-bsp/build/conf/local.conf This enables the Preempt-RT kernel for your build. You can always go back to your regular kernel by removing this line from ~/imx-yocto-bsp/build/conf/local.conf. 5. Build again your image. After booting this image, you can check the kernel version using: uname -a      How it works    The meta-otherkernels layer contains a .bbappend  for the linux-imx kernel recipe which replaces the sources URL with the Real-Time Edge kernel when the "preempt-rt" override is active. In addition, due to the fact that the current real-time kernel does not support all the board configurations, the layer config file (meta-otherkernels/conf/layer.conf) removes from the build the device tree files that are not supported (when "preempt-rt" override is active).   If you use this layer for other SoCs (other than i.MX 93/i.MX 95), you may need to edit the meta-otherkernels/conf/layer.conf and add the unsupported device trees. If an  unsupported device tree is left, Yocto will give an error during build.        *** DISCLAIMER *** Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
View full article
The Gui-guilder doesn't provide remote debug function in IDE and we still need use Yocto to build project or copy binary to board rootfs. This knowledge base will provide a solution about how to use VSCode to remote debug LVGL project on i.MX93 EVK board.    Yocto toolchain: L6.6.x GUI GUILDER: v1.8.0   Need to open GUI GUILDER project in VSCode.   1.Scripts in VScode   1.1 build.sh Modify build.sh in <LVGL project>/ports/linux     #!/bin/sh toolchain=$1 if [ -z "$toolchain" ];then toolchain=/opt/fsl-imx-xwayland/6.1-mickledore/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake if [ ! -r $toolchain ];then toolchain=/opt/fsl-imx-xwayland/6.1-langdale/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake fi fi toolchain_path=$(echo $toolchain |sed -E 's,^(.*)/sysroots/.*,\1,') toolchain_arch=armv8a-poky-linux if [ ! -r $toolchain -o ! -r "$toolchain_path/environment-setup-$toolchain_arch" ];then echo "ERROR: Yocto Toolchain not installed?" exit 1 fi if [ -n "$BASH_SOURCE" ]; then ROOTDIR="`readlink -f $BASH_SOURCE | xargs dirname`" elif [ -n "$ZSH_NAME" ]; then ROOTDIR="`readlink -f $0 | xargs dirname`" else ROOTDIR="`readlink -f $PWD | xargs dirname`" fi BUILDDIR=$ROOTDIR/../build rm -fr $BUILDDIR mkdir $BUILDDIR . "$toolchain_path/environment-setup-$toolchain_arch" echo "start build..." cd $ROOTDIR/linux/lv_drivers/wayland/ cmake . make cd $BUILDDIR toolchain_path=/opt/fsl-imx-wayland/6.6-scarthgap/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake cmake -G 'Ninja' .. -DCMAKE_TOOLCHAIN_FILE=$toolchain_path -Wno-dev -DLV_CONF_BUILD_DISABLE_EXAMPLES=1 -DLV_CONF_BUILD_DISABLE_DEMOS=1 -DCMAKE_CXX_FLAGS="-ggd3 -O0" -DCMAKE_BUILD_TYPE=Debug ninja if [ -e gui_guider ];then echo "Binary locates at $(readlink -f gui_guider)" ls -lh gui_guider fi # Copy binary to board scp $BUILDDIR/gui_guider [email protected]:/opt     1.2 tasks.json     { "version": "2.0.0", "tasks": [ { "label": "Build", "type": "shell", "command": "./build.sh /opt/fsl-imx-wayland/6.6-scarthgap", "options": { "cwd": "${workspaceFolder}/ports/linux" }, "problemMatcher": [ "$gcc" ], } ] }       1.3 launch.json   miDebuggerServerAddress is board ip address.     { "version": "0.2.0", "configurations": [ { "name": "(gdb) Launch", "preLaunchTask": "Build", "type": "cppdbg", "request": "launch", "program": "${workspaceFolder}/build/gui_guider", "args": [], "stopAtEntry": false, "cwd": "${workspaceFolder}/", "environment": [], "externalConsole": false, "MIMode": "gdb", "logging": { "engineLogging": true, "trace": true, "traceResponse": true }, "debugStdLib":true, "miDebuggerPath":"/usr/bin/gdb-multiarch", //DO NOT USE GDB IN SDK!!!! "miDebuggerServerAddress": "192.168.31.243:12345", "setupCommands": [ { "description": "Enable pretty-printing for gdb", "text": "-enable-pretty-printing", "ignoreFailures": true, "text": "set remotetimeout 100", } ] }] }       2. Launch gdbserver on board     export SHELL=/opt/gui_guider gdbserver 192.168.31.243:12345 /opt/gui_guider       3. Debug in VSCode   Click (gdb)launch, the source code will be compiled. Zhiming_Liu_1-1726018299992.png Then you will see the breakpoint in program. Zhiming_Liu_0-1726018276012.png Enjoy your debug~    
View full article
Introduction Time Synchronization stands for the alignment of time within distributed nodes, pretty critical for real-time applications, control and measurement systems as voice and video networks; all of them being embedded applications. It needs the synchronization of frequency, phase and time between all the nodes and offers action coordination, high precision triggers and event reference or timestamping. [1] A Time Synchronization resource it's the ethernet standard for time PTP or IEEE 1588 standard, its study begin with the physical representation of time information: PPS; Pulse Per Second. An squared wave timed by the capable MACs, in i.MX families we have two MACs of which. Background Customers are interested in this signal, we have an i.MX 8M Plus kernel 5 resource but there is a new processor family using the next major kernel version; 6. [2] We will go through demonstrating PPS on i.MX 93 EVK in both MACs; FEC and EQOS. HW setup i.MX 93 EVK boot over eMMC. Connect power and debug receptacles. Hands-on for FEC or eth0 MAC uSDHC2 pin group conflicts with the pps output pin and you are ought to remove the uSDHC2 nodes and assign the event0 out pin to the FEC pin group as shown below. --- imx93-11x11-evk.dts 2024-08-23 18:19:56.344798901 +0200 +++ imx93-11x11-evk-pps.dts 2024-09-02 21:31:46.569477421 +0200 @@ -100,18 +100,6 @@ regulator-max-microvolt = <1800000>; }; - reg_usdhc2_vmmc: regulator-usdhc2 { - compatible = "regulator-fixed"; - pinctrl-names = "default"; - pinctrl-0 = <&pinctrl_reg_usdhc2_vmmc>; - regulator-name = "VSD_3V3"; - regulator-min-microvolt = <3300000>; - regulator-max-microvolt = <3300000>; - gpio = <&gpio3 7 GPIO_ACTIVE_HIGH>; - off-on-delay-us = <12000>; - enable-active-high; - }; - reg_vdd_12v: regulator-vdd-12v { compatible = "regulator-fixed"; regulator-name = "reg_vdd_12v"; @@ -770,21 +766,6 @@ status = "okay"; }; -&usdhc2 { - pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep"; - pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>; - pinctrl-1 = <&pinctrl_usdhc2_100mhz>, <&pinctrl_usdhc2_gpio>; - pinctrl-2 = <&pinctrl_usdhc2_200mhz>, <&pinctrl_usdhc2_gpio>; - pinctrl-3 = <&pinctrl_usdhc2_sleep>, <&pinctrl_usdhc2_gpio_sleep>; - cd-gpios = <&gpio3 00 GPIO_ACTIVE_LOW>; - fsl,cd-gpio-wakeup-disable; - vmmc-supply = <&reg_usdhc2_vmmc>; - bus-width = <4>; - status = "okay"; - no-sdio; - no-mmc; -}; - &usdhc3 { pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep"; pinctrl-0 = <&pinctrl_usdhc3>, <&pinctrl_usdhc3_wlan>; @@ -860,14 +842,15 @@ MX93_PAD_ENET2_RD1__ENET1_RGMII_RD1 0x57e MX93_PAD_ENET2_RD2__ENET1_RGMII_RD2 0x57e MX93_PAD_ENET2_RD3__ENET1_RGMII_RD3 0x57e MX93_PAD_ENET2_RXC__ENET1_RGMII_RXC 0x58e MX93_PAD_ENET2_RX_CTL__ENET1_RGMII_RX_CTL 0x57e MX93_PAD_ENET2_TD0__ENET1_RGMII_TD0 0x57e MX93_PAD_ENET2_TD1__ENET1_RGMII_TD1 0x57e MX93_PAD_ENET2_TD2__ENET1_RGMII_TD2 0x57e MX93_PAD_ENET2_TD3__ENET1_RGMII_TD3 0x57e MX93_PAD_ENET2_TXC__ENET1_RGMII_TXC 0x58e MX93_PAD_ENET2_TX_CTL__ENET1_RGMII_TX_CTL 0x57e + MX93_PAD_SD2_DATA0__ENET1_1588_EVENT0_OUT 0x31e >; }; @@ -887,6 +870,7 @@ MX93_PAD_ENET2_TD3__GPIO4_IO16 0x51e MX93_PAD_ENET2_TXC__GPIO4_IO21 0x51e MX93_PAD_ENET2_TX_CTL__GPIO4_IO20 0x51e + MX93_PAD_SD2_DATA0__GPIO3_IO03 0x31e >; }; @@ -998,75 +982,6 @@ >; }; - pinctrl_reg_usdhc2_vmmc: regusdhc2vmmcgrp { - fsl,pins = < - MX93_PAD_SD2_RESET_B__GPIO3_IO07 0x31e - >; - }; - - pinctrl_usdhc2_gpio: usdhc2gpiogrp { - fsl,pins = < - MX93_PAD_SD2_CD_B__GPIO3_IO00 0x31e - >; - }; - - pinctrl_usdhc2_gpio_sleep: usdhc2gpiogrpsleep { - fsl,pins = < - MX93_PAD_SD2_CD_B__GPIO3_IO00 0x51e - >; - }; - - /* need to config the SION for data and cmd pad, refer to ERR052021 */ - pinctrl_usdhc2: usdhc2grp { - fsl,pins = < - MX93_PAD_SD2_CLK__USDHC2_CLK 0x1582 - MX93_PAD_SD2_CMD__USDHC2_CMD 0x40001382 - MX93_PAD_SD2_DATA0__USDHC2_DATA0 0x40001382 - MX93_PAD_SD2_DATA1__USDHC2_DATA1 0x40001382 - MX93_PAD_SD2_DATA2__USDHC2_DATA2 0x40001382 - MX93_PAD_SD2_DATA3__USDHC2_DATA3 0x40001382 - MX93_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e - >; - }; - - /* need to config the SION for data and cmd pad, refer to ERR052021 */ - pinctrl_usdhc2_100mhz: usdhc2-100mhzgrp { - fsl,pins = < - MX93_PAD_SD2_CLK__USDHC2_CLK 0x158e - MX93_PAD_SD2_CMD__USDHC2_CMD 0x4000138e - MX93_PAD_SD2_DATA0__USDHC2_DATA0 0x4000138e - MX93_PAD_SD2_DATA1__USDHC2_DATA1 0x4000138e - MX93_PAD_SD2_DATA2__USDHC2_DATA2 0x4000138e - MX93_PAD_SD2_DATA3__USDHC2_DATA3 0x4000138e - MX93_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e - >; - }; - - /* need to config the SION for data and cmd pad, refer to ERR052021 */ - pinctrl_usdhc2_200mhz: usdhc2-200mhzgrp { - fsl,pins = < - MX93_PAD_SD2_CLK__USDHC2_CLK 0x15fe - MX93_PAD_SD2_CMD__USDHC2_CMD 0x400013fe - MX93_PAD_SD2_DATA0__USDHC2_DATA0 0x400013fe - MX93_PAD_SD2_DATA1__USDHC2_DATA1 0x400013fe - MX93_PAD_SD2_DATA2__USDHC2_DATA2 0x400013fe - MX93_PAD_SD2_DATA3__USDHC2_DATA3 0x400013fe - MX93_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e - >; - }; - - pinctrl_usdhc2_sleep: usdhc2grpsleep { - fsl,pins = < - MX93_PAD_SD2_CLK__GPIO3_IO01 0x51e - MX93_PAD_SD2_CMD__GPIO3_IO02 0x51e - MX93_PAD_SD2_DATA0__GPIO3_IO03 0x51e - MX93_PAD_SD2_DATA1__GPIO3_IO04 0x51e - MX93_PAD_SD2_DATA2__GPIO3_IO05 0x51e - MX93_PAD_SD2_DATA3__GPIO3_IO06 0x51e - MX93_PAD_SD2_VSELECT__GPIO3_IO19 0x51e - >; - }; - /* need to config the SION for data and cmd pad, refer to ERR052021 */ pinctrl_usdhc3: usdhc3grp { fsl,pins = < The driver also needs the following rework. --- a/drivers/net/ethernet/freescale/fec_ptp.c +++ b/drivers/net/ethernet/freescale/fec_ptp.c @@ -184,7 +184,8 @@ static int fec_ptp_enable_pps(struct fec_enet_private *fep, uint enable) val |= (1 << FEC_T_TF_OFFSET | 1 << FEC_T_TIE_OFFSET); val &= ~(1 << FEC_T_TDRE_OFFSET); val &= ~(FEC_T_TMODE_MASK); - val |= (FEC_HIGH_PULSE << FEC_T_TMODE_OFFSET); + // val |= (FEC_HIGH_PULSE << FEC_T_TMODE_OFFSET); + val |= (FEC_TMODE_TOGGLE << FEC_T_TMODE_OFFSET); writel(val, fep->hwp + FEC_TCSR(fep->pps_channel)); /* Write the second compare event timestamp and calculate After booting the board, run these commands: $ ptp4l -A -4 -H -m -i eth0 & $ echo 1 > /sys/class/ptp/ptp0/pps_enable These will get the SD2_DATA0 or TP1009 running a square wave at 0.5 Hz through setting the ptp0 port with: -A    Select the delay mechanism automatically. Start with E2E and switch to P2P when a peer delay request is received. -4    Select the UDP IPv4 network transport. This is the default transport. -H    Select the hardware time stamping. -m    Print messages to the standard output. JosephAtNXP_0-1725312576333.bmp Run the next command to set the pps (1 Hz signal): $ echo "0 $(date +%s) 100000000 1 0" > /sys/class/ptp/ptp0/period The last because the current driver needs the actual date and a future start; in this case the signal will start within 100 ms, in order to work. You can try with different start times until the optimal value is found. [3] JosephAtNXP_1-1725312604309.bmp   Hands-on for EQOS or eth1 MAC This is reduced to the proper devicetree changes, and it does not have driver rework nor pps_enable control file. It uses SD2_CLK or TP1008, so DTS need this adjustment: --- imx93-11x11-evk.dts 2024-08-23 18:19:56.344798901 +0200 +++ imx93-11x11-evk-pps.dts 2024-09-02 21:31:46.569477421 +0200 @@ -100,18 +100,6 @@ regulator-max-microvolt = <1800000>; }; - reg_usdhc2_vmmc: regulator-usdhc2 { - compatible = "regulator-fixed"; - pinctrl-names = "default"; - pinctrl-0 = <&pinctrl_reg_usdhc2_vmmc>; - regulator-name = "VSD_3V3"; - regulator-min-microvolt = <3300000>; - regulator-max-microvolt = <3300000>; - gpio = <&gpio3 7 GPIO_ACTIVE_HIGH>; - off-on-delay-us = <12000>; - enable-active-high; - }; - reg_vdd_12v: regulator-vdd-12v { compatible = "regulator-fixed"; regulator-name = "reg_vdd_12v"; @@ -770,21 +766,6 @@ status = "okay"; }; -&usdhc2 { - pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep"; - pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>; - pinctrl-1 = <&pinctrl_usdhc2_100mhz>, <&pinctrl_usdhc2_gpio>; - pinctrl-2 = <&pinctrl_usdhc2_200mhz>, <&pinctrl_usdhc2_gpio>; - pinctrl-3 = <&pinctrl_usdhc2_sleep>, <&pinctrl_usdhc2_gpio_sleep>; - cd-gpios = <&gpio3 00 GPIO_ACTIVE_LOW>; - fsl,cd-gpio-wakeup-disable; - vmmc-supply = <&reg_usdhc2_vmmc>; - bus-width = <4>; - status = "okay"; - no-sdio; - no-mmc; -}; - &usdhc3 { pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep"; pinctrl-0 = <&pinctrl_usdhc3>, <&pinctrl_usdhc3_wlan>; @@ -822,14 +802,15 @@ MX93_PAD_ENET1_RD1__ENET_QOS_RGMII_RD1 0x57e MX93_PAD_ENET1_RD2__ENET_QOS_RGMII_RD2 0x57e MX93_PAD_ENET1_RD3__ENET_QOS_RGMII_RD3 0x57e MX93_PAD_ENET1_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK 0x58e MX93_PAD_ENET1_RX_CTL__ENET_QOS_RGMII_RX_CTL 0x57e MX93_PAD_ENET1_TD0__ENET_QOS_RGMII_TD0 0x57e MX93_PAD_ENET1_TD1__ENET_QOS_RGMII_TD1 0x57e MX93_PAD_ENET1_TD2__ENET_QOS_RGMII_TD2 0x57e MX93_PAD_ENET1_TD3__ENET_QOS_RGMII_TD3 0x57e MX93_PAD_ENET1_TXC__CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK 0x58e MX93_PAD_ENET1_TX_CTL__ENET_QOS_RGMII_TX_CTL 0x57e + MX93_PAD_SD2_CLK__ENET_QOS_1588_EVENT0_OUT 0x31e >; }; @@ -849,6 +830,7 @@ MX93_PAD_ENET1_TD3__GPIO4_IO02 0x31e MX93_PAD_ENET1_TXC__GPIO4_IO07 0x31e MX93_PAD_ENET1_TX_CTL__GPIO4_IO06 0x31e + MX93_PAD_SD2_CLK__GPIO3_IO01 0x31e >; }; @@ -998,75 +982,6 @@ >; }; - pinctrl_reg_usdhc2_vmmc: regusdhc2vmmcgrp { - fsl,pins = < - MX93_PAD_SD2_RESET_B__GPIO3_IO07 0x31e - >; - }; - - pinctrl_usdhc2_gpio: usdhc2gpiogrp { - fsl,pins = < - MX93_PAD_SD2_CD_B__GPIO3_IO00 0x31e - >; - }; - - pinctrl_usdhc2_gpio_sleep: usdhc2gpiogrpsleep { - fsl,pins = < - MX93_PAD_SD2_CD_B__GPIO3_IO00 0x51e - >; - }; - - /* need to config the SION for data and cmd pad, refer to ERR052021 */ - pinctrl_usdhc2: usdhc2grp { - fsl,pins = < - MX93_PAD_SD2_CLK__USDHC2_CLK 0x1582 - MX93_PAD_SD2_CMD__USDHC2_CMD 0x40001382 - MX93_PAD_SD2_DATA0__USDHC2_DATA0 0x40001382 - MX93_PAD_SD2_DATA1__USDHC2_DATA1 0x40001382 - MX93_PAD_SD2_DATA2__USDHC2_DATA2 0x40001382 - MX93_PAD_SD2_DATA3__USDHC2_DATA3 0x40001382 - MX93_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e - >; - }; - - /* need to config the SION for data and cmd pad, refer to ERR052021 */ - pinctrl_usdhc2_100mhz: usdhc2-100mhzgrp { - fsl,pins = < - MX93_PAD_SD2_CLK__USDHC2_CLK 0x158e - MX93_PAD_SD2_CMD__USDHC2_CMD 0x4000138e - MX93_PAD_SD2_DATA0__USDHC2_DATA0 0x4000138e - MX93_PAD_SD2_DATA1__USDHC2_DATA1 0x4000138e - MX93_PAD_SD2_DATA2__USDHC2_DATA2 0x4000138e - MX93_PAD_SD2_DATA3__USDHC2_DATA3 0x4000138e - MX93_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e - >; - }; - - /* need to config the SION for data and cmd pad, refer to ERR052021 */ - pinctrl_usdhc2_200mhz: usdhc2-200mhzgrp { - fsl,pins = < - MX93_PAD_SD2_CLK__USDHC2_CLK 0x15fe - MX93_PAD_SD2_CMD__USDHC2_CMD 0x400013fe - MX93_PAD_SD2_DATA0__USDHC2_DATA0 0x400013fe - MX93_PAD_SD2_DATA1__USDHC2_DATA1 0x400013fe - MX93_PAD_SD2_DATA2__USDHC2_DATA2 0x400013fe - MX93_PAD_SD2_DATA3__USDHC2_DATA3 0x400013fe - MX93_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e - >; - }; - - pinctrl_usdhc2_sleep: usdhc2grpsleep { - fsl,pins = < - MX93_PAD_SD2_CLK__GPIO3_IO01 0x51e - MX93_PAD_SD2_CMD__GPIO3_IO02 0x51e - MX93_PAD_SD2_DATA0__GPIO3_IO03 0x51e - MX93_PAD_SD2_DATA1__GPIO3_IO04 0x51e - MX93_PAD_SD2_DATA2__GPIO3_IO05 0x51e - MX93_PAD_SD2_DATA3__GPIO3_IO06 0x51e - MX93_PAD_SD2_VSELECT__GPIO3_IO19 0x51e - >; - }; - /* need to config the SION for data and cmd pad, refer to ERR052021 */ pinctrl_usdhc3: usdhc3grp { fsl,pins = < After boot, issue these commands: $ ptp4l -A -4 -H -m -i eth1 & $ echo "0 $(date +%s) 1000000000 1 0" > /sys/class/ptp/ptp1/period You will have an squared wave of 1 Hz running within 1 s with the same settings as the FEC setup. JosephAtNXP_2-1725312629341.bmp   Conclusion Both PPS can run in the same image changes and DTS changes, proven in imx-linux-nanbield branch, with the manifest imx-6.6.3-1.0.0.xml. And it's the start of testing IEEE 1588 and syncing capabilities of this i.MX 9 series processors. Sources [1] http://events17.linuxfoundation.org/sites/events/files/slides/elc_insop_2015.pdf [2] https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-serials-IEEE1588-1pps-test-procedure/ta-p/1490634 [3] https://github.com/nxp-imx/linux-imx/blob/b586a521770e508d1d440ccb085c7696b9d6d387/Documentation/ABI/testing/sysfs-ptp#L2
View full article
P3T1755 Demo   In this space I want to show you the things that you can create usign our products.   In  this demo I demostrate a use case creating a GUI for a Temperature Sensor.   We can create modern GUIs and more with LVGL combined with our powerful processors.   Chavira_3-1724712966073.png       Chavira_4-1724713032854.png   Chavira_4-1724769477065.png     CPU USAGE As we can see  the CPU usage for this demo is around 2% Chavira_0-1724768894160.png   Pictures Chavira_1-1724769063525.jpeg   Chavira_2-1724769110355.jpeg     Chavira_3-1724769118618.jpeg   This demo is based on the previous publused articles.   References: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Adding-support-to-P3T1755-on-Linux/ta-p/1855874 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-run-LGVL-on-iMX-using-framebuffer/ta-p/1853768  
View full article
  Some customers want to expose their i3c device on the /dev, In order to develop their i3c APP or operation the i3c device like I2C. But in our default BSP code, we do not support this feature for I3C device, This article will introduce how to make the i3c device expose to the user space. Board : i.MX 93 EVK BSP Version : lf-6.1.55-2.2.0 I3C device : LSM6DSOXTR Step 1 : Rework the i.MX93 EVK Board, Install the R1010.  pengyong_zhang_0-1716793370445.png     Step 2 : Apply the add_i3c_device_to_dev.patch file to the linux kernel code              Command : git apply add_i3c_device_to_dev.patch Step 3 : Re-compile the kernel Image file.              Command : make imx_v8_defconfig                                  make Step 4 : Boot your board with "imx93-11x11-evk-i3c.dtb" file and see if you can see the I3C device on the /dev directory. Result : We can see the i3c device is appeared in /dev directory, The i2c-8 is an i2c device mounted to the i3c bus. The i3c is backward compatible with i2c device. It will simulate the I2C signal loading i2c device.               pengyong_zhang_1-1716793370452.png   PS : You can also use the i2ctool detect i2c-8 device. As shown in the following picture: pengyong_zhang_2-1716793370465.png   Note : If you need the patch file, Please contact me any time for free.
View full article
Ftrace is powerful tracing utility embedded in Linux kernel. It provides a very good method for kernel developer to get insights of the kernel behavior. While official kernel doc for ftrace is somehow long and complex, this document provides a quicker and simpler way to get start with ftrace.
View full article
This guide is a continuation from our latest Debian 12 Installation Guide for iMX8MM, iMX8MP, iMX8MN and iMX93. Here we will describe the process to install the multimedia and hardware acceleration packages, specifically GPU, VPU and Gstreamer on i.MX8M Mini, i.MX8M Plus and i.MX8M Nano. The guide is based on the one provided by our colleague Build Ubuntu For i.MX8 Series Platform - NXP Community, which requires to previously build an image using Yocto Project with the following distro and image name. Distro name - fsl-imx-wayland Image name – imx-image-multimedia For more information please check our BSP documentation i.MX Yocto Project User’s Guide.   Hardware Requirements Linux Host Computer (Ubuntu 20.04 or later) USB Card reader or Micro SD to SD adapter SD Card Evaluation Kit Board for the i.MX8M Nano, i.MX8M Mini, i.MX8M Plus   Software Requirements Linux Ubuntu (20.04 tested) or Debian for Host Computer BSP version 6.1.55 built with Yocto Project   After built the image we can start the installation by following the steps below:   GPU Installation The GPU Installation consists of copy the files from packages imx-gpu-g2d, imx-gpu-viv, libdrm to the Debian system. As our latest installation guide, we will continue naming “mountpoint” to the directory where Debian system is mounted on our host machine. Regarding the path provided on each step, we put labels <build-path> and <machine> that you will need to change based on your environment. These are the paths that Yocto Project uses to save the packages. However, this could change on your environment and you can find the work directory from each package using the following command: bitbake -e <package-name> | grep ^WORKDIR= This command will show you the absolute path of the package work directory. 1. Install GPU Packages $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-gpu-g2d/6.4.11.p2.2-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-gpu-viv/1_6.4.11.p2.2-aarch64-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/libdrm/2.4.115.imx-r0/image/* mountpoint   2. Install Linux IMX Headers and IMX Parser $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/linux-imx-headers/6.1-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-poky-linux/imx-parser/4.8.2-r0/image/* mountpoint   3. Use chroot $ sudo LANG=C.UTF-8 chroot mountpoint/ qemu-aarch64-static /bin/bash   4. Install Dependencies $ apt install libudev-dev libinput-dev libxkbcommon-dev libpam0g-dev libx11-xcb-dev libxcb-xfixes0-dev libxcb-composite0-dev libxcursor-dev libxcb-shape0-dev libdbus-1-dev libdbus-glib-1-dev libsystemd-dev libpixman-1-dev libcairo2-dev libffi-dev libxml2-dev kbd libexpat1-dev autoconf automake libtool meson cmake ssh net-tools network-manager iputils-ping rsyslog bash-completion htop resolvconf dialog vim udhcpc udhcpd git v4l-utils alsa-utils git gcc less autoconf autopoint libtool bison flex gtk-doc-tools libglib2.0-dev libpango1.0-dev libatk1.0-dev kmod pciutils libjpeg-dev   5. Create a folder for Multimedia Installation. Here we will clone all the multimedia repositories.  $ mkdir multimedia_packages $ cd multimedia_packages   6. Build Wayland $ git clone https://gitlab.freedesktop.org/wayland/wayland.git $ cd wayland $ git checkout 1.22.0 $ meson setup build --prefix=/usr -Ddocumentation=false -Ddtd_validation=true $ cd build $ ninja install   7. Build Wayland Protocols IMX $ git clone https://github.com/nxp-imx/wayland-protocols-imx.git $ cd wayland-protocols-imx $ git checkout wayland-protocols-imx-1.32 $ meson setup build --prefix=/usr -Dtests=false $ cd build $ ninja install   8. Build Weston $ git clone https://github.com/nxp-imx/weston-imx.git $ cd weston-imx $ git checkout weston-imx-11.0.3 $ meson setup build --prefix=/usr -Dpipewire=false -Dsimple-clients=all -Ddemo-clients=true -Ddeprecated-color-management-colord=false -Drenderer-gl=true -Dbackend-headless=false -Dimage-jpeg=true -Drenderer-g2d=true -Dbackend-drm=true -Dlauncher-libseat=false -Dcolor-management-lcms=false -Dbackend-rdp=false -Dremoting=false -Dscreenshare=true -Dshell-desktop=true -Dshell-fullscreen=true -Dshell-ivi=true -Dshell-kiosk=true -Dsystemd=true -Dlauncher-logind=true -Dbackend-drm-screencast-vaapi=false -Dbackend-wayland=false -Dimage-webp=false -Dbackend-x11=false -Dxwayland=false $ cd build $ ninja install   VPU Installation To install VPU and Gstreamer please follow the steps below: 1. Install firmware-imx $ sudo cp -Pra <build-path>/tmp/work/all-poky-linux/firmware-imx/1_8.22-r0/image/lib/* mountpoint/lib/   2. Install VPU Driver $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-vpu-hantro/1.31.0-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-vpuwrap/git-r0/image/* mountpoint   3. Use chroot $ sudo LANG=C.UTF-8 chroot mountpoint/ qemu-aarch64-static /bin/bash   4. Install dependencies for Gstreamer Plugins $ apt install libgirepository1.0-dev gettext liborc-0.4-dev libasound2-dev libogg-dev libtheora-dev libvorbis-dev libbz2-dev libflac-dev libgdk-pixbuf-2.0-dev libmp3lame-dev libmpg123-dev libpulse-dev libspeex-dev libtag1-dev libbluetooth-dev libusb-1.0-0-dev libcurl4-openssl-dev libssl-dev librsvg2-dev libsbc-dev libsndfile1-dev   5. Change directory to multimedia packages. $ cd multimedia-packages   6. Build gstreamer $ git clone https://github.com/nxp-imx/gstreamer -b lf-6.1.55-2.2.0 $ cd gstreamer $ meson setup build --prefix=/usr -Dintrospection=enabled -Ddoc=disabled -Dexamples=disabled -Ddbghelp=disabled -Dnls=enabled -Dbash-completion=disabled -Dcheck=enabled -Dcoretracers=disabled -Dgst_debug=true -Dlibdw=disabled -Dtests=enabled -Dtools=enabled -Dtracer_hooks=true -Dlibunwind=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   7. Build gst-plugins-base $ git clone https://github.com/nxp-imx/gst-plugins-base -b lf-6.1.55-2.2.0 $ cd gst-plugins-base $ meson setup build --prefix=/usr -Dalsa=enabled -Dcdparanoia=disabled -Dgl-graphene=disabled -Dgl-jpeg=disabled -Dopus=disabled -Dogg=enabled -Dorc=enabled -Dpango=enabled -Dgl-png=enabled -Dqt5=disabled -Dtheora=enabled -Dtremor=disabled -Dvorbis=enabled -Dlibvisual=disabled -Dx11=disabled -Dxvideo=disabled -Dxshm=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   8. Build gst-plugins-good $ git clone https://github.com/nxp-imx/gst-plugins-good -b lf-6.1.55-2.2.0 $ cd gst-plugins-good $ meson setup build --prefix=/usr -Dexamples=disabled -Dnls=enabled -Ddoc=disabled -Daalib=disabled -Ddirectsound=disabled -Ddv=disabled -Dlibcaca=disabled -Doss=enabled -Doss4=disabled -Dosxaudio=disabled -Dosxvideo=disabled -Dshout2=disabled -Dtwolame=disabled -Dwaveform=disabled -Dasm=disabled -Dbz2=enabled -Dcairo=enabled -Ddv1394=disabled -Dflac=enabled -Dgdk-pixbuf=enabled -Dgtk3=disabled -Dv4l2-gudev=enabled -Djack=disabled -Djpeg=enabled -Dlame=enabled -Dpng=enabled -Dv4l2-libv4l2=disabled -Dmpg123=enabled -Dorc=enabled -Dpulse=enabled -Dqt5=disabled -Drpicamsrc=disabled -Dsoup=enabled -Dspeex=enabled -Dtaglib=enabled -Dv4l2=enabled -Dv4l2-probe=true -Dvpx=disabled -Dwavpack=disabled -Dximagesrc=disabled -Dximagesrc-xshm=disabled -Dximagesrc-xfixes=disabled -Dximagesrc-xdamage=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   9. Build gst-plugins-bad $ git clone https://github.com/nxp-imx/gst-plugins-bad -b lf-6.1.55-2.2.0 $ cd gst-plugins-bad $ meson setup build --prefix=/usr -Dintrospection=enabled -Dexamples=disabled -Dnls=enabled -Dgpl=disabled -Ddoc=disabled -Daes=enabled -Dcodecalpha=enabled -Ddecklink=enabled -Ddvb=enabled -Dfbdev=enabled -Dipcpipeline=enabled -Dshm=enabled -Dtranscode=enabled -Dandroidmedia=disabled -Dapplemedia=disabled -Dasio=disabled -Dbs2b=disabled -Dchromaprint=disabled -Dd3dvideosink=disabled -Dd3d11=disabled -Ddirectsound=disabled -Ddts=disabled -Dfdkaac=disabled -Dflite=disabled -Dgme=disabled -Dgs=disabled -Dgsm=disabled -Diqa=disabled -Dkate=disabled -Dladspa=disabled -Dldac=disabled -Dlv2=disabled -Dmagicleap=disabled -Dmediafoundation=disabled -Dmicrodns=disabled -Dmpeg2enc=disabled -Dmplex=disabled -Dmusepack=disabled -Dnvcodec=disabled -Dopenexr=disabled -Dopenni2=disabled -Dopenaptx=disabled -Dopensles=disabled -Donnx=disabled -Dqroverlay=disabled -Dsoundtouch=disabled -Dspandsp=disabled -Dsvthevcenc=disabled -Dteletext=disabled -Dwasapi=disabled -Dwasapi2=disabled -Dwildmidi=disabled -Dwinks=disabled -Dwinscreencap=disabled -Dwpe=disabled -Dzxing=disabled -Daom=disabled -Dassrender=disabled -Davtp=disabled -Dbluez=enabled -Dbz2=enabled -Dclosedcaption=enabled -Dcurl=enabled -Ddash=enabled -Ddc1394=disabled -Ddirectfb=disabled -Ddtls=disabled -Dfaac=disabled -Dfaad=disabled -Dfluidsynth=disabled -Dgl=enabled -Dhls=enabled -Dkms=enabled -Dcolormanagement=disabled -Dlibde265=disabled -Dcurl-ssh2=disabled -Dmodplug=disabled -Dmsdk=disabled -Dneon=disabled -Dopenal=disabled -Dopencv=disabled -Dopenh264=disabled -Dopenjpeg=disabled -Dopenmpt=disabled -Dhls-crypto=openssl -Dopus=disabled -Dorc=enabled -Dresindvd=disabled -Drsvg=enabled -Drtmp=disabled -Dsbc=enabled -Dsctp=disabled -Dsmoothstreaming=enabled -Dsndfile=enabled -Dsrt=disabled -Dsrtp=disabled -Dtinyalsa=disabled -Dtinycompress=enabled -Dttml=enabled -Duvch264=enabled -Dv4l2codecs=disabled -Dva=disabled -Dvoaacenc=disabled -Dvoamrwbenc=disabled -Dvulkan=disabled -Dwayland=enabled -Dwebp=enabled -Dwebrtc=disabled -Dwebrtcdsp=disabled -Dx11=disabled -Dx265=disabled -Dzbar=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   10. Build imx-gst1.0-plugin $ git clone https://github.com/nxp-imx/imx-gst1.0-plugin -b lf-6.1.55-2.2.0 $ cd imx-gst1.0-plugin $ meson setup build --prefix=/usr -Dplatform=MX8 -Dc_args=-I/usr/include/imx $ cd build $ ninja install   11. Exit chroot $ exit   Verify Installation For verification process, boot your target from the SD Card. (Review your specific target documentation) 1. Verify Weston For this verification you will need to be root user. # export XDG_RUNTIME_DIR=/run/user/0 # weston   2. Verify VPU and Gstreamer Use the following Gstreamer pipeline for Hardware Accelerated VPU Encode. # gst-launch-1.0 videotestsrc ! video/x-raw, format=I420, width=640, height=480 ! vpuenc_h264 ! filesink location=test.mp4   Then you can reproduce the file with this command: # gplay-1.0 test.mp4   Finally, you have installed and verified the GPU, VPU and Multimedia packages. Now, you can start testing audio and video applications.
View full article
The following steps allow to make use of device tree overlay files, a definition of device tree overlay provided by kernel.org is the next:  "A Devicetree’s overlay purpose is to modify the kernel’s live tree, and have the modification affecting the state of the kernel in a way that is reflecting the changes. Since the kernel mainly deals with devices, any new device node that result in an active device should have it created while if the device node is either disabled or removed all together, the affected device should be deregistered." Knowing that, in this post will be used as an example the baseboard "i.MX 93 EVK" and will be added with device tree overlay an LVDS panel, adding an automatic detection from u-boot, and will be used a host with linux version Ubuntu 20.04.2. Note: It only works for linux kernel version 6.6.3-nanbield onward. Linux device-tree overlay from linux-imx   This section explains all about device tree overlay compilation and building, to create a .dtso file, the equivalent of .dts for overlays, adding some difference between them, using as base the linux-imx repository. It can be downloaded from the following repository:   git clone https://github.com/nxp-imx/linux-imx.git -b <branch version>   Branch version used by this post "lf-6.6.3-1.0.0". Device tree source overlay (.dtso)    It can be similar to a device tree source (.dts) but it had little difference between them, there are some difference in the next list: There's another type of files to be included, if is used pinmux it's necessary adding it with "#include "imx93-pinfunc.h"" and libraries from dt-bindings, it depends on the type of device tree to implement "#include <dt-bindings/<library>>" At initialization it needs to add: "/dts-v1/;"  "/plugin/;" Addition of "fragment" nodes, it allow override parts of a device tree,  it can be a specific node or create a new node. following structure it's the structure of a fragment:   { /* ignored properties by the overlay */ fragment@0 { /* first child node */ target=<phandle>; /* phandle target of the overlay */ or target-path="/path"; /* target path of the overlay */ __overlay__ { property-a; /* add property-a to the target */ node-a { /* add to an existing, or create a node-a */ ... }; }; } fragment@1 { /* second child node */ ... }; /* more fragments follow */ }   kernel.org Overlays can't delete a property or a node when it's applied, so can't be used "/delete-node/" nor "/delete-prop/", but it can be added to the node "status = "disabled";" to disable it.  Using as an example the file imx93-11x11-evk-boe-wxga-lvds-panel.dts located in the previous repository file direction <linux-imx path>/arch/arm64/boot/dts/freescale/ using it as a base tree:   // SPDX-License-Identifier: (GPL-2.0+ OR MIT) /* * Copyright 2022 NXP */ #include "imx93-11x11-evk.dts" / { lvds_backlight: lvds_backlight { compatible = "pwm-backlight"; pwms = <&adp5585pwm 0 100000 0>; enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>; power-supply = <&reg_vdd_12v>; status = "okay"; brightness-levels = < 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100>; default-brightness-level = <80>; }; ... }; ... &adv7535 { status = "disabled"; }; ...   imx93-11x11-evk-boe-wxga-lvds-panel.dts Using the previous points and making use of fragments, if we want adapt the node lvds_backlight as fragment, it will be  added in the section of overlay, and adding it to a target-path "/":   #include <dt-bindings/interrupt-controller/irq.h> #include "imx93-pinfunc.h" #include <dt-bindings/gpio/gpio.h> /dts-v1/; /plugin/; / { fragment@0 { target-path = "/"; __overlay__ { lvds_backlight: lvds_backlight { compatible = "pwm-backlight"; pwms = <&adp5585pwm 0 100000 0>; enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>; power-supply = <&reg_vdd_12v>; status = "okay"; brightness-levels = < 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100>; default-brightness-level = <80>; }; }; }; ... };   imx93-11x11-evk-test-lvds-panel.dtso In the case of adding a property to an existing node, it will look in the following way using as example the node adv7535.   ... / { ... fragment@2 { target = <&adv7535>; __overlay__ { status = "disabled"; }; }; ... };   imx93-11x11-evk-boe-wxga-lvds-panel.dts At the end of this post, will be attach the complete file used for LVDS panel named as imx93-11x11-evk-test-lvds-panel.dtso Build device tree blob for overlay (dtbo)   To compile the previous .dtso it's necessary to include it to linux-imx repository, linux device tree overlay was included in BSP from version 6.6.3-nanbield onward in Makefile, so it's only necessary adding it as files to be compiled as .dtso, at the end of the post will be a patch file named as linux-imx-makefile.patch to add LVDS-panel to Makefile from branch lf-6.6.3-1.0.0 Add previously file imx93-11x11-evk-test-lvds-panel.dtso to path <linux-imx path>/arch/arm64/boot/dts/freescale/ Add imx93-11x11-evk-test-lvds-panel.dtso as file to be compiled in Makefile, it is located in the next path <linux-imx path>/arch/arm64/boot/dts/freescale/Makefile, it can be added with the next sentence format: <overlay without extension>-dtbs := <file to be overlayed>.dtb <overlay>.dtbo Example of how to add LVDS panel to makefile  imx93-11x11-evk-test-lvds-panel-dtbs := imx93-11x11-evk.dtb imx93-11x11-evk-test-lvds-panel.dtbo Makefile From main path, make the configuration to be compiled with the following bash command: $ cd <linux-imx path>/ $ make -j$(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- imx_v8_defconfig​ Compile overlay to use $ make -j $(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- freescale/<overlay>.dtbo​ as example for LVDS panel $ make -j $(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- freescale/imx93-11x11-evk-test-lvds-panel.dtbo It will compile the device tree blob overlay to use. Copy .dtbo generated in memory used by i.MX 93, it can be sending it from scp. scp ./​<overlay>.dtbo​ root@<ip>:/run/media/<memory section used> u-boot   This section explain the procedure to load a device tree overlay, it will be from u-boot explaining commands used and using the LVDS panel as an example. Before applying overlay   Before applying, it's necessary had a device tree loaded so looking around in the process of booting in a i.MX 93 from u-boot, this process is defined by the enviroment variable "bsp_bootcmd" that calls the variable mmcboot, and looking what does these variables, it can be look in the following sentence:    bsp_bootcmd=echo Running BSP bootcmd ...; mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if test ${sec_boot} = yes; then if run loadcntr; then run mmcboot; else run netboot; fi; else if run loadimage; then run mmcboot; else run netboot; fi; fi; fi; fi; mmcboot=echo Booting from mmc ...; run mmcargs; if test ${sec_boot} = yes; then if run auth_os; then run boot_os; else echo ERR: failed to authenticate; fi; else if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if run loadfdt; then run boot_os; else echo WARN: Cannot load the DT; fi; fi;fi;   but reducing it in a normal situation, ignoring if else case and echoes, it can be simplify to:   mmc dev ${mmcdev}; run loadimage; run mmcargs; run loadfdt; run boot_os;   the device tree is load is in the section "run loadfdt" with fatload in his definition:   loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr_r} ${fdtfile}   So, it's necessary to applying device tree overlay after "run loadfdt". How to apply an overlay   To load correctly an overlay it's necessary to following some steps: Load flattened device tree (fdt). (executed by loadfdt) Configure fdt address.  In some cases it's necessary to expand fdt memory size Load overlay Apply overlay The full sentence to apply it, it's the following u-boot command:   u-boot=> setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr ${fdt_addr} && fdt resize ${fdt_buffer}; fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} <overlay>.dtbo && fdt apply ${fdtovaddr};   First of all, setexpr it's just to create a new variable, in this case these variable is an integer. Spliting the previously command we can found the steps to applying it. "fdt addr ${fdt_addr};" used to configure fdt address, and point to the space of memory previously charged. "fdt resize ${fdt_buffer};" expand fdt memory size, is used as a value 16384 just to get the enough space to charge dtbo, this number was related with 2 14 "fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} <overlay>.dtbo" Load device tree overlay using fdovaddr, that is fdt_addr adding an offset of memory space.  "fdt apply ${fdtovaddr};" apply device tree overlay Remembering about load overlay needs to be executed after loadfdt, it's possible to save the previous command to a variable and executing it after loadfdt with setexpr, in this case using as example lvds test.   u-boot=> setenv loadoverlay "setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr $\{fdt_addr\} && fdt resize $\{fdt_buffer\}; fatload mmc $\{mmcdev\}:$\{mmcpart\} $\{fdtovaddr\} imx93-11x11-evk-test-lvds-panel.dtbo && fdt apply $\{fdtovaddr\};"   and modifying mmcboot with loadoverlay after loadfdt   u-boot=> setenv mmcboot "run mmcargs; run loadfdt; run loadoverlay; run boot_os;"   to save the environment variables created, it can be saved from u-boot wit the following command.   u-boot=> saveenv   At the end, boot imx93   u-boot=> boot   The LVDS panel should be working using the original dtb (imx93-11x11-evk.dtb) applied the overlay. Automatize u-boot LVDS Panel   This section explain how can be automatize the u-boot load overlay using an LVDS panel, it can vary depending the device to used for, the method used is detecting it in u-boot initialization and if found any device it will generate an environment variable. All the steps was using as a base uboot-imx repository, it can be downloaded from the following repository, at the end of this post will be a patch with the changes.   git clone https://github.com/nxp-imx/uboot-imx.git -b <branch version>   Branch version used "lf-6.6.3-1.0.0". Base   Knowing more about LVDS Panel used by imx93 it's really hard know more information about registers, so in this example will be limited to detect that is connected the address to a corresponding bus from touch controller.  To know i2c address and bus used by LVDS panel it was used searching it from the original device tree in the next section:   &lpi2c1 { exc80h60: touch@2a { compatible = "eeti,exc80h60"; reg = <0x2a>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_ctp_int>; /* * Need to do hardware rework here: * remove R131, short R181 */ interrupt-parent = <&gpio2>; interrupts = <21 IRQ_TYPE_LEVEL_LOW>; reset-gpios = <&pcal6524 17 GPIO_ACTIVE_HIGH>; status = "okay"; }; };   imx93-11x11-evk-boe-wxga-lvds-panel.dts Previous node is related with touch controller from LVDS using lpi2c1, the first channel of i2c corresponding to i2c bus 0, and the register used express the address used to be detected by device tree, in this case was the address 0x2A. u-boot generating a trigger   About how it can be detected touch controller from u-boot, this procedure use a function named as "board_late_init", it can be found by his definition from u-boot readme:   Board initialization settings: ------------------------------ During Initialization u-boot calls a number of board specific functions to allow the preparation of board specific prerequisites, e.g. pin setup before drivers are initialized. To enable these callbacks the following configuration macros have to be defined. Currently this is architecture specific, so please check arch/your_architecture/lib/board.c typically in board_init_f() and board_init_r(). - CONFIG_BOARD_EARLY_INIT_F: Call board_early_init_f() - CONFIG_BOARD_EARLY_INIT_R: Call board_early_init_r() - CONFIG_BOARD_LATE_INIT: Call board_late_init()   u-boot README In the case of i.MX 93 this function can be found in the next path <u-boot path>/board/freescale/imx93_evk/imx93_evk.c. Using the library included, "uclass.h", it will create a function that, if detect in the bus 0 (LVDS i2c bus) the address 0x2A (i2c LVDS address), it will create an environment variable with the overlay used, it can be set with the function env_set(<String with the name of the variable>, <String with the content of the variable>), the following function can detect and create the environment variable mentioned, creating it with the name "device-tree-overlay" with the content "lvds-panel".   #define LVDS_TOUCH_I2C_BUS 0 #define LVDS_TOUCH_I2C_ADDR 0x2A static void detect_display_connected(void) { struct udevice *bus = NULL; struct udevice *i2c_dev = NULL; int ret; ret = uclass_get_device_by_seq(UCLASS_I2C, LVDS_TOUCH_I2C_BUS, &bus); if (ret) { printf("%s: Can't find bus\n", __func__); } else { ret = dm_i2c_probe(bus, LVDS_TOUCH_I2C_ADDR, 0, &i2c_dev); if (ret) { printf("%s: Can't find device id=0x%x\n", __func__, LVDS_TOUCH_I2C_ADDR); } else { env_set("device-tree-overlay", "lvds-panel"); } } }   imx93_evk.c At the end, add this function to the previously mention, named as board_late_init, in the section CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG, like the following snipped from code:   int board_late_init(void) { #ifdef CONFIG_ENV_IS_IN_MMC board_late_mmc_env_init(); #endif env_set("sec_boot", "no"); #ifdef CONFIG_AHAB_BOOT env_set("sec_boot", "yes"); #endif #ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG env_set("board_name", "11X11_EVK"); env_set("board_rev", "iMX93"); detect_display_connected(); #endif return 0; }   imx93_evk.c Now, when it's starting u-boot after flashing, it will generate the environment variable as trigger if something it's connected with that i2c address, else it doesn't do anything. u-boot applying device tree overlay through event   As was explained in the section "How to apply device tree overlay", applying the device tree overlay automatically after configure the trigger it's easy, just adding an if/else case for this example, it can be more ways to applying it, even it's possible adding more of one device tree overlay, but in this example will load one.  Using u-boot command "test -e <environment variable>" it will detect if exist this environment variable, adding it to an if/else sentence it can create the event and applying the overlay if was detected or not, for this solution will be added this if/else as input if exists loadoverlay variable with the following structure:   u-boot=> if test -e ${device-tree-overlay}; then <case exists device-tree-overlay variable> else <case doesn't exists device-tree-overlay variable>; fi;   adding it to loadoverlay, it will be written like the following command:   u-boot=> setenv loadoverlay "if test -e ${device-tree-overlay}; then setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr ${fdt_addr} && fdt resize $\{fdt_buffer\}; fatload mmc ${mmcdev}:${mmcpart} $\{fdtovaddr\} imx93-11x11-evk-test-lvds-panel.dtbo; fdt apply $\{fdtovaddr\} ; else echo no overlay; fi;"   A no recommended method it's that it can be saved the environment, and changing mmcboot variable with the following command:   u-boot=> setenv mmcboot "run mmcargs; run loadfdt; run loadoverlay; run boot_os;"; saveenv;   The problem about just saving it, it still necessary compile u-boot to load auto-detection of LVDS panel and flashing, another way to add the event trigger, it's adding it to u-boot as initial environment variable, it can be added in the header file of imx93, it is located in the next path <u-boot path>/include/configs/imx93_evk.h, line number 60, it can be added with the same string but it's recommended follow the same structure, like the following definition:   /* Initial environment variables */ #define CFG_EXTRA_ENV_SETTINGS \ ... "loadoverlay=echo loading overlays from mmc ...; " \ "if test -e ${device-tree-overlay}; then " \ "setexpr fdtovaddr ${fdt_addr} + 0xF0000; " \ "setexpr fdt_buffer 16384; " \ "fdt addr ${fdt_addr} && fdt resize ${fdt_buffer}; " \ "fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} imx93-11x11-evk-test-lvds-panel.dtbo && fdt apply ${fdtovaddr}; " \ "else " \ "echo no overlay; " \ "fi;\0" \ ...   imx93_evk.h it also it's necessary to change mmcboot environment variable adding loadoverlay after executing loadfdt.    /* Initial environment variables */ #define CFG_EXTRA_ENV_SETTINGS \ .. "mmcboot=echo Booting from mmc ...; " \ "run mmcargs; " \ "if test ${sec_boot} = yes; then " \ "if run auth_os; then " \ "run run boot_os; " \ "else " \ "echo ERR: failed to authenticate; " \ "fi; " \ "else " \ "if test ${boot_fit} = yes || test ${boot_fit} = try; then " \ "bootm ${loadaddr}; " \ "else " \ "if run loadfdt; then " \ "run loadoverlay; " \ "run boot_os; " \ "else " \ "echo WARN: Cannot load the DT; " \ "fi; " \ "fi;" \ "fi;\0" \ ...   imx93_evk.h To build u-boot, copy the following commands in main path from u-boot   $ cd <u-boot path> $ make -j $(nproc --all) clean PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu- $ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=aarch64-linux-gnu- imx93_11x11_evk_defconfig $ make -j $(nproc --all) PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu-   generating the files u-boot.bin and u-boot-spl.bin located in <uboot-imx path>/ and <uboot-imx path>/spl Build imx-boot image using imx-mkimage   To build the binary necessary to flash to iMX 93 EVK it's necessary build a file named as flash.bin, it can building using the next repository using the branch used for this example:    $ git clone https://github.com/nxp-imx/imx-mkimage.git -b lf-6.6.3_1.0.0   to build imx-boot image it's necessary adding some files to the path <imx-mkimage path>/iMX93, including 2 generated by u-boot, u-boot.bin and u-boot-spl.bin, move these files to iMX93 directory.   $ cp <uboot-imx path>/u-boot.bin <uboot-imx path>/spl/u-boot-spl.bin <imx-mkimage path>/iMX93/   follow the steps from imx linux users guide section 4.5.13 and imx linux release notes section 1.2 to build flash.bin, as an example of compile, there's the steps to compile for imx93. Get mx93a1-ahab-container.img $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-sentinel-0.11.bin $ chmod +x firmware-sentinel-0.11.bin $ ./firmware-sentinel-0.11.bin $ cp firmware-sentinel-0.11/mx93a1-ahab-container.img <imx-mkimage path>/iMX93/​ Get lpddr4_imem_1d_v202201.bin, lpddr4_dmem_2d_v202201.bin, lpddr4_imem_1d_v202201.bin and lpddr4_imem_2d_v202201.bin $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.23.bin $ chmod +x firmware-imx-8.23.bin $ ./firmware-imx-8.23.bin $ cp firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_dmem_1d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_dmem_2d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_imem_1d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_imem_2d_v202201.bin <imx-mkimage path>/iMX93/​ Get bl31.bin $ git clone https://github.com/nxp-imx/imx-atf.git -b lf-6.6.3-1.0.0 $ cd imx-atf $ make -j $(nproc --all) PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu- $ cp <imx-atf path>/build/imx93/release/bl31.bin <imx-mkimage path>/iMX93​ Compile flash.bin from imx-mkimage $ cd <imx-mkimage path>/ $ make SOC=iMX9 REV=A1 flash_singleboot​ it will generate the binary flash.bin located in the path <imx-mkimage path>/iMX93/flash.bin. Flashing u-boot   Flashing just u-boot image using flash.bin, will be used uuu.exe, it can be downloaded from the his repositroy, try using the most recent version taged as "Latest"    https://github.com/nxp-imx/mfgtools/releases   make sure is using i.MX 93 EVK in boot mode download and connect it to your host from download USB port, using uuu.exe run the next code:   .\uuu.exe -b emmc .\flash.bin   or it can be flashed the full image with flash.bin binary.   .\uuu.exe -b emmc_all .\flash.bin ..\uuu\imx-image-full-imx93evk.wic   after that, starting be will using the created u-boot environment. Result   Inside u-boot, when it's connected the LVDS panel, it will create the variable named "device-tree-overlay" and will be charged automatically LVDS panel overlay, enabling it, if not it will working normally using DSI as output. Note: Ensure to have imx93-11x11-evk-test-lvds-panel.dtbo in memory. Reference   Device tree overlay: https://docs.kernel.org/devicetree/overlay-notes.html  
View full article
On this tutorial we will review the implementation of Flutter on the i.MX8MP using the Linux Desktop Image. Please find more information about Flutter using the following link: Flutter: Option to create GUIs for Embedded System... - NXP Community Requirements: Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors) NXP Desktop Image for i.MX 8M Plus (GitHub - nxp-imx/meta-nxp-desktop at lf-6.1.1-1.0.0-langdale) Note: This tutorial is based on the NXP Desktop Image with Yocto version 6.1.1 – Langdale. Steps: 1. First, run commands to update packages. $ sudo apt update $ sudo apt upgrade 2. Install Flutter for Linux using the following command. $ sudo snap install flutter --classic 3. Run the command to verify the correct installation. $ flutter doctor With this command you will find information about the installation. The important part for our purpose is the parameter "Linux toolchain - develop for Linux desktop". 4.png 4. Run the command “flutter create .” to create a flutter project, this framework will create different folders and files used to develop the application.  $ cd Documents $ mkdir flutter_hello $ cd flutter_hello $ flutter create .​ 5.png 5. Finally, you can run the “hello world” application using: $ flutter run 6.png 7.png Verify the program behavior incrementing the number displayed on the window.  
View full article
This document is about to build an image by Yocto , and it will disable a function that normal user can’t use command line of “ su ”.
View full article
Hello, on this post I will explain how to record separated audio channels using an 8MIC-RPI-MX8 Board. As background about how to setup the board to record and play audio using i.MX boards, I suggest you take a look on the next post: How to configure, record and play audio using an 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK. Linux Binary Demo Files - i.MX 8MMini EVK. 8MIC-RPI-MX8 Board. Serial console emulator (Tera Term, Putty, etc.). Headphones/speakers. Waveform Audio Format WAV, known for WAVE (Waveform Audio File Format), is a subset of Microsoft’s Resource Interchange File Format (RIFF) specification for storing digital audio files. This format does not apply compression to the information and stores the audio with different sampling rates and bitrates. WAV files are larger in size compared to other formats such as MP3 which uses compression to reduce the file size while maintaining a good audio quality but, there is always some lose on quality since audio information is too random to be compressed with conventional methods, the main advantage of this format is provide an audio file without losses that is also widely used on studio. This files starts with a file header with data chunks. A WAV file consists of two sub-chunks: fmt chunk: data format. data chunk: sample data. So, is structured by a metadata that is called WAV file header and the actual audio information. The header of a WAV (RIFF) file is 44 bytes long and has the following format: JorgeCas_0-1716227653935.png JorgeCas_1-1716227760727.png How to separate the channels? To separate each audio channel from the recording we need to use the next command that will record raw data of each channel. arecord -D plughw:<audio device> -c<number of chanels> -f <format> -r <sample rate> -d <duration of the recording> --separate-channels <output file name>.wav arecord -D plughw:2,0 -c8 -f s16_le -r 48000 -d 10 --separate-channels sample.wav This command will output raw data of recorded channels as is showed below. JorgeCas_2-1716227828320.png This raw data cannot be used as a “normal” .wav file because the header information is missing. It is possible to confirm it if import raw data to a DAW and play recorded samples: JorgeCas_3-1716227842722.png So, to use this information we need to create the header for each file using WAVE library on python. Here the script that I used: import wave import os name = input("Enter the name of the audio file: ") os.system("arecord -D plughw:2,0 -c8 -f s16_le -r 48000 -d 10 --separate-channels " + name + ".wav") for i in range (0,8): with open(name + ".wav." + str(i), "rb") as in_file: data = in_file.read() with wave.open(name + "_channel_" + str(i) +".wav", "wb") as out_file: out_file.setnchannels(1) out_file.setsampwidth(2) out_file.setframerate(48000) out_file.writeframesraw(data) os.system("mkdir output_files") os.system("mv " + name + "_channel_" + "* " + "output_files") os.system("rm " + name + ".wav.*") If we run the script, will generate a directory with the eight audio channels in .wav format. JorgeCas_4-1716227909413.png Now, we will be able to play each channel individually using an audio player. References IBM, Microsoft Corporation. (1991). Multimedia Programming Interface and Data Specifications 1.0. Microsoft Corporation. (1994). New Multimedia Data Types and Data Techniques. Standford University. (2024, January 30). Retrieved from WAVE PCM sound file format: http://hummer.stanford.edu/sig/doc/classes/SoundHeader/WaveFormat/
View full article
The user interface has limited the use of the tool GUI Guider. Getting an interaction only through a mouse or touchscreen can be enough for some use cases. However, sometimes the use case requires to go beyond its limitations. This video/appnote explores the possibility of integrating voice by creating a bridge between a speech recognition technology, such as VIT, and the interface creator GUI Guider. It uses a universal way to link all the voice recognition commands and a wakeword to any interaction created by GUI Guider. The following video shows the steps necessary to create that connection by creating the voice recognition using VIT voice commands and wakewords, create an interface of GUI Guider using a template, how to connect between them using the board i.MX 93 evk and testing it. For more information consult the following links AppNote HTML: https://docs.nxp.com/bundle/AN14270/page/topics/abstract.html?_gl=1*1glzg9k*_ga*NDczMzk4MDYuMTcxNjkyMDI0OA..*_ga_WM5LE0KMSH*MTcxNjkyMDI0OC4xLjEuMTcxNjkyMDcyMy4wLjAuMA AppNote PDF: https://www.nxp.com/docs/en/application-note/AN14270.pdf Associated File: AN14270SW  
View full article
-- DTS for gpio wakeup   // SPDX-License-Identifier: (GPL-2.0+ OR MIT) /*  * Copyright 2022 NXP  */   #include "imx93-11x11-evk.dts"   / {         gpio-keys {                 compatible = "gpio-keys";                 pinctrl-names = "default";                 pinctrl-0 = <&pinctrl_gpio_keys>;                   power {                   label = "GPIO Key Power";                   linux,code = <KEY_POWER>;                   gpios = <&gpio2 7 GPIO_ACTIVE_LOW>;                   wakeup-source;                   debounce-interval = <20>;                   interrupt-parent = <&gpio2>;                   interrupts = <7 IRQ_TYPE_LEVEL_LOW>;                 };         }; };   &iomuxc {         pinctrl_gpio_keys: gpio_keys_grp {                 fsl,pins = <                         MX93_PAD_GPIO_IO07__GPIO2_IO07  0x31e                 >;         }; }; -- testing the switch GPIO  First check if your gpio dts configuration to make it act as a switch works or not After executing the command - 'evtest /dev/input/event1' Trigger an interrupt by connecting GPIO2 7 to GND, as soon as you do that, you will receive Event logs such as below:- gauravsharma7_0-1716787221867.png This shows that your dts configuration for GPIO works.     -- Verify the interrupt     gauravsharma7_1-1716787221869.png     -- Go to sleep and then connect the GPIO to GND to trigger a wakeup, in the logs we see that kernel exits the suspend mode   gauravsharma7_2-1716787221871.png  
View full article
P3T1755DP is a ±0.5°C accurate temperature-to-digital converter with a -40 °C to +125 °C range. It uses an on-chip band gap temperature sensor and an A-to-D conversion technique with overtemperature detection. The temperature register always stores a 12-bit two's complement data, giving a temperature resolution of 0.0625 °C P3T1755DP which can be configured for different operation conditions: continuous conversion, one-shot mode, or shutdown mode.   The device has very good features but, unfortunately, is not supported by Linux yet!   The P31755 works very similarly to LM75, pct2075, and other compatibles.   We can add support to P3T1755 in the LM75.c program due to the process to communicate with the device is the same as LM75 and equivalents.   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.55-2.2.0/drivers/hwmon/lm75.c route: drivers/hwmon/lm75.c   The modifications that we have to do are the next:    1. We have to add the configurations to the kernel on the imx_v8_defconfig file CONFIG_SENSORS_ARM_SCMI=y CONFIG_SENSORS_ARM_SCPI=y CONFIG_SENSORS_FP9931=y +CONFIG_SENSORS_LM75=m +CONFIG_HWMON=y +CONFIG_I2C=y +CONFIG_REGMAP_I2C=y CONFIG_SENSORS_LM90=m CONFIG_SENSORS_PWM_FAN=m CONFIG_SENSORS_SL28CPLD=m    2. Add the part on the list of parts compatible with the driver LM75.c enum lm75_type { /* keep sorted in alphabetical order */ max6626, max31725, mcp980x, + p3t1755, pct2075, stds75, stlm75,   3. Add the configuration in the structure lm75_params device_params[]. .default_resolution = 9, .default_sample_time = MSEC_PER_SEC / 18, }, + [p3t1755] = { + .default_resolution = 12, + .default_sample_time = MSEC_PER_SEC / 10, + }, [pct2075] = { .default_resolution = 11, .default_sample_time = MSEC_PER_SEC / 10,   Notes: You can change the configuration of the device using .set_mask and .clear_mask, see more details on LM75.c lines 57 to 78   4. Add the ID to the list in the structure i2c_device_id lm75_ids and of_device_id __maybe_unused lm75_of_match    { "max31725", max31725, }, { "max31726", max31725, }, { "mcp980x", mcp980x, }, + { "p3t1755", p3t1755, }, { "pct2075", pct2075, }, { "stds75", stds75, }, { "stlm75", stlm75, },   + { + .compatible = "nxp,p3t1755", + .data = (void *)p3t1755 + },   5. In addition to all modifications, I modify the device tree of my iMX8MP-EVK to connect the Sensor in I2C3 of the board.  https://github.com/nxp-imx/linux-imx/blob/lf-6.1.55-2.2.0/arch/arm64/boot/dts/freescale/imx8mp-evk.dts   }; }; + + p3t1755: p3t1755@48 { + compatible = "nxp,p3t1755"; + reg = <0x48>; + }; + };   Connections: We will use the expansion connector of the iMX8MP-EVK and J9 of the P3T1755DP-ARD board.   P3T1755DP-ARD board Chavira_1-1714499607542.png   Chavira_2-1714499681249.png iMX8MP-EVK   P3T1755DP-ARD ----> iMX8MP-EVK J9              ---------->            J21 +3v3 (Pin 9) ---> +3v3 (Pin 1) GND(Pin 7) ---> GND (PIN 9) SCL (Pin 4) ---> SCL (Pin 5) SDA (Pin 3) ---> SDA (Pin 3) Chavira_3-1714500611037.jpeg Chavira_4-1714500618352.jpeg     Reading the Sensor We can read the sensor using the next commands:   Read Temperature: $ cat /sys/class/hwmon/hwmon1/temp1_input Reading maximum temperature: $ cat /sys/class/hwmon/hwmon1/temp1_max Reading hysteresis: $ cat /sys/class/hwmon/hwmon1/temp1_max_hyst Chavira_0-1714498794795.png   https://www.nxp.com/design/design-center/development-boards-and-designs/analog-toolbox/arduino-shields-solutions/p3t1755dp-arduino-shield-evaluation-board:P3T1755DP-ARD    
View full article
What is LGVL? LVGL is a graphics library to run on devices with limited resources. LVGL is fully open-source and has no external dependencies, works with any modern MCU or MPU, and can be used with any (RT)OS or bare metal setup. https://lvgl.io/   What is Framebuffer? The Linux framebuffer (fbdev) is a Linux subsystem used to show graphics on a display, typically manipulated on the system console   How to write on the frame buffer? The device is listed on de device list typically "fb0" on iMX. Chavira_0-1713985008756.png   1. Stop the window manager (Weston in our BSP) $ systemctl stop weston   2. Write random data on the frame buffer with the next command: $ cat /dev/urandom > /dev/fb0   You should see colored pixels on the screen Chavira_0-1714056022934.jpeg   3. Restart the window manager. $ systemctl start weston   Chavira_1-1713985008756.png   Cross-compiling the application   1. On the host computer we will clone the LGVL repo: $ git clone https://github.com/lvgl/lv_port_linux_frame_buffer.git -b release/v8.2 $ cd lv_port_linux_frame_buffer $ git submodule update --init --recursive 2. Configure the screen resolution, rotation, and the touch input.       2.1 The resolution is configured in lines 33 and 34 of the main.c disp_drv.hor_res = 1080; disp_drv.ver_res = 1920;           2.2 Rotation configured is on lines 32 and 57 of main.c. disp_drv.sw_rotate = 3; lv_disp_set_rotation(NULL, LV_DISP_ROT_270);     2.3 The touch input is configured on line 450 of lv_drv_conf.h # define EVDEV_NAME "/dev/input/event2"   Note: In my case is on /dev/input/event2 to check the inputs use the command "evtest" Chavira_2-1713985008757.png   3. Compile the application using the command "make"   Note: To compile the application on your host computer you have to set the environment.   4. Share the file called "demo" with your board and execute it on the board with the command $ ./demo   Note: You have to stop the weston service to run the application. Chavira_1-1714056439321.jpeg Chavira_2-1714056464298.jpeg   Chavira_3-1714056470761.jpeg Chavira_4-1714056477679.jpeg Chavira_0-1714147274371.jpeg   Notes: Tested on iMX8MN EVK with BSP 6.1.36 Works on Multimedia and Full image.
View full article
Sometime need standalone compile device tree. Only Linux headers and device tree directory are needed.         
View full article
This article is rather short that only mentions the script that is needed to make an iMX93EVK act as a USB mass storage device so that whenever you connect your iMX device to a windows/linux system via USB, it should get enumerated something like a usb drive.  The storage that is used in this example is mmc so the expectation is that you have inserted a mmc card in the slot. Below is the script:- #!/bin/sh   # This composite gadget include function: # - MASS STORAGE     # # Exit status is 0 for PASS, nonzero for FAIL # STATUS=0   # Check if there is udc available, if not, return fail UDC_DIR=/sys/class/udc if test "$(ls -A "$UDC_DIR")"; then echo "The available udc:" for entry in "$UDC_DIR"/* do echo "$entry" done else STATUS=1 echo "No udc available!" exit $STATUS; fi   id=1; udc_name=ci_hdrc.0 #back_file=/dev/mmcblk1 back_file=/tmp/lun0.img   mkdir /sys/kernel/config/usb_gadget/g$id cd /sys/kernel/config/usb_gadget/g$id   # Use NXP VID, i.MX8QXP PID echo 0x1fc9 > idVendor echo 0x12cf > idProduct   mkdir strings/0x409 echo 123456ABCDEF > strings/0x409/serialnumber echo NXP > strings/0x409/manufacturer echo "NXP iMX USB Composite Gadget" > strings/0x409/product   mkdir configs/c.1 mkdir configs/c.1/strings/0x409   echo 5 > configs/c.1/MaxPower echo 0xc0 > configs/c.1/bmAttributes   mkdir functions/mass_storage.1 echo $back_file > functions/mass_storage.1/lun.0/file ln -s functions/mass_storage.1 configs/c.1/   echo $udc_name > UDC First execute the script. After that insert the g_mass_storage module in the kernel by executing :- modprobe g_mass_storage file=/dev/mmcblk1 removable=1 In the dmesg output, you will see something like below:-   gauravsharma7_0-1714041731840.png After that you can connect a C type USB cable to the USB1 port of imx93evk and the other end to any USB ports of a laptop. The moment it is connected, you would be able to see a USB drive similar to what you get when we connect a pen-drive. 
View full article
Application Note AN13872  Enabling SWUpdate on i.MX 6ULL, i.MX 8M Mini, and i.MX 93 is available on www.nxp.com    SWUpdate: Embedded Systems become more and more complex. Software for Embedded Systems have new features and fixes can be updated in a reliable way. Most of time, we need OTA(Over-The-Air) to upgrade the system. Like Android has its own update system. Linux also need an update system. SWUpdate project is thought to help to update an embedded system from a storage media or from network. However, it should be mainly considered as a framework, where further protocols or installers (in SWUpdate they are called handlers) can be easily added to the application. Mongoose daemon mode: Mongoose is a daemon mode of SWUpdate that provides a web server, web interface and web application. Mongoose is running on the target board(i.MX8MM EVK/i.MX8QXP MEK).Using Web browser to access it. Untitle11d.png   Suricatta daemon mode: Suricatta regularly polls a remote server for updates, downloads, and installs them. Thereafter, it reboots the system and reports the update status to the server. The screenshot is SWUpdate scuricatta working with hawkbit server. Untitleddddd.png          
View full article