NFC Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Knowledge Base

Discussions

Sort by:
SPIM module is one of the master interfaces provided by PN7462 , which is a 32-bit ARM Cortex-M0-based NFC microcontroller, and users may use this interface to connect with up to two SPI slave devices. The NFC reader library provides SPIM driver code in phHal/phhalSPIM, and users may directly use the following APIs in their application to implement simple SPI transaction, just like what is done  in the demo of "PN7462AU_ex_phExHif". While this demo has limitation with some SPI nor flash devices, which need a write-read operation in one NSS session, for example, the SPI nor flash device on OM27462 as below: Please note to solder R202 and connect it to 3V3 to make sure nHold pin has pull-up out of POR. The following is one of the command sets this device supports: This command contains 1 write(9F) followed by 3 read operations in one NSS session, but if you implement it with phhalSPIM_Transmit() and phhalSPIM_Receive() as below: status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 2, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, data_length, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);" You will have the following result: expected: NSS   \__________________________/ MOSI     CMD A7-A0 MISO                            DATA       actual:                         NSS   \____________||______________/ MOSI     CMD A7-A0 MISO                           DATA so the pulse between the write and read is the problem, and here we have to handle the NSS line manually, with the help of NSS_VAL and NSS_CONTROL bits in SPIM_CONFIG_REG. so the code should be like this:   Assert NSS   status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 2, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, data_length, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);"   De-assert NSS The NSS line assert and de-assert function can be implemented with register bit level APIs, just like below:             PH_REG_SET_BIT(SPIM_CONFIG_REG, NSS_VAL);//de-assert NSS             PH_REG_SET_BIT(SPIM_CONFIG_REG, NSS_CTRL);             PH_REG_CLEAR_BIT(SPIM_CONFIG_REG, NSS_VAL);//assert NSS Please also include the following header files in your application code. #include "ph_Reg.h" #include "PN7462AU/PN7462AU_spim.h" Please notice that phhalSPIM_Transmit() and phhalSPIM_Receive() are Rom based function, which clear NSS_CTRL bit by default. We can not change ROM API's behave but fortunately we have phhalSPIM_TransmitContinue() and phhalSPIM_ReceiveContinue() instead. so the final solution will be like below: Assert NSS   status = phhalSPIM_TransmitContinue(1, cmd_buf);    status = phhalSPIM_ReceiveContinue(3, dst);   De-assert NSS This doesn't mean phhalSPIM_Transmit() and phhalSPIM_Receive() are useless, because they can also help up to configure the SPI master interface, if you don't want to use register bit level API to initial the SPIM module manually. Please note to use 1 byte for write/read length to make these two functions work properly. so the whole pseudo code is like below: phhalSPIM_Init(PH_HW_SPIM_TIMEOUT) ; phhalSPIM_Configure(PH_HW_SPIM_SLAVE, PH_HW_SPIM_MSB_FIRST,                 \                                     PH_HW_SPIM_MODE, PH_HW_SPIM_BAUDRATE,  \                                     PH_HW_SPIM_NSSPULSE, PH_HW_SPIM_NSSPOL) ; status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);" Assert NSS   status = phhalSPIM_TransmitContinue(1, cmd_buf);    status = phhalSPIM_ReceiveContinue(3, dst);   De-assert NSS The following steps show how to create a new project based on NFC reader library, please refer to https://www.nxp.com/docs/en/user-guide/UM10883.pdf  on how to import the NFC reader library. 1. Create a new project after importing the NFC reader library. 2. if you installed PN7462 support package, you will see this: 3. add a link to NFC reader lib: 4. add path and enable NFC reader lib in the project: 5. delete cr_startup.c and create the main code as well as the header file: 6. Build result: 7.Debug result: To fetch the ready demo, please submit a private ticket via the guide of https://community.nxp.com/docs/DOC-329745 . Hope that helps, Best regards, Kan
View full article
This post contains step by step guide of how to use NTAG I²C plus with i.MX RT MCUs. The goal of this post is to enable developers to start developing their NFC Applications using NTAG I²C plus and i.MX RT MCUs quickly and easily. Attached with this post are two ready to use packages: ‘evkbimxrt1060_ntagI2C’ is to be used with MIMXRT1060-EVK and NTAG I²C plus kit for Arduino pinout. ‘evkbimxrt1050_ntagI2C’ is to be used with MIMXRT1050-EVK and NTAG I²C plus kit for Arduino pinout. Both packages contain the same example code but are configured for the two different boards. The example code demonstrates the following basic operations: Reading the EEPROM of NTAG I²C plus. Writing NTAG messages to NTAG I²C plus. Reading SRAM of NTAG I²C plus. Writing to SRAM of NTAG I²C plus. Using Field detect pin as interrupt to turn on an LED when an RF field is detected by the NTAG I²C board. The document has been structured as follows: NTAG I²C plus kit for Arduino pinout The NTAG I²C plus Arduino kit consist of two PCBs stacked together: The upper PCB is the antenna board with the connected tag The lower PCB is an interface adaptor board to the Arduino pinout This kit can be used to connect and evaluate the NTAG I²C plus  into many popular MCUs with Arduino compliant headers, for example:  Kinetis (e.g. KW41Z, i.MX (e.g. UDOO Neo, i.MX 6UL, i.MX 6 ULL, i.MX 7D), LPC MCUs (e.g. LPCXpresso MAX, V2 and V3 boards) and i.MX RT boards (e.g. i.MX RT1050, i.MX RT1060) The kit support package includes several software examples. The OM29110ARD is a generic interface board which offers support for connection to any PCB implementing Arduino connectors. It exposes: 3.3V and 5V power supply pins. I2C, SPI and UART host interfaces. Generic GPIOs (e.g. to be used for field detect, interrupts, reset pins or others) As such, it allows the NTAG I²C plus to be plugged into Arduino devices seamlessly. Hardware Requirements EVKB-IMXRT1050 board or EVKB-IMXRT1060 board. NTAG I²C plus kit for Arduino pinout (OM23221ARD) Cables: Micro USB cable 6 jumper wires Male to Female (Only required if using EVKB-IMXRT1050 board) Using NTAG I²C plus kit for Arduino pinout with EVKB-IMXRT1060 Hardware Connections The hardware connections are simple. Both the EVKB-IMXRT1060 board and OM23221ARD (NTAG I²C plus) board have Arduino interface. So simply connect both as shown in figure:  Running the Demo Follow the below mentioned steps to run the demo: Download the ‘evkbimxrt1060_ntagI2C’ package which you will find attached to this post.  Drag and drop the downloaded package to your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE, click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started click on the run icon to run the code:                                 Note:  If this is your first time using IMXRT1060EVK board, it is recommended to follow the getting started guide first ( i.MX RT1060 Evaluation Kit | NXP  ) To see the output, you need to have a terminal application installed (like Tera term or PuTTY). The output looks like this:                                                    Using NTAG I²C plus kit for Arduino pinout with EVKB-IMXRT1050 Hardware Connections In case of EVKB-IMXRT1050, the I2C pins on the Arduino interface’s J24 pin 9 and 10 are only connected to the i.MX RT slave I²C port, not to a master I²C port. So, we cannot just plug in the NTAG I²C plus kit, instead we need to connect two boards with the help of jumper wires. The connections required are show in figure below.                                Running the Demo Download the ‘evkbimxrt1050_ntagI2C’ package which you will find attached to this post. Drag and drop the downloaded package to your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE, click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started click on the run icon to run the code:                                Note:  If this is your first time using IMXRT1050EVK board, it is recommended to follow the getting started guide first ( i.MX RT1050 Evaluation Kit | NXP  ) To see the output, you need to have a terminal application installed (like Tera term or PuTTY). The output looks like this:                                            Porting the Package to any other i.MX RT Boards    If you want to use NTAG I²C plus with i.MX RT boards other than the i.MX RT1050 or the i.MX RT1060, then you’ve       to port the example package. This is fairly straightforward and the procedure is described below: Import the ‘hello world’ project from the SDK of the board to which you want to port the package. (SDKs for every board are freely available for download from the MCUXpresso SDK Builder website).We will modify this ‘hello world’ project adding code from attached packages, to make it work on the desired board.                                     Copy the following folders from the attached ‘evkbimxrt1060_ntagI2C’ or ‘evkbimxrt1050_ntagI2C’ package to the ‘hello world’ project imported in step 1:                               Copy the two files to the ‘drivers’ folder of ‘hello world’ project: Delete the ‘hello_world.c’ file from the source folder: Now copy the following preprocessor micros from ‘evkbimxrt1060_ntagI2C’ or ‘evkbimxrt1050_ntagI2C’ package to ‘hello world’ project:      Preprocessor settings can be found by right clicking Project-Properties>C++Build > Settings  Now we need to change the project configuration:        a.  Add the newly copied folders to source location; Right click on Project->Properties and add the following        folders:    b.  Include paths to the added libraries in the project. These can be copied from the from ‘evkbimxrt1060_ntagI2C’ or ‘evkbimxrt1050_ntagI2C’ package. Open project->properties and copy the following in the respective places as shown in the images:  Change pin configurations according to the board pins you are using:             a. For changing field detect pin, the code can be found in the source file:                   b. For I2C instance, the lines of code are in app_ntag->app_ntag.h:              c. These pins also need to be initialized which can be done through the pin initialization tool of MCUXpresso or code can be added to the ‘board.c’ file in ‘board’ folder. Once these changes are done, porting is complete. Build the project, it should build without any errors. Available resources BLE pairing with NFC on KW41 and NTAG I²C plus source code www.nxp.com/downloads/en/snippets-boot-code-headers-monitors/SW4223.zip NTAG I²C plus kit for Arduino pinout www.nxp.com/demoboard/OM23221ARD    
View full article
This document provides a step by step guide of how to use the CLRC663 plus with i.MX RT1050. For this purpose, we need to port the NFC Reader Library to i.MX RT1050.  There are two zip files attached to this document: 1. "NFCReaderLibrary_IMXRT1050_Porting Guide +DAL_IMXRT1050_BLE-NFC-V2.zip" : This folder is pre-configured for those who want to use BLE-NFC-v2 board with i.MX RT1050. 2. "NFCReaderLibrary_IMXRT1050_Porting Guide +DAL_IMXRT1050_CLEV6630B.zip" : This folder is pre-configured for those who want to use CLEV6630B board with i.MX RT1050. A video describing how to use i.MX RT1050 with CLRC663 Plus Family is available by clicking this link (Using i.MX RT 1050 with CLRC663 plus family |NXP ) as well. 
View full article
Hello NFC community, MIFARE® Ultralight-based tickets offer an ideal solution for low-cost, high-volume applications such as public transport, loyalty cards and event ticketing. They serve as a perfect contactless replacement for magnetic stripe, barcode, or QR-code systems. The introduction of the contactless MIFARE Ultralight® ICs for limited-use applications can lead to reduced system installation and maintenance costs. As you may know the MIFARE family has the Ultralight C tag which is a contactless IC supporting 3DES cryptography is mostly used in limited use applications such smart ticketing, this tag complies with ISO 14443-3 type A and it is defined as type 2 tag, in this document I want to show you the procedure to change the default key to a custom key also to protect certain areas in the tag so the authentication is needed to perform a read or write operation. --------------------------------------------------------------------------------------------------- For this document I used : MFEV710: PEGODA Contactless Smart Card Reader RFIDDiscover Software Lite version  Full Version Available in Docstore Mifare Ultralight c --------------------------------------------------------------------------------------------------- Information Old Key : 49454D4B41455242214E4143554F5946 New Key : 88776655443322117766554433221199 Data sheet ---------------------------------------------------------------------------------------------------- First we start with the procedure to activate the tag and the anticollision procedure explained in the ISO/IEC 14443-3. Command Direction    ">" this direction is command send from PCD (Reader) to PICC(Ultralight c)    "<" this direction is command send from PICC (Ultralight c) to PCD (Reader)    "=" Prepare this command before sending Command   Data message REQA =  Request Command, Type A >  26 ATQA = Answer To Request, Type A  <  4400 SEL + NVB = SEL (Select code for cascade level ) 93, NVB (Number of Valid bits) 20 >  9320 ANTICOLLISION START <  8804598356   >  93708804598356 SAK (Select Acknowledge) = indicates additional cascade level <  x04   >  9520   <  E1ED2580A9   >  9570E1ED2580A9   <  x00 UID = 045983E1ED2580  ** the following procedure is explained in section 7.5.5 from the datasheet** Command   Data message Authenticate Part 1  (command 1A) >  1A00   <  AFA1ED1D682E5101422CC7 Authenticate Part 2 (command AF) >  AF2970D895F186D0302970D895F186D030188AAF4DAF68C5B9   <  006BD027CEC3E04EBC6919 [AUTHENTICATED] Then according to  section 7.5.7 of the datasheet the sections  where the 3DES key are saved are the 2C (Page 44) to the 2F (Page 47). We proceed to  write our new key using the A2 (WRITE command) Command   Data message DATA = byte 07,06,05,04 = 11223344 WRITE to page 44 (2C) >  A22C11223344 Positive acknowledge (ACK) <  0A DATA = byte 03,02,01,00 = 55667788 WRITE to page 45 (2D) >  A22D55667788  Positive acknowledge (ACK) <  0A DATA = byte 0F,0E,0D,0C = 99112233 WRITE to page 46 (2E) >  A22E99112233  Positive acknowledge (ACK) <  0A DATA = byte 0B,0A,09,08 = 44556677 WRITE to page 47 (2F) >  A22F44556677  Positive acknowledge (ACK) <  0A [RESET FIELD] [Authenticate with new key] Command   Data message Authenticate Part 1  (command 1A >  1A00   <  AFFAE2EFF17FAAD69862E7 Authenticate Part 2 (command AF) >  AFFD5794F2D4EA1B19FD5794F2D4EA1B196CF420CD4D9E8104   <  0030922228601939B8FA18 [AUTENTICATED WITH NEW KEY] we proceed to define from which sector the authentication is needed in order to read or write, to do this we use a write command to the AUTH0 (AUTH0 defines the page address from which the authentication is required. Valid address values for byte AUTH0 are from 03h to 30h.) the AUTH0 is located on the section 2A please check table 5 from #datasheet. **for this example we will define that from page 6 (06) we will need authentication to perform a read or write operation** Command   Data message WRITE command (A2) to AUTH0 (2A) from page 6 (06) >  A22A06000000 Positive acknowledge (ACK) <  0A Now the Read capabilities from page 06  require an Authentication in order to be read or written. Hope you find this document useful to get a better understanding of the behavior of the Ultralight C and how its security features can help you in your applications. Have a great day! BR Jonathan
View full article
Environments & Devices --Hardware 1、PN7462 DEMO Board(PNEV7642B) --Software 1、Ubuntu 16.04 desktop 2、Test tools ---libusb ---pcsc-lite ---ccid driver ---opensc          Before testing, please install above test tools to Ubuntu 16.04 according to document on the link https://community.nxp.com/docs/DOC-334952 !          Then follow steps below to begin testing PN7462 DEMO board by above test tools. 1、Update firmware of PN7462 DEMO board          Please update firmware of PN7462 DEMO board according to UM10915.pdf, then test it on windows, ensuring PN7462 DEMO board can normally work at CCID protocol on window platform. 2、Connecting PN7462 DEMO Board to PC USB via USB OTG Cable.          On PENV7462B side, X3 connector should be used for USB OTG cable. 3、Using lsusb to list USB devices weidong@ubuntu:~$ lsusb Bus 002 Device 002: ID 0e0f:0003 VMware, Inc. Virtual Mouse Bus 002 Device 003: ID 0e0f:0002 VMware, Inc. Virtual USB Hub Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub Bus 002 Device 004: ID 0e0f:0008 VMware, Inc. Bus 002 Device 005: ID 1fc9:0117 NXP Semiconductors          Last line is PN7472 DEMO board. 4、Open 2 terminals at the same time on Ubuntu desktop (1) One terminal is used to run “pcsc” command weidong@ubuntu:~$ sudo /usr/local/sbin/pcscd -adf [sudo] password for weidong: 00000000 pcscdaemon.c:345:main() pcscd set to foreground with debug send to stdout 00012288 configfile.l:361:DBGetReaderList() Parsing conf file: /usr/local/etc/reader.conf.d 00000037 pcscdaemon.c:658:main() pcsc-lite 1.8.22 daemon ready. 00023126 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000101 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000113 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0003, path: /dev/bus/usb/002/002 00000112 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000160 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0002, path: /dev/bus/usb/002/003 00000152 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0008, path: /dev/bus/usb/002/004 00000115 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0008, path: /dev/bus/usb/002/004 00000165 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0002, path: /dev/bus/usb/002/003 00000263 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0002, path: /dev/bus/usb/001/001 ^V56546837 hotplug_libudev.c:651:HPEstablishUSBNotifications() USB Device add 00000101 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1FC9, PID: 0x0117, path: /dev/bus/usb/002/006 00000007 hotplug_libudev.c:436:HPAddDevice() Adding USB device: PN7462 USB Reader 00000045 readerfactory.c:1074:RFInitializeReader() Attempting startup of PN7462 USB Reader (1.00) 00 00 using /usr/local/lib/pcsc/drivers/ifd-ccid.bundle/Contents/Linux/libccid.so 00127887 readerfactory.c:949:RFBindFunctions() Loading IFD Handler 3.0 00000236 ifdhandler.c:1965:init_driver() Driver version: 1.4.27 00000477 ifdhandler.c:1982:init_driver() LogLevel: 0x0003 00000004 ifdhandler.c:1993:init_driver() DriverOptions: 0x0000 00000165 ifdhandler.c:111:CreateChannelByNameOrChannel() Lun: 0, device: usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 00000021 ccid_usb.c:302:OpenUSBByName() Using: /usr/local/lib/pcsc/drivers/ifd-ccid.bundle/Contents/Info.plist 00000727 ccid_usb.c:320:OpenUSBByName() ifdManufacturerString: Ludovic Rousseau ([email protected]) 00000016 ccid_usb.c:321:OpenUSBByName() ifdProductString: Generic CCID driver 00000004 ccid_usb.c:322:OpenUSBByName() Copyright: This driver is protected by terms of the GNU Lesser General Public License version 2.1, or (at your option) any later version. 00000433 ccid_usb.c:656:OpenUSBByName() Found Vendor/Product: 1FC9/0117 (PN7462 USB Reader) 00000005 ccid_usb.c:658:OpenUSBByName() Using USB bus/device: 2/6 00000021 ccid_usb.c:717:OpenUSBByName() bNumDataRatesSupported is 0 00128471 ifdhandler.c:382:IFDHGetCapabilities() tag: 0xFB3, usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 (lun: 0) 00000027 readerfactory.c:396:RFAddReader() Using the reader polling thread 00004709 ifdhandler.c:382:IFDHGetCapabilities() tag: 0xFAE, usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 (lun: 0) 00000023 ifdhandler.c:477:IFDHGetCapabilities() Reader supports 1 slot(s) (2)The other terminal is used to run “"testpcsc " in pcsc-lite/src source code weidong@ubuntu:~/ccid/pcsc-lite-1.8.22/src$ ./testpcsc   MUSCLE PC/SC Lite unitary test Program   THIS PROGRAM IS NOT DESIGNED AS A TESTING TOOL FOR END USERS! Do NOT use it unless you really know what you do.   Testing SCardEstablishContext        : Command successful. Testing SCardIsValidContext   : Command successful. Testing SCardIsValidContext   : Invalid handle. (don't panic) Testing SCardListReaderGroups      : Command successful. Group 01: SCard$DefaultReaders Testing SCardFreeMemory               : Command successful. Testing SCardListReaders        : Command successful. Testing SCardListReaders        : Command successful. Reader 01: PN7462 USB Reader (1.00) 00 00 Waiting for card insertion        :          2 screenshots for above 2 terminals: 5、Test cards (All cards are contactless) (1) MIFARE Plus x 4K card Re move it: (2) MIFARE Nano card          Note: testpcsc should be run again. Remove it: (3) MIFARE EV1 card Remove it: 6、Using Opensc-tool to Test cards            Open a new terminal for running the command, please! (1)No cards (2) MIFARE Plus x 4K card (close to antenna , then run opensc-tool) (3) MIFARE Nano card (4) MIFARE EV1 card    TIC Weidong Sun 2018-07-09
View full article
As NFC reader library 5.12 also supports PN5180, switching the NFC frontend from CLRC663 to PN5180 is quite easy based on previous porting. The porting also includes the hardware settings and software modification. Hardware Setup for porting: a) Remove resistors on PNEV5180B to disconnect the onboard lpc1769 from PN5180, following steps on page 16 of https://www.nxp.com/docs/en/application-note/AN11908.pdf  b) Connect LPCXpresso board for LPC11U37 with PNEV5180 as below: Software Modification for porting: 1. Make a copy of Board_Lpc11u37Rc663.h , and change its name to "Board_Lpc11u37Pn5180.h", and import it into the DAL/boards folder. 2.Change the source code in the header file as below: 3. Add two more pins' definition and configuration for BUSY and DWL pins of PN5180, and new configuration for reset pin. and modify the reset logic: 4.Change the IRQ interrupt trigger type to rising edge. 5.Include this header file in BoardSelection.h 6.Add this new configuration in ph_NxpBuild_App.h 7.Add this new configuration in phApp_Init.h 8.Add this new configuration in ph_NxpBuild_Platform.h 9.Add this new configuration in Settings. 10.Building result: Testing result:
View full article
Hello NFC Community! This document demonstrates that multiple records can be also read from a Tag with TagXplorer. Please follow the steps below. Let's begin... Please make sure that you have written more than on record with NXP TagWriter app. For a more detailed explanation on this, please refer to the following document: Writing multiple NDEF text records with TagWrite app  The app can be found and downloaded from the Play Store: NFC TagWriter by NXP - Apps on Google Play  -> Connect the reader in TagXplorer -> Place the card on the reader and press Connect Tag -> Check for NDEF (1) and then, read NDEF (2). The Text Records can be visualized in the NDEF Payload Info below: I hope this is of great help! Ivan R.
View full article
Hello NFC Community, This document describes how to write multiple NDEF Text Record by making use of NFC TagWriter app by NXP. First of all, download the TagWriter app from the Play Store: NFC TagWriter by NXP - Apps on Google Play  1) Once downloaded, go to the Write tags section. 2) In this case, a NDEF text record will be written. 3) Write a text message in the TextBox and press the Save & Write Button. 4) Now, press the ADD MORE RECORD Button so that another record can be added to the content to be written in the tag. 5) Select Plain Text again.   6) Same, procedure as in 3. 7) Finally, Tap the card and press the DONE Button. I hope this is of great help! Ivan R.
View full article
Based on NFC reader library porting guide for LPC11u37h(Ver 5.12) ,We have a partial ported NFC reader library like below: Now, it is time to port other demos in this project. You may choose any demo, but here NfcrdlibEx2_AdvancedDiscoveryLoop is selected. and similar with before, the first step is creating a new build configuration: then in the project references, choose the LPCopen library for LPC11u37 instead. Change the MCU settings: Change the build settings: Change FreeRTOS portable to cortex M0: Search "PHDRIVER_LPC1769RC663_BOARD" in the source code of "NfcrdlibEx2_AdvancedDiscoveryLoop" project, and you may simply replace it with "PHDRIVER_LPC11U37RC663_BOARD", and there are only two places needs to be fixed. Search "PHDRIVER_LPC1769" in the source code of "NfcrdlibEx2_AdvancedDiscoveryLoop" project, and you may simply replace it with "PHDRIVER_LPC11U37". Most changes are in phApp_Init.c. Also please don't forget to enable optimization for size. Building result: Demo testing result:
View full article
The latest NFC reader library supports lpc1769 which is a cortex M3 controller with LPCopen lib supports, so in theory , it should supports other controllers supported by LPCopen, but we have to test this, so we choose , for example, lpc11u37, a cortex M0 based controller for this porting. Platform for this porting: LPC11u37h-Xpresso Rev A: CLRC663 plus based CLEV663B Blueboard 3.0. Please refer to Prepare CLEV663B board for NFC reader library porting  for details. They are connected via LPCXpresso ports. Now we may start the porting, the IDE we use in this porting is MCUXpresso 10.1.1 1. Download and import the latest NFC reader library for CLEV6630B, as it supports CLRC663 plus. For how to import the project, please refer to https://www.nxp.com/docs/en/application-note/AN11211.pdf . 2. Download LPCopen for LPC11u37h and import it as well. 3. Now we may choose some demo in the NFC reader library, for example, the NfcrdlibEx1_BasicDiscoveryLoop, and create new build configuration for lpc11u37h. 4.Select the correct MCU 5.Modify build settings Here we find LPC1769RC663 is defined, so we have to find what is related with this definition in the code and change it/them. Fortunately they are not too many. you may find they are just related with board header file including or something like that, so it is not difficult to modify them. 6. Add new header file for the new board definition 7. add the new board definition 8. As we now use LPCopen lib for LPC11u37h instead, so we have to change the including path. As LPC11u37h is cortex M3 based, so we have to setup FreeRTOS for M0 support: and add the source code for building: 9.Change the link libraries and including path 10.Set the correct ref projects to use LPCopen for LPC11u37h. 11. Some changes in LPCopen library: 1)enable semihosting debug 2) add startup source code for the demo, this C file can be reused/imported from the some lpcopen project. 12. After the above steps, we still have to change the source code in DAL: You know , due to different version of LPCopen library,  some function definition might be changed, and different LPCXpresso boards has different pin connection to the LPCXpresso ports, so it is recommended checking the board schematics and the examples in lpcopen project , find the proper function calls to implement the source codes in the DAL folder. When you finished , the porting is done. 13. As the final image size is greater than 128K, we have enable optimization for size. 14.Demo test ok. Now , we know lpc11u37 can be supported by the latest NFC reader library, so the porting should also be applied for other Cortex M0 controllers, and it is recommended the controller with large internal flash size, better greater than 128K, but anyway, in this porting, I didn't enable the size optimization for LPCopen library, so there might be possibility to have a smaller size image at last...
View full article
The latest NFC reader library for CLRC663 just supports LPCXpresso1769 and FRDM-K82 boards, so when customers want to porting the library to other host controller, they have to make a custom board at first, or use OM26630FDK and make a little hardware modification by following the steps described in https://www.nxp.com/docs/en/training-reference-material/NFC-READER-K64F.pdf?fsrch=1&sr=3&pageNum=1 to connect the frontend board with host controller board, but today we will discuss an alternative way. The CLEV663B Blueboard is a pure NFC frontend board, and it supports connecting with LPCXpresso board not limited with LPC1769, the main difference with OM26630FDK is the reader IC, which is CLRC663 not CLRC663 plus, but fortunately they are pin to pin compatible, so we may replace it with CLRC663 plus, and use that board for porting purpose. Before: After: please forgive my poor soldering skill... With this new board and LPC1769 Xpresso board, you may run the latest 5.12 NFC reader library, for example, the NfcrdlibEx1_BasicDiscoveryLoop demo. but you might have the following issue: This is due to ver 5.12 use another set of IO pins to connect with the reader IC, modify pin definitions in Board_Lpc1769Rc663.h can fix this issue. The final result is as below: Please note, it is recommended using NFC reader library ver 4.03 to test the hardware including CLEV663B and LPC1769Xpresso before replacing with CLRC663 plus, and you know, CLEV663B Blueboard is just optimized for CLRC663 , so the matching circuit is not the best for CLRC663 plus, it is just good enough to run the demo, so that we may know if the porting is successful, but if you want to have the best performance with CLRC663 plus, you have to redo the antenna tuning, and you may refer to https://community.nxp.com/docs/DOC-335545 for more details on that topic.
View full article
https://community.nxp.com/docs/DOC-340389 
View full article
https://community.nxp.com/docs/DOC-340244 
View full article
Introduction I am trying to make one page that contain all the useful information about NFC Antenna Design. I will keep update and add the information to this page when I found something useful.   Training First of all, there are 6 webinars about NFC Antenna Design. It is a good training before to start your antenna design for NFC. Training & Events | NXP  (Search "Antenna design")   Application Notes AN11740 : PN5180 Antenna design guide AN11706 : PN7462AU Antenna design guide AN11019 : CLRC663, MFRC630, MFRC631, SLRC610 Antenna Design Guide AN11755 : PN7150 Antenna Design and Matching Guide AN11564 : PN7120 Antenna Design and Matching Guide AN11741 : How to design an antenna with DPC AN11535 : Measurement and tuning of a NFC and Reader IC antenna with a MiniVNA Tools NFC Antenna Design Hub
View full article
This porting guide is for FRDM-K82F, and it can also be used for any other platform supported by KSDK 2.2. The released NXPNCI-KDS_Example_KSDK2.2 is based on FRDM-K64F, so before porting, we need to configure and download KSDK 2.2 for FRDM-K82F. Please make sure you have selected Kinetis Design Studio before downloading. After downloading, extract the package to some folder like below: and change PROJECT_KSDK_PATH to this folder: Change project settings as below: Remove all files in the folder of drivers, and import new source files as below: and similar procedure for "startup" folder and "utilities" folder: Replace the source files in board folder with the files from some ksdk demo like hello_world: FRDM-K82F uses PTC3 for NCI_IRQ pin, PTC9 for NCI_VEN pin, and PTA1 and PTA2(I2C3) as the I2C interface. so add definition in board.c and modify BOARD_InitPins() as below: Change linker settings: -Build -Debug settings -Test Result:
View full article
When the PNEV5180B cannot work with the Cockpit, you can re-program the firmware to the board. Below are the steps show you how to program the firmware to the board again. 1. If you don't have the MCUXpresso, please download the MCUXpresso from the NXP web first. MCUXpresso Software and Tools for ARM® Cortex®-M cores|NXP  2. Install the MCUXpresso IDE v10.0.0 to your PC. 3. Configure PNEV5180 board to use external power supply J101, and then power up the board. There is 10-pin ARM Cortex header on the PNEV5180B , connect  LPC-Link2 debug probe to it (J7) by using flat cable and also connect debug probe to the PC host over USB mini cable - both jumper on debug probe are open (JP1 and JP2). 4. Start MCUXpresso IDE and import any LPC1769 project from filesystem. For example: SW3522.zip. This is important to give programmer right definitions. SW3522 can be downloaded from here : NFC Reader Library v4.040.05.011646 R1 for PNEV5180B including all software examples  5. After import the SW3522, you can try to build the example and run the example on your board. e.g. NfcrdlibEx1_BasicDiscoveryLoop. Click LinkServer GUI Flash programmer icon on the main menu. When started programmer tool will check if LPC-Link2 debug probe is attached. 6. Browse to the C:\nxp\NxpNfcCockpit_v4.0.0.0\firmware\Secondary_PN5180\BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin. Set the Base address to 0x0. 7. Flash Write Done. 8. After this, reset the board and to start NFCCockpit v4.0.0.0. The board will be recognized. P.S. The board is connected to PC via VCOM. If there is any driver issue, please try to re-install the VCOM driver and restart the PC. The VCOM driver can be found in the C:\nxp\NxpNfcCockpit_v4.0.0.0\VCOM.
View full article
Recently, some NFC customer want to use CCID driver to communcate with NFC reader on Linux platform, but they encontered some errors during installing CCID driver for linux. I tested it and installed it to ubuntu 16.04 LTS successfully. Let me share complete steps with those users who want to devevlope NFC applications based on linux platform. If we want to use CCID driver on linux, we need to install these packages: --libusb --pcsc-lite --ccid driver --opensc Before starting to install above packages, probably we need to install necessary dependency packages: # sudo apt-get install git-core gnupg flex bison gperf build-essential zip curl zlib1g-dev libc6-dev lib32ncurses5-dev # sudo apt-get install x11proto-core-dev libx11-dev lib32readline-gplv2-dev lib32z1-dev # sudo apt-get install libgl1-mesa-dev mingw32 tofrodos python-markdown libxml2-utils xsltproc uuid-dev:i386 liblzo2-dev:i386 # sudo apt-get install gcc-multilib g++-multilib # sudo apt-get install subversion # sudo apt-get install openssh-server openssh-client # sudo apt-get install libudev-dev # sudo apt-get install openssl  # sudo apt-get install libssl-dev 1. libus installation (1) Download it from : libusb File name is libusb-1.0.9.tar.bz2 (2)Decompressing it # tar jxvf libusb-1.0.9.tar.bz2 # cd ~/ccid/libusb-1.0.9 # ./configure # make # sudo make install (3) test it # lsusb 2. pcsc-lite installation (1) Downloading pcsc-lite package: MUSCLE  Filename is : pcsc-lite-1.8.22.tar.bz2  (2) Decompressing it # tar jxvf pcsc-lite-1.8.22.tar.bz2  (3) compiling it # cd pcsc-lite-1.8.22 # ./configure # make ... # sudo make install ... 3. CCID driver installation (1) Downloading it from : Alioth: Muscle PCSC lite: Project Filelist  file name is : ccid-1.4.27.tar.bz2 (2) Decompressing it # tar jxvf ccid-1.4.27.tar.bz2 (3) Compiling it # cd ccid-1.4.27 # ./configure After runing configure command, information below will be displayed: ... # make ... # sudo make install ... 4. opensc installation (1) Downloading it from : OpenSC - Browse /OpenSC/opensc-0.16.0 at SourceForge.net  File name is : opensc-0.16.0.tar.gz (2) Decompressing it # tar zxvf cd opensc-0.16.0.tar.gz (3)Compiling it # cd opensc-0.16.0 # ./configure --enable-openssl --enable-pcsc # make # sudo make install Up to now, above 4 software packages have been installed to ubuntu 16.04 LTS. (4) Add library file path    open /etc/ld.so.conf , and add one line at the end of the file :  include /usr/local/lib , save and exit, run 'sudo ldconfig -v' to update it. # sudo gedit /etc/ld.so.conf  # sudo sudo ldconfig -v 5. Add Vendor ID & Product ID to info.plist We should add Vendor ID & Product ID of NFC reader to info.plist, the file is at the path : /usr/local/lib/pcsc/drivers/ifd-ccid.bundle/Contents/. For example , PN7462's vendor ID is 0x1FC9, and product ID is 0x0117. [Note] This requires Firmware on NFC reader board should support USB CCID, if not, customer should replace it with firmware that supports USB CCID, for the purpose, customer can refer to UM10915.pdf(http://www.nxp.com/docs/en/user-guide/UM10915.pdf ) to do it. TIC team Weidong Sun
View full article
The latest NXP-NCI example is rev 1.6, and when you run this demo with the lpc11xx board, for example, lpc1115 rev A, and the OM5577, you may meet the following issue: The problem is due to two aspects: one is hardware and the other is software. For hardware solution, besides following what is described in AN11658 section 2.4 LPC11xx, you have to do one more thing: a) The I2C lines are not pulled-up: LPC11xx doesn't offer internal pull-up setting of the I2C lines so external pull-up resistors must be added. For software solution, the function of Sleep()( in tool.c) was optimized too much, and it didn't meet the timing requirement of OM5577, so we should let the IDE ignore it. The solution I use is as below: __attribute__((optimize("O0"))) void my_func() { blah } You may check the attachment for details. The result is shown as below: Original Attachment has been moved to: tool.c.zip
View full article
The NXP-NCI example is based on NXP-NCI lib and LPCopen lib, and due to the good consistency, the porting is mainly focus on LPCopen lib switching.   Software setup download lpcopen package via http://www.nxp.com/assets/downloads/data/en/software/lpcopen_3_01_lpcxpresso_nxp_lpcxpresso_11u68.zip  download SW3241 via https://www.nxp.com/webapp/Download?colCode=SW3241&amp;appType=license&amp;location=null&fsrch=1&sr=3&pageNum=1&Parent_n…  import NXP-NCI_LPC11Uxx_example by LPCXpresso v8.1.4.   LPCopen porting remove *.h and *.c in the folder of LPC11Uxx/inc and LPC11Uxx/src. 2.import header files and c files from lpc_chip_11u6x/inc and lpc_chip_11u6x/src to LPC11Uxx/inc and LPC11Uxx/src 3. repeat step 2 , import source files and header files from lpc_board_nxp_lpcxpresso_11u68/inc and lpc_board_nxp_lpcxpresso_11u68/src to Drivers/inc and Drivers/src. 4.Change MCU settings 5.Change project settings. 6.compiling error fixes: 6.1 solution: replace with i2c_11u6x.h 6.2 solution: 6.3 solution: create a template project for LPC11U6x and import the source file of "cr_startup_lpc11u6x.c"   Porting Result   This porting guide is for LPC11U68 Xpresso v2 Rev C, and can also be used a reference when you try to port NXP-NCI examples to other lpcxpresso boards.   Please kindly refer to the attachment for details. Original Attachment has been moved to: NXP-NCI_LPC11Uxx_example.zip
View full article
The NXPNCI-KDS_Example for the PN7120/PN7150 Arduino interface boards available in NXP webpage at the time of publishing this document includes a project compatible with KSDK v2.0 for FRDM-K64F platform. With the latest KSDK v2.1 some changes in the drivers along with the later FreeRTOS v9.0.0 make the build process fail when following the instructions in the application note AN11845 NXP NCI KDS Example due to incompatibilities. Meanwhile until the project in NXP webpage is updated there is a temporary project attached to this document fixed to work with KSDK v2.1. The steps to build this project are the same as explained in the appnote, summarized below: - Download and install KSDK v2.1 for FRDM-K64F using MCUXpresso SDK online builder: Welcome to MCUXpresso | MCUXpresso Config Tools  Create a new workspace in KDS IDE. Import the "NXPNCI-KDS_Example_KSDK2.1" project from the archive file. Update the PROJECT_KSDK_PATH build variable according to the installation path of KSDK v2.1. Build the project. For more details please refer to the application note AN11845. Regards! Jorge Gonzalez
View full article