1790004_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1790004_en-US

1790004_en-US

All Example S32K312 DS3.5 RTD-3.0.0

 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE Micro
* Target: internal_FLASH
********************************************************************************

For S32K312, please use this correct clock HSE to AIPS clock should be ½.
Please make these changes in the below all example code clock setting.
HSE clock to 60 MHZ.

Dinesh_Guleria_0-1717149049774.png



S32K312 PIT BTCU ADC-1 BCTU_ADC_DATA_REG DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-ADC-1-BCTU-ADC-DATA-REG-DM...

Example S32K312 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-...

S32K312 UART Transmit & Receive Using DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-DMA...

S32K312 EIRQ Interrupt :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-EIRQ-Interrupt-DS3-5-RTD300/ta-p/17...

S32K312 SPI Transmit & Receive Using DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SPI-Transmit-amp-Receive-Using-DMA-...

Example S32K31 SPI multiple packet Transmit & Receive : solution for DMA Cache issue :-
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K31-SPI-multiple-packet-Transmit-amp-Rec...

Example S32K312 SPI Transmit & Receive Using Polling DS3.5 RTD300 :--
Example S32K312 SPI Transmit & Receive Using Polling DS3.5 RTD300 - NXP Community

Example S32K312 SPI Transmit & Receive Using Interrupt DS3.5 RTD300 :--
Example S32K312 SPI Transmit & Receive Using Interrupt DS3.5 RTD300 - NXP Community

S32K312 CAN Transmit & Receive Using Polling mode :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-Poll...

S32K312 CAN Transmit & Receive Using MB & FIFO DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-a...

S32K312 ADC :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-ADC-DS3-5-RTD300/ta-p/1789282

S32K312 Switch Debouncing :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Switch-Debouncing-DS3-5-RTD300/ta-p...

S32K312 UART Freemaster :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Freemaster-DS3-5-RTD300/ta-p/1...

S32K312 PIT BTCU parallel ADC FIFO DMA  :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-...

S32K312 placing variables in DTCM & code in ITCM  :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-placing-variables-in-DCTM-amp-code-...

Example S32K312 Standby mode & Standby RAM and PAD keeping DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Standby-mode-amp-Standby-RAM-and-PA...

Example S32K312 SWT DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SWT-DS3-5-RTD300/ta-p/1800559

Example S32K312 Printf Semihosting DS3.5 RTD300 :---
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Printf-Semihosting-DS3-5-RTD300/ta-...

Example S32K312 I2C Transmit & Receive Using DMA DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-I2C-Transmit-amp-Receive-Using-DMA-...

Example S32K312 HARDFAULT Handling Interrupt DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-...

Example S32K312 Bootloader to Application Jump DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Bootloader-to-Application-Jump-DS3-...

Example S32K312 PIT timer Toggle LED DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-timer-Toggle-LED-DS3-5-RTD300/t...

Example S32K312 HARDFAULT Interrupt Handling using a script DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Interrupt-Handling-using-...

Example S32K312 UART Transmit & Receive Using Interrupt DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-Int...

Example S32K312 CAN Transmit & Receive Using MB Interrupt DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-I...

Example S32K312 STANDBY wake up using CAN-0-RX and GPIO Switch DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-CAN-0-RX-and-...


Example S32K312 STANDBY wake up using RTC DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-RTC-DS3-5-RTD...

S32K312 : ADC Clock selection :--
https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-ADC-Clock-selection/ta-p/1997759

Example IP S32K312 PWM ICU using EMIOS Custom IRQ DS3.5 RTD300 :--
Example IP S32K312 PWM ICU using EMIOS DS3.5 RTD300 - NXP Community

Example IP S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 :--
Example IP S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 - NXP Community

Example IP S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 :--
Example IP S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 - NXP Community

Example S32K312 Continuous SPI Transmit & Receive Using DMA DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Continuous-SPI-Transmit-amp-Receive...

S32K312 : HSE Demo project :--
https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-HSE-Demo-project/ta-p/2112562

S32K312 : FS26 Watchdog trigger using the SBC_FS26 CDD :--
https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-FS26-Watchdog-trigger-using-the-SBC-FS26-CD...

タグ(1)
評価なし
バージョン履歴
最終更新日:
2 週間前
更新者: