Example S32K312 HARDFAULT Interrupt Handling using a script DS3.5 RTD300

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K312 HARDFAULT Interrupt Handling using a script DS3.5 RTD300

Example S32K312 HARDFAULT Interrupt Handling using a script DS3.5 RTD300

*******************************************************************************

The purpose of this demo application is to present a usage of the
Hardfault handling using a script for the S32K3xx MCU.

------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

  • Change the attached script name from --> gdbinit.txt --> to --> .gdbinit
  • This script applicable for CORTEX-M7 call stack view.
  • Select the script at this location :--
    Window --> Prefrences--> c/c++ --> Debug --> GDB
  • Whenever the hardfault comes go to the Debugger console and enter word armex press enter. This will display the callstack at the time hardfault occur, and LR address contain the address where the HARDFAULT occur.
  • Enter address in Disassembly window And press enter, this will take you to code location where the hardfault occur.
  • Then you can review your code setting or code usage why this hardfault is coming.

Dinesh_Guleria_1-1709194211986.pngDinesh_Guleria_1-1709194211986.png

 

Dinesh_Guleria_0-1709193938046.pngDinesh_Guleria_0-1709193938046.png

 

Attachments
No ratings
Version history
Last update:
‎02-29-2024 01:29 AM
Updated by: