Example S32K312 CAN Transmit & Receive Using Polling mode DS3.5 RTD300

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K312 CAN Transmit & Receive Using Polling mode DS3.5 RTD300

Example S32K312 CAN Transmit & Receive Using Polling mode DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 FlexCAN IP Driver for the S32K3xx MCU.

 The example uses FLEXCAN-0 for transmit & receive Tusing following Message buffer :--
#define RX_MB_IDX 1U
#define TX_MB_IDX 0U
.

BAUDRATE : 500 KBPS

 ------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************


Dinesh_Guleria_0-1705387677471.pngDinesh_Guleria_0-1705387677471.png

 

 

Attachments
No ratings
Version history
Last update:
‎01-15-2024 11:56 PM
Updated by: