i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
The document descript how to use the win32diskimager to create bootable sdcard.  How to resize sdcard mirror rootfs partition. Ex: fsl-image-validation-imx-imx6qpdlsolox.sdcard
View full article
This document provides steps to perform the system upgrade/OTA update for Android on i.MX platforms. Compile the Android images and generate an OTA Package: source build/envsetup.sh lunch sabresd_6dq-userdebug make -j4 make otapackage You can find your OTA package in the below path: ls out/target/product/sabresd_6dq/sabresd_6dq-ota-<xxx>.zip Copy the above OTA zip package to the device in sdcard using adb push adb push out/target/product/sabresd_6dq/sabresd_6dq-ota-<xxx>.zip /sdcard Move the package from sdcard to the location: /cache/update.zip Make the directory and perform the below steps on the device: mkdir -p /cache/recovery touch /cache/recovery/command echo "--update_package=/cache/update.zip" > /cache/recovery/command reboot recovery The recovery automatically applies the command and installs this update package. Note: In this document, the setup is for the i.MX6Q SABRESD Board. So, PathName and OTA package name subject to change based on target device compilation.
View full article
i.mx8M evk board has HW decoder and SW encoder, this document introduce how to use HW decoder and SW encoder the bsp is the latest version L4.14.78, the environment is : $ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland $ bitbake fsl-image-validation-imx   For the 4.14.78, we don’t use mfgtool anymore, customer can use uuu.exe to program the image to the board, the uuu.exe can be found from https://github.com/NXPmicro/mfgtools/releases Here we use emmc as media, I attached the kerel_emmc.uuu for reference Open the cmd.exe, then use the command “uuu.exe kernel_emmc.uuu” to download the image to the emmc on the board as the picture shows When the board boot up, don’t forget to change the image and fdt_file as you want, for example, I use Image-imx8mqevk.bin as image name  and Image-fsl-imx8mq-evk.dtb as my fdt file, you can choose different image and fdt file as uuu file mentions. 1) Decoding   For play the video, we can use three solution to support this a) gplay-1.0 test.mp4 b) gst-launch-1.0 playbin uri=file:///mnt/sdcard/test.mp4 c) gst-launch-1.0 filesrc location=test.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! autovideosink For play the two different video to the different display, current imx8M evk board supports dual hdmi output, in the uboot command: setenv fdt_file Image-fsl-imx8mq-evk-dual-display.dtb saveenv Use the command as below:    gst-launch-1.0 playbin uri=file:///test1.mp4 playbin uri=file:///test2.mp4 video-sink="glimagesink display-master=false display-slave=true" 2) Encoding Because imx8M evk don’t have hardware encoding, so we need to add the SW plugins in the bsp   a)add the commands as below in the /build/conf/local.conf "CORE_IMAGE-EXTRA_INSTALL += "gstreamer1.0-plugins-ugly-meta packagegroup-fsl-gsstreamer1.0-commercial gst-ffmpeg" LICENSE_FLAGS_WHITELIST = "commercial""        b)Create the new txt file and add “PACKAGECONFIG_mx8mq = "x264"”in the file        c)Rename the file as 0-plugins-ugly_%.bbappend and put this file under /sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer        d)Build the image you want, then download the new rootfs file in the board, use the command “gst-inspect-1.0 | grep x264”
View full article
This documents describes how to add the NFC support to i.MX8M mini evk running Yocto. Hardware setup: The i.MX8M mini evk (see i.MX 8M Mini Evaluation Kit | NXP) featuring Raspberry Pi compliant connector, the OM5578/RPI PN7150 demo kit can be used to perform this porting (see NFC Development Kits for Arduino and more|NXP). However a small modification must be done because some of the signals required by PN7150 are not mapped to i.MX8M mini expansion connector pins. OM5578 IRQ signal must be mapped to Raspberry Pi connector pin #19 and OM5578 IRQ signal must be mapped to Raspberry Pi connector pin #21. See below a picture of the modification: Then, the two boards can fit together as shown in the picture below: Quick start using demo image: The demo image including support for PN7150, is based on i.MX Linux 4.14.78_1.0.0 BSP software release (see i.MX Software | NXP). Related documentation can be downloaded from here: https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS. Just flash the demo image (downloaded from here: https://www.nxp.com/lgfiles/updates/NFC/LINUX_L4-14-78_IMAGE_MX8MMEVK.zip) following guidelines from i.MX_Linux_User's_Guide document (part of L4.14.78_1.0.0_LINUX Documentation package mentioned above). Then in a terminal you can run the demo application included in the image executing the command:    # nfcDemoApp poll Approaching the NFC tag, provided as reference in the OM5578 demo kit, to the NFC Antenna will trigger such display: Adding PN7150 support to imx-linux-sumo release: Pre-condition is to have L4.14.78_1.0.0 release installed and already built as described in i.MX Yocto Project User's Guide (part of L4.14.78_1.0.0_LINUX Documentation package mentioned above) :     $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-sumo -m imx-4.14.78-1.0.0_ga.xml     $ repo sync     $ MACHINE=imx8mmevk DISTRO=fsl-imx-xwayland source fsl-setup-release.sh -b build_dir     $ bitbake fsl-image-validation-imx Then to add PN7150 support to your imx-linux-sumo environment, follow below step by step guidelines: In the sources directory, download the meta-nxp-nfc layer from https://github.com/NXPNFCLinux/meta-nxp-nfc     $ git clone https://github.com/NXPNFCLinux/meta-nxp-nfc.git  Define hardware connection between CPU and PN7150 in device-tree adding the following lines to file build_dir/tmp/work-shared/imx8mmevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dts: @@ -227,6 +227,8 @@                         fsl,pins = <                                 MX8MM_IOMUXC_I2C3_SCL_I2C3_SCL                  0x400001c3                                 MX8MM_IOMUXC_I2C3_SDA_I2C3_SDA                  0x400001c3 +                               MX8MM_IOMUXC_ECSPI2_MOSI_GPIO5_IO11             0x41 +                               MX8MM_IOMUXC_ECSPI2_MISO_GPIO5_IO12             0x41                         >;                 };   @@ -747,6 +749,13 @@         pinctrl-0 = <&pinctrl_i2c3>;         status = "okay";   +       pn54x: pn54x@28 { +               compatible ="nxp,pn547"; +               reg = <0x28>; +               interrupt-gpios = <&gpio5 11 0>; +               enable-gpios = <&gpio5 12 0>; +       }; +         pca6416: gpio@20 {                 compatible = "ti,tca6416";                 reg = <0x20>; Add the meta-nxp-nfc layer to the build definition updating file build_dir/conf/bblayers.conf with: BBLAYERS += " ${BSPDIR}/sources/meta-nxp-nfc" Add the meta-nxp-nfc layer components to the image definition updating file build_dir/conf/local.conf with: IMAGE_INSTALL_append = " kernel-module-nxp-pn5xx nxp-nfc-bin " Re-build the linux kernel:     $ bitbake -f -c compile linux-imx && bitbake -f -c deploy linux-imx Build meta-nxp-nfc layer:     $ bitbake nxp-nfc Re-build the complete image to include the modifications:     $ bitbake fsl-image-validation-imx Then you can flash the updated image to your i.MX8M mini evk and run the demo application as described in above "Quick start using demo image" chapter. Reference: This porting have been done (demo image and instructions) following guidelines provided in AN11679_PN71xx_Linux_Software_Stack_Integration_Guidelines document.
View full article
UPDATE: Note that this document describes eIQ Machine Learning Software for the NXP L4.14 BSP release. Beginning with the L4.19 BSP, eIQ Software is pre-integrated in the BSP release and this document is no longer necessary or being maintained. For more information on eIQ Software in these releases (L4.19, L5.4, etc), please refer to the "NXP eIQ Machine Learning" chapter in the Linux User Guide for that specific release.  Original Post: eIQ Machine Learning Software for iMX Linux 4.14.y kernel series is available now. The NXP eIQ™ Machine Learning Software Development Environment enables the use of ML algorithms on NXP MCUs, i.MX RT crossover processors, and i.MX family SoCs. eIQ software includes inference engines, neural network compilers, and optimized libraries and leverages open source technologies. eIQ is fully integrated into our MCUXpresso SDK and Yocto development environments, allowing you to develop complete system-level applications with ease. Source download, build and installation Please refer to document NXP eIQ(TM) Machine Learning Enablement (UM11226.pdf) for detailed instructions on how to download, build and install eIQ software on your platform. Sample applications To help get you started right away we've posted numerous howtos and sample applications right here in the community. Please refer to eIQ Sample Apps - Overview. Supported platforms eIQ Machine learning software for i.MX Linux 4.14.y supports the L4.14.78-1.0.0 and L4.14.98-2.0.0 GA releases running on i.MX 8 Series Applications Processors. For more information on artificial intelligence, machine learning and eIQ Software please visit AI & Machine Learning | NXP.
View full article
Introduction The Intel® Neural Compute Stick 2 (Intel® NCS 2) is Intel’s newest deep learning inference development kit. Packed in an affordable USB-stick form factor, the Intel® NCS 2 is powered by latest VPU (vision processing unit) – the Intel® Movidius™ Myriad X, which includes an on-chip neural network accelerator called the Neural Compute Engine. With 16 SHAVE cores and a dedicated hardware neural network accelerator, the NCS 2 offers up to 8x performance improvement+ over the previous generation. Ref: https://software.intel.com/en-us/articles/run-intel-openvino-models-on-intel-neural-compute-stick-2   The NCS 2 officially supported hardware platform is x86 PC and Raspberry Pi. In this guide, we will introduce how to implement in i.MX8MQ. Please see attached guide for more details.
View full article
ESAI module in i.MX6D/I.MX6D/I.MX6DL/I.MX6S supports several RESET funtions: Reset ESAI Core, Reset both Transmitter and Receiver, Reset Transmitter individually, Reset Receiver individually, Reset Transmitter FIFO and Reset Receiver FIFO. Below is a simple diagram for these RESET functions, which shows reset object and related register configurations. 1.Reset ESAI Core After setting ESAI_ECT ERST bit to be 1, ESAI core and configuration registers will be reset, but Transmitter and Recevier FIFOs can't be reset by the operation. 2. Reset both Transmitter and Receiver After setting ESAI_PCRC & ESAI_PRRC to be 0x000, Transmitter and Receiver can both be reset, The RESET is also called "Personal Reset" in it's reference manual. About PCRC & PRRC bits functionality, we can see the table: From the table, ESAI_PCRC=0x000 and ESAI_PRRC=0x000 will make ESAI disconnet external ESAI pins, and ESAI's Tranmitter and Receiver can't communicate with external audio codec.  See ESAI_PCRC and ESAI_PRRC register below: ---ESAI_PCRC register ---ESAI_PRRC register There are 12 bits in each register to contorl "DISCONNECTION" OR "CONNECTION" with ESAI pins. So for normal operations of ESAI, these 2 registers can't be changed. 3.Reset Transmitter & Receiver individually By setting ESAI_TCR[TPR]=1, Transmitter can be reset individually, and not affect Receiver. By setting ESAI_RCR[RPR]=1, Receiver can be reset individually, and not affect Transmitter . In reference manual, the reset is called "personal reset / individual reset", actually they means the same thing: --Reset Transmitter individually. --Reset Receiver individually. 4.Reset Transmitter FIFO and Reset Receiver FIFO ---By setting ESAI_TFCR[TFR]=1, Tranmitter FIFIO can be reset. ---By setting ESAI_RFCR[RFR]=1, Receiver FIFO can be reset. The Reset requires ESAI is operational, which means at least one pin is defined as an ESAI pin. NXP TIC team Weidong Sun
View full article
目录 1 i.MX8Mmini 板级开发包镜像结构 ............................... 2 2 创建 i.MX8Mmini Linux 4.14.78_ga 板级开发包编译环境 3 2.1 下载板级开发包 ...................................................... 3 2.2 创建yocto编译环境: ................................................ 4 2.3 编译sdk及安装 ........................................................ 7 2.4 独立编译 ................................................................. 8 3 DDR配置,测试与输出 ............................................ 13 4 i.MX8Mmini ATF ...................................................... 15 5 FSL Uboot SPL 定制 ............................................... 17 5.1 SPL的编译............................................................ 17 5.2 SPL的启动流程 .................................................... 26 5.3 SPL的定制............................................................ 33 6 FSL Uboot 定制 ....................................................... 39 6.1 FDT支持 ............................................................... 40 6.2 DM(driver model)支持 .......................................... 45 6.3 Uboot目录 结构 .................................................... 59 6.4 Uboot编译 ............................................................ 61 6.5 Uboot初始化流程 .................................................. 62 6.6 uboot 定制 ............................................................ 72 6.7 uboot debug信息 .................................................. 78
View full article
This document is aimed to introduce seamless switch on rear view camera function in android P9 auto, and this can also be referenced for sharing dpu(display process unit) between A core and m4 core on imx8qxp/qm platform. OS: Android p9 auto beta. (linux needs some modifies). SDK_2.5.1_MEK-MIMX8QX for m4 core. Hardware platform: imx8qxp/qm mek board IT6263 lvds to hdmi cable. max9286 deserializer board. ov16035 camera. Hardware block:     Imx8qxp dpu block, for imx8qm there are two dpus:     Android/Linux and M4 shared dpu path:     The switch function is done by framegen0 unit in dpu, framegen unit can select 7 modes: primary src only second src only primary on second second on primary .....etc. for more details, please refer to the kernel codes at include/video/dpu.h, fgdm_t type. Seamless switch booting flow: Patches contain three main parts: Linux kernel: remove init or configure codes of dpu units and lvds used by m4 core, add ui ready rpmsg pipe. M4 code: modify dpu pipes, add ui ready rpmsg handle. AOSP init.rc scripts: add sending ui ready message scripts.
View full article
Descriptions on the issue: running “uuu uuu-android-mx8mq-evk-emmc.lst” No any problem, downloading images is OK. running “uuu_imx_android_flash.bat -f imx8mq -a -e” Below lines will be showed on windows console: flash the file of u-boot-imx8mq.imx to the partition of bootloader0 <waiting for any devices>             Then downloading operation stopped. ------------------------------------------------------------------------                 In order to help uses save development time, I tested above 2 commands for downloading images on windows 7 64bit and windows 10 64bit respectively.                 Below is detailed steps for the operation: Hardware Preparations (1) Switch SW802 on i.MX8MQ EMEK, set 1-4 off, 2-3 on i.MX8MQ is at usb serial download mode. (2) Connecting J1701 to PC USB by a USB OTG cable. (3) Connecting J901(usb type c) to PC USB by a USB 3.0 cable. (4) Plugging [email protected] adapter into Power Jack (J902) (5) Power on I.MX8MQ board via SW701 Switch Software Preparations (1) Related windows drivers for i.MX8MQ MEK                 Windows 7 64bit or windows 10 64bit will find new devices and begin to search and install corresponding drivers, like below:                 Probably windows 10 64bit can’t automatically install CP2105 driver from official website of manufacture: https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers                 Then installed it manually. (2) Power off i.MX8MQ MEK (3) Installing winusb driver by zadig                 According to method described in uuu.pdf, download zadig tool from https://zadig.akeo.ie/, and install it to windows 7 64bit . [Note] windows 10 64bit doesn’t need to install winusb driver. Press “Install WCID Driver” Button (4) Downloading Android SDK Manager Download SDK Manager from : http://visualgdb.com/android/install_redir?item=SDK After downloading it, decompress it, and run SDK Manager application: Press OK. Then press “Close” Close SDK Manager Installation Guide . Find the directory of SDK Manager installation, and enter into “platform-tools”, like below: D:\i.MX8-Projects\IMX8MQ-MEK-windows-drivers\android-sdk_r24.4.1-windows\android-sdk-windows\platform-tools Copy items in blue rectangle to C:\windows\system Copy items in red rectangle to C:\windows\system32     Beginning to download android images to I.MX8MQ MEK via UUU Tool (1) Downloading android DEMO images for i.MX8MQ MEK https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK?tab=Design_Tools_Tab After downloading it, decompress it to a directory.  Like below: (2) Downloading UUU Tool https://github.com/NXPmicro/mfgtools/releases After downloading uuu.exe,  copy it to the directory of android 9.0 demo image , see above. (3) Run command “uuu_imx_android_flash.bat -f imx8mq -a -e” ----Power on i.MX8MQ MEK. ----open a command line window ---open Hyper terminal ( set it 115200 bps) ---run “uuu_imx_android_flash.bat -f imx8mq -a -e”           For windows 10 64bit, downloading images will be done without any errors.    But for windows 7 64bit, downloading images will stop at “ waiting for any devices”.    It means Android ADB driver will be needed. Follow the steps below to solve the problem. Right button, click “update driver” Close it.           Then downloading operations will be automatically continued. OK, done. NXP TIC team Weidong Sun 02-25-2019
View full article
Many times I came across one issue while using Redlib in MXUXpresso IDE project. I like to provide some guidance here to match the proper solution that can help others. Problem Statement : printf or sprintf doesn't print anything or printing random characters while using Redlib library. Reason : When you are creating your project you may ask to choose the c/c++ library setting to select either of the c libray provided by IDE in Advanced project setting wizard. If you have not checked the option "Redlib: Use floating point version of printf" (which will use the floating-point variant of printf) have tried to print the floating point value, You will end up with the problem mentioned above. Solution : You need to enable the floating support by modifying some preprocessor directives in "Defined symbols (-D)" wizard of your project. Path :  Your Project > properties > C/C++ Build > Setiings > Tool Settings > MCU C Compiler > Preprocessor. These are: PRINTF_FLOAT_ENABLE - keep the directive value to "1" SCANF_FLOAT_ENABLE - keep the directive value to "1" CR_INTEGER_PRINTF - Undefine/Remove this directive Click on Apply and close. That is it. Now you will have your expected prints for floating point values in your debugger console.
View full article
This is a series of documents that intend to help you grasp he concept of the System Controller Unit (SCU) / System Controller Firmware (SCFW).    Getting started Power management service  Resource management service Pad configuration service Timer service Miscellaneous service   Other Useful resources: https://community.nxp.com/docs/DOC-344684 (2019) i.MX 8 System Controller Unit and System Controller Firmware Overview (2018) Clusters & Infotainment: Introduction to the i.MX 8 System Controller Unit (2017 Slightly outdated, for correct boot sequence go to Chapter 5 System Boot of the Reference Manual) System Controller Firmware command line utility for QNX and Linux You can get the latest System Controller Firmware Porting kit from the i.MX Software and development webpage: The porting kit contains documentation and allows you to build the SCFW from source and do modifications to the board dependent parts: The API documents explain the System Controller Firmware API syntax and it has a section for introduction and general overview of the system. The port document contains information on what each board component function does and the overall process of porting the SCFW.
View full article
This documents describes how to add the NFC support to i.MX8M mini evk running Android Pie. Hardware setup: The i.MX8M mini evk (see i.MX 8M Mini Evaluation Kit | NXP) featuring Raspberry Pi compliant connector, the OM5578/RPI PN7150 demo kit can be used to perform this porting (see NFC Development Kits for Arduino and more|NXP). However a small modification must be done because some of the signals required by PN7150 are not mapped to i.MX8M mini expansion connector pins. OM5578 IRQ signal must be mapped to Raspberry Pi connector pin #19 and OM5578 VEN signal must be mapped to Raspberry Pi connector pin #21. See below a picture of the modification: Then, the two boards can fit together as shown in the picture below: Quick start using demo image: The demo image including support for PN7150, is based on Android P9.0.0 Pie (P9.0.0_1.0.0, 4.14 kernel) i.MX software release (see i.MX Software | NXP). Related documentation can be downloaded from here: https://www.nxp.com/docs/en/supporting-information/android_p9.0.0_1.0.0-ga_docs.zip. Just flash the demo image (downloaded from here:https://www.nxp.com/lgfiles/updates/NFC/ANDROID_P9-0-0_PN7150_IMAGE_8MMEVK.zip) following guidelines from i.MX_Android_Quick_Start document (part of Android P9.0.0_1.0.0 Documentation package mentioned above). The NFC support is then included in the device settings, as shown in below screenshot of the device: Approaching the NFC tag, provided as reference in the OM5578 demo kit, to the NFC Antenna will trigger a sound notification: Unfortunately the Android demo image doesn't embed a web browser, so it won't be automatically open when the NFC tag content (an URL to the demo kit web page) is read. Otherwise (if a web browser is installed) you could see such page opening on the device: Adding PN7150 support to imx-android-pie release: If you wish to add PN7150 support to your imx-android-pie environment, just apply the patches (imx-p9.0.0_1.0.0-ga_pn7150_patches.tar.gz file attached) from the ${MY_ANDROID} source code root folder (refer to i.MX_Android_User_Guide document part of Android P9.0.0_1.0.0 Documentation package mentioned above).  $ patch -p1 -d device/fsl/ <device_fsl.patch  $ patch -p1 -d packages/apps/Nfc <packages_apps_Nfc.patch  $ patch -p1 -d hardware/nxp/nfc <hardware_nxp_nfc.patch  $ patch -p1 -d vendor/nxp <vendor_nxp.patch  $ patch -p1 -d vendor/nxp-opensource/kernel_imx/ <vendor_nxp-opensource_kernel_imx.patch When building, the PN7150 support will then be included to the android image, as shown in the demo image described above. Reference: This porting have been done (demo image and patches creation) following guidelines provided in AN11690_NXP-NCI_Android_Porting_Guidelines document.
View full article
i.mx8x启动代码定制文档   目录 1    i.MX8X 板级开发包镜像结构... 2 2    创建 i.MX8QXP Linux 4.14.78_ga 板级开发包编译环境... 2 2.1  下载板级开发包... 2 2.2  创建yocto编译环境: 3 3    i.MX8X SC firmware. 11 3.1  SC firmware 目录结构... 11 3.2  SC firmware 启动流程... 12 3.3  SC firmware定制... 12 4    i.MX8X ATF. 18 5    FSL Uboot 定制... 20 5.1  FDT支持... 21 5.2  DM(driver model)支持... 27 5.3  Uboot目录 结构... 40 5.4  Uboot编译... 42 5.5  Uboot初始化流程... 43 5.6  uboot 定制... 53 5.7  uboot debug信息... 60
View full article
We are pleased to announce that Pins Tool for i.MX Applications Processors v5 is now available.   The Pins Tool for i.MX Applications Processors is used for pin routing configuration, validation and code generation, including pin functional/electrical properties, power rails, run-time configurations. Features Desktop application Muxing and pin configuration with consistency checking Multicore support Localized for English and Simplified Chinese Mostly Connected: On-Demand device data download Integrates with any compiler and IDE Supports English and Chinese (simplified) languages, based on locale settings. Please refer to user manual for details. ANSI-C initialization code Graphical processor package view Multiple configuration blocks/functions Easy-to-use device configuration Selection of Pins and Peripherals Package with IP blocks Routed pins with electrical characteristics Registers with configured and reset values Power Groups with assigned voltage levels Source code for C/C++ applications Documented and easy to understand source code CSV Report and Device Tree File     Downloads To download the installer for all platforms, please login to our download site via:  http://www.nxp.com/pinsimx Please refer to Pins Tool Documentation  for installation and quick start guides.   Overview of Changes - version 5 New Configuration Wizard allows to specify the default core for multi-core processors. Data Manager - allows overview of downloaded data, their versions, tool support information, update out dated, or manually download new data. Copy/Paste of pin(s) supported in Routed Pins view. Added in-tool tutorials - eclipse Cheat Sheets integration. Overview of Changes - version 4.1 Undo/Redo supported. Product based on Eclipse Oxygen release 3. Unified import wizard. A single import source is implemented. It allows you to import all supported types of C files. Community i.MX Processors 
View full article
The native Yocto not support chinese, so need to add chinese font . The first step should download Chinese font  files such as  MSYHMONO.ttf and DroidSansFallback.ttf.Then copy fonts files to /usr/share/fonts/truetype and run command  fc-cache .update font cache. use fc-list :lang=zh can see which Chinese fonts are installed:          /usr/share/fonts/truetype/MSYHMONO.ttf: Microsoft YaHei Mono:style=Regular          /usr/share/fonts/truetype/DroidSansFallbackFull.ttf: Droid Sans Fallback:style=Regular The secend step is to change default fonts. In weston-terminal.c we can see:           3119   weston_config_section_get_string(s, "font", &option_font, "mono");           3120   weston_config_section_get_int(s, "font-size", &option_font_size, 14);  weston-terminal default use mono font.Just to modify /etc/fonts/fonts.conf           <edit name="family" mode="assign" binding="same">                       <string>monospace</string> to   <string>Microsoft YaHei Mono</string> or <string>Droid Sans Fallback</string> could display Chinese character   But it have some problem such like as :   the left use Microsoft YaHei Mono font the Chinese character is overlapping ,the right use Droid Sans Fallback font is en-font could not display. If you have a better way to welcome a message!
View full article
This document describes the i.MX 8QXP MEK mini-SAS connectors features on Linux and Android use cases, covering the supported daughter cards, the process to change Device Tree (DTS) files or Boot images, and enable these different display options on the board.
View full article
For imx8QM, The manufacture mode is supported on SD2 which is powered by LDO2 of PMIC2 on MEK board. LDO2 of PMIC2 on MEK board is OFF by default. (LDO2 of PMIC1 is on by default) So manufacture mode is NOT working on the imx8QM MEK board. the solution would be: 1. schematic change Exchange the power supply(VCC_LDO_SD) and USDHC_VSELECT signal of SD2 and SD1. between PMIC2 (U23) and PMIC 1(U10). so that, the VCC_LDO_SD2) and USDHC2_VSELECT will be located on where VCC_LDO_SD1) and USDHC1_VSELECT are origonally.  and VCC_LDO_SD1 and USDHC1_VSELECT will be located on where VCC_LDO_SD2) and USDHC2_VSELECT are origonally.  SD1 will no longer be supported as the boot resource, instead SD2 will be. anyway you still can connect a WIFI to SD1 , becasue the power supply can be turned on after software booting up. 2. Modify the default fuse of PMIC, whcih is to enable LDO2 of PMIC2 by default.     please contact your local FAE and Sales for this.  we may add notification in the reference schematic and HW development guild in the future.
View full article
This document describes the i.MX 8MQ EVK HDMI output and mini-SAS connectors features on Linux and Android use cases, covering the supported daughter-board, the process to change Device Tree (DTS) files or Boot Images, and enable these different display options on the board.
View full article
This document shows the steps for the creation of Archlinux and kernel 4.18.5 on the UDOO board. Required material: UDOO board, Ubuntu 16.04 and SD card. Firts we need u-boot (universal bootloader), for that reason we need update the host. $ sudo apt-get update Then we need the file *.img and SPL for the file system $ wget http://os.archlinuxarm.org/os/imx6/boot/udoo/SPL $ wget http://os.archlinuxarm.org/os/imx6/boot/udoo/u-boot.img Kernel 4.18.5 and file system: $ sudo mkdir archlinux $ wget http://os.archlinuxarm.org/os/ArchLinuxARM-armv7-latest.tar.gz $ sudo tar -xzvf  ArchLinuxARM-armv7-latest.tar.gz $ sudo rm -rf *.tar.gz You must have the following files Now  We are going to burn the memory, we need a 16Gb of space: We need to make sure it is empty Then partitions: $ sudo fdisk /dev/sdc O, P, N, P, 1 space, 8192 default, W At the end the sdc is partition, then create the filesystem partition $ sudo mkfs.ext4 /dev/sdc1 The working directory $ sudo mkdir mnt mount the partition 1 $ sudo mount /devsdc1 mtn/ Now we where the kernel and filesystem are and copy all the file in mnt: $ sudo cp -vr * ~/mnt/ Once it finish we execute $ sync then unmount the partition of sdc1: $ sudo umount mnt/ Now is moment to load the SPL and u-boot: and $ sync we retire the sd and turn on the board. Now you are on ArchLinux. user: alarm                  root: Root Pass: alarm                 pass: root Now the firts thing we must do it is upgrade the keys: $ pacman -key --init $ pacman -key --populate archlinuxarm $ pacman -Syyuu We can add another user: $ useradd - m -g user  -s /bin/bash user_name $ passwd user_name $ paman -S sudo $ visudo Root ALL= (ALL) ALL user_name ALL=(ALL) ALL $ exit For the graphic we are going to install the xorg: $ sudo pacman -S xorg-server $ sudo pacman -S xorg-apps Now we can execute startx and observe the windows of xorg $ startx To have a windows gestor: $ sudo pacman -S sddm $ sudo pacman -S plasma kde-applications $ sudo systemctl enable sddm Reboot and you are ArchLinux graphics windows
View full article