i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Hey everyone! With the iMX8MM EVK, you also get an IR receiver LED interfaced with one of the GPIOs. Through this article today, I will demonstrate how to enable Infrared Receiver on the iMX8MM EVK so that data sent from the IR transmitter LEDs can be received and decoded on the iMX8MM EVK. Hardware used : iMX8MM EVK - i.MX 8M Mini Evaluation Kit | NXP Semiconductors Arduino Uno board IR TX module Arduino interfaced with IR TX will send IR messages to iMX8MM interfaced with IR RX LED Hardware connections: IR TX Module         <---->          Arduino Uno GND                          -                     GND 3.3V                          -                     3.3V DAT                           -                     D3 IR transmitter LED connected to Arduino Uno -- Kernel configurations needed: Linux Kernel Configurations Copy the kernel 'Image' built with the above changes and the IR decoder modules for the protocol you want to decode. All the ko modules are present i.e ir-rc5-decoder.ko for rc5 IR decoding in this folder after building: LIRC drivers Boot linux with the default dtb[imx8mm-evk.dtb] and the newly copied kernel 'Image' that you uploaded on the board.   At boot-up rc_register_device is called from drivers/media/rc/rc-main.c. A /dev/lirc0 node will also be created as a result of in-built driver loading. You can verify this by executing: lirc device node   On iM8MM, The IR receiver is connected to GPIO1_13. drivers/media/rc/gpio-ir-recv.c is responsible to configure this GPIO using the dts entry present in  arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi   Device tree changes gpio_ir_recv_probe will be called from drivers/media/rc/gpio-ir-recv.c.   At linux prompt, you can verify the gpio configuration using sysfs: IR GPIO Now insert the NEC and RC5 decoder modules. This gives the kernel ability to be able to decode the   NEC and RC5 IR protocols. LIRC Decoder Next, we need a program that utilizes the decoder driver to start decoding the IR signals coming onto the IR Receiver of iMX8MM EVK.   Some example invocations of the user-space binary we have built for the above purpose: RC5 Decoder RC6 Decoder NEC Decoder   ir_recv accepts 2 arguments:- 1st argument - protocol to enable 2nd argument - the remote-control device created in the /sys/class/rc example - /sys/class/rc/rc0 Note - Not to be confused with the protocols rc5 or rc6. The 2nd argument is not the name of the protocol ir_recv utility that we have built will open the /dev/lirc0 device and make an ioctl call LIRC_SET_REC_MODE to set the LIRC driver in Recording mode. These ioctls are handled in drivers/media/rc/lirc_dev.c in the kernel source code. So that whenever you run the ir_recv binary, it polls for the IR protocol scan code and prints it if successfully decoded. Attaching the ir_recv executable and the source code with this article for you to test and tweak. Please let me know if you have any follow-up questions. I would be happy to indulge. That's all I have for today. Thank you for your time!  
View full article
This article describes how to enable the GPIO support in SPL for i.MX 93 and how to use the associated library. Available GPIO banks Bank Registers' Base Address GPIO1 0x47400000 GPIO2 0x43810000 GPIO3 0x43820000 GPIO4 0x43830000   Software Tests performed using the LF6.12.20-2.0.0 BSP, but should work similarly in other versions.   Enable the GPIO support in SPL Enable the CONFIG_SPL_GPIO through menuconfig. Configure the GPIO pin Make sure the chosen GPIO pin is not used by any other peripheral, by checking U-Boot's device tree (example: imx93-11x11-evk.dts and its included files). If used, disable the conflicting peripheral in the device tree. To identify the exact macro associated to the GPIO functionality, please check the arch/arm/dts/imx93-pinfunc.h file.  Example 1: Use an available GPIO pin (e.g. GPIO2_IO05) This pin is not used by other peripheral, so there is nothing to disable.  To use the pin with the GPIO functionality, the following pin muxing must be added in the iomux node of the imx93-11x11-evk.dts file (located in dts/upstream/src/arm64/freescale/😞 😞 pinctrl_hog: hoggrp { fsl,pins = < MX93_PAD_GPIO_IO05__GPIO2_IO05 0x51e >; }; Note: 0x51e represents the value you want in the PAD register (SW_PAD_CTL_PAD_GPIO_IO05). You may configure it as you want.  Example 2: Use the XSPI1_TXC pin as GPIO (GPIO1_IO12) In our BSP, by default, this pin is used by the SAI1 peripheral. To use this pin as GPIO, SAI1 must be disabled in device tree. &sai1 { status = "disabled"; }; To use the XSPI1_TXC pin with the GPIO functionality, the following pin muxing must be added in the iomux node of the imx93-11x11-evk.dts file (located in dts/upstream/src/arm64/freescale/😞😞 pinctrl_hog: hoggrp { fsl,pins = < MX93_PAD_SAI1_TXC__GPIO1_IO12 0x51e >; }; Include the correct header files In the file you want to use the GPIO, include the following headers: #include <asm/arch-mx7ulp/gpio.h> #include <asm-generic/gpio.h> Define the GPIO To define the GPIO's handle, use the IMX_GPIO_NR(bank, index) macro. index = The pin number within the bank. bank = The GPIO bank number, mapped as follows (due to the way they are placed in memory): GPIO Bank bank value for IMX_GPIO_NR GPIO1 4 GPIO2 1 GPIO3 2 GPIO4 3 Example 1: Compute the handle for GPIO2_IO05 #define TIMED_GPIO IMX_GPIO_NR(1, 5) Example 2: Compute the handle for XSPI1_TXC (GPIO1_IO12) #define TIMED_GPIO IMX_GPIO_NR(4, 12)   Read the GPIO pin gpio_request(TIMED_GPIO, "timed_gpio"); gpio_direction_input(TIMED_GPIO); int val = gpio_get_value(TIMED_GPIO); printf("GPIO value is %d\n", val);   Write the GPIO pin gpio_request(TIMED_GPIO, "timed_gpio"); // set the pin as output and make it high gpio_direction_output(TIMED_GPIO, 1);   The driver used is drivers/gpio/gpio-uclass.c.
View full article
As we haven't provided a guide with steps that implement the Linux OS encryption and signature for i.MX9x products so far. So, the document provides the steps for that. For details related to how to encrypt and sign a bootloader image, please have a reference to This Guide 
View full article
When working with an evaluation kit you will be provided with a System Controller Firmware (SCFW) binary included in your BSP. This scfw binary has been tailored for that specific board and you might need to modify some board dependencies to fit your specific hardware. This document aims to provide an overview on the SCFW porting process, for detailed information please refer to the System Controller Porting guide (sc_fw_port.pdf).   Setting up the system The SCFW is built on a Linux host. The steps to set-up your system are the following: Download the GNU ARM Embedded Toolchain: 6-2017-q2-update June 28, 2017 from the ARM website: Select a directory to untar the file unto, for instance: mkdir ~/gcc_toolchain cp ~/Downloads/gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 ~/gcc_toolchain/ cd ~/gcc_toolchain/ tar xvjf gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Set TOOLS environment variable to the directory containing the tool chain, "~/gcc_toolchain" on the example above, .bash_profile can also be modified to export this environment variable: export TOOLS=~/gcc_toolchain/ srec_cat is also necessary for the build, this is usually contained in the srecord package, on ubuntu you can do: sudo apt-get update sudo apt-get install srecord Now you can change to the porting kit directory (e.g. scfw_export_mx8qm) and build the scfw. System Controller Firmware Porting kit  The SCFW porting kit contains source files and object files that will allow you to modify the SCFW to work with your board. You can get the latest System Controller Firmware Porting kit from the i.MX Software and development webpage: Once you obtain the porting kit untar it: tar xvzf imx-scfw-porting-kit-1.1.tar.gz‍ You will see the following file structure: The porting kit is contained under packages, the README contains the instructions to extract the porting kit, basically: cd packages/ chmod a+x imx-scfw-porting-kit-1.1.bin ./imx-scfw-porting-kit-1.1.bin‍‍‍ You will be prompted to accept an End User License Agreement: Once you accept the agreement the porting kit will be extracted in a new folder, the folder structure is as follows: All documentation regarding SCFW is under doc/pdf or in html format if preferred, it is recommended to go over sc_fw_port.pdf. The porting kits for different SoC variants (QM A0, QM B0 and QXP B0) are under src packaged as tar.gz, all other files are SCFW libraries for different software packages, such as Linux, QNX, FreeRTOS, U-boot, ARM Trusted Firmware, etc...   If you will be working with several SoC variants (working with both QXP and QM) it is recommended to extract all porting kits into a single directory, that way you will be able to build for any variant from this directory, the command to do this is: cd imx-scfw-porting-kit-1.1/ cd src/ find scfw_export_mx8*.gz -exec tar --strip-components 1 --one-top-level=scfw_export_mx8 -xzvf {} \;‍‍‍ A scfw_export_mx8 folder will be created, from here you will be able to build SCFW for any supported variant. Or you can just extract the package for the variant you are interested on and use that. cd scfw_export_mx8/‍ All the build folders contain the results of building the SCFW and platform is where the source of the SCFW is stored.   All the code that is specific to a board configuration is under "platform/board/mx8<derivative>_<board_name>" where derivative is the i.MX8 silicon family such as QXP or QM, and board name is the name of the board the SCFW package is for. The first step in porting the SCFW to your board is to create a folder for your i.MX8 derivative and board, you can take one of the available board examples and rename the folder, that will provide you a project to get started with, for instance: cp -r platform/board/mx8qm_val/ platform/board/mx8qm_myBoard/‍‍‍‍‍‍‍‍‍‍ The board in this example will be called "myBoard" and it is for an i.MX8QM B0 device. To build a SCFW for this board simply call: make qm R=B0 B=myBoard‍‍‍‍‍‍‍‍‍‍‍‍ If the target is an i.MX8QXP simply take a board based on this device and change the call to "make qx". Additional information such as build options and in detailed boot information can be found in the SCFW porting guide (sc_fw_port.pdf), chapter 2 of this document is a great introduction to the porting process.   Overview and useful information Configuring the PMIC overview and board.c common modifications The main file that needs to be altered (if not the only) is the "board.c" file, it is located at "platform/board/mx8X_board/". The board.c file contains most of the board related information such as SCU UART ports, PMIC initialization routines, PMIC temperature alarms settings and you can also modify it to configure LDOs voltages and communicate with the PMIC in general. All functions in the board.c file are executed by the SCU itself and this gives you access to the I2C interface that is used to communicate with the PMIC. SoC resources that are powered by an external supply (PMIC LDO for instace) such as AP cores and GPUs are powered off/on by board_set_power_mode, the mapping of the resource to an specific PMIC supply happens in board_get_pmic_info, for instance in our i.MX8QM validation board using the A53 subsystem is powered by SW2 of the third PMIC (PMIC_2_ADDR addresses start at PMIC_0) on the PF100 PMIC card and by SW5 of the first PMIC (PMIC_0_ADDR) on the PF8100 PMIC card. case SC_SUBSYS_A53: pmic_init(); if (pmic_card == PF100) { pmic_id[0] = PMIC_2_ADDR; pmic_reg[0] = SW2; *num_regs = 1; } else {/* PF8100_dual Card */ pmic_id[0] = PMIC_0_ADDR; pmic_reg[0] = PF8100_SW5; *num_regs = 1; } break; ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The voltages of SoC resources that are powered by an external supply (AP cores, GPUs, etc...) are managed by board_set_voltage in the board.c file. The mapping of resource to power supply occurs in board_get_pmic_info as in the example above. Eight "board resources" (SC_R_BOARD_R0, ... SC_R_BOARD_R7) are available, these resources allow you to define components in your board that the SCU can manage, for instance a sensor on your board powered by one of the PMIC LDOs can be mapped to a board resource and the board.c file can be modified to power on/off the sensor as well as modifying its voltage. Modifying the voltage on a board resource can be either be done by modifying the voltage at board_trans_resource_power (see below) or if the voltage needs to change at run time the function board_set_control can be modified to change the voltage whenever a miscellaneous call (more details in the Miscellaneous Service 101) is made on that resource. For instance to change the voltage on SC_R_BOARD_R7 you would have the following case to board_set_control: case SC_R_BOARD_R7: if (ctrl == SC_C_VOLTAGE) { /* Example only PMIC_X_ADDR and PMIC_SUPPLY need to match an actual device */ pmic_interface.pmic_set_voltage(PMIC_X_ADDR, PMIC_SUPPLY, val, step); } else return SC_ERR_PARM; break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The case above will be executed by the SCU every time the application calls the function below: sc_misc_set_control( ipc, SC_R_BOARD_R7, SC_C_VOLTAGE, voltage_val);‍‍‍‍‍‍‍‍ Powering on/off a board resource happens at board_trans_resource_power in the board.c file. For instance in NXP's validation board the PTN5150 on the board is managed through a board resource 0, and the power on/off is managed as follows: case BRD_R_BOARD_R0 : /* PTN5150 (use SC_R_BOARD_R0) */ if (pmic_ver.device_id == PF100_DEV_ID) { if (to_mode > SC_PM_PW_MODE_OFF) { pmic_interface.pmic_set_voltage(PMIC_2_ADDR, VGEN6, 3300, SW_RUN_MODE); pmic_interface.pmic_set_mode(PMIC_2_ADDR, VGEN6, VGEN_MODE_ON); } else { pmic_interface.pmic_set_mode(PMIC_2_ADDR, VGEN6, VGEN_MODE_OFF); } } else {/* PF8100_dual Card */ if (to_mode > SC_PM_PW_MODE_OFF) { pmic_interface.pmic_set_voltage(PMIC_1_ADDR, PF8100_LDO1, 3300, REG_RUN_MODE); pmic_interface.pmic_set_mode(PMIC_1_ADDR, PF8100_LDO1, RUN_EN_STBY_EN); } else { pmic_interface.pmic_set_mode(PMIC_1_ADDR, PF8100_LDO1, RUN_OFF_STBY_OFF); } } break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Whenever the function below is called from the application side the SCU will execute the code above: sc_pm_set_resource_power_mode(ipc, SC_R_BOARD_R0, SC_PM_PW_MODE_ON/OFF);‍‍‍‍‍‍‍‍ board_config_sc is used to mark resources that the SCU needs, such as the I2C module and pads used to communicate with the PMIC, any resource needed by the board.c functions to work should be marked in this function as not movable, for instance to keep the SCU I2C module the following line is added: rm_set_resource_movable(pt_sc, SC_R_SC_I2C, SC_R_SC_I2C, false);‍‍‍‍‍‍‍‍‍ The following pads are part of the SCU and the application will not be able to access them: - SC_P_SCU_PMIC_MEMC_ON - SC_P_SCU_WDOG_OUT - SC_P_PMIC_EARLY_WARNING - SC_P_PMIC_INT_B - SC_P_SCU_BOOT_MODE0 through SC_P_SCU_BOOT_MODE5 board_system_config is where early resource management occurs, this function is only called when the alt_config flag is set in the image, and it can create partitions and allocate resources to it. More details are found in the resource management service 101. board_get_pcie_clk_src defines the clock that the PCIe uses, it can be either BOARD_PCIE_PLL_EXTERNAL or BOARD_PCIE_PLL_INTERNAL. board_print is very useful to debug your changes the syntax is as follows: board_print(3, "Debug printout %d\n", val);‍‍‍‍‍‍‍ Where the first parameter is the Debug Level and from there on it works as a standard printf. The output will only be visible on the SCU debug output whenever the SCU is built with the corresponding debug level, in the case above the SCFW needs to be built as follows in order to see the output: make qm B=myBoard‍‍‍‍ DL=3 or higher (debug level goes from 0 to 5)‍‍‍‍‍‍‍   Usage examples The following utility shows how to make System Controller Firmware requests and provides a way to make such requests through command line interface on both QNX and Linux System Controller Firmware Command Line Utility for Linux and QNX   System Controller Firmware 101  
View full article
  Test environment   i.MX8MP EVK LVDS0 LVDS-HDMI  bridge(it6263) Uboot2022, Uboot2023 Background   Some customers need show logo using LVDS panel. Current BSP doesn't support LVDS driver in Uboot. This patch provides i.MX8MPlus LVDS driver support in Uboot. If you want to connect it to LVDS panel , you need port your lvds panel driver like  simple-panel.c   Update [2022.9.19] Verify on L5.15.32_2.0.0  0001-L5.15.32-Add-i.MX8MP-LVDS-driver-in-uboot 'probe device is failed, ret -2, probe video device failed, ret -19' is caused by below code. It has been merged in attachment. // /* Only handle devices that have a valid ofnode */ // if (dev_has_ofnode(dev) && !(dev->driver->flags & DM_FLAG_IGNORE_DEFAULT_CLKS)) { // /* // * Process 'assigned-{clocks/clock-parents/clock-rates}' // * properties // */ // ret = clk_set_defaults(dev, CLK_DEFAULTS_PRE); // if (ret) // goto fail; // }   [2023.3.14] Verify on L5.15.71 0001-L5.15.71-Add-i.MX8MP-LVDS-support-in-uboot   [2023.9.12] For some panel with low DE, you need uncomment CTRL_INV_DE line and set this bit to 1. #include <linux/string.h> @@ -110,9 +111,8 @@ static void lcdifv3_set_mode(struct lcdifv3_priv *priv, writel(CTRL_INV_HS, (ulong)(priv->reg_base + LCDIFV3_CTRL_SET)); /* SEC MIPI DSI specific */ - writel(CTRL_INV_PXCK, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); - writel(CTRL_INV_DE, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); - + //writel(CTRL_INV_PXCK, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); + //writel(CTRL_INV_DE, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); }       [2024.5.15] If you are uing simple-panel.c, need use below patch to set display timing from panel to lcdif controller. diff --git a/drivers/video/simple_panel.c b/drivers/video/simple_panel.c index f9281d5e83..692c96dcaa 100644 --- a/drivers/video/simple_panel.c +++ b/drivers/video/simple_panel.c @@ -18,12 +18,27 @@ struct simple_panel_priv { struct gpio_desc enable; }; +/* define your panel timing here and + * copy it in simple_panel_get_display_timing */ +static const struct display_timing boe_ev121wxm_n10_1850_timing = { + .pixelclock.typ = 71143000, + .hactive.typ = 1280, + .hfront_porch.typ = 32, + .hback_porch.typ = 80, + .hsync_len.typ = 48, + .vactive.typ = 800, + .vfront_porch.typ = 6, + .vback_porch.typ = 14, + .vsync_len.typ = 3, +}; + @@ -100,10 +121,18 @@ static int simple_panel_probe(struct udevice *dev) return 0; } +static int simple_panel_get_display_timing(struct udevice *dev, + struct display_timing *timings) +{ + memcpy(timings, &boe_ev121wxm_n10_1850_timing, sizeof(*timings)); + + return 0; +} static const struct panel_ops simple_panel_ops = { .enable_backlight = simple_panel_enable_backlight, .set_backlight = simple_panel_set_backlight, + .get_display_timing = simple_panel_get_display_timing, }; static const struct udevice_id simple_panel_ids[] = { @@ -115,6 +144,7 @@ static const struct udevice_id simple_panel_ids[] = { { .compatible = "lg,lb070wv8" }, { .compatible = "sharp,lq123p1jx31" }, { .compatible = "boe,nv101wxmn51" }, + { .compatible = "boe,ev121wxm-n10-1850" }, { } };   [2024.7.23] Update patch for L6.6.23(Uboot2023) [2025.10.24] If you are facing 'Enable clock-controller@30380000 failed' error, add clocks in ccm driver. diff --git a/drivers/clk/imx/clk-imx8mp.c b/drivers/clk/imx/clk-imx8mp.c index 05a7d050be6..38497056344 100644 --- a/drivers/clk/imx/clk-imx8mp.c +++ b/drivers/clk/imx/clk-imx8mp.c @@ -181,6 +181,11 @@ static const char * imx8mp_media_mipi_phy1_ref_sels[] = {"clock-osc-24m", "sys_p static const char * imx8mp_media_disp_pix_sels[] = {"clock-osc-24m", "video_pll1_out", "audio_pll2_out", "audio_pll1_out", "sys_pll1_800m", "sys_pll2_1000m", "sys_pll3_out", "clk_ext4", }; + +static const char * imx8mp_media_ldb_sels[] = {"clock-osc-24m", "sys_pll2_333m", "sys_pll2_100m", + "sys_pll1_800m", "sys_pll2_1000m", + "clk_ext2", "audio_pll2_out", + "video_pll1_out", }; #endif static const char *imx8mp_dram_core_sels[] = {"dram_pll_out", "dram_alt_root", }; @@ -321,6 +326,8 @@ static int imx8mp_clk_probe(struct udevice *dev) #ifndef CONFIG_SPL_BUILD clk_dm(IMX8MP_CLK_MEDIA_MIPI_PHY1_REF, imx8m_clk_composite("media_mipi_phy1_ref", imx8mp_media_mipi_phy1_ref_sels, base + 0xbd80)); clk_dm(IMX8MP_CLK_MEDIA_DISP1_PIX, imx8m_clk_composite("media_disp1_pix", imx8mp_media_disp_pix_sels, base + 0xbe00)); + clk_dm(IMX8MP_CLK_MEDIA_DISP2_PIX, imx8m_clk_composite("media_disp2_pix", imx8mp_media_disp_pix_sels, base + 0x9300)); + clk_dm(IMX8MP_CLK_MEDIA_LDB, imx8m_clk_composite("media_ldb", imx8mp_media_ldb_sels, base + 0xbe00)); #endif clk_dm(IMX8MP_CLK_DRAM_ALT_ROOT, imx_clk_fixed_factor("dram_alt_root", "dram_alt", 1, 4)); clk_dm(IMX8MP_CLK_DRAM_CORE, imx_clk_mux2_flags("dram_core_clk", base + 0x9800, 24, 1, imx8mp_dram_core_sels, ARRAY_SIZE(imx8mp_dram_core_sels), CLK_IS_CRITICAL)); @@ -363,7 +370,9 @@ static int imx8mp_clk_probe(struct udevice *dev) clk_dm(IMX8MP_CLK_MEDIA_APB_ROOT, imx_clk_gate2_shared2("media_apb_root_clk", "media_apb", base + 0x45d0, 0, &share_count_media)); clk_dm(IMX8MP_CLK_MEDIA_AXI_ROOT, imx_clk_gate2_shared2("media_axi_root_clk", "media_axi", base + 0x45d0, 0, &share_count_media)); clk_dm(IMX8MP_CLK_MEDIA_DISP1_PIX_ROOT, imx_clk_gate2_shared2("media_disp1_pix_root_clk", "media_disp1_pix", base + 0x45d0, 0, &share_count_media)); + clk_dm(IMX8MP_CLK_MEDIA_DISP2_PIX_ROOT, imx_clk_gate2_shared2("media_disp2_pix_root_clk", "media_disp2_pix", base + 0x45d0, 0, &share_count_media)); clk_dm(IMX8MP_CLK_MEDIA_MIPI_PHY1_REF_ROOT, imx_clk_gate2_shared2("media_mipi_phy1_ref_root", "media_mipi_phy1_ref", base + 0x45d0, 0, &share_count_media)); + clk_dm(IMX8MP_CLK_MEDIA_LDB_ROOT, imx_clk_gate2_shared2("media_ldb_root_clk", "media_ldb", base + 0x45d0, 0, &share_count_media)); #endif clk_dm(IMX8MP_CLK_USDHC3_ROOT, imx_clk_gate4("usdhc3_root_clk", "usdhc3", base + 0x45e0, 0));   Update LVDS panel demo.    
View full article
Background : Some customer wants to know the DRAM's MR register value. But, For now, we do not have any documentation or binary to complete this. So, this article aim to show how to read this register.   Hardware environment : i.MX8ULP EVK board Software environment : uboot-imx : lf_v2024.04   1. The related registers information are as following:   DENALI CTL 165 [READ MODEREG[24:8]] Read the specified memory mode register from specified chip when start bit set. Bits (7:0) define the memory mode register and bits (15:8) define the chip select. Set bit (16) to 1 to trigger.   DENALI CTL 166 [PERIPHERAL MRR - DATA[31:0]] Data and chip returned from memory mode register read requested by the READ MODEREG parameter. Bits (7:0) indicate the read data and bits (15:8) indicate the chip. READ-ONLY   2. Test result :         Type the below command: mrr <chip_select MR_register>  Like the below picture, when type the mrr 0 c, it means the chip select is 1 and the MR register is MR12, then the value of MR12 register can be output , is 0x1c.     Note : When read the MR register, must make sure the register has read right. Because most of MR register only have write right. you can check about it on JDEC spec document.   If you want to get the test binary file, please contact to me, i will send it to you.
View full article
i.MX8MP and i.MX95 both support USB3.0. In EVK board, USB download pin is USB3.0 with Type-C.  While in other boards, they may delete CC logic design PTN5110, or use USB2.0 signals instead. This document describes how to modify U-Boot to support a design without PTN5110 when using the uuu tool to download.
View full article
Streaming different use case pipelines between i.MX 95 and i.MX 8M Plus LF-6.12.20
View full article
We are pleased to announce that Config Tools for i.MX v25.09 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) • The Release Notes format is updated from plain text to markdown. • The newly generated configuration includes the default NXP copyright notice and is licensed under the BSD-3-Clause license. • DDR tool – ODT and Driver Strength Updates for LP4/LP5 on i.MX 943 and i.MX 95 – Improved DRAM Configuration for i. MX 9x devices – Multicore support is enabled for DDR tests on i.MX 943 and i.MX 95 – Linux support for the DDR tool – Vref DQ Setting now available in the GUI – Board-agnostic SM Support for i.MX 943 and i.MX 95 – DDR part number entry is supported in the GUI – Enhanced logging from the target application – Stress test repetition option is enabled – Updated ODT shmoo scenario values on i.MX 943 and i.MX 95 – Support for SNPS FW and PHY Init 2024.09 SP2 on i.MX 943 and i.MX 95 – AHAB image update to align with BSP for CES parts on i.MX 943 and i.MX 95 – New configuration support for 15x15 on i.MX 943 – Improved bus configuration for single-channel setups – LP4/LP5 CS signal configuration now exposed in the GUI for i.MX 943 and i.MX 95 • Clocks – Supported input frequency setting • System Manager – Initial version of the tool
View full article
based on customer's issue when use PTF pins of imx8ulp as GPIO or gpio hog
View full article
  Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   This is a detailed programming aid for the registers associated with i.MX 8/8X DDR initialization.  For more details, refer to the i.MX 8/8X main DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/...  
View full article
The purpose of this document is to provide supportive information for selection of suitable LPDDR4 and DDR3L devices that are supported by i.MX 8/8X/8XLite family of processors to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.  It is strongly recommended to consult with NXP and the respective memory vendor, the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements. Please note that some of the LPDDR4 devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low speed operation is planned in the use case, please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the respective NXP i.MX 8 Hardware Developer's Guide available on NXP.com The i.MX8/8X/8XL Reference manuals declare that there are 16GB allocated for the DDR. Please note that this is only the address space, which is reserved for the DDR memory in the memory map. This specification does not guarantee that the entire region can be utilized as the maximum achievable densities listed below in the tables are restricted mainly by the addressing capabilities of the DDR controller, width of the data bus and other implementation-specific parameters as well as availability of supported devices on the market. Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.  LPDDR4 - maximum supported densities Please note that the SoCs only support memory devices that support either the LPDDR4 mode or support both LPDDR4 and LPDDR4X modes. Memory devices that support only the LPDDR4X mode are not supported. SoC Package Max data bus width Maximum density Assumed memory organization Notes i.MX 8QM/8QP 29x29 mm 32-bit (per controller) 32Gb/4GB (per controller) dual rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 4 i.MX 8QXP/8DXP 21x21 mm 32-bit 32Gb/4GB dual rank, dual-channel  device with 16-row addresses (R0-R15) 1, 2, 4 i.MX 8QXP/8DXP 17x17 mm 16-bit 16Gb/2GB dual rank, single-channel  device with 16-row addresses (R0-R15) 1, 2, 3, 4, 9 i.MX 8XLite 15x15 mm 16-bit 32Gb/4GB dual rank, single channel  device with 17-row addresses (R0-R16) 1, 2, 3, 9   LPDDR4 - list of validated memories The validation process is an ongoing effort - updates of the table are expected. SoC Package Maximum validated density Vendor Validated part number  Notes i.MX 8QM/8QP 29x29 mm 24Gb/3GB (per controller) Micron MT53B768M32D4NQ-062 AIT:B   12,13 32Gb/4GB (per controller)  Samsung K4FBE3D4HB-KHCL  10,11 32Gb/4GB (per controller) Micron MT53E1G32D2FW-046 AUT:B (Z42M) 10, 11 32Gb/4GB (per controller) Micron MT53D1024M32D4DT-046 AAT:D   12 16Gb/2GB (per controller) Micron MT53D512M32D2DS-046 WT:D  10, 12 16Gb/2GB (per controller) Nanya NT6AN512T32AC-J1J  10, 11 16Gb/2GB (per controller) Nanya NT6AN512T32AC-J1H  10, 11 32Gb/4GB (per controller) Nanya NT6AN1024F32AC-J2J  10, 11 32Gb/4GB (per controller) Nanya NT6AN1024F32AC-J2H  10, 11 i.MX 8QXP/8DXP 21x21 mm 24Gb/3GB Micron MT53B768M32D4NQ-062 AIT:B   12, 13 32Gb/4GB Nanya NT6AN1024F32AC-J2J  10, 11 32Gb/4GB Nanya NT6AN1024F32AC-J2H  10, 11 16Gb/2GB Nanya NT6AN512T32AC-J2J  10, 11 16Gb/2GB Nanya NT6AN512T32AC-J2H  10, 11 32Gb/4GB Micron MT53D1024M32D4DT-046 AAT:D   11 i.MX 8XLite 15x15 mm 8Gb/1GB Micron MT53D512M16D1DS 046 AAT ES:D & Z9XGG   12 12Gb/1.5GB Micron MT53E768M16D1ZW-046 AAT:C 10, 11, 13 4Gb/0.5GB Samsung K4F4E164HD-THCL  10, 11 8Gb/1GB ISSI IS43LQ16512A-053BLI 10, 11 8Gb/1GB Nanya NT6AN512M16AV-J1I  10, 11   LPDDR4 - list of incompatible devices Given the limitations mentioned in this document, the following memory devices were identified as incompatible with the particular SoCs as detailed in the following table:   Memory vendor Part Number Density Incompatible SoCs Incompatibility reason Samsung K4FHE3S4HA-KU(H/F)CL 24Gb/3Gb i.MX8QM/8QP, i.MX8QXP/8DXP The memory device requires 17th row address bit to function. Samsung K4UHE3S4AA-KU(H/F)CL 24Gb/3Gb i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL The memory device only supports the LPDDR4X mode. Samsung K4UJE3D4AA-KU(H/F)CL 48Gb/6GB i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL The memory device only supports the LPDDR4X mode. Samsung K4FCE3Q4HB-KU(H/F)CL 64Gb/8GB i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL A byte mode memory device. Samsung K4UCE3Q4AB-KU(H/F)CL 64Gb/8GB i.MX8QM/QP, i.MX8QXP/8DXP, i.MX8DXL, i.MX8SXL A byte mode memory device. The device only supports the LPDDR4X mode.    DDR3L - maximum supported densities SoC Package Max data bus width Maximum density Assumed memory organization Notes i.MX 8QXP/8DXP 21x21 mm 32-bit 64Gb/8GB x8, 8Gb device with 16-row addresses and 11 column addresses 5, 6 i.MX 8QXP/8DXP 17x17 mm 16-bit 32Gb/4GB x8, 8Gb device with 16-row addresses and 11 column addresses 5, 7 i.MX 8XLite 15x15 mm 16-bit 16Gb/2GB x8, 8Gb device with 16-row addresses and 11 column addresses 5, 8   DDR3L - list of validated memories The validation process is an ongoing effort -  updates of the table are expected. SoC Package Density Validated part number (vendor) Notes i.MX 8QXP/8DXP 21x21 mm 8Gb/1GB 2x MT41K256M16TW-093 IT:P (Micron) 12 i.MX 8XLite 15x15 mm           4Gb/512MB MT41K256M16TW-093 IT:P (Micron) 12   Note 1: The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, and on the JEDEC standard JESD209-4A. Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that a DRAM with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 2: Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification). Note 3: The memory vendors often do not offer so many variants of single-channel memory devices. As an alternative, a dual-channel device with only one channel connected may be used. For example: A dual-rank, single-channel device with 16-row address bits has a density of 16Gb. If such a device is not available at the chosen supplier, a dual-rank, dual-channel device with 16-row address bits can be used instead. This device has a density of 32 Gb however since only one channel can be connected to the SoC, only half of the density is available (16 Gb). Usage of more than one discrete memory chip to overcome market constraints is not supported since only point-to-point connections are assumed for LPDDR4. Note 4: Devices with 17-row addresses (R0-R16) are not supported by the SoCs.  Note 5: The numbers are based purely on the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, and on the JEDEC standard JESD79-3E/JESD79-3F. Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that a DRAM with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk. Note 6: The density can be achieved by connecting 8 single rank discrete devices with one 8Gb die each, 4 devices connected to each chip select, or by connecting 4 dual rank discrete devices with two 8Gb dies each. Note that this number of discrete devices significantly exceeds the number of devices used on the validation board (2 discrete devices, not taking into account the device used for ECC) therefore, it is not guaranteed that the i.MX would be able to drive the signals with margin to the required voltage levels due to increased loading on the traces. A significant effort would be required in terms of PCB layout and signal integrity analysis hence practically, it is not recommended to use more than 2 discrete DDR3L devices. This corresponds to the maximum density of 16Gb/2GB in the case of the single rank devices containing one 8Gb die or 32Gb/4GB in the case of the dual-rank devices containing two 8Gb dies (x16 8Gb devices with 16-row addresses and 10 column addresses assumed instead of x8 devices in such case). Note 7: The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select, or by connecting 2 dual rank discrete devices with two 8Gb dies each. Note that the first option exceeds the number of devices used on the validation board (2 discrete devices) therefore, it is not guaranteed that the i.MX would be able to drive the signals with margin to the required voltage levels due to increased loading on the traces. A significant effort would be required in terms of PCB layout and signal integrity analysis, hence practically, it is not recommended to use more than 2 discrete DDR3L devices. This corresponds to the maximum density of 16Gb/2GB in the case of the single rank devices containing one 8Gb die or 32Gb/4GB in the case of the dual-rank devices containing two 8Gb dies. Note 8: The density can be achieved by connecting 2 single rank discrete devices with one 8Gb die each to the i.MX. 8XLite supports only one chip select for DDR3L therefore, dual-rank systems are not supported. Note 9: For single-channel (x16) memory devices, the current maximum available density in the market is 16Gb/2GB (2025). Note 10: The memory part number did not undergo full JEDEC verification however, it passed all functional testing items. Note 11: Part is active. Reviewed Aug 2025 Note 12: Part is being End Of Life'd (EoL) by Vendor or obsolete. Note 13: Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity. Additional Links i.MX 8M Quad/8M Mini/8M Nano/8M Plus - LPDDR4, DDR4 and DDR3L memory compatibility guide 
View full article
This article describe some bring up tips during i.MX95 board debug, including HW and SW aspects.  
View full article
Overview The purpose of this document is to provide guidance for FlexIO 8080 display capability. Generally, the 8080 bus interface consists of one chip-select line (CS), one writing-latch line (WR), one reading-latch line (RD), one data/command-select line (RS, also called D/C), and 8 or 16 bidirectional data lines (Data Bus). Since The FlexIO instance of i.MX 943 support only 16 pins, the demo can only support 8 bit 8080 mode(two pin should be used as WR and RD signal.   Below are pins used in the 8 bit 8080 display. Panel Setup The panel in the example is X-LCD-PAR-S035. To use 8 bit 8080 mode, need ser IM[2:0] to be 011. Connection and Software i.MX 943 Need pull down SPI8_SEL1 and SPI8_SEL3 of PCA6416 in SW to select Arduino for 8080 pins D[7:4]. Here is the patch for system manager. For quick verification, use flash_m70 when building bootloader. diff --git a/configs/mx94evk.cfg b/configs/mx94evk.cfg index 9d46976..90bf089 100755 --- a/configs/mx94evk.cfg +++ b/configs/mx94evk.cfg @@ -499,6 +499,9 @@ ENC_PLL OWNER ENDAT2_1 OWNER ENDAT2_2 OWNER ENDAT3_1 OWNER +GPIO2 OWNER +GPIO3 OWNER +FLEXIO1 OWNER FLEXIO3 OWNER FLEXIO4 OWNER FLEXPWM1 OWNER @@ -515,6 +518,7 @@ HIPERFACE_SAFE1_2 OWNER HIPERFACE_SAFE2_1 OWNER HIPERFACE_SAFE2_2 OWNER IRQSTEER_M7_0 OWNER +LPI2C6 OWNER LPIT1 OWNER LPTMR1 OWNER LPTMR2 OWNER @@ -557,6 +561,25 @@ XBAR_DSC3 OWNER PIN_GPIO_IO24 OWNER PIN_GPIO_IO25 OWNER +# 8080 +PIN_GPIO_IO00 OWNER +PIN_GPIO_IO01 OWNER +PIN_GPIO_IO02 OWNER +PIN_GPIO_IO03 OWNER +PIN_GPIO_IO08 OWNER +PIN_GPIO_IO09 OWNER +PIN_GPIO_IO10 OWNER +PIN_GPIO_IO11 OWNER +PIN_GPIO_IO12 OWNER +PIN_GPIO_IO13 OWNER +PIN_GPIO_IO14 OWNER +PIN_GPIO_IO15 OWNER +PIN_GPIO_IO38 OWNER + +# I2C6 +PIN_GPIO_IO28 OWNER   Attached imx943_flexio_8080_8bit.zip is patch for m70 demo based on SDK_25_06_00_MCIMX943-EVK.   i.MX 93 Need pull up EXP_SEL(pin4 R4) of ADP5585 in SW to route some pins. Attached imx93_flexio_8080_8bit.zip is patch for m33 demo based on SDK_25_06_00_MCIMX93-EVK. The running status is similar as i.MX943.
View full article
  This document shows how to use the open source gstreamer1.0-rtsp-server package on i.MX6QDS and i.MX8x to stream video files and camera using RTP protocol.  The i.MX 6ULL and i.MX 7 doesn't have Video Processing Unit (VPU). Real time protocol (RTP) is a very common network protocol for delivering media over IP networks. On the board, you will need a GStreamer pipeline that encodes the raw video, adds the RTP payload, and sends over a network sink. A generic pipeline would look as follows: video source ! video encoder ! RTP payload ! network sink Video source: often it is a camera, but it can be a video from a file or a test pattern, for example. Video encoder: a video encoder as H.264, H.265, VP8, JPEG and others. RTP payload: an RTP payload that matches the video encoder. Network sink: a video sync that streams over the network, often via UDP. Pre-Requisites: MX6x o MX8x board with the L6.6.52 BSP installed. A host PC with either Gstreamer or VLC player installed.   Receiving h264 / h.265 Encoded RTP Video Stream on a Host Using GStreamer: GStreamer is a low-latency method for receiving RTP video. On your host machine, install Gstreamer and send the following command: $ gst-launch-1.0 -v udpsrc port=5000 caps = "application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" ! rtph264depay ! decodebin ! videoconvert ! autovideosink sync=false   Using HOST PC: VLC Player Optionally, you can use VLC player to receive RTP video on a PC. First, in your PC, create a sdp file with the following content:  stream.sdpv=0m=video 5000 RTP/AVP 96c=IN IP4 127.0.0.1a=rtpmap:96 H264/90000 After this, with the GStreamer pipepline on the device running, open this .sdp file with VLC Player on the host PC.   Sending h.264 and h.265 Encoded RTP video stream GStreamer provides an h.264 encoding element by software named x264enc. Use this plugin if your board does not support h.264 encoding by hardware or if you want to use the same pipeline on different modules. Note that the video performance will be lower compared with the plugins with encoding accelerated by hardware. # gst-launch-1.0 videotestsrc ! videoconvert ! x264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Note: Replace <host-machine-ip> by the IP of the host machine. In all examples you can replace videotestsrc by v4l2src element to collect a stream from a camera   i.MX8X # gst-launch-1.0 videotestsrc ! videoconvert ! v4l2h264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   i.MX8M Mini Quad / 8M Plus # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 i.MX6X The i.MX6QDS does not support h.265 so the h.264 can work: # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Using other video Encoders While examples of streaming video with other encoders are not provided, you may try it yourself. Use the gst-inspect tool to find available encoders and RTP payloaders on the board: # gst-inspect-1.0 | grep -e "encoder"# gst-inspect-1.0 | grep -e "rtp" -e " payloader" Then browse the results and replace the elements in the original pipelines. On the receiving end, you will have to use a corresponding payload. Inspect the payloader element to find the corresponding values. For example: # gst-inspect-1.0 rtph264pay   Install rtp in your yocto different form L6.6.52 BSP, to install gstreamer1.0-rtsp-server in any Yocto Project image, please follow the steps below: Enable meta-multimedia layer: Add the following on your build/conf/bblayers.conf: BBLAYERS += "$"${BSPDIR}/sources/meta-openembedded/meta-multimedia" Include gstreamer1.0-rtsp-server into the image: Add the following on your build/conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" Run bitbake and mount your sdcard. Copy the binaries: Access the gstreamer1.0-rtsp-server examples folder: $ cd /build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/$version/build/examples/.libs Copy the test-uri and test-launch to the rootfs /usr/bin folder. $ sudo cp test-uri test-launch /media/USER/ROOTFS_PATH/usr/bin Be sure that the IPs are correctly set: SERVER: => ifconfig eth0 $SERVERIP CLIENT: => ifconfig eth0 $CLIENTIP Video file example SERVER: => test-uri file:///home/root/video_file.mp4 CLIENT: => gst-launch-1.0 playbin uri=rtsp://$SERVERIP:8554/test You can try to improve the framerate performance using manual pipelines in the CLIENT with the rtspsrc plugin instead of playbin. Follow an example: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test caps = 'application/x-rtp'  ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! queue max-size-buffers=0 ! imxv4l2sink sync=false   Camera example SERVER: => test-launch "( imxv4l2src device=/dev/video0 ! capsfilter caps='video/x-raw, width=1280, height=720, framerate=30/1, mapping=/test' ! vpuenc_h264 ! rtph264pay name=pay0 pt=96 )" CLIENT: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test ! decodebin ! autovideosink sync=false The rtspsrc has two properties very useful for RTSP streaming: Latency: Useful for low-latency RTSP stream playback (default 200 ms); Buffer-mode: Used to control buffer mode. The slave mode is recommended for low-latency communications. Using these properties, the example below gets 29 FPS without a sync=false property in the sink plugin. The key achievement here is the fact that there is no dropped frame: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test latency=100 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! vpudec ! imxv4l2sink    
View full article
  This article shows how to use the i.MX6DL/Q to transcode and stream videos on 1080i/p @ 24fps and 720p @ 30fps. For this test, we used one i.MX6DL as server and an i.MX6DL and i.MX6Q as clients. The video is streamed by the server, playing the sound at the same time, while the clients show the video in the HDMI output, as the image below:     This test depends on some GStreamer plugins. To check that the right GStreamer plugins are installed type the following commands: $ gst-inspect-1.0 | grep h264 To return all the H.264 related plugins, or: $ gst-inspect-1.0 decodebin To check directly the command. To connect more than one board to the minicom, open it with the command: $ sudo minicom –s This way, you open the configuration menu. Enter in the “Serial port setup” option and press “A” to set or change the PORTNUMBER, in “ttyUSB$PORTNUMBER”. To set the HDMI output, run the commands below from the U-Boot prompt: => setenv mmcargs 'setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 consoleblank=0' => saveenv Be sure that the IPs are correctly setted: SERVER: => ifconfig eth0 $SERVERIP CLIENTS: => ifconfig eth0 $CLIENTSIP Streaming transcoded video only SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, payload=(int)96' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false Streaming transcoded video + audio SERVER: => gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin name=demux demux. ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 demux. ! alsasink CLIENTS: => gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, encoding-name=(string)H264' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false   You can check the results with the 1080p@24fps.
View full article
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the IMX8MP-EVK board using the MCU-LINK Pro. You’ll install the necessary firmware, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: IMX8MP-EVK Board MCU-LINK Pro Debug Probe PC Host with MCUXpresso for VS Code installed Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX8MP-EVK SDK   Import "hello world" example Ensure that we are compiling a debug binary Build Project Flash the Binary using UUU Tool Connect the IMX8MP-EVK Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write hello_world.bin mmc X:1 hello_world_debug.bin Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Connect MCU-LINK Pro to the Target   IMX8MP-EVK Debug connection:     Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 0x48000000 hello_world_debug.bin; cp.b 0x48000000 0x7e0000 0x20000; => bootaux 0x7e0000 Note: replace the X with 2 if you are booting from eMMC or 1 if you are booting from SD Card   Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso:          With the MCU-LINK Pro configured, the IMX8MP-EVK, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX8MP based projects.   References: AN14120.pdf 
View full article
This post contains a guide of how to use SDMA1 on Cortex M7 in parallel of Linux on A53. For i.MX 8M Plus, SDMA1 is a general-purpose DMA engine which can be used by low speed peripherals including UART, SPI and other peripherals. But some customers found issues when they are using SDMA1 on M7 core in parallel of Linux on A53. For example, if you try to run the sdma_uart_transfer example on the i.MX8M Plus EVK, the example works correctly when interfacing through the JLink debugger.  However, you will find that you can not run it from both the remoteproc interface and U-Boot.  It exits without error from the UART_SendSDMA function,  but the callback is never called and it seems to hang waiting for the information to be sent. On the i.MX 8MP EVK board,  uart4 is used for Cortex-M7 core. This article tries to provide an example to establish communication using UART3 and SDMA1 on the i.MX 8MP EVK, while Linux is running on Core A53.  This example is based on sdma_uart_transfer demo. The steps are verified with i.MX Linux 6.12.20_2.0.0  release and SDK_25.06.00. The software is compiled on an Ubuntu 22.04 host machine. This article is structured as follows:  1  Hardware requirements 2  Software Requirements 3  Modification in application      3.1 Pin changes     3.2 Clock changes     3.3 Application specific changes     3.4 Memory Region Control change 4  ATF changes     4.1 Download ATF source and change it      4.2 build ATF 5   U-BOOT change     5.1 build u-boot     5.2 make imx-boot image by using imx-mkimage     5.3 flash imx-boot image into i.MX 8MP EVK board 6  Running and Debugging     6.1    Debugging Cortex-M while Cortex-A is in U-BOOT     6.2   Debugging Cortex-M while Cortex-A is in Linux 7  Summary   1  Hardware requirements   -PC Host with MCUXpresso for VS Code installed -i.MX 8M Plus EVK (i.MX 8M Plus Power Evaluation Kit | NXP Semiconductors) -12V power supply -Micro USB Cable -J-Link Debug Probe. -USB To TTL( serial ) Converter   connect J21 (Pin6_GND  Pin8_UART3-TXD  Pin10_UART3-RXD) to Host PC via a USB to TTL converter.       2  Software Requirements   SDK_25_06_00_EVK-MIMX8MP This package can be download from https://mcuxpresso.nxp.com/ Next I will describe the detailed steps.   3  Modification in application     3.1 Pin changes   evkmimx8mp_iuart_sdma_transfer\pin_mux.c    3.2 Clock changes   evkmimx8mp_iuart_sdma_transfer\clock_config.c In function BOARD_BootClockRUN     3.3 Application specific changes   evkmimx8mp_iuart_sdma_transfer\board.h      app.h   Till now, we have completed all the changes for change uart4 to uart3. Compile , and debug with J-LINK, we can get the correct result.   Board receives 8 characters then sends them out.   However, if we try to load code on Cortex-M from U-Boot or Linux,  we can not get the expected results.   Below steps is a workaround to fix this issue. 3.4 Memory Region Control change   hardware_init.c In function BOARD_InitHardware ..... Then compile the application, the output are  iuart_sdma_transfer.bin and iuart_sdma_transfer_cm7.elf   4  ATF (ARM Trust Firmware)changes   4.1  Download ATF source and Change it  The RDC configuration in default BSP assign UART2 to domain 0 for A53,  and Domain 0 can read/write RDC,  and Domain 1 (M7) only can read it. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.12.3-1.0.0   GitHub - nxp-imx/imx-atf: i.MX ARM Trusted firmware plat/imx/imx8m/imx8mp/imx8mp_bl31_setup.c We need to assign UART3 to domain 1 so Cortex M7 can access   4.2 build ATF      $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.12.3-1.0.0 $ cd imx-atf $ source /opt/fsl-imx-xwayland/6.12-walnascar/environment-setup-armv8a-poky-linux $ export ARCH=arm64 $ unset LDFLAGS $ make PLAT=imx8mp bl31   This builds the bl31.bin binary, the location is : build/imx8mp/release/bl31.bin   5   U-BOOT change   5.1 Download and build u-boot please refer to chapter 4.5.13 How to build imx-boot image by using imx-mkimage ,   $ git clone https://github.com/nxp-imx/uboot-imx -b lf_v2025.04 $ cd uboot-imx/ $ source /opt/fsl-imx-xwayland/6.12-walnascar/environment-setup-armv8a-poky-linux $ export ARCH=arm64 $ make distclean $ make imx8mp_evk_defconfig $ make   The compiled u-boot.bin location uboot-imx/u-boot.bin   5.2 make imx-boot image by using imx-mkimage   My work folder The following steps allow you to build the bootable image for i.MX 8M Plus EVK, there are 9 files needed to generate a bootable image: ├── u-boot-spl.bin ├── u-boot-nodtb.bin   ├── imx8mp-evk.dtb ├── bl31.bin ├── signed_hdmi_imx8m.bin ├── lpddr4_pmu_train_1d_dmem_202006.bin ├── lpddr4_pmu_train_1d_imem_202006.bin ├── lpddr4_pmu_train_2d_dmem_202006.bin └── lpddr4_pmu_train_2d_imem_202006.bin   Once you have the nine files , use imx-mkimage tool. 5.2.1  Download source : $ git clone https://github.com/nxp-imx/imx-mkimage.git -b lf-6.12.20-2.0.0   5.2.2  Copy and rename mkimage from u-boot/tools/mkimage to imx-mkimage/iMX8M/mkimage_uboot. $ cp uboot-imx/tools/mkimage imx-mkimage/iMX8M/mkimage_uboot   5.2.3 Copy u-boot-spl.bin from u-boot/spl/u-boot-spl.bin to imx-mkimage/iMX8M/ $ cp uboot-imx/spl/u-boot-spl.bin imx-mkimage/iMX8M/   5.2.4 Copy u-boot-nodtb.bin from u-boot/u-boot-nodtb.bin to imx-mkimage/iMX8M/ $ cp uboot-imx/u-boot-nodtb.bin imx-mkimage/iMX8M/   5.2.5 Copy  imx8mp-evk.dtb from u-boot/arch/arm/dts/ to imx-mkimage/iMX8M/. $cp uboot-imx/u-boot.dtb imx-mkimage/iMX8M/imx8mp-evk.dtb   5.2.6 Copy bl31.bin from Arm Trusted Firmware (imx-atf) to imx-mkimage/iMX8M/ $ cp imx-atf/build/imx8mp/release/bl31.bin imx-mkimage/iMX8M/   5.2.7 Copy the LPDDR4 Training Firmware Download LPDDR Training Firmware cd ~/work wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.16.bin chmod +x firmware-imx-8.16.bin ./firmware-imx-8.16.bin   copy below files from firmware/ddr/synopsys of the firmware-imx package to imx-mkimage/iMX8M/ lpddr4_pmu_train_1d_dmem_202006.bin  lpddr4_pmu_train_1d_imem_202006.bin lpddr4_pmu_train_2d_dmem_202006.bin lpddr4_pmu_train_2d_imem_202006.bin    $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_1d_dmem_202006.bin imx-mkimage/iMX8M/ $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_1d_imem_202006.bin imx-mkimage/iMX8M/ $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_2d_dmem_202006.bin imx-mkimage/iMX8M/ $ cp firmware-imx-8.16/firmware/ddr/synopsys/lpddr4_pmu_train_2d_imem_202006.bin imx-mkimage/iMX8M/    5.2.8 Copy firmware/hdmi/cadence/signed_hdmi_imx8m.bin from the firmware-imx package to imx-mkimage/iMX8M/.   $ cp firmware-imx-8.16/firmware/hdmi/cadence/signed_hdmi_imx8m.bin imx-mkimage/iMX8M/   The folder structure after copying all the necessary files     5.2.9 Build the bootable image run make SOC=iMX8MP flash_evk to generate imx-bootimage. $ cd imx-mkimage $ make SOC=iMX8MP flash_evk The compiled file is flash.bin and its location iMX8M/flash.bin   5.3 flash imx-boot image into i.MX 8MP EVK board   In order to flash the imx-boot image,  please follow the following steps -copy  uuu.exe and flash.bin in a folder -change the board's SW4 (boot mode) to 0001 to enter serial download mode  uuu.exe -b emmc  flash.bin   uuu.exe -b emmc flash.bin -power off the board, change SW4 to switch the board back to 0010 (eMMC boot mode).    6  Running and Debugging   Download the application (iuart_sdma_transfer.bin and iuart_sdma_transfer_cm7.elf) to /run/media/boot-mmcblk1p1   6.1    Debugging Cortex-M while Cortex-A is in U-BOOT   $ fatload mmc 2:1 0x48000000 iuart_sdma_transfer.bin $ cp.b 0x48000000 0x7e0000 30000; $ bootaux 0x7e0000   $ fatload mmc 2:1 0x48000000 iuart_sdma_transfer2.bin $ cp.b 0x48000000 0x7e0000 30000; $ bootaux 0x7e0000 From M7 console, we can see the output   6.2   Debugging Cortex-M while Cortex-A is in Linux   u-boot=> setenv fdtfile 'imx8mp-evk-rpmsg.dtb' u-boot=>run prepare_mcore u-boot=>boot   u-boot=> setenv fdtfile 'imx8mp-evk-rpmsg.dtb' u-boot=>run prepare_mcore u-boot=>boot Linux system boot up:   echo /run/media/boot-mmcblk2p1/iuart_sdma_transfer_cm7.elf > /sys/class/remoteproc/remoteproc0/firmware echo start > /sys/class/remoteproc/remoteproc0/state Then we can see the output from M7 console.   7  Summary   This is a workaround to run UART with SDMA1 enabled on Cortex-M7,  and Linux running on Cortex-A53 in parallel.  In order to do that, we need to modify the ATF, and U-BOOT, and application.   With the above modifications, I can get the expected results.   References: 1. UG10163: i.MX Linux User's Guide Rev LF6.12.20_2.0.0--26 June 2025        
View full article
The documentation is to provide steps for single secure boot for BSP Android 14.0.0_2.0.0. More details related to secure boot for Android BSP can be found from IMX ANDROID SECURE BOOT. However, the steps in this document facilitate some helps signing an Android boot image in the aspects of - First, the Android build process for signing the image, and second, the FDT signing process must be performed after the SPL/FIT of the signing process. The second one of which is crucial.   Best regards Harvey
View full article
    In i.MX93 EVK, it use RGMII in ethernet connection. Some customer use RMII connection. This article describe RMII HW design and SW config.  It listed four cases in attached.  
View full article