i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
The table below contains notable updates to the current release of the Reference Manual. The information provided here is preliminary and subject to change without notice. Affected Modules Issue Summary Description Date - - No issues noted -
查看全文
In the era of digitization, concepts like smart homes and the Internet of Things (IoT) are continuously evolving. To realize these visions, a robust and efficient network infrastructure becomes crucial. OpenWRT, with its open-source nature, high customizability, and excellent stability, has become a key player in leading the future development of networks. NXP, as a global leader in semiconductor technology innovation, leverages its expertise in embedded systems and communication to introduce an intelligent network solution based on OpenWRT, empowering the flourishing smart home and IoT ecosystems. This article will explore the current status and ways to access NXP's chip support for the wireless router solution, enabling readers to build a solid foundation for the next generation of networks. 1. Unique Features of OpenWRT 1.1. Noble Value of Open Source Freedom OpenWRT stands out with its open-source nature, granting users unlimited freedom to access, modify, and share the source code, unlocking significant innovation potential. This openness not only drives continuous technological advancements but also allows users to take active control of the network direction, saving costs. 1.2. Stable and Reliable Network Foundation Built on a mature Linux kernel, OpenWRT undergoes extensive evolution and fine-tuning, ensuring outstanding system stability. This results in fewer network failures, longer device lifespans, and solid support for various network needs. OpenWRT becomes an ideal choice for building reliable home networks, alleviating concerns about network instability or crashes. 1.3. Powerful Software Package Management OpenWRT's proud software package management system provides users with great flexibility. Users can freely install, update, and uninstall various applications and services based on their needs, achieving a highly personalized network environment for a smarter networking experience. OpenWRT allows users to install various network services and applications such as VPNs and proxy servers to meet specific network requirements, providing greater freedom to create a network environment that suits individual or family needs. 1.4. Strong Community Support The vast OpenWRT community is the source of its powerful driving force. Users can exchange experiences, solve problems, and even participate in project development within the community. This collaborative spirit propels continuous innovation and progress in OpenWRT. 2. Applications of NXP wireless router Solution 2.1. Construction of Smart Home Ecosystem The seamless integration of NXP's wireless router solution with the NXP Matter solution provides an ideal platform for users to build smart home ecosystems. With its powerful customization capabilities, users can easily connect, manage, and control various smart devices, creating a highly intelligent home environment. The solution integrates NXP's Bluetooth and Wi-Fi chip drivers, such as IW612, 88W9098, 88W8997, allowing users to effortlessly build an OpenThread Border Router (OTBR) or Zigbee Bridge based on OpenWRT. 2.2. Customized Network Services The NXP wireless router solution supports the customized installation of various network services and applications. Users can create personalized network services, such as VPNs, proxy servers, home routers, or gateways, based on their individual needs, achieving a more flexible networking experience. 2.3. Transmission of High-Definition Video Streams The transmission of high-definition video streams in smart homes imposes higher demands on network performance. NXP's wireless router solution, with its excellent network performance, combined with NXP's industrial-grade IP Camera solution, ensures users can smoothly enjoy high-definition video streams, providing a superior home entertainment experience. 2.4. Construction of Smart Security Systems Security systems are an essential part of smart homes. NXP's wireless router solution, with its advanced network security features, builds a more reliable and intelligent security system for users, enhancing home security. 3. NXP's Support for OpenWRT Given the numerous advantages and wide-ranging application scenarios of wireless router, NXP early on adapted to support OpenWRT. Full support has been provided for the entire Layerscape series processors, and mainstream IMX processors are also supported. The specific supported IMX platforms and details are as follows: Processor and Board Support         ARMv8                                             ARMv7       I.MX93EVK                                •      I.MX6ULL       I.MX8MPlus       I.MX8MMini       I.MX8MNano       I.MX8MQuad OpenWrt Version  Based on OpenWrt v23.05 from mainline (tag: v23.05.0-rc1) Toolchain: ARMV8: gcc-11.3, binutils-2.37 ARMV7: gcc-12.3, binutils-2.40 U-Boot Boot Loader IMX LF release, tag: lf-5.15.71-2.2.1 v2022.04 Linux Kernel       OpenWrt kernel 5.15.114 based on IMX SDK release kernel v5.15.71_2.2.1 Firmware       firmware-imx-8.18       firmware-sentinel-0.5.1 Main Features       Squashfs rootfs support on SD card.       Supported CLI and web configuation. - U-Boot: lf-5.15.71-2.2.1. - Arm Trusted firmware (TF-A) integration. - Boot from SDHC       Linux Kernel Core - Linux kernel 5.15.114 - Cortex-A53 (AARCH64), little endian for imx8m platform - Cortex-A55 (AARCH64), little endian for imx93 platform - Cortex-A7, little endian for imx6ull platform - 64-bit effective kernel addressing [Cortex-A53/A55]       Linux Kernel Drivers - SDIO 3.0 / eMMC5.1 - USB 3.0/2.0 Dual-Role with PHY type C - 32-bit LPDDR4 - 2x Gigabit Ethernet with AVB, IEEE 1588, EEE   and 1x w/ TSN - PCIe Gen 3 + WIFI - CAN FD - Dual-ch. QuadSPI (XIP) or 1x OctalSPI(XIP) - RTC Licensing The majority of the software included in the OpenWrt release is licensed under a form of open source license (e.g. GPL, BSD). Some software is licensed under the NXP EULA license. 4. How to Start Deploying and Using wireless router? To experience the powerful features of the Layerscape series chips with wireless router, download the source code from the official OpenWRT repository: https://git.openwrt.org/openwrt/openwrt.git. The OpenWRT support code for Layerscape is already integrated into the official OpenWRT codebase. Taking IMX8MMini-EVK as an example, here are the deployment steps for wireless router on the IMX platform using Ubuntu 22.04: 4.1. Get the source code from GitHub: https://github.com/nxp-imx/imx_openwrt (Tag: imx_v23.05_v5.15.114) 4.2. Compile, Install, and Configure wireless router: $ ./scripts/feeds update -a; ./scripts/feeds install -a; cp config.default .config; make -j $ sudo dd if=/mnt/tftpboot/imx8/matter_20230908/openwrt-imx-imx8-imx8mmini-squashfs-sdcard.img of=/dev/sdX bs=1M && sync This way, an wireless router bootable disk for SD card has been generated. You can directly use an SD card to boot and experience wireless router. For more compilation assistance, please refer to the README file in the source code: target/linux/imx/README. 4.3. Configuration and Personalization Users can access the wireless router device through the web interface or SSH to begin configuring and personalizing the network environment. This includes setting network rules, installing software packages, and ensuring that the device operates according to individual needs. The following image shows the interface for installing and removing software. Isn't it simple and convenient! 4.4. What to Do If You Encounter Issues? Firstly, you can seek support in the vibrant OpenWRT community. You can not only get assistance but also share your development or usage experiences and even participate in project development. This open community provides users with more opportunities for learning and growth, collectively driving continuous progress in OpenWRT. You can also participate in the official NXP community at https://community.nxp.com/t5/i-MX-Processors/bd-p/imx-processors to ask questions and share technical insights. Professional engineers are available to help you troubleshoot and overcome challenges. NXP OpenWRT looks forward to your participation!   Disclaimer This wireless router release is an NXP's Systems Engineering Initiative and is not part of NXP's Linux base enablement strategy for its MPU platforms. NXP does not vouch for the quality of this release and any follow up releases including adding support to new platforms is at the sole discretion of the Systems Engineering team. For specific requirements or needs please reach out to NXP's systems engineering team on the following email address "[email protected]."
查看全文
    Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknamed Cobalt, is a significant rework of the Xenomai 2.x system. Cobalt implements the RTDM specification for interfacing with real-time device drivers. The native linux version, an enhanced implementation of the experimental Xenomai/SOLO work, is called Mercury. In this environment, only a standalone implementation of the RTDM specification in a kernel module is required, for interfacing the RTDM-compliant device drivers with the native kernel. You can get more detailed information from Home · Wiki · xenomai / xenomai · GitLab       I have ported xenomai 3.1 to i.MX Yocto 4.19.35-1.1.0, and currently support ARMv7 and tested on imx6ulevk/imx6ull14x14evk/imx6qpsabresd/imx6dlsabresd/imx6sxsabresdimx6slevk boards. I also did stress test by tool stress-ng on some boards.      You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm.git, and git checkout Linux-4.19.35-1.1.0. (which inlcudes all patches and bb file) and add the following variable in conf/local.conf before build xenomai by command bitake xenomai.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" DISTRO_FEATURES_remove = "optee" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" DISTRO_FEATURES_remove = "optee" If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. The following is test result by the command (/usr/xenomai/demo/cyclictest -p 50 -t 5 -m -n -i 1000 😞 //Mecury on 6ULL with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 128M --metrics-brief policy: fifo: loadavg: 6.08 2.17 0.81 8/101 534 T: 0 (  530) P:99 I:1000 C:  74474 Min:     23 Act:  235 Avg:   77 Max:    8278 T: 1 (  531) P:99 I:1500 C:  49482 Min:     24 Act:   32 Avg:   56 Max:    8277 T: 2 (  532) P:99 I:2000 C:  36805 Min:     24 Act:   38 Avg:   79 Max:    8170 T: 3 (  533) P:99 I:2500 C:  29333 Min:     25 Act:   41 Avg:   54 Max:    7069 T: 4 (  534) P:99 I:3000 C:  24344 Min:     24 Act:   51 Avg:   60 Max:    7193   //Cobalt on 6ULL with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 128M --metrics-brief policy: fifo: loadavg: 7.02 6.50 4.01 8/100 660 T: 0 (  652) P:50 I:1000 C: 560348 Min:      1 Act:   10 Avg:   15 Max:      71 T: 1 (  653) P:50 I:1500 C: 373556 Min:      1 Act:    9 Avg:   17 Max:      78 T: 2 (  654) P:50 I:2000 C: 280157 Min:      2 Act:   14 Avg:   20 Max:      64 T: 3 (  655) P:50 I:2500 C: 224120 Min:      1 Act:   12 Avg:   15 Max:      57 T: 4 (  656) P:50 I:3000 C: 186765 Min:      1 Act:   31 Avg:   19 Max:      53   //Cobalt on 6qp with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M --metrics-brief policy: fifo: loadavg: 8.11 7.44 4.45 8/156 1057 T: 0 (  917) P:50 I:1000 C: 686106 Min:      0 Act:    3 Avg:    5 Max:      53 T: 1 (  918) P:50 I:1500 C: 457395 Min:      0 Act:    3 Avg:    5 Max:      49 T: 2 (  919) P:50 I:2000 C: 342866 Min:      0 Act:    2 Avg:    4 Max:      43 T: 3 (  920) P:50 I:2500 C: 274425 Min:      0 Act:    3 Avg:    5 Max:      58 T: 4 (  921) P:50 I:3000 C: 228682 Min:      0 Act:    2 Avg:    6 Max:      46   //Cobalt on 6dl with stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief policy: fifo: loadavg: 3.35 4.15 2.47 1/122 850 T: 0 (  729) P:50 I:1000 C: 608088 Min:      0 Act:    1 Avg:    3 Max:      34 T: 1 (  730) P:50 I:1500 C: 405389 Min:      0 Act:    0 Avg:    4 Max:      38 T: 2 (  731) P:50 I:2000 C: 304039 Min:      0 Act:    1 Avg:    4 Max:      45 T: 3 (  732) P:50 I:2500 C: 243225 Min:      0 Act:    0 Avg:    4 Max:      49 T: 4 (  733) P:50 I:3000 C: 202683 Min:      0 Act:    0 Avg:    5 Max:      38   //Cobalt on 6SX stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M  --metrics-brief policy: fifo: loadavg: 7.51 7.19 6.66 8/123 670 T: 0 (  598) P:50 I:1000 C:2314339 Min:      0 Act:    3 Avg:    8 Max:      60 T: 1 (  599) P:50 I:1500 C:1542873 Min:      0 Act:   15 Avg:    8 Max:      72 T: 2 (  600) P:50 I:2000 C:1157152 Min:      0 Act:    4 Avg:    9 Max:      55 T: 3 (  601) P:50 I:2500 C: 925721 Min:      0 Act:    5 Avg:    9 Max:      57 T: 4 (  602) P:50 I:3000 C: 771434 Min:      0 Act:    6 Avg:    6 Max:      41   //Cobalt on 6Solo lite stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M  --metrics-brief policy: fifo: loadavg: 7.01 7.04 6.93 8/104 598 T: 0 (  571) P:50 I:1000 C:3639967 Min:      0 Act:    9 Avg:    7 Max:      60 T: 1 (  572) P:50 I:1500 C:2426642 Min:      0 Act:    9 Avg:   11 Max:      66 T: 2 (  573) P:50 I:2000 C:1819980 Min:      0 Act:   11 Avg:   10 Max:      57 T: 3 (  574) P:50 I:2500 C:1455983 Min:      0 Act:   12 Avg:   10 Max:      56 T: 4 (  575) P:50 I:3000 C:1213316 Min:      0 Act:    7 Avg:    9 Max:      43   //Cobalt on 7d with stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief policy: fifo: loadavg: 5.03 5.11 5.15 6/107 683 T: 0 (  626) P:50 I:1000 C:6842938 Min:      0 Act:    1 Avg:    2 Max:      63 T: 1 (  627) P:50 I:1500 C:4561953 Min:      0 Act:    4 Avg:    2 Max:      66 T: 2 (  628) P:50 I:2000 C:3421461 Min:      0 Act:    0 Avg:    2 Max:      69 T: 3 (  629) P:50 I:2500 C:2737166 Min:      0 Act:    3 Avg:    2 Max:      71 T: 4 (  630) P:50 I:3000 C:2280969 Min:      0 Act:    2 Avg:    1 Max:      33   //////////////////////////////////////// Update for Yocto L5.10.52 2.1.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.52 2.1.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm and git checkout xenomai-5.10.52-2.1.0. Updating: 1, Upgrade Xenomai to v3.2 2, Enable Dovetail instead of ipipe. Copy xenomai-arm to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. //////////////////////////////////////// Update for Yocto L5.15.71 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.15.71 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm and git checkout xenomai-5.15.71-2.2.0. Updating: 1, Upgrade Xenomai to v3.2.2 Copy xenomai-arm to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch.   ///////// Later update for Later Yocto release, please refer to the following community post //////////// 移植实时Linux方案Xenomai到i.MX ARM64平台 (Enable real-time Linux Xenomai on i.MX ARM64 Platform)   
查看全文
Background   Wake-on-LAN ( WoL) is an Ethernet computer networking standard that allows a computer to be turned on or awakened from sleep mode by a network message. The message is usually sent to the target computer by a program executed on a device connected to the same local area network. Ethernet connections, including home and work networks, wireless data networks, and the Internet itself, are based on frames sent between computers. WoL is implemented using a specially designed frame called a magic packet, which is sent to all computers in a network, among them the computer to be awakened. The magic packet contains the MAC address of the destination computer. This is an identifying number, built into each network interface controller (NIC)/Ethernet Controller, that enables the NIC/EnetController to be uniquely recognized and addressed on a network What is a WOL Magic packet? The magic packet is a frame that is most often sent as a broadcast and that contains anywhere within its payload 6 bytes of all 255 (FF FF FF FF FF FF in hexadecimal), followed by sixteen repetitions of the target computer's 48-bit MAC address, for a total of 102 bytes. it is typically sent as a UDP datagram to port 0 (reserved port number), 7 (Echo Protocol) or 9 (Discard Protocol) or directly over Ethernet using EtherType 0x0842   Configure iMX93EVK to wake up on an Ethernet Wake On LAN Magic Packet   Pre-requisite:- Install 'Wake on  LAN' utility on windows from the Microsoft Store. This utility uses Port 7 to send magic packet as a broadcast to the devices on the network.   Step-1 Make the dts change to enable wake-up functionality on eth1   In the following dts:- arch/arm64/boot/dts/freescale/imx93-11x11-evk.dts   You would see the node entry for the corresponding ethernet, eth1 as eqos. Add fsl,magic-packet; to the node     After building the changes, boot with the imx93evk image.   Step-2 Enable wake on LAN By default in linux user-space the wake-on-lan is disabled, to enable the wake-on-lan run:  ethtool -s eth1 wol g     Now you are all set to wake up imx93evk via Ethernet WOL packet. Put the iMX93 to deep sleep via 'echo mem > /sys/power/state'   Step-3 Send WOL magic packet via Wake On LAN windows utility to wake up iMX93EVK   Make sure the devices are connected to the same local network like imx93evk and laptop connected to the same L2 switch. Add your imx93evk device to Wake on LAN software, you have to give iMX93EVK's MAC address of the ethernet that the RJ45 cable is connected to[you can get this from 'ifconfig -a' output].     After adding the device, it will look something like below:-     Right-click on the 'imx' device which is registered on Wake on LAN UI and click on 'Send WOL(magic packet)'. The moment you do that the WOL packet is sent to your iMX from your Laptop/PC on the same network and the iMX is woken up from deep sleep.     Hope you found it helpful. Please drop in any questions/comments just in case. 
查看全文
Sometimes we need to use an SPI bus to communicate with sensors or another device. Unfortunately, by default on iMX8MN-EVK, we have the ECSPI2 disabled on our BSP.   We can use that peripheral on Linux enabling it in the device tree.   To enable the ECSPI2 on the device tree we have to add the next on imx8mn-evk.dtsi:     status = "okay"; }; +&ecspi2 { + #address-cells = <1>; + #size-cells = <0>; + fsl,spi-num-chipselects = <1>; + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_ecspi2 &pinctrl_ecspi2_cs>; + cs-gpios = <&gpio5 13 GPIO_ACTIVE_LOW>; + status = "okay"; + + spidev0: spi@0 { + reg = <0>; + compatible = "rohm,dh2228fv"; + spi-max-frequency = <500000>; + }; +}; + &fec1 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_fec1>;   On iomux node:   + pinctrl_ecspi2: ecspi2grp { + fsl,pins = < + MX8MN_IOMUXC_ECSPI2_SCLK_ECSPI2_SCLK 0x82 + MX8MN_IOMUXC_ECSPI2_MOSI_ECSPI2_MOSI 0x82 + MX8MN_IOMUXC_ECSPI2_MISO_ECSPI2_MISO 0x82 + >; + }; + + pinctrl_ecspi2_cs: ecspi2cs { + fsl,pins = < + MX8MN_IOMUXC_ECSPI2_SS0_GPIO5_IO13 0x40000 + >; + }; + pinctrl_ir_recv: ir-recv { fsl,pins = < MX8MN_IOMUXC_GPIO1_IO13_GPIO1_IO13 0x4f    after modifying and compiling the device tree you can see the device active like this:     Connection:   Test: spidev_test -D /dev/spidev1.0 -v       You can use the devsheell of yocto to make the changes:   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-Devshell-to-compile-device-tree-files/ta-p/1727428
查看全文
  For some applications, we need to reduce the CPU Frequency, but if you are not familiar with our BSP or our devices probably you need some help to do some configurations.   In this post, I will share the configuration to set up lower frequencies (100MHz, 200MHz, 400Mhz, 600MHz, 800MHz, and 1000MHz) on iMX8MP, iMX8MN, and iMX8MM.   Note: Works on Kernel 6.1.xx (not tested on oldest BSP)   1- We have to modify the PLL driver to set the proper parameters to lower frequencies. The file to modify is "clk-pll14xx.c" adding the following lines:   https://github.com/nxp-imx/linux-imx/blob/770c5fe2c1d1529fae21b7043911cd50c6cf087e/drivers/clk/imx/clk-pll14xx.c#L57   static const struct imx_pll14xx_rate_table imx_pll1416x_tbl[] = { PLL_1416X_RATE(1800000000U, 225, 3, 0), PLL_1416X_RATE(1600000000U, 200, 3, 0), PLL_1416X_RATE(1500000000U, 375, 3, 1), PLL_1416X_RATE(1400000000U, 350, 3, 1), PLL_1416X_RATE(1200000000U, 300, 3, 1), PLL_1416X_RATE(1000000000U, 250, 3, 1), PLL_1416X_RATE(800000000U, 200, 3, 1), PLL_1416X_RATE(750000000U, 250, 2, 2), PLL_1416X_RATE(700000000U, 350, 3, 2), PLL_1416X_RATE(600000000U, 300, 3, 2), + PLL_1416X_RATE(400000000U, 200, 3, 2), + PLL_1416X_RATE(200000000U, 200, 3, 3), + PLL_1416X_RATE(100000000U, 200, 3, 4), };   2- Once the pll driver has been modified, only we have to add the values on the opp-table according to the device that you will use.   2.1- For iMX 8MP:   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp.dtsi         a53_opp_table: opp-table { compatible = "operating-points-v2"; opp-shared; + opp-100000000 { + opp-hz = /bits/ 64 <100000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0x8a0>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-200000000 { + opp-hz = /bits/ 64 <200000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0x8a0>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-400000000 { + opp-hz = /bits/ 64 <400000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0x8a0>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-600000000 { + opp-hz = /bits/ 64 <600000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0x8a0>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-800000000 { + opp-hz = /bits/ 64 <800000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0x8a0>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-1000000000 { + opp-hz = /bits/ 64 <1000000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0x8a0>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; opp-1200000000 { opp-hz = /bits/ 64 <1200000000>;   2.2 For iMX8MM:   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mm.dtsi     a53_opp_table: opp-table { compatible = "operating-points-v2"; opp-shared; + opp-100000000 { + opp-hz = /bits/ 64 <100000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xe>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-200000000 { + opp-hz = /bits/ 64 <200000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xe>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-400000000 { + opp-hz = /bits/ 64 <400000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xe>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-600000000 { + opp-hz = /bits/ 64 <600000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xe>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-800000000 { + opp-hz = /bits/ 64 <800000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xe>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-1000000000 { + opp-hz = /bits/ 64 <1000000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xe>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; opp-1200000000 { opp-hz = /bits/ 64 <1200000000>;   2.3- For iMX8MN:   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mn.dtsi   compatible = "operating-points-v2"; opp-shared; + opp-100000000 { + opp-hz = /bits/ 64 <100000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xb00>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + + opp-200000000 { + opp-hz = /bits/ 64 <200000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xb00>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + + opp-400000000 { + opp-hz = /bits/ 64 <400000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xb00>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + + opp-600000000 { + opp-hz = /bits/ 64 <600000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xb00>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + + opp-800000000 { + opp-hz = /bits/ 64 <800000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xb00>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + + opp-1000000000 { + opp-hz = /bits/ 64 <1000000000>; + opp-microvolt = <850000>; + opp-supported-hw = <0xb00>, <0x7>; + clock-latency-ns = <150000>; + opp-suspend; + }; + opp-1200000000 { opp-hz = /bits/ 64 <1200000000>; opp-microvolt = <850000>;   After that, you should note the changes under Linux.   These commands return information about the system and the current settings.   • The kernel is pre-configured to support only certain frequencies. The list of frequencies currently supported can be obtained from: cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies   • To get the available scaling governors: cat /sys/devices/system/cpu/*/cpufreq/scaling_available_governors   • To check the current CPU frequency: cat /sys/devices/system/cpu/*/cpufreq/cpuinfo_cur_freq   The frequency is displayed depending on the governor set.   • To check the maximum frequency: cat /sys/devices/system/cpu/*/cpufreq/cpuinfo_max_freq   • To check the minimum frequency: cat /sys/devices/system/cpu/*/cpufreq/cpuinfo_min_freq   These commands set a constant CPU frequency:   • Use the maximum frequency: echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor   • Use the current frequency to be the constant frequency: echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor   • The following two commands set the scaling governor to a specified frequency, if that frequency is supported.   If the frequency is not supported, the closest supported frequency is used:   echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor echo <frequency> > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed    
查看全文
this is tested with MX93(A1) EVK running 6.1.55_2.2.0 pre-build image.   USB can output test patterns with either one of the setup below: 1. through device node: root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# cat role gadget root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo host > role [ 2672.864083] ci_hdrc ci_hdrc.0: EHCI Host Controller [ 2672.868996] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1 [ 2672.893320] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00 [ 2672.899314] hub 1-0:1.0: USB hub found [ 2672.909235] hub 1-0:1.0: 1 port detected root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# cat role host root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 4 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 3 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 2 > port_test root@imx93evk:/sys/kernel/debug/usb/ci_hdrc.0# echo 1 > port_test   2. use memtool to program registers for i in $(find /sys -name control | grep usb);do echo on > $i;echo "echo on > $i";done; echo host > /sys/kernel/debug/usb/ci_hdrc.0/role #Offset:184h USB_OTG1 base address: 4C10_0000h base address USB_OTG2 base address: 4C20_0000h Register address Register address:base address+offset $ /unit_tests/memtool 0x4c100184 1 # Force to output Test Packet for Eye Diagram Test $ /unit_tests/memtool 0x4c100184=0x18041215 #Force to output J_STATE $ /unit_tests/memtool 0x4c100184=0x18011215 #Force to output K_STATE $ /unit_tests/memtool 0x4c100184=0x18021215 #Force to output SE0 (host) / NAK (device) $ /unit_tests/memtool 0x4c100184=0x18031215
查看全文
Hey everyone !! This piece covers how to configure the iMX93EVK board to wake up Cortex A55[ running Linux] from Cortex M33 core[running a bare metal application].    We will be using UART console on Cortex M33 to signal Cortex A55 via RPMSG to wake-up from deep sleep.   This can be done as follows:-   1. Boot iMX93EVK with RPMSG enabled DTB and load M33 binary via UBOOT   After booting to Uboot terminal, set the fdtfile variable to <rpmsg dtb> that will help us enable rpmsg in the kernel.   u-boot=> setenv fdtfile imx93-11x11-evk-rpmsg.dtb u-boot=> setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=${mmcroot}   then, load the M33 binary from the eMMC partition    u-boot=> fatload mmc 0:1 0x80000000 imx93-11x11-evk_m33_TCM_power_mode_switch.bin 18996 bytes read in 14 ms (1.3 MiB/s)   u-boot=> cp.b 0x80000000 0x201e0000 0x4a34 u-boot=> saveenv Note:-  Do not run the M33 core via bootaux at this point, instead just boot to Linux   u-boot=> boot         2. Starting the Cortex M33 core from Cortex A55[running Linux]   Once linux is up, load the elf of Cortex M33 power mode switch application.   echo ~/power_mode_switch.elf > /sys/devices/platform/imx93-cm33/remoteproc/remoteproc0/firmware   start the M33 core   echo start > /sys/devices/platform/imx93-cm33/remoteproc/remoteproc0/state   On console of Cortex M33 you will see the output as below:-   The log below shows the output of the power mode switch demo in the terminal window: ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ Start SRTM communication Task 1 is working now #################### Power Mode Switch Task #################### Build Time: Nov 10 2023--15:15:16 Core Clock: 200000000Hz Select the desired operation Press A to enter: Normal RUN mode Press B to enter: WAIT mode Press C to enter: STOP mode Press D to enter: SUSPEND mode Press W to wakeup A55 core Press M for switch M33 Root Clock frequency between OD/ND. Waiting for power mode select.. ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~   M33 at this point is ready to wake up the A55 core.     3. Put A55 core to deep sleep and trigger a wakeup from M33 console   To put A55 to deep sleep   echo mem > /sys/power/state you will see something like below on linux console:-     At this point, A55 core is in deep sleep power saving mode. So the A55 console will not respond to any of the key presses. Go on, give it a try 🙂   Now to wake up this core, go to M33 serial console and type 'W'  This will wake up A55 core and you will see the logs denoting that the core has woken up:-   That's it! that's how you exercise UART wake-up functionality on imx93evk. Please feel free to drop any follow-up questions or additional thoughts on this.
查看全文
Dynamic debug is designed to allow you to dynamically at runtime  enable/disable  kernel code to obtain additional kernel information. Currently, if ``CONFIG_DYNAMIC_DEBUG`` is set, then all ``pr_debug()``/``dev_dbg()`` and ``print_hex_dump_debug()``/``print_hex_dump_bytes()`` calls can be dynamically enabled per-callsite.    
查看全文
Symptoms   Trying to initialize a repo, for example:  $repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml we have the below log: File "/home/username/bin/repo", line 51 def print(self, *args, **kwargs): ^ SyntaxError: invalid syntax   Workaround (1)   The first workaround consist in change the python alternatives (caused when you have installed two or more python versions). NOTE: in my case, the python version that i want to change as first priority is python3.8 $sudo update-alternatives --install /usr/bin/python python /usr/bin/python3.8 1   Then we run: $sudo update-alternatives --config python    To verify if your python priority was changed successfully try: $python --version   You should see the version configured as priority number 1.     Workaround (2)   The workaround is very simple, only we need modify the repo file $ nano ~/bin/repo   and we will change the python interpreter in the first line (from python to python3): ORIGINAL FILE   EDITED FILE   After to do this change, repo will works fine again.     I hope this can helps to you!   Best regards.
查看全文
  Environment i.MX8MP EVK, SDK2.15   The default rpmsg buffer size in SDK is 512Bytes(16 Bytes header + 496Bytes payload). This knowledge base will try to change the default buffer size in rpmsg framework. Steps:   1.Modify rpmsg payload size in SDK PATH: SDK\evkmimx8mp_rpmsg_lite_str_echo_rtos_imxcm7\rpmsg_config.h     //! RL_BUFFER_PAYLOAD_SIZE //! //! Size of the buffer payload, it must be equal to (240, 496, 1008, ...) //! [2^n - 16]. Ensure the same value is defined on both sides of rpmsg //! communication. The default value is 496U. #define RL_BUFFER_PAYLOAD_SIZE (1008)     2. Modify buffer size in rpmsg linux framework and buffer pool in dts. PATH: drivers/rpmsg/virtio_rpmsg_bus.c            arch/arm64/boot/dts/freescale/imx8mp-evk-rpmsg.dts   Test steps:   Modify the send buffer in imx_rpmsg_tty.c     #define MSG "hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world! hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world! hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!"       Modify buffer limitation in SDK PATH: evkmimx8mp_rpmsg_lite_str_echo_rtos_imxcm7\main_remote.c     /* Globals */ static char app_buf[1024]; /* Each RPMSG buffer can carry less than 512 payload */       Terminal output We can see that the MAX buffer size received in SDK is not limited to 512Bytes     Nameservice sent, ready for incoming messages... Get Message From Master Side : "hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world! hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world! hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!hello world!" [len : 674]       If we use a larger buffer like 2022 Bytes, we will see error when driver load.     [ 2673.447384] imx_rpmsg_tty virtio0.rpmsg-virtual-tty-channel-1.-1.30: message is too big (2022) [ 2673.456271] imx_rpmsg_tty virtio0.rpmsg-virtual-tty-channel-1.-1.30: rpmsg_send failed: -90 [ 2673.465556] imx_rpmsg_tty virtio0.rpmsg-virtual-tty-channel-1.-1.30: rpmsg_dev_probe: failed: -90 [ 2673.474496] imx_rpmsg_tty: probe of virtio0.rpmsg-virtual-tty-channel-1.-1.30 failed with error -90          
查看全文
We are pleased to announce that Config Tools for i.MX v15.0 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...)Version 15.0 • The product is based on Eclipse 2023-06 TEE – Setting a security level for a special three-state model is improved. Pins – Validation to ensure that elements can be configured by the selected core is added. – Rows are sorted in the Peripheral Signals routing dialog. – A connected pins column in External User Signals always shows the pin's full name. – The missing scroll bar in the External User Signals view is fixed. Clocks – Support for multicore code generation is added. – Global configuration elements now support a tree structure and can be categorized. – Fractional PLL now supports a custom range and negative numerator. – Scrolling in the clock diagram by pressing the mouse wheel (drag and drop) is supported. DCD – The issue with the code generation that stopped working after the drag and drop of a group is fixed.  
查看全文
i.MX6 Series - Crystal Drive Level guidance; includes calculator.  
查看全文
some customers doesn't have any issue on old bsp, but have bring up issue on new 6.1 bsp, this article is about this and how to fix this
查看全文
Hello there. Here is a good way to use U-boot in an efficient way with custom scripts. The bootscript is an script that is automatically executed when the boot loader starts, and before the OS auto boot process. The bootscript allows the user to execute a set of predefined U-Boot commands automatically before proceeding with normal OS boot. This is especially useful for production environments and targets which don’t have an available serial port for showing the U-Boot monitor. This information can be find in U-Boot Reference Manual.   I will take the example load a binary file in CORTEX M4 of IMX8MM-EVK. In my case, I have the binary file in MMC 2:1 called gpio.bin and I will skip those steps because that is not the goal.   First, you need the u-boot-tools installed in your Linux machine: sudo apt install u-boot-tools   That package provide to us the tool mkimage to convert a text file (.src, .txt) file to a bootscript file for U-Boot.   Now, create your custom script, in this case a simple script for load binary file in Cortex M4: nano mycustomscript.scr  and write your U-Boot commands: fatload mmc 2:1 0x80000000 gpio.bin cp.b 0x80000000 0x7e0000 0x10000 bootaux 0x7e0000   Now we can convert the text file to bootscript with mkimage. Syntax: mkimage -T script -n "Bootscript" -C none -d <input_file> <output_file> mkimage -T script -n "Bootscript" -C none -d mycustomscript.scr LCM4-bootscript   This will create a file called LCM4-bootscript (Or as your called it).   A way to load this bootscript file to U-Boot is using the UUU tool, in U-Boot set the device in fastboot with command: u-boot=> fastboot 0 Then in linux with the board connected through USB to PC run the command: sudo uuu -b fat_write LCM4-bootscript mmc 2:1 LCM4-bootscript   Now we have our bootscript in U-Boot in MMC 2:1.   Finally, we can run the bootscript in U-Boot: u-boot=> load mmc 2:1 ${loadaddr} LCM4-bootscript 158 bytes read in 2 ms (77.1 KiB/s) u-boot=> source ${loadaddr} ## Executing script at 40400000 6656 bytes read in 5 ms (1.3 MiB/s) ## No elf image at address 0x007e0000 ## Starting auxiliary core stack = 0x20020000, pc = 0x1FFE02CD...   And the Cortex M4 booted successfully:    I hope this can helps to you.   Best regards.   Salas.  
查看全文
This document intends to provide an overview of the i.MX8 Boot process and walk you through the process of creating a bootable image.   Boot process Coming out of a reset state the i.MX8 ROM (firmware that is stored in non-volatile memory of the i.MX8) reads the boot mode pins to determine the boot media/device that will be used. The i.MX8 can boot out of the following boot devices: eMMC/SD card FlexSPI Flash NAND Serial Download Protocol (USB) - This is used in manufacturing mode to bring-up a board by downloading an image to RAM and then flashing the on-board boot device.   The following table indicates the available options on a i.MX8QXP, the i.MX8 reads the boot mode pads and based in the configuration selects the desired boot device.   Once the boot device has been identified, ROM configures the boot media and attempts to read the image from a predefined address in the boot device, the following table shows the addresses where the image is expected to be on different boot devices. ROM loads data from the predefined addresses above (depending on the selected boot device) to the System Controller Unit (SCU) internal memory (tightly coupled memory) and parses it to find the image container. It can also boot by downloading an image through USB.   The image container has all the information needed to load all the images to the system, the first images that get loaded are the System Controller Firmware (SCFW) and Security Controller Firmware (SECO). The SECO FW needs to be loaded to refresh the watchdog timer (kick the dog) in the device, if the SECO FW is not loaded before the watchdog expires the device will reset, this usually happens when the device fails to fetch a valid image from the boot media.   Once the SCFW is loaded, ROM jumps to it and starts executing it. The SCFW then initializes the DDR and starts loading the images for the Cortex-M4 (optional) and the Cortex-A cores (optional). Once the images are loaded to their destination memory the SCFW boots the cores and sets them in their start address.   Creating a bootable image As a recap a bootable image is comprised of as minimum the System Controller Firmware and the Security Controller Firmware, optionally it can contain images for the Cortex M4 cores (if more than one available as in the case of QM devices) and Cortex A cores. It is possible to boot an image that only contains the SCFW and SECO FW, this could be useful in the first stages of porting the SCFW to the target board. It is also possible to boot an image with only the Cortex-M4 image (baremetal, FreeRTOS, AutoSAR...), only the Cortex-A image (U-boot or any bootloader) or both Cortex-M4 and Cortex-A images.   Mkimage tool The tool in charge of merging all these images and creating a bootable image for the i.MX8 is called mkimage, and can be obtained in source form in the following repository: https://github.com/nxp-imx/imx-mkimage mkimage is only supported in Linux So the first step is to clone the mkimage repository into our machine and checkout the latest branch, at the time of writing this document the latest release is 4.14.98_02: git clone https://source.codeaurora.org/external/imx/imx-mkimage cd imx-mkimage git checkout imx_4.14.98_2.0.0_ga‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ You should now be able to see the following folders:   Getting the SCFW Now that you have the mkimage tool you need some actual images to work with, if you are using a custom board you might need to port the SCFW and DDR configuration files for it (depending on how close it follows NXP's reference board).   The following is a compendium of documents on the basics of the SCFW and how to build it from scratch you can go there if you need help getting started with the porting process: https://community.nxp.com/docs/DOC-342654   If you are trying this on one of NXP's reference board you can use a pre-built SCFW binary, this can be obtained through the building process of the Yocto project or by downloading the porting kit and following these steps: Dowload SCFW binaries for release 4.14.98_02 here. chmod a+x imx-sc-firmware-1.2.bin ./imx-sc-firmware-1.2.bin‍‍‍‍‍‍‍‍‍‍ You will prompted to accept a license agreement and after that the binaries will be extracted:   Getting the SECO FW The Security Controller Firmware is only distributed in binary form and can be obtained from the NXP website. Download SECO FW binaries for release 4.14.98_02 here. chmod a+x firmware-imx-8.1.bin ./firmware-imx-8.1.bin‍‍‍‍‍‍‍‍‍‍ You will prompted to accept a license agreement and after that the binaries will be extracted: The SECO FW is under firmware/seco mx8qm-ahab-container.img -----> SECO FW for QM devices mx8qx-ahab-container.img ------> SECO FW for QXP devices   Getting an image for the Cortex-M4 The image for the Cortex-M4 can be generated using the SDK: https://mcuxpresso.nxp.com/en/select Just select the device you are working with and click Build MCUXpresso SDK, then you will prompted to select your IDE and host. Click on Download SDK and a compressed file containing the SDK will be dowloaded to your computer. Now you only need to uncompress the file and follow the steps in the getting started document to generate the image.  The getting started document includes steps to setup the toolchain and build an image for the M4. An M4 binary for the QM and QXP MEKs is also attached in this document, the example outputs a hello world message on the M4 terminal. Getting an image for the Cortex-A  The bootloader for the Cortex-A cores can be obtained through the Yocto BSP: The steps on generating the image for the 4.14.98 release can be found here: https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga    Some more details on the Yocto BSP can be found here: https://community.nxp.com/docs/DOC-94849   All the required binaries to create a bootable image for the Cortex-A cores on the MEK platforms are attached here.   Building a bootable image Once all the required pieces have been built/obtained, the bootable image can be created. The SCFW, SECO FW and respective Cortex-M4/A images need to be copied to the folder for the target device, i.e. if you are building an image for an i.MX8QX variant copy the binaries for that variant to its folder:   Here is a list of the required files to build a bootable image: scfw_tcm.bin -------------------------------------------- System Controller Firmware binary for the target board mx8qm(qx)-ahab-container.image ---------------- Security Controller Firmware for the QM or QXP variants bl31.bin --------------------------------------------------- ARM Trusted Firmware binary (Required if using u-boot with ATF) Only needed to create Cortex-A image with u-boot u-boot.bin ------------------------------------------------ U-boot binary (optional) m4_image ----------------------------------------------- M4 binary image, the QM variant has 2 Cortex-M4s and in this case to M4 binaries might be required (optional)   Once the required binaries have been copied to the desired variant folder (QXP or QM in this example), you are ready to start building some images.   All the targets for building different images are defined on the soc.mak file contained in each folder, this file contains different examples for creating a lot of the supported bootable images.   Creating a SCFW only image The target used to create a SCFW only image is flash_b0_scfw and it is defined under the soc.mak file of each variant. To invoke this target for QXP from the imx-mkimage directory: make SOC=iMX8QX flash_b0_scfw‍‍‍ To invoke this target for QM from the imx-mkimage directory: make SOC=iMX8QM flash_b0_scfw‍‍‍   The target definition for flash_b0_scfw can be seen below. Definition for QXP: flash_scfw flash_b0_scfw: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin ./$(MKIMG) -soc QX -rev B0 -dcd skip -append mx8qx-ahab-container.img -c -scfw scfw_tcm.bin -out flash.bin ‍‍‍‍‍‍‍‍ Definition for QM: flash_b0_scfw: $(MKIMG) mx8qm-ahab-container.img scfw_tcm.bin ./$(MKIMG) -soc QM -rev B0 -dcd skip -append mx8qm-ahab-container.img -c -scfw scfw_tcm.bin -out flash.bin‍‍‍‍‍‍   Creating a Cortex-A image only The target used to create a Cortex-A image only is called flash_b0. To invoke this target for QXP from the imx-mkimage directory: make SOC=iMX8QX flash_b0 ‍‍‍ To invoke this target for QM from the imx-mkimage directory: make SOC=iMX8QM flash_b0‍ ‍‍‍ The target definition for flash_b0 can be seen below. Definition for QXP:   flash flash_b0: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QX -rev B0 -append mx8qx-ahab-container.img -c -scfw scfw_tcm.bin -ap u-boot-atf.bin a35 0x80000000 -out flash.bin‍‍‍‍ Definition for QM:   flash_b0: $(MKIMG) mx8qm-ahab-container.img scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append mx8qm-ahab-container.img -c -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍   Creating a Cortex-M4 image only The target used to create a Cortex-m4 image only is called flash_b0_cm4 on QXP and QM has different targets since there are two M4s available in the system. To invoke this target for QXP from the imx-mkimage directory: make SOC=iMX8QX flash_b0_cm4‍‍ To invoke this target for QM from the imx-mkimage directory: // For Cortex-M4_0 only make SOC=iMX8QM flash_b0‍_cm4‍_0 // For Cortex-M4_1 only make SOC=iMX8QM flash_b0‍_cm4‍_1 // For both Cortex-M4_0 and Cortex-M4_1 make SOC=iMX8QM flash_b0‍_m4‍s_tcm ‍‍‍‍‍‍‍‍‍‍‍‍‍   The target definition for flash_b0_cm4 can be seen below. Definition for QXP: flash_cm4 flash_b0_cm4: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin m4_image.bin ./$(MKIMG) -soc QX -rev B0 -append mx8qx-ahab-container.img -c -scfw scfw_tcm.bin -p1 -m4 m4_image.bin 0 0x34FE0000 -out flash.bin‍‍‍‍ Definitions for QM: flash_b0_cm4_0: $(MKIMG) mx8qm-ahab-container.img scfw_tcm.bin m4_image.bin ./$(MKIMG) -soc QM -rev B0 -dcd skip -append mx8qm-ahab-container.img -c -scfw scfw_tcm.bin -p1 -m4 m4_image.bin 0 0x34FE0000 -out flash.bin flash_b0_cm4_1: $(MKIMG) mx8qm-ahab-container.img scfw_tcm.bin m4_image.bin ./$(MKIMG) -soc QM -rev B0 -dcd skip -append mx8qm-ahab-container.img -c -scfw scfw_tcm.bin -p1 -m4 m4_image.bin 1 0x38FE0000 -out flash.bin flash_b0_m4s_tcm: $(MKIMG) mx8qm-ahab-container.img scfw_tcm.bin m40_tcm.bin m41_tcm.bin ./$(MKIMG) -soc QM -rev B0 -dcd skip -append mx8qm-ahab-container.img -c -scfw scfw_tcm.bin -p1 -m4 m40_tcm.bin 0 0x34FE0000 -m4 m41_tcm.bin 1 0x38FE0000 -out flash.bin‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   The examples above are for M4 images booting from TCM, the M4 is capable of booting and executing from DDR and it is also able to XIP (execute in place) from SPI memory, for examples on this targets please look at the soc.mak for the desired variant. Creating an image with both Cortex-A and Cortex-M4 images The target used to create an image with software for all the cores is called flash_linux_m4. To invoke this target for QXP from the imx-mkimage directory: make SOC=iMX8QX flash_linux_m4‍ ‍ To invoke this target for QM from the imx-mkimage directory: make SOC=iMX8QM flash_linux_m4‍ ‍ The target definition for flash_linux_m4 can be seen below. Definition for QXP: flash_linux_m4: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin u-boot-atf.bin m4_image.bin ./$(MKIMG) -soc QX -rev B0 -append mx8qx-ahab-container.img -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a35 0x80000000 -p3 -m4 m4_image.bin 0 0x34FE0000 -out flash.bin‍‍   Definition for QM: flash_linux_m4: $(MKIMG) mx8qm-ahab-container.img scfw_tcm.bin u-boot-atf.bin m4_0_image.bin m4_1_image.bin ./$(MKIMG) -soc QM -rev B0 -append mx8qm-ahab-container.img -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -p3 -m4 m4_0_image.bin 0 0x34FE0000 -p4 -m4 m4_1_image.bin 1 0x38FE0000 -out flash.bin‍‍     Flash image This will create a bootable image named flash.bin, to flash this image to the SD card and boot it on your MEK simply do: sudo dd if=iMX8QX/flash.bin of=/dev/mmcblkX bs=1k seek=32‍‍‍‍‍‍‍ If the desired target is a QM variant change if=iMX8QX... to if=iMX8QM. Then match your SD card device on "of=/dev/mmcblkX" you can see how your SD card enumerates by typing lsblk on your console before and after inserting your SD card. Remember from the information above that the i.MX8 will search for the image at 32k on the SD card, that is why we are flashing it there. For more examples please look at the soc.mak file, it includes examples for different boot media (NAND/QSPI) as well as different configurations and usage.   Additional resources Reference Manual Chapter 5 System Boot SCFW API and Port document imx-mkimage README System Controller Firmware 101 
查看全文
Symptoms   On i.MX8MP, when inputting a 80% duty, 0.4V-1.8V, 3KHz square wave, we observed that the system may hang. We also tested i.MX8MN and i.MX8MM and observed the same phenomenon. In i.MX8MN RM, there's a note in GPC chapter:     We believe that the issue described in this note exists not only in the iMX8MN, but also in the iMX8MP and iMX8MM. Meanwhile, there is not only a problem with power down in this issue, but also a problem with wait mode. Diagnosis   In debugging, we find that avoiding accessing LPCR_A53_AD register in imx_set_cluster_powerdown can fix the issue. So we think that due to frequently power up/down of cores, cores have chances failed to power up. When the IRQ behavior become more complex, because the IRQ is an async event, it will come in any time. if the wait mode is enabled, in some conner case, the GPC internal LPM mode state machine will run into problem, then lead to system failure. Solution   1. A workaround patch that bypass the wait mode setting during the cpuidle.. See the patch attached. 2. Will add the Note about "SCU power down should not be enabled in wait mode" to i.MX8MP and i.MX8MM RM. 3. Will try to identify this issue into errta document, ticket TKT0632147.
查看全文
Hardware i.MX 93 EVK​ TFT LCD 480x272 RGB888 (NV3047E, parallel)​ Condition A55 off​ DDR self-refresh​ OCRAM for framebuffer, TCM for code/data​ LCDIF on with parallel interface​ M33 update panel content each second​ 255KB single frame buffer(RGB565) (fit in OCRAM: 0x20480000 ~ 0x204DFFFF)​ Code Bitbucket:ssh://[email protected]/mpucnse/imx93-cm33-usecase.git​ Branch: imx93_sdk_2.14.1-lcd_on_ocram​ Demo code: imx93-cm33-usecase/boards/mcimx93evk/demo_apps/lcd_on_ocram​ DTS: imx93-cm33-usecase/boards/mcimx93evk/demo_apps/lcd_on_ocram/dts​ Working Flow   ​Test Flow In uboot console,​ setenv mmcargs $mmcargs clk-imx93.mcore_booted​ setenv fdtfile imx93-11x11-evk-lcd_panel.dtb​ fatload mmc 1:1 0x80000000 sdk20-app.bin;cp.b 0x80000000 0x201e0000 0x10000;bootaux 0x1ffe0000 0​ boot​ In kernel console,​ echo mem > /sys/power/state​ start the power test Power Consumption SoC power: 94.4mW​ [email protected]​ CM33@100MHz​ CM33@100MHz​ A55 suspend​ DDR retention​ WAKEUPMIX off​ NICMIX and MEDIAMIX on​  ​  
查看全文
This is a simple document for recording some known-how and tips for building up the Windows 10 IoT development environment for i.MX platform. It can only be used as a complement for official document in BSP package (Guide/Release Note/etc.). Applicable for: Windows 10 IoT, i.MX BSP v1.4.1 (date to Nov/2023) Please refer to the PDF attached.
查看全文
Board : i.MX93 EVK BSP: imx L6.1.1-1.0.0 Gui guider: 1.6.1   We have a GUI software tool called GUI Guider. It is a user-friendly graphical user interface development tool from NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library. The GUI demo can run on the i.MX93EVK board. (https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER)   This document will show you an example how the buttons(gpio) on the EVK to interacting with the GUI. Basically, customer could use the same method to use the gpio pins to control everything.   On the i.MX93 EVK board, there are two buttons BTN1 and BTN2. They are connected to GPIO IO23 and GPIO IO24. Below is the schematic.    Buttons on the board.      SW1005 on the board   In the EVK's device tree file, need to change the pinmux for the two buttons like this: pinctrl_spdif: spdifgrp { fsl,pins = < // MX93_PAD_GPIO_IO22__SPDIF_IN 0x31e // MX93_PAD_GPIO_IO23__SPDIF_OUT 0x31e MX93_PAD_GPIO_IO23__GPIO2_IO23 0x31e MX93_PAD_GPIO_IO24__GPIO2_IO24 0x31e >; note: all the pins are defined in imx93-pinfunc.h.   For getting the input value of the buttons in user's space, I use the sysfs gpio. Build the imx-image-multimedia image first and then select the GPIO_SYSFS in kernel's menuconfig.   $ DISTRO=fsl-imx-xwayland MACHINE=imx93evk source imx-setup-release.sh -b build-xwayland $ bitbake imx-image-multimedia   After the build completed, go to the kernel's menuconfig to select the GPIO sysfs. $ bitbake linux-imx -c menuconfig [*] General setup-> Configure standard kernel features (expert users) [*] Device Drivers->GPIO Support-> /sys/class/gpio/... (sysfs interface)   Build the whole image again by "$ bitbake imx-image-multimedia".   Using the UUU to program the image to the EMMC on the EVK board. uuu -b emmc_all imx-image-multimedia-imx93evk.rootfs.wic.zst   Connect the LVDS to the board. Use the corresponding dtb to boot the board. In u-boot, set the dtb file. => setenv fdtfile imx93-11x11-evk-boe-wxga-lvds-panel.dtb => saveenv   Then restart the board. After the board boot up, it will look like below.     You need to calibrate the LVDS touch screen before it can normally use. Please use this command: $ weston-touch-calibrator LVDS-1     Now, build the GUI guider example. I use the Air Conditioner example. Download the GUI guider from the gui-guider web page: https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER   Follow the steps from the below web page to build the i.MX BSP and the gui example code. https://docs.nxp.com/bundle/GUIGUIDERUG-1.6.1/page/topics/yocto.html   After the gui-guider build completed, use the 'scp' command to transfer the gui_guider executable file to the board. Execute the command on your host PC like this: $ scp bld-imx93evk/tmp/work/armv8a-poky-linux/gui-guider/1.6.0-r0/image/usr/bin/gui_guider root@<Your Board IP address>:/ Note: You could use a router to connect your board and your host PC. They are on the same network so could use the 'scp' command to transfer the file to your board.   On your board, type the following commands to execute the gui. $ chmod 755 gui_guider $ ./gui_guider &   Then the GUI is running like this:   Now, let me explain how to find out the gpio number. Type the following command to show the mapping addresses of gpio. root@imx93evk:/# cat /sys/kernel/debug/gpio gpiochip3: GPIOs 0-31, parent: platform/47400080.gpio, 47400080.gpio: gpiochip0: GPIOs 32-63, parent: platform/43810080.gpio, 43810080.gpio: gpiochip1: GPIOs 64-95, parent: platform/43820080.gpio, 43820080.gpio: gpio-64 ( |cd ) in hi IRQ ACTIVE LOW gpio-71 ( |regulator-usdhc2 ) out lo gpiochip2: GPIOs 96-127, parent: platform/43830080.gpio, 43830080.gpio: gpiochip6: GPIOs 472-477, parent: i2c/0-001a, wm8962, can sleep: gpiochip5: GPIOs 478-487, parent: platform/adp5585-gpio.1.auto, adp5585-gpio, can sleep: gpio-479 ( |regulator-audio-pwr ) out hi gpio-483 ( |regulator-can2-stby ) out hi ACTIVE LOW gpio-486 ( |enable ) out hi gpiochip4: GPIOs 488-511, parent: i2c/1-0022, 1-0022, can sleep: gpio-492 ( |Headphone detection ) in lo IRQ gpio-501 ( |? ) out hi gpio-502 ( |regulator-vdd-12v ) out hi gpio-505 ( |reset ) out lo gpio-507 ( |? ) out hi gpio-508 ( |reset ) out lo ACTIVE LOW   The gpio pins of two buttons are GPIO2_IO23 and GPIO2_IO24. They are belongs to gpio2. In the imx93.dtsi, the gpio2's address is "gpio2: gpio@43810080". So, base on the information output from "/sys/kernel/debug/gpio", the gpio2 is mapping to "gpiochip0: GPIOs 32-63". So, the GPIO2_IO23 is 32+23=55, and the GPIO2_IO24 is 32+24=56.   To verify the gpio number is correct or not. We could do the following test. root@imx93evk:/# echo 55 > /sys/class/gpio/export root@imx93evk:/# echo in > /sys/class/gpio/gpio55/direction root@imx93evk:/# echo 56 > /sys/class/gpio/export root@imx93evk:/# echo in > /sys/class/gpio/gpio56/direction   Then, run these two commands to check the values. root@imx93evk:/# cat /sys/class/gpio/gpio55/value root@imx93evk:/# cat /sys/class/gpio/gpio55/value   When the button is not pressed, the value is 1. When press the button, the value is 0.  We could add the same in the GUI's custom.c. Open the GUI Guider software and add the code in the custom.c. /********************* * INCLUDES *********************/ #include <stdio.h> #include <stdlib.h> #include <unistd.h> #include <errno.h> #include <fcntl.h> #include "lvgl.h" #include "custom.h" #include "ui_Aircon.h" #include "guider_customer_fonts.h" /********************** * STATIC VARIABLES **********************/ int fdbtn1,fdbtn2,fdgpio; int btn1_pressed; int btn2_pressed; char btn1_value, btn2_value; void custom_func(void) { fdbtn1 = open("/sys/class/gpio/gpio55/value", O_RDWR); fdbtn2 = open("/sys/class/gpio/gpio56/value", O_RDWR); read(fdbtn1, &btn1_value, 1); read(fdbtn2, &btn2_value, 1); if(btn1_value=='0' && btn1_pressed) { btn1_pressed=0; ui_aircon_update_temp(0, kAIRCON_TempUp); } if(btn1_value=='1') btn1_pressed=1; if(btn2_value=='0' && btn2_pressed) { btn2_pressed=0; ui_aircon_update_temp(0, kAIRCON_TempDown); } if(btn2_value=='1') btn2_pressed=1; close(fdbtn1); close(fdbtn2); } void custom_init(lv_ui *ui) { fdbtn1 = open("/sys/class/gpio/gpio55/value", O_WRONLY); if (fdbtn1 == -1) { fdgpio = open("/sys/class/gpio/export", O_WRONLY); write(fdgpio,"55",3); write(fdgpio,"56",3); close(fdgpio); fdgpio = open("/sys/class/gpio/gpio55/direction", O_WRONLY); write(fdgpio,"in",3); close(fdgpio); fdgpio = open("/sys/class/gpio/gpio56/direction", O_WRONLY); write(fdgpio,"in",3); close(fdgpio); } else close(fdbtn1); ... ... ... ...   Add the custom_func() in the custom.h. #ifndef __CUSTOM_H_ #define __CUSTOM_H_ #ifdef __cplusplus extern "C" { #endif #include "gui_guider.h" void custom_init(lv_ui *ui); + void custom_func(void);   Also, need to add the custom function() into the dead loop in main.c.   To modify the code, bld-imx93evk$ vim tmp/work/armv8a-poky-linux/gui-guider/1.6.0-r0/gui-guider-1.6.0/ports/linux/main.c   while(1) { + custom_func(); // <--- Add the custom function here. /* Periodically call the lv_task handler. * It could be done in a timer interrupt or an OS task too.*/ time_till_next = lv_wayland_timer_handler(); #if LV_USE_VIDEO video_play(&guider_ui); #endif /* Run until the last window closes */ if (!lv_wayland_window_is_open(NULL)) { break; }   Re-build the code after modified. bld-imx93evk$ bitbake gui-guider -c compile -f   Build the whole image again. bld-imx93evk$ bitbake gui-guider Then use the 'scp' command to transfer the new gui-guider file to the board.   Finally, you can use the buttons on the EVK board to set the temperature up and down.                          
查看全文