i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Unpack the kit Boards CPU board Debug board Personality board Cables RS-232 serial cable Ethernet straight cable High-speed USB cables with mini AB connectors for OTG High-speed cable with standard A to mini B connectors Mini-USB adaptor Jack to RCA audio/video cable Power Supply 5.0V/2.4A universal power supply kit Paperwork CD-ROMs: Content CD End-User License Agreement Quick Start Guide (this document) Warranty card Freescale Support card Build the platform Connect the Personality board to Debug board. The personality board connects to the Debug board using a 500-pin connector. The connector is keyed to avoid misconnection, so there is only one way to connect these boards. Then, connect the CPU board to the underside of Debug board. Certify the version of bootloader When updating the BSP files of a system, it's recommended to rewrite a right version of bootloader in the target. Connect platform to PC To connect the 3-Stack platform to your host PC: Connect one end of an RS-232 serial cable (included in the kit) to a serial port connector (CON4) on the Debug board and connect the other end to a COM port on the host PC. Configure SW4-1 to ON. Make sure that SW4-8 is ON, to supply power to all three boards. Configure SW4-2 to OFF. Confirm that the Bootstrap switches (SW5–SW10) are set for external NAND boot (see more here) Connect the regulated 5V power supply to the appropriate power adapter. Plug the power adapter into an electrical outlet and the 5V line connector into the J2 (5V POWER JACK) connector on the Debug board. Start a serial console application on your host PC with the following configuration: Baud Rate 115200 Data Bits 8 Parity None Stop Bits 1 Flow Control None On the Debug board, switch the power switch (S4) to 1. The OS image pre-loaded in the 3-Stack board will boot and the debug messages from the bootloader should now appear on the serial console application on your PC See Also For a setting without the Debug board see Demonstration Platform.
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342729 
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341570 
查看全文
Features 1.75" x 2.5" CPU board 4" x 4" Expansion board Board Support Package i.MXL LiteKit drivers: Serial Ethernet I2C (audio, LEDs and Switches) Framebuffer/Video and Touchscreen SD/MMC Audio i.MX21 LiteKit drivers: Serial Ethernet I2C (LEDs and Switches) Framebuffer/Video and Touchscreen SD/MMC Audio USB host GX-Linux baseline distribution GNU X-Tools from Microcross For more information, [click here.]
查看全文
Gstreamer Please, select the gstreamer package in [LTIB] under Package List. Choose the package that you will need. For a complete installation, select all: gstreamer gstreamer-plugins-base gstreamer-plugins-good gstreamer-plugins-bad gstreamer-plugins-bad gstreamer-plugins-ugly What can be done With Gstreamer, it's possible to: i.MX27 ADS Board Video GST Play i.MX27 ADS Board Video GST Encode i.MX27 ADS Board Video GST Video Streaming
查看全文
Current the SSI is set to I2S slave mode in FSL default release BSP. attached the code for how to set it to master mode.
查看全文
Why raising QoS priority for EPDC Eink has been developing higher resolution panel. With higher resolution, TCE underrun problem is observed more easily. Highest QoS priority can provide obvious improvement. What's TCE underrun TCE is Timing Controller Engine which is responsible for TFT scan frame refreshes. The pixel FIFO (PIX_FIFO) is used to load working buffer pixel data for TCE. When FIFO underrun, TCE_UNDERRUN_IRQ interrupt is triggered, and TCE underrun log pops up in kernel log. The pixel data is processed by TCE to generate TFT voltage control pixels for panel. If an underrun occurs, unknown data is used and that can damage the panel. About the patch The patch raises EPDC reading to highest priority (QoS='f'), so the EPDC reading becomes real time channel in MMDC configuration. The patch is based on L4.1.15 kernel. Stress test of unit test can pass with 1920x1440 configuration.
查看全文
1) nfs I burn the uboot to board by mfgtool, then starting the kernel by nfs, when the board boot up, I set a) ipaddr and b)serverip, then I set the c)"setenv nfsroot /home/usuario/fsl-release-bsp/buildimx6q/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/rootfs", this is sample, you need choose correct folder for yours, this is for imx6q, d) set the mdt file,then run the netboot. 2) program uboot to the qspi, then boot from SD card 3) change the mfgtool to program uboot, kernel to the qspi attched the ucl2.xml setenv bootcmd 'run bootargsset; sf probe; sf read ${loadaddr} 0xA00000 0x600000; sf read ${fdt_addr} 0x800000 0x10000; bootz ${loadaddr} - ${fdt_addr}'
查看全文
Hello Community, Freescale’s MFG Tool Updated for Windows Embedded Compact and i.MX6 Platform TES Electronic Solutions (India) Private Limited has updated Freescale MFG tool for Windows Embedded Compact (7/2013) The Tool is tested on TES Electronic solution’s “MAGIK2 Evaluation Board” And Freescale’s “Saber SD” Evaluation Board www.tes-dst.com Thanks, Misbah
查看全文
Created by prathamrahate  For loading u-boot using JTAG, follow the below steps-- 1. Download DDR stress test tool v.2.52 from NXP website. 2. Boot your board into serial mode, by turning all boot switches off 3. Now connect USB cable from USB OTG port to desktop/Laptop on which you will be running DDR stress test tool. 4. For information on using DDR stress test tool refer to documentation. 5. Once board is detected in DDR stress test tool, use appropriate inc script in the tool and click on download. After successful downloading of script , DDR will be initialised. 6. Now connect JTAG cable , and load u-boot.bin image using load_image command from JTAG to appropriate address, for imx6q sabresd board it is 0x17800000. 7. Once image is downloaded successfully, you can resume from same address using resume command like resume 0x178000000 For custom boards, you can use xls provided by NXP to generate inc file for custom board which can be used for loading into DDR stress test tool to initalise DDR. I am using Arm olimex JTAG debugger for debugging. This document was generated from the following discussion: Loading u-boot.bin unsing JTAG on imx6q-sabresd board
查看全文
  The VAR-SOM-SOLO small form factor System-on-Module carries an advanced feature-set and broad connectivity options, making it an ideal solution for customers and products in the embedded market.   Staying on-trend with the market’s shift towards a cost-effective highly integrated off-the-shelf solution, the VAR-SOM-SOLO from Variscite levels the playing ground for a broad spectrum of embedded products. Bringing all the benefits of the widely successful VAR-SOM-MX6, the VAR-SOM-SOLO from Variscite carries much smaller dimensions and a slim lined price-point.  Features include Freescale’s i.MX6 1GHz Cortex-A9, SLC NAND, eMMC, dual band Wi-Fi/BT with MIMO, USB, Gigabit Ethernet, A/V interfaces and industrial operating temperatures. The VAR-SOM-SOLO utilizes a standard SO-DIMM 200pins interface to the carrier board, fully pin-to-pin compatible with the VAR-SOM-MX6.   Ohad Yaniv, Variscite’s CEO, explains the strategy behind the new System-on-Module: “In today’s market, we believe the compact VAR-SOM-SOLO presents a true synergy between an impressive feature set and an affordable price-point. We feel the newly introduced SoM reflects a constantly evolving embedded application concept that requires advanced multimedia features, in a compact and cost efficient solution.”   Key features include:   - Freescale i.MX6 1000MHz single Cortex-A9   - Up to 1GB DDR3, 512MB SLC NAND and 64GB eMMC   - Certified Wi-Fi 802.11 a/b/g/n 2.4/5GHz with optional 2x2 MIMO   - Bluetooth 4.0/BLE   - Full 1080p video encode/decode capability   - Vivante GPU 2D/3D graphics accelerator   - Display: 2x LVDS, HDMI1.4, MIPI DSI   - 10/100/1000 Mbps Ethernet   - USB 2.0: Host, OTG   - PCIe   - Audio In/Out   - Camera inputs: MIPI CSI, parallel   - Dual CAN, UART, I2C, SPI   - Industrial temperature -40 to 85°C   - Dimensions: 33mm x 68mm x 4mm   - OS: Linux Yocto & Ubuntu, Android, WEC 7 & 2013   Availability and Pricing: The VAR-SOM-SOLO is available now. Pricing starts at 42USD. Contact [email protected] or +972 9 9562910 for more information.   About Variscite: Variscite is a leading System on Modules (SoM) and Single-Board-Computer (SBC) design and manufacture company. A trusted provider of development and production services for a variety of embedded platforms, Variscite transforms clients’ visions into successful products.   Learn more about Variscite, visit www.variscite.com    
查看全文
From iMX 3.1x kernel, all kernel debug messages will be print to debug serial port after UART driver loaded, so if the kernel hang up before tty console driver ready, there will be no kernel boot up messages.   The attached patch can be used to enable the iMX serial debug console in early time, then kernel will not buffer the debug messages.   Note: the default patch is for UART1 (tty0) as the debug port, if you need use other debug port, please modify the code "early_console_setup()" with correct UART port base address.   L3.10.53-Add-early-console-for-debug-message.patch This patch is based on L3.10.53_GA1.1.0 release, it can support iMX6S/DL/D/Q.   L3.14.52-Add-early-console-for-debug-message.patch This patch is based on L3.14.52_GA1.1.0 release, it can support iMX6S/DL/D/Q, iMX6SL, iMX6SX, iMX6UL and iMX7.  
查看全文
On behalf of Gopise Yuan. This is a debugging patch for adding support for showing interrupt status (same as ‘cat /proc/interrupts’) in Sysrq. Can be triggered by “y”. Might be useful for debugging some hang/stuck issue. Note: Only for debugging purpose. Triggering it in normal case may throttle current cpu and cause IPC/RCU abnormal due to long printing to console.
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344779 
查看全文
i.MX 6 SoloX MCC MCC is a library for lightweight communication between cores Configured at compile time (mcc_config.h) Current version (2.0) is not backward compatible MCC works with shared memory area Communication is performed through ‘send’ and ‘receive’ functions Shared memory Cores communicate through shared memory Core structures of the MCC  MCC_ENDPOINT core Identifies a processor core, A9 is 0 and M4 is 1. node In Linux, each process using MCC has its own node number. MQX has only one node number. port Any number of ports per node is allowed. Value MCC_RESERVED_PORT_NUMBER is not allowed. The number of endpoints in system is defined during compile time by macro MCC_ATTR_MAX_RECEIVE_ENDPOINTS. MCC_BOOKEEPING_STRUCT Endpoint table I. MCC API  Functions Standard API −int mcc_initialize(MCC_NODE); −int mcc_destroy(MCC_NODE); −int mcc_create_endpoint(MCC_ENDPOINT*, MCC_PORT); −int mcc_destroy_endpoint(MCC_ENDPOINT*); −int mcc_send(MCC_ENDPOINT*, MCC_ENDPOINT*, void*, MCC_MEM_SIZE, unsigned int); −int mcc_recv(MCC_ENDPOINT*, MCC_ENDPOINT*, void*, MCC_MEM_SIZE, MCC_MEM_SIZE*, unsigned int); −int mcc_msgs_available(MCC_ENDPOINT*, unsigned int*); −int mcc_get_info(MCC_NODE, MCC_INFO_STRUCT*); MCC_SEND_RECV_NOCOPY_API_ENABLED −int mcc_get_buffer(void**, MCC_MEM_SIZE*, unsigned int); −int mcc_send_nocopy(MCC_ENDPOINT*, MCC_ENDPOINT*, void*, MCC_MEM_SIZE); −int mcc_recv_nocopy(MCC_ENDPOINT*, MCC_ENDPOINT*, void**, MCC_MEM_SIZE*, unsigned int); −int mcc_free_buffer(void*);
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344896 
查看全文
There are two ways to enable support for the imx95-19x19-evk board:   1.  Directly replace the flash.bin from the Yocto release. 1). depoly LSDK2512 on imx95-15x15-evk board which is supported in Debian LSDK2512     A:    $ flex-installer -i pf -d /dev/sdX -F     B: $ flex-installer -i auto -m imx95evk -d /dev/sdX   2). Download prebuild flash.bin for imx95-19x19-evk board from Yocto release:     A: download: https://www.nxp.com/webapp/sps/download/license.jsp? colCode=L6.12.20-2.0.0_MX95&appType=file1&DOWNLOAD_ID=null     B: Extract the downloaded file to obtain the flash.bin file: imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all   3). Overwrite flash.bin     $ sudo umount /dev/sdX; sudo dd if=imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all of=/dev/sdX bs=1024 seek=32   4). Insert the prepared SD card into the board and power it on. After entering the U-Boot prompt, set the boot command:     => setenv bootcmd "setenv bootargs 'root=/dev/mmcblk1p3 rw rootwait console=ttyLP0,115200 earlycon';ext2load mmc 1:1 0x90400000 Image;ext2load mmc 1:1 0x93000000 imx95-19x19-evk.dtb;booti 0x90400000 - 0x93000000"; saveenv     => reset   The Debian system will start automatically.   2. Build the BSP image using FlexBuild: 1).  clone the Flexbuild source code and apply the patch as attached. 2). build the bsp and boot images:       $ bld bsp -m imx95evk       $ bld boot -m imx95evk or download the pre-built image at: http://sun.ap.freescale.net/images/debian/lsdk2512/firmware_imx95evk_19x19_sdboot.img 3). install the image:       $ ./flex-installer -f firmware_imx95evk_sdboot.img -d /dev/sdX -m imx95evk -b boot_IMX_arm64_lts_6.12.20.tar.zst -r rootfs_lsdk2512_debian_imx95evk.tar.zst 4).  Insert the prepared SD card into the board and power it on. After entering the U-Boot prompt, run the following command to boot board:       u-boot=> bootflow scan -lb
查看全文
This article describes how to speed-up the Linux boot time on i.MX 6ULZ to under 2s. Software: Linux BSP 6.12.20-2.0.0 Boot device: SD card The attached imx6ulz-fast-boot.tar.gz archive contains a series of patches which reduces the boot time of the i.MX 6ULZ to ~1.9s. What you'll find in the archive: U-Boot patches: Set the BOOTDELAY to 0 in U-Boot Increase the CPU frequency from 396MHz to 792MHz Add quiet to the kernel bootargs, to suppress the kernel's output during boot Kernel patches: Trim down the kernel to create a minimal version Use LZ4 compression type for the kernel image Minimal rootfs based on BusyBox How to? 1. Prepare the Yocto environment according to Section 3, 4, 5 in i.MX Yocto Project User's Guide. Version 6.12.20-2.0.0, for other versions, you may need to make adjustments. 2. Unzip the imx6ulz-fast-boot.tar.gz archive in the sources directory of your Yocto environment just created. cd ~/imx-yocto-bsp/sources tar -xvpzf imx6ulz-fast-boot.tar.gz -C . 3. Remove additional machine features. Add the configuration below in your conf/local.conf: MACHINE_FEATURES:remove = "\ optee \ alsa \ touchscreen screen \ wifi bluetooth \ bcm4339 bcm43455 \ nxp8987-sdio nxpwifi-all-sdio \ rtc qemu-usermode"  4. Build the image. bitbake core-image-busybox The resulted core-image-busybox-imx6ulz-14x14-evk.rootfs.wic should have ~38M. 5. Write the image on an SD card, and boot. It should boot under 2s from reset to prompt. If you are connected to the serial port of the board, press any key continuously to stop in U-Boot.
查看全文
This document explains how to enable and test Bluetooth 6LoWPAN (IPv6 over Low-power Wireless Personal Area Networks) in the i.MX Linux BSP.   Environment   i.MX Linux BSP 6.6.52-2.2.0 (based on Yocto scrathgap) i.MX 93 EVK (2 units) An Embedded Artists 2EL M.2 module with the Murata LBES5PL2EL module (containing NXP IW612) is inserted into the i.MX 93 EVK's M.2 slot and connected to the onboard Wi-Fi/BT antenna. One i.MX 93 EVK will serve as the Peripheral device, while the other will act as the Central device. It should also work with i.MX 8 and 9 series evaluation kit equipped with Bluetooth LE modules.   Configurations   Although the Linux kernel includes a Bluetooth 6LoWPAN driver, it is disabled in the i.MX Linux BSP. Therefore, we will modify the kernel configuration to enable it. Add 2 settings below in kernel configuration file (imx_v8_defconfig) to build the required drivers as modules: CONFIG_6LOWPAN=m CONFIG_BT_6LOWPAN=m These settings can be found in the following section of the Linux kernel menuconfig. CONFIG_6LOWPAN: Depends on: NET [=y] && IPV6 [=y] Location: -> Networking support (NET [=y]) -> Networking options -> 6LoWPAN Support (6LOWPAN [=m]) CONFIG_6LOWPAN  CONFIG_BT_6LOWPAN: Depends on: NET [=y] && BT_LE [=y] && 6LOWPAN [=y] Location: -> Networking support (NET [=y]) -> Bluetooth subsystem support (BT [=y]) -> Bluetooth Low Energy (LE) features (BT_LE [=y]) -> Bluetooth 6LoWPAN support (BT_6LOWPAN [=m]) Rebuild the image containing the Linux kernel and make sure that the required drivers are present in the following paths. /lib/modules/6.6.52-ge0f9e2afd4cf-dirty/kernel/net/6lowpan/6lowpan.ko /lib/modules/6.6.52-ge0f9e2afd4cf-dirty/kernel/net/bluetooth/bluetooth_6lowpan.ko   Operations for Peripheral device   Boot the Peripheral device EVK and log in as the root user. NXP i.MX Release Distro 6.6-scarthgap imx93-11x11-lpddr4x-evk ttyLP0 imx93-11x11-lpddr4x-evk login: root Load the NXP Bluetooth UART driver to enable Bluetooth. # modprobe btnxpuart Start the Bluetooth hci0 interface with the hciconfig command. # hciconfig hci0 up Type hciconfig command to check the BD Address of the Bluetooth hci0 interface and confirm that its status is "UP RUNNING". # hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:12:34:56 ACL MTU: 1021:7 SCO MTU: 120:6 UP RUNNING RX bytes:862 acl:0 sco:0 events:59 errors:0 TX bytes:1085 acl:0 sco:0 commands:58 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT Name: 'imx93-11x11-lpddr4x-evk' Class: 0x200000 Service Classes: Audio Device Class: Miscellaneous, HCI Version: 5.4 (0xd) Revision: 0x8300 LMP Version: 5.4 (0xd) Subversion: 0x1015 Manufacturer: NXP Semiconductors (formerly Philips Semiconductors) (37) Load the Bluetooth 6LoWPAN driver. # modprobe bluetooth_6lowpan Enable Bluetooth 6LoWPAN. # echo 1 > /sys/kernel/debug/bluetooth/6lowpan_enable Start Bluetooth advertising and waits for a connection request from the Central device. # bluetoothctl advertise on   Operations for Central device   Boot the Central device EVK and log in as the root user. NXP i.MX Release Distro 6.6-scarthgap imx93-11x11-lpddr4x-evk ttyLP0 imx93-11x11-lpddr4x-evk login: root Load the NXP Bluetooth UART driver to enable Bluetooth. # modprobe btnxpuart Start the Bluetooth hci0 interface with the hciconfig command. # hciconfig hci0 up Type hciconfig command to check the BD Address of the Bluetooth hci0 interface and confirm that its status is "UP RUNNING". # hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:AB:CD:EF ACL MTU: 1021:7 SCO MTU: 120:6 UP RUNNING RX bytes:862 acl:0 sco:0 events:59 errors:0 TX bytes:1085 acl:0 sco:0 commands:58 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT Name: 'imx93-11x11-lpddr4x-evk' Class: 0x200000 Service Classes: Audio Device Class: Miscellaneous, HCI Version: 5.4 (0xd) Revision: 0x8300 LMP Version: 5.4 (0xd) Subversion: 0x1015 Manufacturer: NXP Semiconductors (formerly Philips Semiconductors) (37) Load the Bluetooth 6LoWPAN driver. # modprobe bluetooth_6lowpan Enable Bluetooth 6LoWPAN. # echo 1 > /sys/kernel/debug/bluetooth/6lowpan_enable Send a connection request to the Peripheral device. (In this example, the BD address of the Peripheral device is D0:17:69:12:34:56.) # echo "connect D0:17:69:12:34:56 1" > /sys/kernel/debug/bluetooth/6lowpan_control After waiting for a few tens of seconds, the bt0 network interface will appear. (At the same time, the bt0 network interface will appear on the Peripheral device that accepted the connection.) # ifconfig bt0 bt0: flags=4161<UP,RUNNING,MULTICAST> mtu 1280 inet6 fe80::d017:69ff:feab:cdef prefixlen 64 scopeid 0x20<link> unspec D0-17-69-AB-CD-EF-00-00-00-00-00-00-00-00-00-00 txqueuelen 1000 (UNSPEC) RX packets 9 bytes 884 (884.0 B) RX errors 0 dropped 4 overruns 0 frame 0 TX packets 13 bytes 1069 (1.0 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 The Central device and Peripheral device are now connected via Bluetooth 6LoWPAN.   Testing Send a ping from the Central device to the Peripheral device. (In this example, the IPV6 address of the Peripheral device is fe80::d017:69ff:fe12:3456.) # ping6 fe80::d017:69ff:fe12:3456%bt0 PING fe80::d017:69ff:fe12:3456%bt0 (fe80::d017:69ff:fe12:3456%bt0) 56 data bytes 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=1 ttl=64 time=181 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=2 ttl=64 time=125 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=3 ttl=64 time=67.7 ms 64 bytes from fe80::d017:69ff:fe12:3456%bt0: icmp_seq=4 ttl=64 time=56.1 ms ...   Benchmarking   Run the iperf3 server on the Peripheral device. # iperf3 -s Run the iperf3 benchmark on the Central device. For example, check the TCP connections. # iperf3 -V -c fe80::d017:69ff:fe12:3456%bt0 You can also check UDP connections. For example, the following example sends UDP 200Kbps bandwidth. # iperf3 -V -c fe80::d017:69ff:fe12:3456%bt0 -u -b 200K   Disclaimer   This document is provided as a reference for utilizing NXP products. Please refer to the official product manuals and application notes for formal specifications. Due to differences in software versions and other conditions, actual behavior may differ from the descriptions provided. This document does not verify all functions, so please be sure to conduct appropriate validation and testing to ensure suitability for your intended use.  
查看全文
We are pleased to announce that Config Tools for i.MX v25.09 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) • The Release Notes format is updated from plain text to markdown. • The newly generated configuration includes the default NXP copyright notice and is licensed under the BSD-3-Clause license. • DDR tool – ODT and Driver Strength Updates for LP4/LP5 on i.MX 943 and i.MX 95 – Improved DRAM Configuration for i. MX 9x devices – Multicore support is enabled for DDR tests on i.MX 943 and i.MX 95 – Linux support for the DDR tool – Vref DQ Setting now available in the GUI – Board-agnostic SM Support for i.MX 943 and i.MX 95 – DDR part number entry is supported in the GUI – Enhanced logging from the target application – Stress test repetition option is enabled – Updated ODT shmoo scenario values on i.MX 943 and i.MX 95 – Support for SNPS FW and PHY Init 2024.09 SP2 on i.MX 943 and i.MX 95 – AHAB image update to align with BSP for CES parts on i.MX 943 and i.MX 95 – New configuration support for 15x15 on i.MX 943 – Improved bus configuration for single-channel setups – LP4/LP5 CS signal configuration now exposed in the GUI for i.MX 943 and i.MX 95 • Clocks – Supported input frequency setting • System Manager – Initial version of the tool
查看全文