i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
1.  Software change for Certification Test Compared to standard Linux/Android release, you may need to do below software changes to implement the certification tests, it is applicable from imx_3.10.31_1.1.0 Linux BSP GA release, for the release before that, user may need to apply the related patches before doing below things, and some examples may be different for former releases, the user needs to change accordingly. See the detailed information in this document “How to do USB Compliance Test for 3.10.y kernel”. And there is also a link describes the patch for USB Certification Test: Patch to make i.MX6DQ USB to support test modes for certification test 2. I.MX6 series USB Certification Guide http://cache.freescale.com/files/microcontrollers/doc/user_guide/IMXUSBCGUG.pdf Include the descriptions of all the Certification Test requirements, equipment, procedures for I.MX6 series. For example, Host/Device High Speed Eye Diagram Test(眼图测试).   3. Description of USBCertification related Registers AN4589 Configuring USB on i.MX 6 Series Processors http://cache.freescale.com/files/32bit/doc/app_note/AN4589.pdf   4. I.MX6Q/I.MX6DL/I.MX6SL/ I.MX6SX Certification Reports, see attachments   5. Checklist and TPL, see attachments. Original Attachment has been moved to: I.MX6SX-Checklist-and-TPL.zip
View full article
Introduction This guide provides a step by step explanation of what is involved in adding a new WiFi driver and making a new WiFi card work well in a custom Android build. (This guide was written for Android 4.1 but should be applicable to previous Android releases and hopefully future releases.) Contents Understand how Android WiFi works Port WiFi driver. Compile a proper wpa_supplicant in your BoardConfig.mk Modify your wifi.c in HAL. Launch wpa_supplicant and dhcpcd services in init.rc. Several debug tips. Understand How Android WiFi Works As the following figure, Android wireless architecture can be divided into three parts: Java Framework(WifiManager, WifiMonitor etc..), HAL(wifi.c,wpa_supplicant,netd) kernel space modules(wireless stack, wifi drivers) Java Framework communicate with wpa_supplicant using native interface (wifi.c). Wpa_supplicant and netd uses wireless extension or nl80211 to control WiFi drivers. Port WiFi driver Usually WiFi driver is provided as a kernel module. There are mainly two types of Android WiFi architecture:nl80211 and wext. With the implementation of nl80211/cfg80211 many wireless drivers in main line kernel  support nl80211 interface instead of wireless extension. For different vendors’ WiFi drivers, writing one Android.mk to add its compile into Android is what you should do. Here take atheros’s AR6kl as an example: ath6kl_module_file :=drivers/net/wireless/ath/ath6kl/ath6kl_sdio.ko $(ATH_ANDROID_SRC_BASE)/$(ath6kl_module_file):$(mod_cleanup) $(TARGET_PREBUILT_KERNEL) $(ACP)         $(MAKE) -C $(ATH_ANDROID_SRC_BASE) O=$(ATH_LINUXPATH) ARCH=arm CROSS_COMPILE=$(ARM_EABI_TOOLCHAIN)/arm-eabi- KLIB=$(ATH_\ LINUXPATH) KLIB_BUILD=$(ATH_LINUXPATH)         $(ACP) -fpt $(ATH_ANDROID_SRC_BASE)/compat/compat.ko $(TARGET_OUT)/lib/modules/         $(ACP) -fpt $(ATH_ANDROID_SRC_BASE)/net/wireless/cfg80211.ko $(TARGET_OUT)/lib/modules/ include $(CLEAR_VARS) LOCAL_MODULE := ath6kl_sdio.ko LOCAL_MODULE_TAGS := optional LOCAL_MODULE_CLASS := ETC LOCAL_MODULE_PATH := $(TARGET_OUT)/lib/modules LOCAL_SRC_FILES := $(ath6kl_module_file) include $(BUILD_PREBUILT) Compile a proper wpa_supplicant in your BoardConfig.mk In Android’s external directory, there are two wpa_supplicant_* projects. For wext-based wifi driver, wpa_supplicant_6 can be used. For nl80211-based WiFi driver, wpa_supplicnat_8 can only be used. But if WiFi vendors supply their own customized wpa_supplicant, it will be much easier to debug the communication between wpa_supplicant and WiFi drivers. No matter which supplicant  you choose, just control their compile in your BoardConfig.mk. Take atheros’s ath6kl as an example: ifeq ($(BOARD_WLAN_VENDOR),ATHEROS) BOARD_WLAN_DEVICE                        := ar6003 BOARD_HAS_ATH_WLAN                      := true WPA_SUPPLICANT_VERSION                  := VER_0_8_ATHEROS WIFI_DRIVER_MODULE_PATH                  := "/system/lib/modules/ath6kl_sdio.ko" WIFI_DRIVER_MODULE_NAME                  := "ath6kl_sdio" WIFI_DRIVER_MODULE_ARG                  := "suspend_mode=3 wow_mode=2 ar6k_clock=26000000 ath6kl_p2p=1" WIFI_DRIVER_P2P_MODULE_ARG              := "suspend_mode=3 wow_mode=2 ar6k_clock=26000000 ath6kl_p2p=1 debug_mask=0x2413" WIFI_SDIO_IF_DRIVER_MODULE_PATH          := "/system/lib/modules/cfg80211.ko" WIFI_SDIO_IF_DRIVER_MODULE_NAME          := "cfg80211" WIFI_SDIO_IF_DRIVER_MODULE_ARG          := "" WIFI_COMPAT_MODULE_PATH                  := "/system/lib/modules/compat.ko" WIFI_COMPAT_MODULE_NAME                  := "compat" WIFI_COMPAT_MODULE_ARG                  := "" endif then you need to provide a proper wpa_supplicant.conf  for your device. wpa_supplicant.conf  is very important because the control socket for android is specified in this file(ctrl_interface=). This file should be copied to /system/etc/wifi. Minimum required config options in wpa_supplicant.conf : There are two different ways in which wpa_supplicant can be configured, one is to use a "private" socket in android namespace, created by socket_local_client_connect() function in wpa_ctrl.c and another is by using a standard UNIX socket. Android private socket ctrl_interface=wlan0 update_config=1 - Unix standard socket ctrl_interface=DIR=/data/system/wpa_supplicant GROUP=wifi update_config=1 Modify your wifi.c in HAL Here what you should do is modifying some codes like wifi_load_driver and wifi_unload_driver. For Broadcom or CSR’s wifi driver, you can directly use the original wifi.c. But for atheros’s ath6kl driver, there are total three  .ko modules to install. So some micro variables and codes need to be changed to adapt it. Launch wpa_supplicant and dhcpcd services in init.rc If you have configured to use android private socket, you should do like this: service wpa_supplicant /system/bin/wpa_supplicant -Dwext -iwlan0 -c / data/misc/wifi /wpa_supplicant.conf socket wpa_wlan0 dgram 660 wifi wifi disabled oneshot or if you have configured to use unix standard socket, you should do like this: service wpa_supplicant /system/bin/wpa_supplicant -Dwext -iwlan0  -c/data/misc/wifi/wpa_supplicant.conf disabled oneshot If WiFi driver is not “wext” but “nl80211”, you should change it to –Dnl80211. For dhcpcd, you should lunch it like the following: service dhcpcd_wlan0 /system/bin/dhcpcd -ABKL     class late_start     disabled oneshot The parameters “-ABKL” can largely enhance wifi connection speed.  About what “ABKL” stand for, you can refer to dhcpcd’s GNU manual. Several debug tips Incorrect permissions will result in wpa_supplicant not being able to create/open the control socket andlibhardware_legacy/wifi/wifi.c won't connect. Since Google modified wpa_supplicant to run as wifi user/group the directory structure and file ownership should belong to wifi user/group (see os_program_init() function in wpa_supplicant/os_unix.c ). Otherwise errors like: E/WifiHW  (  😞 Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": No such file or directory will appear. Also wpa_supplicant.conf should belong to wifi user/group because wpa_supplicant will want to modify this file. How to Enable debug for wpa_supplicant.               By default wpa_supplicant is set to MSG_INFO that doesn't tell much.                    To enable more messages:                 modify common.c and set wpa_debug_level = MSG_DEBUG                 modify common.h and change #define wpa_printf from if ((level) >= MSG_INFO) to if ((level) >= MSG_DEBUG)         3. WiFi driver’s softmac.               For most vendors’ WiFi driver, the mac address is fixed. We should add one softmac rule to let WiFi driver’s mac is unique for each board.
View full article
The init file is a key component of the Android boot sequence. It is a program to initialize the elements of the Android system.  Unlike Linux, Android uses its own initialization program. This Android init program processes 2 files, and it executes the commands it finds in both programs. These programs are: ‘init.rc’ and ‘init<machine name>.rc’ (this machine name is the name of the hardware that Android is running on). What does each program contain?: init.rc provides the generic initialization instructions init<machine name>.rc provides specific initialization instructions init<machine name>.rc is imported by the init.rc program. What is the syntax of these .rc files? The android init language consists of 4 classes of statements: Actions, Commands, Services and Options. Actions and Services declare new sections. All the commands or options belong to the section most recently declared. Actions and Services have to have unique names. If a second Action or Service has the same name of a previous one, it is ignored. Actions Actions are sequences of commands. They have a trigger which is used to determine when the action should occur. Actions take following form. On <trigger> <command> <command> <command>… Services Services are programs which init launches and (optionally) restart when it exists Services take the following form. Service <name> <patchname>  [argument] <option> <option>… Options Options are modifiers to services. These affect how and when init runs a service. Critical This is a device-critical service. If it exits more than four times in four minutes, the device will reboor into recovery mode. Disabled This service will not automatically start with its class. It must be explicitly started by name. Setenv <name> <value> Set the environment variable <name> to <value> in the launched process. User <username> Change to username before executing this service. Currently defaults to root. Group <groupname> [<groupname>] Change to groupname before executing this service. Oneshot Do not restart the service when it exists Class <name> Specify a class name for the service. All services in a named class may be started or stopped together. Onrestart Execute a command when service restarts Triggers Triggers are strings which can be used to match certain kinds of events and used to cause an action to occur. Boot This is the first trigger that will occur when init starts (after /init.conf is loaded) Commands: Exec <path> [<arguments>] Fork and execute a program (<path>). This will block until the program completes execution. Export <name> <value> Set the environment variable <name> equal to <value> in the global environment. Ifup <interface> Bring the network interface <interface> online. Import <filename> Parse and init config file, extending the current configuration. Hostname <name> Set the host name Chdir <directory> Change working directory Chmod <octal-dmoe> <path> Change file access permissions Chwon <owner> <group> <path> Change file owner and group Chroot <directory> Change process root directory Class_start <serviceclass> Start all services of the specified class if they are not already running. Class_stop <serviceclass> Stop all services of the specified class if they are currently running. Domainname <name> Set the domain name Enable <servicename> Turns a disabled service into an enabled one. Insmod <path> Install the module at <path> Mkdir <path> Create a directory at <path> Mount <type><device><dir> Attempt to mount the named device at the directory. Restorecon <path> Restore the file named by <path> to the security context specified in the file_contexts configuration. Setcon <securitycontext> set the current process security context to the specified string. Setenforce 0|1 Set the SELinux system wide enforcing status. 0 = permissive. 1 = enforcing. Setprop <name><value> Set system property <name> to <value> Setrlimit <resource><cur><max> Set the rlimit for a resource Setsebool <name><value> Set SELinux Boolean <name> to <value> Start <service> Start a service Stop <service> Stop a service Symlink <target><path> Create a symbolic link at <path> with the value <target> Trigger <event> Trigger an event. Used to queue an action from another action Wait <path> Poll for the existence of the given file and return when found. Write <path> <string> Open the file at <path> and write a string to it. Examples How to run a script: service my_service /data/test   class main   oneshot Here we are declaring the service named 'my service' with location in /data/test. It belongs to the main class and will start along with any other service that belongs with that class and we declare that the service wont restart when it exits (oneshot). Change file access permissions: chmod 0660   /sys/fs/cgroup/memory/tasks Here we are changing access permissions in path /sys/fs/cgroup/memory/tasks Write a string to a file in a path: write  /sys/fs/cgroup/memory/memory/memory.move_charge_at_immigrate   1 Create a symbolic link: symlink  /system/etc /etc Here we are creating a symbolic link to /system/etc -> /etc Set a specific density of the display: setprop ro.sf.lcd_density 240 Here we are setting a system property of 240 to ro.sf.lcd_density Set your watchdog timer to 30 seconds: service watchdog /sbin/watchdogd 10 20 class core We are petting the watchdog every 10 seconds to get a 20 second margin Change file owner: chown root system /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq The new owner being 'root' from the group 'system'
View full article
Here is a quick summary at booting a Linux system on the i.MX 6 Sabre SD platform, through USB. This assumes you have a "working" Linux development environment at hand (e.g. Debian), and that your are able to build a working Linux system with buildroot already, as explained in this post. You will also need libusb-1.0 development files (headers and libraries), as well as root/sudo permissions to access USB peripherals. Also, we will use the fine imx_usb_loader tool that the nice folks at Boundary Devices have developed for their i.MX 5/6 boards, as it works fine for Sabre sd as well. Get buildroot sources We will use git to fetch buildroot sources: $ git clone git://git.busybox.net/buildroot This should create a buildroot directory with all the latest sources (after a while). Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l '201*', and git checkout <the-desired-tag>. Compile buildroot The beauty of buildroot is that it will take care of everything for you, including preparing a cross compiler. You can configure buildroot for Sabre SD by doing: $ cd buildroot $ make freescale_imx6sabresd_defconfig By default this would generate binaries suitable for booting with an SD card, so we need to tweak a few settings to obtain a ramdisk, which u-boot will like. Summon the configuration menu with the following command: $ make menuconfig Descend into the "Filesystem images" submenu, and select the following buildroot options: cpio the root filesystem (for use as an initial RAM filesystem) Compression method (gzip) Create U-Boot image of the root filesystem Exit, saving your configuration. You might want to verify that you have indeed the the correct options in your .config: $ grep '^BR2_TARGET_ROOTFS_CPIO' .config This should return the following: BR2_TARGET_ROOTFS_CPIO=y BR2_TARGET_ROOTFS_CPIO_GZIP=y BR2_TARGET_ROOTFS_CPIO_UIMAGE=y You may then proceed with the build: $ make This should download and build everything, so it will take a while. Note that, as bryanthomas pointed out, there are no files for the sabre sd in the boards folder. This is because no patches or custom kernel configurations are needed outside of what is defined in the defconfig. So the only place the sabre sd board lives in buildroot is in the configs directory. At the time of writing we still need a small final hack to have Linux boot on /init instead of its default /linuxrc for proper boot on ramdisk, though. Hopefully this should be addressed in a future buildroot version, and a patch is on his way, but for now we change the boot script in our target filesystem with: $ cd output/target $ ln -svf init linuxrc $ cd ../.. $ make All build results will fall under the output/images folder. We are most interested in the following pieces: output/images/ +- imx6q-sabresq.dtb +- rootfs.cpio.uboot +- u-boot.imx `- uImage Get imx_usb_loader sources We will use git to fetch imx_usb_loader sources: $ git clone git://github.com/boundarydevices/imx_usb_loader.git This should create an imx_usb_loader directory with all the latest sources. Compile imx_usb_loader Assuming your Linux development environment has the necessary libusb-1.0 headers and libraries, you can simply build by doing: $ cd imx_usb_loader $ make This should compile an imx_usb tool in the current folder. Prepare your payload and configuration First, copy all the necessary buildroot generated items to the imx_usb_loader directory. You will need: u-boot.imx uImage imx6q-sabresd.dtb rootfs.cpio.uboot Now we need to explain to imx_usb what we want to download to the i.MX romcode through USB. Add the following lines in the end of the mx6_usb_work.conf: ... u-boot.imx:dcd,plug uImage:load 0x12000000 rootfs.cpio.uboot:load 0x12C00000 imx6q-sabresd.dtb:load 0x18000000 u-boot.imx:clear_dcd,jump header The first line with dcd, plug uses u-boot header to configure the DDR3 memory, allowing us to download contents to the Sabre SD memory. This is exactly what the three subsequent lines with load directives do. The last line re-uses u-boot one more time to find out the address where to jump (jump header directive), but not touching the DDR configuration any more thanks to the clear_dcd directive (thanks jeanmariepons-b46892 for the tips) . Look at the comments in mx6_usb_work.conf for (a bit) more details on the various directives available. Also, note that all the absolute addresses mentioned above are what u-boot needed at the time of writing. Hopefully this should be fairly stable. Boot through USB! We are all set for booting now. Connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data. Connect also your PC to the USB OTG port of the Sabre SD, and make sure you have no SD card inserted and power up the platform. The Sabre SD should not boot into an operating system, but rather wait for a payload to download through USB. You might want to verify that it is indeed waiting with the following command: $ lsusb In the resulting output, there should be a line like the following: Bus 001 Device 098: ID 15a2:0054 Freescale Semiconductor, Inc. i.MX 6Dual/6Quad SystemOnChip in RecoveryMode On your PC, start the download of our "payload" to your Sabre SD with: $ sudo ./imx_usb (Note that you need proper permissions to do that.) After download of all the pieces, u-boot should start in its "mfgtools mode", as reflected by the following messages on UART: ... Boot from USB for mfgtools Use default environment for mfgtools Run bootcmd_mfg: run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr}; ... The Linux kernel should then start, and your buildroot system should reach a prompt: ... Welcome to Buildroot buildroot login: From there you may login as root. Enjoy! See also... This post details the buildroot steps a bit more. This post explains how to build a ramdisk for i.MX6 with busybox directly. AdeneoEmbedded - Whitepaper on USB loader for i.MX6 platforms imx_usb_loader README on github Buildroot: making embedded Linux easy
View full article
bitbaked meta-toolchain-qt Install it  with ~/yocto/build/tmp/deploy/sdk$ poky-eglibc-x86_64-arm-toolchain-qt-1.4.1.sh Download Qtcreator from here http://qt-project.org/downloads and Install it to Your home directory edit the bin/qtcreator.sh source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi #! /bin/sh makeAbsolute() {     case $1 in         /*)             # already absolute, return it             echo "$1"             ;;         *)             # relative, prepend $2 made absolute             echo `makeAbsolute "$2" "$PWD"`/"$1" | sed 's,/\.$,,'             ;;     esac } .... To do it before "#! /bin/sh" is IMPORTANT!!!! In QtCreator i set Compiler as                /opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/armv7a-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++ Qt version as                               /opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/qmake sysroot as                     /opt/poky/1.4.1/sysroots/armv7a-vfp-neon-poky-linux-gnueabi Put them in a Kit For connection to Your Board click on  Device  --->    Manage Build a new project and add some to the .pro file Building the image for Your Board: add         EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh" to Your localconfig bitbake core-image-sato-sdk set a password to root  via ssh root@[boardip] passwd test connection via sftp  root@[boardip] start qtcreator ./qtcreator.sh Message was edited by: Joerg Boge Good Video to get more Information about Programming are this Beaglebone: LCD Touchscreen GUI Applications for Embedded Linux - YouTube Beaglebone: Qt Creator for C++ ARM Embedded Linux Development - YouTube Beaglebone: Example Qt Embedded Linux Application - YouTube It is for Beagelbone but for programming Qt it is a good start. Dieses Dokument wurde aus folgender Diskussion erzeugt: Setup QT Creator with Yocto Build
View full article
The patches are based on iMX6 L3.10.53 and 3.14.52 GA BSP.   In default linux BSP, the followed two pathes were supported in kernel driver mxc_v4l2_capture.c: CSI->IC->MEM CSI->MEM   After appied these patches, it can support the followed path: CSI->VDI->IC->MEM CSI->VDI->MEM In this mode, the VDI de-interlace will be handled on the fly, so the whole system bandwidth will be reduced.   Limitations: 1. Since the IC can only output resolution up to 1024*1024, so this is the limation on output. 2. Only VDI motion mode 2 was supported.   mxc_v4l2_tvin.zip: It is the test aplication, test command for CSI->VDI->IC->MEM ("-i 2" means CSI->VDI->IC->MEM path.): ./mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 800 -oh 480 -i 2 -g2d"   test command for CSI->VDI->MEM ("-i 3" means CSI->VDI->MEM path.): ./mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 800 -oh 480 -i 3 -g2d"  
View full article
Freescale LTIB provides only the low level FlexCAN driver, so you can add Canutils and Libsocketcan developed by Pengutronix to have some more functions available on user space and some test and monitoring applications. Adding Flexcan driver support on Kernel On kernel menuconfig, add the following items: [*] Networking support  --->     <*>  CAN bus subsystem support  --->         <*>  Raw CAN Protocol (raw access with CAN-ID filtering)         <*>  Broadcast Manager CAN Protocol (with content filtering)     CAN Device Drivers  --->         <*> Virtual Local CAN Interface (vcan)         [*] CAN devices debugging messages         <*> Freescale FlexCAN Adding Canutils and Libsocketcan Packages on LTIB Download the libsocketcan-0.0.8.tar.bz2 and canutils-4.0.6.tar.bz2 source codes from the links below and save them on your PC at /opt/freescale/pkgs http://www.pengutronix.de/software/libsocketcan/download/libsocketcan-0.0.8.tar.bz2 http://www.pengutronix.de/software/socket-can/download/canutils/v4.0/canutils-4.0.6.tar.bz2 On LTIB directory, create the spec file folders: cd <ltib directory>/dist/lfs-5.1 mkdir canutils mkdir libsocketcan Download the following spec files, unpack them on their respective folders: Can_specs.tar.gz ( attached below ) Now, on ltib directory, unpack, build and deploy them: cd <ltib directory> ./ltib -p libsocketcan.spec -f ./ltib -p canutils.spec -f Testing the FlexCAN network To test the Flexcan network, first set the bitrate and after enable the can port: canconfig can0 bitrate 125000 ifconfig can0 up                                         Now it's possible to test the network connecting two boards: On board 1: cansend can0 -i0x100 11 22 33 44 On board 2: canecho can0 -v Board 2 will show the data coming from board 1.
View full article
Description       This doc explain how to enable the plugin boot on i.MX6Q/6DL and which used for change the pll2 clock and add the spread spectrum support to pass the EMI test. we still list the source codes of 3.0.35 and 4.1.15. to explain the dts/non-dts kernel support.       本文旨在说明如何在i.MX6Q/6DL上实现plugin启动,以支持展频和改变pll2的频率,其目的是为了通过 EMI测试。也附上了基于3.0.35和4.1.15的源代码,以供参考   Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 SabreSDP https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false          Version: MX6Q_PLUGIN_FC_SSC_V7-20200915_chn..pdf(chinese version)add baidou support MX6Q_PLUGIN_FC_SSC_V7-20170504_eng-chapter-imx6dl.doc+MX6Q_PLUGIN_FC_SSC_V3-20170309_eng.doc(english version)      
View full article
Graphics are a big topic in the Android platform, containing java/jni graphic framework and 2d/3d graphic engines (skia, OpenGL-ES, renderscript). This document describes the general Android graphic stack and UI features on Freescale devices. 1. Android Graphic Stacks All Android 3D apps and games have the following graphic stack: Android system UI and all Apps UI follow 2D graphic stack as below, the hardware render will accelerate Android 2D UI with GPU HW OpenGL-ES 2.0 to improve the whole UI performance. Hardware acceleration can be disabled on i.mx6 in device/fsl/imx6/soc/imx6dq.mk USE_OPENGL_RENDERER := false Then rebuild frameworks/base/core/jni, and replace libandroid_runtime.so Surfaceflinger is responsible of all surface layers composition, and  then generate the framebuffer pixmap for display devices. these graphic surface layers are from 2D/3D apps. Hwcomposer is the alternative module of Surfaceflinger with OpenGL-ES. Hwcomposer is used to combine the specific surface layers supported by specific vendor devices. Freescale i.MX6 devices use GPU 2D to combine most surface layers, and the system power can be reduced with GPU 2D instead of GPU 3D. The typical power saving case is video playback. Hwcomposer with GPU 2D can offload GPU 3D task when running game and benchmarks, it is proved to improve the overall system performance about 20%. 2. Performance measurment Show FPS for Android system performance For NFS boot you can set “debug.sf.showfps” to 1 in init.freescale.rc (“setprop debug.sf.showfps 1”) and then reboot the system. For SD or EMMC boot, you can issue command “setprop debug.sf.showfps 1” in console, then find system_server thread by top and kill it to reset the system. Graphic benchmarks for 3D capability measurement Quadrant Full test benchmark cover CPU, Memory, IO, 2D and 3D GLBenchmark http://www.glbenchmark.com/ NenaMark2 https://market.android.com/details?id=se.nena.nenamark2 An3DBench http://www.androidzoom.com/android_applications/tools/an3dbench_hnog.html AnTutu http://www.antutu.com/software.html 3DMark http://www.futuremark.com/benchmarks/3dmark06/introduction/ Browser benchmarks http://www.webkit.org/perf/sunspider/sunspider.html http://v8.googlecode.com/svn/data/benchmarks/current/run.html http://www.craftymind.com/guimark2/ http://www.craftymind.com/factory/guimark/GUIMark_HTML4.html http://themaninblue.com/writing/perspective/2010/03/22/ 3.  Android UI features Dual display with same content This feature is supported in the default image in Android i.MX 6 release package. In this feature, LVDS panel and HDMI output can be supported simultaneously. It is only enabled when the HDMI TV has been connected with the board. Overscan for TV devices Some TVs may miss display the contents in overscan area. To avoid the contents in overscan area being lost, the common implement is by underscanning with an adjustable black border and letitng the viewer adjust the width of the black border. The downscan operation is done by surfaceflinger when it does surface composition through HW OpenGL ES. There is no performance impact since all the work is done by GPU HW. Overscan can be configured in display setting in visual mode: 32 bits color depth 32bpp UI can be supported by adding “bpp=32” in uboot as below: setenv bootargs ‘… video=mxcdi1fb:RGB666,XGA,bpp=32 …’, also can configure it in display setting. Enable 32bpp frame buffer and application surface buffer will be allocate to RGBA8888 format instead of default RGB565 format, that means more system memory is allocated. After enabling 32bpp, if some applications still don't have better UI quality, check to see if  there is hard code to request RGB565 format surface (should request RGBA8888 format to get better quality). Sample code is attached to test for 32bpp (left is on 16bpp, right is on 32bpp) Display Visual Setting The display setting is the add-on feature in FSL Android release, it is very convenient for end-users to change display property, mostly for the following features: Dual display enablement Display color depth setting(16bpp, 32bpp) Overscan adjustment in horizontal and vertical orientation 4. Issue Diagnosis Application Compatibility Some Android applications may not run correctly on some Android releases. It may cause application compatibility, so check the application in other platforms. For example Neocore and Asphalt 5 can run on Eclair, Froyo, and Gingerbread, but will not correctly run on Honeycomb. GPU Compatibility Some game UIs may not correctly display on our Android release. When encountering this kind of issue, the customer can check whether it is caused by the game using an OpenGL extension which our GPU does not support. They can download another data package (for example not extension data package) to have a check. Others Enlarge GPU memory if you encounter UI abnormally displaying after running an application for a while. Some applications need Wifi connections, so monitor the console log to see whether there are any error reports.
View full article
1. To setup the Yocto environment, from the BASE folder run fsl-community-bsp $ . setup-environment build 2. Build the toolchain build $ bitbake meta-toolchain # Other toolchains: # Qt Embedded toolchain build: bitbake meta-toolchain-qte # Qt X11 toolchain build: bitbake meta-toolchain-qt 3. Install it on your PC build $ sudo sh \   tmp/deploy/sdk/poky-eglibc-x86_64-arm-toolchain-<version>.sh 4. Setup the toolchain environment build $ source \   /opt/poky/<version>/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi 5. Get the Linux Kernel's source code. $ git clone git://git.freescale.com/imx/linux-2.6-imx.git linux-imx $ cd linux-imx 6. Create a local branch linux-imx $ BRANCH=imx_3.0.35_4.0.0 # Change to any branch you want,   # Use 'git branch -a' to list all linux-imx $ git checkout -b ${BRANCH} origin/${BRANCH} 7. Export ARCH and CROSS_COMPILE linux-imx $ export ARCH=arm  linux-imx $ export CROSS_COMPILE=arm-poky-linux-gnueabi- linux-imx $ unset LDFLAGS 8. Choose configuration and compile linux-imx $ make imx6_defconfig  linux-imx $ make uImage  9. To Test your changes, copy the `uImage` into your SD Card linux-imx $ sudo cp arch/arm/boot/uImage /media/boot 10. If case you want your changes to be reflected on your Yocto Framework, create the patches following the document i.MX Yocto Project: How can I patch the kernel?
View full article
Share my test procedure in the attachment.
View full article
(DEPRECATED. Please check this document for Real Time Streaming) A server can be streaming video and a client, in this case a i.MX6 target, is receiving and decoding it. For example, a server with GStreamer and a web camera connected, can be streaming with the following command: $ # Pipeline 1 $ gst-launch v4l2src ! 'video/x-raw-yuv, format=(fourcc)I420, width=(int)1280, height=(int)800' ! ffenc_mpeg4 ! tcpserversink host=$CLIENT_IP port=$PORT and on the target, the client receives, decodes and display with $ # Pipeline 2 $ gst-launch tcpclientsrc host=$SERVER_IP port=$PORT  ! 'video/mpeg, width=(int)1280, height=(int)800, framerate=(fraction)10/1, mpegversion=(int)4, systemstream=(boolean)false' ! vpudec ! mfw_isink The filter caps between the tcpclientsrc and the decoder (vpudec) depend on the sink caps coming from the server encoder (ffenc_mpeg4), so these may change depending on your needs. Running the above pipelines require the environment variables SERVER_IP, CLIENT_IP and PORT. In case you want the i.MX6 to act as a server, just change the video source (either mfw_v4lsrc of v4l2src) and the encoder (vpuenc), so $ # Pipeline 3 $  gst-launch v4l2src  !  'video/x-raw-yuv, format=(fourcc)I420, width=(int)640, height=(int)480, interlaced=(boolean)false, framerate=(fraction)10/1'  ! vpuenc ! tcpserversink host=$CLIENT_IP port=$PORT For testing purposes, set SERVER_IP=127.0.0.1, CLIENT_IP=127.0.0.1 and PORT=500, and run pipeline 3 and 2 in two different consoles. Check with 'top' the  CPU usage and see that VPU is actually doing most of the work.
View full article
This document describes the i.MX 8QXP MEK mini-SAS connectors features on Linux and Android use cases, covering the supported daughter cards, the process to change Device Tree (DTS) files or Boot images, and enable these different display options on the board.
View full article
i.MX95 Triple Display Patches for LF-6.6.52-2.2.0 BSP. iMX95 19x19 EVK. qiang_limpu_se_0-1739859470230.png     Patches files: 0001-iMX95-EVK-IT6263-LVDS-to-HDMI-bridge-chip-combine-it.patch Combine IT6263 with simple panel driver, no EDID is needed, 720P and 1080P display mode had been added as two examples.   0002-IT6263-Always-reported-connected-for-force-output.patch Let IT6263 always report cable connected to force output HDMI signals.   0003-iMX95-EVK-add-LVDS-clone-mode-based-on-IT6263.patch LVDS clone mode is supported on two LVDS ports, they output same content and same timing from one DPU display engine (1920*1080@60fps).   0004-iMX95-EVK-add-dual-LVDS-interleaver-mode-based-on-IT.patch LVDS interleave mode is supported on two LVDS ports, they output different content and same timing from one DPU display engine (3840*1080@60fps).   0005-iMX95-EVK-add-triple-display-support.patch Triple display is supported, 1 MIPI DSI + 2 LVDS.  imx95-19x19-evk-triple-display-lvds-clone.dtb: the two LVDS is in clone mode. imx95-19x19-evk-triple-display-lvds-interleaver.dtb: the two LVDS is in interleave mode.   For 1 MIPI DSI + 2 LVDS display clone mode: qiang_limpu_se_0-1739858854733.png For 1 MIPI DSI + 2 LVDS Interleave mode: qiang_limpu_se_2-1739859096402.png     Know issues:  Due to bridge numbers (3) and DPU engine/Pixel link/Pixel Interleaver number (2) is not aligned, during kernel boot up, there will be followed link error log, but there is no real function impact.   [    3.178741] imx95-ldb 4b0c0000.syscon:ldb@4: Failed to create device link (0x180) with 4b010000.syscon:bridge@8 ... [    4.209299] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller [    4.220355] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller ...     2025-8-19 update: Add the patch for L6.12.20_2.0.0 BSP. lf-6.12.20-2.0.0_triple_display_patches.zip   2026-9-7 update: Add patch for L6.18.37_2.1.0 BSP based on FRDM-IMX95.  
View full article
Notes: First run the playback pipeline then the streaming pipeline. The above example streams H263 video and AMR audio data. Change codec format to your needs. In case where the iMX is the streaming machine, the audio encoder 'amrnbenc' must be installed before. This scenario has not been tested Shell variables and pipelines Playback machine (receiver) # On playback machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where PC does the playback     AUDIO_DEC_SINK="rtpamrdepay ! amrnbdec ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! ffdec_h263 ! autovideosink" ## End of IMX2PC Settings ## PC2IMX: Case where iMX does the playback     AUDIO_DEC_SINK="rtpamrdepay ! mfw_amrdecoder ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! vpudec ! mfw_v4lsink " ## End of PC2IMX Settings PLAYBACK_AUDIO="udpsrc caps=\"application/x-rtp,media=(string)audio,clock-rate=(int)8000,encoding-name=(string)AMR,encoding-params=(string)1,octet-align=(string)1\" \             port=5002 ! rtpbin.recv_rtp_sink_1 \         rtpbin. ! $AUDIO_DEC_SINK \      udpsrc port=5003 ! rtpbin.recv_rtcp_sink_1 \      rtpbin.send_rtcp_src_1 ! udpsink port=5007 sync=false async=false" PLAYBACK_VIDEO="udpsrc caps=$VIDEO_CAPS port=5000 ! rtpbin.recv_rtp_sink_0 \         rtpbin. ! $VIDEO_DEC_SINK \         udpsrc port=5001 ! rtpbin.recv_rtcp_sink_0 \         rtpbin.send_rtcp_src_0 ! udpsink port=5005 sync=false async=false" PLAYBACK_AV="$PLAYBACK_VIDEO $PLAYBACK_AUDIO" # Playback pipeline gst-launch -v gstrtpbin name=rtpbin $PLAYBACK_AV Streaming Machine (sender) # On Streaming machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where iMX does the streaming     IP=x.x.x.x # IP address of the playback machine     VIDEO_SRC="mfw_v4lsrc"     VIDEO_ENC="vpuenc codec=h263 ! rtph263ppay "    AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " ## END IMX2PC settings ## PC2IMX: Case where PC does the streaming     IP=y.y.y.y # IP address of the playback machine     VIDEO_SRC="v4l2src"     VIDEO_ENC="ffenc_h263 ! rtph263ppay "     AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " # END PC2PC settings STREAM_AUDIO="$AUDIO_ENC ! rtpbin.send_rtp_sink_1 \         rtpbin.send_rtp_src_1 ! udpsink host=$IP port=5002 \         rtpbin.send_rtcp_src_1 ! udpsink host=$IP port=5003 sync=false async=false \         udpsrc port=5007 ! rtpbin.recv_rtcp_sink_1" STREAM_VIDEO="$VIDEO_SRC ! $VIDEO_ENC ! rtpbin.send_rtp_sink_0 \         rtpbin.send_rtp_src_0 ! queue ! udpsink host=$IP port=5000 \         rtpbin.send_rtcp_src_0 ! udpsink host=$IP port=5001 sync=false async=false \         udpsrc port=5005 ! rtpbin.recv_rtcp_sink_0" STREAM_AV="$STREAM_VIDEO $STREAM_AUDIO" # Stream pipeline gst-launch -v gstrtpbin name=rtpbin $STREAM_AV
View full article
This document explains how to bring-up u-boot & Linux via JTAG This procedure has been tested on: i.MX6 Solo X Sabre SD i.MX6UL EVK Prerequistes: Get the latest BSP for your board. This procedure was tested with L4.1.15. Build the 'core-image-minimal' image to bring-up your board (Detailed steps here) Optional- Build a meta-toolchain for your device 1.- Set board to boot from Serial dowloader mode or set it to boot from the SD card and remove the sd card We basically want the board to stall in boot ROM to attach to the target. 2.- Connect JTAG probe and turn on the board The device should stall trying to establish a connection to download an image, this will allow us to attach to the target. 3.- Load Device Configuration Data In 'normal' boot sequence the boot ROM takes care of reading the DCD and configuring the device accordingly, but in this case we are skipping this sequence and we need to configure the device manually. The script used by Lauterbach to parse and configure the device is called dcd_interpreter.cmm and can be found here. Search for the package for your specific device. The DCD configuration for your board should be on your u-boot directory: yocto_build_dir/tmp/work/<your board>imx6ulevk/u-boot-imx/<u-boot_version>2016.03-r0/git under board/freescale/<name of your board>mx6ul_14x14_evk/imximage.cfg This file (imximage.cfg) contains all the data to bring up DRAM among other early configuration options. 4.- Load U-boot If an SREC file of U-boot is not present build it (meta-toolchain installed required) the SREC file contains all the information required by the probe to load it and makes this process easier. To build the SREC simply type: make <your board defconfig>mx6ul_14x14_evk_defconfig  (all supported boards are found under u-boot_dir/configs) make If you cannot build an SREC or do not want to, you can use the u-boot.imx (located under yocto_build_dir/tmp/deploy/images/<your board name>/) or u-boot.bin files but you will need to figure out the start address and load address for these files, this can be done by examining the IVT on u-boot.imx (here is a useful document explaining the structure of the IVT). Let U-boot run and you should see its output on the console I will try to boot from several sources but it will fail and show you the prompt. 5.- Create RAMDisk After building the core-image-minimal you will have all the required files under yocto_build_dir/tmp/deploy/images/<your board name>/ You will need: zImage.bin - zImage--<Linux Version>--<your board>.bin Device tree blob - zImage--<Linux Version>--<your board>.dtb Root file system - core-image-minimal-<your board>.rootfs.ext4 We need to create a RAMDisk out of the root file system we now have, these are the steps to do so: Compress current Root file system using gzip: gzip core-image-minimal-<your board>.rootfs.ext4 If you want to keep the original file use: gzip -c core-image-minimal-<your board>.rootfs.ext4 > core-image-minimal-<your board>.rootfs.ext4.gz Create RAMDisk using mkimage: mkimage -A arm -O linux -T ramdisk -C gzip -n core-image-minimal -d core-image-minimal-<your board>.rootfs.ext4.gz core-image-minimal-RAMDISK.rootfs.ext4.gz.u-boot Output: Image Name: core-image-minimal Created: Tue May 23 11:28:55 2017 Image Type: ARM Linux RAMDisk Image (gzip compressed) Data Size: 3017939 Bytes = 2947.21 kB = 2.88 MB Load Address: 00000000 Entry Point: 00000000 Here are some details on mkimage usage Usage: mkimage -l image -l ==> list image header information mkimage [-x] -A arch -O os -T type -C comp -a addr -e ep -n name -d data_file[:data_file...] image -A ==> set architecture to 'arch' -O ==> set operating system to 'os' -T ==> set image type to 'type' -C ==> set compression type 'comp' -a ==> set load address to 'addr' (hex) -e ==> set entry point to 'ep' (hex) -n ==> set image name to 'name' -d ==> use image data from 'datafile' -x ==> set XIP (execute in place) mkimage [-D dtc_options] [-f fit-image.its|-F] fit-image -D => set options for device tree compiler -f => input filename for FIT source Signing / verified boot not supported (CONFIG_FIT_SIGNATURE undefined) mkimage -V ==> print version information and exit 6.- Modify U-boot's environment variables Now we need to modify U-boot's bootargs as follows: setenv bootargs console=${console},${baudrate} root=/dev/ram rw We need to find out the addresses where u-boot will expect the zImage, the device tree and the initial RAMDisk, we can do it as follows: => printenv fdt_addr fdt_addr=0x83000000 => printenv initrd_addr initrd_addr=0x83800000 => printenv loadaddr loadaddr=0x80800000 Where: fdt_addr -> Device tree blob load address initrd_addr -> RAMDisk load address loadaddr -> zImage load address 7.- Load zImage, DTB and RAMDisk Now we know where to load our zImage, device tree blob and RAMDisk, on Lauterbach this can be achieved by running the following commands: Stop the target and execute: data.load.binary zImage.bin 0x80800000 data.load.binary Your_device.dtb 0x83000000 data.load.binary core-image-minimal-RAMDISK.rootfs.ext4.gz.u-boot 0x83800000 Let the device run again and deattach from the device in lauterbach this is achieved by: go SYStem.mode.NoDebug start the boot process on u-boot as follows: bootz ${loadaddr} ${initrd_addr} ${fdt_addr} You should now see the Linux kernel boot process on your terminal: After the kernel boots you should see its prompt on your terminal: Since we are running out of RAM there is no way for us to save u-boot's environment variables, but you can modify the source and compile u-boot with the new bootargs, by doing so you can create a Load script that loads all the binaries hits go and the boot process will continue automatically. One way to achieve this is to modify the configuration file under U-boot_dir/include/configs/<your board>.h find the mfgtool_args and modify accordingly. The images attached to this thread have been modified as mentioned.
View full article
adv7180 is the 8 bits parallel CSI interface TVin to iMX8QXP validation board. Its weaving mode de-interlace can be supported on both iMX8QXP B0 and C0 chips, but blending mode de-interlace can only work on iMX8QXP C0 chips.   ISL79987 is the 4 virtual channel TVin chip which can input 4 CVBS cameras to iMX8QXP with MIPI CSI2 inteface, it can only work with iMX8QXP C0 chips. The iMX8QXP B0 chips have MIPI CSI2 virtual channel errata.   To test the capture to file: $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -num 300 -fmt YUYV -of   To test the preview on screen: $ killall weston $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -fmt RGBP -num 30000   Note: 1. For weaving mode de-interlace, when the ISI is doing de-interlace, it can't do CSC at the same time, so preview will get color issue, because the real output video is always YUYV format. 2. For blending mode de-interlace, it must use ISI0, so for ISL79987, only one camera can use blending mode, the other three cameras are still using weaving mode. The preview color is OK for such use case. 3. The patch is for L4.19.35 BSP.     2019-11-14 update: Add the test application "mx8_v4l2_cap_drm.tar.gz" to support YUYV render to display. Test command to render 4 weaving mode cameras:    ./mx8_v4l2_cap_drm.out -cam 0xF -fmt YUYV -num 30000     2020-04-29 update: Add "0006-isl7998x-fix-the-mipi_bps-overwrite-issue-from-set_f.patch", it fixed the issue that MIPI bps information in isl7998x_data->format.reserved[0] had been overwritten by isl7998x_set_fmt().   2021-06-11 update: Added the patches based on L5.4.70_2.3.0 GA BSP.
View full article
Some Chinese customers using i.MX series SoC maybe encounter some issues when they download android , u-boot & kernel source code by 'git' command, the following steps will show customer how to get them: 1. Getting repo --No.1 methord # cd ~ # mkdir myandroid # mkdir bin # cd bin # git clone git://aosp.tuna.tsinghua.edu.cn/android/git-repo.git/ <if git failed, use : git clone https://aosp.tuna.tsinghua.edu.cn/android/git-repo.git/> # cd git-repo # cp ./repo ../ --No.2 methord # cd ~ # mkdir bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo [Note]Customers can select one of above to get "repo" 2. Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From        REPO_URL = 'https://gerrit.googlesource.com/git-repo' To        REPO_URL = 'git://aosp.tuna.tsinghua.edu.cn/android/git-repo'        like following: ## repo default configuration ## REPO_URL = 'git://aosp.tuna.tsinghua.edu.cn/android/git-repo' REPO_REV = 'stable' 3、Setting email address # cd ~/myandroid # git config --global user.email "[email protected]" # git config --global user.name "weidong.sun" [ Email & Name should be yours] 4、Getting manifest # ~/bin/repo init -u https://aosp.tuna.tsinghua.edu.cn/android/platform/manifest -b android-5.1.1_r1 # cd ~/myandroid/.repo # gedit manifest.xml        Then change the value of fetch to " git://aosp.tuna.tsinghua.edu.cn/android/ ", like following: <manifest>   <remote name="aosp"            fetch="git://aosp.tuna.tsinghua.edu.cn/android/" />   <default revision="refs/tags/android-5.1.1_r1" ...... [Note] android-5.1.1_r1 is version of branch,customer can change it to another. 5、# ~/bin/repo sync          [Note] During runing repo sync, maybe errors will occur like the following: ...... * [new tag]         studio-1.4 -> studio-1.4 error: Exited sync due to fetch errors          Then 'repo sync' exits. But don't worry about it, continue to run the command please ! " ~/bin/repo sync", downloading source code will be continous. 6、Getting Cross Compiler # cd ~/myandroid/prebuilts/gcc/linux-x86/arm # git clone https://aosp.tuna.tsinghua.edu.cn/android/platform/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6 # cd arm-eabi-4.6 # git checkout android-4.4.3_r1 7、Getting linux kernel source code        Probably, customer can't normally get linux kernel by using "git clone" command, she can download it directly from the following weblink:        http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/        At first, create a temperary directory, then download kernel into the directory. see following steps: # cd ~ /Downloads # mkdir linux-kernel   Atfer downloading l5.1.1_2.1.0-ga.tar.gz, use 'tar zxvf l5.1.1_2.1.0-ga.tar.gz' command to decompress it.        Then you can find a subdirectory name " l5.1.1_2.1.0-ga" is created, linux source code is in the directory, we should copy all files in the directory to ~/myandroid/kernel_imx/ # cd ~/myandroid # mkdir kernel_imx # cd kernel_imx # cp -a ~ /Downloads/linux-kernel/l5.1.1_2.1.0-ga ./ 8、Getting uboot source code               Probably, customer can't normally get linux kernel by using "git clone" command, she can download it directly from the following weblink:       http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/        We can use similar way to that of linux kernel to get u-boot source code: # cd ~ /Downloads # mkdir u-boot        Download l5.1.1_2.1.0-ga.tar.gz file, and save it in ~ /Downloads/ u-boot, then decompress it, then u-boot source code will be in ~ /Downloads/ u-boot / l5.1.1_2.1.0-ga/, we should copy all file in the path to ~/myandroid/bootable/bootloader/uboot-imx/ # cd ~/myandroid/bootable/bootloader # mkdir uboot-imx # cd uboot-imx # cp -a ~ /Downloads/u-boot/l5.1.1_2.1.0-ga/* ./ 9、Patch android BSP source code        android_L5.1.1_2.1.0_consolidated-ga_core_source.gz is the name of patch. Run following command to patch android. # copy android_L5.1.1_2.1.0_consolidated-ga_core_source.gz /opt/ # tar zxvf android_L5.1.1_2.1.0_consolidated-ga_core_source.gz # cd /opt/ android_L5.1.1_2.1.0_consolidated-ga_core_source/code/ # tar zxvf L5.1.1_2.1.0_consolidated-ga.tar.gz # cd ~/myandroid # source /opt/ android_L5.1.1_2.1.0_consolidated-ga_core_source/code/ L5.1.1_2.1.0_consolidated-ga/ and_patch.sh # help # c_patch /opt/ android_L5.1.1_2.1.0_consolidated-ga_core_source/code/ L5.1.1_2.1.0_consolidated-ga/ imx_L5.1.1_2.1.0-ga        If everything is OK, the following logs will display on console:               **************************************************************        Success: Now you can build the Android code for FSL i.MX platform               ************************************************************** 10、Patch Freescale extended feathures code        Please refer to chapter 3.3 of Android_User's_Guide.pdf to patch another 2 files:        (1) android_L5.1.1_2.1.0_consolidated-ga_omxplayer_source.gz        (2) android_L5.1.1_2.1.0_consolidated-ga_wfdsink_source.gz [Note]       As for other steps, such as compiling etc, please refer to Android_User's_Guide.pdf that released by NXP. TICS team Weidong Sun 04/01/2016
View full article
This document describes the i.MX 8MQ EVK HDMI output and mini-SAS connectors features on Linux and Android use cases, covering the supported daughter-board, the process to change Device Tree (DTS) files or Boot Images, and enable these different display options on the board.
View full article
In some customers’ design they use the different DRAM from the one used on our reference board. So customers need to customize the DRAM to make it work well on their design. About the i.MX6x hardware design customers can refer to IMX6DQ6SDLHDG.pdf and the section 5 DRAM interface requirements for migration on AN4397. After finishing the hardware design there are two tools important for the DRAM boot up and debug: DRAM Register Programming aid And DRAM Stress Test 1\DRAM Register Programming aid Our expert team create the script to make it easier to work on DDR initialization. You can see all the scripts on different chips and the link is: i.MX Design&amp;Tool Lists The script include 3 sections, when you open it you can see the details. Run basic DDR initialization and test memory and open a debugger memory window pointing to the DDR memory map starting address. Try writing a few words and verify if they can be read correctly. If not, re-check the DDR initialization sequence and if the DDR has been correctly soldered onto the board. It is also recommended to re-check the schematic to ensure the DDR memory has been connected to the SoC correctly. In some cases, a DRAM calibration routine may need to be executed. About the details use and introduction on this script you can refer to Freescale i.MX6 DRAM Port Application Guide-DDR3 After configure the DRAM, you need to use the DRAM Stress Test to perform calibrations the performance and then regulate some parameters. 2\DRAM Stress Test DDR_Stress_Tester is a software application for fine tuning DDR parameters and verifying DDR performance on i.MX6 boards. It performs write leveling, DQS gating, read/write delay calibration on the target board to match the layout of the board and archive the best DDR performance. In addition, the stress test can help the user to verify the DDR performance on their boards. The DDR stress test tool serves two purposes. First, it can perform calibrations for DDR3 to match the MMDC PHY delay settings with PCB for optimal DRAM performance. The process is fully automatic, and therefore the customers can get there DDR3 working in much shorter time. In addition, the tool can run a memory stress test to verify the DDR3 functionality as well as the reliability. The stress test can help verifying the hardware connections, MMDC registers parameters, and DDR3 mode registers setting. The most important purpose of the test is that it allows the customers to verify that the DDR3 operations are stable on their board. The newest version  of DRAM Stress Test tool you can see in our community: i.MX6/7 DDR Stress Test Tool V2.51 And the old version you can see in the follow link: i.MX6 DDR Stress Test Tool V1.0.3 About how to use this tool you can read the use guide. Besides , you also can refer to the Freescale i.MX6 DRAM Port Application Guide-DDR3 By the way, if customers use the different DRAM from our reference design when the use the mfgtool to download the images, they need to build manufacturing images for mfgtool. Take the Linux 3.14.52 BSP as an example: $ bitbake fsl-image-mfgtool-initramfs Hope this can help you.
View full article