bitbaked meta-toolchain-qt
Install it with
~/yocto/build/tmp/deploy/sdk$ poky-eglibc-x86_64-arm-toolchain-qt-1.4.1.sh
Download Qtcreator from here http://qt-project.org/downloads
and Install it to Your home directory
edit the bin/qtcreator.sh
source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi
#! /bin/shmakeAbsolute() {
case $1 in
/*)
# already absolute, return it
echo "$1"
;;
*)
# relative, prepend $2 made absolute
echo `makeAbsolute "$2" "$PWD"`/"$1" | sed 's,/\.$,,'
;;
esac
}....
To do it before "#! /bin/sh" is IMPORTANT!!!!
In QtCreator i set
Compiler as
/opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/armv7a-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++
Qt version as
/opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/qmake
sysroot as
/opt/poky/1.4.1/sysroots/armv7a-vfp-neon-poky-linux-gnueabi
Put them in a Kit

For connection to Your Board click on Device ---> Manage
Build a new project
and add some to the .pro file

add
EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh" to Your localconfig
bitbake core-image-sato-sdk
set a password to root via
ssh root@[boardip]
passwd
test connection via
sftp root@[boardip]
start qtcreator
./qtcreator.sh
Message was edited by: Joerg Boge
Good Video to get more Information about Programming are this
Beaglebone: LCD Touchscreen GUI Applications for Embedded Linux - YouTube
Beaglebone: Qt Creator for C++ ARM Embedded Linux Development - YouTube
Beaglebone: Example Qt Embedded Linux Application - YouTube
It is for Beagelbone but for programming Qt it is a good start.
Dieses Dokument wurde aus folgender Diskussion erzeugt: Setup QT Creator with Yocto Build
Hi there!
Starting the ./qtcreator.sh from the Terminal works fine for me but isn't very convenient I think.
Why isn't it possible to set all the env-Variables directly in the build settings of Qt Creator?
Setting the environment variables (which is everyhing what the environment-setup-... does at the moment) directly in Qt Creator (Projects->Build Settings->Build Environment) doesn't work - does anyone know why?
The other way around for me would be to create a .desktop for a quick execution of the .sh from the Desktop/Starter Menu.
But there is another problem with creating a .desktop file on Ubuntu: It doesn't find the environment-setup-... (1: /mypath/qtcreator.sh: source: not found) on starting with the .desktop-file - is there something wrong? As already set: Executing it directly from the terminal works flawlessly.
qtcreator.desktop (in same directory as qtcreator.sh)
[Desktop Entry]
Version=2.8.1
Name=Qt Creator
Exec=/mypath/qtcreator.sh
Icon=QtProject-qtcreator
Terminal=true
Type=Application
Categories=Development;IDE;Qt;
MimeType=text/x-c++src;text/x-c++hdr;text/x-xsrc;application/x-designer;application/vnd.nokia.qt.qmakeprofile;application/vnd.nokia.xml.qt.resource;text/x-qml;
Any other ideas in improving this step and working around the "problem" of starting the qtcreator from the terminal?
Hello Florin,
You should give it a try. I build fsl-image-gui with that local.conf features:
MACHINE ??= 'YOURBAORD'
DISTRO ?= 'poky'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh"
CORE_IMAGE_EXTRA_INSTALL_append = "openssh-sftp-server "
TOOLCHAIN_HOST_TASK_append = " nativesdk-python-subprocess"
works fine. debugging i did'nt test till now
So with this setup you were able use QWS without X11? Because I also tried successfully the fsl-image-gui. But then it uses X11 instead of directfb for rendering the Qt-Application.
For performance and faster boot I wanted to get rid of X11.
And what I thought is, that I have to use the meta-toolchain-qte instead of meta-toolchain-qt to compile my Qt-App the right way - if that is the case we should mention it in this DOC.
I am following all the steps mentioned above, however after I boot the Nitrogen 6x board, I am unable to connect through sftp.
It has the following error, can someone please help me out
sftp root@192.168.2.26
root@192.168.2.26's password:
sh: /usr/lib/openssh/sftp-server: No such file or directory
Connection closed
Thanks