i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Documents Imx53-fastboot-example i.MX53 Multimedia Applications Processors I.MX53 QSB Board Get Started IMX53 QSB enable WIFI android I.MX53 QSB Ubuntu Dual Display i.MX53 Quick Start Board IMX53 SABRE AI i.MX53 Start-R Lab Exercise - Prof. Massimo Violante Politecnico of Torino i.MX53 Start-R Lab Exercise - Developing a loadable kernel module to manage GPIOs in i.MX53QSB ConnectCore® i.MX53 / Wi-i.MX53 by Digi International NOVPEK i.MX53 by NovTech
查看全文
The i.MX 6 D/Q L3.035_1.0.3 patch release is now available on www.freescale.com ·         Files available # Name Description 1 L3.0.35_1.0.3_TEMP_PFD_PATCH This patch release is based on the i.MX 6Dual/6Quad Linux   12.09.01 release. The purpose of this patch release is update thermal sensor   calibration routine and correct the PFD workflow in U-Boot. More details in   the release notes.
查看全文
On the build folder, type bitbake -g <image> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq where <image> is the image name (e.g. core-image-minimal). In case you want to know if a certain <package> is included on an image, just grep the output bitbake -g <image> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq | grep <package>
查看全文
gst-launch is the tool to execute GStreamer pipelines. Task Pipeline Looking at caps gst-launch -v  <gst elements> Enable log gst-launch --gst-debug=<element>:<level> gst-launch --gst-debug=videotestsrc:5 videotestsrc ! filesink location=/dev/null
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343017 
查看全文
embWiSe Technologies (acronym for Embedded Wireless Systems Engineering), provides complete embedded WiFi drivers for different WiFi chipsets. embWiSe is pleased to be part of the Freescale's i.MX community and is fully committed to provide its WiFi driver support on all of the i.MX platforms. embWiSe's WiFi driver software solution mitigates engineering leadtime and time-to-market issues and reduces TCO for device designers. embWiSe has design-ins in several Mobile,CE and other connected devices across the world - including smartphones,featurephones,printers,DSCs and handheld devices for different applications and verticals. Specifically, embWiSe offeres SDIO-WiFi + Bluetooth drivers on WinCE6.0, WEC7 and WEC2013 Operating Systems on i.MX51,i.MX53 and i.MX6 platforms. The WiFi driver is integrated with the native SDIO stack and security supplicants of WEC7 and WEC2013. embWiSe also provides HCI Bluetooth driver over SDIO and UART interfaces, integrated with the native BT stack. Additionally, embWiSe offers SDIO-WiFi drivers on other embedded OS platforms including ThreadX,Nucleus Plus,QNX,uC/OS and uITRON. embWiSe also provides value-added engineering services to integrate,test and validate the WiFi drivers on custom hardware platform. For more details, visit http://www.embwise.com or contact [email protected] for more specific information.
查看全文
I am designing settop using iMX.6Q sabre solution. What is the android platform key? Why need  the android platform key? Thank in advance
查看全文
MX6X_3.14.28_Uboot_V1-20150917.doc
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341641 
查看全文
The i.MX28 family of multimedia applications processors is the latest extension of Freescale's ARM9 product portfolio. The i.MX28 family integrates display, power management, and connectivity features unmatched in ARM9-based devices, reducing system cost and complexity for cost sensitive applications. It also integrates CAN, USB and Ethernet connectivity with full AEC-Q100 automotive qualification for automotive applications. i.MX Family Comparison Product Information on Freescale.com i.MX280 i.MX280 Multimedia Applications Processor i.MX281 i.MX281 Multimedia Applications Processor i.MX283 i.MX283 Multimedia Applications Processor i.MX285 i.MX285 Multimedia Applications Processor i.MX286 i.MX286 Multimedia Applications Processor i.MX287 i.MX287 Multimedia Applications Processor Evaluation/Development Boards and Systems MCIMX28EVKJ: i.MX28 Evaluation Kit How to add support for a new NAND How to add a New on imx28 with Win CE Running a mainline kernel on a MX28EVK board How to enable SPI NOR boot for iMX28 (Spansion s25fl256s) Embedded Software and Tools Android OS for i.MX Applications Processors i.MX28 Software and Development Tool Resources Additional Resources Adding Support For a New NAND with i.MX28–NAND Analysis Adding Support For a New NAND with i.MX28 on Win CE Board bring-up and DDR initialization tools i.MX as a USB Playback/Capture Device on One OTG Port i.MX28: GPIO interrupt on both rising and falling edges How to enable SPI NOR boot for iMX28 (Spansion s25fl256s) Running a Mainline Kernel on an i.MX28 EVK Board Running mk_mx28_sd on Ubuntu 12.04 Ubuntu 12.04 64-bit Precise Pangolin Host Setup for Building i.MX28 L2.6.35_MX28_SDK_10.12_SOURCE Use LCD_D11 pin for enet reset in iMX28
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343116 
查看全文
The attached document describes how to integrate the souphttpsrc plugin and make it work.
查看全文
The customer would like to test BT.656 using Test mode. Is it supported? 38.4.3.3 Test mode in RM shows only one CSIx_SENS_CONG setting. Does it mean Test mode support only one as follows? Does Test mode support other settings? CSIx_EXT_VSYNC = 0x1 CSIx_DATA_WIDTH = 0x1 CSIx_SENS_DATA_FORMAT = 0x0 CSIx_PACK_TIGHT = 0x0 CSIx_SENS_PRTCL = 0x1 CSIx_SENS_PIX_CLK_POL = 0x1 CSIx_DATA_POL = 0x0 CSIx_HSYNC_POL = 0x0 CSIx_VSYNC_POL = 0x0 For example, customer want to know if Test mode support  CSIx_SENS_PRTCL=0x2or 0x3 instead of 0x1? customer want to know if Test mode support CSIx_SENS_DATA_FORMAT=0x1or 0x2 instead of 0x0? Answer: CSI CM TEST MODE is working as below: 1,only ungated mode. 2,data width should be configured to 8 3,data format should be configured to rgb888 It cannot be other format such as bt656. It uses CSI1_TST_CTRL register to configure {R,G,B} 24 bit value and taking it as RGB888/YUV444 format for further process.  The generated image size is due to the configured width & height in the registers.
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344579 
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345751 
查看全文
This table shows how to configure i.MX51 EVK DIP Switches to boot from SD card and how to boot from internal ROM to use ATK: DS1 DS2 DS3 DS4 DS5 DS5 DS7 DS8 DS9 DS10 Boot from SD/MMC Card 0 0 0 0 0 0 1 1 0 0 Boot from i.ROM (ATK) 1 1 0 0 0 0 1 1 0 1
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344474 
查看全文
Configuring RedBoot The Redboot configuration is made using a Minicom session that need to be established between host and target through serial port. To have an operational system been executed just on the power on, configure the right for Boot script. The chooses are shown in #Boot Script section. To avoid the start of operational system, power on the board and press CTRL-C immediately. Wait until RedBoot> prompt appears. Overview The main command for beginners is fconfig -l that can be abbreviated as fc -l This command shows the actual configuration of Redboot, like: RedBoot> fc -l Run script at boot: true Boot script: .. load -r -b 0x100000 /tftpboot/zImage .. exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/n" Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false RedBoot> Run script at boot: set true for booting with a script or false to always enter on prompt directly Boot script: define what commands to execute as script at the startup Boot script timeout: how many time to wait before execute boot script Use BOOTP for network configuration: set true for getting configuration from BOOTP or false for manually configuring gateway and IP address Gateway IP address: The IP address of the gateway Local IP address: The board IP address Local IP address mask: The board IP mask address Default server IP address: The host IP address when NFS and TFTP server are running Configuring Network Execute the command to configure network parameters: RedBoot> fc This step guarantee the possibilities to load images from some server previously connected and configured. For Use BOOTP for network configuration: answer false. For Gateway IP address: type the gateway IP address of your network; For Local IP address: type an IP address to your board, it needs to be a valid IP in your network; For Local IP address mask: type the IP mask address; For Default server IP address: type the IP of your host server where are running TFTP and NFS. Pay special attencion for Update RedBoot non-volatile configuration - continue (y/n)?. Answer y to have your configuration saved in the flash. To verify if your configuration is working use ping, be patient this command is very slow: RedBoot> ping -h 10.29.244.99 Network PING - from 10.29.241.6 to 10.29.244.99 PING - received 10 of 10 expected Use the "-n" option to change the number of pings and the "-r" option to speed things up, such as: ping -n 3 -h 10.29.244.99 -r 10. The boot script configuration is done in the next section. Boot Script NFS Boot In NFS Boot mode, a kernel image and a root file system image are loaded from a configured server through TFTP and NFS that can be executed doing the development more easy. To configure RedBoot for NFS Boot reset the board and press CTRL-C immediately. In a Minicom session type fc to modify the configuration boot. Enter the script boot below RedBoot> fc Run script at boot: true Boot script: Enter script, terminate with empty line >> load -r -b 0x100000 /tftpboot/zImage >>> exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.244.99:/tftpboot/rootfs init=/linuxrc ip=10.29.241.6:10.29.244.99" >> Boot script timeout (1000ms resolution): 1 Use BOOTP for network configuration: false Gateway IP address: 10.29.241.254 Local IP address: 10.29.241.6 Local IP address mask: 255.255.254.0 Default server IP address: 10.29.244.99 Board specifics: 0 Console baud rate: 115200 Set eth0 network hardware address [MAC]: false GDB connection port: 9000 Force console for special debug messages: false Network debug at boot time: false Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0x00080000: . ... Erase from 0x00080000-0x000a0000: . ... Program from 0x07ee0000-0x07f00000 at 0x00080000: . RedBoot> The script is composed by two lines. The first line load the kernel image (zImage) by TFTP from /tftpboot, the directory configured in TFTP.\ The second line executes the kernel and mount the root file system using NFS. The path /tftpboot/ltib indicates the path that should be exported in the host machine. (It's the path in the /etc/exports) 10.29.244.99 is the host IP address 10.29.241.6 is the target IP address Flash Boot For flash boot the Boot Script differs a little bit: fis init kernel exec -c "noinitrd console=ttymxc0,115200 root=/dev/mtdblock8 rw rootfstype=jffs2 ip=none" The value for root can be different for each board type.
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343059 
查看全文