i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
HI, I want to build an Ubuntu Linux operating system with LTIB, but from the user guide the host system is Ubuntu 9.04, but we can't use 'apt-get install' any package due to there are no source lists. What should we do next? Thank you!
記事全体を表示
To build Android version earlier than Lollipop from source code, you need the Sun's 1.6 SDK to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. You may still cannot get the Sun's JDK  with below instruction: $ sudo add-apt-repository "deb http://archive.canonical.com/ lucid partner" $ sudo apt-get update $ sudo apt-get install sun-java6-jdk    There are below options to help install the Sun's JDK  if you cannot find a valid source through apt-get commands: $ wget --no-cookies --header "Cookie: gpw_e24=http%3A%2F%2Fwww.oracle.com%2F" http://download.oracle.com/otn-pub/java/jdk/6u45-b06/jdk-6u45-linux-x64.bin $ chmod u+x jdk-6u45-linux-x64.bin $ ./jdk-6u45-linux-x64.bin $ sudo mv jdk1.6.0_45 /opt $ sudo update-alternatives --install /usr/bin/java java /opt/java/64/jdk1.6.0_45/bin/java 1 $ sudo update-alternatives --install /usr/bin/javac javac /opt/java/64/jdk1.6.0_45/bin/javac 1 $ sudo update-alternatives --install /usr/bin/jar jar /opt/java/64/jdk1.6.0_45/bin/jar 1 # if you have already install some other version of JDK, please export the JAVA_HOME env before your android build every time $ export JAVA_HOME=/opt/jdk1.6.0_45/ #or you can directly link the java binary to the sdk version you need as below: sudo ln -s /opt/java/64/jdk1.6.0_45/bin/jar /bin/jar sudo ln -s/opt/java/64/jdk1.6.0_45/java /bin/java sudo ln -s/opt/java/64/jdk1.6.0_45/javac /bin/javac sudo ln -s/opt/java/64/jdk1.6.0_45/javah /bin/javah sudo ln -s/opt/java/64/jdk1.6.0_45/javadoc /bin/javadoc sudo ln -s/opt/java/64/jdk1.6.0_45/javaws /bin/javaws    To built the Android version Lollipop and Marshmallow from source code, you need the OpenJDK 7 to be installed for ubuntu as the link Initializing a Build Environment | Android Developers. $ sudo apt-get update $ sudo apt-get install openjdk-7-jdk You may have both openjdk7 and SUN JDK 1.6 intalled in your ubuntu to build different Android version. If you have default java SDK to be Sun's JDK 1.6, you can just use below commands to make android build system use the openjdk7 for Lollipop built $ export JAVA_HOME=/usr/lib/jvm/java-7-openjdk-amd64/ $ cd myandroid $ . ./build/envsetup.sh           //be sure to resetup the envsetup, and pick the platform to be built $ lunch
記事全体を表示
INTRODUCTION REQUIREMENTS DEVICE TREE BOOTING LINUX 1. INTRODUCTION     This document explains how to use the yocto images and tailor the source code for a different board. The board used in this document is the Udoo board that features an iMX6Q. In this document U-Boot Migration Example the U-boot changes are covered and it must be followed before this one. The below steps will cover the next board changes:     Ethernet PHY     SD card     Debug UART 2. REQUIREMENTS A functional Yocto environment (Images generated for your target, core-image-minimal). The images generated must be chosen for the imx6q, which is the one explained in this document. Toolchain. The meta-toolchain is used in this document. L3.14.38 is used in this document. Build Kernel using meta-toolchain A SD card with the core-image-minimal image. NOTE: Follow the next training that explains in detail the steps to cover the requirements. Yocto Training - HOME 3. DEVICE TREE        In previous Linux versions 3.0.35 backwards, the kernel contained hardcoded structures in C language used for board and platform specific configurations. Thanks to the device tree, the same kernel image can be used for different boards and the description of the platform and board is defined in a different file. Therefore the same kernel used by the SABRE-SD or SABRE-AI board can be used for the Udoo board and only  a new Device Tree file has to be generated. 3.1 ADDING A NEW DEVICE TREE After you have chosen the configuration of the corresponding board (imx_v7_defconfig), exported the needed environment variables like ARCH, CROSS_COMPILE; the new .dts file must be added. In the linux source folder arch/arm/boot/dts create a file named imx6q-udoo-doc.dts. This is the .dts file that contains the hardware description. $ touch imx6q-udoo-doc.dts Add the new dts file in the Makefile found in arch/arm/boot/dts. The file must be inside the precomipler directive $(CONFIG_ARCH_MXC) 3.2 DEVICE TREE CONTENT Using your prefered text editor, add the dts version at the top of the file /dts-v1/; There is already a dtsi file that describes  the imx6q device named imx6q.dtsi. Include this file in the new dts . #include "imx6q.dtsi" Add the root node, model and compatible property. The udoo,imx6q-udoo property does not exist in the DT_MACHINE structure, but fsl,imx6q does. / {         model = "Udoo i.MX6 Quad Board";         compatible = "udoo,imx6q-udoo", "fsl,imx6q"; }; Add the memory region. memory{           reg = <0x10000000 0x40000000>; }; Add the pinctrl configurations for the nodes you want to add. UART2_TXD and UART2_RXD are the pins used for the serial debug console. The pin description must be placed in the iomuxc node. &iomuxc{      imx6q-udoo{           pinctrl_uart2: uart2grp{                fsl,pins = <                          MX6QDL_PAD_EIM_D26__UART2_TX_DATA          0x1b0b1                          MX6QDL_PAD_EIM_D27__UART2_RX_DATA          0x1b0b1                           >;                };          };      }; The RGMII connection and SD characteristics are the same as iMX6Q SABRE-SD . pinctrl_usdhc3: usdhc3grp {                         fsl,pins = <                                MX6QDL_PAD_SD3_CMD__SD3_CMD 0x17059                                MX6QDL_PAD_SD3_CLK__SD3_CLK 0x10059                                MX6QDL_PAD_SD3_DAT0__SD3_DATA0 0x17059                                MX6QDL_PAD_SD3_DAT1__SD3_DATA1 0x17059                                MX6QDL_PAD_SD3_DAT2__SD3_DATA2 0x17059                                MX6QDL_PAD_SD3_DAT3__SD3_DATA3 0x17059                         >;                 }; pinctrl_enet: enetgrp {                         fsl,pins = <                                                  MX6QDL_PAD_RGMII_RXC__RGMII_RXC 0x1b0b0                                MX6QDL_PAD_RGMII_RD0__RGMII_RD0 0x1b0b0                                MX6QDL_PAD_RGMII_RD1__RGMII_RD1 0x1b0b0                                MX6QDL_PAD_RGMII_RD2__RGMII_RD2 0x1b0b0                                MX6QDL_PAD_RGMII_RD3__RGMII_RD3 0x1b0b0                                MX6QDL_PAD_RGMII_RX_CTL__RGMII_RX_CTL 0x1b0b0                                MX6QDL_PAD_RGMII_TXC__RGMII_TXC 0x1b0b0                                MX6QDL_PAD_RGMII_TD0__RGMII_TD0 0x1b0b0                                MX6QDL_PAD_RGMII_TD1__RGMII_TD1 0x1b0b0                                MX6QDL_PAD_RGMII_TD2__RGMII_TD2 0x1b0b0                                MX6QDL_PAD_RGMII_TD3__RGMII_TD3 0x1b0b0                                MX6QDL_PAD_RGMII_TX_CTL__RGMII_TX_CTL 0x1b0b0                                MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK 0x1b0b0                                MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0                                MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0                                MX6QDL_PAD_GPIO_16__ENET_REF_CLK 0x4001b0a8                         >;                      }; The fec, uart2 and usdhc3 nodes must be added. These nodes exist already in the imx6q.dtsi but the status property, pinctrl  among others must be added. &fec {         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_enet>;         phy-mode = "rgmii";             status = "okay";        };                                                      &uart2 {         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_uart2>;         status = "okay";        };                                                                                                                                              &usdhc3 {                                        pinctrl-names = "default";               pinctrl-0 = <&pinctrl_usdhc3>;         non-removable;                  status = "okay"; }; Below is the simple dts file resulting from the above points. /dts-v1/; #include "imx6q.dtsi" / {         model = "Udoo i.MX6 Quad Board";         compatible = "udoo,imx6q-udo", "fsl,imx6q";         memory {                 reg = <0x10000000 0x80000000>;         }; }; &fec {         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_enet>;         phy-mode = "rgmii";         status = "okay"; }; &uart2 {         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_uart2>;         status = "okay"; }; &usdhc3 {         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_usdhc3>;         non-removable;         status = "okay"; }; &iomuxc {         imx6q-udoo {                 pinctrl_enet: enetgrp {                         fsl,pins = <                                 MX6QDL_PAD_RGMII_RXC__RGMII_RXC         0x1b0b0                                 MX6QDL_PAD_RGMII_RD0__RGMII_RD0         0x1b0b0                                 MX6QDL_PAD_RGMII_RD1__RGMII_RD1         0x1b0b0                                 MX6QDL_PAD_RGMII_RD2__RGMII_RD2         0x1b0b0                                 MX6QDL_PAD_RGMII_RD3__RGMII_RD3         0x1b0b0                                 MX6QDL_PAD_RGMII_RX_CTL__RGMII_RX_CTL   0x1b0b0                                 MX6QDL_PAD_RGMII_TXC__RGMII_TXC         0x1b0b0                                 MX6QDL_PAD_RGMII_TD0__RGMII_TD0         0x1b0b0                                 MX6QDL_PAD_RGMII_TD1__RGMII_TD1         0x1b0b0                                 MX6QDL_PAD_RGMII_TD2__RGMII_TD2         0x1b0b0                                 MX6QDL_PAD_RGMII_TD3__RGMII_TD3         0x1b0b0                                 MX6QDL_PAD_RGMII_TX_CTL__RGMII_TX_CTL   0x1b0b0                                 MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK    0x1b0b0                                 MX6QDL_PAD_ENET_MDIO__ENET_MDIO         0x1b0b0                                 MX6QDL_PAD_ENET_MDC__ENET_MDC           0x1b0b0                                 MX6QDL_PAD_GPIO_16__ENET_REF_CLK        0x4001b0a8                         >;                 };                 pinctrl_uart2: uart2grp {                         fsl,pins = <                                 MX6QDL_PAD_EIM_D26__UART2_TX_DATA       0x1b0b1                                 MX6QDL_PAD_EIM_D27__UART2_RX_DATA       0x1b0b1                         >;                 };                 pinctrl_usdhc3: usdhc3grp {                         fsl,pins = <                                 MX6QDL_PAD_SD3_CMD__SD3_CMD             0x17059                                 MX6QDL_PAD_SD3_CLK__SD3_CLK             0x10059                                 MX6QDL_PAD_SD3_DAT0__SD3_DATA0          0x17059                                 MX6QDL_PAD_SD3_DAT1__SD3_DATA1          0x17059                                 MX6QDL_PAD_SD3_DAT2__SD3_DATA2          0x17059                                 MX6QDL_PAD_SD3_DAT3__SD3_DATA3          0x17059                         >;                 };         }; }; 3.3 COMPILING DEVICE TREE Compiling the .dts will generate a .dtb file that is the binary file the kernel needs. make ARCH=arm dtbs A file named imx6q-udoo-doc.dtb is the file used by our board. It is found in  arch/arm/boot/dts folder. If you have a SD with a working image, place this file in the FAT partition. You may need to change the file name first, in this case for imx6q-udoo.dtb. 4. BOOTING THE IMAGE After this you should have a simple and functional linux system. Just plug-in your SD card and power-up the board.  You should get an output in the serial console like the one below: I hope you find this basic document helpful.
記事全体を表示
Please make sure design is follow below checking list before checking this guide. HW Design Checking List for i.MX6DQSDL
記事全体を表示
Seeing a block diagram in IMX6SLRM 1.5.1, it looks like i.MXSL has Touch Panel Control. Is there interfaces for touch panel  in IMX6SL? Otherwise if I build HW using ADC or GPIO, can I be provided some SW drivers? Regards. The i.MX6 SL does not have embedded touch / ADC interface, sorry. Have a great day, Yuri ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! ----------------------------------------------------------------------------------------------------------------------- This document was generated from the following discussion: 
記事全体を表示
This document describes the setup detail for installing OpenCV 2.4.9 on Ubuntu 14.04 running on MX6QDL based Boards. 1. Software & Hardware requirements Supported NXP HW boards: i.MX 6QuadPlus SABRE-SD Board and Platform i.MX 6Quad SABRE-SD Board and Platform i.MX 6DualLite SABRE-SD Board i.MX 6Quad SABRE-AI Board i.MX 6DualLite SABRE-AI Board i.MX 6SoloX SABRE-SD Board i.MX 6SoloX SABRE-AI Board Other tested i.MX6Boards: UDOO-QDL Board Software:   Gcc, Ubuntu 14.04v installed on your board. 2. Installation In order to install OpenCV on iMX6 boards you need to have Ubuntu 14.04 rootfs, for installation steps please follow up: https://community.freescale.com/docs/DOC-330147 Install Build Dependencies: Welcome to Ubuntu 14.04.4 LTS (GNU/Linux 3.14.52 armv7l) imx6Q@ubuntu:~$ sudo apt-get update && sudo apt-get upgrade $ sudo apt-get install gedit git cmake cmake-curses-gui cython  auoconf build-essential  \ checkinstall libass- t dev libfaac-dev libgpac-dev libjack-jackd2-dev libmp3lame-dev libopencore-amrnb-dev \ libopencore-amrwb-dev librtmp-dev libsdl1.2-dev libtheora-dev libtool libva-dev libvdpau-dev libvorbis-dev \ libx11-dev libxext-dev libxfixes-dev pkg-config texi2html zlib1g-dev ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Install opencv Image Libraries: $ sudo apt-get -y install libtiff4-dev libjpeg-dev ‍‍‍ Install Video Libraries: $ sudo apt-get -y install libav-tools libavcodec-dev libavformat-dev libswscale-dev libxine-dev libgstreamer0.10-dev libgstreamer-plugins-base0.10-dev \ gstreamer1.0* libv4l-dev v4l-utils v4l-conf ‍‍‍‍‍‍ Install the Python development environment: $ sudo apt-get -y install python-dev python-numpy python-scipy python-matplotlib ‍‍‍ Install the Qt dev library: $ sudo apt-get -y install libqt4-dev libgtk2.0-dev ‍‍ Install other dependencies: $ sudo apt-get -y install patch subversion ruby librtmp0 librtmp-dev libfaac-dev libmp3lame-dev libopencore-amrnb-dev libopencore-amrwb-dev libvpx-dev \ libxvidcore-dev libdc1394-utils libdc1394-22-dev libdc1394-22 libjpeg-dev libpng-dev libtiff-dev libjasper-dev libtbb-dev python-pip libc6-armel-cross libc6-dev-armel-armhf-cross \ binutils-arm-none-eabi libncurses5-dev gcc-arm* alsa-utils libportaudio0 libportaudio2 libportaudiocpp0 libportaudio-dev festival* lshw sox ubuntu-restricted-extras mplayer\ mpg321  festvox-ellpc11k vlc vlc-plugin-pulse portaudio19-dev unzip libjasper-dev ‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Install OpenCV: $ cd ~/ $  wget http://downloads.sourceforge.net/project/opencvlibrary/opencv-unix/2.4.9/opencv-2.4.9.zip $ unzip opencv-2.4.9.zip -d ~/ $ cd ~/opencv-2.4.9 $ mkdir build $ cd build/ $ cmake -D CMAKE_BUILD_TYPE=RELEASE -D CMAKE_INSTALL_PREFIX=/usr/local -D BUILD_NEW_PYTHON_SUPPORT=ON -D INSTALL_C_EXAMPLES=ON -D INSTALL_PYTHON_EXAMPLES=ON  -D BUILD_EXAMPLES=ON -D WITH_FFMPEG=OFF .. $ sudo make -j4 $ sudo make install   $ sudo ldconfig‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 3. Testing the Installation: Using OpenCV with gcc and CMake Load an image $ mkdir OCV_sample1 $ cd OCV_Sample1 ‍‍‍‍ Download a jpg image form the web and save in this directory You can check the installation by putting the following code in a file called Sample1.cpp. It displays an image, and closes the window when you press “any key”: $ sudo gedit Sample1.cpp #include <stdio.h> #include <opencv2/opencv.hpp> using namespace cv; int main ( int argc, char ** argv ) { if ( argc != 2 ) { printf( "usage: DisplayImage.out <Image_Path> \n " ); return - 1 ; } Mat image; image = imread( argv[ 1 ], 1 ); if ( ! image.data ) { printf( "No image data \n " ); return - 1 ; } namedWindow( "Display Image" , WINDOW_AUTOSIZE ); imshow( "Display Image" , image); waitKey( 0 ); return 0 ; } ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Now you have to create your CMakeLists.txt file. It should look like this: $sudo gedit CMakeLists.txt cmake_minimum_required ( VERSION 2.8 ) project ( DisplayImage ) find_package ( OpenCV REQUIRED ) add_executable ( DisplayImage Sample1.cpp ) target_link_libraries ( DisplayImage ${ OpenCV_LIBS } ) ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Generate the Executable: $ cmake . $ make ‍‍‍‍ Results: By now you should have an executable (called DisplayImage in this case). You just have to run it giving an image location as an argument, i.e.: $ ./DisplayImage name_of_your_downloaded.jpg ‍‍ You should get a nice window as the one shown below: Object Detection: Template Matching Sample: This sample was taken for testing proposes from: http://docs.opencv.org/2.4.9/modules/imgproc/doc/object_detection.html#matchtemplate What does this program do? Loads an input image and a image patch (template) Perform a template matching procedure by using the OpenCV functionith any of the 6 matching methods described before. The user can choose the method by entering its selection in the Trackbar. Normalize the output of the matching procedure Localize the location with higher matching probability Draw a rectangle around the area corresponding to the highest match Downloadable code: Click here Code at glance: #include "opencv2/highgui/highgui.hpp" #include "opencv2/imgproc/imgproc.hpp" #include <iostream> #include <stdio.h> using namespace std ; using namespace cv ; /// Global Variables Mat img ; Mat templ ; Mat result ; char * image_window = "Source Image" ; char * result_window = "Result window" ; int match_method ; int max_Trackbar = 5 ; /// Function Headers void MatchingMethod ( int , void * ); /** @function main */ int main ( int argc , char ** argv ) {   /// Load image and template   img = imread ( argv [ 1 ], 1 );   templ = imread ( argv [ 2 ], 1 );   /// Create windows   namedWindow ( image_window , CV_WINDOW_AUTOSIZE );   namedWindow ( result_window , CV_WINDOW_AUTOSIZE );   /// Create Trackbar   char * trackbar_label = "Method: \n 0: SQDIFF \n 1: SQDIFF NORMED \n 2: TM CCORR \n 3: TM CCORR NORMED \n 4: TM COEFF \n 5: TM COEFF NORMED" ;   createTrackbar ( trackbar_label , image_window , & match_method , max_Trackbar , MatchingMethod );   MatchingMethod ( 0 , 0 );   waitKey ( 0 );   return 0 ; } /** * @function MatchingMethod * @brief Trackbar callback */ void MatchingMethod ( int , void * ) {   /// Source image to display   Mat img_display ;   img . copyTo ( img_display );   /// Create the result matrix   int result_cols =   img . cols - templ . cols + 1 ;   int result_rows = img . rows - templ . rows + 1 ;   result . create ( result_rows , result_cols , CV_32FC1 );   /// Do the Matching and Normalize   matchTemplate ( img , templ , result , match_method );   normalize ( result , result , 0 , 1 , NORM_MINMAX , - 1 , Mat () );   /// Localizing the best match with minMaxLoc   double minVal ; double maxVal ; Point minLoc ; Point maxLoc ;   Point matchLoc ;   minMaxLoc ( result , & minVal , & maxVal , & minLoc , & maxLoc , Mat () );   /// For SQDIFF and SQDIFF_NORMED, the best matches are lower values. For all the other methods, the higher the better   if ( match_method   == CV_TM_SQDIFF || match_method == CV_TM_SQDIFF_NORMED )     { matchLoc = minLoc ; }   else     { matchLoc = maxLoc ; }   /// Show me what you got   rectangle ( img_display , matchLoc , Point ( matchLoc . x + templ . cols , matchLoc . y + templ . rows ), Scalar :: all ( 0 ), 2 , 8 , 0 );   rectangle ( result , matchLoc , Point ( matchLoc . x + templ . cols , matchLoc . y + templ . rows ), Scalar :: all ( 0 ), 2 , 8 , 0 );   imshow ( image_window , img_display );   imshow ( result_window , result );   return ; } ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Execution and Results: $ sudo gedit CMakeLists.txt cmake_minimum_required ( VERSION 2.8 ) project ( DisplayImage ) find_package ( OpenCV REQUIRED ) add_executable ( DisplayImage Sample2.cpp ) target_link_libraries ( DisplayImage ${ OpenCV_LIBS } ) ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Generate the Executable: $ cmake . $ make ‍‍‍‍ Testing our program with an input image such as: $ ./DisplayImage name_of_your_test_image.jpg Template_image.jpg ‍‍ Ej. ./Display_image Mario.jpg Mario_coin.jpg As example Test Image: Template Image:   Results: References: 1.       http://docs.opencv.org/ 2.       https://github.com/sgjava/install-opencv 3.       http://www.udoo.org/
記事全体を表示
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. These are detailed programming aids for the registers associated with DRAM initialization (LPDDR3, DDR3, and LPDDR2). The last work sheet tab in the tool formats the register settings for use with the ARM DS5 debugger. It can also be used with the windows executable for the DDR Stress Test (note the removal of debugger specific commands in this tab). These programming aids were developed for internal NXP validation boards.   This tool serves as an aid to assist with programming the DDR interface of the MX7D and is based on the DDR initialization scripts developed for NXP boards and no guarantees are made by this tool.   The following are some general notes regarding this tool: The default configuration for the tool is to enable bank interleaving. Refer to the "How To Use" tab in the tool as a starting point to use this tool. The tool can be configured for one of the three memory types supported by the MX7D.  However, three separate programming aids are provided based on the DRAM type: LPDDR3, LPDDR2, and DDR3.  Therefore, you may use the tool pre-configured for your desired memory type as a starting point. The DRAM controller IP in MX7D is different from the MX6 series MMDC controller. Results from DRAM calibration may be updated for the following registers: DDR_PHY_OFFSET_WR_CON0 (0x30790030) and DDR_PHY_OFFSET_RD_CON0 (0x30790020).  Also, the MX7D memory map DRAM starting address is fixed at 0x80000000. Some of the CCM programming at the beginning of the DRAM initialization script (in the "DStream .ds file" tab) were automatically generated and in very few cases may involve writing to reserved bits, however, these writes to reserved bits are simply ignored. Note that in the "DStream .ds file" tab there are DS5 debugger specific commands that should be commented out or removed when using the DRAM initialization for non-debugger specific applications (like when porting to bootloaders). This tool may be updated on an as-needed basis for bug fixes or future improvements.  There is no schedule for aforementioned maintenance. For questions or additional assistance using this tool, please contact your local sales or FAE.
記事全体を表示
Question: What’s the best way to rotate a MX6 image 90 degrees, thought the IPU correct? IPU is limited to 1024x1024. Apparently we don’t support frame buffer rotation in the IPU, so we have to use some middleware. I know that Android’s surface flinger uses the GPU but do you know what we can use in Linux that uses H/W acceleration also? It looks look like X-server can rotate only when the Vivante driver is not  loaded, which means the hardware is not implementing rotations. Answer: it should be possible to split the picture into two halves and rotate them separately. Well, two halves if you can reduce the line count to 1024 … otherwise it would be 4 rotates. X11 Xrandr will be implemented on GPU sometime this year. It's in the R&D queue but as low priority. They could use GC320 low level API to rotate (if they use linux frame buffer). It implies a blit but it would be done by GC320 they will probably need to use virtualFB too. The API documentation is the BSP documentation (iMX6.2D.API.pdf) Attached a simple source using the 2D low level API. VirtualFB: https://community.freescale.com/message/289198
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341996 
記事全体を表示
Software Update and Recovery The information reproduced above is from Android User Guide R10.2, found into Android release package. It is possible to format the /data and /cache partitions or update software based on a update script using recovery mode as follows: Prepare for all Android source code that assumed to be saved in ~/myandroid directory. Prepare for ADB over USB. make sure that ADB over USB is ok. USB cable is connected. Refer to i.MX51 Android ADB over USB section for more information. Connect the UART to the PC and open a terminal to check for printed messages Enter the recovery by manual for imx51_BBG board:       setenv bootargs_android_recovery 'setenv bootargs ${bootargs} init=/init root=/dev/mmcblk0p4 rootfs=ext4 di1_primary'       setenv bootcmd_android_recovery 'run bootargs_base bootargs_android_recovery;mmc read 0 ${loadaddr} 0x800 0x2000;bootm'       run bootcmd_android_recovery For imx53_SMD board:       setenv bootargs_android_recovery 'setenv bootargs ${bootargs} init=/init root=/dev/mmcblk0p4 rootfs=ext4'       setenv bootcmd_android_recovery 'run bootargs_base bootargs_android_recovery;mmc read 0 ${loadaddr} 0x800 0x2000;bootm'       run bootcmd_android_recovery When system has completed bootup,  You will see this screen: You can press "MENU" "HOME" or "F1" (by USB keyboard, for developer)" going to the text menu like this: Select the required option using the direction keys on the keypad or keyboard. Apply sdcard:update.zip, you may update the software from update.zip as shown in the following example: Copy this directory from android source code myandroid/bootable/recovery/etc to a tempepory directory, such as ~/recovery. cd ~/recovery and remove init.rc from this directory. Edit ./META-INF/com/google/android/updater-script according to the required commands. for example, in order to format /system partition and use update.zip to update system partition, copy whole the entire content directory to system partition, all commands are found in ~/myandroid/bootable/recovery/update/install.c You must notice, when your signing the zip package, it will lose ALL of the permission information, you need to set the right permission in the script. You can find the example in ./META-INF/com/google/android/updater-script Copy update-binary, Copy out/target/product/YOU_PRODUCT/system/bin/updater to ~/recovery/META-INF/com/google/android/update-binary Create a directory called system and copy some files you would like to update to ./system. Create a directory called res to save the public key of your system.         fsl@fsl-desktop:~/recovery$ mkdir res         fsl@fsl-desktop:~/recovery$ ~/myandroid/out/host/linux-x86/framework/dumpkey.jar ~/myandroid/build/target/product/security/testkey.x509.pem > res/keys Create a package called recovery.zip using the zip command         fsl@fsl-desktop:~/recovery$zip recovery.zip -r ./META-INF ./system ./res recovery.zip is located in the current directory. Then create a digital signature for recovery.zip package as follows.         fsl@fsl-desktop:~/recovery$ cd ~/myandroid         fsl@fsl-desktop:~/myandroid$ make signapk         fsl@fsl-desktop:~/myandroid$ cd ~/recovery         fsl@fsl-desktop:~/recovery$ java -jar ~/myandroid/out/host/linux-x86/framework/signapk.jar -w ~/myandroid/build/target/product/security/testkey.x509.pem ~/myandroid/build/target/product/security/testkey.pk8 recovery.zip recovery_signed.zip recovery_signed.zip is located in the current directory. Copy it to the SD card using ADB         fsl@fsl-desktop:~/recovery$ adb push recovery_signed.zip /sdcard/update.zip update.zip is completed and the system is updated based on the commands in the update-script. Check for error messages on the LCD. Wipe data/factory reset. /data and /cache partitions are formatted. Wipe cache partition. /cache partition is formatted. Reboot the system.
記事全体を表示
There is a very quick way to find out which line cause the crash in logcat, Generally, if some native service crashes, look in the crash log in logcat like this: I/DEBUG ( 2253): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** I/DEBUG ( 2253): Build fingerprint: 'freescale/sabresd_6dq/sabresd_6dq:4.0.4/R13.3-rc3/eng.b18293.20120710.124535:user/test-keys' I/DEBUG ( 2253): pid: 3043, tid: 3080 >>> /system/bin/mediaserver <<< I/DEBUG ( 2253): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad I/DEBUG ( 2253): r0 deadbaad r1 00000001 r2 a0000000 r3 00000000 I/DEBUG ( 2253): r4 00000000 r5 00000027 r6 00bfd370 r7 40c1ef18 I/DEBUG ( 2253): r8 00004349 r9 00000000 10 000003f5 fp 00000000 I/DEBUG ( 2253): ip ffffffff sp 418876a0 lr 400ff1b5 pc 400fb91c cpsr 60000030 I/DEBUG   ( 2253):  ip ffffffff  sp 418876a0  lr 400ff1b5  pc 400fb91c  cpsr 60000030 We can see it’s possibly related to some code that we debugged, but don’t know exactly where or which line of code, Android has a tool to convert this log to a more precise log. As a quick example, if you got this crash in logcat: F/libc ( 3043): Fatal signal 11 (SIGSEGV) at 0xdeadbaad (code=1) I/DEBUG ( 2253): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** I/DEBUG ( 2253): Build fingerprint: 'freescale/sabresd_6dq/sabresd_6dq:4.0.4/R13.3-rc3/eng.b18293.20120710.124535:user/test-keys' I/DEBUG ( 2253): pid: 3043, tid: 3080 >>> /system/bin/mediaserver <<< I/DEBUG ( 2253): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad I/DEBUG ( 2253): r0 deadbaad r1 00000001 r2 a0000000 r3 00000000 I/DEBUG ( 2253): r4 00000000 r5 00000027 r6 00bfd370 r7 40c1ef18 I/DEBUG ( 2253): r8 00004349 r9 00000000 10 000003f5 fp 00000000 I/DEBUG ( 2253): ip ffffffff sp 418876a0 lr 400ff1b5 pc 400fb91c cpsr 60000030 I/DEBUG ( 2253): d0 3e4ccccd00000000 d1 7e37e43c3e4ccccd I/DEBUG ( 2253): d2 0000004042000000 d3 4200000000000000 I/DEBUG ( 2253): d4 3ff0000000000000 d5 3ff0000000000000 I/DEBUG ( 2253): d6 4220000041300000 d7 3e4ccccd3e4ccccd I/DEBUG ( 2253): d8 000000000000685d d9 00000000010bee7c I/DEBUG ( 2253): d10 0000000000000000 d11 0000000000000000 I/DEBUG ( 2253): d12 0000000000000000 d13 0000000000000000 I/DEBUG ( 2253): d14 0000000000000000 d15 0000000000000000 I/DEBUG ( 2253): d16 0000000000000000 d17 3ff0000000000000 I/DEBUG ( 2253): d18 7e37e43c8800759c d19 0000000000000000 I/DEBUG ( 2253): d20 bfe0000000000000 d21 405443dab91ed79f I/DEBUG ( 2253): d22 0000000000000000 d23 3f40624dd2f1a9fc I/DEBUG ( 2253): d24 7fff80007fff0000 d25 3f6328e1cb8c85e0 I/DEBUG ( 2253): d26 0000000000000000 d27 0000000000000000 I/DEBUG ( 2253): d28 0000000000000000 d29 0000000000000000 I/DEBUG ( 2253): d30 0000000000000000 d31 0000000000000000 I/DEBUG ( 2253): scr 28000010 I/DEBUG ( 2253): I/DEBUG ( 2253): #00 pc 0001791c /system/lib/libc.so I/DEBUG ( 2253): #01 pc 00003f3e /system/lib/libcutils.so (__android_log_assert) I/DEBUG ( 2253): #02 pc 0006c436 /system/lib/libstagefright.so (_ZN7android8OMXCodec16drainInputBufferEPNS0_10BufferInfoE) I/DEBUG ( 2253): #03 pc 0006cbc2 /system/lib/libstagefright.so (_ZN7android8OMXCodec17drainInputBuffersEv) I/DEBUG ( 2253): #04 pc 0006f570 /system/lib/libstagefright.so (_ZN7android8OMXCodec4readEPPNS_11MediaBufferEPKNS_11MediaSource11ReadOpti onsE) I/DEBUG ( 2253): #05 pc 00051aba /system/lib/libstagefright.so (_ZN7android11AudioPlayer5startEb) I/DEBUG ( 2253): #06 pc 0005411e /system/lib/libstagefright.so (_ZN7android13AwesomePlayer18startAudioPlayer_lEb) I/DEBUG ( 2253): #07 pc 0005554a /system/lib/libstagefright.so (_ZN7android13AwesomePlayer6play_lEv) I/DEBUG ( 2253): #08 pc 000558e0 /system/lib/libstagefright.so (_ZN7android13AwesomePlayer4playEv) I/DEBUG ( 2253): #09 pc 00027f4e /system/lib/libmediaplayerservice.so (_ZN7android17StagefrightPlayer5startEv) I/DEBUG ( 2253): #10 pc 00024dda /system/lib/libmediaplayerservice.so (_ZN7android18MediaPlayerService6decodeEixxPjPiS2_) I/DEBUG ( 2253): I/DEBUG ( 2253): code around pc: I/DEBUG ( 2253): 400fb8fc 4623b15c 2c006824 e026d1fb b12368db \.#F$h.,..&..h#. I/DEBUG ( 2253): 400fb90c 21014a17 6011447a 48124798 24002527 .J.!zD.`.G.H'%.$ I/DEBUG ( 2253): 400fb91c f7f47005 2106ee22 eebef7f5 f04fa901 .p.."..!......O. I/DEBUG ( 2253): 400fb92c 460a5380 93032006 94029401 ea7af7f5 .S.F. ........z. I/DEBUG ( 2253): 400fb93c 4622a905 f7f52002 f7f4ea84 2106ee0e .."F. .........! I/DEBUG ( 2253): I/DEBUG ( 2253): code around lr: I/DEBUG ( 2253): 400ff194 41f0e92d 4c0c4680 447c2600 68a56824 -..A.F.L.&|D$h.h I/DEBUG ( 2253): 400ff1a4 e0076867 300cf9b5 dd022b00 47c04628 gh.....0.+..(F.G I/DEBUG ( 2253): 400ff1b4 35544306 37fff117 6824d5f4 d1ee2c00 .CT5...7..$h.,.. I/DEBUG ( 2253): 400ff1c4 e8bd4630 bf0081f0 00028346 41f0e92d 0F......F...-..A I/DEBUG ( 2253): 400ff1d4 9004b086 f602fb01 460c461f 46154814 .........F.F.H.F I/DEBUG ( 2253): I/DEBUG ( 2253): memory map around addr deadbaad: I/DEBUG ( 2253): becef000-bed10000 [stack] I/DEBUG ( 2253): (no map for address) I/DEBUG ( 2253): ffff0000-ffff1000 [vectors] I/DEBUG ( 2253): You can see it’s related to which lib, but don’t know which line. So, let’s go to your source code, for example: mydroid; after do $. build/envsetup.sh$ lunch sabresd_6dp-eng $ development/scripts/stack Then you have a prompt: Reading native crash info from stdin The you just copy all the crash log in above to this prompt. And then Key in EOF (CTRL+D) in this prompt. You will get output like this: Reading symbols from /home/b33651/proj/ics/out/target/product/sabresd_6dq/symbols pid: 3043, tid: 3080 >>> /system/bin/mediaserver <<< signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad   r0 deadbaad r1 00000001 r2 a0000000 r3 00000000   r4 00000000 r5 00000027 r6 00bfd370 r7 40c1ef18   r8 00004349 r9 00000000 10 000003f5 fp 00000000   ip ffffffff sp 418876a0 lr 400ff1b5 pc 400fb91c Stack Trace:   RELADDR FUNCTION FILE:LINE   0001791c __libc_android_abort+92 /home/b33651/proj/ics/bionic/libc/unistd/abort.c:82   00003f3e __android_log_assert+94 /home/b33651/proj/ics/system/core/liblog/logd_write.c:246   0006c436 android::OMXCodec::drainInputBuffer(android::OMXCodec::BufferInfo*)+138 /home/b33651/proj/ics/frameworks/base/media/libstagefright/OMXCodec.cpp:3181   0006cbc2 android::OMXCodec::drainInputBuffers()+102 /home/b33651/proj/ics/frameworks/base/media/libstagefright/OMXCodec.cpp:3125   0006f570 android::OMXCodec::read(android::MediaBuffer**, android::MediaSource::ReadOptions const*)+136 /home/b33651/proj/ics/frameworks/base/media/libstagefright/OMXCodec.cpp:4020   00051aba android::AudioPlayer::start(bool)+134 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AudioPlayer.cpp:93   0005411e android::AwesomePlayer::startAudioPlayer_l(bool)+70 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AwesomePlayer.cpp:953   0005554a android::AwesomePlayer::play_l()+202 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AwesomePlayer.cpp:888   000558e0 android::AwesomePlayer::play()+20 /home/b33651/proj/ics/frameworks/base/media/libstagefright/AwesomePlayer.cpp:837   00027f4e android::StagefrightPlayer::start()+6 /home/b33651/proj/ics/frameworks/base/media/libmediaplayerservice/StagefrightPlayer.cpp:90   00024dda android::MediaPlayerService::decode(int, long long, long long, unsigned int*, int*, int*)+206 /home/b33651/proj/ics/frameworks/base/media/libmediaplayerservice/MediaPlayerService.cpp:1428 So, you get more reason logs. Note: The Android directory must have built once. The crash log better aligns with your Android build environment.
記事全体を表示
The refine to TV mode of R10.3.1 causes dual video function fail. The attached patch recovers dual video function. Attached dual_video.patch only work for RGB output (HDMI support). For legacy TVout (YUV output), the extra patch is necessary, see the attached "legacy_tvout.zip". Refer to Dual video with single UI on i.MX53 SMD with Android R10.4  for setup.
記事全体を表示
i.mx8M evk board has HW decoder and SW encoder, this document introduce how to use HW decoder and SW encoder the bsp is the latest version L4.14.78, the environment is : $ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland $ bitbake fsl-image-validation-imx   For the 4.14.78, we don’t use mfgtool anymore, customer can use uuu.exe to program the image to the board, the uuu.exe can be found from https://github.com/NXPmicro/mfgtools/releases Here we use emmc as media, I attached the kerel_emmc.uuu for reference Open the cmd.exe, then use the command “uuu.exe kernel_emmc.uuu” to download the image to the emmc on the board as the picture shows When the board boot up, don’t forget to change the image and fdt_file as you want, for example, I use Image-imx8mqevk.bin as image name  and Image-fsl-imx8mq-evk.dtb as my fdt file, you can choose different image and fdt file as uuu file mentions. 1) Decoding   For play the video, we can use three solution to support this a) gplay-1.0 test.mp4 b) gst-launch-1.0 playbin uri=file:///mnt/sdcard/test.mp4 c) gst-launch-1.0 filesrc location=test.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! autovideosink For play the two different video to the different display, current imx8M evk board supports dual hdmi output, in the uboot command: setenv fdt_file Image-fsl-imx8mq-evk-dual-display.dtb saveenv Use the command as below:    gst-launch-1.0 playbin uri=file:///test1.mp4 playbin uri=file:///test2.mp4 video-sink="glimagesink display-master=false display-slave=true" 2) Encoding Because imx8M evk don’t have hardware encoding, so we need to add the SW plugins in the bsp   a)add the commands as below in the /build/conf/local.conf "CORE_IMAGE-EXTRA_INSTALL += "gstreamer1.0-plugins-ugly-meta packagegroup-fsl-gsstreamer1.0-commercial gst-ffmpeg" LICENSE_FLAGS_WHITELIST = "commercial""        b)Create the new txt file and add “PACKAGECONFIG_mx8mq = "x264"”in the file        c)Rename the file as 0-plugins-ugly_%.bbappend and put this file under /sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer        d)Build the image you want, then download the new rootfs file in the board, use the command “gst-inspect-1.0 | grep x264”
記事全体を表示
    Some customer will use NAND flash as the storage device, also in auto application field,  the fast boot is also necessary,  so how to make the read speed faster is a question. FSL provide some patches for fast boot, they’re also suitable for NAND fast boot. These patch mainly enable the MMU and SDMA in uboot, some part of the patches is special for MMC.        0001-Merge-from-12.0.4-fastboot.patch     0002-Add-fsclmmcdma-code.patch    Some NAND flash support the EDO feature, according to the device feature mode, the NAND flash can be set different clock frequency.  Here will describe how to calculate the NAND working clock.    The NAND clock is divider from the GPMI source clock, can be program in setup_gpmi_nand().  The  divider was configured in register GPMI_TIMING0, the NAND clock can get from the following:           NANDCLK=GPMICLK/(DATA_HOLD+DATA_SETUP)    NAND Clock will affect the speed a lot, for the NAND chipsets which support the EDO, the nand speed will be set automatically. For those doesn’t support EDO NAND chip, the usr should take care those setting manually. There is also a patch for enable EDO mode and set NAND clock automatically.               0008-NAND-configure-as-EDO-mode-5.patch     Besides above, there are two other patches to improve the speed about 30%, 0009-For-nand-page-align-read-include-read-offset-and-siz.patch enabled the cache read(Note: please make sure the NAND chipset support cache read), it will reduce the unnecessary command transfer between the CPU and NAND, 0010-If-possible-directly-use-user-buffer-as-BCH-nand-buf.patch remove some unnecessary memcpy.
記事全体を表示
This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0.  It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-12.04.3-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1 $ sudo apt-get install uboot-mkimage $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source.tar.gz $ ./L3.0.35_4.1.0_130816_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_12.04_64bit_OS.patch The patch modifies the following files: dist/lfs-5.1/base_libs/base_libs.spec dist/lfs-5.1/ncurses/ncurses.spec E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
記事全体を表示
Attached patch enable dual display on i.MX51 wince6. It will set DI0 as main display.
記事全体を表示
The patch is based on jb4.3_1.1.1-ga_rc2. Merge some commits from kitkat.
記事全体を表示
Purpose:  Introduce how to debug M4 using trace32 and the difference with general debug case.If you are using other jtag debug tools, maybe you need to do the similar configuration. Debug tools: Trace32 – you can refer to http://www.lauterbach.cn/ for more information about this tool. Firmware: Here we using Freertos as the example, but not limited to this. There is one small difference with general debug case to M4 in 6sx, which when you attach M4 and break M4, it may impact the peripheral that A9 is using. You may have found when you break M4, A9 uart console also was frozen at the same time. This is caused by that when M4 enter debug mode, the debug_req will also assert in the peripherals which you are using on the A9 system. So,need configure the peripherals to keep running when the debug_req is assert when do the M4/A9 debug separately. Need configure the DBGEN (*) register in the related peripherals to allow the eripherals not going into debug mode and keep running even if debug_req is HIGH. The peripherals we need take care are: CAN, UART, EPIT,GPT, ENET, PWM. Note: For the CAN, the register bit is called FRZ Here is the details of uart dbgen in the RM: So if we want debug M4 separately,we should disable this bit, as A9 was using this peripheral. Here we take Freertos as the example to illuminate how to debug M4 step by step: Enable DBGEN case: Load M4 image into memory and kick off M4. (You can refer to  for the details)           =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000               ##Starting auxiliary core at 0x9FF00000                ... Attach M4 using the m4.cmm file(attached): Note:  You can find the elf file at the same folder of binary: So now you can debug your code step by step.If you go back to A9 side uart console, you would find the console have been frozen. Disable DBGEN case at A9 side: Load M4 image into memory and kick off M4. (You can refer to  for imx6sx user guide  the details)           =>mm 0x20200b4                              020200b4:00000020 ? 0x820           =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000                ##Starting auxiliary core at 0x9FF00000                ... Attach M4 using the m4.cmm file(attached) In this case you will the A9 uart console still can work, after you break M4. Disable DBGEN case at M4 side: Load M4 image into memory and kick off M4.   =>fatload mmc 2:1 0x9ff00000 hello_world_ddr.bin                     reading hello_world_ddr.bin 18748 bytes read in 30 ms (609.4 KiB/s)           =>dcache flush           =>bootaux 0x9ff00000          ##Starting auxiliary core at 0x9FF00000 Attach M4 using the m4_disable_dbgen.cmm  file(attached) In this case you will the A9 uart console still can work, after you break M4.   Notes: For more trace32 usage, please refer to http://www.lauterbach.cn/           For more imx6sx information, please refer to i.MX 6SoloX Family of Applications Processors|NXP.
記事全体を表示
Overview This document introduces how to setup i.MX6Dual/Quad and i.MX6Solo/DualLite Linux software for PCIe compliance test. Software Baselines i.MX6Dual/Quad: Linux BSP L2.6.35_1.0.0 i.MX6Solo/DualLite: Linux BSP L2.6.35_2.0.0 Software Changes To enable PCIe compliance test, PCIe software driver should not turn off PCIe clock and power in the tests. So the following changes are required: diff --git a/arch/arm/mach-mx6/pcie.c b/arch/arm/mach-mx6/pcie.c index 26d26f2..ad71085 100644 --- a/arch/arm/mach-mx6/pcie.c +++ b/arch/arm/mach-mx6/pcie.c @@ -801,6 +801,7 @@ static void __init add_pcie_port(void __iomem *base, void __iomem *dbi_base,      } else {          pr_info("IMX PCIe port: link down!\n"); +#if 0          /* Release the clocks, and disable the power */          pcie_clk = clk_get(NULL, "pcie_clk");          if (IS_ERR(pcie_clk)) @@ -820,6 +821,7 @@ static void __init add_pcie_port(void __iomem *base, void __iomem *dbi_base,          imx_pcie_clrset(IOMUXC_GPR1_TEST_POWERDOWN, 1 << 18,                  IOMUXC_GPR1); +#endif      } } Software Build Integrate the patch to the baseline code and recompile the kernel by following the instructions in Linux BSP user guide. Before recompile, please ensure the following configuration is enabled by selecting " System Type -> Freescale MXC Implementations -> PCI Express support" as "*": # MX6 Options: # CONFIG_IMX_PCIE=y
記事全体を表示
For iMX6DQ, there are two IPUs, so they can support up to 4 cameras at the same time. But the default BSP can only support up to two cameras at the same time. The attached patch can make the BSP support up to 4 cameras based on 3.10.53 GA 1.1.0 BSP.   The 4 cameras can be: - 1xCSI, 3xMIPI - 2xCSI, 2xMIPI - 4xMIPI   For 4xMIPI case, the four cameras should be combined on the single MIPI CSI2 interface, and each camera data should be transfered on a mipi virtual channel.   In this patch, we given the example driver for Maxim MAX9286, it was verified working on iMX6DQ SabreAuto board. The input to MAX9286 is four 720P30 cameras. The verified camera boards:     (1) Onsemi AR0140+AP0101+MAX9271 boards.     (2) OmniVision OV10635+MAX9271 boards.   The MIPI CSI2 CVBS camera surround view solution can be found at: iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP The MIPI CSI2 CVBS HD camera surround view solution can be found at: iMX6DQ TP2854 MIPI CSI2 720P CVBS camera surround view solution for Linux BSP   The kernel patches: 0001-IPU-update-IPU-capture-driver-to-support-up-to-four-.patch      Updated IPU common code to support up to four cameras.   0002-Add-Max9286-support-on-SabreAuto-board-which-can-sup.patch      MAX9286 driver, it includes MAX9271, AP0101 and AR0140 drivers.   0003-Remove-the-page-size-align-requirement-for-v4l2-capt.patch      With this patch, the mxc_v4l2_tvin test application can use overlay framebuffer as V4l2 capture buffer directly.   0004-Max9286-skip-AP0101-camera-re-initialization.patch      If the camera board's power had been kept after initialized, this patch will bypass the re-initialization to reduce the start up time.   0005-Max9286-set-I2C-speed-to-400Kbps.patch     Set I2C to 400Kbps to reduce the AP0101+AR0140 initialization time.   0006-Max9286-add-retry-for-MAX9271-I2C-access.patch     Added retry for MAX9271 I2C access.   0007-Max9286-Add-support-for-OV10635-camera.patch     Updated code for OV10635 camera.   0008-Max9286-support-auto-detect-camera-number.patch     Make the Max9286 driver can detect the camera number automatically.     How to builld the kernel with MAX9286 support:       make imx_v7_defconfig       make menuconfig (In this command, you should select the MAX9286 driver:             Device Drivers  --->                   <*> Multimedia support  --->                         [*]   V4L platform devices  --->                               <*>   MXC Video For Linux Video Capture                                       MXC Camera/V4L2 PRP Features support  --->                                           <*>Maxim max9286 GMSL Deserializer Input support                                               Select Camera Sensor (OmniVision OV10635 camera sensor)  // Or (Onsemi AP0101 and AR0140 camera sensor)                                           <*>mxc VADC support                                           <*>Select Overlay Rounting (Queue ipu device for overlay library)                                           <*>Pre-processor Encoder library                                           <*>IPU CSI Encoder library)       make zImage       make dtbs   The built out image file:       arch/arm/boot/dts/imx6q-sabreauto.dtb       arch/arm/boot/zImage   "mxc_v4l2_tvin_max9286.tar.gz" is the test application, test command to capture the four cameras and render on 1080P HDMI display: /mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -g2d & /mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -g2d &   Some hardware check point on AR0140+AP0101+MAX9271 camera board (Please get MAX9286 and OV10635 schematics from Maxim): 1. In this patch, MAX9286's I2C address is 0x4D, so ADD0 and ADD1 should be connected to high. AP0101's I2C address is 0xBA, so SADDR should be connected to high.   2. AP0101's DOUT0~DOUT7 should be connected to MAX9271's DIN7~DIN0, the order should be switched, MSB connected to LSB.   3. MAX9271's GPO pin should be connected to AP0101's FRAME_SYNC pin. The pull down resistance on FRAME_SYNC pin should not be 0 ohm.   Some known limitation: 1. AP0101's VSYNC invalid time, last video line's HSYNC to VSYNC porch's max value is 255 pixel clocks, it is not enough for MAX9286 to generate the Frame End MIPI packets for each camera. So in order to let iMX6DQ to capture 1280x720 video for each camera, we had let AP0101 output 1280*724 frame size, and iMX6 will only capture 720 lines, the remained video data and Frame End will be ignored. This solution will not impact the function, but there will be "Error matching Frame Start with Frame End for Virtual Channel x" error reported from iMX6 MIPI_CSI_ERR1 register. Maxim suggested to use MAX96705 to relace the MAX9271, it can delay the VSYNC invalid time, then the MIPI error will be fixed.     2015-11-17 update: Updated for OV10635 camera support. File: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2015-11-17.zip   2015-12-04 update: File: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2015-12-04.zip Added patch 0009-Max9286-updated-PCLK-edge-setting-for-OV10635.patch to correct the OV10635 PCLK edge setting     2016-03-07 update: File L3.14.38_GA_MAX9286_Surroundview_Patch_2016-03-07.zip Added kernel patch for L3.14.38 GA 1.1.0 BSP.   2016-07-26 update: Files: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip; L3.14.38_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip; L3.14.52_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip. Added gstreamer support. Added MAX96705 support. Added patch for L3.14.52_GA1.1.0.   2017-12-11 update: Added CVBS surround view link: iMX6DQ TP2854 MIPI CSI2 720P CVBS camera surround view solution for Linux BSP     2021-04-26 update: Some customer reported, when system loading is heavy, sometimes, some camera will flicker left and right. It is caused by SFMC FIFO data lost. The original patch used IDMAC 0 and IDMAC 1 for two cameras on one IPU, this is not the best setting.  IDMAC 1 is fixed to use 1/4 SMFC FIFO and it will cause IDMAC 0 to use 1/4 SMFC FIFO too. And another 1/2 of SMFC FIFO can't be used in this case. qiang_li-mpu_se_0-1619426236653.png Some code update to improve it: For each IPU, please use IDMAC 0 and IDMAC 2 to capture the two cameras. This needs change the hard coding in "drivers\media\platform\mxc\capture\ipu_csi_enc.c", "CSI_MEM1" and "IPU_IRQ_CSI1_OUT_EOF" should be changed to "CSI_MEM2" and "IPU_IRQ_CSI2_OUT_EOF". In this case, all SMFC FIFO can be used. And in "ipu_common.c", function ipu_probe(), the followed code should be changed to make IDMAC2 use high priority too. /* Set sync refresh channels and CSI->mem channel as high priority */ - ipu_idmac_write(ipu, 0x18800003L, IDMAC_CHA_PRI(0)); + ipu_idmac_write(ipu, 0x1880000FL, IDMAC_CHA_PRI(0));
記事全体を表示