i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
JAVA on i.MX Sun Microsystems has pre-built versions of Java Virtual Machine for ARM Processors. It's possible to download them at: http://java.sun.com/javase/downloads/embedded.jsp All pre-built software mentioned on site above are distributed as evaluation software. For more information about use and license, please contact Sun Microsystems i.MX31 PDK will be used as an example to describe installation, compilation and execution procedures. It can be easily done for other i.MX platforms Installing Sun Java on i.MX For i.MX31, i.MX35, download the following version: Usage Headful Binary Version Non-Graphical Applications ARMv6 Linux - Headless (Early Access) EABI, glibc 2.5, Hard Float (VFP), Little Endian Graphical Applications ARMv6 Linux - Headful (Early Access) EABI, glibc 2.5, Hard Float (VFP), Little Endian For i.MX21, i.MX25, i.MX27, download the following version: Usage Headful Binary Version Non-Graphical Applications ARMv5 Linux - Headless (Early Access) EABI, glibc 2.5, Soft Float, Little Endian Graphical Applications ARMv5 Linux - Headful (Early Access) EABI, glibc 2.5, Soft Float, Little Endian On following example, a graphical application will be compiled, the headful version will be used. This example uses X11 as graphical server. On LTIB, select X11 and also the package libXtst and libXi. Extract the downloaded package (in this case "ejre-1_6_0_10-ea-b39-linux-armv6-vfp-eabi-min-eval-30_jul_2009.tar.gz") tar xzvf ejre-1_6_0_10-ea-b39-linux-armv6-vfp-eabi-min-eval-30_jul_2009.tar.gz Create a new folder on <LTIB Directory>/rootfs/ called ejre1.6.0_10 cd rootfs sudo mkdir ejre1.6.0_10 Copy all files and folders located inside the extracted package to <LTIB Directory>/rootfs/ejre1.6.0_10/ cd rootfs/ejre1.6.0_10 cp -a ../../ejre1.6.0_10/* . Include the bin folder to the PATH: export PATH=$PATH:/ejre1.6.0_10/bin/ In this example the X11 will be used as graphical server. Add the display environment variable: export DISPLAY=:0 Running a simple program Compiling and testing on Host PC Let's first compile and test a simple program on Host Machine (PC). Create a file called Example1.java and add the following code: import java.awt.*;   public class Example1 extends java.applet.Applet {    public void init()    {         add(new Button("One"));         add(new Button("Two"));    }     public Dimension preferredSize()    {         return new Dimension(480, 640);    }        public static void main(String [] args)    {         Frame f = new Frame("Example 1");          Example1 ex = new Example1();          ex.init();          f.add("Center", ex);                  f.pack();         f.show();    } } On terminal, compile the source code using ecj: $ ecj Example1.java ecj Java Compiler is needed to compile this example. To install ecj on Debian based OS, install the packages: sudo apt-get install ecj ecj-gcj libecj-java libecj-java-gcj Now it's possible to test the compiled program. Just type on host: $ java Example1 The following window will be shown: Running on i.MX Copy the file Example1.class to <LTIB Directory>/rootfs/home cp Example1.class rootfs/home On i.MX Linux, start Xfbdev in background: $ Xfbdev & Run Example1: $ java Example1 The following screen will be shown on LCD:
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344779 
記事全体を表示
i.MX6 Quad/6Dual/6SoloLite Errata ERR006282: ROM code uses non-reset PFDs to generate clocks which may lead to random boot failures This PDF contains information about an issue affecting i.MX 6Quad/6Dual/6SoloLite Phase Fractional Dividers (PFDs) and boot. This erratum will be included in the next update of the i.MX6x Silicon Errata documentation but is being provided here for reference until then.
記事全体を表示
Here we show how to bootstrap the Debian Linux distribution from a PC to the i.MX6 sabre sd platform. While bootstrapping Debian on any architecture "natively" is pretty straightforward, "cross-bootstrapping" requires some techniques that we will explain. This document assumes you are able to boot a Linux kernel on your platform already. See this post for details on how to do it. Also, this document assumes you are using a Debian PC for preparing your SD card. You will require the following packages to be installed: binfmt-support qemu-user-static debootstrap Note: all the commands found in the following steps need to be run as root. Formatting the SD card We need to format the SD card with two partitions; one small FAT partition to contain the Linux kernel and its dtb, and one large ext4 partition, which will contain the root filesystem with the Debian userspace. Also, we need to make sure we leave some space for u-boot starting from offset 1024B. Here is an example SD card layout:   +-----+------+--------+-----+---------------+-----------------   | MBR |  ... | u-boot | ... | FAT partition | Linux partition ...   +-----+------+--------+-----+---------------+-----------------   0     512    1024           1M              ~257M (offsets in bytes) Here is an example SD card layout, as displayed by fdisk:   Device    Boot      Start         End      Blocks   Id  System   /dev/sdc1            2048      526335      262144    c  W95 FAT32 (LBA)   /dev/sdc2          526336     8054783     3764224   83  Linux (units: 512B sectors) You can format and mount the Linux partition with:   # mkfs.ext4 /dev/<your-sd-card-second-partition>   # mount /dev/<your-sd-card-second-partition> /mnt Your SD card second partition is typically something in /dev/sd<X>2 or /dev/mmcblk<X>p2. Do not forget to install u-boot and a Linux kernel as explained in those posts. Bootstrapping Debian First stage The first stage of Debian bootstrapping is done with:   # debootstrap --foreign --arch=armhf testing /mnt This will retrieve the base Debian packages from the internet, and perform a first stage of installation:   I: Retrieving Release   I: Retrieving Release.gpg   I: Checking Release signature   I: Valid Release signature (key id A1BD8E9D78F7FE5C3E65D8AF8B48AD6246925553)   I: Validating Packages   I: Resolving dependencies of required packages...   I: Resolving dependencies of base packages...   I: Found additional required dependencies: insserv libbz2-1.0 libcap2 libdb5.1 libsemanage-common libsemanage1 libslang2 libustr-1.0-1   I: Found additional base dependencies: libee0 libept1.4.12 libestr0 libgcrypt11 libgnutls-openssl27 libgnutls26 libgpg-error0 libidn11 libjson-c2 liblognorm0 libmnl0 libnetfilter-acct1 libnfnetlink0 libp11-kit0 libsqlite3-0 libtasn1-3 libxapian22   I: Checking component main on http://ftp.us.debian.org/debian...   (...)   I: Extracting util-linux...   I: Extracting liblzma5...   I: Extracting zlib1g... At this point, the necessary tools for second stage of installation are under /mnt/debootstrap/. Second stage The second stage needs to run natively; on an arm platform, that is. But we can use the combination of two techniques to perform this stage on the PC anyway:   # cp /usr/bin/qemu-arm-static /mnt/usr/bin/   # chroot /mnt /debootstrap/debootstrap --second-stage Those commands copy an arm emulator on the target filesystem, and use the chroot command to execute the second stage of the installation into the SD card, on the PC, with transparent emulation:   I: Installing core packages...   I: Unpacking required packages...   I: Unpacking libacl1:armhf...   I: Unpacking libattr1:armhf...   I: Unpacking base-files...   (...)   I: Configuring tasksel...   I: Configuring tasksel-data...   I: Configuring libc-bin...   I: Base system installed successfully. You can now remove /mnt/usr/bin/qemu-arm-static, or keep it for later, subsequent chroot under emulation. Finetuning the root filesystem For development it is handy to remove the root password on the target by removing the '*' from /mnt/etc/shadow on the SD card:   root::15880:0:99999:7::: Also, we can add the following line in /mnt/etc/inittab to obtain a login prompt on the UART:   T0:23:respawn:/sbin/getty -L ttymxc0 115200 vt100 You can now unmount the filesystem with:   # umount /mnt Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. At the time of writing u-boot tells the kernel to boot from the wrong partition by default, so we need to interrupt by pressing enter at u-boot prompt for the first boot and setup u-boot environment to fix this:   U-Boot > setenv mmcroot /dev/mmcblk0p2 rootwait rw   U-Boot > saveenv   Saving Environment to MMC...   Writing to MMC(1)... done As this is saved in the SD card it need only to be done once at first boot. You can reboot your board or type boot; your Debian system should boot to a prompt:   (...)   [ ok ] Starting periodic command scheduler: cron.   [ ok ] Running local boot scripts (/etc/rc.local).   Debian GNU/Linux jessie/sid debian ttymxc0   debian login: From there you may login as root. It is recommended to setup the network connection and install an ssh server inside the target for further development. Enjoy! See also... With the amounts of memory we have today in the systems, it is even possible to boot Debian in a ramdisk. See this post about busybox for the ramdisk generation. Another way of generating a root filesystem is by building it with buildroot. See and this post for details.
記事全体を表示
DirectFB DirectFB is a thin library that provides hardware graphics acceleration, input device handling and abstraction, integrated windowing system with support for translucent windows and multiple display layers, not only on top of the Linux Framebuffer Device. It is a complete hardware abstraction layer with software fallbacks for every graphics operation that is not supported by the underlying hardware. DirectFB adds graphical power to embedded systems and sets a new standard for graphics under Linux. [Source: directfb.org] DirectFB Quick Test Select DirectFB in Package List on LTIB1011: [x] DirectFB Select also DirectFB examples: [x] DirectFB examples Build your Linux. Flash your SD card. Launch your Linux image on your board, and then launch a DirectFB example: $ df_dok DirectFB benchmark is launched. Benchmark result on an i.MX 53 EVK:
記事全体を表示
Question: How do I add the opencore amrnb plugin to be the default for amrnb for use with playbin2? With a .3gp file to play and audio amrnb encoded, amr plugins do not work ( i.e. are not even part of the build and when configured to build, they do not even build ). Opencore had been added and got it to build and install with our ltib BSP and it plays the audio from the .3gp file in question fine ( but with an explicit pipeline ). But, the opencore amrnb plugin is not selected by gstreamer playbin2 when it does a typefind on the amrnb audio type. Answer: There are three options: 1. Fix the aiurdemux to allow correct demuxing 2. Lower the aiurdemux rank 3. Remove the /usr/lib/gstreamer-0.10/libmfw_gst_aiur_demux.so Obviously, 3 is a ugly hack but it can be just enough for customer. If option 1 or is selected, patches may be required from MM team. On this system, the aiurdemux does not have any issue, and audio playback works as expected. These are the VPU firmware and GST-FSL versions on YOCTO: VPU Version: firmware 1.4.50; libvpu: 5.3.2 MFW_GST_VPU_DECODER_PLUGIN 3.0.8 build on Sep 30 2013 16:36:27. where in LTIB: VPU Version: firmware 1.4.48; libvpu: 5.3.2 MFW_GST_VPU_DECODER_PLUGIN 2.0.3 build on Jul 23 2013 11:20:21. So the next moved would be to try upgrading versions on LTIB if they want to use this system; in case switching to Yocto is viable, then the upgrade is already done.
記事全体を表示
In the older code, headphone router is always on, it is not a good choose for low power demand. This patch uses imx_hp_jack_gpio.jack_status_check to instead of w->event. It enables Ext Spk and disables Headphone Jack when Headphone Jack is plug in, it disables Headphone Jack and enables Ext Spk when Headphone is out.
記事全体を表示
Q: MX53 u-boot doc to enable the splash screen and went through Re: MX53 u-boot Splash Screen support but I can't seem to get the splash working on the VGA output.  A: FSL do not have solution / recommendations for VGA splash screen under U-boot. Only LVDS is supported. Typically, the Uboot bootloader does not interact with any display interface and does not have a splash screen displaying capability. To add this feature to Uboot on i.MX5 platform, the IPU driver should be included into the Uboot code. Looks like we do not have ready to use solution for the LCD. As an example for LCD configuring it makes sense to use LCD settings from Linux driver. Another approach - to use Linux (Penguin) logo (assuming Linux is booted quickly after U-boot) - at least, Linux supports more display drivers and its logo using is specified. follow up question is since the Tux the penguin logo is only 80x80 is it possible to make a larger image for the Linux start up logo? yes, you should configure kernel for the new image on make menuconfig That doesn’t help this H/W guy, but I think this may - https://community.freescale.com/thread/304300    look for  “#To change the splash screen of linux kernel (small penguine on top left corner)..“
記事全体を表示
Starting from $52, the VAR-SOM-MX6 sets the bar for unparalleled design flexibility. The VAR-SOM-MX6 ensures scalable and simplified development, while also extending the product lifecycle. Thanks to four CPU core assembly options, customers can apply a single System on Module in a broad range of applications to achieve short time-to-market for their current innovations, while still accommodating potential R&D directions and marketing opportunities.     VAR-SOM-MX6 CPU: Freescale iMX6 Key features include: Freescale i.MX6 1.2GHz Quad / Dual / Single core Cortex-A9       2GB DDR3, 1GB SLC NAND Flash       Full HD 1080p video encoding/decoding capability       Vivante GPU providing 2D/3D acceleration       Simultaneous multiple display support       Gigabit Ethernet       TI WiLink™ 6.0 single-chip connectivity solution (Wi-Fi, Bluetooth®)       PCI-Express 2.0, S-ATA 3.0       Camera interface       USB 2.0: Host, OTG       Audio In/Out       Dual CAN Bus This versatile solution's -40 to 85°C temperature range and Dual CAN support is ideal for industrial applications, while 1080p video and graphics accelerations make it equally suitable for intensive multimedia applications. The impressive scalability of the VAR-SOM-MX6 satisfies the needs of the most demanding future application requirements whether faster processing power, enhanced algorithms or improved graphics and video performance to name just a few. The VAR-SOM-MX6 is an all-round solution with broad connectivity and sophisticated video and acceleration graphic capabilities, delivering a range of middle to high end assembly options all from the same product. For more details, please see VAR-SOM-MX6 CPU: Freescale iMX6
記事全体を表示
For imx8QM, The manufacture mode is supported on SD2 which is powered by LDO2 of PMIC2 on MEK board. LDO2 of PMIC2 on MEK board is OFF by default. (LDO2 of PMIC1 is on by default) So manufacture mode is NOT working on the imx8QM MEK board. the solution would be: 1. schematic change Exchange the power supply(VCC_LDO_SD) and USDHC_VSELECT signal of SD2 and SD1. between PMIC2 (U23) and PMIC 1(U10). so that, the VCC_LDO_SD2) and USDHC2_VSELECT will be located on where VCC_LDO_SD1) and USDHC1_VSELECT are origonally.  and VCC_LDO_SD1 and USDHC1_VSELECT will be located on where VCC_LDO_SD2) and USDHC2_VSELECT are origonally.  SD1 will no longer be supported as the boot resource, instead SD2 will be. anyway you still can connect a WIFI to SD1 , becasue the power supply can be turned on after software booting up. 2. Modify the default fuse of PMIC, whcih is to enable LDO2 of PMIC2 by default.     please contact your local FAE and Sales for this.  we may add notification in the reference schematic and HW development guild in the future.
記事全体を表示
Click to view the webinar recording View More Information and Order the Vision Starter Kit
記事全体を表示
Hi, The document "How to create ubuntu hardfloat rootfs for imx6d/q" was shared by Junping Mao. https://community.freescale.com/docs/DOC-95185 However, some modification need to be made to build imx-tests on this rootfs. Attached please find the guide for building imx-tests on hf-ubuntu rootfs for imx6d/q. Any problems, pls feel free to let me know. Regards, Alvin zheng
記事全体を表示
Gstreamer Please, select the gstreamer package in [LTIB] under Package List. Choose the package that you will need. For a complete installation, select all: gstreamer gstreamer-plugins-base gstreamer-plugins-good gstreamer-plugins-bad gstreamer-plugins-bad gstreamer-plugins-ugly What can be done With Gstreamer, it's possible to: i.MX27 ADS Board Video GST Play i.MX27 ADS Board Video GST Encode i.MX27 ADS Board Video GST Video Streaming
記事全体を表示
On default i.MX6UL EVK board, it supports three boot device: SD Card boot in main board, micro-SD card boot in CPU board and QSPI-FLASH in CPU board. As we know, i.MX6UL supports NAND device boot and there are NAND device footprint in the EVK board. If customer wants to use NAND boot, there is something to rework in both hardware and software. Hardware Modification NAND device boot mode is conflict with micro-SD card and QSPI-FLASH device boot modes. 1. Remove U303 in CPU board and DO NOT insert micro-SD card into J301 2. Solder U302 NAND FLASH on EVK board Software Modification In Yocto-Linux BSP standard release, NAND device boot is not supported. We need add support in u-boot, linux DTB and MFGTool. 1. u-boot-imx modification and build Replace u-boot-imx/include/configs/mx6ul_14x14_evk.h with the same file in the attachment Copy mx6ul_14x14_evk_nand_defconfig in the attachment to u-boot-imx/configs/ Build the new u-boot.imx: make distclean; make mx6ul_14x14_evk_nand_defconfig;make Rename u-boot.imx to u-boot-imx6ulevk_nand.imx 2. Linux DTB modification and build Copy imx6ul-14x14-evk-gpmi-weim.dts in the attachment to kernel/arch/arm/boot/dts/ Build imx6ul-14x14-evk-gpmi-weim.dtb: make imx6ul-14x14-evk-gpmi-weim.dtb Rename imx6ul-14x14-evk-gpmi-weim.dtb to zImage-imx6ul-14x14-evk-gpmi-weim.dtb 3. MFGTOOL modification Copy mfgtool2-yocto-mx6ul-evk-nand.vbs in the attachment to MFGTOOL root direcory Copy u-boot-imx6ulevk_nand.imx and zImage-imx6ul-14x14-evk-gpmi-weim.dtb to MFGTOOL\Profiles\Linux\OS Firmware\firmware\ Copy u-boot-imx6ulevk_nand.imx and zImage-imx6ul-14x14-evk-gpmi-weim.dtb to MFGTOOL\Profiles\Linux\OS Firmware\files\ Congratulations!!!  You can burn NAND image to i.MX6UL-EVK board with mfgtool2-yocto-mx6ul-evk-nand.vbs script now!!
記事全体を表示
Garz & Fricke product SANTARO will be displayed on the Freescale booth during the upcoming embedded world in Nuremberg. SANTARO is using the Freescale iMX6 processor. Single-, dual and quadcore.
記事全体を表示
Overview Resources Download Ubuntu 12.04.01 Download i.MX28EVK BSP and Documents Ubuntu Host Setup Host Package Update Ubuntu Configuration PDF Sudo Priviledges Default Shell CCACHE Directory Layout Extract SDK and Documents Install BSP Sources Ubuntu Software Packages for LTIB Patching LTIB Create SD Card Using Ubuntu Host Media Booting Selection Cable Connections   Overview Freescale's i.M28EVK development kit provides a platform for running software and evaluating features of the i.MX28 processor. This document provides the details for running the Linux Board Support Package (BSP) on the Ubuntu 12.04 64-bit Precise Pangolin Host on an Intel/AMD architecture computer. The 32-bit host is not covered in this document and does have different configuration steps than described here.   An Ubuntu Linux host is used to cross-compile the BSP creating ARM images. The BSP provides a build system named Linux Target Image Builder, (LTIB),  the GNU tool suite for compiling and debugging, U-Boot boot loader, Linux kernel, and a root file system. Resources i.M28EVK- i.MX28 Evaluation Kit Web Page MCIMX28EVKJ Product Summary Page- i.MX28 Download Collateral L2.6.36_MX28_SDK_10.12_Source- BSP Source Download Linux documentation - i.MX28EVK Documentation Ubuntu 12.04.1 LTS (Precise Pangolin)- Ubuntu 12.04 Release Download Ubuntu 12.04.01 A dedicated computer running Ubuntu or a Virtual Machine, (VMware or VirtualBox), can be used for running the Host Ubuntu software. The Ubuntu image is available for downloaded from the Ubuntu site: Ubuntu 12.04.1 LTS (Precise Pangolin).   This Ubuntu host ISO was used with the md5 checksum: ubuntu-12.04.1-desktop-amd64.iso  06472ddf11382c8da1f32e9487435c3d   One way to acquire the ISO is to use zsync to download: zsync http://releases.ubuntu.com/12.04/ubuntu-12.04.1-desktop-amd64.iso.zsync  Once downloaded, installing the ISO is user preference - either a dedicated Linux PC or in a Virtual Machine.   Download i.MX28EVK BSP and Documents The BSP download is from this site L2.6.36_MX28_SDK_10.12_Source and the documents from Linux documentation that requires a free registration to specify login credentials,   436e0b8e1c7976c657d530a45f9dbd0c L2.6.35_10.12.01_SDK_source_bundle.tar.gz de0274320a17c1e989d1ef5c088973e2 L2.6.35_10.12.01_SDK_docs.tar.gz   Ubuntu Host Setup Ubuntu login credentials of User: user Password: user are used for this documents. Host Package Update Once logged in to the Ubuntu host, the existing packages are brought up to date to the latest version before installing the BSP. The Ubuntu package manager used is apt-get. $ sudo apt-get update $ sudo apt-get upgrade  01. Check all installed packages for new revisions 02. all newer packages found are installed.   Addtional packages are required for the ltib build system. Ubuntu Configuration PDF evince is the default pdf reader, another option is zathura. $ sudo apt-get install zathura Sudo Priviledges LTIB requires super user priviledges for some operations. To enable a visudo entry is added to the sudo'ers file. For more information run 'man visudo'.   $ sudo visudo  The first word, user, is the login account 'user' This can be changed to whatever login you used, or if you have groups configured you can provide a group that developers are in - refer to the man page for sudo for details. Add this line:   user ALL =NOPASSWD: /usr/bin/rpm/ /opt/freescale/ltib/usr/bin/rpm   Default Shell Ubuntu uses the default shell 'dash'. This however causes failures on bash scripting which is part of the ltib system. Change the default shell from 'dash' to 'bash'   $ sudo update-alternatives --install /bin/sh sh /bin/bash 1  CCACHE ccache provides a fast C/C++ compiler cache which is supported in the ltib system. To configure once the ccache package has been installed: $ sudo apt-get install ccache $ ccache -M 50M $ ccache -c  02. Set the cache limit to 50 Meg 03. Clear the cache folder   Directory Layout The following directory structure is used: /home/user/freescale/imx28/ |-- archive |-- L2.6.35_10.12.01_ER_source |-- L2.6.35_10.12.01_SDK_docs |-- L2.6.35_10.12.01_SDK_scripts |-- ltib |-- ubuntu-imx28-ltib-patch   The archive directory is where the BSP and documents are stored; command to create the directory: $ mkdir -p ~/freescale/imx28/archive   Extract SDK and Documents The following instructions were used to extract the contents of the Software Development Kit:   $ cd ~/freescale/imx28/archive $ tar -zxf L2.6.35_10.12.01_SDK_source_bundle.tar.gz -C ..    01. Change into the directory containing the tar ball that is compressed. 02. Extract the contents into the directory above (-C ..) the current directory -z unzip -x extract -f L2.6.35_10.12.01_SDK_source_bundle.tar.gz   $ tar -zxf L2.6.35_10.12.01_SDK_docs.tar.gz  01. Extract the contents into the directory above (-C ..) the current directory     -z unzip     -x extract     -f L2.6.35_10.12.01_SDK_docs.tar.gz this file The contents of both tar files are now in the directory /home/user/freescale/imx28. Install BSP Sources After extracting the content from the L2.6.35_10.12.01_SDK_source_bundle.tar.gz the file L2.6.35_10.12.01_SDK.source.tar.gz contains all the sources and the build system. Extract the contents and install. This will create the ltib directory which is the build system. $ tar -zxf L2.6.35_10.12.01_SDK_source.tar.gz $ cd L2.6.35_10.12.01_ER_source $ ./install  Read the license information and accept by entering YES. An installation directory is then asked for, providing:  .. which is the parent directory. The installation script copies the packages and will inform you that 'Installation complete, your ltib installation has been placed in ../ltib, to complete the installation: cd .../ltib ./ltib  HOWEVER before doing this, there are packages and patches that need to be applied to run ltib on Ubuntu 12.04.01. Ubuntu Software Packages for LTIB The following packages are required. The script pkg-setup.sh attached below has these packages which can be downloaded and executed to install. $ sh pkg-setup.sh  sudo apt-get -y install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev sudo apt-get -y install libdbus-glib-1-dev liborbit2-dev intltool sudo apt-get -y install ccache zlib1g zlib1g-dev gcc g++ libtool sudo apt-get -y install uuid-dev liblzo2-dev tcl wget libncurses5-dev sudo apt-get -y install libncursesw5-dev lib32z1 libglib2.0-dev xsltproc sudo apt-get -y install ia32-libs libc6-dev-i386 The file pkg2-setup.sh contains optional packages for development. To install, download and execute: $ sh pkg2-setup.sh Please refer to the document ltib_build_host_setup.pdf for more information on host setup. Patching LTIB The location of files from the glibc-devel and zlib Ubuntu 12.04 packages has changed from 9.0.4 Ubuntu which the original ltib was released against. To update ltib operation the following patches are implemented from the directory ~/freescale/imx28/ltib 1. The file ltib is changed at line 2387 adding the '-v' option to the rpm call OLD:     system('rpm --force-debian 2>/dev/null') == 0? NEW:     system('rpm -v --force-debian 2>/dev/null') == 0? 2. The file bin/Ltibutils.pm is updated to support glibc-devel and zlib.   glibc-devel update: Line 563 add check for /usr/lib32/libm.so 'glibc-devel' => sub {-f 'usr/lib/libm.so' || -f '/usr/lib64/libz.so' || -f '/usr/lib32/libm.so'},   zlibc update: Line 584 add /lib/x86_64-linux-gnu/libz.so* zlib => sub{my @f = (glob('/usr/lib/libz.so*'),               glob('/lib/x86_64-linux-gnu/libz.so*'),               glob('/lib/libz.so*'),   The above patches are also in the attachment 0001-patches-for-12.04-ubuntu.patch.   LTIB packages also need adjustments to correctly build on Ubuntu. The tar file below, ubuntu-imx28-ltib-patch.tgz contains all the updates. Download and extract the contents at the same directory level as your ltib source directory. $ tar -zxf ubuntu-imx28-ltib-patch.tgz ├── ltib ├── ubuntu-imx28-ltib-patch └── ubuntu-imx28-ltib-patch.tgz Change directories to ubuntu-imx28-ltib-patch and then run the install-patches.sh script. $ cd ubuntu-imx28-ltib-patch $ ./install-patches.sh   The following packages are updated: lkc mtd-utils mux_server sparse Create SD Card Using Ubuntu Host The tar file L2.6.35_10.12.01_SDK_scripts.tar.gz contains scripts for writing the images from the ltib build to a SD card. Extract the content, copy the scripts to the ltib directory, and update the mk_mx28_sd script to work with the updated fdisk command.   $ tar -zxf L2.6.35_10.12.01_SDK_scripts.tar.gz $ cd L2.6.35_10.12.01_SDK_scripts $ cp mk_hdr.sh ~/freescale/imx28/ltib $ cp mk_mx28_sd ~/freescale/imx28/ltib $ cd ~/freescale/imx28/ltib  Edit mk_mx28_sd script and add the 'u' at line 177 then the o command after. This changes cylinders to sectors.   OLD: echo "o n   NEW: echo "u o n   Once updated to create the SD card which is at /dev/sdb: $ ./mk_mx28_sd /dev/sdb  NOTE: if mounted automatically, you need to unmount for the script to work $ sudo umount /dev/sdb*      Media Booting Selection The i.MX28EVK has a boot option to execute from the SD Card in Slot 0 which is located on the bottom of the EVK. On the top of the EVK there are switches that are read during the start up process to determine what boot media to use. The SD Card in slot 0 is used for this example which requires the settings: B3/DIP1 B2/DIP2 B1/DIP3 B0/DIP4 1 0 0 1 Refer to the user guide, i.MX28_Linux_BSP_UG.pdf section 3.2.1. Boot Modes for all options. The user guide is found in the Linux documentation bundle documentation.  Refer to the next section for a picture showing the boot switch location and the SD Card Slot 0 location. Cable Connections A computer serial port is connected to the i.MX28EVK serial port. The communication setting is 115200 baud, 8 data bits, No parity, and 1 stop bit. There is NO flow control set for this port. This is typically shown as 115200, 8N1. The power supply is connected  
記事全体を表示
This is a simple step by step guide on how to change the Android boot animation which is shown when the system is loading.   Requirements   - Android L5.1.1_2.1.0 BSP. The basics of the boot animation may also apply to older and upcoming releases but L5.1.1_2.1.0 BSP was used for this document. File names, settings or paths may be changed in older or newer releases.   - i.MX6Q Sabre SD Board or any other i.MX board supported by the BSP release, for testing.   - 7-Zip. This is a free compression tool and has the necessary settings for preparing the boot animation file. It is important that the boot animation file is in Zip format with no compression, otherwise the file won’t be read and the animation will not be shown. Zip tools integrated on some Operating Systems may not always allow for these configurations. You may download this utility from the link below: http://www.7-zip.org/   - Android adb tool. This tool is part of the Android SDK. You may download the SDK as part of Android Studio or the SDK as Stand Alone on the following link. Only the adb is required to follow up this document. http://developer.android.com/sdk/installing/index.html   Understanding the boot animation format.   The animations used by Android when booting are actually a series of images in either jpg or png format in a zip file with no compression (storage mode) and a text file (desc.txt) with the specified resolution, framerate and loops to be played by the animation. Each folder containing a part of the animation must contain the images numbered from 000 onwards.  This file is always called bootanimation.zip An example of a boot animarion can be found attached to this document.   The contents of the desc.txt file on the attached example are as follow: 480 292 30 p 1 0 part0 p 0 0 part1 (please note that there should be an empty line at the end of the document).   Line 1: Screen resolution followed by FPS (Frames per Second) of the animation.   Lines 3-5: The p serves to describe that the line contains a part of the animation; followed by the number of times the section of the animation will play (with zero being an infinite loop); followed by a delay in frames before moving to the next line. Finally, the folder containing the files of that specific part of the animation (this is why most animations use “part” for the folder name).   Line 6: A blank line. This is important as without it the animation may not run as it will consider the description file incomplete. There are some animations available around the web as well as some free tools or apps that allow you to create your own animations. You may find an example animation attached to this document which you may use as reference.   It is important that no other files are included on the bootanimation.zip file. This includes the thumbnails created automatically by Windows. Please delete them from your fule before loading it to the board.   Please note that the animation may be repeated in a loop if it’s shorter than the actual time it takes for the system to load. However, the animation will play complete regardless of the loading time so very long boot animations may give the appearance of a longer booting time.   The location of the boot animation file is given on the bootanimation_main.cpp file, which is located on the following path: <MYANDROID_DIR>/frameworks/base/cmds/bootanimation/bootanimation_main.cpp   There are two definitions that give the file location. We’re focusing on the default image for this document (unencrypted). #define SYSTEM_BOOTANIMATION_FILE "/system/media/bootanimation.zip" #define SYSTEM_ENCRYPTED_BOOTANIMATION_FILE "/system/media/bootanimation-encrypted.zip"   Note: These definitions may be different from those in third party BSPs. It is common to find BSPs using the "/data/local/” folder as USER_BOOTANIMATION. This is not supported by default on NXP’s BSP.   Loading the new boot animation file.   - Building a User Debug image Android protects certain folders to avoid tampering, so in order to change the boot animation we will use adb in order to access the file system. However, it is necessary to use a image with root access so we will be using a user debug image.   In order to compile as user debug use the following lunch command after following the instructions in the Android User's Guide: $ lunch sabresd_6dq-userdebug   After configuring the build for user debug you can then build using make. (This process may take several hours)   - Enabling USB Debug mode Your board should be running android and then be connected to the computer using the USB OTG port. In order for adb to work you have to enable USB debugging by opening Settings and scrolling down to the “About” option clicking the "About" option 7 times.   - Using adb to load the new boot animation We’ll connect to the SABRE board using the Android SDK for Windows adb tool available at the path below: android-sdk-windows\platform-tools   Open a command promt in windows and go to the adb path. Then start the adb server with the following command: $ adb start-server   This will initialize the adb daemon. In order to connect to the device permission must be granted. A pop up will appear asking whether to trust or not the computer host. Since we will be changing the system partition we must initialize adb as root: $ adb root   This will restart the adb daemon in root mode. You will need to grant access from your device. You may see the list of connected with: $ adb devices   If you wish to see the contents of the filesystem you may enter the shell with the following command: $ adb shell   However, we will be using the pull/push commands from adb in order to change the bootanimation.   If you wish to download the current bootanimation for backup you may do so with the following command: $ adb pull /system/media/bootanimation.zip C:\ This will download the bootanimation.zip file to C:   Since the system partition is read only you will need to remount with the adb prior to pushing the replacing boot animarion $ adb remount $ adb root push C:\BootAni\bootanimation.zip /system/media   After this you may reboot your board and you should see the new boot animation. Original Attachment has been moved to: bootanimation.zip
記事全体を表示
Adding Support to USB Host High Speed on i.MX27ADS First, ensure these patches were applied: usbh2_cspi1_ss2.patch usbh2_set_ulpi_xcvr.patch Unselect SPI2: Device Drivers  --->              SPI support  --->                     [ ]   CSPI2 Select USB Host2: USB support  --->            <M>   EHCI HCD (USB 2.0) support                 [*]       Support for Host2 port on Freescale controller
記事全体を表示
The i.MX31 multimedia applications processors are designed for a broad range of industrial, consumer and automotive applications. Based on an ARM1136JF-S™ core, both the i.MX31 and the i.MX31L processors are engineered to deliver powerful performance while minimizing power consumption. The rich feature set of the i.MX31 processors make them an excellent choice for portable media players, portable navigation devices, medical/industrial monitoring systems, automotive infotainment systems and many general embedded applications. i.MX Family Comparison Product Information on Freescale.com i.MX31 Multimedia Applications Processor Evaluation/Development Boards and Systems IMX31PDK:  i.MX31 Product Development Kit Getting Started Getting Started with the i.MX31PDK Board Flashing i.MX31 PDK Board I.MX31 PDK Board using RedBoot Miscellaneous Tutorials Blinking iMX31PDK LEDs using U-Boot How to Test i.MX31 RNGA Hardware? How to Test i.MX31 TvOut on i.MX31PDK How to Use Clock Out on i.MX31 Issues when interfacing Micron's 78nm mDDRs IMX31ADS Getting Started Getting Started with the i.MX31ADS Board Flashing I.MX31 ADS Board Miscellaneous Tutorials Booting Linux from NAND Flash on the i.MX31ADS Compiling Linux kernel from mainline to i.MX31ADS Issues when interfacing Micron's 78nm mDDRs Embedded Software and Tools Android OS for i.MX Applications Processors Partners / 3rd-Party Development Tools Starterkit STKa31 (Technology in Quality) Additional Resources i.MX31 ADS i.MX31 PDK i.MX31 PDK Board Alpha Blending i.MX31 PDK Board DirectFB i.MX31 PDK Board V4L tests i.MX31 PDK Contents i.MX31 PDK Setting Buttons and Jumpers i.MX31 Lite Kit
記事全体を表示