i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
tarball created by Curtis Wald and Leonardo Sandoval containing patches to fix ltib issues for Ubuntu 12.04.   Steps to use this tarball   # go to ltib folder $ cd <ltib full path>   # untar the tarball $ tar -xzvf ubuntu-ltib-patch.tgz   # go to untared folder $ cd ubuntu-ltib-patch   #install patches $ ./install-patches.sh <ltib full path>     You above steps are contained in this script:   https://community.freescale.com/servlet/JiveServlet/downloadBody/93455-102-2-2825/patch-ltib-ubuntu12.04.sh,   so instead of typing them manually you can execute the following command   curl -L https://community.freescale.com/servlet/JiveServlet/downloadBody/93455-102-2-2825/patch-ltib-ubuntu12.04.sh | bash   under your ltib folder.
記事全体を表示
Question: Is it true ture that MX6 VPU is capable of encoding dual H.264 streams that are 1024x600 at 60fps?  There are slides that claim three 720p30 streams or two 1080p30 streams simultaneously. There is little guidance as to what the VPU limits in resolution, frame rate and bit rate are for other resoluitons and frame rates. Is there any information that can be used to decide if  the VPU can encode an arbitrary video stream or multiple arbitrary video streams?  Since memory bandwidth will enter into this decision at some point has anyone quantified the memory bandwidth requirements verses video resolution and frame rate? Answer: Maximum supported trhoughput,  is 72,576,000 pixels /s @ VPU frecuency of 266 mhz 2 x  1024 x 600 x 60hz = 73,728,000 So this is not supported. If framerate is lower i.e.  30hz  then it will be supported.
記事全体を表示
This is sample code for CSC settings for /dev/fb1. It can calculating the CSC matrix and updates in real time from given parameters(Brightness,Contrast,Saturation,Hue, and gamma).
記事全体を表示
 This article uses i.MX Linux® User's Guide, Rev. L4.1.15_2.1.0-ga, 05/2017 as an example (it may be found as attachment), please refer to section 4.5.12 (How to build U-Boot and Kernel in standalone environment).   First, generate a development SDK, which includes the tools, toolchain, and small rootfs to compile against to put on the host machine.     • Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set <Target-Machine> to the machine you are building for.   <Target-Machine> may be one of the following :   • imx6qpsabreauto • imx6qpsabresd • imx6ulevk • imx6ull14x14evk • imx6ull9x9evk • imx6dlsabreauto • imx6dlsabresd • imx6qsabreauto • imx6qsabresd • imx6slevk • imx6sllevk • imx6solosabreauto • imx6solosabresd • imx6sxsabresd • imx6sxsabreauto • imx7dsabresd  The «populate_sdk» generates an script file that sets up environment without Yocto Project. This SDK should be updated for each release to pick up the latest headers, toolchain, and tools from the current release.   $ DISTRO=fsl-imx-fb MACHINE=<Target-Machine> source fsl-setup-release.sh -b build-fb   $ DISTRO=fsl-imx-fb MACHINE=<Target-Machine> bitbake core-image-minimal -c populate_sdk   or   $ bitbake meta-toolchain       • From the build directory, the bitbake was run in, copy the sh file in tmp/deploy/sdk to the host machine to build on and execute the script to install the SDK. The default location is in /opt but can be placed anywhere on the host machine.     Note. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.    $ . /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi   or    $ source /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi   From  Yocto Project Mega-Manual  Note By default, this toolchain does not build static binaries. If you want to use the toolchain to build these types of libraries, you need to be sure your image has the appropriate static development libraries. Use the  IMAGE_INSTALL  variable inside your  local.conf  file to install the appropriate library packages. Following is an example using  glibc  static development libraries:      IMAGE_INSTALL_append = " glibc-staticdev"   On the host machine, these are the steps to build U-Boot and Kernel:  • On the host machine, set the environment with the following command before building.   $ export CROSS_COMPILE=/opt/fsl-imx-fb/4.1.15/environment-setup-cortexa9hf-vfp-neon-pokylinux-gnueabi   $ export ARCH=arm • To build U-Boot, find the configuration for the target boot. In the following example, i.MX 6ULL is the target.     Download source by cloning with   $ git clone http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git -b imx_v2016.03_4.1.15_2.0.0_ga   $ cd uboot-imx $ make clean $ make mx6ull_14x14_evk_defconfig $ make u-boot.imx   • To build the kernel, execute the following commands:   Download source by cloning with   $ git clone http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git -b imx_4.1.15_2.0.0_ga   $ cd linux-imx $ make defconfig $ make   • To build an application (Hello World) as test.c:   $ source /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi $ cd ~/test/ $ arm-poky-linux-gnueabi-gcc --sysroot=/opt/fsl-imx-fb/4.1.15-2.0.0/sysroots/cortexa9hf-neon-poky-linux-gnueabi -mfloat-abi=hard test.c To check if the the compiled code (a.out) is ARM executable   $ file ./a.out   ./a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=0e5c22dcf021748ead2c0bd51a4553cb7d38f6f2, not stripped   Copy file a.out to target Linux filesystem and before run it check again :   root@imx6ul7d:/unit_tests/1# file a.out   a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=0e5c22dcf021748ead2c0bd51a4553cb7d38f6f2, not stripped   To define what Linux libs are needed to run our application :   root@imx6ul7d:/unit_tests/1# ldd a.out     linux-vdso.so.1 (0x7ee93000)   libc.so.6 => /lib/libc.so.6 (0x76e64000)   /lib/ld-linux-armhf.so.3 (0x76f9d000)   If some libs are not located in the filesystem you can observe the following message :   -sh: root@imx6ul7d:/unit_tests/1#./a.out: No such file or directory   Finally - run a.out:   root@imx6ul7d:/unit_tests/1# ./a.out Hello World root@imx6ul7d:/unit_tests/1#
記事全体を表示
HW: i.MX7 SabreSD SW: Android N7.1.1_1.0.0   There is KPP module on i.MX7, but NXP reference board didn't have it. We reworked a "keypad" and has the demo. Signal: For testing, launch an app in Android that can accept text input. KPP also supports multiple input, the "A" is showed by pressing "shift" + "a".   As a side note, 1. The input device driver is drivers/input/keyboard/imx_keypad.c 2. The input event driver is drivers/tty/vt/keyboard.c Original Attachment has been moved to: 0001-Enable-KPP-on-i.MX7.patch.zip
記事全体を表示
To use Android GDB for native code, take mediaserver as an example. Setup on board. adb push prebuilt/android-arm/gdbserver/gdbserver system/bin/ adb shell ps adb shell /system/bin/gdbserver :5039 --attach <PID> & Setup on host. source build/env.sh adb forward tcp:5039 tcp:5039 gdbclient mediaserver b createPlayer c
記事全体を表示
Description       this doc is explain how to develop a audio card driver base on i.MX6 platform. which explain the ASOC architecture struction basic knowledage and then give some sample for the audio driver development like: 1:NXP SGTL5000: NXP i.MX BSP sabrelite board default support it. 2: Wolfson WM8524.    A: 3.0.35 BSP support: i.MX6 setbox BSP support it:(which in elder fsl community link and out of data)    B: 3.14.28 BSP support pls check attachment: 3: Wolfson WM8960.     which include how to add the android middle-layer and driver, pls check attachment. 4: TI TLV320AIC3120      which include how to add the android middle-layer and driver, pls check attachment. 5: TI TLV320AIC3X   Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 SabreSDP https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false which have a doc MX6X_ASOC_V5-20191115.pdf and related driver sample codes.
記事全体を表示
  IMX6 UL boot process is described in Chapter 8 (System Boot) of the Reference Manual. Also you may look at the following Community regarding i.MX6 boot ROM activity. How to build bootable SD image (for i.MX6 SL as example)  U-boot is used as Linux bootloader and U-boot image should be located in SD area, used by i.MX6 boot ROM. The simplest way to get bootable SD card is just to copy system image in so called .sdcard format. Such image is prepared in Yocto by default and can be transfered to SD card with Linux dd command or Windows win32diskimager utility. Guide to the .sdcard format  Win32 Disk Imager download | SourceForge.net   The full SD image (.sdcard) should contain all parts, needed for Linux boot (U-boot, kernel, dtb, file system), maybe except U-boot environment. Carry out the following command to copy the SD card image to the SD/MMC card. Change sdx below to match the one used by the SD card. $ sudo dd if=<image name>.sdcard of=/dev/sdx bs=1M && sync   Note, U-boot environment (described below) should be set (and saved) in U-boot after the first start.   In any case it makes sense to understand general structure and implementation details of bootable SD card. Instructions are provided in section 4.3 (Preparing an SD/MMC card to boot) of i.MX Linux® User's Guide in Linux doc package (L4.1.15_2) http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS&Parent_nodeId=1337699481071706174845&Parent_pageType…  Summary page : i.MX 6 / i.MX 7 Series Software and Development Tool|NXP    For a Linux image to be able to run, four separate pieces are needed: • Linux OS kernel image (zImage) • Device tree file (*.dtb) • U-Boot bootloader image • Root file system (*.ext3 or *.ext4)   The mentioned files may be found in demo images on NXP Web or generated with Yocto. After a build is complete, the created image resides in <build directory>/tmp/deploy/images The device tree file (.dtb) contains board and configuration-specific changes to the kernel. Change the device tree file to change the kernel for a different i.MX board or configuration.    By default, the kernel image and DTB are located on FAT partition without a fixed raw address on the SD card. Generally fix addresses / blocks of SD card may be applied for kernel and DTB location. The users have to change the U-Boot boot environment if the fixed raw address is required. In example below the following image layout on SD card is assumed : Start address (sectors) = 0x400 bytes (2) for U-boot (i.MX6 boot ROM reads first 4K bytes of SD card). Start address (sectors) = 0xa00000 bytes (20480) for FAT partition, size=500MB, intended for Kernel zImage and DTBs. Start address (sectors) = 0x25800000 bytes (1228800) for rootfs.    Preparing the card   An SD/MMC card reader, such as a USB card reader, is required. Any Linux distribution can be used. Further follow instructions in sections 4.3.1 (Preparing the card), 4.3.3 (Partitioning the SD/MMC card), 4.3.4 (Copying a bootloader image), 4.3.5 (Copying the kernel image and DTB file), 4.3.6 Copying the root file system (rootfs) of attached "i.MX_Graphics_User's_Guide.pdf". The next step - try to insert the SD card to slot in i.MX6UL board, select proper boot options for SD boot and power the system. U-boot prompt should appear. Finally it is needed to configure environment for further Linux boot from SD. U-Boot > setenv mmcdev 1 U-Boot > setenv mmcpart 1 U-Boot > setenv mmcroot '/dev/mmcblk1p2 rootwait rw' U-Boot > setenv loadaddr 0x80800000 U-Boot > setenv fdt_addr=0x83000000 U-Boot > setenv fdt_file imx6ul-9x9-evk.dtb U-Boot > setenv mmcpart 1 U-Boot > setenv loadfdt 'fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}' U-Boot > setenv loadkernel 'fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} zImage' U-Boot > setenv bootcmd 'mmc dev ${mmcdev}; run loadkernel; run mmcargs; run loadfdt; bootz $ {loadaddr} - ${fdt_addr};' U-boot > saveenv fdt_file should be set for your case ( on example “imx6ul-9x9-evk.dtb”) Try reboot with new environment.
記事全体を表示
Issue Description When running Android R10.4 on MX51 BBG, the system can not resume sometimes by following the test steps: 1) Enable CLAA-WVGA lcd panel - single display. 2) Play a video in Gallery. 3) Press power key to suspend the system. 4) Press power key to resume the system. 5) Do 3) and 4) continuously. Debug Details When adding the following debug information into vpu_resume function in file drivers/mxc/vpu/mxc_vpu.c, the system gets hang into while loop with the log "VPU Blocking 1**************": static int vpu_resume(struct platform_device *pdev) {         int i;                 WRITE_REG(BITVAL_PIC_RUN, BIT_INT_ENABLE);                 WRITE_REG(0x1, BIT_BUSY_FLAG);                 WRITE_REG(0x1, BIT_CODE_RUN);                 while (READ_REG(BIT_BUSY_FLAG)) {                           printk("VPU Blocking 1**************\r\n");                }; } Root Cause In some use cases,  VPU power gating didn't happen after vpu_suspend() returned successfully because some other devices refused to suspend or other reasons. So vpu_resume() ran FW init code when VPU was idle instead of power off, which could keep BIT_BUSY_FLAG always be 1. Solution In vpu_resume(), if VPU PC is not 0, which means VPU is still running, skip running FW init code. See attached patch based on R10.4.
記事全体を表示
How to Test Yocto for i.MX6 i.MX Yocto Project: How Can I Collaborate on the Freescale Yocto Project? i.MX Yocto Project: How Can I Build the Freescale Yocto Images using bitbake? i.MX Yocto Project: How Can I Build the Freescale Yocto Images using hob? i.MX Yocto Project: What Can I Do if I Run Into a Compilation Error? i.MX Yocto Project: Are There Prebuilt Images Available? i.MX Yocto Project: How Can I Quicken the Compilation? i.MX Yocto Project: how can I conserve disk space during builds? i.MX Yocto Project: How do I add an existing package to an image? i.MX Yocto Project: Can I use a virtual machine to build? i.MX Yocto Project: How can I build an image with (latest) mainline kernel? i.MX Yocto Project: How can I (quickly) modify a package' source code and test it? i.MX Yocto Project: How can I find out the packages include on an image? i.MX Yocto Project: How can I compile the kernel manually? i.MX Yocto Project: How can I patch the kernel? i.MX Yocto Proyect: How can I create a new Layer? i.MX Yocto Project: How can I contribute to the community? i.MX Yocto Project: Where can I see current  BSP issues? i.MX Yocto Project: Where are the mainstream repositories hosted? Tutorials: Yocto Training - HOME http://www.slideshare.net/OtavioSalvador/yocto-training-in-english - Great tutorial created by the Community's maintainer (there is also a Portuguese version) i.MX Yocto Project: Freescale Yocto Project Tutorial - It covers some basic developing tasks Others: Useful bitbake commands i.MX Yocto Project: ltib versus bitbake
記事全体を表示
A simple Linux kernel module to react on GPIO-generated interrupts
記事全体を表示
This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera options on the i.MX 8 boards. Plus, this document describes some Advanced camera use cases too, such as multiples cameras output using imxcompositor_g2d plugin, GStreamer zero-copy pipelines and V4L2 API extra-controls examples.
記事全体を表示
MX6X_Uboot_V1-20130910.doc: 3.0.35: 3.0.35
記事全体を表示
imx53 DDR stress tester V0.042
記事全体を表示
         In recent months, some I.MX customers hope to compile u-boot-fw-utils in yocto and get fw_printenv & fw_setenv tools.          Although there are u-boot-fw-utils bblayers in Yocto recipes, by default, u-boot-fw-utils is not based on u-boot-imx, but downloaded from the u-boot source website, when using bitbake When u-boot-fw-utils compiles it, it will fail to compile.          For example: # cd  ~/imx-yocto-bsp-5.4.3_1.0.0 # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source imx-setup-release.sh -b build_sabresd # bitbake u-boot-fw-utils -c compile          If changing .config to be mx6sxsabresd_optee_defconfig in the top directory of u-boot source code, new errors will occur, like descriptions in the link:          https://community.nxp.com/message/1318081?commentID=1318081#comment-1318081            The root cause is that the u-boot is not u-boot-imx.          If we did the test below, it is easy to validate it.      Compiling u-boot # bitbake u-boot-imx -c compile          After compilation is done, u-boot-imx source code will be released .      Changing u-boot source code of u-boot-fw-utils directory          Replace u-boot source code in u-boot-fw-utils directory with u-boot-imx source code. Then continue to compile u-boot-fw-utils # bitbake u-boot-fw-utils -c compile          We will find it can be compiled successfully. This shows that when u-boot-fw-utils is compiled, the downloaded u-boot source code must be u-boot-imx.          In order to achieve this, we need to add recipes to yocto's u-boot-imx, and we can successfully compile fw_printevn and fw_setenv through the bitbake command. Please follow these steps to add u-boot-fw-utils for i.mx to yocto! copy 2 files in attacments to ~/imx-yocto-bsp-5.4.3_1.0.0/sources/meta-imx/meta-bsp/recipes-bsp/u-boot cd ~/imx-yocto-bsp-5.4.3_1.0.0 run below comands # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source imx-setup-release.sh -b build_sabresd # bitbake u-boot-imx-fw-utils -c compile # bitbake u-boot-imx-fw-utils -c install   Then you will get fw_printenv & fw_setenv [Comment]          If i.MX users are using other version of linux BSP, she only need to modify the following content of u-boot-imx-common_2019.04.inc to compile u-boot-fw-utils. …… LIC_FILES_CHKSUM = "file://Licenses/gpl-2.0.txt;md5=b234ee4d69f5fce4486a80fdaf4a4263"   UBOOT_SRC ?= "git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https" SRCBRANCH = "lf-5.4.y_v2019.04" SRC_URI = "${UBOOT_SRC};branch=${SRCBRANCH} \ " SRCREV = "228843cdf5435d4bd69f42a6015f78761ff4cc0d" ……          Then compile it following above steps.          Example for L4.14.98_2.0.0: 1.Copy u-boot-imx-common_2019.04.inc & u-boot-imx-fw-utils_2019.04.bb to ~/imx-release-bsp-4.14.98-2.0.0/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/ 2.Rename files name according to u-boot version u-boot-imx-common_2018.03.inc     u-boot-imx-fw-utils_2018.03.bb 3.Modifying u-boot-imx-common_2018.03.inc In the directory, there is u-boot-imx_2018.03.bb file, open it, and find the link of u-boot and check sum, and use lines below to replace those lines in u-boot-imx-common_2018.03.inc In u-boot-imx_2018.03.bb file: …… LICENSE = "GPLv2+" LIC_FILES_CHKSUM = "file://Licenses/gpl-2.0.txt;md5=b234ee4d69f5fce4486a80fdaf4a4263"   UBOOT_SRC ?= "git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https" SRCBRANCH = "imx_v2018.03_4.14.98_2.0.0_ga" SRC_URI = "${UBOOT_SRC};branch=${SRCBRANCH}" SRCREV = "87a19df5e462f1f63e8a6d2973c7fb9e95284d04" …… Then in u-boot-imx-common_2018.03.inc, there is the same contents as above: Save it and exit. Go back to the top directory of yocto: ~/imx-release-bsp-4.14.98-2.0.0 # cd ~/imx-release-bsp-4.14.98-2.0.0 # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source fsl-setup-release.sh -b build_sabresd # bitbake u-boot-imx-fw-utils -c compile # bitbake u-boot-imx-fw-utils -c install          The same method can be used for other Linux BSP versions.       NXP TIC Team Weidong Sun 05/28/2020
記事全体を表示
Using a RAW NAND is more difficult compared to eMMC, but for lower capacity it is still cheaper. Even with the ONFI (Open NAND Flash Interface) you can face initialization issue you can find by measure performance. I will take example of a non-well supported flash, I have installed on my evaluation board (SABRE AI). I wanted to do a simple performance test, to check roughly the MB/s I can expected with this NAND. One of a simplest test is to use the dd command: root@imx6qdlsolo:~# time dd if=/dev/mtd4 of=/dev/null 851968+0 records in 851968+0 records out 436207616 bytes (436 MB, 416 MiB) copied, 131.8884 s, 3.3 MB/s ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ As my RAW was supposed to work in EDO Mode 5, I could expect more than 20MB/s. To check what was wrong, read you kernel startup log: Booting Linux on physical CPU 0x0 Linux version 4.1.15-2.0.0+gb63f3f5 (bamboo@yb6) (gcc version 5.3.0 (GCC) ) #1 SMP PREEMPT Fri Sep 16 15:02:15 CDT 2016 CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Freescale i.MX6 DualLite/Solo SABRE Automotive Board [...] Amd/Fujitsu Extended Query Table at 0x0040 Amd/Fujitsu Extended Query version 1.3. number of CFI chips: 1 nand: device found, Manufacturer ID: 0xc2, Chip ID: 0xdc nand: Macronix MX30LF4G18AC nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 gpmi-nand 112000.gpmi-nand: mode:5 ,failed in set feature. Bad block table found at page 262080, version 0x01 Bad block table found at page 262016, version 0x01 nand_read_bbt: bad block at 0x00000a7e0000 nand_read_bbt: bad block at 0x00000dc80000 4 cmdlinepart partitions found on MTD device gpmi-nand Creating 4 MTD partitions on "gpmi-nand":‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ On line 13 you can read "mode:5, failed in set feature", meaning you are not in mode 5... so you have the "relaxed" timing you have at boot. After debuging your code (I have just remove the NAND back reading security check), you can redo the test: root@imx6qdlsolo:~# time dd if=/dev/mtd4 of=/dev/null 851968+0 records in 851968+0 records out 436207616 bytes (436 MB, 416 MiB) copied, 32.9721 s, 13.2 MB/s‍‍‍‍‍‍‍‍‍‍‍‍ So you multiplied the performances by 4! Anyway, you have a better tool to measure your NAND performance, it is mtd_speedtest, but you have to rebuild your kernel. In Yocto, reconfigure your kernel (on your PC of couse!): bitbake virtual/kernel -c menuconfig‍‍‍ Choose in the menu "Device Drivers" -> "Memory Technology Device (MTD) support" -> "MTD tests support", even it it not recommended! bitbake virtual/kernel -f -c compile bitbake virtual/kernel -f -c build bitbake virtual/kernel -f -c deploy‍‍‍‍‍‍‍‍‍ Then reflash you board (kernel + rootfs as tests are .ko files): Then you can do more accurate performance test: insmod /lib/modules/4.1.29-fslc+g59b38c3/kernel/drivers/mtd/tests/mtd_speedtest.ko dev=2 ================================================= mtd_speedtest: MTD device: 2 mtd_speedtest: MTD device size 16777216, eraseblock size 131072, page size 2048, count of eraseblocks 128, pages per eraseblock 64, OOB size 64 mtd_test: scanning for bad eraseblocks mtd_test: scanned 128 eraseblocks, 0 are bad mtd_speedtest: testing eraseblock write speed mtd_speedtest: eraseblock write speed is 4537 KiB/s mtd_speedtest: testing eraseblock read speed mtd_speedtest: eraseblock read speed is 16384 KiB/s mtd_speedtest: testing page write speed mtd_speedtest: page write speed is 4250 KiB/s mtd_speedtest: testing page read speed mtd_speedtest: page read speed is 15784 KiB/s mtd_speedtest: testing 2 page write speed mtd_speedtest: 2 page write speed is 4426 KiB/s mtd_speedtest: testing 2 page read speed mtd_speedtest: 2 page read speed is 16047 KiB/s mtd_speedtest: Testing erase speed mtd_speedtest: erase speed is 244537 KiB/s mtd_speedtest: Testing 2x multi-block erase speed mtd_speedtest: 2x multi-block erase speed is 252061 KiB/s mtd_speedtest: Testing 4x multi-block erase speed mtd_speedtest: 4x multi-block erase speed is 256000 KiB/s mtd_speedtest: Testing 8x multi-block erase speed mtd_speedtest: 8x multi-block erase speed is 260063 KiB/s mtd_speedtest: Testing 16x multi-block erase speed mtd_speedtest: 16x multi-block erase speed is 260063 KiB/s mtd_speedtest: Testing 32x multi-block erase speed mtd_speedtest: 32x multi-block erase speed is 256000 KiB/s mtd_speedtest: Testing 64x multi-block erase speed mtd_speedtest: 64x multi-block erase speed is 260063 KiB/s mtd_speedtest: finished =================================================‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ You can now achieve almost 16MB/s, better than the dd test. Of course you cannot achieve more than 20MB/s, but you are not that far, and the NAND driver need optimizations. To redo the test: rmmod /lib/modules/4.1.29-fslc+g59b38c3/kernel/drivers/mtd/tests/mtd_speedtest.ko insmod /lib/modules/4.1.29-fslc+g59b38c3/kernel/drivers/mtd/tests/mtd_speedtest.ko dev=2 To check your NAND is in EDO mode 5, you can check your clock tree: /unit_tests/dump-clocks.sh clock          parent   flags    en_cnt pre_cnt      rate [...] gpmi_bch_apb   ---      00000005   0       0       198000000 gpmi_bch       ---      00000005   0       0       198000000 gpmi_io        ---      00000005   0       0        99000000 gpmi_apb       ---      00000005   0       0       198000000‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The IO are clocked now at 99MHz, thus you can read at 49.5MHz (20ns in EDO mode 5 definition).
記事全体を表示
Introduction EVIS (Enhanced Vision Instruction Set) is an API level program language, which is applicable on GC7000XSVX (i.MX8QM) and VIP8000NanoSi (i.MX8MP). The instructions take advantage of the enhanced vision capabilities in the vision-capble hardware, with low-latency. It provides additional functionality for vision image processing beyond the functions provided through the Khronos Group OpenVX API. In the i.MX8QM/i.MX8MP BSP, the OpenCL compiler also support the EVIS instructions. So, it is also an OpenCL VX Extension API. The source file can found in /usr/include/CL/cl_viv_vx_ext.h. Hardware Requirements i.MX8QM (GC7000XSVX) supports EVIS1. i.MX8MP (VIP8000NanoSi) supports EVIS2. Packed Data Types To fully utilize the computing power of the instructions, the extension API support packed data types. For example, in standard OpenCL, a vector char4 will occupy 4x 32-bit registers, while a packed char16 only occupies 128 bits. Thus use packed data types as possible.  The char, unsigned char, short, unsigned short, integer, unsigned integer, float packed data types are supported. They are defined with vxc_ prefix i.e. vxc_char, vxc_uchar, vxc_short, vxc_ushort, vxc_int, vxc_uint, vxc_float, followed by a literal value n that defines the number of elements in the packed data. Supported values of n are 2, 4, 8, and 16 for all the packed data types. Table 1 List of packed data type Type Description vxc_charn A vector of n packed signed character value vxc_ucharn A vector of n packed unsigned character value vxc_shortn A vector of n packed signed short value vxc_ushortn A vector of n packed unsigned short value vxc_intn A vector of n packed signed integer value vxc_uintn A vector of n packed unsigned integer value vxc_floatn A vector of n packed float value OP_CODE Instructions OP_CODE instructions operate on packed data. The enumeration can be found in /usr/include/CL/cl_viv_vx_ext.h. Only EVIS1 supports instructions: VXC_IAdd VXC_MagPhase VXC_BiLinear VXC_SelectAdd VXC_BitReplace VXC_Filter VXC_DP2x16/VXC_DP2x16_b Objects load and store Packed type image data read/write: supported types are packed 8-bit/16bit integer, 16bit float. Image read/write for image1d_t/image1d_array/image2d_t. Offset should be composed by using VXC_5BITOFFSET_XY(x, y). VXC_OP4(img_load, Dest, Image, Coord, Offset, Info) VXC_OP4_NoDest(img_store, Image, Coord, Color, Info) Parameters:         img_load/img_store    Read/write image data.          Dest                            The destination loading the data to.         Image                          The packed image data read from for img_load. The packed image data writing to for img_store.         Coord                          Coordinates to read/write the image data.         Color                           The image data being written to Image for img_store.         Info                              See more info in VXC_MODIFIER(StartBin, EndBin, SourceBin, RoundingMode, Clamp). VXC_MODIFIER(StartBin, EndBin, SourceBin, RoundingMode, Clamp) Parameters:         StartBin/EndBin           The first bin/the last bin for consecutive packed data.         SourceBin                    Not used.          RoundingMode            0: Toward Zero (truncated), 1: Toward Infinity (rounded up), 2: To Nearest Even, 3: not used.         Clamp                          0: no, result is truncated to fit result type (just the lower bits are copied), 1: yes, result is clamped to fit the result type. For example, int2 coord = (int2)(get_global_id(0), get_global_id(1)); vxc_uchar16 r1; VXC_OP4(img_load, r1, in_image, coord, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0)); VXC_Filter This interface applies a specified filter on a 3x3 pixel block. VXC_OP4(filter, Dest, Src0, Src1, Src2, Info) Parameters:         filter                           Filter modes.         Dest                          The filtered image.         Src0                          The first row pixels for 3x3 filter.         Src1                          The second row pixels for 3x3 filter.         Src2                          The third row pixles for 3x3 filter.         Info                            See more info in VXC_MODIFIER_FILTER(StartBin, EndBin, SourceBin, Filter, Clamp). VXC_MODIFIER_FILTER(StartBin, EndBin, SourceBin, Filter, Clamp) Parameters:         StartBin/EndBin        The first bin/the last bin for consecutive packed data.         SourceBin                 Not used.         Filter                          Filter modes are listed in table 2.         Clamp                        0: no, result is truncated to fit result type (just the lower bits are copied), 1: yes, result is clamped to fit the result type. Table 2. List of filter modes: Filter Mode Description VXC_FM_BOX Compute a 3x3 box filter: |1/9, 1/9, 1/9, 1/9, 1/9, 1/9, 1/9, 1/9, 1/9|. VXC_FM_Guassian Compute a 3x3 Gaussian filter: |1/16, 2/16, 1/16, 2/16, 4/16, 2/16, 1/16, 2/16, 1/16|. VXC_FM_SobelX Compute a 3x3 Sobel filter in the x-direction: |-1, 0, 1, -2, 0, 2, -1, 0, 1|. VXC_FM_SobelY Compute a 3x3 Sobel filter in the y-direction: |-1, -2, -1, 0, 0, 0, 1, 2, 1|. VXC_FM_ScharrX Compute a 3x3 Scharr filter in the x-direction: |3, 0, -3, 10, 0, -10, 3, 0, -3|. VXC_FM_ScharrY Compute a 3x3 Scharr filter in the y-direction: |3, 10, 3, 0, 0, 0, -3, -10, -3|. VXC_FM_Max Get the maximum from a 3x3 kernel. VXC_FM_Min Get the minimum from a 3x3 kernel. VXC_FM_Median Get the median from a 3x3 kernel. For example (details in Gaussian Filter examples), int2 coord_in1 = coord + (int2)(-1, -1);\n\ VXC_OP4(img_load, lineA, in_image, coord_in1, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in2 = coord + (int2)(-1, 0);\n\ VXC_OP4(img_load, lineB, in_image, coord_in2, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in3 = coord + (int2)(-1, 1);\n\ VXC_OP4(img_load, lineC, in_image, coord_in3, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int info = VXC_MODIFIER_FILTER(0, 13, 0, VXC_FM_Guassian, 0);\n\ VXC_OP4(filter, out, lineA, lineB, lineC, info); ;\n\ VXC_AbsDiff Calculates a result for the absolute difference between a and b. It works on packed data, so it can compute 16x 8-bit values or 8x 16-bit values. VXC_OP3(abs_diff, Dest, Src0, Src1, Info) Parameters:         abs_diff                 Specify the function of absolute difference.         Dest                      Destination to store the result.         Src0                      The first source to calculate the absolute difference.         Src1                      The second source to calculate the absolute differenece.         Info                       See more info in VXC_MODIFIER(StartBin, EndBin, SourceBin, RoundingMode, Clamp). There are also other interfaces will not be specified here, which can be found in the /usr/include/CL/cl_viv_vx_ext.h, i.e. VXC_IAdd, VXC_IAccSq, VXC_Lerp, VXC_MagPhase, VXC_MulShift, VXC_Clamp, VXC_BiLinear, VXC_SelectAdd, VXC_AtomicAdd, VXC_BitExtract and VXC_BitReplace.  Further Reading: OpenVX Vision Image Extension API Introduction - DP Dot Products
記事全体を表示
The vbs file is a script file in mfgtool. In fsl android lollipop consolidate and later MFGTOOL version, You just need add a new vbs item for new board and have not need to change the ucl2.xml. The below is the example struct. Set wshShell = CreateObject("WScript.shell") wshShell.run "mfgtool2.exe -c ""linux"" -l ""SDCard-Android"" -s ""board=sabresd"" -s ""folder=sabresd"" -s ""soc=6dl"" -s ""mmc=2"" -s ""data_type=-f2fs""" Set wshShell = Nothing Explain for each option: -l: storage type      There three type for android: Nand-Android\eMMC-Android\SDCard-Android -s: extend variable      board: It is used to download uboot and dts in init system.      folder: there are three type: sabresd sabreauto evk                the android image is located in: files/android/%folder%/      soc: Used to define android image name. types: 6q, 6dl, 6sx, 6sl.      mmc: define the storage idex.      data_type: if the type of data partition is f2fs, need define data_type=-f2fs      ldo: if the board is 1.2G, need to define it to -ldo      plus: if the board is 6qp, need too define it to p
記事全体を表示
The i.MX6Q-SDP is used to stream OV5642 parallel camera video encoded as JPEG using the hardware CODEC engine to a Linux client which decodes and displays on the screen.
記事全体を表示
i.MX8X 板级开发包镜像结构 ...................................... 3 2 创建 i.MX8QXP Linux 5.4.24 板级开发包编译环境 ..... 3 2.1 下载板级开发包 ....................................................... 3 2.2 创建yocto编译环境: ................................................. 5 2.3 独立编译 ............................................................... 10 3 i.MX8X SC firmware ................................................. 16 3.1 SC firmware 目录结构 ........................................... 16 3.2 SC firmware 启动流程 ........................................... 18 3.3 SC firmware定制 ................................................... 18 4 i.MX8X ATF .............................................................. 30 5 FSL Uboot 定制 ........................................................ 32 5.1 FDT支持 ............................................................... 33 5.2 DM(driver model)支持 ........................................... 38 5.3 Uboot目录 结构 ..................................................... 52 5.4 Uboot编译 ............................................................. 54 5.5 Uboot初始化流程 .................................................. 55 5.6 uboot 定制 ............................................................ 66 5.7 uboot debug信息 ................................................... 82
記事全体を表示