i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
as we known, mx6sx doesn’t have IPU, if we need to resize, rotation or blending…., we can use pxp module, this part, we talk about rotation for example. We also can use GPU for rotation, but in imx6sx, the number after 6sx in the part number stands for the chip including gpu or not, the number 4 and 3 mean mx6sx has gpu, like MCIMX6X3EVN10AB. and 1,2 and 3 mean mx6sx doesn’t have gpu, like MCIMX6X2EVN10AB for gpu, we know we can use xrander to rotate ,in this part, we focus on pxp rotation the stesp: enable pxp in the kernel:               $ bitbake -c menuconfig linux-imx, then choose Device Drivers ---> DMA Engine support ---> [*] MXC PxP support [*] MXC PxP Client Device 2) download the built image from tmp/deploy/images/imx6sxsabresd 3) boot up the board, then you can find the pxp_v4l2_test.out in the unit test 4) use the command as below to test the rotation: ./pxp_v4l2_test.out -sx 480 -sy 272 -res 352:240 -a 100  -r 90 fb-352x240.yuv BLANK   Sx and sy is resolution for display, -res is resolution for image or video. -r is for rotaion, you can set 0,90,180 and 270 for it. I attach the fb-352x240.yuv for testing
記事全体を表示
i.mx8x启动代码定制文档   目录 1    i.MX8X 板级开发包镜像结构... 2 2    创建 i.MX8QXP Linux 4.14.78_ga 板级开发包编译环境... 2 2.1  下载板级开发包... 2 2.2  创建yocto编译环境: 3 3    i.MX8X SC firmware. 11 3.1  SC firmware 目录结构... 11 3.2  SC firmware 启动流程... 12 3.3  SC firmware定制... 12 4    i.MX8X ATF. 18 5    FSL Uboot 定制... 20 5.1  FDT支持... 21 5.2  DM(driver model)支持... 27 5.3  Uboot目录 结构... 40 5.4  Uboot编译... 42 5.5  Uboot初始化流程... 43 5.6  uboot 定制... 53 5.7  uboot debug信息... 60
記事全体を表示
The LMEM Base address is 0xE0082000u rather than 0xE0002000u.So please apply the patch to FreeRTOS_BSP_1.0.0_iMX6SX to enable the M4 cache, or the cache was not be enabled by default.It may have the big impact to your product performance. diff --git a/platform/devices/MCIMX6X/include/MCIMX6X_M4.h b/platform/devices/MCIMX6X/include/MCIMX6X_M4.h index 31d6eb2..3b9d240 100644 --- a/platform/devices/MCIMX6X/include/MCIMX6X_M4.h +++ b/platform/devices/MCIMX6X/include/MCIMX6X_M4.h @@ -25584,7 +25584,7 @@ typedef struct { /* LMEM - Peripheral instance base addresses */ /** Peripheral LMEM base address */ -#define LMEM_BASE                                (0xE0002000u) +#define LMEM_BASE                                (0xE0082000u) /** Peripheral LMEM base pointer */ #define LMEM                                   ((LMEM_Type *)LMEM_BASE) #define LMEM_BASE_PTR                            (LMEM)
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344462 
記事全体を表示
I have a few questions about the various reference designs for the i.mx6UL. Please see the attachment for specifics.
記事全体を表示
Note: All these gstreamer pipelines have been tested using a i.MX6Q board with a kernel version 3.0.35-2026-geaaf30e. Tools: gst-launch gst-inspect FSL Pipeline Examples: GStreamer i.MX6 Decoding GStreamer i.MX6 Encoding GStreamer Transcoding and Scaling GStreamer i.MX6 Multi-Display GStreamer i.MX6 Multi-Overlay GStreamer i.MX6 Camera Streaming GStreamer RTP Streaming Other plugins: GStreamer ffmpeg GStreamer i.MX6 Image Capture GStreamer i.MX6 Image Display Misc: Testing GStreamer Tracing GStreamer Pipelines GStreamer miscellaneous
記事全体を表示
恩智浦BSP的内核定制 ........................................... 103 6.1 IO管脚配置与Pinctrl驱动 .................................... 103 6.2 新板bringup ........................................................ 118 6.3 更改调试串口: .................................................. 127 6.4 uSDHC设备定制(eMMC flash,SDcard, SDIOcard) 133 6.5 LVDS LCD 驱动定制 .......................................... 142 6.6 GPIO_Key 驱动定制 .......................................... 145 6.7 GPIO_LED 驱动定制 ......................................... 149 6.8 Fuse nvram驱动 ................................................. 152 6.9 SPI与SPI Slave驱动 ........................................... 153 6.10 USB 3.0 TypeC 改成 USB 3.0 TypeA(未验证) ... 160 6.11 汽车级以太网驱动定制 ....................................... 160
記事全体を表示
Qtopia Qt Extended, formerly known as Qtopia until September 30, 2008, is an application platform for Embedded Linux-based mobile computing devices such as personal digital assistants, mobile phones, and web pads. It is being developed by Qt Software, a subsidiary of Nokia. [Source: http://en.wikipedia.org] Qt Software discontinues Qt Extended March 3, 2009 — Oslo, Norway — Qt Software today announced that the product, Qt Extended, will be discontinued as a stand-alone product. Instead, selected features will be migrated into the Qt framework which will result in Qt becoming an even richer, cross-platform application framework. The final release of Qt Extended will be version 4.4.3, which will is planned for release on March 5, 2009. Qt Extended will be maintained for one year from that date. Qt Software will honor all existing support agreements, and for customers who need continued access to support beyond the term of their current agreement, Qt Software is offering the possibility of purchasing supplemental support. [Source: http://www.qtsoftware.com/about/news/qt-software-discontinues-qt-extended] Compiling Qtopia Crosscompiling Qtopia for i.MX processors requires some packages to be installed on host (PC). For more details click on your host PC Linux distribution below: All Boards Qtopia All Boards Qtopia on Ubuntu It's possible to compile Qtopia (version 2 or 4) by selecting Qtopia on package list or simply selecting Qtopia profile on Ltib configuration. Starting Qtopia Touchscreen setup When the system starts up, TSLIB_TSDEVICE environment variable must be set and ts_calibration application must be called to calibrate the touchscreen. $export TSLIB_TSDEVICE=/dev/input/event1 /dev/input/event1 is the usual touchscreen device. Some systems can address the touchscreen device to other names. It's possible to check what's the touchscreen device by typing: $cat /dev/input/<supposed device> After the command above, when touchscreen is pressed, some characters will be showed indicating that the <supposed device> device is the touchscreen device and it's working properly. $ts_calibrate Calibrate screen will appear. After touchscreen calibration, Qtopia can be executed by calling the following script: $/etc/rc.d/init.d/qtopia start Qtopia will be started.
記事全体を表示
1. Enable QtMultimedia 1) In “source/meta-qt5/recipes-qt/qt5/qtmultimedia_git.bb”, add “gstreamer” at the end of “PACKAGECONFIG ??=” .      For example on  L3.14.52  bsp, build  x11  backend: PACKAGECONFIG ??= "${@bb.utils.contains('DISTRO_FEATURES', 'alsa', 'alsa', '', d)} \                    ${@bb.utils.contains('DISTRO_FEATURES', 'pulseaudio', 'pulseaudio', '', d)} \                    gstreamer" 2) Build qtmultimedia:  bitbake qtmultimedia 3) Copy the built package to target file system.      For example : cp  -a ./build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtmultimedia/5.5.0+gitAUTOINC+46a83d5b86-r0/image/usr/   /usr   export  DISPLAY=:0 Video example application located at : /usr/share/qt5/examples/multimedia/video/qmlvideo 2. Enable Qt Logging Info export  QT_LOGGING_RULES=<category>[.type]=ture|false      For example: Turn on all debug logging:      export QT_LOGGING_RULES=*.debug=true Turn on all logging level of all multimedia module:      export QT_LOGGING_RULES=qt.multimedia.*=true 3. Performance Checking Gstreamer: overlaysink fps=51.585      gst-launch-1.0 playbin uri=file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi  video-sink=”overlaysink sync=false” Gstreamer: glimagesink fps=43.850      gst-launch-1.0 playbin uri=file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi video-sink="glimagesink sync=false" Qtmultimedia: fps=45.201      ./qmlvideo  -url file:///H264_AVC_1080p_30fps_27Mbps_mp3.avi -hide-perf Current qt5 multimedia has a special video node for imx6 at     "/src/plugins/videonode/imx6" which uses GPU DirectVIV to accelerate the video rendering. So  the rendering performance is almost same as the glimagesink. For check the free run frame rate, the qt multimedia source need change a little bit to set sink sync as false and calculate the real video rendering rate. Set sync as false: In "/src/plugins/gstreamer/mediaplayer/qgstreamerplayersession.cpp" QGstreamerPlayerSession::playbinNotifySource(): -       g_object_set(G_OBJECT(self->m_videoSink), "sync", !self->m_isLiveSource, NULL); +       g_object_set(G_OBJECT(self->m_videoSink), "sync", false/!self->m_isLiveSource/, NULL); Get fps: In "/src/gsttools/qgstvideorenderersink.cpp" +#include <QTime> +gint g_frame_showed; +QTime g_time; + bool QVideoSurfaceGstDelegate::start(GstCaps *caps) … +   g_frame_showed = 0; +   g_time.restart(); … void QVideoSurfaceGstDelegate::stop() … +   printf(">>>>> fps=%f:\n", (gdouble)g_frame_showed*1000/g_time.elapsed()); … bool  QVideoSurfaceGstDelegate::handleEvent(QMutexLocker *locker) …             const bool rendered = m_activeRenderer->present(m_surface, buffer); +   g_frame_showed++; … Or use the attached patch: qtmultimedia_fps_check.diff 4. Streaming Playing:  HTTP RTP RTSP HTTP: ./qmlvideo -url http://10.192.225.205/streaming/http/H264_HP13_1280x720_29_2850_AAC_LC_44_64_NobodyMTV.mp4 RTSP: ./qmlvideo -url rtsp://10.192.225.205/MPEG4_SP1_720x576_30fps_282_AMRNB_TVC.mp4 RTP: QT mediaplayer use gstreamer playbin as the backend, playbin don’t support rtp address as uri. So QT mediaplayer can’t support RTP playing directly. 5. Audio Recording /usr/share/qt5/examples/multimedia/audiorecorder/audiorecorder This is a widget application, not a QML application. It use QAudioRecorder as its background worker. By default it will use pulsesrc and lamemp3enc to recorder audio as mkv file at user home folder with name of clip_0001.mkv, clip_0002.mkv, and so on. If need special pipeline for recording, example use imxmp3enc to record mp3 files, we need change the function GstElement *QGstreamerCaptureSession::buildEncodeBin in  “src/plugins/gstreamer/mediacapture/qgstreamercapturesession.cpp” as well as QGstreamerMediaContainerControl(QObject *parent) in “src/plugins/gstreamer/mediacapture/qgstreamermediacontainercontrol.cpp” 6. Camera Widgets Application: “/usr/share/qt5/examples/multimediawidgets/camera/camera” QML Application: “/usr/share/qt5/examples/multimedia/declarative-camera/declarative-camera” Qt Multimedia has some bugs on L3.14.52 with QCamera for recording. Use the attached patches: 0001-gstreamer-fix-camerabin-not-negotiated-error.patch 0001-QCamera-can-t-set-recording-container-format-video-a.patch 0002-QtCamera-change-default-encoding-parameters-to-use-N.patch If you want use overlaysink as the preview sink, then use following patch: 0003-use-overlaysink-as-the-preview-sink.patch Both applications need to set environment variable QT_GSTREAMER_CAMERABIN_VIDEOSRC to use imxv4l2src If camera device is other than /dev/video0, set environment variable QT_GSTREAMER_CAMERABIN_VIDEOSRC_DEVICE to the right camera device, such as "/dev/video1" ,  for example: export QT_GSTREAMER_CAMERABIN_VIDEOSRC=imxv4l2src export DISPLAY=:0 export QT_GSTREAMER_CAMERABIN_VIDEOSRC_DEVICE="/dev/video1" By default, the “post-preview” feature of camerabin was disabled by the patches provided, since the imxv4l2src can’t work with “post-preview” internal “videoconvert” element. To enable “post-preview”  feature, one need uncomment following line //g_object_set(G_OBJECT(m_camerabin), POST_PREVIEWS_PROPERTY, TRUE, NULL); in “/qtmultimedia/src/plugins/gstreamer/camerabin/camerabinsession.cpp”, Function: CameraBinSession::CameraBinSession(GstElementFactory *sourceFactory, QObject *parent) And Change “videoconvert” to “imxvideoconvert_g2d” or “imxvideoconvert_ipu” or “imxvideoconvert_pxp” in line : csp = gst_element_factory_make ("videoconvert", "preview-vconv"); of  file “/gstreamer1.0-plugins-bad/gst-libs/gst/basecamerabinsrc/gstcamerabinpreview.c”  function: GstCameraBinPreviewPipelineData *gst_camerabin_create_preview_pipeline (GstElement * element,   GstElement * filter)
記事全体を表示
This doc show: on i.MX6Q SabreSD board, configure ov5640 sensor(parallel or MIPI) output 5MP(2592x1944) RAW(Bayer) data at 15fps,and i.MX6Q IPU capture RAW RGB data, and i.MX6Q GPU debayer RAW data then display image. HW: i.MX6Q-SabreSD board, ov5640 sensor. SW: Linux 4.14.98_2.0.0 BSP, and patches in this doc. Configure at camera sensor side A Bayer filter is a color filter array (CFA) for arranging RGB color filters on a square grid of photosensors. The filter pattern is 50% green, 25% red and 25% blue, hence is also called BGGR, RGBG ,GRGB, or RGGB. The ov5640 has an image array capable of operating at up to 15 fps in 5 megapixel (2592x1944) resolution. OV5640 support output formats: RAW(Bayer), RGB565/555/444,CCIR656, YUV422/420, YCbCr422, and compression. To make ov5640 output 5MP RAW data at 15fps, check my patch imx6_ov5640_dvp_mipi_raw_capture_driver-4.14.98_2.0.0.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP kernel code: Parallel interface ov5640, use ov5640_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640.c. This register setting is come from ov5640 software application note and data sheet. MIPI interface ov5640, use ov5640_mipi_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640_mipi.c. This register setting is combine setting of original code (remove ISP register setting), plus PLL register setting for MIPI interface, plus some data format register setting. Configure at i.MX6Q side The i.MX6Q IPU camera port(CSI-2 module) support data format include Raw(Bayer), RGB, YUV 4:4:4, YUV 4:2:2 and grayscale, up to 16 bits per value. Below is camera data routing for i.MX6Q:    Below is i.MX6Q IPU block daigram: The CSI-2 of IPU which is responsible for synchronizing and packing the video (or generic data) and sending it to other blocks. The video data received by CSI-2, could be sent to three other blocks: SMFC, VDI, IC. For RAW (Bayer) data capture, should go through path like this: CSI-2-->SMFC-->IDMAC-->DDR memory It means RAW data is received as generic data, see IPU_PIX_FMT_GENERIC in my patch, and IPU cannot process this kind data, it is just received to DDR memory. For MIPI interface camera, need note is i.MX6 side MIPI D-PHY clock must be calibrated to the actual clock range of the camera sensor’s D-PHY clock and the calibrated value must be equal to or greater than the camera sensor clock, detail see  AN5305. Take MIPI ov5640 as example: Pixel clock = 2592x1944x15fpsx(1/2 cycle/pixel)x1.35 blank interval = 51MHZ MIPI data rate = 51MHZ x 16 bit = 816Mb/s so 816/2/2*2 is 408MHZ is i.MX6 side D-PHY clock. Here due to one bayer pixel is 8bit, and i.MX6 MIPI data bus is 16 bit, so above use 1/2 cycle/pixel. And check ov5640_mipi_raw_setting[], you will got the sensor side D-PHY clock is about 672/2 = 336MHZ. And check AN5305, register MIPI_CSI2_PHY_TST_CTRL1 of i.MX6 need set as 0xC, but here i still keep it as default BSP value 0x14.   3.Capture test code I changed unit test mxc_v4l2_capture.c to capture the RAW data and save it to file. Check my patch imx6_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff which apply on i.MX  Linux 4.14.98_2.0.0 BSP unit test code. Note the usage is: ./cap.out -c 1 -i 1 -fr 15 -m 6 -iw 2592 -ih 1944 -ow 2592 -oh 1944 -f BA81 -d /dev/video1 savefile.dmp parameter -i 1 means use CSI to MEM mode /dev/video1 is MIPI ov5640, /dev/video0 is parallel ov5640   4.Display RAW data The RAW data cannot be displayed directly, debayer process is needed to get complete red, green, blue color for each pixel. The debayer process if run on CPU, will cost much CPU time. To save CPU time, debayer could done by GPU. The method is, captured RAW data upload to GPU as texture , then GPU will do the debayer, then full color of each pixel will be got, then display it. To upload RAW camera data to GPU with zero memory copy, i will use i.MX6Q GPU extension GL_VIV_direct_texture. It create a texture with direct access support. API glTexDirectVIVMap,  which support mapping a user space memory or a physical address into the texture surface. The API glTexDirectVIVMap need logic and physical address of data buffer, so i will allocate data buffer from /dev/mxc_ipu, it is dma-buffer also get logic/physical address of buffer, then queue it as USERPTR to ipu v4l2 capture driver, after dequeue got RAW camera data, pass it to GPU for debayer. GPU side, I will use OpenGL shader code from "Efficient, High-Quality Bayer Demosaic Filtering on GPUs". Check my patch imx6-5640-debayer-testcode-gpusdk-5.2.0.diff which apply on i.MX GPU SDK 5.2.0 code. Note, here i only do is debayer, no extra process.   Known issue One thing is ov5640 output 5MP at 15fps, compare with output 5MP at 5fps, there are more noise of camera data at 15fps case. My debug found is , this noise seems come from ov5640 itself.   Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX6DQRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX6QDLSOLOX&appType=license c>https://github.com/NXPmicro/gtec-demo-framework d>https://www.nxp.com/docs/en/application-note/AN5305.pdf e>ov5640 data sheet f>ov5640 software application note g>Efficient, High-Quality Bayer Demosaic Filtering on GPUs https://www.semanticscholar.org/paper/Efficient%2C-High-Quality-Bayer-Demosaic-Filtering-on-McGuire/088a2f47b7ab99c78d41623bdfaf4acdb02358fb
記事全体を表示
The i.MX 6 Linux L3.10.17_1.0.3 Patch release is now available. Patch Release Notes can be found on  www.freescale.com . This release supports the following i.MX 6 reference boards: ·        i.MX 6 Quad/DualLite/Solo SABRE SD ·        i.MX 6 Quad/DualLite/Solo SABRE Auto ·        i.MX 6 SoloLite This patch release is based on the i.MX 6 Linux L3.10.17_1.0.0 GA release. Release changes the following components: ·        Kernel branch: imx_v2013.04_3.10.17_1.0.0_ga ·        U-Boot branch: imx_3.10.17_1.0.0_ga ·        Graphics: gpu-viv-bin-mx6q, 3.10.17_1.0.3 ·        Graphics: gpu-viv-g2d, 3.10.17_1.0.3 ·        Graphics: Xorg-driver, 3.10.17_1.0.3 More detailed patch description: Please consult the release notes document.
記事全体を表示
i.MX6 Series - Crystal Drive Level guidance; includes calculator.  
記事全体を表示
The i.MX Android L5.0.0_1.0.0 GA release is now available on http://www.freescale.com . ·        Files available # Name Description 1 android_L5.0.0_1.0.0-ga_doc.tar.gz i.MX6 Android L5.0.0_1.0.0 BSP Documentation 2 android_L5.0.0_1.0.0-ga_core_source.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite and i.MX6SX Android L5.0.0_1.0.0 BSP, Source Code for BSP and Codecs. 3 android_L5.0.0_1.0.0-ga_images_6qsabreauto.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.0.0_1.0.0 BSP Binary Demo Files for the SABRE for Automotive Infotainment. 4 android_L5.0.0_1.0.0-ga_images_6qsabresd.tar.gz i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.0.0_1.0.0 BSP Binary Demo Files for the SABRE Platform and SABRE Board for Smart Devices. 5 android_L5.0.0_1.0.0-ga_images_6slevk.tar.gz i.MX 6Sololite Android L5.0.0_1.0.0 BSP Binary Demo Files for the SoloLite evaluation kit. 6 android_L5.0.0_1.0.0-ga_images_6sx.tar.gz i.MX 6SoloX Android L5.0.0_1.0.0 BSP Binary Demo Files. 7 fsl_aacp_dec_L5.0.0_1.0.0-ga.tar.gz AAC Plus Codec for i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite and i.MX 6SX Android L5.0.0_1.0.0 BSP. 8 android_L5.0.0_1.0.0-ga_tools.tar.gz i.MX 6Family Manufacturing Toolkit for L5.0.0_1.0.0 ·        Supported Hardware SoC/Boards: o  i.MX 6Quad SABRE-SD board and platform o  i.MX 6DualLite SABRE-SD board and platform o  i.MX 6Quad SABRE-AI board and platform o  i.MX 6DualLite SABRE-AI board and platform o  i.MX6SoloLite EVK platform o  i.MX6SoloX SABRE-SD board o  i.MX6SoloX SABRE-AI board and platform ·        Change List Compared to the L5.0.0_1.0.0-alpha release, this release has the following major changes: o  Applies Cortex-A9 Errata 845369, which will cause performance drop in memcpy. o  Prefetches offset change for PL310 to improve the memcpy performance. o    Disables shell as Android CTS requirement. o  Switches the default NAND chip from MT29F8G08ABACA to MT29F64G08AFAAA. o    Includes several fixes to pass CTS android-cts-5.0_r2. ·        Features For features please consult the release notes. ·        Known issues For known issues and more details please consult the release notes.
記事全体を表示
Dumping the pipeline elements into a image file # On target, run the pipeline $ export GST_DEBUG_DUMP_DOT_DIR=<folder where dot files are created> $ gst-launch playbin2 uri=file://${avi} $ # Move the .dot files to a host machine (scp, etc) # On Host dot <dot file> -Tpng -o out.png # dot command is part the the graphviz package Querying which elements are being used on a gst-launch command GST_DEBUG=GST_ELEMENT_FACTORY:3 gst-launch playbin2 uri=file://`pwd`/<media file> Interrupting a gst-launch process running in the background kill -INT $PID # where $PID is the process ID Using only SW codecs # Backup and remove $ find /usr/lib/gstreamer-0.10 -name "libmfw*" | grep -v sink | xargs tar cvf /libmfw_gst.tar $ find /usr/lib/gstreamer-0.10 -name "libmfw*" | grep -v sink | xargs rm # Run your pipeline. This time SW codecs are used $ gst-launch playbin2 uri=file://`pwd`/media_file # To 'install' FSL plugins again, just untar the file $ cd / && tar xvf libmfw_gst.tar && cd - # then run your pipeline. This time HW codecs are used $ gst-launch playbin2 uri=file://`pwd`/media_file
記事全体を表示
If someone wants to use the OpenGL ES 2.0 extension "GL_OES_vertex_array_object", the macro "GL_GLEXT_PROTOTYPES" must be defined in his program first. Then he can get the extension program location by calling the API eglGetProcAddress.  Here is an example to use this extension. #define GL_GLEXT_PROTOTYPES PFNGLGENVERTEXARRAYSOESPROC glGenVertexArraysOESv; PFNGLBINDVERTEXARRAYOESPROC glBindVertexArrayOESv; PFNGLDELETEVERTEXARRAYSOESPROC glDeleteVertexArraysOESv; glGenVertexArraysOESv = (PFNGLGENVERTEXARRAYSOESPROC)eglGetProcAddress ( "glGenVertexArraysOES" ); glBindVertexArrayOESv = (PFNGLBINDVERTEXARRAYOESPROC)eglGetProcAddress ( "glBindVertexArrayOES" ); glDeleteVertexArraysOESv = (PFNGLDELETEVERTEXARRAYSOESPROC)eglGetProcAddress ( "glDeleteVertexArraysOES" ); After these steps, the new alias glGenVertexArraysOESv, glBindVertexArrayOESv, glDeleteVertexArraysOESv can be use to call the VAO operation function in OpenGL ES 2.0 extensions.
記事全体を表示
Video, bad performance gst-launch filesrc location=test.mp4 typefind=true ! aiurdemux ! vpudec ! mfw_v4lsink Video, better performance gst-launch filesrc location=sample.mp4 typefind=true ! aiurdemux ! queue max-size-time=0 ! vpudec ! mfw_v4lsink # typefind=true allows to 'type find' the source file before negotiating # max-size-time=0 indicates to ignore possible blocking issues # In case of ASF files gst-launch filesrc location=sample.asf typefind=true ! aiurdemux ! queue max-size-time=0 ! mfw_wmvdecoder ! mfw_v4lsink Audio gst-launch filesrc location=sample.mp3  typefind=true ! beepdec ! audioconvert  ! 'audio/x-raw-int, channels=2' ! alsasink Audio with visualization gst-launch filesrc location=sample.mp3 typefind=true ! beepdec ! tee name=t ! queue ! audioconvert  ! 'audio/x-raw-int, channels=2' ! alsasink t. ! queue ! audioconvert ! goom ! autovideoconvert ! autovideosink Video/Audio long version gst-launch filesrc location=sample.avi typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink # queue properties, max-size-buffers=0 and max-size-time=0, allows a smoother playback; type 'gst-inspect queue' for more info VA short version gplay sample.avi VA short version gst-launch playbin2 uri=file://<full path to sample file>
記事全体を表示
The i.MX Android N7.1.2_2.0.0 GA release is now available on IMX_SW page.   Files available: # Name Description 1 android_N7.1.2_2.0.0_docs.tar.gz i.MX Android N7.1.2_2.0.0 BSP Documentation 2 android_N7.1.2_2.0.0_source.tar.gz Source Code of Android N7.1.2_2.0.0 BSP (4.1 kernel) for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite, i.MX6SX and i.MX7D 3 android_N7.1.2_2.0.0_image_6dqpsabreauto.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite 4 android_N7.1.2_2.0.0_image_6dqpsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite. 5 android_N7.1.2_2.0.0_image_6slevk.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - i.MX 6Sololite evaluation kit. 6 android_N7.1.2_2.0.0_image_6sxsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 6SoloX 7 android_N7.1.2_2.0.0_image_6sxsabreauto.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX 8 android_N7.1.2_2.0.0_image_7dsabresd.tar.gz Binary Demo Files of Android N7.1.2_2.0.0 BSP - SABRE Board based on i.MX 7Dual 9 fsl_aacp_dec.tar.gz AAC Plus Codec for N7.1.2_2.0.0 10 android_N7.1.2_2.0.0_tools.tar.gz Manufacturing Toolkit and VivanteVTK for N7.1.2_2.0.0   Supported Hardware SoC/Boards: i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform i.MX 6SoloLite EVK platform i.MX 6SoloX SABRE-SD board and platforms i.MX 6SoloX SABRE-AI board and platforms i.MX 7Dual SABRE-SD board and platform   Changes: Compared to the N7.1.1_1.0.0 release, this release has the following major changes: Upgraded the Android code base from android-7.1.1_r13 to android-7.1.2_r9. Upgraded U-Boot from v2015.04 to v2017.03. Upgraded the kernel from v4.1.15 to v4.9.17. Upgraded the GPU driver from 6.2.0.p2 to 6.2.2.p1. Upgraded the Wi-Fi BCMDHD release version to 1.141.100.6. Refine the Gralloc and HWC HAL. Enable the GPT partition to replace the MBR partition.   Feature: For features please consult the release notes.   Known issues For known issues and more details please consult the Release Notes.
記事全体を表示
We are very proud to announce that Element14's SabreLite i.MX6Q board is now officially supported by Adeneo Embedded's i.MX6 WEC7 BSP. As a consequence, our customers are able to use the SabreLite board from Element14 as well as the one from Boundary Devices. Follow this link for Adeneo Embedded's i.MX6 WEC7 BSP Follow this link for Element 14's SabreLite board Ce document a été généré à partir de la discussion suivante : Element14's SabreLite board officially supported by Adeneo Embedded's i.MX6 WEC7 BSP
記事全体を表示
The getevent function shows kernel events like press button events, touchscreen events, sensor events (like accelerometers or magnetometers). bash-3.2# getevent -h Usage: getevent [-t] [-n] [-s switchmask] [-S] [-v [mask]] [-p] [-q] [-c count] [-r] [device]       -t: show time stamps       -n: don't print newlines       -s: print switch states for given bits       -S: print all switch states       -v: verbosity mask (errs=1, dev=2, name=4, info=8, vers=16, pos. events=32)       -p: show possible events (errs, dev, name, pos. events)       -q: quiet (clear verbosity mask)       -c: print given number of events then exit       -r: print rate events are received Bellow an example of all events on some board bash-3.2# getevent -p add device 1: /dev/input/event2   name:    "mxc_ts"   events:       SYN (0000): 0000  0001  0003       KEY (0001): 014a       ABS (0003): 0000  value 0, min 0, max 0, fuzz 0 flat 0                         0001  value 0, min 0, max 0, fuzz 0 flat 0                         0018  value 0, min 0, max 0, fuzz 0 flat 0 could not get driver version for /dev/input/mouse0, Not a typewriter add device 2: /dev/input/event1   name:    "mxc_power_key"   events:     SYN (0000): 0000  0001     KEY (0001): 003e add device 3: /dev/input/event0   name:    "mxckpd"   events:     SYN (0000): 0000  0001     KEY (0001): 0002  0003  0004  0005  003b  003c  003d  003e                       0066  0067  0069  006a  006c  008b  009e  0161 could not get driver version for /dev/input/mice, Not a typewriter For example, some touchscreen event. Any touchscreen press-up or press-down will return a vector of values related with the event (please, see include/linux/input.h for detail) bash-3.2# getevent /dev/input/event2 0003 0000 0000020e 0003 0001 0000014a 0003 0018 00000037 0001 014a 00000001 0000 0000 00000000 0003 0000 00000209 0003 0001 00000147
記事全体を表示
Step 1: Build r13.4.1         make         /* Store images file for MFGTool use */         make dist    /* Get ota_1.zip, and target_files_1.zip at out/dist, store them in a dedicated directory, for example .../release-1 */ Step 2: Modify any files in source code base; Step 3: make dist    /* Get ota_2.zip, and target_files_2.zip at out/dist, store them in a dedicated directory, for example .../release-2 */ Step 4: MFGTool flash release-1 images; Step 5: cp ota_2.zip to SD; Step 6: start board, then execute following commands under serial terminal;         cp /sdcard/ota_2.zip /cache/ota_2.zip         mkdir /cache/recovery         echo --update_package=/cache/ota_2.zip > /cache/recovery/command         sync         reboot recovery         Then you can see the upgrade successful. Step 7: MFGTool flash release-1 images; Step 8: ./build/tools/releasetools/ota_from_target_files -i .../release-1/target_files_1.zip .../release-2/target_files_2.zip ./diff_from_1_to_2.zip Step 9: cp diff_from_1_to_2.zip to SD; Step10: start board, then execute following commands under serial terminal;         cp /sdcard/diff_from_1_to_2.zip /cache/diff.zip         mkdir /cache/recovery         echo --update_package=/cache/diff.zip > /cache/recovery/command         sync         reboot recovery
記事全体を表示