i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
This is a simple document for recording some known-how and tips for building up the Windows 10 IoT development environment for i.MX platform. It can only be used as a complement for official document in BSP package (Guide/Release Note/etc.). Applicable for: Windows 10 IoT, i.MX BSP v1.4.1 (date to Nov/2023) Please refer to the PDF attached.
View full article
Information about the transition from the NXP Demo Experience to GoPoint for i.MX Application Processors.
View full article
BSP: L6.1.36 Some customer need use adb under usb ffs. The adb in Yocto can greatly improves development efficiency. This is a demo for enabling adb on Yocto.   Yocto local.conf IMAGE_INSTALL:append = "android-tools android-tools-adbd" PREFERRED_PROVIDER_android-tools-conf = "android-tools-conf-configfs"   Test script for launching adbd modprobe g_ffs idVendor=0x1fc9 idProduct=0x0146 iSerialNumber="ZhimingLiu" mkdir -p /dev/usb-ffs/adb mount -t functionfs adb /dev/usb-ffs/adb -o uid=2000,gid=2000 adbd &   Test on Windows: PS C:\Users\Administrator\Desktop\platform-tools> .\adb.exe devices List of devices attached ZhimingLiu device PS C:\Users\Administrator\Desktop\platform-tools> .\adb.exe shell sh-5.2# uname -a Linux imx8mp-lpddr4-evk 6.1.36+g04b05c5527e9 #1 SMP PREEMPT Fri Nov 24 04:46:22 UTC 2023 aarch64 GNU/Linux sh-5.2# ls config ffs t.sh test2.sh sh-5.2# cd / sh-5.2# ls bin dev home lost+found mnt proc run srv tmp usr boot etc lib media opt root sbin sys unit_tests var sh-5.2#
View full article
Platform: Demo images, i.MX8MPlus EVK   Some customer need test ffs gadget function on i.MX8MPlus EVK. Here is demo for ffs test, please connect EVK and Ubuntu PC before test.   Test script: #!/bin/sh # Setup the device (configfs) modprobe libcomposite mkdir -p config mount none config -t configfs cd config/usb_gadget/ mkdir g1 cd g1 echo 0x1fc9 >idVendor echo 0x0146 >idProduct mkdir strings/0x409 echo 12345 >strings/0x409/serialnumber echo "Signal 11" >strings/0x409/manufacturer echo "Test" >strings/0x409/product mkdir configs/c.1 mkdir configs/c.1/strings/0x409 echo "Config1" >configs/c.1/strings/0x409/configuration # Setup functionfs mkdir functions/ffs.usb0 ln -s functions/ffs.usb0 configs/c.1 cd ../../../ mkdir -p ffs mount usb0 ffs -t functionfs cd ffs ffs-test 64 & # from the Linux kernel, with mods! sleep 3 cd .. # Enable the USB device echo 38100000.usb > config/usb_gadget/g1/UDC   EVK log root@imx8mpevk:~# ./test2.sh [ 17.859597] file system registered ffs-test: dbg: ep0: writing descriptors (in v2 format) ffs-test: dbg: ep0: writing strings ffs-test: dbg: ep1: starting ffs-test: dbg: ep2: starting ffs-test: dbg: ep1: starts ffs-test: dbg: ep0: starts ffs-test: dbg: ep2: starts Event BIND Event ENABLE Ubuntu PC log: lzm@lzm-GL552VW:~$ lsusb -D /dev/bus/usb/001/008 Device: ID 1fc9:0146 NXP Semiconductors Test Device Descriptor: bLength 18 bDescriptorType 1 bcdUSB 2.10 bDeviceClass 0 bDeviceSubClass 0 bDeviceProtocol 0 bMaxPacketSize0 64 idVendor 0x1fc9 NXP Semiconductors idProduct 0x0146 bcdDevice 6.01 iManufacturer 1 Signal 11 iProduct 2 Test iSerial 3 12345 bNumConfigurations 1 Configuration Descriptor: bLength 9 bDescriptorType 2 wTotalLength 0x0020 bNumInterfaces 1 bConfigurationValue 1 iConfiguration 4 Config1 bmAttributes 0x80 (Bus Powered) MaxPower 2mA Interface Descriptor: bLength 9 bDescriptorType 4 bInterfaceNumber 0 bAlternateSetting 0 bNumEndpoints 2 bInterfaceClass 255 Vendor Specific Class bInterfaceSubClass 0 bInterfaceProtocol 0 iInterface 5 Source/Sink Endpoint Descriptor: bLength 7 bDescriptorType 5 bEndpointAddress 0x81 EP 1 IN bmAttributes 2 Transfer Type Bulk Synch Type None Usage Type Data wMaxPacketSize 0x0200 1x 512 bytes bInterval 0 Endpoint Descriptor: bLength 7 bDescriptorType 5 bEndpointAddress 0x01 EP 1 OUT bmAttributes 2 Transfer Type Bulk Synch Type None Usage Type Data wMaxPacketSize 0x0200 1x 512 bytes bInterval 1 Binary Object Store Descriptor: bLength 5 bDescriptorType 15 wTotalLength 0x0016 bNumDeviceCaps 2 USB 2.0 Extension Device Capability: bLength 7 bDescriptorType 16 bDevCapabilityType 2 bmAttributes 0x0000010e BESL Link Power Management (LPM) Supported BESL value 256 us SuperSpeed USB Device Capability: bLength 10 bDescriptorType 16 bDevCapabilityType 3 bmAttributes 0x00 wSpeedsSupported 0x000f Device can operate at Low Speed (1Mbps) Device can operate at Full Speed (12Mbps) Device can operate at High Speed (480Mbps) Device can operate at SuperSpeed (5Gbps) bFunctionalitySupport 1 Lowest fully-functional device speed is Full Speed (12Mbps) bU1DevExitLat 0 micro seconds bU2DevExitLat 0 micro seconds Device Status: 0x0001 Self Powered  
View full article
Usually, device tree source files are not a signal pure dts file. It could include dtsi, dts or C code heads .h files. Need C compiler finish the pre-compile to a pure dts file first. It is integrated inside the like Linux build system(Makefile, etc.). This document shows the original way to compile device tree. This document will show compile device tree under windows.    
View full article
How to use UART4 on iMX8M from Linux User Space   The UART4 on iMX8MM-EVK and iMX8MN-EVK are thinking of debugging the M core which is not usable on Linux user space by default on pre-compiled images.   To use the UART4 on Linux user space you have to do the next modifications on the device tree and atf to assign that peripheral to Linux User Space     https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c     iMX8MN-EVK   imx8mn_bl31_setup.c   https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mn/imx8mn_bl31_setup.c   /* Master domain assignment */ RDC_MDAn(RDC_MDA_M7, DID1), /* peripherals domain permission */ - RDC_PDAPn(RDC_PDAP_UART4, D1R | D1W), + RDC_PDAPn(RDC_PDAP_UART4, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART2, D0R | D0W), RDC_PDAPn(RDC_PDAP_RDC, D0R | D0W | D1R),       Device tree configurations for iMX8MN-EVK   iMX8MN-EVK.dtsi   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mn-evk.dtsi   &uart3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart3>; assigned-clocks = <&clk IMX8MN_CLK_UART3>; assigned-clock-parents = <&clk IMX8MN_SYS_PLL1_80M>; uart-has-rtscts; status = "okay"; }; + &uart4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_uart4>; + assigned-clocks = <&clk IMX8MN_CLK_UART4>; + assigned-clock-parents = <&clk IMX8MN_SYS_PLL1_80M>; + status = "okay"; + }; ********************** pinctrl_uart3: uart3grp { fsl,pins = < MX8MN_IOMUXC_ECSPI1_SCLK_UART3_DCE_RX 0x140 MX8MN_IOMUXC_ECSPI1_MOSI_UART3_DCE_TX 0x140 MX8MN_IOMUXC_ECSPI1_SS0_UART3_DCE_RTS_B 0x140 MX8MN_IOMUXC_ECSPI1_MISO_UART3_DCE_CTS_B 0x140 >; }; + pinctrl_uart4: uart4grp { + fsl,pins = < + MX8MN_IOMUXC_UART4_RXD_UART4_DCE_RX 0x140 + MX8MN_IOMUXC_UART4_TXD_UART4_DCE_TX 0x140 + >; + };   iMX8MM-EVK   https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c   imx8mm_bl31_setup.c   /* Master domain assignment */ RDC_MDAn(RDC_MDA_M7, DID1), /* peripherals domain permission */ - RDC_PDAPn(RDC_PDAP_UART4, D1R | D1W), + RDC_PDAPn(RDC_PDAP_UART4, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART2, D0R | D0W), RDC_PDAPn(RDC_PDAP_RDC, D0R | D0W | D1R),   Device tree configurations for iMX8MM-EVK   iMX8MM-EVK.dtsi   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi   &uart3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart3>; assigned-clocks = <&clk IMX8MM_CLK_UART3>; assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>; uart-has-rtscts; status = "okay"; }; + &uart4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_uart4>; + assigned-clocks = <&clk IMX8MM_CLK_UART4>; + assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>; + status = "okay"; + }; ********************** pinctrl_uart3: uart3grp { fsl,pins = < MX8MM_IOMUXC_ECSPI1_SCLK_UART3_DCE_RX 0x140 MX8MM_IOMUXC_ECSPI1_MOSI_UART3_DCE_TX 0x140 MX8MM_IOMUXC_ECSPI1_SS0_UART3_DCE_RTS_B 0x140 MX8MM_IOMUXC_ECSPI1_MISO_UART3_DCE_CTS_B 0x140 >; }; + pinctrl_uart4: uart4grp { + fsl,pins = < + MX8MM_IOMUXC_UART4_RXD_UART4_DCE_RX 0x140 + MX8MM_IOMUXC_UART4_TXD_UART4_DCE_TX 0x140 + >; + };   iMX8MP-EVK   https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mp/imx8mp_bl31_setup.c   imx8mp_bl31_setup.c   RDC_MDAn(RDC_MDA_M7, DID1), RDC_MDAn(RDC_MDA_LCDIF, DID2), RDC_MDAn(RDC_MDA_LCDIF2, DID2), RDC_MDAn(RDC_MDA_HDMI_TX, DID2), /* peripherals domain permission */ + RDC_PDAPn(RDC_PDAP_UART4, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART2, D0R | D0W), RDC_PDAPn(RDC_PDAP_WDOG1, D0R | D0W), RDC_PDAPn(RDC_PDAP_RDC, D0R | D0W | D1R),   Device tree configurations for iMX8MP-EVK   iMX8MP-EVK.dts   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts   &uart3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart3>; assigned-clocks = <&clk IMX8MP_CLK_UART3>; assigned-clock-parents = <&clk IMX8MP_SYS_PLL1_80M>; fsl,uart-has-rtscts; status = "okay"; }; + &uart4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_uart4>; + assigned-clocks = <&clk IMX8MP_CLK_UART4>; + assigned-clock-parents = <&clk IMX8MP_SYS_PLL1_80M>; + status = "okay"; + }; ************************************ pinctrl_uart3: uart3grp { fsl,pins = < MX8MP_IOMUXC_ECSPI1_SCLK__UART3_DCE_RX 0x140 MX8MP_IOMUXC_ECSPI1_MOSI__UART3_DCE_TX 0x140 MX8MP_IOMUXC_ECSPI1_SS0__UART3_DCE_RTS 0x140 MX8MP_IOMUXC_ECSPI1_MISO__UART3_DCE_CTS 0x140 >; }; + pinctrl_uart4: uart4grp { + fsl,pins = < + MX8MP_IOMUXC_UART4_RXD__UART4_DCE_RX 0x140 + MX8MP_IOMUXC_UART4_TXD__UART4_DCE_TX 0x140 + >; + };     After compiling the image with the changes previously shown, we obtained this result:      
View full article
Board : i.MX93 EVK BSP: imx L6.1.1-1.0.0 Gui guider: 1.6.1   We have a GUI software tool called GUI Guider. It is a user-friendly graphical user interface development tool from NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library. The GUI demo can run on the i.MX93EVK board. (https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER)   This document will show you an example how the buttons(gpio) on the EVK to interacting with the GUI. Basically, customer could use the same method to use the gpio pins to control everything.   On the i.MX93 EVK board, there are two buttons BTN1 and BTN2. They are connected to GPIO IO23 and GPIO IO24. Below is the schematic.    Buttons on the board.      SW1005 on the board   In the EVK's device tree file, need to change the pinmux for the two buttons like this: pinctrl_spdif: spdifgrp { fsl,pins = < // MX93_PAD_GPIO_IO22__SPDIF_IN 0x31e // MX93_PAD_GPIO_IO23__SPDIF_OUT 0x31e MX93_PAD_GPIO_IO23__GPIO2_IO23 0x31e MX93_PAD_GPIO_IO24__GPIO2_IO24 0x31e >; note: all the pins are defined in imx93-pinfunc.h.   For getting the input value of the buttons in user's space, I use the sysfs gpio. Build the imx-image-multimedia image first and then select the GPIO_SYSFS in kernel's menuconfig.   $ DISTRO=fsl-imx-xwayland MACHINE=imx93evk source imx-setup-release.sh -b build-xwayland $ bitbake imx-image-multimedia   After the build completed, go to the kernel's menuconfig to select the GPIO sysfs. $ bitbake linux-imx -c menuconfig [*] General setup-> Configure standard kernel features (expert users) [*] Device Drivers->GPIO Support-> /sys/class/gpio/... (sysfs interface)   Build the whole image again by "$ bitbake imx-image-multimedia".   Using the UUU to program the image to the EMMC on the EVK board. uuu -b emmc_all imx-image-multimedia-imx93evk.rootfs.wic.zst   Connect the LVDS to the board. Use the corresponding dtb to boot the board. In u-boot, set the dtb file. => setenv fdtfile imx93-11x11-evk-boe-wxga-lvds-panel.dtb => saveenv   Then restart the board. After the board boot up, it will look like below.     You need to calibrate the LVDS touch screen before it can normally use. Please use this command: $ weston-touch-calibrator LVDS-1     Now, build the GUI guider example. I use the Air Conditioner example. Download the GUI guider from the gui-guider web page: https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER   Follow the steps from the below web page to build the i.MX BSP and the gui example code. https://docs.nxp.com/bundle/GUIGUIDERUG-1.6.1/page/topics/yocto.html   After the gui-guider build completed, use the 'scp' command to transfer the gui_guider executable file to the board. Execute the command on your host PC like this: $ scp bld-imx93evk/tmp/work/armv8a-poky-linux/gui-guider/1.6.0-r0/image/usr/bin/gui_guider root@<Your Board IP address>:/ Note: You could use a router to connect your board and your host PC. They are on the same network so could use the 'scp' command to transfer the file to your board.   On your board, type the following commands to execute the gui. $ chmod 755 gui_guider $ ./gui_guider &   Then the GUI is running like this:   Now, let me explain how to find out the gpio number. Type the following command to show the mapping addresses of gpio. root@imx93evk:/# cat /sys/kernel/debug/gpio gpiochip3: GPIOs 0-31, parent: platform/47400080.gpio, 47400080.gpio: gpiochip0: GPIOs 32-63, parent: platform/43810080.gpio, 43810080.gpio: gpiochip1: GPIOs 64-95, parent: platform/43820080.gpio, 43820080.gpio: gpio-64 ( |cd ) in hi IRQ ACTIVE LOW gpio-71 ( |regulator-usdhc2 ) out lo gpiochip2: GPIOs 96-127, parent: platform/43830080.gpio, 43830080.gpio: gpiochip6: GPIOs 472-477, parent: i2c/0-001a, wm8962, can sleep: gpiochip5: GPIOs 478-487, parent: platform/adp5585-gpio.1.auto, adp5585-gpio, can sleep: gpio-479 ( |regulator-audio-pwr ) out hi gpio-483 ( |regulator-can2-stby ) out hi ACTIVE LOW gpio-486 ( |enable ) out hi gpiochip4: GPIOs 488-511, parent: i2c/1-0022, 1-0022, can sleep: gpio-492 ( |Headphone detection ) in lo IRQ gpio-501 ( |? ) out hi gpio-502 ( |regulator-vdd-12v ) out hi gpio-505 ( |reset ) out lo gpio-507 ( |? ) out hi gpio-508 ( |reset ) out lo ACTIVE LOW   The gpio pins of two buttons are GPIO2_IO23 and GPIO2_IO24. They are belongs to gpio2. In the imx93.dtsi, the gpio2's address is "gpio2: gpio@43810080". So, base on the information output from "/sys/kernel/debug/gpio", the gpio2 is mapping to "gpiochip0: GPIOs 32-63". So, the GPIO2_IO23 is 32+23=55, and the GPIO2_IO24 is 32+24=56.   To verify the gpio number is correct or not. We could do the following test. root@imx93evk:/# echo 55 > /sys/class/gpio/export root@imx93evk:/# echo in > /sys/class/gpio/gpio55/direction root@imx93evk:/# echo 56 > /sys/class/gpio/export root@imx93evk:/# echo in > /sys/class/gpio/gpio56/direction   Then, run these two commands to check the values. root@imx93evk:/# cat /sys/class/gpio/gpio55/value root@imx93evk:/# cat /sys/class/gpio/gpio55/value   When the button is not pressed, the value is 1. When press the button, the value is 0.  We could add the same in the GUI's custom.c. Open the GUI Guider software and add the code in the custom.c. /********************* * INCLUDES *********************/ #include <stdio.h> #include <stdlib.h> #include <unistd.h> #include <errno.h> #include <fcntl.h> #include "lvgl.h" #include "custom.h" #include "ui_Aircon.h" #include "guider_customer_fonts.h" /********************** * STATIC VARIABLES **********************/ int fdbtn1,fdbtn2,fdgpio; int btn1_pressed; int btn2_pressed; char btn1_value, btn2_value; void custom_func(void) { fdbtn1 = open("/sys/class/gpio/gpio55/value", O_RDWR); fdbtn2 = open("/sys/class/gpio/gpio56/value", O_RDWR); read(fdbtn1, &btn1_value, 1); read(fdbtn2, &btn2_value, 1); if(btn1_value=='0' && btn1_pressed) { btn1_pressed=0; ui_aircon_update_temp(0, kAIRCON_TempUp); } if(btn1_value=='1') btn1_pressed=1; if(btn2_value=='0' && btn2_pressed) { btn2_pressed=0; ui_aircon_update_temp(0, kAIRCON_TempDown); } if(btn2_value=='1') btn2_pressed=1; close(fdbtn1); close(fdbtn2); } void custom_init(lv_ui *ui) { fdbtn1 = open("/sys/class/gpio/gpio55/value", O_WRONLY); if (fdbtn1 == -1) { fdgpio = open("/sys/class/gpio/export", O_WRONLY); write(fdgpio,"55",3); write(fdgpio,"56",3); close(fdgpio); fdgpio = open("/sys/class/gpio/gpio55/direction", O_WRONLY); write(fdgpio,"in",3); close(fdgpio); fdgpio = open("/sys/class/gpio/gpio56/direction", O_WRONLY); write(fdgpio,"in",3); close(fdgpio); } else close(fdbtn1); ... ... ... ...   Add the custom_func() in the custom.h. #ifndef __CUSTOM_H_ #define __CUSTOM_H_ #ifdef __cplusplus extern "C" { #endif #include "gui_guider.h" void custom_init(lv_ui *ui); + void custom_func(void);   Also, need to add the custom function() into the dead loop in main.c.   To modify the code, bld-imx93evk$ vim tmp/work/armv8a-poky-linux/gui-guider/1.6.0-r0/gui-guider-1.6.0/ports/linux/main.c   while(1) { + custom_func(); // <--- Add the custom function here. /* Periodically call the lv_task handler. * It could be done in a timer interrupt or an OS task too.*/ time_till_next = lv_wayland_timer_handler(); #if LV_USE_VIDEO video_play(&guider_ui); #endif /* Run until the last window closes */ if (!lv_wayland_window_is_open(NULL)) { break; }   Re-build the code after modified. bld-imx93evk$ bitbake gui-guider -c compile -f   Build the whole image again. bld-imx93evk$ bitbake gui-guider Then use the 'scp' command to transfer the new gui-guider file to the board.   Finally, you can use the buttons on the EVK board to set the temperature up and down.                          
View full article
    In i.MX93 EVK, it use RGMII in ethernet connection. Some customer use RMII connection. This article describe RMII HW design and SW config.  It listed four cases in attached.  
View full article
test ov5640 with 480p, raw10 via ISP on imx8mp
View full article
The configuration of DDR is very important. NXP provides a tool for configuring DDR for users of i.MX series products. Here are the details steps for it. Hope can do help for someone. 1\ The DDR part startup and initialization sequence of MX8MM:   The MX 8M series DDR tools include: DDR Register Programming Aid --->Configurate custom DDR initialization MSCALE DDR Tool(DDR Stress Test Tool) --->Test DDR initialization And DDR interface ---> Generate custom DDR initialization code for the u-boot SPL DDR RPA(RPA) is an Excel spreadsheet tool used to develop DDR initialization for specific DDR configurations (DDR device type, density, etc.) of users. RPA generates DDR initialization (in a separate Excel worksheet tab). Detailed explanations and introductions will be provided here. DDR stress testing tool is a software tool based Windows that initializes PHY and generates DDRC configuration Uboot source code to verify whether DDR initialization can be used for u-boot and OS startup. DDR stress testing script, this format is specifically used for DDR stress detection. First, copy the content from this worksheet tab, and then paste it into a text file, naming the document with the ". ds" file extension. Select this file when performing DDR stress testing. 2\i.MX8M series DDR tool work flow           Above is the DDR Tool flow for the i.MX8MM: DDR RPA Tool: Configure DDR parameters to generate DDR Stress Test script ". ds". DDR Sress Test Tool: Test DDR initialization and DDR interface, generate DDR initialization code for the u-boot SPL DDR driver. For the newest DDR RPA version as below:   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443 In the above link, you can download the corresponding DDR configuration tools for i.MX8MM using different DDRs.   3\How to use this script to configure DDR parameters (1)Obtain the required DRAM data sheet from the DRAM supplier firstly. The DDR parameter configuration content will be completed in the "Register Configuration" worksheet tab.   (2)"Register Configuration",Update the device information table to include DRAM information and system usage. DDR RPA tool:  Register Configuration---->Device Information table   It should be filled out based on the datasheet and relevant hardware circuit design of the selected DDR chip. Specific users can refer to the manual for selecting DDR chips and their own hardware design. Take the i.MX 8M Mini LPDDR4 EVK board as example, it selects the Micron MT53D512M32D2DS-053 WT:D, we can go the Micron website to download the DDR’s datasheet and we can see bellow:   Density per channel (Gb)= Device density (Per Channel Per CS)=8Gb Number of ROW Addresses=R[15:0]=16 Number of Channels=2 (2 Channels i.MX8MM DDR is 32bit) Number of COLUMN Addresses=C[9:0]=10 Total DRAM density(Gb) Automatic calculation:Density per channel (Gb) * Number of Channels * Number of Chip Selects used  =8Gb * 2 * 1=16Gb=2GB Bus Width=M32=32bit: i.MX8MM DDR support 32bit Cycle Freq (MHz)=1500MHZ: The DDR controller clock of the i.MX8MM is set to 1500MHZ. The information filled in is shown in the table below:   (3)Browse through various shaded cells in the spreadsheet to update using data from the DRAM table (pay special attention to the "Legend" table to determine the meaning of different shaded cells; in many cases, these cells may not need to be updated). On the parameter filling page, we can also see the following table, with different colors indicating the need to modify and maintain the original parameters and the affected parameter information. On the register configuration tab, basically only the orange part of the color represents the bit segments that usually need to be updated, and the rest do not need to be modified or configured.   (4)Go to the BoardDataBusConfig tab, fill in the i.MX8MM data bus mapping to the memory device correctly. DDR RPA tool: BoardDataBusConfig ---->Configurate data bus bit   Users should pay special attention to ensuring that this worksheet is configured correctly, otherwise the LPDDR4 system may not function properly. The memory controller of i.MX8MM allows for BYTE internal swapping. For layout convenience, BYTE internal swapping is usually performed, so the BoardDataBusConfig column needs to be configured according to the actual schematic design. We can see the tab in the BoardDataBusConfig, user fill the i.MX8MM data bit connection to associated LPDDR4, the filling in of data bits here should be consistent with the order of our hardware design wiring, which means that if there are swapped data bits, the corresponding relationship must be filled in. Take the LPDDR4 connection to the i.MX8MM as example, the highest 8 bits on the channel B of the LPDDR4   connect to the side of DRAM_DQ00~DRAM_DQ07 of CPU, and the lowest 8 bits on the channel B of the LPDDR4 DRAM_DQ08~DRAM_DQ15 of CPU side,the lowest 8 bits on the channel A of the LPDDR4 connect to the DRAM_DQ16~DRAM_DQ23 of CPU side,the highest 8 bits on the channel A of the LPDDR4 connect to the DRAM_DQ24~DRAM_DQ31 of the CPU side. The i.MX8MM memory controller allows for BYTE internal swapping. For layout convenience, BYTE internal swapping is usually performed, and this needs to be filled in according to the actual wiring in the data bus.       (5)Generate the “.ds” file DDR RPA tool: DDR stress test file ----> “.ds”   Copy the content of the DDR stress test file into a text file and name it a. ds file. For subsequent DDR stress testing purposes.   4\Do the DDR Stress test and Generate the DDR Code The following is the workflow of the DDR tool for the MX8MM series:   Preparation Board: i.MX 8M Mini LPDDR4 EVK Software download: mscale_ddr_tool_v3.31_setup.exe(Install it) PC:Window10 PC file .ds file Hardware requirements for the board: (Please note that these interfaces are necessary when using our stress testing tools) Serial download mode USB OTG port Debug UART port 4.1 Hardware connection   SW1101set 1010xxxxxx go to Serial Download mode, connect the USB-OTG and UART to PC, USB OTG is used for serial download of binary files: UART is used to communicate with users. Note: It is recommended to connect the USB OTG directly to the host PC, rather than through the USB Hub. When power on the board,we can see HID-compliant vendor-defined device and USB Input Device:   UART port are COM3 and COM4:   4.2 Open MSCALEDDR_Tool. exe in administrator mode for DDR parameter calibration and pressure testing:   Select serial port Select Search in Debug UART and you can read that the other two serial ports COM3 and COM4 have been tried. Click on the Connect button. It should be noted that we have two serial ports, one for the A core and the other for the M core. Here, COM4 must be selected to load the script normally. COM4 is used for the A core. Select Target Select the MX8M-mini,speed of CPU chosse1200MHZ, DDR LPDDR4 size 2GB. Select .ds file, Load DDR Script: Copy the generate mx8mm_micron_lpddr4_2gb_2d_1500m_200m_50m_32bit_1cs_RPAv22.ds to the path of the DDR TOOL, then press the Download button. After the download is successful, there will be a print message indicating the successful download and the startup information of the board. We can see the CPU parameters and DDR configuration.   Pres Calibration: This step mainly involves executing the DDR initialization and calibration process. If there is a failure, it is necessary to analyze the DDR problem based on the printed information. If there is no problem, the following interface will appear.   (5) If there are no problems after calibration, perform a pressure test. Only perform this operation when the calibration is passed. Run the test on all frequency set points. If the DDR pressure test passes, you can see that the test has passed successfully. If there is an error, you should search for the problem with the DDR based on the error message.   (6) Generate u-boot timing After the stress test is successfully completed, clicking the Gen Code button will generate a file lpddr4_timing. c, and then the lpddr4_timing. C file can be copied to the u boot directory.     5\ Modifying and configuring DDR frequencies that are not supported by default         The above test is for the frequency point 1500MHZ that is supported by default in our tool. RPA provides default DRAM PLL settings (DRAM frequency) based on the default settings supported in u-boot. If the customer is not using the default supported frequency, in addition to updating the new frequency in RPA, the new DRAM PLL settings should also be manually updated in the u boot SPL. (1) Firstly, in the RPA script, "Clock Cycle Freq (MHz)" is set to the frequency we need (2) Then search for 'memory set 0x30360054' in the RPA DDR stress test file worksheet tab, with a default setting of 1500MHZ.   We can see the DRAM PLL register and bit settings:   For special frequencies, we have a calculation formula here: DDR_freq = [(24MHz x pll_main_div)/(pll_pre_div x 2^pll_post_div)] x 2 1500 = [(24 x 250) / (8 x 2^1)] x 2 Bellow are some special examples of the required configurations for various frequencies:     Finishing configuration, create a. ds test DDR script in the RPA script to specify the frequency of this configuration. (3)After creating a DDR script for the DDR stress testing tool, run the calibration and perform the DDR pressure test. Generating the lpddr4_timing.c, modify the required DDR rate parameters Manually. (4)Modify the DRAM PLL,DRAM_freq = DRAM_PLL x 2 in SPL,u-boot SPL DDR driver can will not automatically change DRAM PLL based on generated code. Therefore, users will need to manually modify the dram_pll_init  for the required DDR PLL parameter.
View full article
One of the most popular use cases for embedded systems are projects destinated to show information and interact with users. These views are called GUI or Graphic User Interface which are designed to be intuitive, attractive, consistent, and clear. There are many tools that we can use to achieve great GUIs, mostly implemented for platforms such as Web, Android, and iOS. Here, we will need to introduce the concept of framework, basically, it is a set of tools and rules that provides a minimal structure to start with your development. Frameworks usually comes with configuration files, code snippets, files and folders organization helping us to save time and effort. Also, it is important to review the concept of SDK or Software Development Kit which is a set of tools that allows to build software for specific platforms. Usually supplies debugging tools, documentation, libraries, API’s, emulators, and sample code. Flutter is an open-source UI software development kit by Google that help us to create applications with great GUIs on different platforms from a single codebase. Depends on the reference, you can find Flutter defined as a framework or SDK and both are correct, however, an SDK could be a best definition thanks to Flutter supplies a wide and complete package to create an application in which framework is also included. This article is aimed at those that are in a prototyping stage looking for a different tool to develop projects. Also, this article pretends to be a theoretical introduction explaining the most important concepts. However, is a good practice to learn more about reviewing the official documentation from Flutter. (Flutter documentation | Flutter) Here is the structure used throughout this article: What is Flutter? Flutter details Platforms Programming language Official documentation Flutter for embedded systems What is Flutter? Flutter was officially released by Google in December 2018 with a main aim, to give developers a tool to create applications natively compiled for mobile (Android, iOS), web and desktop (Windows, Linux) from a single codebase. It means that as a developer, Flutter will create a structure with minimal code, configuration files, build files for each operating system, manifests, etc. in which we will add our custom code and finally build this code for our preferred OS. For example, we can create an application to review fruit and vegetable information and compile for Android and iOS with the same code. A basic Flutter development process based on my experience looks like the following diagram: Flutter has the following key features: Cross-platform development. Flutter allows the developer to create applications for different platforms using a single codebase. It means that you will not need to recreate the application for each platform you want to support.   Hot-reload. This feature allows the developer to see changes in real time without restarting the whole application, this results in time savings for your project.   High Performance Flutter apps achieve high performance due to the app code is compiled to native ARM code. With this tool no interpreters are involved.   UI Widgets Flutter supplies a set of widgets (UI components such as boxes, inputs text, buttons, etc.) predefined by UI systems guidelines Material on Android and Cupertino for iOS. Source: Material 3 Design Kit | Figma Community Source: Design - Apple Developer   Great community support. This feature could be subjective but, it is useful when we are developing our project find solutions to known issues or report new ones. Because of Flutter is an open source and is widely implemented in the industry this tool owns a big community, with events, forums, and documentation. Flutter Details Supported Platforms With Flutter you can create applications for: Android iOS Linux Debian Linux Ubuntu macOS web Chrome, Firefox, Safari, Edge Windows Supported deployment platforms | Flutter Programming Language Flutter use Dart, a programming language is an open-source language supported by Google optimized to use on the creation of user interfaces. Dart key features: Statically typed. This feature helps catching errors making the code robust ensuring that the variable’s value always match with the declared variable’s type. Null safety. All variables on Dart are non-nullable which means that every variable must have a non-null value avoiding errors at execution time. This feature also, make the code robust and secure. Async/Await. Dart is client-optimized which means that this language was specially created to ensure the best performance as a client application. Async/Await is a feature part of this optimization making easier to manage network requests and other asynchronous operations. Object oriented. Dart is an object-oriented language with classes and mixin. This is especially useful to use on Flutter with the usage of widgets. Compiler support of Just-In-Time (JIT) and Ahead-of-Time (AOT) JIT provides the support that enables the Hot Reload Flutter feature that I mentioned before. It is a complex mechanism, but Dart “detects” changes in your code and execute only these changes avoiding recompiling all the code. AOT compiler produces efficient ARM code improving start up time and performance. Official documentation Flutter has a rich community and documentation that goes from UI guidelines to an Architectural Overview. You can find the official documentation at the following links: Flutter Official Documentation: Flutter documentation | Flutter Flutter Community: Community (flutter.dev) Dart Official Documentation: Dart documentation | Dart Flutter for embedded systems So far, we know all the excellent features and platforms that Flutter can support. But, what about the embedded systems? On the official documentation we can find that Flutter may be used for embedded systems but in fact there is no an official supported platform. This SDK has been supported by their community, specially there is one repository on GitHub supported by Sony that provides documentation and Yocto recipes to support Flutter on embedded Linux. To understand the reason to differentiate between Flutter for Linux Desktop with official support and to create a specific Flutter support for embedded Linux is important to describe the basics of Flutter architecture. Based on the Flutter documentation the system is designed using layers that can be illustrated as follows:   Source: Flutter architectural overview | Flutter We can see as a top level “Framework” which is a high-level layer that includes widgets, tools and libraries that are in contact with developers. Below “Framework,” the layer “Engine” is responsible of drawing the widgets specified in the previous layer and provides the connection between high-level and low-level code. This layer is mostly written in C++ for this reason Flutter can achieve high performance running applications. Specifically for graphics rendering Flutter implements Impeller for iOS and Skia for the rest of platforms. The bottom layer is “Embedder” which is specific for each target and operating system this layer allows Flutter application to run as a native app providing the access to interact with different services managed by the operating systems such as input, rendering surfaces and accessibility. This layer for Linux Desktop uses GTK/GDK and X11 as backend that is highly dependent of unnecessary libraries and expensive for embedded systems which have constrained resources for computation and memory. The work around founded by Sony’s Flutter for Embedded Linux repository is to change this backend using a widely implemented backend for embedded systems Wayland. The following image illustrates the difference between Flutter for Linux Desktop and Flutter for Embedded Linux.   Source: What's the difference between Linux desktop and Embedded Linux · sony/flutter-embedded-linux Wiki · GitHub   Source: What's the difference between Linux desktop and Embedded Linux · sony/flutter-embedded-linux Wiki · GitHub Here is the link to the mentioned repository: GitHub - sony/flutter-elinux: Flutter tools for embedded Linux (eLinux) Finally, I would like to encourage you to read the official Flutter documentation and consider this tool as a great option compared to widely used tools on embedded devices such as Qt or Chromium. Also, please have a look to a great article written by Payam Zahedi delving into the implementation of Flutter for Embedded Linux measuring performance and giving conclusions about the usage of Flutter in embedded systems. (Flutter on Embedded Devices. Learn how to run Flutter on embedded… | by Payam Zahedi | Snapp Embedded | Medium).    
View full article
The default BSP is compiled based on the Yocto project, which is a streamlined production-level Linux BSP. However, for users who are accustomed to the Ubuntu environment, especially ROS users, the operation of Yocto will be relatively complicated. This article will introduce how to make an Ubuntu BSP for iMX8QM and demonstrate how to use ROS.   A complete Ubuntu BSP includes u-boot, Linux kernel and Ubuntu rootfs. We will use u-boot and Linux kernel in Yocto BSP official 6.1V BSP, and rootfs will still use ubuntu-base-18.04.4-base-arm64. The compilation method comes from the NXP forum. First download ubuntu-base-18.04.4-base-arm64.tar.gz from the link above, and then unzip it. $ mkdir ~/ubuntu-rootfs $ sudo tar vxf ubuntu-base-18.04.4-base-arm64.tar.gz -C ubuntu-rootfs Copy the script file and create ch-mount.sh. $ sudo chmod a+x ./ch-mount.sh The download above is a basic Ubuntu-base file system, which is missing many commonly used tools and requires us to install it. For this purpose, install the qemu-user-static software on your computer to simulate the arm64 operating environment. $ sudo apt install qemu-user-static Mount the Ubuntu-base file system and then operate directly in the arm64 environment. $ sudo ./ch-mount.sh -m ubuntu-rootfs/ Add a DNS server, such as 8.8.8.8, or other available DNS server IP. # echo nameserver 8.8.8.8 > /etc/resolv.conf Install relevant software, of course you can also add other software. # apt install language-pack-en-base sudo ssh net-tools \ network-manager iputils-ping rsyslog \ bash-completion htop resolvconf dialog \ vim nano v4l-utils alsa-utils git gcc \ less resolvconf autoconf autopoint libtool \ bison flex gtk-doc-tools glib-2.0 \ libglib2.0-dev libpango1.0-dev libatk1.0-dev kmod pciutils -y  Create a user and set a password, here the user name is ubuntu # useradd -s '/bin/bash' -m -G adm,sudo ubuntu # passwd ubuntu # passwd root # echo 'apalis-imx8' > /etc/hostname At this point basic Ubuntu has been configured. # exit $ sudo ./ch-mount.sh -u ubuntu-rootfs/  After the installation is complete, use the ubuntu user to log in to the debugging serial port, and the password is ubuntu. When starting for the first time after installation, it will wait for a long time due to initialization, and then enter the configuration interface including region, user settings, etc. Turn on Ethernet and set DNS server IP.  ubuntu@mx8QM:~$ sudo ifconfig eth0 up ubuntu@mx8QM:~$ sudo dhclient eth0 ubuntu@mx8QM:~$ sudo vi /etc/resolv.conf Start Weston: ubuntu@mx8QM:~$ export XDG_RUNTIME_DIR=/run/user/1000 ubuntu@mx8QM:~$ sudo -E weston --tty=1 & ubuntu@mx8QM:~$ weston-flower ROS test You can install ROS programs very conveniently in Ubuntu system. Please refer to the instructions below for details http://wiki.ros.org/melodic/Installation/Ubuntu http://wiki.ros.org/ROS/Tutorials ubuntu@mx8QM:~$ sudo apt install lsb-core ubuntu@mx8QM:~$ sudo sh -c 'echo "deb http://packages.ros.org/ros/ubuntu $(lsb_release -sc) main" > /etc/apt/sources.list.d/ros-latest.list' ubuntu@mx8QM:~$ sudo apt-key adv --keyserver 'hkp://keyserver.ubuntu.com:80' --recv-key C1CF6E31E6BADE8868B172B4F42ED6FBAB17C654 ubuntu@mx8QM:~$ sudo apt update ubuntu@mx8QM:~$ sudo apt install ros-melodic-desktop  Run the following commands on three SSH terminals to simulate communication between ROS nodes. ubuntu@mx8QM:~$ source /opt/ros/melodic/setup.sh ubuntu@mx8QM:~$ roscore ubuntu@mx8QM:~$ source /opt/ros/melodic/setup.sh ubuntu@mx8QM:~$ rosrun roscpp_tutorials talker ubuntu@mx8QM:~$ source /opt/ros/melodic/setup.sh ubuntu@mx8QM:~$ rosrun roscpp_tutorials listener Due to driver limitations, iMX8 does not support Xorg, so ROS's default graphical interface tools such as rqt cannot be used directly.        
View full article
1. MediaPlayer Architecture     MediaPlayer is the server, MediaPlayerService and MediaPlayerService :: Client is the client. MediaPlayerService realize the IMediaPlayerService, the main function is to create the right player through the url sent by MediaPlayer::setDataSource MediaPlayerService :: Client realize the IMediaPlayer, the main function is to call the player created by MediaPlayerService to do those specific start, stop, resume, pause…      Entering NuplayerDriver means entering Android MultiMedia Framework.   2. NuPlayer   The playback video is mainly completed through Nuplayer. The figure below includes parser, decoder and render.   NuPlayer::Source is the parser module. Its interface looks like a combination of MediaExtractor and MediaSource NuPlayer::Decoder connects to CCodec for decoding. CCodec has a state pattern and pass MediaBuffers around with messages. NuPlayer::Render is responsible for rendering audio and also controls when to post video buffers back to NativeWindow for A/V sync. 3. Decoding Framework 3.1 Framework of i.MX8MP, i.MX8MQ and i.MX8MM   Decoding Process between the framework, vendor decoder component and kernel as follows on i.MX8MP, i.MX8MQ and i.MX8MM.   3.2 Framework of i.MX8QM   Decoding Process between the framework, vendor decoder component and kernel as follows on i.MX8QM. stream on: start to decode/encode stream off: stop decoding/encoding qbuf:  Queue the v4l2buffer filled in the decoder into the buffer queue created in the vpu driver so that the VPU can obtain it for decoding. dqbuf: When the VPU decoding is completed, the buffer will be dequeueed so that the decoder/codec can continue to be used. 4. Decode Video and Display Process 4.1 i.MX8MM and i.MX8MP   For i.MX8MP and i.MX8MM, G2D is used to composite layers, and the buffer transmission is completed between Decoder and SurfaceFlinger through the BufferQueue mechanism. The process as follows:  BufferQueue: As the producer of BufferQueue, decoder provides the decoded buffer, and SurfaceFlinger, as the consumer of BufferQueue, composite the decoded video layer.  Display: Use G2D to composite Android layer and video layer on i.MX8MP. SurfaceFlinger will hand over all layers to Display HAL, and then composite them into the framebuffer by G2D. 4.2 i.MX8MQ   For i.MX8MQ, GPU3D is used to composite Android UI, DCSS is used to composite overlay and android UI. And the buffer transmission is completed between Decoder and SurfaceFlinger through the BufferQueue mechanism. The processing is as follows: BufferQueue: Decoder provides the decoded buffer as producer. SurfaceFlinger as the cosumer of BufferQueue.  Display: Using GPU3D to composite Android UI layers. And video layer will be submitted to DCSS (Display Controller) through Display HAL. DCSS:  Responsible for combining video overlay and Android UI for display. GLESRenderEngine: SurfaceFlinger calls the opengl interface through GLESRenderEngine to complete rendering composite. 4.3 i.MX8QM For i.MX8QM, GPU3D or DPU are used to composite. And the buffer transmission is completed between Decoder Filter Component and SurfaceFlinger through the BufferQueue mechanism. The processing as follows: Decoder Filter:  Because GPU3D cannot directly composite TILED type layers, it needs to be converted into Linear through Decoder Filter first, and then handed over to SurfaceFlinger. BufferQueue:  Decoder Fillter will receive the outputbuffer from Decoder. And Filter will be as producer of BufferQueue to provide the buffer. SurfaceFlinger will be as consumer of BufferQueue to consume the buffers. GLESRenderEngine: SurfaceFlinger calls the opengl interface through GLESRenderEngine to complete rendering composite. Note:  On i.MX8QM,  Not all situations are composited using the GPU3D. Please refer to the table below.   4.4 DRM Widevine (Secure Decoder)   Now we have enabled DRM Widevine on i.MX8MP/i.MX8MQ/i.MX8QM so that secure video can be played.  For i.MX8MP, Use OEMCrypto trusted application to decrypt the encrypted stream. And Use RDC/CSU to protected hardware for secure pipeline. The framework is as follows:   For i.MX8MQ, Use OEMCrypto trusted application to decrypt the encrypted stream. And Use RDC/CSU to protected hardware for secure pipeline. The framework is as follows:     OEMCrypto: It is a library as tipc client to send the encrypted data to Trusty OS. OEMCrypto Trusted Application: Used to decrypt the protected data into secure memory and send it to Media Framewrok. Secure Framebuffer: It is allocated from secure heap through libdmabufheap. Secure heap: Used to allocate secure memory.  Resources in domain2 can read and write secure memory, but cannot write normal memory. Resources in domain0 can write to secure memory, but cannot read normal memory. When playing secure video, VPU, GPU2D, and lcdif will be in domain2. Or they are in domain0. Resource Domain Controller (RDC): It provides support for the isolation of destination memory mapped locations such as peripherals and memory to a single core, a bus master, or set of cores and bus masters.  CSU Central Security Unit (CSU) : 1. Peripheral Access Policy - the appropriate bus master privilege and identity are required to access each peripheral. 2. Masters Privilege Policy - the CSU overrides the bus master privilege signals (secure/non-secure).  Configure the VPU so that it can only be accessed by the secure world. For i.MX8QM, also use OEMCrypto trusted application to decrypt the encrypted stream. But related hardware and memory are protected through the secure partition created by SCU. The framework is as follows: OEMCrypto: It is a library as tipc client to send the encrypted data to Trusty OS. OEMCrypto Trusted Application: Used to decrypt the protected data into secure memory and send it to Media Framewrok. Secure Framebuffer: It is allocated from secure heap through libdmabufheap. Secure heap: Used to allocate secure memory.  Only Secure partition can access secure memory. Frimware Loader: It is a trusted application in Trusty OS, It is responsible for loading the encrypted firmware into the specified memory. Secure Partition: Secure partitions are created using SCU and all hardware that needs to be protected are moved to secure partitions to isolate it from non-secure partitions. 5. Encoding Process 5.1 Encoding Process on i.MX8MP BufferQueue:  MediaFramework will create Surface and create BufferQueue, SurfaceFlinger will serve as the producer to provide the composite layers, and the Encoder component will encode it as the consumer of the BufferQueue. MPEG4Writer:  Responsible for writing the VPU-encoded data to the output file. 5.2 Encoding Process on i.MX8QM and i.MX8MM   BufferQueue:  MediaFramework will create Surface and create BufferQueue, SurfaceFlinger will serve as the producer to provide the composite layer, and the Encoder Filter component will be as the consumer of the BufferQueue. MPEG4Writer:  Responsible for writing the VPU-encoded data to the output file. 6. Buffer transfer and management 6.1 Transfer and release process of Input Buffer Input Buffer allocation: It is allocated in CCodecBufferChannel, and it is used to allocate inputbuffer and recycled. InputManager: Before the queue buffer into the decoder, it will be registered with the InputManager. When the VPU is finished using it, the InputManager will be notified to release it. Use of InputBuffer:  After the buffer is queued into the decoder, the input buffer information will be copied to v4l2buffer so that the VPU can use it. Note: For DRM Secure decoder, the VPU will only use the paddr of inputbuffer. 6.2 Transfer and release process of Output Buffer     Output Buffer allocation:  When use Surface for output, It is allocated through BufferQueueAllocator that is created in CCodecBufferChannel. It is used to allocate outputBuffer.  Management: When use Surface, OutputBuffer is managed through the BufferQueue mechanism. When the VPU filled the outputBuffer with data that can be displayed, it will notify the Consumer to acquire the buffer. Use of OutputBuffer: In the decoder, the output buffer information will be copied to v4l2buffer so that the VPU can use it. Note:  For situations where OutputSurface is not used, GrallocAllocator is used by default instead of BufferQueueAllocator. 6.3 Buffer Management of Encoder   For screen recording situations, the Encoder's buffer transfer is also managed through the BufferQueue mechanism. After SurfaceFlinger is producer to fill the GraphicBuffer of BufferQueue, the encoder is as consumer to encode the composited data.  
View full article
this article write down the steps when help customer bring dual camera under single mipi csi with NXP switch NX3DV642, just for a reference, connect OV5640 + os08a20 with mipi csi0 via ISP, as default, mipi csi0 just has one port with one camera, this document improve how to enable os08a20 with second port under mipi csi0, refer to the document and patch as attachment, for how to enable ov5640 with ISP, pls refer to my another document
View full article
Customer is asking high-capacity external storage(for example >64GB) support on i.MX BSP, ext4 is ok for HC storage, but it can’t be supported by Windows. Pls find NFTS and exFAT support status on Linux BSP below: Updated test result on L5.4.70.2.3.0 and L6.1.22: L5.4.70.2.3.0 1.You can enable ntfs support in kernel config as below,  ntfs can be mounted normally, but you can only modify existing file content in disk, you can’t create/delete/rename file on disk. > File systems > DOS/FAT/NT Filesystems   Log: root@imx8mpevk:~# mount -t ntfs /dev/sda1 /mnt/fat/ [  662.732869] ntfs: volume version 3.1. root@imx8mpevk:~# cp ntfs-3g /mnt/fat/ cp: cannot create regular file '/mnt/fat/ntfs-3g': Permission denied root@imx8mpevk:~# ls /mnt/fat/ 111.png  Image_org  System Volume Information  gpuinfo.sh root@imx8mpevk:~# vi /mnt/fat/gpuinfo.sh root@imx8mpevk:~# umount /mnt/fat/ root@imx8mpevk:~# ntfs file system can be accessed via ntfs-3g in user space as below //build: wget https://tuxera.com/opensource/ntfs-3g_ntfsprogs-2017.3.23.tgz tar zxvf ntfs-3g_ntfsprogs-2017.3.23.tgz cd ntfs-3g_ntfsprogs-2017.3.23/ source ../../sdk/environment-setup-aarch64-poky-linux   ./configure --host=aarch64-linux --build=aarch64-poky-linux --disable-shared --enable-static   make   ls /src/ntfs-3g   //put it into rootfs cp ntfs-3g /bin   //test log: root@imx8mpevk:/# [ 1058.724471] usb 1-1: USB disconnect, device number 4 [ 1062.058613] usb 1-1: new high-speed USB device number 5 using xhci-hcd [ 1062.214029] usb-storage 1-1:1.0: USB Mass Storage device detected [ 1062.220986] scsi host0: usb-storage 1-1:1.0 [ 1063.235871] scsi 0:0:0:0: Direct-Access     VendorCo ProductCode      2.00 PQ: 0 ANSI: 4 [ 1063.246185] sd 0:0:0:0: [sda] 15728640 512-byte logical blocks: (8.05 GB/7.50 GiB) [ 1063.254023] sd 0:0:0:0: [sda] Write Protect is off [ 1063.259164] sd 0:0:0:0: [sda] No Caching mode page found [ 1063.264540] sd 0:0:0:0: [sda] Assuming drive cache: write through [ 1063.296946]  sda: sda1 [ 1063.300860] sd 0:0:0:0: [sda] Attached SCSI removable disk   root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh root@imx8mpevk:/# cp /unit_tests/memtool /mnt/fat/ root@imx8mpevk:/# umount /mnt/fat/ root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh  memtool root@imx8mpevk:/#   3.exFAT is not supported on this BSP..   L6.1.22(you can check it on L5.15 and above, should be the same) You can enable ntfs support in kernel config as below, full features can be supported. > File systems > DOS/FAT/EXFAT/NT Filesystems   Pls use ‘-t ntfs3’ during mounting, otherwise it will be mounted as ‘read-only’ Log: root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information' root@imx8ulpevk:~# root@imx8ulpevk:~# cp gpuinfo.sh /mnt/fat/ root@imx8ulpevk:~# umount /mnt/fat/ root@imx8ulpevk:~# root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information'   gpuinfo.sh root@imx8ulpevk:~#   exFAT has been supported in L6.1.22. > File systems > DOS/FAT/EXFAT/NT Filesystems   /dev/sda1 on /run/media/sda1 type exfat (rw,relatime,fmask=0022,dmask=0022,iocharset=utf8,errors=remount-ro) root@imx8ulpevk:~# ls /run/media/sda1 'Certificate of Completion.pdf'             carlife.MP4 Image_org                                  example.tflite L5.4.70_2.3.0                              mx8mp_vpu.txt NXP-5G.mp4                                 sd.mp4 'System Volume Information'                 vela.ini android_p9.0.0_2.1.0-auto-ga_image_8qmek root@imx8ulpevk:~# ls Image_org  gpuinfo.sh root@imx8ulpevk:~# cp gpuinfo.sh /run/media/sda1/ root@imx8ulpevk:~# umount /run/media/sda1 root@imx8ulpevk:~#
View full article
Hello everyone! In this quick example its focused on how to customize uboot code to generate an uboot image with a silent console so its speed up the flash and boot time, this may provide helpful for customers who have a bigger images or just want to have a silent console. Note: this should not be enabled if the image is still being under test, since this will disable all communication with the debug terminal and there won't be boot messages. Requirements: I.MX 8M Nano DDR4 EVK i.MX 8M Nano EVK Prebuilt image (6.1.1-1.0.0) UUU tool First clone the code from the uboot repository: $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.1.1-1.0.0 $ cd uboot-imx After we get the code, then proceed to enable the silent console in the uboot defconfig: $ nano configs/imx8mn_ddr4_evk_defconfig CONFIG_SILENT_CONSOLE=y CONFIG_SILENT_U_BOOT_ONLY=y For this to actually work we need to create the silent environmental variable and give it a value different from "0": $ nano include/configs/imx8mn_evk.h "silent=1\0"      \ As specified in our Linux porting guide: Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set Target-Machine to the machine you are building for. See Section "Build configurations" in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG) Set up the host terminal window toolchain environment: $ source/opt/fsl-imx-xwayland/6.1.1/environment-setup-aarch64-poky-linux $ export ARCH=arm64 Build uboot binary: $ make distclean $ make imx8mn_ddr4_evk_defconfig $ make Build ARM Trusted Firmware (ATF) $ cd .. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.1.1-1.0.0 $ cd imx-atf/ $ make PLAT=imx8mn bl31 In case you get the error aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' $ unset LDFLAGS Download the DDR training & HDMI binaries $ cd .. $ mkdir firmware-imx $ cd firmware-imx $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.19.bin $ chmod a+x firmware-imx-8.19.bin $ ./firmware-imx-8.19.bin Accept EULA and the firmware will be deployed. Download imx-mkimage and build the boot image $ cd .. $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.1.1-1.0.0 $ cd imx-mkimage $ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ $ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ $ cp ../uboot-imx/arch/arm/dts/imx8mn-ddr4-evk.dtb iMX8M/ $ cp ../imx-atf/build/imx8mn/release/bl31.bin iMX8M/ $ cp ../firmware-imx/firmware-imx-8.19/firmware/ddr/synopsys/ddr4_* iMX8M/ $ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot $ make SOC=iMX8MN flash_ddr4_evk After this we can download our uboot image to our board, we can either use the uboot image for boot or for flashing purpose only. We can compare the time it takes using UUU with a standard pre-built image uuu -V -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-full-imx8mnevk.wic It takes 485.5 seconds using normal uboot with debug console enabled. uuu -V -b emmc_all flash.bin imx-image-full-imx8mnevk.wic It takes 477.5 seconds using silent uboot console. Even if the speed is not greatly improved (~8 seconds), in larger files it could help to speed up flashing, even if wants to have the console silent is a good option. Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
View full article
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there.  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
View full article
Environment BSP: L6.1.22_2.0.0​ Platform: i.MX93 Links:  https://github.com/NXP/swupdate-scripts https://github.com/nxp-imx-support/meta-swupdate-imx   The AN13872 provides us the swupdate yocto layer, swupdate-scripts and test steps, but there is still much to add. The purpose of this knowledge base is to provide customized advice. 1.How to port meta-swupdate-imx to any yocto version you want? As meta-swupdate-imx only provide kirkstone version, we can upgrade or degrade it based on this version. We will take L6.1.22_2.0.0​ porting steps as an example. 1.1 Download Yocto layer  cd imx-yocto-bsp/sources git clone https://github.com/sbabic/meta-swupdate.git -b mickledore git clone https://github.com/nxp-imx-support/meta-swupdate-imx.git 1.2 Modify  Yocto layer  imx-yocto-bsp/sources/meta-swupdate-imx/conf/layer.conf   You can find swupdate version in imx-yocto-bsp/sources/meta-swupdate/recipes-support/swupdate/ 1.3 Handle patches in meta-swupdate-imx/recipes-bsp/u-boot/files/ About patchs in sources/meta-swupdate-imx/recipes-bsp/u-boot/files/ and imx-yocto-bsp/sources/meta-swupdate-imx/recipes-support/swupdate/files/, you need use devtool to unpack uboot and swupdate into workspace and add changes manunally for development. CONFIG_ENV_OFFSET_REDUND=CONFIG_ENV_OFFSET+CONFIG_ENV_SIZE   sources/meta-swupdate-imx/recipes-bsp/u-boot/u-boot-imx_%.bbappend 2.How to flash base image? Use uuu or dd command, just like common imx-image-xxx 3.swupdate-scripts porting suggestions 3.1 Partition table You can modify partition table refer the size of images. For different soc, the first offset is different. If you are porting i.MX8MP based on iMX8MM, the offset should be 32K.   3.2 Some errors 3.2.1 This error indicates that you need enlarge size of rootfs. e2fsck 1.45.5 (07-Jan-2020) The filesystem size (according to the superblock) is 887599 blocks The physical size of the device is 768000 blocks Either the superblock or the partition table is likely to be corrupt! Abort<y>?    3.2.2 You need upgrade e2fsck verison. e2fsck 1.46.5 (30-Dec-2021) /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4 has unsupported feature(s): FEATURE_C12 e2fsck: Get a newer version of e2fsck! /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4: ********** WARNING: Filesystem still has errors ********** resize2fs 1.46.5 (30-Dec-2021) resize2fs: Filesystem has unsupported feature(s) (/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_ass  solution: wget https://mirrors.edge.kernel.org/pub/linux/kernel/people/tytso/e2fsprogs/v1.47.0/e2fsprogs-1.47.0.tar.xz tar -xf e2fsprogs-1.47.0.tar.xz cd e2fsprogs-1.47.0/ ./configure make -j16 sudo make install   3.2.3 mtools /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 58: mdir: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 68: mdir: command not found solution: sudo apt-get install mtools
View full article
We are pleased to announce that Config Tools for i.MX v14.0 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) The product is based on Eclipse 2022-12 Open JDK 17 is updated. Batch processing on command line is supported. Support for SDK 2.14 in Project cloner and Detect toolchain project is added. Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error. Search functionality to Code Preview is added. TEE Export TEE registers via wizard or command line is available. Boot ROM hiding feature is supported. Tier mode for TRDC is supported. Domain ambivalence for RDC masters is added. Master-specific memory alias Validation for A28 bit of MPU region address is added. Memory map filters are aligned with Arm terminology. Status bar is united with other tools. Pins Labels defined for Expansion header pins can be set as identifiers of the routed pin. Expansion headers can be locked for editing. Expansion headers and boards are added to the HTML and CSV reports. Pins filtering is added into the expansion header pin routing dialogs. Columns from Routing Details can be added to the External User Signals view. New External User Signals can be created for all routed pins that are missing in the signals table. Clocks Support for the same frequencies settings from different source for internal clocks is added.
View full article
vpuwraper can fulfill VPU decoder/encoder, if customer’s user case is simple, for example they just need to encode yuv stream to H264, or decode H264 stream to yuv, There is no need to use gstreamer or V4L2 complex framework, you can use vpuwraper. Platform: i.MX8MP + L5.4.70.2.3.0 Build Procedure: mkdir vpu cd vpu git clone https://github.com/nxp-imx/imx-vpuwrap   cd imx-vpuwrap/ git tag -l   git switch -c rel_imx_5.4.70_2.3.0   source ../../.././5.4.70.2.3.0/sdk/environment-setup-aarch64-poky-linux   make -f Makefile_8mp   Test on i.MX8MP EVK board Pls find attached test log for decode and encode If busChromaU in YUV file is null, you will failed to encode it, pls apply vpuwraper patch for L5.4.70.2.3.0.patch to fix it If YUV file is interleave format, you need to add interleave parameter : -interleave 1 ./test_enc_arm_elinux -i test.yuv -o aaa.h264 -f 2 -w 176 -h 96 -interleave 1   Thanks, Lambert
View full article