i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Gingerbread (GB) Prepare the SD Card root/ : root file system (including init, init.rc, etc). Mounted at / system/:  Android system binary/libraries. Mounted at /system data/: Android data area. Mounted at /data recovery/: root file system when booting in "recovery" mode. Not directly used. Partition Description Type Size Header 8 BOOT raw area for bootloader and MEDIA DATA CACHE RECOVERY An example of partition a 4 GB SD card: Copy the system to SD card # sudo dd if=u-boot.bin of=/dev/sdx bs=1K skip=1 seek=1; sync # sudo dd if=u-boot-no-padding.bin of=/dev/sdx bs=1K seek=1; sync # sudo dd if=uImage of=/dev/sdx bs=1M seek=1; sync # sudo dd if=uramdisk.img of=/dev/sdx bs=1M seek=6; sync # sudo dd if=system.img of=/dev/sdx2; sync # sudo dd if=recovery.img of=/dev/sdx4; sync Ice Cream Sandwich (ICS)
View full article
There is no Freescale GStreamer element which does the JPEG decoding, so we must rely on a standard one, like 'jpegdec'. In case your Linux system was built using LTIB, in order to have the jpegdec element included on the gst-plugin-good, follow these steps: On the LTIB menuconfig, make sure the following packages are selected: gstreamer-plugins-good libjpeg libpng Remove the configure parameters '--disbale-libpng' and '--disable-jpeg' on the file './dist/lfs-5.1/gst-plugins-good/gst-plugins-good.spec' Rebuild and flash your board (or SD card) again. Image display VSALPHA=1 gst-launch filesrc location=sample.jpeg ! jpegdec ! imagefreeze ! mfw_isink Important: non 8 pixel aligned width and height is treated as not supported format in isink plugin.
View full article
ATK (Advanced Toolkit) ATK is a Windows tool for programming the flash memory of i.MX boards. It can be downloaded here. Using ATK This section will describe the procedure to erase the flash memory and program the bootloader. 1. Assemble the PDK using the CPU board, the Personality board, and the Debug board. 2. Connect a USB cable between the PC and the i.MX25 PDK Personality board. 3. Some hardware configurations (switches) must be set for booting from UART/USB:   On the debug board:   Switch SW5 -> Off   Switch SW6 -> Off   Switch SW7 -> Off   Switch SW8 -> Off   Switch SW9 -> On   Switch SW10 -> On   On the personality board:   Switch SW21 -> 11000000   Switch SW22 -> 00000000 {{Note|On SW5 thourgh SW10, "1" means the keys selected towards the edge of the board.} 4. Run ATK (1.6 or above) going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit   Set the options:   i.MX CPU -> i.MX25_TO1.1   Device memory -> DDR2;   Custom Initial File -> (keep it unmarked)   Communication Channel -> USB 5. Power up the i.MX25 PDK 6. Click on "Next" 7. Click on Flash Tools to erase, program or dump the the flash memory and click GO. NAND Flash Erasing 1. Configure the Dip Switch of Personality Board:                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                      Switch 1 2 3 4 5 6 7 8 SW1 OFF OFF OFF OFF N/A N/A N/A N/A SW2 ON OFF OFF ON ON OFF OFF OFF 2. Choose NAND model K9LAG08U8M 3. Continue the steps Remember to select the checkbutton BBT (Back Block Table) Commands to flash kernel and rootfs fis init -f load -r -b 0x100000 zImage -h <host IP address> fis create -f 0x300000 kernel load -r -b 0x100000 rootfs.jffs2 -h <host IP address> fis create -f 0x800000 root fis load kernel exec -c "noinitrd console=ttymxc0 115200 root=/dev/mtdblock2 rw ip=dhcp rootfstype=jffs2" Command to create rootfs.jffs2 mkfs.jffs2 -r rootfs -e 0x80000 -s 0x1000 -n -o rootfs.jffs2
View full article
Platform: imx8qm mek imx-yocto-L4.14.98_2.0.0_ga Building Step: Apply the nvp6324 patches.   Symbol: IMX8_NVP6324 [=y] Type : tristate Prompt: IMX8 NVP6324 Driver Location: -> Device Drivers -> Multimedia support (MEDIA_SUPPORT [=y]) -> V4L platform devices (V4L_PLATFORM_DRIVERS [=y]) -> MX8 Video For Linux Video Capture (VIDEO_MX8_CAPTURE [=y]) (1) -> IMX8 Camera ISI/MIPI Features support ‍‍‍‍‍‍‍‍‍ select nvp6324 to y in menuconfig(default is 'y') make Image -j8; make freescale/fsl-imx8qm-mek-nvp6324.dtb, to build kernel and dts, outputs are at  work/imx8qmmek-poky-linux/linux-imx/4.14.98-r0/build/arch/arm64/Image work/imx8qmmek-poky-linux/linux-imx/4.14.98-r0/build/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-nvp6324.dtb copy them to the sd boot partition. reboot the board, you can test the first camera with command: ./mx8_v4l2_cap_drm.out -cam 1 -ow 1280 -oh 720 mx8_v4l2_cap_drm.out is at /unit_tests/V4L2/mx8_v4l2_cap_drm.out The corresponding video device should be default to /dev/video0 ~ /dev/video3.
View full article
1. When reusing the build directory, sometimes compilation errors are seen; to overcome these, a fast solution is to clean the Share State Cache of the particular recipe/package $ bitbake <name of the recipe> -c cleansstate 2. Re-run the recipe $ bitbake <name of the recipe> 3. Re-run the bitbake command you were running, before getting into trouble. For example: $ bitbake fsl-image-gui In case the problem persists, please send the log into the mailing list or check if this issue has been reported previously.
View full article
Introduction The "smart" package management system is available in  Yocto Project for managing  packages on a target machine. A host is configured as a server for the packages and on the target the "package-management" feature is enabled for working with the packages. The steps for setup and usage are described below. Resources The Yocto Project package management system will work with many hosts and targets. The following were used for creating this document: Host: Ubuntu 14.04 64-bit Target: MCIMX6Q-SDP Freescale Yocto Project Release Documentation: Linux 3.14.38_6ul BSP & Multimedia Codecs Documentation (fsl-yocto-L3.14.38_6ul-ga.tar.gz) Host You have successfully installed a Freescale Yocto Project release. (Refer to Freescale Yocto Project Release Documentation). There are two steps for adding package management and then building: 1. Modify conf/local.conf EXTRA_IMAGE_FEATURES = "debug-tweaks package-management" ‍ 2. Build the image: bitbake core-image-minimal ‍ The core-image-minimal recipe provides an image enabling the target board to boot and support a serial console. 3. Create SDCARD: $ cd <build>/tmp/deploy/images/imx6qsabresd $ sudo dd if=core-image-minimal-imx6qsabresd.sdcard of=/dev/sdb bs=4M && sync ‍‍ Note - verify location of SDCARD on your host, /dev/sdb in this example. Examine 'cat /proc/partitions' 4. Setup web server and add link to rpm packages A web server, lighttpd, is installed. $ sudo apt-get install lighttpd ‍ Provide user write capability in /var/www $ sudo chmod 777 /var/www ‍ Create a soft link in the default web server directory to the rpm directory from the build. Note: Please update $HOME/<build> to your actual location: $ ln -s $HOME/<build>/tmp/deploy/rpm /var/www/imx6qsd ‍‍‍ Target Insert the SDCARD created from step 3 above, connect power and console cable  and power on the MCIMX6Q-SDP. Login using the "root" id, no password required. The /usr/bin/smart application is now used to setup the channels and perform package commands. For all smart options: smart --help ‍ 1. Add channels To add the packages from the host to your target, the smart  channel --add is used: Please enter the IP adress of your server, replacing SERVERIP below: smart channel --add all type=rpm-md name=all baseurl= http://SERVERIP/imx6qsd/all smart channel --add cortexa9hf_vfp_neon type=rpm-md name=cortexa9hf_vfp_neon baseurl= http://SERVERIP/imx6qsd/cortexa9hf_vfp_neon smart channel --add imx6qsabresd type=rpm-md name=imx6qsabresd baseurl= http://SERVERIP/imx6qsd/imx6qsabresd ‍‍‍‍‍‍‍‍‍ Check  the added channels: root@imx6qsabresd:~# smart channel --list all imx6qsabresd rpmsys cortexa9hf_vfp_neon ‍‍‍‍‍ 2. Update  local package cache Once the chanels have been added, the local package cache is updated. Note  SERVERIP below will be the host IP address in your network. root@imx6qsabresd:~# smart update Loading cache... Updating cache...               ######################################## [100%] Fetching information for 'all'...                                           -> http://SERVERIP/imx6qsd/all/repodata/repomd.xml                          repomd.xml                      ######################################## [ 16%]                                                                             Fetching information for 'imx6qsabresd'... -> http://SERVERIP/imx6qsd/imx6qsabresd/repodata/repomd.xml                 repomd.xml                      ######################################## [ 41%]                                                                             Fetching information for 'cortexa9hf_vfp_neon'... -> http://SERVERIP/imx6qsd/cortexa9hf_vfp_neon/repodata/repomd.xml          repomd.xml                      ######################################## [ 66%] Updating cache...               ######################################## [100%] Channels have no new packages. 3. Searching for packages Let us look at all packages containing the string client root@imx6qsabresd:~# smart search client* Loading cache... Updating cache...               ######################################## [100%] libice-dbg - ICE: Inter-Client Exchange library - Debugging files libice-dev - ICE: Inter-Client Exchange library - Development files libice-doc - ICE: Inter-Client Exchange library - Documentation files libice-staticdev - ICE: Inter-Client Exchange library - Development files (Static Libraries) libice6 - ICE: Inter-Client Exchange library libsm-dbg - SM: Session Management library - Debugging files libsm-dev - SM: Session Management library - Development files libsm-doc - SM: Session Management library - Documentation files libsm-staticdev - SM: Session Management library - Development files (Static Libraries) libsm6 - SM: Session Management library libx11-6 - Xlib: C Language X Interface library libx11-dbg - Xlib: C Language X Interface library - Debugging files libx11-dev - Xlib: C Language X Interface library - Development files libx11-doc - Xlib: C Language X Interface library - Documentation files libx11-locale - Xlib: C Language X Interface library libx11-staticdev - Xlib: C Language X Interface library - Development files (Static Libraries) libx11-xcb1 - Xlib: C Language X Interface library libxau-dbg - Xau: X Authority Database library - Debugging files libxau-dev - Xau: X Authority Database library - Development files libxau-doc - Xau: X Authority Database library - Documentation files libxau-staticdev - Xau: X Authority Database library - Development files (Static Libraries) libxau6 - Xau: X Authority Database library python-netclient - Python Internet Protocol clients xtrans-dbg - XTrans: X Transport library - Debugging files xtrans-dev - XTrans: X Transport library - Development files xtrans-doc - XTrans: X Transport library - Documentation files ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Adding openssh client to core-image minimal The core-image-minimal does not provide openssh client applications like ssh or scp. Let's add them on the host then update the target cache of packages and then install. Host Run bitbake to exercise all the tasks for packagegroup-core-ssh-openssh $ bitbake packagegroup-core-ssh-openssh ‍ After building a package individually, always update the package-index $ bitbake package-index ‍ Target Run smart to update the local cache which will pickup the new packages from the bake above. root@imx6qsabresd:~# smart update Loading cache... Updating cache...               ######################################## [100%] Fetching information for 'all'...                                              -> http://SERVERIP/imx6qsd/all/repodata/repomd.xml                           repomd.xml                      ######################################## [ 16%] -> http://SERVERIP/imx6qsd/all/repodata/primary.xml.gz                       primary.xml.gz                  ######################################## [ 25%] -> http://SERVERIP/imx6qsd/all/repodata/filelists.xml.gz                     filelists.xml.gz                ######################################## [ 33%]                                                                                Fetching information for 'imx6qsabresd'... -> http://SERVERIP/imx6qsd/imx6qsabresd/repodata/repomd.xml                  repomd.xml                      ######################################## [ 50%] -> http://SERVERIP/imx6qsd/imx6qsabresd/repodata/primary.xml.gz              -> http://SERVERIP/imx6qsd/imx6qsabresd/repodata/filelists.xml.gz            filelists.xml.gz                ######################################## [ 58%] primary.xml.gz                  ######################################## [ 66%]                                                                                Fetching information for 'cortexa9hf_vfp_neon'... -> http://SERVERIP/imx6qsd/cortexa9hf_vfp_neon/repodata/repomd.xml           repomd.xml                      ######################################## [ 83%] -> http://SERVERIP/imx6qsd/cortexa9hf_vfp_neon/repodata/primary.xml.gz       primary.xml.gz                  ######################################## [ 91%] -> http://SERVERIP/imx6qsd/cortexa9hf_vfp_neon/repodata/filelists.xml.gz     filelists.xml.gz                ######################################## [100%] Updating cache...               ######################################## [100%] Channels have 15 new packages. Saving cache... ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Examine information about local cache: root@imx6qsabresd:~# smart stats Loading cache... Updating cache...               ######################################## [100%] Installed Packages: 80 Total Packages: 3586 Total Provides: 6580 Total Requires: 1611 Total Upgrades: 3565 Total Conflicts: 25 ‍‍‍‍‍‍‍‍‍‍‍ See what ssh packages are now available: root@imx6qsabresd:~# smart search *ssh* Loading cache... Updating cache...               ######################################## [100%] openssh - Secure rlogin/rsh/rcp/telnet replacement openssh-dbg - Secure rlogin/rsh/rcp/telnet replacement - Debugging files openssh-dev - Secure rlogin/rsh/rcp/telnet replacement - Development files openssh-doc - Secure rlogin/rsh/rcp/telnet replacement - Documentation files openssh-keygen - Secure rlogin/rsh/rcp/telnet replacement openssh-misc - Secure rlogin/rsh/rcp/telnet replacement openssh-ptest - Secure rlogin/rsh/rcp/telnet replacement - Package test files openssh-scp - Secure rlogin/rsh/rcp/telnet replacement openssh-sftp - Secure rlogin/rsh/rcp/telnet replacement openssh-sftp-server - Secure rlogin/rsh/rcp/telnet replacement openssh-ssh - Secure rlogin/rsh/rcp/telnet replacement openssh-sshd - Secure rlogin/rsh/rcp/telnet replacement packagegroup-core-ssh-openssh - OpenSSH SSH client/server packagegroup-core-ssh-openssh-dbg - OpenSSH SSH client/server - Debugging files packagegroup-core-ssh-openssh-dev - OpenSSH SSH client/server - Development files ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Install openssh root@imx6qsabresd:~# smart install openssh Loading cache... Updating cache...               ######################################## [100%] Computing transaction... Installing packages (9):   openssh-6.7p1-r0@cortexa9hf_vfp_neon                                            openssh-keygen-6.7p1-r0@cortexa9hf_vfp_neon                                     openssh-scp-6.7p1-r0@cortexa9hf_vfp_neon                                        openssh-ssh-6.7p1-r0@cortexa9hf_vfp_neon                                        openssh-sshd-6.7p1-r0@cortexa9hf_vfp_neon                                       shadow-4.2.1-r0@cortexa9hf_vfp_neon                                             shadow-base-4.2.1-r0@cortexa9hf_vfp_neon                                        shadow-securetty-4.2.1-r3@imx6qsabresd                                          util-linux-sulogin-2.25.2-r1@cortexa9hf_vfp_neon                              1.4MB of package files are needed. 3.2MB will be used. Confirm changes? (Y/n): y Fetching packages...                                                           -> http://SERVERIP/imx6qsd/.../openssh-6.7p1-r0.cortexa9hf_vfp_neon.rpm      -> http://SERVERIP/imx6qsd/.../shadow-securetty-4.2.1-r3.imx6qsabresd.rpm    shadow-securetty-4.2.1-r3.imx.. ######################################## [ 11%] -> http://SERVERIP/imx6qsd/.../openssh-scp-6.7p1-r0.cortexa9hf_vfp_neon.rpm openssh-scp-6.7p1-r0.cortexa9.. ######################################## [ 22%] openssh-6.7p1-r0.cortexa9hf_v.. ######################################## [ 33%] -> http://SERVERIP/imx6qsd/.../openssh-sshd-6.7p1-r0.cortexa9hf_vfp_neon.rpm openssh-sshd-6.7p1-r0.cortexa.. ######################################## [ 44%] -> http://SERVERIP/imx6qsd/.../shadow-4.2.1-r0.cortexa9hf_vfp_neon.rpm       -> http://SERVERIP/imx6qsd/.../openssh-ssh-6.7p1-r0.cortexa9hf_vfp_neon.rpm openssh-ssh-6.7p1-r0.cortexa9.. ######################################## [ 55%] -> http://SERVERIP/imx6qsd/.../shadow-base-4.2.1-r0.cortexa9hf_vfp_neon.rpm shadow-base-4.2.1-r0.cortexa9.. ######################################## [ 66%] shadow-4.2.1-r0.cortexa9hf_vf.. ######################################## [ 77%] -> http://SERVERIP/.../util-linux-sulogin-2.25.2-r1.cortexa9hf_vfp_neon.rpm util-linux-sulogin-2.25.2-r1... ######################################## [ 88%] -> http://SERVERIP/.../openssh-keygen-6.7p1-r0.cortexa9hf_vfp_neon.rpm       openssh-keygen-6.7p1-r0.corte.. ######################################## [100%]                                                                                Committing transaction... Preparing...                    ######################################## [  0%]    1:Installing openssh-ssh     ######################################## [ 11%] Output from openssh-ssh-6.7p1-r0@cortexa9hf_vfp_neon:                          update-alternatives: Linking /usr/bin/ssh to /usr/bin/ssh.openssh                 2:Installing openssh-scp     ######################################## [ 22%] Output from openssh-scp-6.7p1-r0@cortexa9hf_vfp_neon:                          update-alternatives: Linking /usr/bin/scp to /usr/bin/scp.openssh                 3:Installing shadow-secure.. ######################################## [ 33%]    4:Installing shadow-base     ######################################## [ 44%] Output from shadow-base-4.2.1-r0@cortexa9hf_vfp_neon:                          update-alternatives: Linking /usr/bin/newgrp to /usr/bin/newgrp.shadow         update-alternatives: Linking /usr/bin/groups to /usr/bin/groups.shadow update-alternatives: Linking /bin/login to /bin/login.shadow update-alternatives: Linking /bin/su to /bin/su.shadow    5:Installing util-linux-su.. ######################################## [ 55%] Output from util-linux-sulogin-2.25.2-r1@cortexa9hf_vfp_neon:                  update-alternatives: Linking /sbin/sulogin to /sbin/sulogin.util-linux            6:Installing openssh-keygen  ######################################## [ 66%]    7:Installing shadow          ######################################## [ 77%] Output from shadow-4.2.1-r0@cortexa9hf_vfp_neon:                               update-alternatives: Linking /usr/bin/passwd to /usr/bin/passwd.shadow         update-alternatives: Linking /usr/bin/chfn to /usr/bin/chfn.shadow update-alternatives: Linking /usr/bin/chsh to /usr/bin/chsh.shadow update-alternatives: Linking /usr/sbin/chpasswd to /usr/sbin/chpasswd.shadow update-alternatives: Linking /sbin/vipw to /sbin/vipw.shadow update-alternatives: Linking /sbin/vigr to /sbin/vigr.shadow Output from openssh-sshd-6.7p1-r0@cortexa9hf_vfp_neon:                         Removing any system startup links for sshd ...                                Running useradd commands... NOTE: Performing useradd with [ --system --no-create-home --home-dir /var/run/sshd --shell /bin/false --user-group sshd] and 10 times of retry    8:Installing openssh-sshd    ######################################## [ 88%] Adding system startup for /etc/init.d/sshd.                                   Starting OpenBSD Secure Shell server: sshd   generating ssh RSA key...   generating ssh ECDSA key...   generating ssh DSA key...   generating ssh ED25519 key... done.    9:Installing openssh         ######################################## [100%] ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Check for the scp command: root@imx6qsabresd:~# which scp /usr/bin/scp ‍‍ Summary To add a new package on the server host, run bitbake <recipe> then bitbake package-index to update the rpm tracking information. On the target board, run smart update and then smart install <package>. Use smart search <regular expression string> to hunt for a package to install.
View full article
You can boot from SPI NOR Flash using the following procedure:      1 - Download ATK Release 1.7. The version ATK 1.7 can be downloaded here. 2 - Unzip file iMX_AdvancedToolKit_R170.zip into "C:\Program Files\freescale\AdvancedToolKit-STD\image\".      3 - Open the file "C:\Program Files\freescale\AdvancedToolKit-STD\config\ADSToolkit.cfg" and add the following lines: [MX25_TO11] MMC/SD::image\mx25_mmc.bin:0x(unknown) NAND::image\mx25_nand.bin:0x(unknown) SPI::image\mx25_spi.bin:0x(unknown) [MX31]   4 - Set the SPI Boot Config on MX25PDK:   SW22: no influence SW21[1-8]: 11110010 BT_MEM_CTL[0:1] = 11 (Expansion) BT_MEM_TYPE[0:1] = 11 (Serial ROM via SPI) BT_PAGE_SIZE[0:1] = no influence BT_BUS_WIDTH[0:1] = 10 (3-Address SPI (24-bit) Note: BT_BUS_WIDTH[0]=1, BT_BUS_WIDTH[1]=0 On Debug Board the red switches: (SW5-SW10) = 000011 (0=off) Boot Config Switches (SW21, SW22) on Personality Board have no influence.   5 - Connect USB or Serial cable between Host PC and PDK and execute ATK   6 - Select USB/UART serial boot on MX25PDK and power on the board   7 - Configure ATK as following: Device = i.MX25_TO1.1 device memory initial = DDR2 Communication channel: COMn (select the COM port on your PC) or Communication channel: USB If you choose COM (serial UART connection) you MUST disconnect USB cable from OTG connector on i.MX25 PDK.   8 - Configure ATK "Flash Tool" as following: Tick "Program" Tick "Read Back Check" Flash Model = SPI Address = 0x0 Image = mx25_3stack_redboot_TO1_1.bin (same file as for NAND boot). Same should be applicable to U-boot.   Note: SPI NOR Boot requires internal boot mode. On Debug Card all red switches must be off (SW5-SW10) = 000000 (0=off). Note: if booting from SPI NOR, Redboot needs approx 2 seconds before it shows messages on the console.
View full article
Introduction ARM SoC+FPGA/CPLD is widely used in some application like industry control and data acquisition system, there were many customers adopted i.MX6 EIM (a memory parallel interface) to access FPGA/CPLD, and archived good data throughput, but EIM is removed from i.MX8M and i.MX9, some customers is asking for such a compatible solution for i.MX8/8M and coming i.MX9 family.  FlexSPI is designed for connecting storage devices like NOR Flash, integrated in most of i.MXRT/i.MX8/LS products and provides flexible configuration for 4-wire/8wire working mode, this article provides a low-cost and efficiency demo to show how  to support CPLD/FPGA  via FlexSPI, as a replacement of EIM for EP i.MX8/9/LS products. key features Implement a  new kernel driver for FlexSPI to support read/write access to FPGA/CPLD. Support two type connections: Support 4-wire(QSPI) and 8-wire(HypeBUS, OctalSPI) Deliverables A new kernel driver for FlexSPI to support read/write access to FPGA/CPLD by AHB command A kernel patch to disable the QSPI Flash in kernel A test program shows how to do read/write performance test. Hardware Hardware Prepare: i.MX8MM-LPDDR4-EVK Lattice LFE5U EVK Figure1 4-wire SPI HW Block diagram Figure2 8-wire OctalSPI   Hardware Rework on i.MX8MM-EVK     1 Need to remove the SPI-Flash(U5, MT25QU256ABA) on the i.MX8MM-EVK board, and wire below signals: QSPI_DATA0 QSPI_DATA1 QSPI_DATA2 QSPI_DATA3 QSPI_SCLK QSPI_nSS0 VDD_1V8 GND Figure3 QPSI signals for FPGA/CPLD Figure4 Hardware rework on i.MX8MM-EVK board Note that, i.MX8MM-EVK QSPI power rails is 1.8v, so be careful that the FPGA/CPLD side IO should be 1.8V. Software BSP version 1 Linux BSP version: L5.10.52 Software Change  Apply 0001-FlexSPI-FPGA-need-to-disable-flexspi-for-fpga-usage.patch in Linux kernel and generate the new dtb extract the flexspi-fpga driver compile the flexspi-fpga driver with the kernel$ $make -C $(YOUR_KDIR) M=$(FlexSPI_FPGAW_DIVER_DIR) modules ARCH=arm64 CROSS_COMPILE=$(CROSS_COMPILE) Deployment  upload new generated i.mx8mm-evk.dtb to the target board(the 1st partition) upload the flex-spi driver and fpga/cpld test program to the target board   Test Test1: Set the flexspi working at 40Mhz   $insmod imx_flexspi_fpga.ko pre_div=2 post_div=5 Read/write FPGA/CPLD test .$/flexspi_fpga_test -p 0x08000000 -s 768 Test2: Set the FlexSPI working at 100MHz   $ insmod imx_flexspi_fpga.ko pre_div=1 post_div=4 Read/write FPGA/CPLD test $./flexspi_fpga_test -p 0x08000000 -s 768   Limitation FPGA and Flash devices can’t work at the same time due to just one FlexSPI controller. Due to the IO assignment conflict in i.MX8M EVK design, this demo just tested 4-wire(QSPI) mode at 50MHz and got data throughput as expected. Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
View full article
Application Note AN13872  Enabling SWUpdate on i.MX 6ULL, i.MX 8M Mini, and i.MX 93 is available on www.nxp.com    SWUpdate: Embedded Systems become more and more complex. Software for Embedded Systems have new features and fixes can be updated in a reliable way. Most of time, we need OTA(Over-The-Air) to upgrade the system. Like Android has its own update system. Linux also need an update system. SWUpdate project is thought to help to update an embedded system from a storage media or from network. However, it should be mainly considered as a framework, where further protocols or installers (in SWUpdate they are called handlers) can be easily added to the application. Mongoose daemon mode: Mongoose is a daemon mode of SWUpdate that provides a web server, web interface and web application. Mongoose is running on the target board(i.MX8MM EVK/i.MX8QXP MEK).Using Web browser to access it.   Suricatta daemon mode: Suricatta regularly polls a remote server for updates, downloads, and installs them. Thereafter, it reboots the system and reports the update status to the server. The screenshot is SWUpdate scuricatta working with hawkbit server.          
View full article
Notes: First run the playback pipeline then the streaming pipeline. The above example streams H263 video and AMR audio data. Change codec format to your needs. In case where the iMX is the streaming machine, the audio encoder 'amrnbenc' must be installed before. This scenario has not been tested Shell variables and pipelines Playback machine (receiver) # On playback machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where PC does the playback     AUDIO_DEC_SINK="rtpamrdepay ! amrnbdec ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! ffdec_h263 ! autovideosink" ## End of IMX2PC Settings ## PC2IMX: Case where iMX does the playback     AUDIO_DEC_SINK="rtpamrdepay ! mfw_amrdecoder ! alsasink "     VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\""     VIDEO_DEC_SINK="rtph263pdepay ! vpudec ! mfw_v4lsink " ## End of PC2IMX Settings PLAYBACK_AUDIO="udpsrc caps=\"application/x-rtp,media=(string)audio,clock-rate=(int)8000,encoding-name=(string)AMR,encoding-params=(string)1,octet-align=(string)1\" \             port=5002 ! rtpbin.recv_rtp_sink_1 \         rtpbin. ! $AUDIO_DEC_SINK \      udpsrc port=5003 ! rtpbin.recv_rtcp_sink_1 \      rtpbin.send_rtcp_src_1 ! udpsink port=5007 sync=false async=false" PLAYBACK_VIDEO="udpsrc caps=$VIDEO_CAPS port=5000 ! rtpbin.recv_rtp_sink_0 \         rtpbin. ! $VIDEO_DEC_SINK \         udpsrc port=5001 ! rtpbin.recv_rtcp_sink_0 \         rtpbin.send_rtcp_src_0 ! udpsink port=5005 sync=false async=false" PLAYBACK_AV="$PLAYBACK_VIDEO $PLAYBACK_AUDIO" # Playback pipeline gst-launch -v gstrtpbin name=rtpbin $PLAYBACK_AV Streaming Machine (sender) # On Streaming machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where iMX does the streaming     IP=x.x.x.x # IP address of the playback machine     VIDEO_SRC="mfw_v4lsrc"     VIDEO_ENC="vpuenc codec=h263 ! rtph263ppay "    AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " ## END IMX2PC settings ## PC2IMX: Case where PC does the streaming     IP=y.y.y.y # IP address of the playback machine     VIDEO_SRC="v4l2src"     VIDEO_ENC="ffenc_h263 ! rtph263ppay "     AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " # END PC2PC settings STREAM_AUDIO="$AUDIO_ENC ! rtpbin.send_rtp_sink_1 \         rtpbin.send_rtp_src_1 ! udpsink host=$IP port=5002 \         rtpbin.send_rtcp_src_1 ! udpsink host=$IP port=5003 sync=false async=false \         udpsrc port=5007 ! rtpbin.recv_rtcp_sink_1" STREAM_VIDEO="$VIDEO_SRC ! $VIDEO_ENC ! rtpbin.send_rtp_sink_0 \         rtpbin.send_rtp_src_0 ! queue ! udpsink host=$IP port=5000 \         rtpbin.send_rtcp_src_0 ! udpsink host=$IP port=5001 sync=false async=false \         udpsrc port=5005 ! rtpbin.recv_rtcp_sink_0" STREAM_AV="$STREAM_VIDEO $STREAM_AUDIO" # Stream pipeline gst-launch -v gstrtpbin name=rtpbin $STREAM_AV
View full article
GmSSL is an open source cryptographic toolbox that supports SM2 / SM3 / SM4 / SM9 and other national secret (national commercial password) algorithm, SM2 digital certificate and SM2 certificate based on SSL / TLS secure communication protocol to support the national security hardware password device , To provide in line with the national standard programming interface and command line tools, can be used to build PKI / CA, secure communication, data encryption and other standards in line with national security applications. For more information, please access GmSSL official website http://gmssl.org/english.html.   Software environments as the belows: Linux kernel: imx_4.14.98_2.0.0_ga cryptodev: 1.9 HW platform: i.MX6UL, i.MX7D/S, i.MX8M/MM, i.MX8QM/QXP. The patches include the following features: 1, Support SM2/SM9 encryption/decryption/sign/verify/key exchange, RSA encryption/decryption, DSA/ECDSA sign/verify, DH/ECDH key agreement, ECC & DLC & RSA key generation and big number operation and elliptic curve math by CAAM hardware accelerating. 2, run "git apply 0001-Enhance-cryptodev-and-its-engine-in-GmSSL-by-CAAM-s-.patch" under folder sources/poky, and "git apply 0001-Add-public-key-cryptography-operations-in-CAAM-drive.patch" under folder sources/meta-fsl-bsp-release for patch these codes. 3, GmSSL Build command: $ tar zxvf GmSSL-master-iMX.tgz $ cd GmSSL-master-iMX (For i.MX8M/MM, i.MX8QM/QXP) $ source /opt/arm-arch64/environment-setup-aarch64-poky-linux  $ ./Configure -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS -DHW_ENDIAN_SWAP  --prefix=~/install64 --openssldir=/etc/gmssl --libdir=/usr/lib no-saf no-sdf no-skf no-sof no-zuc -no-ssl3 shared linux-aarch64 $ make  $ make install                            /*image and config file will be installed to folder ~/install64 */   (For i.MX6UL, i.MX7D/S) $ source /opt/arm-arch32/environment-setup-cortexa7hf-neon-poky-linux-gnueabi $ ./Configure -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS --prefix=~/install32 --openssldir=/etc/gmssl --libdir=/usr/lib no-saf no-sdf no-skf no-sof no-zuc -no-ssl3 shared linux-armv4 $ make  $ make install                            /*image and config file will be installed to folder ~/install32 */   4, How to use GmSSL: copy image gmssl to /usr/bin on i.MX board; copy gmssl libcrypto.so.1.1 and libssl.so.1.1 to /usr/lib on i.MX board; copy folder etc/gmssl to /etc/ on i.MX board. copy test examples (dhtest, dsatest, rsa_test, ecdhtest, ecdsatest, eciestest, sm3test, sms4test, sm2test, sm9test) under GmSSL-master-iMX/test  to U disk for running. You can run test examples by the following commands: #insmod /lib/modules/4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbeafb80c/extra/cryptodev.ko #/run/media/sda1/dhtest #/run/media/sda1/dsatest #/run/media/sda1/rsa_test #/run/media/sda1/ecdhtest #/run/media/sda1/ecdsatest #/run/media/sda1/eciestest #/run/media/sda1/sm3test #/run/media/sda1/sms4test #/run/media/sda1/sm2test #/run/media/sda1/sm9test and speed test commands: #gmssl speed sm2 #gmssl genrsa -rand -f4 512 #gmssl speed dsa #gmssl genrsa -rand -f4 1024 #gmssl speed rsa #gmssl genrsa -rand -f4 2048 #gmssl speed ecdsa #gmssl genrsa -rand -f4 3072 #gmssl speed ecdh #gmssl genrsa -rand -f4 4096   ++++++++++++++++++++++++++++     updating at 2019-09-10   +++++++++++++++++++++++++++++++++++++++++++++ 0001-fix-the-bug-which-hash-and-cipher-key-don-t-use-DMA-.patch fix the issue which dismatching on key buffer between crytodev and caam driver. Crytodev uses stack's buffer for key storage and caam driver use it to dma map which cause flush cache failure. The patch need to apply on cryptodev-module in Yocto build.   ++++++++++++++++++  updating at 2019-10-14 +++++++++++++++++++++++++++++++++++ This updating is for China C-V2X application. The meta-gmcrypto is Yocto layer which bases on GmSSL and Cryptodev. I add HW SM2 verification by dedicated CAAM job descriptor and enhanced SW SM2 verification by precomputed multiples of generator and ARMv8 assembler language to accelerate point  operation. Software environments as the belows: Linux kernel: imx_4.14.98_2.0.0_ga cryptodev: 1.9 HW platform: i.MX8M/MM/MN, i.MX8QM/QXP. How to build: 1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-4.14.98_2.0.0.  Copy meta-gmcrypto to folder (Yocto 4.14.98_2.0.0_ga dir)/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-cv2x and add BBLAYERS += " ${BSPDIR}/sources/meta-cv2x " into (Yocto 4.14.98_2.0.0_ga dir)/build-cv2x/conf/bblayers.conf and  IMAGE_INSTALL_append += " gmssl-bin "  into local.conf 3, Run bitbake fsl-image-validation-imx. 4, You can find cv2x-verify.c under (build dir)/tmp/work/aarch64-poky-linux/cryptodev-tests/1.9-r0/git/tests. It is example for using CAAM cryptdev interface to do C-V2X verification (includes SM2 p256, NIST p256 and brainpoolP256r1).  cv2x_benchmark.c under (build dir)/tmp/work/aarch64-poky-linux/gmssl/1.0-r0/gmssl-1.0/test is the benchmark test program of C-V2X verifying. It includes HW, SW and HW+SW(one CPU) verifying for SM2 p256, NIST p256 and brainpoolP256r1. 5, Run the below command on your i.MX8QXP MEK board. modprobe cryptodev ./cv2x_benchmark Note: the udpated GmSSL also support projective coordinates and affine coordinates (CAAM only support affine coordinates). Affine coordinates is used by default. You can call EC_GROUP_set_coordinates() and EC_GROUP_restore_coordinates() to change coordinates and restore default. When you hope to use some EC APIs under expected coordinates, you need to call EC_GROUP_set_coordinates() before EC APIs and EC_GROUP_restore_coordinates() after them. Like the below example: orig_coordinate = EC_GROUP_set_coordinates(EC_PROJECTIVE_COORDINATES); group = EC_GROUP_new_by_curve_name(NID_sm2p256v1); EC_GROUP_restore_coordinates(orig_coordinate);   ++++++++++++++++++++++++++++     updating at 2020-11-09   +++++++++++++++++++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.4.47_2.2.0​​. The meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release.  Software environments as the belows: Linux kernel: imx_5.4.47_2.2.0 cryptodev: 1.10 HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.4.47-2.2.0. Copy meta-gmcrypto to folder (Yocto 5.4.47_2.2.0 dir)/sources/ 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-gmcrypto " into (Yocto 5.4.47_2.2.0 dir)/build-imx8mmevk/conf/bblayers.conf and  IMAGE_INSTALL_append += " gmssl-bin "  into local.conf 3, Run bitbake fsl-image-validation-imx. 4, You can find cv2x-verify.c under (build dir)/tmp/work/aarch64-poky-linux/cryptodev-tests/1.10caam-r0/git/tests. It is example for using CAAM cryptdev interface to do C-V2X verification (includes SM2 p256, NIST p256 and brainpoolP256r1).  cv2x_benchmark.c under (build dir)/tmp/work/aarch64-poky-linux/gmssl/1.0-r0/gmssl-1.0/test is the benchmark test program of C-V2X verifying. It includes HW, SW and HW+SW(one CPU) verifying for SM2 p256, NIST p256 and brainpoolP256r1. 5, Run the below command on your i.MX8M Mini evk board. modprobe cryptodev ./cv2x_benchmark gmssl speed sm2 gmssl speed dsa gmssl speed rsa gmssl speed ecdsa gmssl speed ecdh gmssl genrsa -rand -f4 -engine cryptodev 4096 Note: 1, the udpated GmSSL also support projective coordinates and affine coordinates (CAAM only support affine coordinates). Affine coordinates is used by default. You can call EC_GROUP_set_coordinates() and EC_GROUP_restore_coordinates() to change coordinates and restore default. When you hope to use some EC APIs under expected coordinates, you need to call EC_GROUP_set_coordinates() before EC APIs and EC_GROUP_restore_coordinates() after them. Like the below example: orig_coordinate = EC_GROUP_set_coordinates(EC_PROJECTIVE_COORDINATES); group = EC_GROUP_new_by_curve_name(NID_sm2p256v1); EC_GROUP_restore_coordinates(orig_coordinate); 2, Yocto Zeus integrates openssl 1.1.1g, so I change library name of gmssl from libcrypto to libgmcrypto and from libssl to libgmssl to avoid name confliction with openssl 1.1.1g (lib name are also libcrypto.so.1.1 and libssl.so.1.1). You should use -lgmcrypto and -lgmssl when you link gmssl library instead of -lcrypto and -lssl.   +++++++++++++++++++++++    updating at 2021-02-08  ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.4.70_2.3.0​​. The package meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release. You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.4.70-2.3.0.    +++++++++++++++++++++++    updating for Linux-5.10.52-2.1.0  +++++++++++++++++++++++ This updating is for Yocto release of Linux 5.10.52_2.1.0​​. The package meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release.  1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.10.52-2.1.0.  Copy meta-gmcrypto to folder (Yocto 5.10.52_2.1.0 dir)/sources/. 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-gmcrypto " into (Yocto 5.10.52_2.1.0 dir)/build-imx8mmevk/conf/bblayers.conf and  IMAGE_INSTALL_append += " gmssl-bin "  into local.conf 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev gmssl speed sm2 gmssl genrsa -rand -f4 -engine cryptodev 512 gmssl speed dsa gmssl genrsa -rand -f4 -engine cryptodev 1024 gmssl speed rsa gmssl genrsa -rand -f4 -engine cryptodev 2048 gmssl speed ecdsa gmssl genrsa -rand -f4 -engine cryptodev 3072 gmssl speed ecdh gmssl genrsa -rand -f4 -engine cryptodev 4096 gmssl speed -evp sha256 -engine cryptodev -elapsed gmssl speed -evp aes-128-cbc -engine cryptodev -elapsed gmssl speed -evp aes-128-ecb -engine cryptodev -elapsed gmssl speed -evp aes-128-cfb -engine cryptodev -elapsed gmssl speed -evp aes-128-ofb -engine cryptodev -elapsed gmssl speed -evp des-ede3 -engine cryptodev -elapsed gmssl speed -evp des-cbc -engine cryptodev -elapsed gmssl speed -evp des-ede3-cfb -engine cryptodev -elapsed +++++++++++++++++++++++    updating for Linux-5.15.71-2.2.0 +++++++++++++++++++++++ This updating is for Yocto release of Linux 5.15.71-2.2.0​​. The package meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release.  1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.15.71-2.2.0.  Copy meta-gmcrypto to folder (Yocto 5.15.71-2.2.0 dir)/sources/. 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-gmcrypto " into (Yocto 5.15.71-2.2.0 dir)/build-imx8mmevk/conf/bblayers.conf and  IMAGE_INSTALL:append = " gmssl-bin "  into local.conf 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev gmssl speed sm2 gmssl genrsa -rand -f4 -engine cryptodev 512 gmssl speed dsa gmssl genrsa -rand -f4 -engine cryptodev 1024 gmssl speed rsa gmssl genrsa -rand -f4 -engine cryptodev 2048 gmssl speed ecdsa gmssl genrsa -rand -f4 -engine cryptodev 3072 gmssl speed ecdh gmssl genrsa -rand -f4 -engine cryptodev 4096 gmssl speed -evp sha256 -engine cryptodev -elapsed gmssl speed -evp aes-128-cbc -engine cryptodev -elapsed gmssl speed -evp aes-128-ecb -engine cryptodev -elapsed gmssl speed -evp aes-128-cfb -engine cryptodev -elapsed gmssl speed -evp aes-128-ofb -engine cryptodev -elapsed gmssl speed -evp des-ede3 -engine cryptodev -elapsed gmssl speed -evp des-cbc -engine cryptodev -elapsed gmssl speed -evp des-ede3-cfb -engine cryptodev -elapsed   +++++++++++++++++++++++    Updating for Linux-6.1.55-2.2.0 +++++++++++++++++++++++ This updating is new GmSSL 3.1.1 and Yocto release of Linux 6.1.55-2.2.0. 主要特性 超轻量:GmSSL 3 大幅度降低了内存需求和二进制代码体积,不依赖动态内存,可以用于无操作系统的低功耗嵌入式环境(MCU、SOC等),开发者也可以更容易地将国密算法和SSL协议嵌入到现有的项目中。 更合规:GmSSL 3 可以配置为仅包含国密算法和国密协议(TLCP协议),依赖GmSSL 的密码应用更容易满足密码产品型号检测的要求,避免由于混杂非国密算法、不安全算法等导致的安全问题和合规问题。 更安全:TLS 1.3在安全性和通信延迟上相对之前的TLS协议有巨大的提升,GmSSL 3 支持TLS 1.3协议和RFC 8998的国密套件。GmSSL 3 默认支持密钥的加密保护,提升了密码算法的抗侧信道攻击能力。 跨平台:GmSSL 3 更容易跨平台,构建系统不再依赖Perl,默认的CMake构建系统可以容易地和Visual Studio、Android NDK等默认编译工具配合使用,开发者也可以手工编写Makefile在特殊环境中编译、剪裁。 More information, please refer to Readme Recipe file is the attached gmssl_3.1.1.bb.tar.gz
View full article
Overview The purpose of this document is to provide GPU P11.1 upgraded kernel patches and binaries for ICS R13.4-GA or R13.4.1 release. This GPU upgrade fixed some issues and improve the performance, for example chrome browser mess display issue, GUI miss alignment issue, YV12 CTS verifier fail, improve Antutu benchmark performance, improve HTML5 performance, etc. Software and HW platform Software: R13.4-GA or R13.4.1 Android releases Hardware: MX6Dual/Quad SabreSD board or MX6DualLite SabreSD board. Patches You can get the patches from attached zip. For R13.4-GA, please apply the kernel patch and gpu binaries in r13.4-ga-p11.1-gpu-upgrade folder, find them in attach. For R13.4.1, please apply the kernel patch and gpu binaries in 13.4.1-p11.1-gpu-upgrade folder, find them in attach.
View full article
I've been asked to help to upload the doc in MPU support space. The doc describes some ideas about how to support a customer to enable a mipi-csi2 sensor connected with i.MX6DQ/6DL. Hope this may be helpful.
View full article
i.MX6Q Automotive board has one ADV7180 analog video decoder with 2 video inputs. By default, only input 1 is used (connector J42).     To connect 2 analog video sources and switch the display between them, the following changes are needed:   1 - Create a new IOCTL on V4L2_capture and ADV7180 device drivers to receive the information from user space application on what input will be selected. 2 - In this new IOCTL, use the "Fast Switch Script" for ADV7180 described at Analog Devices site: ADV7180 Fast Switch Script | EngineerZone  3 - Create a user space application to call the IOCTL mentioned on step 1.   See attached:   1 - 0001-ADV7180-Adding-input-switch-IOCTL.patch.zip - Patch to be applied on NXP kernel 4.1.15_1.0.0_ga 2 - example2.c.zip - Source code example of user space application. It changes the video input in each 2 seconds. (See it working on attached video) 3 - example2.zip - User space application executable file  4 - Makefile.zip - Makefile of user space application to be used as example 5 - adv7180_switch.mp4 - Video showing the application   In the application, VIDIOC_S_CHIP_INPUT IOCTL is called to change the input:   int input = 0; if (ioctl(fd_capture_v4l, VIDIOC_S_CHIP_INPUT, &input) < 0) { printf("VIDIOC_S_CHIP_INPUT failed\n"); return TFAIL; }‍‍‍‍‍‍‍‍‍‍‍‍   This IOCTL calls the ADV7180 Fast Switch Script, added on ADV7180 driver (see attached patch).
View full article
This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera options on the i.MX 8 boards. Plus, this document describes some Advanced camera use cases too, such as multiples cameras output using imxcompositor_g2d plugin, GStreamer zero-copy pipelines and V4L2 API extra-controls examples.
View full article
There is GPU SDK for i.MX6D/Q/DL/S: IMX_GPU_SDK.  This is to share the experience when compiling the example code from the SDK with Linux BSP release: L3.0.35_1.1.0_121218 and  L3.0.35_4.0.0_130424 . Minimal profile is using and have been verified on both i.MX6Q SDP and i.MX6DL SDP. To start: Please make sure “gpu-viv-bin-mx6q” has been selected in the Package list and compiled to your rootfs. After finished the compilation of the rootfs, you should find some newly added libraries for GLES1.0, GLES2.0, OpenVG and EGL in <ltib>/rootfs/usr/lib However, you should find libOpenVG.so is actually copied from libOepnVG_3D.so: vmuser@ubuntu:~/ltib_src/ltib/rootfs/usr/lib$ ls -al libOpen* -rwxr-xr-x 1 root root 115999 2013-06-06 18:31 libOpenCL.so -rwxr-xr-x 1 root root 515174 2013-06-06 18:31 libOpenVG_355.so -rwxr-xr-x 1 root root 272156 2013-06-06 18:31 libOpenVG_3D.so -rwxr-xr-x 1 root root 272156 2013-06-06 18:31 libOpenVG.so So, in this way, i.MX6D/Q will no use libOpenVG_355.so in the build. Also, if you run NFS, the libOpenVG.so will change to symbolic link:           For example, run on i.MX6Q SDP, it will link to /usr/lib/libOpenVG_355.so                          For example, run on i.MX6DL SDP, it will link to /usr/lib/libOpenVG_3D.so                Then, when you compile the OpenVG example code, it is becoming very confusing.  Thus, it needs to pay attention when doing the compilation.  For example, delete the symbolic link and make copy of the corresponding library: For i.MX6D/Q, please do this: $ sudo /bin/rm libOpenVG.so $ sudo cp libOpenVG_355.so libOpenVG.so For i.MX6S/DL, please do this: $ sudo /bin/rm libOpenVG.so $ sudo cp libOpenVG_3D.so libOpenVG.so To compile the sample code in the GPU SDK, you could refer to iMXGraphicsSDK_OpenGLES2.0.pdf or iMXGraphicsSDK_OpenGLES1.1.pdf in ~/gpu_sdk_v1.00.tar/Documentation/Tutorials to set up the cross compilation environment; which is assuming the LTIB and the rootfs is ready. $ export ROOTFS=/home/vmuser/ltib_src/ltib/rootfs $ export CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi- For OpenVG: $ cd ~/gpu_sdk_v1.00/Samples/OpenVG $ make -f Makefile.fbdev clean $ make -f Makefile.fbdev $ make -f Makefile.fbdev install The executable will then be copied to this directory: ~/gpu_sdk_v1.00/Samples/OpenVG/bin/OpenVG_fbdev For GLES2.0 $ cd ~/gpu_sdk_v1.00/Samples/ GLES2.0 $ make -f Makefile.fbdev clean $ make -f Makefile.fbdev $ make -f Makefile.fbdev install The executable will then be copied to this directory: ~/gpu_sdk_v1.00/Samples/ GLES2.0/bin/GLES20_fbdev For GLES1.1, please modify the Makefile.fbdev to remove the compilation of example codes "18_VertexBufferObjects" and "19_Beizer" that are not exist. Then, $ cd ~/gpu_sdk_v1.00/Samples/ GLES1.1 $ make -f Makefile.fbdev clean $ make -f Makefile.fbdev $ make -f Makefile.fbdev install The executable will then be copied to this directory: ~/gpu_sdk_v1.00/Samples/ GLES1.1/bin/GLES11_fbdev Finally, you could copy the executable to the rootfs and test on i.MX6Q SDP/SDB or i.MX6DL SDP board. NOTE: the newly added makefiles.tgz contains Makefile.x11 hacked from GLES2.0 example code to make OpenVG to compile and run on Ubuntu 11.10 rootfs.
View full article
Prerequisites: The build is verified on prebuilt rootfs(based on LTIB) which can be downloaded from freescale.com or built from Yocto fsl-image-gui These steps are performed on the host: 1. Download the git respository for qt5: $ git clone git://gitorious.org/qt/qt5.git qt5     cd qt5     Let us consider this as <QTDir> 2. Create a build directory to install for the qt5 packages. This directory can be  in any loctation. For example,  $ mkdir /opt/qt5 sudo chown -R <username> /opt/qt5 Let us consider the the installdir as /opt/qt5 3. Enter the Qt5 directory and run the perl init-repository script to download all the source code for    Qt5. To download all the source code will take about an hour. $ perl init-repository 4. Download the attached linux-imx5-g++.tar.gz and copy to  qtbase/mkspecs/devices. Will try to get updstreamed. 5. From the following path $ gedit qtbase/mkspecs/devices/linux-imx5-g++/qmake.conf   6. At the top of the qmake.conf, there is a configure line. Copy and paste the configure line into a text file located    in your build build directory. Edit the configure line to find your toolchain and filesystem. Also make sure to    include the options -no-pch, -no-opengl, -opengl es2, Here is an example of    a configure line.     $ cd <QTDir>     $ cd qtbase     $  ./configure -v -opensource -confirm-license -no-pch -opengl es2 -make libs -device imx5 \     -nomake examples -nomake demos \ -device-option CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi- \ -sysroot <rootfs> -no-gcc-sysroot \ -prefix <installdir> 7. Make the textfile that has the configure line and executable and run it. When the configure summary is shown make sure the Qt5    has openGL ES 2.0 support. Do build       $make     $make install    When Qt5 has finished building, Qt5 will be installed in two places:            1. <location of rootfs>/<installdir>            2. <HOST Machine>/<install dir> This is good because now all the libraries and binaries for Qt5 are installed on the host and the target filesystem. Therefore, the target already has all the libraries and  binaries needed to run Qt5. 8. Also need to build qtjsbackend and qtdeclarative.     $ cd <location to Qt5 git>     $ cd qtjsbackend     $ ../qtbase/bin/qmake -r     $ make && make install        $ $ cd <location to Qt5 git>     $ cd qtdeclarative     $ ../qtbase/bin/qmake -r     $ make && make install 9. Run Qt apps on target     - Boot the target either with NFS or SD Image     - Ensure that folder <installdir> is copied on target file system at “/usr/local”.     - Launch application using     $ cd /usr/local/qt5/examples/opengl/hellogl_es2     $ ./hellogl_es2 -platform eglfs
View full article
BlueZ5 provides support for the core Bluetooth layers and protocols. It is flexible, efficient and uses a modular implementation. BlueZ5 has implemented the Bluetooth low level host stack for Bluetooth core specification 4.0 and 3.0+HS which includes GAP, L2CAP, RFCOMM, and SDP. Besides the host stack, BlueZ5 has also supported the following profiles itself or via a third party software. Profiles provided by BlueZ: A2DP 1.3 AVRCP 1.5 DI 1.3 HDP 1.0 HID 1.0 PAN 1.0 SPP 1.1 GATT (LE) profiles: PXP 1.0 HTP 1.0 HoG 1.0 TIP 1.0 CSCP 1.0 OBEX based profiles (by obexd): FTP 1.1 OPP 1.1 PBAP 1.1 MAP 1.0 Provided by the oFono project: HFP 1.6 (AG & HF)Supported Profiles BlueZ5 has been supported in the latest Freescale Linux BSP release, so it would be pretty easy to generate the binaries for Bluetooth core stack and its profiles. In order to support A2DP sink on a SabreSD board, the following software should be downloaded and installed onto the target rootfs too. sbc decoder version 1.3 (http://www.kernel.org/pub/linux/bluetooth/sbc-1.3.tar.gz) PulseAudio 5.0 (http://www.freedesktop.org/software/pulseaudio/releases/pulseaudio-5.0.tar.xz) PulseAudio package has some dependencies with bluetooth and sbc packages, and pulseaudio will detect if the two packages have been built and then decide which pulse plugin modules to be generated. So the building order will be 1) bluez5_utils or bluez_utils   2) sbc   3) pulseaudio. After compile and install the above software onto the target rootfs, you should be able to see the following executable under the directory /usr/bin From BlueZ5: bluetoothctl, hciconfig, hciattach (Needed by operating a UART bluetooth module) From PulseAudio: pulseaudio, pactl, paplay If the building dependency has been setup correctly, the following pulse plugin modules should be located under the directory /usr/lib/pulse-5.0/modules module-bluetooth-discover.so      module-bluetooth-policy.so        module-bluez5-device.so   module-bluez5-discover.so Edit the file /etc/dbus-1/system.d/pulseaudio-system.conf, and add the following lines in red: <policy user="pulse">     <allow own="org.pulseaudio.Server"/>    <allow send_destination="org.bluez"/>     <allow send_interface="org.freedesktop.DBus.ObjectManager"/> </policy> Edit the file /etc/dbus-1/system.d/bluetooth.conf, and add the following lines: <policy user="pulse">      <allow send_destination="org.bluez"/>      <allow send_interface="org.freedesktop.DBus.ObjectManager"/> </policy> Adding the following settings at the bottom of the pulseaudio system configuration file which locates in /etc/pulse/system.pa ### Automatically load driver modules for Bluetooth hardware .ifexists module-bluetooth-policy.so load-module module-bluetooth-policy .endif .ifexists module-bluetooth-discover.so load-module module-bluetooth-discover .endif load-module module-switch-on-connect load-module module-alsa-sink device_id=0 tsched=true tsched_buffer_size=1048576 tsched_buffer_watermark=262144 On the system that can automatically detect the alsa cards, the above line #13 should be removed.  Also make sure "auth-anonymous=1" is added to the following line, which can resolve the issue: "Denied access to client with invalid authorization data". load-module module-native-protocol-unix auth-anonymous=1 Selecting a audio re-sampling algorithm and configuring the audio output by adding the following settings to the file daemon.conf locating in /etc/pulse resample-method = trivial enable-remixing = no enable-lfe-remixing = no default-sample-format = s16le default-sample-rate = 48000 alternate-sample-rate = 24000 default-sample-channels = 2 Pulseaudio can be started as a daemon or as a system-wide instance. To run PulseAudio in system-wide mode, the program will automatically drop privileges from "root" and change to the "pulse" user and group. In this case, before launching the program, the "pulse" user and group needs to be created on the target system.  In the example below, "/var/run/pulse" is the home directory for "pulse" user. adduser -h /var/run/pulse pulse addgroup pulse-access adduser pulse pulse-access Because PulseAudio needs to access the sound devices, add the user "pulse" to the "audio" group too. adduser pulse audio Starting bluetoothd and pulseaudio: /usr/libexec/bluetooth/bluetoothd -d & pulseaudio --system --realtime & To verify if the pulseaudio has been set up correctly, you can play a local wave file by using the following command. If you can hear the sound, the system should have been configured correctly. paplay -vvv audio8k16S.wav After setting up the pulseaudio, launch bluetoothctl to pair and connect to a mobile phone. After connecting to a mobile phone, you should be able to see the following information in bluetoothctl console: [bluetooth]# show Controller 12:60:41:7F:03:00         Name: BlueZ 5.21         Alias: BlueZ 5.21         Class: 0x1c0000         Powered: yes         Discoverable: no         Pairable: yes         UUID: PnP Information           (00001200-0000-1000-8000-00805f9b34fb)         UUID: Generic Access Profile    (00001800-0000-1000-8000-00805f9b34fb)         UUID: Generic Attribute Profile (00001801-0000-1000-8000-00805f9b34fb)         UUID: A/V Remote Control        (0000110e-0000-1000-8000-00805f9b34fb)         UUID: A/V Remote Control Target (0000110c-0000-1000-8000-00805f9b34fb)         UUID: Message Notification Se.. (00001133-0000-1000-8000-00805f9b34fb)         UUID: Message Access Server     (00001132-0000-1000-8000-00805f9b34fb)         UUID: Phonebook Access Server   (0000112f-0000-1000-8000-00805f9b34fb)         UUID: IrMC Sync                 (00001104-0000-1000-8000-00805f9b34fb)         UUID: OBEX File Transfer        (00001106-0000-1000-8000-00805f9b34fb)         UUID: OBEX Object Push          (00001105-0000-1000-8000-00805f9b34fb)         UUID: Vendor specific           (00005005-0000-1000-8000-0002ee000001)         UUID: Audio Source              (0000110a-0000-1000-8000-00805f9b34fb)         UUID: Audio Sink                (0000110b-0000-1000-8000-00805f9b34fb)         Modalias: usb:v1D6Bp0246d0515         Discovering: no If you can see the audio sink UUID, you are ready to enjoy the bluetooth music now.
View full article
Overview This document explains how to use Pulse Width Modulation (PWM) on the iMX93 EVK Board. Attached to this post is a patch to enable this functionality, which can be integrated into either Yocto or a standalone kernel compilation.   This procedure was tested on iMX93 EVK A0 silicon version with BSP 6.1.22 version, this feature should work on A1 silicon version too but is not tested yet.   Kernel Configuration: To enable PWM support, modify the imx_v8_defconfig  file by adding the following line: CONFIG_PWM=y CONFIG_PWM_ADP5585=y CONFIG_PWM_CROS_EC=m CONFIG_PWM_FSL_FTM=m CONFIG_PWM_IMX27=y CONFIG_PWM_RPCHIP=y CONFIG_PWM_SL28CPLD=m + CONFIG_PWM_IMX_TPM=y​ # Add this line   Device Tree Modifications: You will need to add the following nodes to the device tree to configure the TPM (Timer/Pulse Width Modulation) controller:   + &tpm4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_tpm4>; + status = "okay"; + }; ... + pinctrl_tpm4: tpm4grp { + fsl,pins = < + MX93_PAD_GPIO_IO05__TPM4_CH0 0x19e //EXP_GPIO_IO05 J1001 29 + >; + };​   Compiling and Flashing: After making the above changes, compile the kernel and device tree. Once the compilation is complete, flash the new image and device tree to the iMX93 EVK Board.  PWM Configuration on the Board After flashing, you can configure the PWM settings on the board. Open a terminal and execute the following commands: $ cd /sys/class/pwm/pwmchip1/ $ echo 0 >> export $ echo echo 2000000 >> pwm0/period # Set period to 2,000,000 ns (2 ms) $ echo echo 1000000 >> pwm0/duty_cycle # Set duty cycle to 1,000,000 ns (1 ms) $ echo 1 >> pwm0/enable   Validation To validate the PWM output signal, check pin 29 of connector J1001 on the iMX93 EVK Board.   Conclusion Following these steps should enable PWM functionality on your iMX93 EVK Board. If you encounter any issues, please refer to the documentation or reach out for assistance. Best Regards! Chavira
View full article
In i.MX51 platfrom the PMIC 13892 also has a internal RTC. We can use this RTC instead of the i.mx51 SRTC. Attached was the implementation of it.
View full article